diff --git a/lib/CodeGen/SelectionDAG/SelectionDAGISel.cpp b/lib/CodeGen/SelectionDAG/SelectionDAGISel.cpp
index 754294129a839f80c374bad48089bbccf0ee61f6..1d0ed3af453c4b43b2eff36a40487cca72b38cd5 100644 (file)
//===----------------------------------------------------------------------===//
#define DEBUG_TYPE "isel"
+#include "llvm/CodeGen/SelectionDAGISel.h"
#include "ScheduleDAGSDNodes.h"
#include "SelectionDAGBuilder.h"
-#include "llvm/Constants.h"
-#include "llvm/DebugInfo.h"
-#include "llvm/Function.h"
-#include "llvm/InlineAsm.h"
-#include "llvm/Instructions.h"
-#include "llvm/Intrinsics.h"
-#include "llvm/IntrinsicInst.h"
-#include "llvm/LLVMContext.h"
-#include "llvm/Module.h"
+#include "llvm/ADT/PostOrderIterator.h"
+#include "llvm/ADT/Statistic.h"
#include "llvm/Analysis/AliasAnalysis.h"
#include "llvm/Analysis/BranchProbabilityInfo.h"
+#include "llvm/Analysis/CFG.h"
+#include "llvm/Analysis/TargetTransformInfo.h"
#include "llvm/CodeGen/FastISel.h"
#include "llvm/CodeGen/FunctionLoweringInfo.h"
-#include "llvm/CodeGen/GCStrategy.h"
#include "llvm/CodeGen/GCMetadata.h"
+#include "llvm/CodeGen/GCStrategy.h"
#include "llvm/CodeGen/MachineFrameInfo.h"
#include "llvm/CodeGen/MachineFunction.h"
#include "llvm/CodeGen/MachineInstrBuilder.h"
#include "llvm/CodeGen/ScheduleHazardRecognizer.h"
#include "llvm/CodeGen/SchedulerRegistry.h"
#include "llvm/CodeGen/SelectionDAG.h"
-#include "llvm/CodeGen/SelectionDAGISel.h"
-#include "llvm/Target/TargetRegisterInfo.h"
-#include "llvm/Target/TargetIntrinsicInfo.h"
+#include "llvm/DebugInfo.h"
+#include "llvm/IR/Constants.h"
+#include "llvm/IR/Function.h"
+#include "llvm/IR/InlineAsm.h"
+#include "llvm/IR/Instructions.h"
+#include "llvm/IR/IntrinsicInst.h"
+#include "llvm/IR/Intrinsics.h"
+#include "llvm/IR/LLVMContext.h"
+#include "llvm/IR/Module.h"
+#include "llvm/Support/Compiler.h"
+#include "llvm/Support/Debug.h"
+#include "llvm/Support/ErrorHandling.h"
+#include "llvm/Support/Timer.h"
+#include "llvm/Support/raw_ostream.h"
#include "llvm/Target/TargetInstrInfo.h"
+#include "llvm/Target/TargetIntrinsicInfo.h"
#include "llvm/Target/TargetLibraryInfo.h"
#include "llvm/Target/TargetLowering.h"
#include "llvm/Target/TargetMachine.h"
#include "llvm/Target/TargetOptions.h"
+#include "llvm/Target/TargetRegisterInfo.h"
+#include "llvm/Target/TargetSubtargetInfo.h"
#include "llvm/Transforms/Utils/BasicBlockUtils.h"
-#include "llvm/Support/Compiler.h"
-#include "llvm/Support/Debug.h"
-#include "llvm/Support/ErrorHandling.h"
-#include "llvm/Support/Timer.h"
-#include "llvm/Support/raw_ostream.h"
-#include "llvm/ADT/PostOrderIterator.h"
-#include "llvm/ADT/Statistic.h"
#include <algorithm>
using namespace llvm;
STATISTIC(NumFastIselBlocks, "Number of blocks selected entirely by fast isel");
STATISTIC(NumDAGBlocks, "Number of blocks selected using DAG");
STATISTIC(NumDAGIselRetries,"Number of times dag isel has to try another path");
+STATISTIC(NumEntryBlocks, "Number of entry blocks encountered");
+STATISTIC(NumFastIselFailLowerArguments,
+ "Number of entry blocks where fast isel failed to lower arguments");
#ifndef NDEBUG
static cl::opt<bool>
EnableFastISelVerbose2("fast-isel-verbose2", cl::Hidden,
cl::desc("Enable extra verbose messages in the \"fast\" "
"instruction selector"));
+
// Terminators
STATISTIC(NumFastIselFailRet,"Fast isel fails on Ret");
STATISTIC(NumFastIselFailBr,"Fast isel fails on Br");
"instruction selector"));
static cl::opt<bool>
EnableFastISelAbort("fast-isel-abort", cl::Hidden,
- cl::desc("Enable abort calls when \"fast\" instruction fails"));
+ cl::desc("Enable abort calls when \"fast\" instruction selection "
+ "fails to lower an instruction"));
+static cl::opt<bool>
+EnableFastISelAbortArgs("fast-isel-abort-args", cl::Hidden,
+ cl::desc("Enable abort calls when \"fast\" instruction selection "
+ "fails to lower a formal argument"));
static cl::opt<bool>
UseMBPI("use-mbpi",
/// for the target.
ScheduleDAGSDNodes* createDefaultScheduler(SelectionDAGISel *IS,
CodeGenOpt::Level OptLevel) {
- const TargetLowering &TLI = IS->getTargetLowering();
+ const TargetLowering *TLI = IS->getTargetLowering();
+ const TargetSubtargetInfo &ST = IS->TM.getSubtarget<TargetSubtargetInfo>();
- if (OptLevel == CodeGenOpt::None ||
- TLI.getSchedulingPreference() == Sched::Source)
+ if (OptLevel == CodeGenOpt::None || ST.useMachineScheduler() ||
+ TLI->getSchedulingPreference() == Sched::Source)
return createSourceListDAGScheduler(IS, OptLevel);
- if (TLI.getSchedulingPreference() == Sched::RegPressure)
+ if (TLI->getSchedulingPreference() == Sched::RegPressure)
return createBURRListDAGScheduler(IS, OptLevel);
- if (TLI.getSchedulingPreference() == Sched::Hybrid)
+ if (TLI->getSchedulingPreference() == Sched::Hybrid)
return createHybridListDAGScheduler(IS, OptLevel);
- if (TLI.getSchedulingPreference() == Sched::VLIW)
+ if (TLI->getSchedulingPreference() == Sched::VLIW)
return createVLIWDAGScheduler(IS, OptLevel);
- assert(TLI.getSchedulingPreference() == Sched::ILP &&
+ assert(TLI->getSchedulingPreference() == Sched::ILP &&
"Unknown sched type!");
return createILPListDAGScheduler(IS, OptLevel);
}
// SelectionDAGISel code
//===----------------------------------------------------------------------===//
-SelectionDAGISel::SelectionDAGISel(const TargetMachine &tm,
+SelectionDAGISel::SelectionDAGISel(TargetMachine &tm,
CodeGenOpt::Level OL) :
- MachineFunctionPass(ID), TM(tm), TLI(*tm.getTargetLowering()),
- FuncInfo(new FunctionLoweringInfo(TLI)),
+ MachineFunctionPass(ID), TM(tm),
+ FuncInfo(new FunctionLoweringInfo(TM)),
CurDAG(new SelectionDAG(tm, OL)),
SDB(new SelectionDAGBuilder(*CurDAG, *FuncInfo, OL)),
GFI(),
RegInfo = &MF->getRegInfo();
AA = &getAnalysis<AliasAnalysis>();
LibInfo = &getAnalysis<TargetLibraryInfo>();
+ TTI = getAnalysisIfAvailable<TargetTransformInfo>();
GFI = Fn.hasGC() ? &getAnalysis<GCModuleInfo>().getFunctionInfo(Fn) : 0;
+ TargetSubtargetInfo &ST =
+ const_cast<TargetSubtargetInfo&>(TM.getSubtarget<TargetSubtargetInfo>());
+ ST.resetSubtargetFeatures(MF);
+ TM.resetTargetOptions(MF);
+
DEBUG(dbgs() << "\n\n\n=== " << Fn.getName() << "\n");
SplitCriticalSideEffectEdges(const_cast<Function&>(Fn), this);
- CurDAG->init(*MF);
+ CurDAG->init(*MF, TTI);
FuncInfo->set(Fn, *MF);
if (UseMBPI && OptLevel != CodeGenOpt::None)
SDB->init(GFI, *AA, LibInfo);
+ MF->setHasMSInlineAsm(false);
SelectAllBasicBlocks(Fn);
// If the first basic block in the function has live ins that need to be
// Insert DBG_VALUE instructions for function arguments to the entry block.
for (unsigned i = 0, e = FuncInfo->ArgDbgValues.size(); i != e; ++i) {
MachineInstr *MI = FuncInfo->ArgDbgValues[e-i-1];
- unsigned Reg = MI->getOperand(0).getReg();
+ bool hasFI = MI->getOperand(0).isFI();
+ unsigned Reg = hasFI ? TRI.getFrameRegister(*MF) : MI->getOperand(0).getReg();
if (TargetRegisterInfo::isPhysicalRegister(Reg))
EntryMBB->insert(EntryMBB->begin(), MI);
else {
MachineInstr *Def = RegInfo->getVRegDef(Reg);
- MachineBasicBlock::iterator InsertPos = Def;
- // FIXME: VR def may not be in entry block.
- Def->getParent()->insert(llvm::next(InsertPos), MI);
+ if (Def) {
+ MachineBasicBlock::iterator InsertPos = Def;
+ // FIXME: VR def may not be in entry block.
+ Def->getParent()->insert(llvm::next(InsertPos), MI);
+ } else
+ DEBUG(dbgs() << "Dropping debug info for dead vreg"
+ << TargetRegisterInfo::virtReg2Index(Reg) << "\n");
}
// If Reg is live-in then update debug info to track its copy in a vreg.
DenseMap<unsigned, unsigned>::iterator LDI = LiveInMap.find(Reg);
if (LDI != LiveInMap.end()) {
+ assert(!hasFI && "There's no handling of frame pointer updating here yet "
+ "- add if needed");
MachineInstr *Def = RegInfo->getVRegDef(LDI->second);
MachineBasicBlock::iterator InsertPos = Def;
const MDNode *Variable =
MI->getOperand(MI->getNumOperands()-1).getMetadata();
- unsigned Offset = MI->getOperand(1).getImm();
+ bool IsIndirect = MI->isIndirectDebugValue();
+ unsigned Offset = IsIndirect ? MI->getOperand(1).getImm() : 0;
// Def is never a terminator here, so it is ok to increment InsertPos.
BuildMI(*EntryMBB, ++InsertPos, MI->getDebugLoc(),
- TII.get(TargetOpcode::DBG_VALUE))
- .addReg(LDI->second, RegState::Debug)
- .addImm(Offset).addMetadata(Variable);
+ TII.get(TargetOpcode::DBG_VALUE),
+ IsIndirect,
+ LDI->second, Offset, Variable);
// If this vreg is directly copied into an exported register then
// that COPY instructions also need DBG_VALUE, if it is the only
if (CopyUseMI) {
MachineInstr *NewMI =
BuildMI(*MF, CopyUseMI->getDebugLoc(),
- TII.get(TargetOpcode::DBG_VALUE))
- .addReg(CopyUseMI->getOperand(0).getReg(), RegState::Debug)
- .addImm(Offset).addMetadata(Variable);
+ TII.get(TargetOpcode::DBG_VALUE),
+ IsIndirect,
+ CopyUseMI->getOperand(0).getReg(),
+ Offset, Variable);
MachineBasicBlock::iterator Pos = CopyUseMI;
EntryMBB->insertAfter(Pos, NewMI);
}
// Determine if there are any calls in this machine function.
MachineFrameInfo *MFI = MF->getFrameInfo();
- if (!MFI->hasCalls()) {
- for (MachineFunction::const_iterator
- I = MF->begin(), E = MF->end(); I != E; ++I) {
- const MachineBasicBlock *MBB = I;
- for (MachineBasicBlock::const_iterator
- II = MBB->begin(), IE = MBB->end(); II != IE; ++II) {
- const MCInstrDesc &MCID = TM.getInstrInfo()->get(II->getOpcode());
-
- if ((MCID.isCall() && !MCID.isReturn()) ||
- II->isStackAligningInlineAsm()) {
- MFI->setHasCalls(true);
- goto done;
- }
+ for (MachineFunction::const_iterator I = MF->begin(), E = MF->end(); I != E;
+ ++I) {
+
+ if (MFI->hasCalls() && MF->hasMSInlineAsm())
+ break;
+
+ const MachineBasicBlock *MBB = I;
+ for (MachineBasicBlock::const_iterator II = MBB->begin(), IE = MBB->end();
+ II != IE; ++II) {
+ const MCInstrDesc &MCID = TM.getInstrInfo()->get(II->getOpcode());
+ if ((MCID.isCall() && !MCID.isReturn()) ||
+ II->isStackAligningInlineAsm()) {
+ MFI->setHasCalls(true);
+ }
+ if (II->isMSInlineAsm()) {
+ MF->setHasMSInlineAsm(true);
}
}
}
- done:
// Determine if there is a call to setjmp in the machine function.
MF->setExposesReturnsTwice(Fn.callsFunctionThatReturnsTwice());
if (J == E) break;
To = J->second;
}
+ // Make sure the new register has a sufficiently constrained register class.
+ if (TargetRegisterInfo::isVirtualRegister(From) &&
+ TargetRegisterInfo::isVirtualRegister(To))
+ MRI.constrainRegClass(To, MRI.getRegClass(From));
// Replace it.
MRI.replaceRegWith(From, To);
}
+ // Freeze the set of reserved registers now that MachineFrameInfo has been
+ // set up. All the information required by getReservedRegs() should be
+ // available now.
+ MRI.freezeReservedRegs(*MF);
+
// Release function-specific state. SDB and CurDAG are already cleared
// at this point.
FuncInfo->clear();
DEBUG(dbgs() << "Optimized type-legalized selection DAG: BB#" << BlockNumber
<< " '" << BlockName << "'\n"; CurDAG->dump());
+
}
{
} // end anonymous namespace
void SelectionDAGISel::DoInstructionSelection() {
- DEBUG(errs() << "===== Instruction selection begins: BB#"
+ DEBUG(dbgs() << "===== Instruction selection begins: BB#"
<< FuncInfo->MBB->getNumber()
<< " '" << FuncInfo->MBB->getName() << "'\n");
if (ResNode == Node || Node->getOpcode() == ISD::DELETED_NODE)
continue;
// Replace node.
- if (ResNode)
+ if (ResNode) {
ReplaceUses(Node, ResNode);
+ }
// If after the replacement this node is not used any more,
// remove this dead node.
CurDAG->setRoot(Dummy.getValue());
}
- DEBUG(errs() << "===== Instruction selection ends:\n");
+ DEBUG(dbgs() << "===== Instruction selection ends:\n");
PostprocessISelDAG();
}
.addSym(Label);
// Mark exception register as live in.
- unsigned Reg = TLI.getExceptionPointerRegister();
- if (Reg) MBB->addLiveIn(Reg);
+ const TargetLowering *TLI = getTargetLowering();
+ const TargetRegisterClass *PtrRC = TLI->getRegClassFor(TLI->getPointerTy());
+ if (unsigned Reg = TLI->getExceptionPointerRegister())
+ FuncInfo->ExceptionPointerVirtReg = MBB->addLiveIn(Reg, PtrRC);
// Mark exception selector register as live in.
- Reg = TLI.getExceptionSelectorRegister();
- if (Reg) MBB->addLiveIn(Reg);
-}
-
-/// TryToFoldFastISelLoad - We're checking to see if we can fold the specified
-/// load into the specified FoldInst. Note that we could have a sequence where
-/// multiple LLVM IR instructions are folded into the same machineinstr. For
-/// example we could have:
-/// A: x = load i32 *P
-/// B: y = icmp A, 42
-/// C: br y, ...
-///
-/// In this scenario, LI is "A", and FoldInst is "C". We know about "B" (and
-/// any other folded instructions) because it is between A and C.
-///
-/// If we succeed in folding the load into the operation, return true.
-///
-bool SelectionDAGISel::TryToFoldFastISelLoad(const LoadInst *LI,
- const Instruction *FoldInst,
- FastISel *FastIS) {
- // We know that the load has a single use, but don't know what it is. If it
- // isn't one of the folded instructions, then we can't succeed here. Handle
- // this by scanning the single-use users of the load until we get to FoldInst.
- unsigned MaxUsers = 6; // Don't scan down huge single-use chains of instrs.
-
- const Instruction *TheUser = LI->use_back();
- while (TheUser != FoldInst && // Scan up until we find FoldInst.
- // Stay in the right block.
- TheUser->getParent() == FoldInst->getParent() &&
- --MaxUsers) { // Don't scan too far.
- // If there are multiple or no uses of this instruction, then bail out.
- if (!TheUser->hasOneUse())
- return false;
-
- TheUser = TheUser->use_back();
- }
-
- // If we didn't find the fold instruction, then we failed to collapse the
- // sequence.
- if (TheUser != FoldInst)
- return false;
-
- // Don't try to fold volatile loads. Target has to deal with alignment
- // constraints.
- if (LI->isVolatile()) return false;
-
- // Figure out which vreg this is going into. If there is no assigned vreg yet
- // then there actually was no reference to it. Perhaps the load is referenced
- // by a dead instruction.
- unsigned LoadReg = FastIS->getRegForValue(LI);
- if (LoadReg == 0)
- return false;
-
- // Check to see what the uses of this vreg are. If it has no uses, or more
- // than one use (at the machine instr level) then we can't fold it.
- MachineRegisterInfo::reg_iterator RI = RegInfo->reg_begin(LoadReg);
- if (RI == RegInfo->reg_end())
- return false;
-
- // See if there is exactly one use of the vreg. If there are multiple uses,
- // then the instruction got lowered to multiple machine instructions or the
- // use of the loaded value ended up being multiple operands of the result, in
- // either case, we can't fold this.
- MachineRegisterInfo::reg_iterator PostRI = RI; ++PostRI;
- if (PostRI != RegInfo->reg_end())
- return false;
-
- assert(RI.getOperand().isUse() &&
- "The only use of the vreg must be a use, we haven't emitted the def!");
-
- MachineInstr *User = &*RI;
-
- // Set the insertion point properly. Folding the load can cause generation of
- // other random instructions (like sign extends) for addressing modes, make
- // sure they get inserted in a logical place before the new instruction.
- FuncInfo->InsertPt = User;
- FuncInfo->MBB = User->getParent();
-
- // Ask the target to try folding the load.
- return FastIS->TryToFoldLoad(User, RI.getOperandNo(), LI);
+ if (unsigned Reg = TLI->getExceptionSelectorRegister())
+ FuncInfo->ExceptionSelectorVirtReg = MBB->addLiveIn(Reg, PtrRC);
}
/// isFoldedOrDeadInstruction - Return true if the specified instruction is
// Initialize the Fast-ISel state, if needed.
FastISel *FastIS = 0;
if (TM.Options.EnableFastISel)
- FastIS = TLI.createFastISel(*FuncInfo, LibInfo);
+ FastIS = getTargetLowering()->createFastISel(*FuncInfo, LibInfo);
// Iterate over all basic blocks in the function.
ReversePostOrderTraversal<const Function*> RPOT(&Fn);
if (AllPredsVisited) {
for (BasicBlock::const_iterator I = LLVMBB->begin();
- isa<PHINode>(I); ++I)
- FuncInfo->ComputePHILiveOutRegInfo(cast<PHINode>(I));
+ const PHINode *PN = dyn_cast<PHINode>(I); ++I)
+ FuncInfo->ComputePHILiveOutRegInfo(PN);
} else {
for (BasicBlock::const_iterator I = LLVMBB->begin();
- isa<PHINode>(I); ++I)
- FuncInfo->InvalidatePHILiveOutRegInfo(cast<PHINode>(I));
+ const PHINode *PN = dyn_cast<PHINode>(I); ++I)
+ FuncInfo->InvalidatePHILiveOutRegInfo(PN);
}
FuncInfo->VisitedBBs.insert(LLVMBB);
}
- FuncInfo->MBB = FuncInfo->MBBMap[LLVMBB];
- FuncInfo->InsertPt = FuncInfo->MBB->getFirstNonPHI();
-
BasicBlock::const_iterator const Begin = LLVMBB->getFirstNonPHI();
BasicBlock::const_iterator const End = LLVMBB->end();
BasicBlock::const_iterator BI = End;
+ FuncInfo->MBB = FuncInfo->MBBMap[LLVMBB];
FuncInfo->InsertPt = FuncInfo->MBB->getFirstNonPHI();
// Setup an EH landing-pad block.
+ FuncInfo->ExceptionPointerVirtReg = 0;
+ FuncInfo->ExceptionSelectorVirtReg = 0;
if (FuncInfo->MBB->isLandingPad())
PrepareEHLandingPad();
- // Lower any arguments needed in this block if this is the entry block.
- if (LLVMBB == &Fn.getEntryBlock())
- LowerArguments(LLVMBB);
-
// Before doing SelectionDAG ISel, see if FastISel has been requested.
if (FastIS) {
FastIS->startNewBlock();
// Emit code for any incoming arguments. This must happen before
// beginning FastISel on the entry block.
if (LLVMBB == &Fn.getEntryBlock()) {
- CurDAG->setRoot(SDB->getControlRoot());
- SDB->clear();
- CodeGenAndEmitDAG();
+ ++NumEntryBlocks;
+
+ // Lower any arguments needed in this block if this is the entry block.
+ if (!FastIS->LowerArguments()) {
+ // Fast isel failed to lower these arguments
+ ++NumFastIselFailLowerArguments;
+ if (EnableFastISelAbortArgs)
+ llvm_unreachable("FastISel didn't lower all arguments");
+
+ // Use SelectionDAG argument lowering
+ LowerArguments(Fn);
+ CurDAG->setRoot(SDB->getControlRoot());
+ SDB->clear();
+ CodeGenAndEmitDAG();
+ }
// If we inserted any instructions at the beginning, make a note of
// where they are, so we can be sure to emit subsequent instructions
}
if (BeforeInst != Inst && isa<LoadInst>(BeforeInst) &&
BeforeInst->hasOneUse() &&
- TryToFoldFastISelLoad(cast<LoadInst>(BeforeInst), Inst, FastIS)) {
+ FastIS->tryToFoldLoad(cast<LoadInst>(BeforeInst), Inst)) {
// If we succeeded, don't re-select the load.
BI = llvm::next(BasicBlock::const_iterator(BeforeInst));
--NumFastIselRemaining;
}
bool HadTailCall = false;
+ MachineBasicBlock::iterator SavedInsertPt = FuncInfo->InsertPt;
SelectBasicBlock(Inst, BI, HadTailCall);
- // Recompute NumFastIselRemaining as Selection DAG instruction
- // selection may have handled the call, input args, etc.
- unsigned RemainingNow = std::distance(Begin, BI);
- NumFastIselFailures += NumFastIselRemaining - RemainingNow;
-
// If the call was emitted as a tail call, we're done with the block.
+ // We also need to delete any previously emitted instructions.
if (HadTailCall) {
+ FastIS->removeDeadCode(SavedInsertPt, FuncInfo->MBB->end());
--BI;
break;
}
+ // Recompute NumFastIselRemaining as Selection DAG instruction
+ // selection may have handled the call, input args, etc.
+ unsigned RemainingNow = std::distance(Begin, BI);
+ NumFastIselFailures += NumFastIselRemaining - RemainingNow;
NumFastIselRemaining = RemainingNow;
continue;
}
}
FastIS->recomputeInsertPt();
+ } else {
+ // Lower any arguments needed in this block if this is the entry block.
+ if (LLVMBB == &Fn.getEntryBlock()) {
+ ++NumEntryBlocks;
+ LowerArguments(Fn);
+ }
}
if (Begin != BI)
delete FastIS;
SDB->clearDanglingDebugInfo();
+ SDB->SPDescriptor.resetPerFunctionState();
+}
+
+/// Given that the input MI is before a partial terminator sequence TSeq, return
+/// true if M + TSeq also a partial terminator sequence.
+///
+/// A Terminator sequence is a sequence of MachineInstrs which at this point in
+/// lowering copy vregs into physical registers, which are then passed into
+/// terminator instructors so we can satisfy ABI constraints. A partial
+/// terminator sequence is an improper subset of a terminator sequence (i.e. it
+/// may be the whole terminator sequence).
+static bool MIIsInTerminatorSequence(const MachineInstr *MI) {
+ // If we do not have a copy or an implicit def, we return true if and only if
+ // MI is a debug value.
+ if (!MI->isCopy() && !MI->isImplicitDef())
+ // Sometimes DBG_VALUE MI sneak in between the copies from the vregs to the
+ // physical registers if there is debug info associated with the terminator
+ // of our mbb. We want to include said debug info in our terminator
+ // sequence, so we return true in that case.
+ return MI->isDebugValue();
+
+ // We have left the terminator sequence if we are not doing one of the
+ // following:
+ //
+ // 1. Copying a vreg into a physical register.
+ // 2. Copying a vreg into a vreg.
+ // 3. Defining a register via an implicit def.
+
+ // OPI should always be a register definition...
+ MachineInstr::const_mop_iterator OPI = MI->operands_begin();
+ if (!OPI->isReg() || !OPI->isDef())
+ return false;
+
+ // Defining any register via an implicit def is always ok.
+ if (MI->isImplicitDef())
+ return true;
+
+ // Grab the copy source...
+ MachineInstr::const_mop_iterator OPI2 = OPI;
+ ++OPI2;
+ assert(OPI2 != MI->operands_end()
+ && "Should have a copy implying we should have 2 arguments.");
+
+ // Make sure that the copy dest is not a vreg when the copy source is a
+ // physical register.
+ if (!OPI2->isReg() ||
+ (!TargetRegisterInfo::isPhysicalRegister(OPI->getReg()) &&
+ TargetRegisterInfo::isPhysicalRegister(OPI2->getReg())))
+ return false;
+
+ return true;
+}
+
+/// Find the split point at which to splice the end of BB into its success stack
+/// protector check machine basic block.
+///
+/// On many platforms, due to ABI constraints, terminators, even before register
+/// allocation, use physical registers. This creates an issue for us since
+/// physical registers at this point can not travel across basic
+/// blocks. Luckily, selectiondag always moves physical registers into vregs
+/// when they enter functions and moves them through a sequence of copies back
+/// into the physical registers right before the terminator creating a
+/// ``Terminator Sequence''. This function is searching for the beginning of the
+/// terminator sequence so that we can ensure that we splice off not just the
+/// terminator, but additionally the copies that move the vregs into the
+/// physical registers.
+static MachineBasicBlock::iterator
+FindSplitPointForStackProtector(MachineBasicBlock *BB, DebugLoc DL) {
+ MachineBasicBlock::iterator SplitPoint = BB->getFirstTerminator();
+ //
+ if (SplitPoint == BB->begin())
+ return SplitPoint;
+
+ MachineBasicBlock::iterator Start = BB->begin();
+ MachineBasicBlock::iterator Previous = SplitPoint;
+ --Previous;
+
+ while (MIIsInTerminatorSequence(Previous)) {
+ SplitPoint = Previous;
+ if (Previous == Start)
+ break;
+ --Previous;
+ }
+
+ return SplitPoint;
}
void
<< FuncInfo->PHINodesToUpdate[i].first
<< ", " << FuncInfo->PHINodesToUpdate[i].second << ")\n");
+ const bool MustUpdatePHINodes = SDB->SwitchCases.empty() &&
+ SDB->JTCases.empty() &&
+ SDB->BitTestCases.empty();
+
// Next, now that we know what the last MBB the LLVM BB expanded is, update
// PHI nodes in successors.
- if (SDB->SwitchCases.empty() &&
- SDB->JTCases.empty() &&
- SDB->BitTestCases.empty()) {
+ if (MustUpdatePHINodes) {
for (unsigned i = 0, e = FuncInfo->PHINodesToUpdate.size(); i != e; ++i) {
- MachineInstr *PHI = FuncInfo->PHINodesToUpdate[i].first;
+ MachineInstrBuilder PHI(*MF, FuncInfo->PHINodesToUpdate[i].first);
assert(PHI->isPHI() &&
"This is not a machine PHI node that we are updating!");
if (!FuncInfo->MBB->isSuccessor(PHI->getParent()))
continue;
- PHI->addOperand(
- MachineOperand::CreateReg(FuncInfo->PHINodesToUpdate[i].second, false));
- PHI->addOperand(MachineOperand::CreateMBB(FuncInfo->MBB));
+ PHI.addReg(FuncInfo->PHINodesToUpdate[i].second).addMBB(FuncInfo->MBB);
}
- return;
}
+ // Handle stack protector.
+ if (SDB->SPDescriptor.shouldEmitStackProtector()) {
+ MachineBasicBlock *ParentMBB = SDB->SPDescriptor.getParentMBB();
+ MachineBasicBlock *SuccessMBB = SDB->SPDescriptor.getSuccessMBB();
+
+ // Find the split point to split the parent mbb. At the same time copy all
+ // physical registers used in the tail of parent mbb into virtual registers
+ // before the split point and back into physical registers after the split
+ // point. This prevents us needing to deal with Live-ins and many other
+ // register allocation issues caused by us splitting the parent mbb. The
+ // register allocator will clean up said virtual copies later on.
+ MachineBasicBlock::iterator SplitPoint =
+ FindSplitPointForStackProtector(ParentMBB, SDB->getCurDebugLoc());
+
+ // Splice the terminator of ParentMBB into SuccessMBB.
+ SuccessMBB->splice(SuccessMBB->end(), ParentMBB,
+ SplitPoint,
+ ParentMBB->end());
+
+ // Add compare/jump on neq/jump to the parent BB.
+ FuncInfo->MBB = ParentMBB;
+ FuncInfo->InsertPt = ParentMBB->end();
+ SDB->visitSPDescriptorParent(SDB->SPDescriptor, ParentMBB);
+ CurDAG->setRoot(SDB->getRoot());
+ SDB->clear();
+ CodeGenAndEmitDAG();
+
+ // CodeGen Failure MBB if we have not codegened it yet.
+ MachineBasicBlock *FailureMBB = SDB->SPDescriptor.getFailureMBB();
+ if (!FailureMBB->size()) {
+ FuncInfo->MBB = FailureMBB;
+ FuncInfo->InsertPt = FailureMBB->end();
+ SDB->visitSPDescriptorFailure(SDB->SPDescriptor);
+ CurDAG->setRoot(SDB->getRoot());
+ SDB->clear();
+ CodeGenAndEmitDAG();
+ }
+
+ // Clear the Per-BB State.
+ SDB->SPDescriptor.resetPerBBState();
+ }
+
+ // If we updated PHI Nodes, return early.
+ if (MustUpdatePHINodes)
+ return;
+
for (unsigned i = 0, e = SDB->BitTestCases.size(); i != e; ++i) {
// Lower header first, if it wasn't already lowered
if (!SDB->BitTestCases[i].Emitted) {
// Update PHI Nodes
for (unsigned pi = 0, pe = FuncInfo->PHINodesToUpdate.size();
pi != pe; ++pi) {
- MachineInstr *PHI = FuncInfo->PHINodesToUpdate[pi].first;
+ MachineInstrBuilder PHI(*MF, FuncInfo->PHINodesToUpdate[pi].first);
MachineBasicBlock *PHIBB = PHI->getParent();
assert(PHI->isPHI() &&
"This is not a machine PHI node that we are updating!");
// This is "default" BB. We have two jumps to it. From "header" BB and
// from last "case" BB.
- if (PHIBB == SDB->BitTestCases[i].Default) {
- PHI->addOperand(MachineOperand::
- CreateReg(FuncInfo->PHINodesToUpdate[pi].second,
- false));
- PHI->addOperand(MachineOperand::CreateMBB(SDB->BitTestCases[i].Parent));
- PHI->addOperand(MachineOperand::
- CreateReg(FuncInfo->PHINodesToUpdate[pi].second,
- false));
- PHI->addOperand(MachineOperand::CreateMBB(SDB->BitTestCases[i].Cases.
- back().ThisBB));
- }
+ if (PHIBB == SDB->BitTestCases[i].Default)
+ PHI.addReg(FuncInfo->PHINodesToUpdate[pi].second)
+ .addMBB(SDB->BitTestCases[i].Parent)
+ .addReg(FuncInfo->PHINodesToUpdate[pi].second)
+ .addMBB(SDB->BitTestCases[i].Cases.back().ThisBB);
// One of "cases" BB.
for (unsigned j = 0, ej = SDB->BitTestCases[i].Cases.size();
j != ej; ++j) {
MachineBasicBlock* cBB = SDB->BitTestCases[i].Cases[j].ThisBB;
- if (cBB->isSuccessor(PHIBB)) {
- PHI->addOperand(MachineOperand::
- CreateReg(FuncInfo->PHINodesToUpdate[pi].second,
- false));
- PHI->addOperand(MachineOperand::CreateMBB(cBB));
- }
+ if (cBB->isSuccessor(PHIBB))
+ PHI.addReg(FuncInfo->PHINodesToUpdate[pi].second).addMBB(cBB);
}
}
}
// Update PHI Nodes
for (unsigned pi = 0, pe = FuncInfo->PHINodesToUpdate.size();
pi != pe; ++pi) {
- MachineInstr *PHI = FuncInfo->PHINodesToUpdate[pi].first;
+ MachineInstrBuilder PHI(*MF, FuncInfo->PHINodesToUpdate[pi].first);
MachineBasicBlock *PHIBB = PHI->getParent();
assert(PHI->isPHI() &&
"This is not a machine PHI node that we are updating!");
// "default" BB. We can go there only from header BB.
- if (PHIBB == SDB->JTCases[i].second.Default) {
- PHI->addOperand
- (MachineOperand::CreateReg(FuncInfo->PHINodesToUpdate[pi].second,
- false));
- PHI->addOperand
- (MachineOperand::CreateMBB(SDB->JTCases[i].first.HeaderBB));
- }
+ if (PHIBB == SDB->JTCases[i].second.Default)
+ PHI.addReg(FuncInfo->PHINodesToUpdate[pi].second)
+ .addMBB(SDB->JTCases[i].first.HeaderBB);
// JT BB. Just iterate over successors here
- if (FuncInfo->MBB->isSuccessor(PHIBB)) {
- PHI->addOperand
- (MachineOperand::CreateReg(FuncInfo->PHINodesToUpdate[pi].second,
- false));
- PHI->addOperand(MachineOperand::CreateMBB(FuncInfo->MBB));
- }
+ if (FuncInfo->MBB->isSuccessor(PHIBB))
+ PHI.addReg(FuncInfo->PHINodesToUpdate[pi].second).addMBB(FuncInfo->MBB);
}
}
SDB->JTCases.clear();
// If the switch block involved a branch to one of the actual successors, we
// need to update PHI nodes in that block.
for (unsigned i = 0, e = FuncInfo->PHINodesToUpdate.size(); i != e; ++i) {
- MachineInstr *PHI = FuncInfo->PHINodesToUpdate[i].first;
+ MachineInstrBuilder PHI(*MF, FuncInfo->PHINodesToUpdate[i].first);
assert(PHI->isPHI() &&
"This is not a machine PHI node that we are updating!");
- if (FuncInfo->MBB->isSuccessor(PHI->getParent())) {
- PHI->addOperand(
- MachineOperand::CreateReg(FuncInfo->PHINodesToUpdate[i].second, false));
- PHI->addOperand(MachineOperand::CreateMBB(FuncInfo->MBB));
- }
+ if (FuncInfo->MBB->isSuccessor(PHI->getParent()))
+ PHI.addReg(FuncInfo->PHINodesToUpdate[i].second).addMBB(FuncInfo->MBB);
}
// If we generated any switch lowering information, build and codegen any
// FuncInfo->MBB may have been removed from the CFG if a branch was
// constant folded.
if (ThisBB->isSuccessor(FuncInfo->MBB)) {
- for (MachineBasicBlock::iterator Phi = FuncInfo->MBB->begin();
- Phi != FuncInfo->MBB->end() && Phi->isPHI();
- ++Phi) {
+ for (MachineBasicBlock::iterator
+ MBBI = FuncInfo->MBB->begin(), MBBE = FuncInfo->MBB->end();
+ MBBI != MBBE && MBBI->isPHI(); ++MBBI) {
+ MachineInstrBuilder PHI(*MF, MBBI);
// This value for this PHI node is recorded in PHINodesToUpdate.
for (unsigned pn = 0; ; ++pn) {
assert(pn != FuncInfo->PHINodesToUpdate.size() &&
"Didn't find PHI entry!");
- if (FuncInfo->PHINodesToUpdate[pn].first == Phi) {
- Phi->addOperand(MachineOperand::
- CreateReg(FuncInfo->PHINodesToUpdate[pn].second,
- false));
- Phi->addOperand(MachineOperand::CreateMBB(ThisBB));
+ if (FuncInfo->PHINodesToUpdate[pn].first == PHI) {
+ PHI.addReg(FuncInfo->PHINodesToUpdate[pn].second).addMBB(ThisBB);
break;
}
}
std::vector<SDValue> Ops(N->op_begin(), N->op_end());
SelectInlineAsmMemoryOperands(Ops);
- std::vector<EVT> VTs;
- VTs.push_back(MVT::Other);
- VTs.push_back(MVT::Glue);
- SDValue New = CurDAG->getNode(ISD::INLINEASM, N->getDebugLoc(),
+ EVT VTs[] = { MVT::Other, MVT::Glue };
+ SDValue New = CurDAG->getNode(ISD::INLINEASM, SDLoc(N),
VTs, &Ops[0], Ops.size());
New->setNodeId(-1);
return New.getNode();
if (!NowDeadNodes.empty())
CurDAG->RemoveDeadNodes(NowDeadNodes);
- DEBUG(errs() << "ISEL: Match complete!\n");
+ DEBUG(dbgs() << "ISEL: Match complete!\n");
}
enum ChainResult {
SDNode *User = *UI;
+ if (User->getOpcode() == ISD::HANDLENODE) // Root of the graph.
+ continue;
+
// If we see an already-selected machine node, then we've gone beyond the
// pattern that we're selecting down into the already selected chunk of the
// DAG.
- if (User->isMachineOpcode() ||
- User->getOpcode() == ISD::HANDLENODE) // Root of the graph.
- continue;
-
unsigned UserOpcode = User->getOpcode();
- if (UserOpcode == ISD::CopyToReg ||
+ if (User->isMachineOpcode() ||
+ UserOpcode == ISD::CopyToReg ||
UserOpcode == ISD::CopyFromReg ||
UserOpcode == ISD::INLINEASM ||
UserOpcode == ISD::EH_LABEL ||
}
}
- SDValue Res;
if (InputChains.size() == 1)
return InputChains[0];
- return CurDAG->getNode(ISD::TokenFactor, ChainNodesMatched[0]->getDebugLoc(),
+ return CurDAG->getNode(ISD::TokenFactor, SDLoc(ChainNodesMatched[0]),
MVT::Other, &InputChains[0], InputChains.size());
}
return Res;
}
-/// CheckPatternPredicate - Implements OP_CheckPatternPredicate.
+/// CheckSame - Implements OP_CheckSame.
LLVM_ATTRIBUTE_ALWAYS_INLINE static bool
CheckSame(const unsigned char *MatcherTable, unsigned &MatcherIndex,
SDValue N,
LLVM_ATTRIBUTE_ALWAYS_INLINE static bool
CheckType(const unsigned char *MatcherTable, unsigned &MatcherIndex,
- SDValue N, const TargetLowering &TLI) {
+ SDValue N, const TargetLowering *TLI) {
MVT::SimpleValueType VT = (MVT::SimpleValueType)MatcherTable[MatcherIndex++];
if (N.getValueType() == VT) return true;
// Handle the case when VT is iPTR.
- return VT == MVT::iPTR && N.getValueType() == TLI.getPointerTy();
+ return VT == MVT::iPTR && N.getValueType() == TLI->getPointerTy();
}
LLVM_ATTRIBUTE_ALWAYS_INLINE static bool
CheckChildType(const unsigned char *MatcherTable, unsigned &MatcherIndex,
- SDValue N, const TargetLowering &TLI,
+ SDValue N, const TargetLowering *TLI,
unsigned ChildNo) {
if (ChildNo >= N.getNumOperands())
return false; // Match fails if out of range child #.
return ::CheckType(MatcherTable, MatcherIndex, N.getOperand(ChildNo), TLI);
}
-
LLVM_ATTRIBUTE_ALWAYS_INLINE static bool
CheckCondCode(const unsigned char *MatcherTable, unsigned &MatcherIndex,
SDValue N) {
LLVM_ATTRIBUTE_ALWAYS_INLINE static bool
CheckValueType(const unsigned char *MatcherTable, unsigned &MatcherIndex,
- SDValue N, const TargetLowering &TLI) {
+ SDValue N, const TargetLowering *TLI) {
MVT::SimpleValueType VT = (MVT::SimpleValueType)MatcherTable[MatcherIndex++];
if (cast<VTSDNode>(N)->getVT() == VT)
return true;
// Handle the case when VT is iPTR.
- return VT == MVT::iPTR && cast<VTSDNode>(N)->getVT() == TLI.getPointerTy();
+ return VT == MVT::iPTR && cast<VTSDNode>(N)->getVT() == TLI->getPointerTy();
}
LLVM_ATTRIBUTE_ALWAYS_INLINE static bool
Result = !::CheckOpcode(Table, Index, N.getNode());
return Index;
case SelectionDAGISel::OPC_CheckType:
- Result = !::CheckType(Table, Index, N, SDISel.TLI);
+ Result = !::CheckType(Table, Index, N, SDISel.getTargetLowering());
return Index;
case SelectionDAGISel::OPC_CheckChild0Type:
case SelectionDAGISel::OPC_CheckChild1Type:
case SelectionDAGISel::OPC_CheckChild5Type:
case SelectionDAGISel::OPC_CheckChild6Type:
case SelectionDAGISel::OPC_CheckChild7Type:
- Result = !::CheckChildType(Table, Index, N, SDISel.TLI,
+ Result = !::CheckChildType(Table, Index, N, SDISel.getTargetLowering(),
Table[Index-1] - SelectionDAGISel::OPC_CheckChild0Type);
return Index;
case SelectionDAGISel::OPC_CheckCondCode:
Result = !::CheckCondCode(Table, Index, N);
return Index;
case SelectionDAGISel::OPC_CheckValueType:
- Result = !::CheckValueType(Table, Index, N, SDISel.TLI);
+ Result = !::CheckValueType(Table, Index, N, SDISel.getTargetLowering());
return Index;
case SelectionDAGISel::OPC_CheckInteger:
Result = !::CheckInteger(Table, Index, N);
SmallVector<SDNode*, 3> ChainNodesMatched;
SmallVector<SDNode*, 3> GlueResultNodesMatched;
- DEBUG(errs() << "ISEL: Starting pattern match on root node: ";
+ DEBUG(dbgs() << "ISEL: Starting pattern match on root node: ";
NodeToMatch->dump(CurDAG);
- errs() << '\n');
+ dbgs() << '\n');
// Determine where to start the interpreter. Normally we start at opcode #0,
// but if the state machine starts with an OPC_SwitchOpcode, then we
// Already computed the OpcodeOffset table, just index into it.
if (N.getOpcode() < OpcodeOffset.size())
MatcherIndex = OpcodeOffset[N.getOpcode()];
- DEBUG(errs() << " Initial Opcode index to " << MatcherIndex << "\n");
+ DEBUG(dbgs() << " Initial Opcode index to " << MatcherIndex << "\n");
} else if (MatcherTable[0] == OPC_SwitchOpcode) {
// Otherwise, the table isn't computed, but the state machine does start
if (!Result)
break;
- DEBUG(errs() << " Skipped scope entry (due to false predicate) at "
+ DEBUG(dbgs() << " Skipped scope entry (due to false predicate) at "
<< "index " << MatcherIndexOfPredicate
<< ", continuing at " << FailIndex << "\n");
++NumDAGIselRetries;
continue;
case OPC_CheckType:
- if (!::CheckType(MatcherTable, MatcherIndex, N, TLI)) break;
+ if (!::CheckType(MatcherTable, MatcherIndex, N, getTargetLowering()))
+ break;
continue;
case OPC_SwitchOpcode: {
if (CaseSize == 0) break;
// Otherwise, execute the case we found.
- DEBUG(errs() << " OpcodeSwitch from " << SwitchStart
+ DEBUG(dbgs() << " OpcodeSwitch from " << SwitchStart
<< " to " << MatcherIndex << "\n");
continue;
}
case OPC_SwitchType: {
- MVT CurNodeVT = N.getValueType().getSimpleVT();
+ MVT CurNodeVT = N.getSimpleValueType();
unsigned SwitchStart = MatcherIndex-1; (void)SwitchStart;
unsigned CaseSize;
while (1) {
MVT CaseVT = (MVT::SimpleValueType)MatcherTable[MatcherIndex++];
if (CaseVT == MVT::iPTR)
- CaseVT = TLI.getPointerTy();
+ CaseVT = getTargetLowering()->getPointerTy();
// If the VT matches, then we will execute this case.
if (CurNodeVT == CaseVT)
if (CaseSize == 0) break;
// Otherwise, execute the case we found.
- DEBUG(errs() << " TypeSwitch[" << EVT(CurNodeVT).getEVTString()
+ DEBUG(dbgs() << " TypeSwitch[" << EVT(CurNodeVT).getEVTString()
<< "] from " << SwitchStart << " to " << MatcherIndex<<'\n');
continue;
}
case OPC_CheckChild2Type: case OPC_CheckChild3Type:
case OPC_CheckChild4Type: case OPC_CheckChild5Type:
case OPC_CheckChild6Type: case OPC_CheckChild7Type:
- if (!::CheckChildType(MatcherTable, MatcherIndex, N, TLI,
+ if (!::CheckChildType(MatcherTable, MatcherIndex, N, getTargetLowering(),
Opcode-OPC_CheckChild0Type))
break;
continue;
if (!::CheckCondCode(MatcherTable, MatcherIndex, N)) break;
continue;
case OPC_CheckValueType:
- if (!::CheckValueType(MatcherTable, MatcherIndex, N, TLI)) break;
+ if (!::CheckValueType(MatcherTable, MatcherIndex, N, getTargetLowering()))
+ break;
continue;
case OPC_CheckInteger:
if (!::CheckInteger(MatcherTable, MatcherIndex, N)) break;
SDValue Imm = RecordedNodes[RecNo].first;
if (Imm->getOpcode() == ISD::Constant) {
- int64_t Val = cast<ConstantSDNode>(Imm)->getZExtValue();
- Imm = CurDAG->getTargetConstant(Val, Imm.getValueType());
+ const ConstantInt *Val=cast<ConstantSDNode>(Imm)->getConstantIntValue();
+ Imm = CurDAG->getConstant(*Val, Imm.getValueType(), true);
} else if (Imm->getOpcode() == ISD::ConstantFP) {
const ConstantFP *Val=cast<ConstantFPSDNode>(Imm)->getConstantFPValue();
- Imm = CurDAG->getTargetConstantFP(*Val, Imm.getValueType());
+ Imm = CurDAG->getConstantFP(*Val, Imm.getValueType(), true);
}
RecordedNodes.push_back(std::make_pair(Imm, RecordedNodes[RecNo].second));
if (InputChain.getNode() == 0)
InputChain = CurDAG->getEntryNode();
- InputChain = CurDAG->getCopyToReg(InputChain, NodeToMatch->getDebugLoc(),
+ InputChain = CurDAG->getCopyToReg(InputChain, SDLoc(NodeToMatch),
DestPhysReg, RecordedNodes[RecNo].first,
InputGlue);
for (unsigned i = 0; i != NumVTs; ++i) {
MVT::SimpleValueType VT =
(MVT::SimpleValueType)MatcherTable[MatcherIndex++];
- if (VT == MVT::iPTR) VT = TLI.getPointerTy().SimpleTy;
+ if (VT == MVT::iPTR) VT = getTargetLowering()->getPointerTy().SimpleTy;
VTs.push_back(VT);
}
if (Opcode != OPC_MorphNodeTo) {
// If this is a normal EmitNode command, just create the new node and
// add the results to the RecordedNodes list.
- Res = CurDAG->getMachineNode(TargetOpc, NodeToMatch->getDebugLoc(),
- VTList, Ops.data(), Ops.size());
+ Res = CurDAG->getMachineNode(TargetOpc, SDLoc(NodeToMatch),
+ VTList, Ops);
// Add all the non-glue/non-chain results to the RecordedNodes list.
for (unsigned i = 0, e = VTs.size(); i != e; ++i) {
bool mayStore = MCID.mayStore();
unsigned NumMemRefs = 0;
- for (SmallVector<MachineMemOperand*, 2>::const_iterator I =
- MatchedMemRefs.begin(), E = MatchedMemRefs.end(); I != E; ++I) {
+ for (SmallVectorImpl<MachineMemOperand *>::const_iterator I =
+ MatchedMemRefs.begin(), E = MatchedMemRefs.end(); I != E; ++I) {
if ((*I)->isLoad()) {
if (mayLoad)
++NumMemRefs;
MF->allocateMemRefsArray(NumMemRefs);
MachineSDNode::mmo_iterator MemRefsPos = MemRefs;
- for (SmallVector<MachineMemOperand*, 2>::const_iterator I =
- MatchedMemRefs.begin(), E = MatchedMemRefs.end(); I != E; ++I) {
+ for (SmallVectorImpl<MachineMemOperand *>::const_iterator I =
+ MatchedMemRefs.begin(), E = MatchedMemRefs.end(); I != E; ++I) {
if ((*I)->isLoad()) {
if (mayLoad)
*MemRefsPos++ = *I;
->setMemRefs(MemRefs, MemRefs + NumMemRefs);
}
- DEBUG(errs() << " "
+ DEBUG(dbgs() << " "
<< (Opcode == OPC_MorphNodeTo ? "Morphed" : "Created")
- << " node: "; Res->dump(CurDAG); errs() << "\n");
+ << " node: "; Res->dump(CurDAG); dbgs() << "\n");
// If this was a MorphNodeTo then we're completely done!
if (Opcode == OPC_MorphNodeTo) {
// If the code reached this point, then the match failed. See if there is
// another child to try in the current 'Scope', otherwise pop it until we
// find a case to check.
- DEBUG(errs() << " Match failed at index " << CurrentOpcodeIndex << "\n");
+ DEBUG(dbgs() << " Match failed at index " << CurrentOpcodeIndex << "\n");
++NumDAGIselRetries;
while (1) {
if (MatchScopes.empty()) {
MatchedMemRefs.resize(LastScope.NumMatchedMemRefs);
MatcherIndex = LastScope.FailIndex;
- DEBUG(errs() << " Continuing at " << MatcherIndex << "\n");
+ DEBUG(dbgs() << " Continuing at " << MatcherIndex << "\n");
InputChain = LastScope.InputChain;
InputGlue = LastScope.InputGlue;