diff --git a/lib/CodeGen/SelectionDAG/SelectionDAGISel.cpp b/lib/CodeGen/SelectionDAG/SelectionDAGISel.cpp
index fab75227d9f5637528b69b38c9c6d0ede99fd33e..1d0ed3af453c4b43b2eff36a40487cca72b38cd5 100644 (file)
#include "llvm/ADT/Statistic.h"
#include "llvm/Analysis/AliasAnalysis.h"
#include "llvm/Analysis/BranchProbabilityInfo.h"
+#include "llvm/Analysis/CFG.h"
#include "llvm/Analysis/TargetTransformInfo.h"
#include "llvm/CodeGen/FastISel.h"
#include "llvm/CodeGen/FunctionLoweringInfo.h"
const TargetLowering *TLI = IS->getTargetLowering();
const TargetSubtargetInfo &ST = IS->TM.getSubtarget<TargetSubtargetInfo>();
- if (OptLevel == CodeGenOpt::None || ST.enableMachineScheduler() ||
+ if (OptLevel == CodeGenOpt::None || ST.useMachineScheduler() ||
TLI->getSchedulingPreference() == Sched::Source)
return createSourceListDAGScheduler(IS, OptLevel);
if (TLI->getSchedulingPreference() == Sched::RegPressure)
EntryMBB->insert(EntryMBB->begin(), MI);
else {
MachineInstr *Def = RegInfo->getVRegDef(Reg);
- MachineBasicBlock::iterator InsertPos = Def;
- // FIXME: VR def may not be in entry block.
- Def->getParent()->insert(llvm::next(InsertPos), MI);
+ if (Def) {
+ MachineBasicBlock::iterator InsertPos = Def;
+ // FIXME: VR def may not be in entry block.
+ Def->getParent()->insert(llvm::next(InsertPos), MI);
+ } else
+ DEBUG(dbgs() << "Dropping debug info for dead vreg"
+ << TargetRegisterInfo::virtReg2Index(Reg) << "\n");
}
// If Reg is live-in then update debug info to track its copy in a vreg.
MachineBasicBlock::iterator InsertPos = Def;
const MDNode *Variable =
MI->getOperand(MI->getNumOperands()-1).getMetadata();
- unsigned Offset = MI->getOperand(1).getImm();
+ bool IsIndirect = MI->isIndirectDebugValue();
+ unsigned Offset = IsIndirect ? MI->getOperand(1).getImm() : 0;
// Def is never a terminator here, so it is ok to increment InsertPos.
BuildMI(*EntryMBB, ++InsertPos, MI->getDebugLoc(),
- TII.get(TargetOpcode::DBG_VALUE))
- .addReg(LDI->second, RegState::Debug)
- .addImm(Offset).addMetadata(Variable);
+ TII.get(TargetOpcode::DBG_VALUE),
+ IsIndirect,
+ LDI->second, Offset, Variable);
// If this vreg is directly copied into an exported register then
// that COPY instructions also need DBG_VALUE, if it is the only
if (CopyUseMI) {
MachineInstr *NewMI =
BuildMI(*MF, CopyUseMI->getDebugLoc(),
- TII.get(TargetOpcode::DBG_VALUE))
- .addReg(CopyUseMI->getOperand(0).getReg(), RegState::Debug)
- .addImm(Offset).addMetadata(Variable);
+ TII.get(TargetOpcode::DBG_VALUE),
+ IsIndirect,
+ CopyUseMI->getOperand(0).getReg(),
+ Offset, Variable);
MachineBasicBlock::iterator Pos = CopyUseMI;
EntryMBB->insertAfter(Pos, NewMI);
}
if (J == E) break;
To = J->second;
}
+ // Make sure the new register has a sufficiently constrained register class.
+ if (TargetRegisterInfo::isVirtualRegister(From) &&
+ TargetRegisterInfo::isVirtualRegister(To))
+ MRI.constrainRegClass(To, MRI.getRegClass(From));
// Replace it.
MRI.replaceRegWith(From, To);
}
// Mark exception register as live in.
const TargetLowering *TLI = getTargetLowering();
- unsigned Reg = TLI->getExceptionPointerRegister();
- if (Reg) MBB->addLiveIn(Reg);
+ const TargetRegisterClass *PtrRC = TLI->getRegClassFor(TLI->getPointerTy());
+ if (unsigned Reg = TLI->getExceptionPointerRegister())
+ FuncInfo->ExceptionPointerVirtReg = MBB->addLiveIn(Reg, PtrRC);
// Mark exception selector register as live in.
- Reg = TLI->getExceptionSelectorRegister();
- if (Reg) MBB->addLiveIn(Reg);
+ if (unsigned Reg = TLI->getExceptionSelectorRegister())
+ FuncInfo->ExceptionSelectorVirtReg = MBB->addLiveIn(Reg, PtrRC);
}
/// isFoldedOrDeadInstruction - Return true if the specified instruction is
FuncInfo->InsertPt = FuncInfo->MBB->getFirstNonPHI();
// Setup an EH landing-pad block.
+ FuncInfo->ExceptionPointerVirtReg = 0;
+ FuncInfo->ExceptionSelectorVirtReg = 0;
if (FuncInfo->MBB->isLandingPad())
PrepareEHLandingPad();
delete FastIS;
SDB->clearDanglingDebugInfo();
+ SDB->SPDescriptor.resetPerFunctionState();
+}
+
+/// Given that the input MI is before a partial terminator sequence TSeq, return
+/// true if M + TSeq also a partial terminator sequence.
+///
+/// A Terminator sequence is a sequence of MachineInstrs which at this point in
+/// lowering copy vregs into physical registers, which are then passed into
+/// terminator instructors so we can satisfy ABI constraints. A partial
+/// terminator sequence is an improper subset of a terminator sequence (i.e. it
+/// may be the whole terminator sequence).
+static bool MIIsInTerminatorSequence(const MachineInstr *MI) {
+ // If we do not have a copy or an implicit def, we return true if and only if
+ // MI is a debug value.
+ if (!MI->isCopy() && !MI->isImplicitDef())
+ // Sometimes DBG_VALUE MI sneak in between the copies from the vregs to the
+ // physical registers if there is debug info associated with the terminator
+ // of our mbb. We want to include said debug info in our terminator
+ // sequence, so we return true in that case.
+ return MI->isDebugValue();
+
+ // We have left the terminator sequence if we are not doing one of the
+ // following:
+ //
+ // 1. Copying a vreg into a physical register.
+ // 2. Copying a vreg into a vreg.
+ // 3. Defining a register via an implicit def.
+
+ // OPI should always be a register definition...
+ MachineInstr::const_mop_iterator OPI = MI->operands_begin();
+ if (!OPI->isReg() || !OPI->isDef())
+ return false;
+
+ // Defining any register via an implicit def is always ok.
+ if (MI->isImplicitDef())
+ return true;
+
+ // Grab the copy source...
+ MachineInstr::const_mop_iterator OPI2 = OPI;
+ ++OPI2;
+ assert(OPI2 != MI->operands_end()
+ && "Should have a copy implying we should have 2 arguments.");
+
+ // Make sure that the copy dest is not a vreg when the copy source is a
+ // physical register.
+ if (!OPI2->isReg() ||
+ (!TargetRegisterInfo::isPhysicalRegister(OPI->getReg()) &&
+ TargetRegisterInfo::isPhysicalRegister(OPI2->getReg())))
+ return false;
+
+ return true;
+}
+
+/// Find the split point at which to splice the end of BB into its success stack
+/// protector check machine basic block.
+///
+/// On many platforms, due to ABI constraints, terminators, even before register
+/// allocation, use physical registers. This creates an issue for us since
+/// physical registers at this point can not travel across basic
+/// blocks. Luckily, selectiondag always moves physical registers into vregs
+/// when they enter functions and moves them through a sequence of copies back
+/// into the physical registers right before the terminator creating a
+/// ``Terminator Sequence''. This function is searching for the beginning of the
+/// terminator sequence so that we can ensure that we splice off not just the
+/// terminator, but additionally the copies that move the vregs into the
+/// physical registers.
+static MachineBasicBlock::iterator
+FindSplitPointForStackProtector(MachineBasicBlock *BB, DebugLoc DL) {
+ MachineBasicBlock::iterator SplitPoint = BB->getFirstTerminator();
+ //
+ if (SplitPoint == BB->begin())
+ return SplitPoint;
+
+ MachineBasicBlock::iterator Start = BB->begin();
+ MachineBasicBlock::iterator Previous = SplitPoint;
+ --Previous;
+
+ while (MIIsInTerminatorSequence(Previous)) {
+ SplitPoint = Previous;
+ if (Previous == Start)
+ break;
+ --Previous;
+ }
+
+ return SplitPoint;
}
void
<< FuncInfo->PHINodesToUpdate[i].first
<< ", " << FuncInfo->PHINodesToUpdate[i].second << ")\n");
+ const bool MustUpdatePHINodes = SDB->SwitchCases.empty() &&
+ SDB->JTCases.empty() &&
+ SDB->BitTestCases.empty();
+
// Next, now that we know what the last MBB the LLVM BB expanded is, update
// PHI nodes in successors.
- if (SDB->SwitchCases.empty() &&
- SDB->JTCases.empty() &&
- SDB->BitTestCases.empty()) {
+ if (MustUpdatePHINodes) {
for (unsigned i = 0, e = FuncInfo->PHINodesToUpdate.size(); i != e; ++i) {
MachineInstrBuilder PHI(*MF, FuncInfo->PHINodesToUpdate[i].first);
assert(PHI->isPHI() &&
continue;
PHI.addReg(FuncInfo->PHINodesToUpdate[i].second).addMBB(FuncInfo->MBB);
}
- return;
}
+ // Handle stack protector.
+ if (SDB->SPDescriptor.shouldEmitStackProtector()) {
+ MachineBasicBlock *ParentMBB = SDB->SPDescriptor.getParentMBB();
+ MachineBasicBlock *SuccessMBB = SDB->SPDescriptor.getSuccessMBB();
+
+ // Find the split point to split the parent mbb. At the same time copy all
+ // physical registers used in the tail of parent mbb into virtual registers
+ // before the split point and back into physical registers after the split
+ // point. This prevents us needing to deal with Live-ins and many other
+ // register allocation issues caused by us splitting the parent mbb. The
+ // register allocator will clean up said virtual copies later on.
+ MachineBasicBlock::iterator SplitPoint =
+ FindSplitPointForStackProtector(ParentMBB, SDB->getCurDebugLoc());
+
+ // Splice the terminator of ParentMBB into SuccessMBB.
+ SuccessMBB->splice(SuccessMBB->end(), ParentMBB,
+ SplitPoint,
+ ParentMBB->end());
+
+ // Add compare/jump on neq/jump to the parent BB.
+ FuncInfo->MBB = ParentMBB;
+ FuncInfo->InsertPt = ParentMBB->end();
+ SDB->visitSPDescriptorParent(SDB->SPDescriptor, ParentMBB);
+ CurDAG->setRoot(SDB->getRoot());
+ SDB->clear();
+ CodeGenAndEmitDAG();
+
+ // CodeGen Failure MBB if we have not codegened it yet.
+ MachineBasicBlock *FailureMBB = SDB->SPDescriptor.getFailureMBB();
+ if (!FailureMBB->size()) {
+ FuncInfo->MBB = FailureMBB;
+ FuncInfo->InsertPt = FailureMBB->end();
+ SDB->visitSPDescriptorFailure(SDB->SPDescriptor);
+ CurDAG->setRoot(SDB->getRoot());
+ SDB->clear();
+ CodeGenAndEmitDAG();
+ }
+
+ // Clear the Per-BB State.
+ SDB->SPDescriptor.resetPerBBState();
+ }
+
+ // If we updated PHI Nodes, return early.
+ if (MustUpdatePHINodes)
+ return;
+
for (unsigned i = 0, e = SDB->BitTestCases.size(); i != e; ++i) {
// Lower header first, if it wasn't already lowered
if (!SDB->BitTestCases[i].Emitted) {
SDNode *User = *UI;
+ if (User->getOpcode() == ISD::HANDLENODE) // Root of the graph.
+ continue;
+
// If we see an already-selected machine node, then we've gone beyond the
// pattern that we're selecting down into the already selected chunk of the
// DAG.
- if (User->isMachineOpcode() ||
- User->getOpcode() == ISD::HANDLENODE) // Root of the graph.
- continue;
-
unsigned UserOpcode = User->getOpcode();
- if (UserOpcode == ISD::CopyToReg ||
+ if (User->isMachineOpcode() ||
+ UserOpcode == ISD::CopyToReg ||
UserOpcode == ISD::CopyFromReg ||
UserOpcode == ISD::INLINEASM ||
UserOpcode == ISD::EH_LABEL ||
}
}
- SDValue Res;
if (InputChains.size() == 1)
return InputChains[0];
return CurDAG->getNode(ISD::TokenFactor, SDLoc(ChainNodesMatched[0]),
}
case OPC_SwitchType: {
- MVT CurNodeVT = N.getValueType().getSimpleVT();
+ MVT CurNodeVT = N.getSimpleValueType();
unsigned SwitchStart = MatcherIndex-1; (void)SwitchStart;
unsigned CaseSize;
while (1) {
bool mayStore = MCID.mayStore();
unsigned NumMemRefs = 0;
- for (SmallVector<MachineMemOperand*, 2>::const_iterator I =
- MatchedMemRefs.begin(), E = MatchedMemRefs.end(); I != E; ++I) {
+ for (SmallVectorImpl<MachineMemOperand *>::const_iterator I =
+ MatchedMemRefs.begin(), E = MatchedMemRefs.end(); I != E; ++I) {
if ((*I)->isLoad()) {
if (mayLoad)
++NumMemRefs;
MF->allocateMemRefsArray(NumMemRefs);
MachineSDNode::mmo_iterator MemRefsPos = MemRefs;
- for (SmallVector<MachineMemOperand*, 2>::const_iterator I =
- MatchedMemRefs.begin(), E = MatchedMemRefs.end(); I != E; ++I) {
+ for (SmallVectorImpl<MachineMemOperand *>::const_iterator I =
+ MatchedMemRefs.begin(), E = MatchedMemRefs.end(); I != E; ++I) {
if ((*I)->isLoad()) {
if (mayLoad)
*MemRefsPos++ = *I;