diff --git a/lib/IR/DebugInfo.cpp b/lib/IR/DebugInfo.cpp
index db9e56defa12d5680765d8c8d7caaa0fc9c52993..42b0dc0fc271b0cf1544b5b8ac66a47d269c395d 100644 (file)
--- a/lib/IR/DebugInfo.cpp
+++ b/lib/IR/DebugInfo.cpp
#include "llvm/ADT/SmallString.h"
#include "llvm/Analysis/ValueTracking.h"
#include "llvm/IR/Constants.h"
+#include "llvm/IR/DIBuilder.h"
#include "llvm/IR/DerivedTypes.h"
#include "llvm/IR/Instructions.h"
#include "llvm/IR/IntrinsicInst.h"
DILexicalBlockFile(DbgNode).Verify() ||
DISubrange(DbgNode).Verify() || DIEnumerator(DbgNode).Verify() ||
DIObjCProperty(DbgNode).Verify() ||
- DIUnspecifiedParameter(DbgNode).Verify() ||
DITemplateTypeParameter(DbgNode).Verify() ||
DITemplateValueParameter(DbgNode).Verify() ||
- DIImportedEntity(DbgNode).Verify());
+ DIImportedEntity(DbgNode).Verify() || DIExpression(DbgNode).Verify());
}
static Value *getField(const MDNode *DbgNode, unsigned Elt) {
}
}
-unsigned DIVariable::getNumAddrElements() const {
- return DbgNode->getNumOperands() - 8;
-}
-
/// getInlinedAt - If this variable is inlined then return inline location.
MDNode *DIVariable::getInlinedAt() const { return getNodeField(DbgNode, 7); }
+/// Return the size reported by the variable's type.
+unsigned DIVariable::getSizeInBits(const DITypeIdentifierMap &Map) {
+ DIType Ty = getType().resolve(Map);
+ // Follow derived types until we reach a type that
+ // reports back a size.
+ while (Ty.isDerivedType() && !Ty.getSizeInBits()) {
+ DIDerivedType DT(&*Ty);
+ Ty = DT.getTypeDerivedFrom().resolve(Map);
+ }
+ assert(Ty.getSizeInBits() && "type with size 0");
+ return Ty.getSizeInBits();
+}
+
+uint64_t DIExpression::getElement(unsigned Idx) const {
+ unsigned I = Idx + 1;
+ if (I < DbgNode->getNumOperands())
+ if (auto *CI = dyn_cast_or_null<ConstantInt>(DbgNode->getOperand(I)))
+ return CI->getZExtValue();
+
+ assert(false && "non-existing complex address element requested");
+ return 0;
+}
+
+bool DIExpression::isVariablePiece() const {
+ return getNumElements() && getElement(0) == dwarf::DW_OP_piece;
+}
+
+uint64_t DIExpression::getPieceOffset() const {
+ assert(isVariablePiece());
+ return getElement(1);
+}
+
+uint64_t DIExpression::getPieceSize() const {
+ assert(isVariablePiece());
+ return getElement(2);
+}
+
//===----------------------------------------------------------------------===//
// Predicates
//===----------------------------------------------------------------------===//
+bool DIDescriptor::isSubroutineType() const {
+ return isCompositeType() && getTag() == dwarf::DW_TAG_subroutine_type;
+}
+
/// isBasicType - Return true if the specified tag is legal for
/// DIBasicType.
bool DIDescriptor::isBasicType() const {
getTag() == dwarf::DW_TAG_constant);
}
-/// isUnspecifiedParmeter - Return true if the specified tag is
-/// DW_TAG_unspecified_parameters.
-bool DIDescriptor::isUnspecifiedParameter() const {
- return DbgNode && getTag() == dwarf::DW_TAG_unspecified_parameters;
-}
-
/// isScope - Return true if the specified tag is one of the scope
/// related tag.
bool DIDescriptor::isScope() const {
/// lexical block with an extra file.
bool DIDescriptor::isLexicalBlockFile() const {
return DbgNode && getTag() == dwarf::DW_TAG_lexical_block &&
- (DbgNode->getNumOperands() == 3);
+ (DbgNode->getNumOperands() == 4);
}
/// isLexicalBlock - Return true if the specified tag is DW_TAG_lexical_block.
getTag() == dwarf::DW_TAG_imported_declaration);
}
+/// \brief Return true if the specified tag is DW_TAG_imported_module or
+/// DW_TAG_imported_declaration.
+bool DIDescriptor::isExpression() const {
+ return DbgNode && (getTag() == dwarf::DW_TAG_expression);
+}
+
//===----------------------------------------------------------------------===//
// Simple Descriptor Constructors and other Methods
//===----------------------------------------------------------------------===//
-unsigned DIArray::getNumElements() const {
- if (!DbgNode)
- return 0;
- return DbgNode->getNumOperands();
-}
-
/// replaceAllUsesWith - Replace all uses of the MDNode used by this
/// type with the one in the passed descriptor.
-void DIType::replaceAllUsesWith(LLVMContext &VMContext, DIDescriptor D) {
+void DIDescriptor::replaceAllUsesWith(LLVMContext &VMContext, DIDescriptor D) {
assert(DbgNode && "Trying to replace an unverified type!");
const Value *V = cast_or_null<Value>(DN);
Node->replaceAllUsesWith(const_cast<Value *>(V));
MDNode::deleteTemporary(Node);
- DbgNode = D;
+ DbgNode = DN;
}
/// replaceAllUsesWith - Replace all uses of the MDNode used by this
/// type with the one in D.
-void DIType::replaceAllUsesWith(MDNode *D) {
+void DIDescriptor::replaceAllUsesWith(MDNode *D) {
assert(DbgNode && "Trying to replace an unverified type!");
assert(DbgNode != D && "This replacement should always happen");
Tag != dwarf::DW_TAG_inheritance && Tag != dwarf::DW_TAG_friend &&
getFilename().empty())
return false;
+
// DIType is abstract, it should be a BasicType, a DerivedType or
// a CompositeType.
if (isBasicType())
// Make sure that type @ field 5 is a DITypeRef.
if (!fieldIsTypeRef(DbgNode, 5))
return false;
- return DbgNode->getNumOperands() >= 8;
+
+ // Variable without an inline location.
+ if (DbgNode->getNumOperands() == 7)
+ return true;
+
+ return DbgNode->getNumOperands() == 8;
+}
+
+/// Verify - Verify that a variable descriptor is well formed.
+bool DIExpression::Verify() const {
+ // Empty DIExpressions may be represented as a nullptr.
+ if (!DbgNode)
+ return true;
+
+ return isExpression();
}
/// Verify - Verify that a location descriptor is well formed.
/// \brief Verify that the lexical block descriptor is well formed.
bool DILexicalBlock::Verify() const {
- return isLexicalBlock() && DbgNode->getNumOperands() == 7;
+ return isLexicalBlock() && DbgNode->getNumOperands() == 6;
}
/// \brief Verify that the file-scoped lexical block descriptor is well formed.
bool DILexicalBlockFile::Verify() const {
- return isLexicalBlockFile() && DbgNode->getNumOperands() == 3;
-}
-
-/// \brief Verify that an unspecified parameter descriptor is well formed.
-bool DIUnspecifiedParameter::Verify() const {
- return isUnspecifiedParameter() && DbgNode->getNumOperands() == 1;
+ return isLexicalBlockFile() && DbgNode->getNumOperands() == 4;
}
/// \brief Verify that the template type parameter descriptor is well formed.
#endif
/// \brief Set the array of member DITypes.
-void DICompositeType::setTypeArray(DIArray Elements, DIArray TParams) {
- assert((!TParams || DbgNode->getNumOperands() == 15) &&
- "If you're setting the template parameters this should include a slot "
- "for that!");
+void DICompositeType::setArraysHelper(MDNode *Elements, MDNode *TParams) {
TrackingVH<MDNode> N(*this);
if (Elements) {
#ifndef NDEBUG
/// copyWithNewScope - Return a copy of this location, replacing the
/// current scope with the given one.
DILocation DILocation::copyWithNewScope(LLVMContext &Ctx,
- DILexicalBlock NewScope) {
+ DILexicalBlockFile NewScope) {
SmallVector<Value *, 10> Elts;
assert(Verify());
for (unsigned I = 0; I < DbgNode->getNumOperands(); ++I) {
if (DT.isCompositeType()) {
DICompositeType DCT(DT);
processType(DCT.getTypeDerivedFrom().resolve(TypeIdentifierMap));
- DIArray DA = DCT.getTypeArray();
+ if (DT.isSubroutineType()) {
+ DITypeArray DTA = DISubroutineType(DT).getTypeArray();
+ for (unsigned i = 0, e = DTA.getNumElements(); i != e; ++i)
+ processType(DTA.getElement(i).resolve(TypeIdentifierMap));
+ return;
+ }
+ DIArray DA = DCT.getElements();
for (unsigned i = 0, e = DA.getNumElements(); i != e; ++i) {
DIDescriptor D = DA.getElement(i);
if (D.isType())
DINameSpace(DbgNode).printInternal(OS);
} else if (this->isScope()) {
DIScope(DbgNode).printInternal(OS);
+ } else if (this->isExpression()) {
+ DIExpression(DbgNode).printInternal(OS);
}
}
OS << " [private]";
else if (isProtected())
OS << " [protected]";
+ else if (isPublic())
+ OS << " [public]";
if (isArtificial())
OS << " [artificial]";
void DICompositeType::printInternal(raw_ostream &OS) const {
DIType::printInternal(OS);
- DIArray A = getTypeArray();
+ DIArray A = getElements();
OS << " [" << A.getNumElements() << " elements]";
}
OS << " [private]";
else if (isProtected())
OS << " [protected]";
+ else if (isPublic())
+ OS << " [public]";
if (isLValueReference())
OS << " [reference]";
OS << " [line " << getLineNumber() << ']';
}
+void DIExpression::printInternal(raw_ostream &OS) const {
+ for (unsigned I = 0; I < getNumElements(); ++I) {
+ uint64_t OpCode = getElement(I);
+ OS << " [" << OperationEncodingString(OpCode);
+ switch (OpCode) {
+ case DW_OP_plus: {
+ OS << " " << getElement(++I);
+ break;
+ }
+ case DW_OP_piece: {
+ unsigned Offset = getElement(++I);
+ unsigned Size = getElement(++I);
+ OS << " offset=" << Offset << ", size=" << Size;
+ break;
+ }
+ default:
+ // Else bail out early. This may be a line table entry.
+ OS << "Unknown]";
+ return;
+ }
+ OS << "]";
+ }
+}
+
void DIObjCProperty::printInternal(raw_ostream &OS) const {
StringRef Name = getObjCPropertyName();
if (!Name.empty())
return 0;
return cast<ConstantInt>(Val)->getZExtValue();
}
+
+llvm::DenseMap<const llvm::Function *, llvm::DISubprogram>
+llvm::makeSubprogramMap(const Module &M) {
+ DenseMap<const Function *, DISubprogram> R;
+
+ NamedMDNode *CU_Nodes = M.getNamedMetadata("llvm.dbg.cu");
+ if (!CU_Nodes)
+ return R;
+
+ for (MDNode *N : CU_Nodes->operands()) {
+ DICompileUnit CUNode(N);
+ DIArray SPs = CUNode.getSubprograms();
+ for (unsigned i = 0, e = SPs.getNumElements(); i != e; ++i) {
+ DISubprogram SP(SPs.getElement(i));
+ if (Function *F = SP.getFunction())
+ R.insert(std::make_pair(F, SP));
+ }
+ }
+ return R;
+}