diff --git a/lib/IR/DebugInfo.cpp b/lib/IR/DebugInfo.cpp
index f7215dc51e1e2d996739c6617f15b4a01b0585e7..42b0dc0fc271b0cf1544b5b8ac66a47d269c395d 100644 (file)
--- a/lib/IR/DebugInfo.cpp
+++ b/lib/IR/DebugInfo.cpp
//
//===----------------------------------------------------------------------===//
-#include "llvm/DebugInfo.h"
+#include "llvm/IR/DebugInfo.h"
+#include "LLVMContextImpl.h"
#include "llvm/ADT/STLExtras.h"
#include "llvm/ADT/SmallPtrSet.h"
#include "llvm/ADT/SmallString.h"
#include "llvm/Analysis/ValueTracking.h"
#include "llvm/IR/Constants.h"
+#include "llvm/IR/DIBuilder.h"
#include "llvm/IR/DerivedTypes.h"
#include "llvm/IR/Instructions.h"
#include "llvm/IR/IntrinsicInst.h"
#include "llvm/IR/Intrinsics.h"
#include "llvm/IR/Module.h"
+#include "llvm/IR/ValueHandle.h"
#include "llvm/Support/Debug.h"
#include "llvm/Support/Dwarf.h"
-#include "llvm/Support/ValueHandle.h"
#include "llvm/Support/raw_ostream.h"
using namespace llvm;
using namespace llvm::dwarf;
DIObjCProperty(DbgNode).Verify() ||
DITemplateTypeParameter(DbgNode).Verify() ||
DITemplateValueParameter(DbgNode).Verify() ||
- DIImportedEntity(DbgNode).Verify());
+ DIImportedEntity(DbgNode).Verify() || DIExpression(DbgNode).Verify());
}
static Value *getField(const MDNode *DbgNode, unsigned Elt) {
- if (DbgNode == 0 || Elt >= DbgNode->getNumOperands())
- return 0;
+ if (!DbgNode || Elt >= DbgNode->getNumOperands())
+ return nullptr;
return DbgNode->getOperand(Elt);
}
}
uint64_t DIDescriptor::getUInt64Field(unsigned Elt) const {
- if (DbgNode == 0)
+ if (!DbgNode)
return 0;
if (Elt < DbgNode->getNumOperands())
}
int64_t DIDescriptor::getInt64Field(unsigned Elt) const {
- if (DbgNode == 0)
+ if (!DbgNode)
return 0;
if (Elt < DbgNode->getNumOperands())
}
GlobalVariable *DIDescriptor::getGlobalVariableField(unsigned Elt) const {
- if (DbgNode == 0)
- return 0;
+ if (!DbgNode)
+ return nullptr;
if (Elt < DbgNode->getNumOperands())
return dyn_cast_or_null<GlobalVariable>(DbgNode->getOperand(Elt));
- return 0;
+ return nullptr;
}
Constant *DIDescriptor::getConstantField(unsigned Elt) const {
- if (DbgNode == 0)
- return 0;
+ if (!DbgNode)
+ return nullptr;
if (Elt < DbgNode->getNumOperands())
return dyn_cast_or_null<Constant>(DbgNode->getOperand(Elt));
- return 0;
+ return nullptr;
}
Function *DIDescriptor::getFunctionField(unsigned Elt) const {
- if (DbgNode == 0)
- return 0;
+ if (!DbgNode)
+ return nullptr;
if (Elt < DbgNode->getNumOperands())
return dyn_cast_or_null<Function>(DbgNode->getOperand(Elt));
- return 0;
+ return nullptr;
}
void DIDescriptor::replaceFunctionField(unsigned Elt, Function *F) {
- if (DbgNode == 0)
+ if (!DbgNode)
return;
if (Elt < DbgNode->getNumOperands()) {
}
}
-unsigned DIVariable::getNumAddrElements() const {
- return DbgNode->getNumOperands() - 8;
-}
-
/// getInlinedAt - If this variable is inlined then return inline location.
MDNode *DIVariable::getInlinedAt() const { return getNodeField(DbgNode, 7); }
+/// Return the size reported by the variable's type.
+unsigned DIVariable::getSizeInBits(const DITypeIdentifierMap &Map) {
+ DIType Ty = getType().resolve(Map);
+ // Follow derived types until we reach a type that
+ // reports back a size.
+ while (Ty.isDerivedType() && !Ty.getSizeInBits()) {
+ DIDerivedType DT(&*Ty);
+ Ty = DT.getTypeDerivedFrom().resolve(Map);
+ }
+ assert(Ty.getSizeInBits() && "type with size 0");
+ return Ty.getSizeInBits();
+}
+
+uint64_t DIExpression::getElement(unsigned Idx) const {
+ unsigned I = Idx + 1;
+ if (I < DbgNode->getNumOperands())
+ if (auto *CI = dyn_cast_or_null<ConstantInt>(DbgNode->getOperand(I)))
+ return CI->getZExtValue();
+
+ assert(false && "non-existing complex address element requested");
+ return 0;
+}
+
+bool DIExpression::isVariablePiece() const {
+ return getNumElements() && getElement(0) == dwarf::DW_OP_piece;
+}
+
+uint64_t DIExpression::getPieceOffset() const {
+ assert(isVariablePiece());
+ return getElement(1);
+}
+
+uint64_t DIExpression::getPieceSize() const {
+ assert(isVariablePiece());
+ return getElement(2);
+}
+
//===----------------------------------------------------------------------===//
// Predicates
//===----------------------------------------------------------------------===//
+bool DIDescriptor::isSubroutineType() const {
+ return isCompositeType() && getTag() == dwarf::DW_TAG_subroutine_type;
+}
+
/// isBasicType - Return true if the specified tag is legal for
/// DIBasicType.
bool DIDescriptor::isBasicType() const {
getTag() == dwarf::DW_TAG_constant);
}
-/// isUnspecifiedParmeter - Return true if the specified tag is
-/// DW_TAG_unspecified_parameters.
-bool DIDescriptor::isUnspecifiedParameter() const {
- return DbgNode && getTag() == dwarf::DW_TAG_unspecified_parameters;
-}
-
/// isScope - Return true if the specified tag is one of the scope
/// related tag.
bool DIDescriptor::isScope() const {
/// lexical block with an extra file.
bool DIDescriptor::isLexicalBlockFile() const {
return DbgNode && getTag() == dwarf::DW_TAG_lexical_block &&
- (DbgNode->getNumOperands() == 3);
+ (DbgNode->getNumOperands() == 4);
}
/// isLexicalBlock - Return true if the specified tag is DW_TAG_lexical_block.
getTag() == dwarf::DW_TAG_imported_declaration);
}
+/// \brief Return true if the specified tag is DW_TAG_imported_module or
+/// DW_TAG_imported_declaration.
+bool DIDescriptor::isExpression() const {
+ return DbgNode && (getTag() == dwarf::DW_TAG_expression);
+}
+
//===----------------------------------------------------------------------===//
// Simple Descriptor Constructors and other Methods
//===----------------------------------------------------------------------===//
-unsigned DIArray::getNumElements() const {
- if (!DbgNode)
- return 0;
- return DbgNode->getNumOperands();
-}
-
/// replaceAllUsesWith - Replace all uses of the MDNode used by this
/// type with the one in the passed descriptor.
-void DIType::replaceAllUsesWith(DIDescriptor &D) {
+void DIDescriptor::replaceAllUsesWith(LLVMContext &VMContext, DIDescriptor D) {
assert(DbgNode && "Trying to replace an unverified type!");
// which, due to uniquing, has merged with the source. We shield clients from
// this detail by allowing a value to be replaced with replaceAllUsesWith()
// itself.
- if (DbgNode != D) {
- MDNode *Node = const_cast<MDNode *>(DbgNode);
- const MDNode *DN = D;
- const Value *V = cast_or_null<Value>(DN);
- Node->replaceAllUsesWith(const_cast<Value *>(V));
- MDNode::deleteTemporary(Node);
+ const MDNode *DN = D;
+ if (DbgNode == DN) {
+ SmallVector<Value*, 10> Ops(DbgNode->getNumOperands());
+ for (size_t i = 0; i != Ops.size(); ++i)
+ Ops[i] = DbgNode->getOperand(i);
+ DN = MDNode::get(VMContext, Ops);
}
+
+ MDNode *Node = const_cast<MDNode *>(DbgNode);
+ const Value *V = cast_or_null<Value>(DN);
+ Node->replaceAllUsesWith(const_cast<Value *>(V));
+ MDNode::deleteTemporary(Node);
+ DbgNode = DN;
}
/// replaceAllUsesWith - Replace all uses of the MDNode used by this
/// type with the one in D.
-void DIType::replaceAllUsesWith(MDNode *D) {
+void DIDescriptor::replaceAllUsesWith(MDNode *D) {
assert(DbgNode && "Trying to replace an unverified type!");
-
- // Since we use a TrackingVH for the node, its easy for clients to manufacture
- // legitimate situations where they want to replaceAllUsesWith() on something
- // which, due to uniquing, has merged with the source. We shield clients from
- // this detail by allowing a value to be replaced with replaceAllUsesWith()
- // itself.
- if (DbgNode != D) {
- MDNode *Node = const_cast<MDNode *>(DbgNode);
- const MDNode *DN = D;
- const Value *V = cast_or_null<Value>(DN);
- Node->replaceAllUsesWith(const_cast<Value *>(V));
- MDNode::deleteTemporary(Node);
- }
+ assert(DbgNode != D && "This replacement should always happen");
+ MDNode *Node = const_cast<MDNode *>(DbgNode);
+ const MDNode *DN = D;
+ const Value *V = cast_or_null<Value>(DN);
+ Node->replaceAllUsesWith(const_cast<Value *>(V));
+ MDNode::deleteTemporary(Node);
}
/// Verify - Verify that a compile unit is well formed.
if (getFilename().empty())
return false;
- return DbgNode->getNumOperands() == 13;
+ return DbgNode->getNumOperands() == 14;
}
/// Verify - Verify that an ObjC property is well formed.
/// Check if a value can be a ScopeRef.
static bool isScopeRef(const Value *Val) {
return !Val ||
- (isa<MDString>(Val) && !cast<MDString>(Val)->getString().empty()) ||
- (isa<MDNode>(Val) && DIScope(cast<MDNode>(Val)).isScope());
+ (isa<MDString>(Val) && !cast<MDString>(Val)->getString().empty()) ||
+ // Not checking for Val->isScope() here, because it would work
+ // only for lexical scopes and not all subclasses of DIScope.
+ isa<MDNode>(Val);
}
/// Check if a field at position Elt of a MDNode can be a ScopeRef.
Tag != dwarf::DW_TAG_inheritance && Tag != dwarf::DW_TAG_friend &&
getFilename().empty())
return false;
+
// DIType is abstract, it should be a BasicType, a DerivedType or
// a CompositeType.
if (isBasicType())
if (getDisplayName().empty())
return false;
- // Make sure context @ field 2 and type @ field 8 are MDNodes.
+ // Make sure context @ field 2 is an MDNode.
if (!fieldIsMDNode(DbgNode, 2))
return false;
- if (!fieldIsMDNode(DbgNode, 8))
+ // Make sure that type @ field 8 is a DITypeRef.
+ if (!fieldIsTypeRef(DbgNode, 8))
return false;
// Make sure StaticDataMemberDeclaration @ field 12 is MDNode.
if (!fieldIsMDNode(DbgNode, 12))
if (!isVariable())
return false;
- // Make sure context @ field 1 and type @ field 5 are MDNodes.
+ // Make sure context @ field 1 is an MDNode.
if (!fieldIsMDNode(DbgNode, 1))
return false;
- if (!fieldIsMDNode(DbgNode, 5))
+ // Make sure that type @ field 5 is a DITypeRef.
+ if (!fieldIsTypeRef(DbgNode, 5))
return false;
- return DbgNode->getNumOperands() >= 8;
+
+ // Variable without an inline location.
+ if (DbgNode->getNumOperands() == 7)
+ return true;
+
+ return DbgNode->getNumOperands() == 8;
+}
+
+/// Verify - Verify that a variable descriptor is well formed.
+bool DIExpression::Verify() const {
+ // Empty DIExpressions may be represented as a nullptr.
+ if (!DbgNode)
+ return true;
+
+ return isExpression();
}
/// Verify - Verify that a location descriptor is well formed.
/// \brief Verify that the file-scoped lexical block descriptor is well formed.
bool DILexicalBlockFile::Verify() const {
- return isLexicalBlockFile() && DbgNode->getNumOperands() == 3;
+ return isLexicalBlockFile() && DbgNode->getNumOperands() == 4;
}
/// \brief Verify that the template type parameter descriptor is well formed.
#endif
/// \brief Set the array of member DITypes.
-void DICompositeType::setTypeArray(DIArray Elements, DIArray TParams) {
- assert((!TParams || DbgNode->getNumOperands() == 15) &&
- "If you're setting the template parameters this should include a slot "
- "for that!");
+void DICompositeType::setArraysHelper(MDNode *Elements, MDNode *TParams) {
TrackingVH<MDNode> N(*this);
if (Elements) {
#ifndef NDEBUG
return DIScopeRef(DINameSpace(DbgNode).getContext());
assert((isFile() || isCompileUnit()) && "Unhandled type of scope.");
- return DIScopeRef(NULL);
+ return DIScopeRef(nullptr);
}
// If the scope node has a name, return that, else return an empty string.
return DIArray(getNodeField(DbgNode, 11));
}
+/// copyWithNewScope - Return a copy of this location, replacing the
+/// current scope with the given one.
+DILocation DILocation::copyWithNewScope(LLVMContext &Ctx,
+ DILexicalBlockFile NewScope) {
+ SmallVector<Value *, 10> Elts;
+ assert(Verify());
+ for (unsigned I = 0; I < DbgNode->getNumOperands(); ++I) {
+ if (I != 2)
+ Elts.push_back(DbgNode->getOperand(I));
+ else
+ Elts.push_back(NewScope);
+ }
+ MDNode *NewDIL = MDNode::get(Ctx, Elts);
+ return DILocation(NewDIL);
+}
+
+/// computeNewDiscriminator - Generate a new discriminator value for this
+/// file and line location.
+unsigned DILocation::computeNewDiscriminator(LLVMContext &Ctx) {
+ std::pair<const char *, unsigned> Key(getFilename().data(), getLineNumber());
+ return ++Ctx.pImpl->DiscriminatorTable[Key];
+}
+
/// fixupSubprogramName - Replace contains special characters used
/// in a typical Objective-C names with '.' in a given string.
static void fixupSubprogramName(DISubprogram Fn, SmallVectorImpl<char> &Out) {
DIGlobalVariable DIG(GVs.getElement(i));
if (addGlobalVariable(DIG)) {
processScope(DIG.getContext());
- processType(DIG.getType());
+ processType(DIG.getType().resolve(TypeIdentifierMap));
}
}
DIArray SPs = CU.getSubprograms();
DIArray Imports = CU.getImportedEntities();
for (unsigned i = 0, e = Imports.getNumElements(); i != e; ++i) {
DIImportedEntity Import = DIImportedEntity(Imports.getElement(i));
- DIDescriptor Entity = Import.getEntity();
+ DIDescriptor Entity = Import.getEntity().resolve(TypeIdentifierMap);
if (Entity.isType())
processType(DIType(Entity));
else if (Entity.isSubprogram())
if (DT.isCompositeType()) {
DICompositeType DCT(DT);
processType(DCT.getTypeDerivedFrom().resolve(TypeIdentifierMap));
- DIArray DA = DCT.getTypeArray();
+ if (DT.isSubroutineType()) {
+ DITypeArray DTA = DISubroutineType(DT).getTypeArray();
+ for (unsigned i = 0, e = DTA.getNumElements(); i != e; ++i)
+ processType(DTA.getElement(i).resolve(TypeIdentifierMap));
+ return;
+ }
+ DIArray DA = DCT.getElements();
for (unsigned i = 0, e = DA.getNumElements(); i != e; ++i) {
DIDescriptor D = DA.getElement(i);
if (D.isType())
}
}
-/// processLexicalBlock
-void DebugInfoFinder::processLexicalBlock(DILexicalBlock LB) {
- DIScope Context = LB.getContext();
- if (Context.isLexicalBlock())
- return processLexicalBlock(DILexicalBlock(Context));
- else if (Context.isLexicalBlockFile()) {
- DILexicalBlockFile DBF = DILexicalBlockFile(Context);
- return processLexicalBlock(DILexicalBlock(DBF.getScope()));
- } else
- return processSubprogram(DISubprogram(Context));
-}
-
/// processSubprogram - Process DISubprogram.
void DebugInfoFinder::processSubprogram(DISubprogram SP) {
if (!addSubprogram(SP))
if (!NodesSeen.insert(DV))
return;
processScope(DIVariable(N).getContext());
- processType(DIVariable(N).getType());
+ processType(DIVariable(N).getType().resolve(TypeIdentifierMap));
}
void DebugInfoFinder::processValue(const Module &M, const DbgValueInst *DVI) {
@@ -1119,7 +1184,7 @@ void DebugInfoFinder::processValue(const Module &M, const DbgValueInst *DVI) {
if (!NodesSeen.insert(DV))
return;
processScope(DIVariable(N).getContext());
- processType(DIVariable(N).getType());
+ processType(DIVariable(N).getType().resolve(TypeIdentifierMap));
}
/// addType - Add type into Tys.
DINameSpace(DbgNode).printInternal(OS);
} else if (this->isScope()) {
DIScope(DbgNode).printInternal(OS);
+ } else if (this->isExpression()) {
+ DIExpression(DbgNode).printInternal(OS);
}
}
OS << " [private]";
else if (isProtected())
OS << " [protected]";
+ else if (isPublic())
+ OS << " [public]";
if (isArtificial())
OS << " [artificial]";
void DICompositeType::printInternal(raw_ostream &OS) const {
DIType::printInternal(OS);
- DIArray A = getTypeArray();
+ DIArray A = getElements();
OS << " [" << A.getNumElements() << " elements]";
}
OS << " [private]";
else if (isProtected())
OS << " [protected]";
+ else if (isPublic())
+ OS << " [public]";
if (isLValueReference())
OS << " [reference]";
OS << " [line " << getLineNumber() << ']';
}
+void DIExpression::printInternal(raw_ostream &OS) const {
+ for (unsigned I = 0; I < getNumElements(); ++I) {
+ uint64_t OpCode = getElement(I);
+ OS << " [" << OperationEncodingString(OpCode);
+ switch (OpCode) {
+ case DW_OP_plus: {
+ OS << " " << getElement(++I);
+ break;
+ }
+ case DW_OP_piece: {
+ unsigned Offset = getElement(++I);
+ unsigned Size = getElement(++I);
+ OS << " offset=" << Offset << ", size=" << Size;
+ break;
+ }
+ default:
+ // Else bail out early. This may be a line table entry.
+ OS << "Unknown]";
+ return;
+ }
+ OS << "]";
+ }
+}
+
void DIObjCProperty::printInternal(raw_ostream &OS) const {
StringRef Name = getObjCPropertyName();
if (!Name.empty())
// the module.
if (Function *Declare = M.getFunction("llvm.dbg.declare")) {
while (!Declare->use_empty()) {
- CallInst *CI = cast<CallInst>(Declare->use_back());
+ CallInst *CI = cast<CallInst>(Declare->user_back());
CI->eraseFromParent();
}
Declare->eraseFromParent();
if (Function *DbgVal = M.getFunction("llvm.dbg.value")) {
while (!DbgVal->use_empty()) {
- CallInst *CI = cast<CallInst>(DbgVal->use_back());
+ CallInst *CI = cast<CallInst>(DbgVal->user_back());
CI->eraseFromParent();
}
DbgVal->eraseFromParent();
return 0;
return cast<ConstantInt>(Val)->getZExtValue();
}
+
+llvm::DenseMap<const llvm::Function *, llvm::DISubprogram>
+llvm::makeSubprogramMap(const Module &M) {
+ DenseMap<const Function *, DISubprogram> R;
+
+ NamedMDNode *CU_Nodes = M.getNamedMetadata("llvm.dbg.cu");
+ if (!CU_Nodes)
+ return R;
+
+ for (MDNode *N : CU_Nodes->operands()) {
+ DICompileUnit CUNode(N);
+ DIArray SPs = CUNode.getSubprograms();
+ for (unsigned i = 0, e = SPs.getNumElements(); i != e; ++i) {
+ DISubprogram SP(SPs.getElement(i));
+ if (Function *F = SP.getFunction())
+ R.insert(std::make_pair(F, SP));
+ }
+ }
+ return R;
+}