index b0cd415186379840c27b6aad25ee4dce171d1d57..ae7f7dcb0d0555d0aee934c1f10617464e8e077b 100644 (file)
this->setError(CurrentNode, Message);
}
+bool Input::canElideEmptySequence() {
+ return false;
+}
+
Input::MapHNode::~MapHNode() {
for (MapHNode::NameToNode::iterator i = Mapping.begin(), End = Mapping.end();
i != End; ++i) {
void Output::setError(const Twine &message) {
}
+bool Output::canElideEmptySequence() {
+ // Normally, with an optional key/value where the value is an empty sequence,
+ // the whole key/value can be not written. But, that produces wrong yaml
+ // if the key/value is the only thing in the map and the map is used in
+ // a sequence. This detects if the this sequence is the first key/value
+ // in map that itself is embedded in a sequnce.
+ if (StateStack.size() < 2)
+ return true;
+ if (StateStack.back() != inMapFirstKey)
+ return true;
+ return (StateStack[StateStack.size()-2] != inSeq);
+}
+
void Output::output(StringRef s) {
Column += s.size();
Out << s;