index 13a22b1c3fb4ea5cf65c02986c3fb7da7916f6f6..0127c488362d9397c4499da8f15dd83973ce29a5 100644 (file)
#define DEBUG_TYPE "asm-printer"
#include "ARMAsmPrinter.h"
#include "ARM.h"
-#include "ARMBuildAttrs.h"
#include "ARMConstantPoolValue.h"
+#include "ARMFPUName.h"
#include "ARMMachineFunctionInfo.h"
#include "ARMTargetMachine.h"
#include "ARMTargetObjectFile.h"
#include "MCTargetDesc/ARMMCExpr.h"
#include "llvm/ADT/SetVector.h"
#include "llvm/ADT/SmallString.h"
-#include "llvm/Assembly/Writer.h"
#include "llvm/CodeGen/MachineFunctionPass.h"
#include "llvm/CodeGen/MachineJumpTableInfo.h"
#include "llvm/CodeGen/MachineModuleInfoImpls.h"
#include "llvm/DebugInfo.h"
#include "llvm/IR/Constants.h"
#include "llvm/IR/DataLayout.h"
+#include "llvm/IR/Mangler.h"
#include "llvm/IR/Module.h"
#include "llvm/IR/Type.h"
#include "llvm/MC/MCAsmInfo.h"
#include "llvm/MC/MCSectionMachO.h"
#include "llvm/MC/MCStreamer.h"
#include "llvm/MC/MCSymbol.h"
+#include "llvm/Support/ARMBuildAttributes.h"
#include "llvm/Support/CommandLine.h"
#include "llvm/Support/Debug.h"
#include "llvm/Support/ELF.h"
#include "llvm/Support/ErrorHandling.h"
#include "llvm/Support/TargetRegistry.h"
#include "llvm/Support/raw_ostream.h"
-#include "llvm/Target/Mangler.h"
#include "llvm/Target/TargetMachine.h"
#include <cctype>
using namespace llvm;
-namespace {
-
- // Per section and per symbol attributes are not supported.
- // To implement them we would need the ability to delay this emission
- // until the assembly file is fully parsed/generated as only then do we
- // know the symbol and section numbers.
- class AttributeEmitter {
- public:
- virtual void MaybeSwitchVendor(StringRef Vendor) = 0;
- virtual void EmitAttribute(unsigned Attribute, unsigned Value) = 0;
- virtual void EmitTextAttribute(unsigned Attribute, StringRef String) = 0;
- virtual void Finish() = 0;
- virtual ~AttributeEmitter() {}
- };
-
- class AsmAttributeEmitter : public AttributeEmitter {
- MCStreamer &Streamer;
-
- public:
- AsmAttributeEmitter(MCStreamer &Streamer_) : Streamer(Streamer_) {}
- void MaybeSwitchVendor(StringRef Vendor) { }
-
- void EmitAttribute(unsigned Attribute, unsigned Value) {
- Streamer.EmitRawText("\t.eabi_attribute " +
- Twine(Attribute) + ", " + Twine(Value));
- }
-
- void EmitTextAttribute(unsigned Attribute, StringRef String) {
- switch (Attribute) {
- default: llvm_unreachable("Unsupported Text attribute in ASM Mode");
- case ARMBuildAttrs::CPU_name:
- Streamer.EmitRawText(StringRef("\t.cpu ") + String.lower());
- break;
- /* GAS requires .fpu to be emitted regardless of EABI attribute */
- case ARMBuildAttrs::Advanced_SIMD_arch:
- case ARMBuildAttrs::VFP_arch:
- Streamer.EmitRawText(StringRef("\t.fpu ") + String.lower());
- break;
- }
- }
- void Finish() { }
- };
-
- class ObjectAttributeEmitter : public AttributeEmitter {
- // This structure holds all attributes, accounting for
- // their string/numeric value, so we can later emmit them
- // in declaration order, keeping all in the same vector
- struct AttributeItemType {
- enum {
- HiddenAttribute = 0,
- NumericAttribute,
- TextAttribute
- } Type;
- unsigned Tag;
- unsigned IntValue;
- StringRef StringValue;
- } AttributeItem;
-
- MCObjectStreamer &Streamer;
- StringRef CurrentVendor;
- SmallVector<AttributeItemType, 64> Contents;
-
- // Account for the ULEB/String size of each item,
- // not just the number of items
- size_t ContentsSize;
- // FIXME: this should be in a more generic place, but
- // getULEBSize() is in MCAsmInfo and will be moved to MCDwarf
- size_t getULEBSize(int Value) {
- size_t Size = 0;
- do {
- Value >>= 7;
- Size += sizeof(int8_t); // Is this really necessary?
- } while (Value);
- return Size;
- }
-
- public:
- ObjectAttributeEmitter(MCObjectStreamer &Streamer_) :
- Streamer(Streamer_), CurrentVendor(""), ContentsSize(0) { }
-
- void MaybeSwitchVendor(StringRef Vendor) {
- assert(!Vendor.empty() && "Vendor cannot be empty.");
-
- if (CurrentVendor.empty())
- CurrentVendor = Vendor;
- else if (CurrentVendor == Vendor)
- return;
- else
- Finish();
-
- CurrentVendor = Vendor;
-
- assert(Contents.size() == 0);
- }
-
- void EmitAttribute(unsigned Attribute, unsigned Value) {
- AttributeItemType attr = {
- AttributeItemType::NumericAttribute,
- Attribute,
- Value,
- StringRef("")
- };
- ContentsSize += getULEBSize(Attribute);
- ContentsSize += getULEBSize(Value);
- Contents.push_back(attr);
- }
-
- void EmitTextAttribute(unsigned Attribute, StringRef String) {
- AttributeItemType attr = {
- AttributeItemType::TextAttribute,
- Attribute,
- 0,
- String
- };
- ContentsSize += getULEBSize(Attribute);
- // String + \0
- ContentsSize += String.size()+1;
-
- Contents.push_back(attr);
- }
-
- void Finish() {
- // Vendor size + Vendor name + '\0'
- const size_t VendorHeaderSize = 4 + CurrentVendor.size() + 1;
-
- // Tag + Tag Size
- const size_t TagHeaderSize = 1 + 4;
-
- Streamer.EmitIntValue(VendorHeaderSize + TagHeaderSize + ContentsSize, 4);
- Streamer.EmitBytes(CurrentVendor);
- Streamer.EmitIntValue(0, 1); // '\0'
-
- Streamer.EmitIntValue(ARMBuildAttrs::File, 1);
- Streamer.EmitIntValue(TagHeaderSize + ContentsSize, 4);
-
- // Size should have been accounted for already, now
- // emit each field as its type (ULEB or String)
- for (unsigned int i=0; i<Contents.size(); ++i) {
- AttributeItemType item = Contents[i];
- Streamer.EmitULEB128IntValue(item.Tag);
- switch (item.Type) {
- default: llvm_unreachable("Invalid attribute type");
- case AttributeItemType::NumericAttribute:
- Streamer.EmitULEB128IntValue(item.IntValue);
- break;
- case AttributeItemType::TextAttribute:
- Streamer.EmitBytes(item.StringValue.upper());
- Streamer.EmitIntValue(0, 1); // '\0'
- break;
- }
- }
-
- Contents.clear();
- }
- };
-
-} // end of anonymous namespace
-
/// EmitDwarfRegOp - Emit dwarf register operation.
void ARMAsmPrinter::EmitDwarfRegOp(const MachineLocation &MLoc,
bool Indirect) const {
const GlobalValue *GV = dyn_cast<GlobalValue>(CV->stripPointerCasts());
assert(GV && "C++ constructor pointer was not a GlobalValue!");
- const MCExpr *E = MCSymbolRefExpr::Create(Mang->getSymbol(GV),
- (Subtarget->isTargetDarwin()
- ? MCSymbolRefExpr::VK_None
- : MCSymbolRefExpr::VK_ARM_TARGET1),
+ const MCExpr *E = MCSymbolRefExpr::Create(getSymbol(GV),
+ (Subtarget->isTargetELF()
+ ? MCSymbolRefExpr::VK_ARM_TARGET1
+ : MCSymbolRefExpr::VK_None),
OutContext);
OutStreamer.EmitValue(E, Size);
else if ((Modifier && strcmp(Modifier, "hi16") == 0) ||
(TF & ARMII::MO_HI16))
O << ":upper16:";
- O << *Mang->getSymbol(GV);
+ O << *getSymbol(GV);
printOffset(MO.getOffset(), O);
if (TF == ARMII::MO_PLT)
O << "(PLT)";
break;
}
- case MachineOperand::MO_ExternalSymbol: {
- O << *GetExternalSymbolSymbol(MO.getSymbolName());
- if (TF == ARMII::MO_PLT)
- O << "(PLT)";
- break;
- }
case MachineOperand::MO_ConstantPoolIndex:
O << *GetCPISymbol(MO.getIndex());
break;
- case MachineOperand::MO_JumpTableIndex:
- O << *GetJTISymbol(MO.getIndex());
- break;
}
}
MCSymbol *ARMAsmPrinter::
GetARMJTIPICJumpTableLabel2(unsigned uid, unsigned uid2) const {
+ const DataLayout *DL = TM.getDataLayout();
SmallString<60> Name;
- raw_svector_ostream(Name) << MAI->getPrivateGlobalPrefix() << "JTI"
+ raw_svector_ostream(Name) << DL->getPrivateGlobalPrefix() << "JTI"
<< getFunctionNumber() << '_' << uid << '_' << uid2;
return OutContext.GetOrCreateSymbol(Name.str());
}
MCSymbol *ARMAsmPrinter::GetARMSJLJEHLabel() const {
+ const DataLayout *DL = TM.getDataLayout();
SmallString<60> Name;
- raw_svector_ostream(Name) << MAI->getPrivateGlobalPrefix() << "SJLJEH"
+ raw_svector_ostream(Name) << DL->getPrivateGlobalPrefix() << "SJLJEH"
<< getFunctionNumber();
return OutContext.GetOrCreateSymbol(Name.str());
}
if (!FlagsOP.isImm())
return true;
unsigned Flags = FlagsOP.getImm();
+
+ // This operand may not be the one that actually provides the register. If
+ // it's tied to a previous one then we should refer instead to that one
+ // for registers and their classes.
+ unsigned TiedIdx;
+ if (InlineAsm::isUseOperandTiedToDef(Flags, TiedIdx)) {
+ for (OpNum = InlineAsm::MIOp_FirstOperand; TiedIdx; --TiedIdx) {
+ unsigned OpFlags = MI->getOperand(OpNum).getImm();
+ OpNum += InlineAsm::getNumOperandRegisters(OpFlags) + 1;
+ }
+ Flags = MI->getOperand(OpNum).getImm();
+
+ // Later code expects OpNum to be pointing at the register rather than
+ // the flags.
+ OpNum += 1;
+ }
+
unsigned NumVals = InlineAsm::getNumOperandRegisters(Flags);
unsigned RC;
InlineAsm::hasRegClassConstraint(Flags, RC);
}
void ARMAsmPrinter::EmitStartOfAsmFile(Module &M) {
- if (Subtarget->isTargetDarwin()) {
+ if (Subtarget->isTargetMachO()) {
Reloc::Model RelocM = TM.getRelocationModel();
if (RelocM == Reloc::PIC_ || RelocM == Reloc::DynamicNoPIC) {
// Declare all the text sections up front (before the DWARF sections
void ARMAsmPrinter::EmitEndOfAsmFile(Module &M) {
- if (Subtarget->isTargetDarwin()) {
+ if (Subtarget->isTargetMachO()) {
// All darwin targets use mach-o.
const TargetLoweringObjectFileMachO &TLOFMacho =
static_cast<const TargetLoweringObjectFileMachO &>(getObjFileLowering());
// generates code that does this, it is always safe to set.
OutStreamer.EmitAssemblerFlag(MCAF_SubsectionsViaSymbols);
}
- // FIXME: This should eventually end up somewhere else where more
- // intelligent flag decisions can be made. For now we are just maintaining
- // the status quo for ARM and setting EF_ARM_EABI_VER5 as the default.
- if (MCELFStreamer *MES = dyn_cast<MCELFStreamer>(&OutStreamer))
- MES->getAssembler().setELFHeaderEFlags(ELF::EF_ARM_EABI_VER5);
}
//===----------------------------------------------------------------------===//
// to appear in the .ARM.attributes section in ELF.
// Instead of subclassing the MCELFStreamer, we do the work here.
-void ARMAsmPrinter::emitAttributes() {
-
- emitARMAttributeSection();
+static ARMBuildAttrs::CPUArch getArchForCPU(StringRef CPU,
+ const ARMSubtarget *Subtarget) {
+ if (CPU == "xscale")
+ return ARMBuildAttrs::v5TEJ;
- /* GAS expect .fpu to be emitted, regardless of VFP build attribute */
- bool emitFPU = false;
- AttributeEmitter *AttrEmitter;
- if (OutStreamer.hasRawTextSupport()) {
- AttrEmitter = new AsmAttributeEmitter(OutStreamer);
- emitFPU = true;
- } else {
- MCObjectStreamer &O = static_cast<MCObjectStreamer&>(OutStreamer);
- AttrEmitter = new ObjectAttributeEmitter(O);
- }
-
- AttrEmitter->MaybeSwitchVendor("aeabi");
-
- std::string CPUString = Subtarget->getCPUString();
-
- if (CPUString == "cortex-a8" ||
- Subtarget->isCortexA8()) {
- AttrEmitter->EmitTextAttribute(ARMBuildAttrs::CPU_name, "cortex-a8");
- AttrEmitter->EmitAttribute(ARMBuildAttrs::CPU_arch, ARMBuildAttrs::v7);
- AttrEmitter->EmitAttribute(ARMBuildAttrs::CPU_arch_profile,
- ARMBuildAttrs::ApplicationProfile);
- AttrEmitter->EmitAttribute(ARMBuildAttrs::ARM_ISA_use,
- ARMBuildAttrs::Allowed);
- AttrEmitter->EmitAttribute(ARMBuildAttrs::THUMB_ISA_use,
- ARMBuildAttrs::AllowThumb32);
- // Fixme: figure out when this is emitted.
- //AttrEmitter->EmitAttribute(ARMBuildAttrs::WMMX_arch,
- // ARMBuildAttrs::AllowWMMXv1);
- //
-
- /// ADD additional Else-cases here!
- } else if (CPUString == "xscale") {
- AttrEmitter->EmitAttribute(ARMBuildAttrs::CPU_arch, ARMBuildAttrs::v5TEJ);
- AttrEmitter->EmitAttribute(ARMBuildAttrs::ARM_ISA_use,
- ARMBuildAttrs::Allowed);
- AttrEmitter->EmitAttribute(ARMBuildAttrs::THUMB_ISA_use,
- ARMBuildAttrs::Allowed);
- } else if (Subtarget->hasV8Ops())
- AttrEmitter->EmitAttribute(ARMBuildAttrs::CPU_arch, ARMBuildAttrs::v8);
+ if (Subtarget->hasV8Ops())
+ return ARMBuildAttrs::v8;
else if (Subtarget->hasV7Ops()) {
- AttrEmitter->EmitAttribute(ARMBuildAttrs::CPU_arch, ARMBuildAttrs::v7);
- AttrEmitter->EmitAttribute(ARMBuildAttrs::THUMB_ISA_use,
- ARMBuildAttrs::AllowThumb32);
+ if (Subtarget->isMClass() && Subtarget->hasThumb2DSP())
+ return ARMBuildAttrs::v7E_M;
+ return ARMBuildAttrs::v7;
} else if (Subtarget->hasV6T2Ops())
- AttrEmitter->EmitAttribute(ARMBuildAttrs::CPU_arch, ARMBuildAttrs::v6T2);
+ return ARMBuildAttrs::v6T2;
+ else if (Subtarget->hasV6MOps())
+ return ARMBuildAttrs::v6S_M;
else if (Subtarget->hasV6Ops())
- AttrEmitter->EmitAttribute(ARMBuildAttrs::CPU_arch, ARMBuildAttrs::v6);
+ return ARMBuildAttrs::v6;
else if (Subtarget->hasV5TEOps())
- AttrEmitter->EmitAttribute(ARMBuildAttrs::CPU_arch, ARMBuildAttrs::v5TE);
+ return ARMBuildAttrs::v5TE;
else if (Subtarget->hasV5TOps())
- AttrEmitter->EmitAttribute(ARMBuildAttrs::CPU_arch, ARMBuildAttrs::v5T);
+ return ARMBuildAttrs::v5T;
else if (Subtarget->hasV4TOps())
- AttrEmitter->EmitAttribute(ARMBuildAttrs::CPU_arch, ARMBuildAttrs::v4T);
+ return ARMBuildAttrs::v4T;
else
- AttrEmitter->EmitAttribute(ARMBuildAttrs::CPU_arch, ARMBuildAttrs::v4);
+ return ARMBuildAttrs::v4;
+}
- if (Subtarget->hasNEON() && emitFPU) {
- /* NEON is not exactly a VFP architecture, but GAS emit one of
- * neon/neon-vfpv4/vfpv3/vfpv2 for .fpu parameters */
- if (Subtarget->hasVFP4())
- AttrEmitter->EmitTextAttribute(ARMBuildAttrs::Advanced_SIMD_arch,
- "neon-vfpv4");
- else
- AttrEmitter->EmitTextAttribute(ARMBuildAttrs::Advanced_SIMD_arch, "neon");
- /* If emitted for NEON, omit from VFP below, since you can have both
- * NEON and VFP in build attributes but only one .fpu */
- emitFPU = false;
+void ARMAsmPrinter::emitAttributes() {
+ MCTargetStreamer &TS = *OutStreamer.getTargetStreamer();
+ ARMTargetStreamer &ATS = static_cast<ARMTargetStreamer &>(TS);
+
+ ATS.switchVendor("aeabi");
+
+ std::string CPUString = Subtarget->getCPUString();
+
+ // FIXME: remove krait check when GNU tools support krait cpu
+ if (CPUString != "generic" && CPUString != "krait")
+ ATS.emitTextAttribute(ARMBuildAttrs::CPU_name, CPUString);
+
+ ATS.emitAttribute(ARMBuildAttrs::CPU_arch,
+ getArchForCPU(CPUString, Subtarget));
+
+ // Tag_CPU_arch_profile must have the default value of 0 when "Architecture
+ // profile is not applicable (e.g. pre v7, or cross-profile code)".
+ if (Subtarget->hasV7Ops()) {
+ if (Subtarget->isAClass()) {
+ ATS.emitAttribute(ARMBuildAttrs::CPU_arch_profile,
+ ARMBuildAttrs::ApplicationProfile);
+ } else if (Subtarget->isRClass()) {
+ ATS.emitAttribute(ARMBuildAttrs::CPU_arch_profile,
+ ARMBuildAttrs::RealTimeProfile);
+ } else if (Subtarget->isMClass()) {
+ ATS.emitAttribute(ARMBuildAttrs::CPU_arch_profile,
+ ARMBuildAttrs::MicroControllerProfile);
+ }
}
- /* V8FP + .fpu */
- if (Subtarget->hasV8FP()) {
- AttrEmitter->EmitAttribute(ARMBuildAttrs::VFP_arch,
- ARMBuildAttrs::AllowV8FPA);
- if (emitFPU)
- AttrEmitter->EmitTextAttribute(ARMBuildAttrs::VFP_arch, "v8fp");
- /* VFPv4 + .fpu */
- } else if (Subtarget->hasVFP4()) {
- AttrEmitter->EmitAttribute(ARMBuildAttrs::VFP_arch,
- ARMBuildAttrs::AllowFPv4A);
- if (emitFPU)
- AttrEmitter->EmitTextAttribute(ARMBuildAttrs::VFP_arch, "vfpv4");
-
- /* VFPv3 + .fpu */
- } else if (Subtarget->hasVFP3()) {
- AttrEmitter->EmitAttribute(ARMBuildAttrs::VFP_arch,
- ARMBuildAttrs::AllowFPv3A);
- if (emitFPU)
- AttrEmitter->EmitTextAttribute(ARMBuildAttrs::VFP_arch, "vfpv3");
-
- /* VFPv2 + .fpu */
- } else if (Subtarget->hasVFP2()) {
- AttrEmitter->EmitAttribute(ARMBuildAttrs::VFP_arch,
- ARMBuildAttrs::AllowFPv2);
- if (emitFPU)
- AttrEmitter->EmitTextAttribute(ARMBuildAttrs::VFP_arch, "vfpv2");
+ ATS.emitAttribute(ARMBuildAttrs::ARM_ISA_use, Subtarget->hasARMOps() ?
+ ARMBuildAttrs::Allowed : ARMBuildAttrs::Not_Allowed);
+ if (Subtarget->isThumb1Only()) {
+ ATS.emitAttribute(ARMBuildAttrs::THUMB_ISA_use,
+ ARMBuildAttrs::Allowed);
+ } else if (Subtarget->hasThumb2()) {
+ ATS.emitAttribute(ARMBuildAttrs::THUMB_ISA_use,
+ ARMBuildAttrs::AllowThumb32);
}
- /* TODO: ARMBuildAttrs::Allowed is not completely accurate,
- * since NEON can have 1 (allowed) or 2 (MAC operations) */
if (Subtarget->hasNEON()) {
- if (Subtarget->hasV8Ops())
- AttrEmitter->EmitAttribute(ARMBuildAttrs::Advanced_SIMD_arch,
- ARMBuildAttrs::AllowedNeonV8);
+ /* NEON is not exactly a VFP architecture, but GAS emit one of
+ * neon/neon-fp-armv8/neon-vfpv4/vfpv3/vfpv2 for .fpu parameters */
+ if (Subtarget->hasFPARMv8()) {
+ if (Subtarget->hasCrypto())
+ ATS.emitFPU(ARM::CRYPTO_NEON_FP_ARMV8);
+ else
+ ATS.emitFPU(ARM::NEON_FP_ARMV8);
+ }
+ else if (Subtarget->hasVFP4())
+ ATS.emitFPU(ARM::NEON_VFPV4);
else
- AttrEmitter->EmitAttribute(ARMBuildAttrs::Advanced_SIMD_arch,
- ARMBuildAttrs::Allowed);
+ ATS.emitFPU(ARM::NEON);
+ // Emit Tag_Advanced_SIMD_arch for ARMv8 architecture
+ if (Subtarget->hasV8Ops())
+ ATS.emitAttribute(ARMBuildAttrs::Advanced_SIMD_arch,
+ ARMBuildAttrs::AllowNeonARMv8);
+ } else {
+ if (Subtarget->hasFPARMv8())
+ ATS.emitFPU(ARM::FP_ARMV8);
+ else if (Subtarget->hasVFP4())
+ ATS.emitFPU(Subtarget->hasD16() ? ARM::VFPV4_D16 : ARM::VFPV4);
+ else if (Subtarget->hasVFP3())
+ ATS.emitFPU(Subtarget->hasD16() ? ARM::VFPV3_D16 : ARM::VFPV3);
+ else if (Subtarget->hasVFP2())
+ ATS.emitFPU(ARM::VFPV2);
}
// Signal various FP modes.
if (!TM.Options.UnsafeFPMath) {
- AttrEmitter->EmitAttribute(ARMBuildAttrs::ABI_FP_denormal,
- ARMBuildAttrs::Allowed);
- AttrEmitter->EmitAttribute(ARMBuildAttrs::ABI_FP_exceptions,
- ARMBuildAttrs::Allowed);
+ ATS.emitAttribute(ARMBuildAttrs::ABI_FP_denormal, ARMBuildAttrs::Allowed);
+ ATS.emitAttribute(ARMBuildAttrs::ABI_FP_exceptions,
+ ARMBuildAttrs::Allowed);
}
if (TM.Options.NoInfsFPMath && TM.Options.NoNaNsFPMath)
- AttrEmitter->EmitAttribute(ARMBuildAttrs::ABI_FP_number_model,
- ARMBuildAttrs::Allowed);
+ ATS.emitAttribute(ARMBuildAttrs::ABI_FP_number_model,
+ ARMBuildAttrs::Allowed);
else
- AttrEmitter->EmitAttribute(ARMBuildAttrs::ABI_FP_number_model,
- ARMBuildAttrs::AllowIEE754);
+ ATS.emitAttribute(ARMBuildAttrs::ABI_FP_number_model,
+ ARMBuildAttrs::AllowIEE754);
- // FIXME: add more flags to ARMBuildAttrs.h
+ // FIXME: add more flags to ARMBuildAttributes.h
// 8-bytes alignment stuff.
- AttrEmitter->EmitAttribute(ARMBuildAttrs::ABI_align8_needed, 1);
- AttrEmitter->EmitAttribute(ARMBuildAttrs::ABI_align8_preserved, 1);
+ ATS.emitAttribute(ARMBuildAttrs::ABI_align_needed, 1);
+ ATS.emitAttribute(ARMBuildAttrs::ABI_align_preserved, 1);
+
+ // ABI_HardFP_use attribute to indicate single precision FP.
+ if (Subtarget->isFPOnlySP())
+ ATS.emitAttribute(ARMBuildAttrs::ABI_HardFP_use,
+ ARMBuildAttrs::HardFPSinglePrecision);
// Hard float. Use both S and D registers and conform to AAPCS-VFP.
- if (Subtarget->isAAPCS_ABI() && TM.Options.FloatABIType == FloatABI::Hard) {
- AttrEmitter->EmitAttribute(ARMBuildAttrs::ABI_HardFP_use, 3);
- AttrEmitter->EmitAttribute(ARMBuildAttrs::ABI_VFP_args, 1);
- }
- // FIXME: Should we signal R9 usage?
+ if (Subtarget->isAAPCS_ABI() && TM.Options.FloatABIType == FloatABI::Hard)
+ ATS.emitAttribute(ARMBuildAttrs::ABI_VFP_args, ARMBuildAttrs::HardFPAAPCS);
- if (Subtarget->hasDivide())
- AttrEmitter->EmitAttribute(ARMBuildAttrs::DIV_use, 1);
+ // FIXME: Should we signal R9 usage?
- AttrEmitter->Finish();
- delete AttrEmitter;
+ if (Subtarget->hasFP16())
+ ATS.emitAttribute(ARMBuildAttrs::FP_HP_extension, ARMBuildAttrs::AllowHPFP);
+
+ if (Subtarget->hasMPExtension())
+ ATS.emitAttribute(ARMBuildAttrs::MPextension_use, ARMBuildAttrs::AllowMP);
+
+ // Hardware divide in ARM mode is part of base arch, starting from ARMv8.
+ // If only Thumb hwdiv is present, it must also be in base arch (ARMv7-R/M).
+ // It is not possible to produce DisallowDIV: if hwdiv is present in the base
+ // arch, supplying -hwdiv downgrades the effective arch, via ClearImpliedBits.
+ // AllowDIVExt is only emitted if hwdiv isn't available in the base arch;
+ // otherwise, the default value (AllowDIVIfExists) applies.
+ if (Subtarget->hasDivideInARMMode() && !Subtarget->hasV8Ops())
+ ATS.emitAttribute(ARMBuildAttrs::DIV_use, ARMBuildAttrs::AllowDIVExt);
+
+ if (Subtarget->hasTrustZone() && Subtarget->hasVirtualization())
+ ATS.emitAttribute(ARMBuildAttrs::Virtualization_use,
+ ARMBuildAttrs::AllowTZVirtualization);
+ else if (Subtarget->hasTrustZone())
+ ATS.emitAttribute(ARMBuildAttrs::Virtualization_use,
+ ARMBuildAttrs::AllowTZ);
+ else if (Subtarget->hasVirtualization())
+ ATS.emitAttribute(ARMBuildAttrs::Virtualization_use,
+ ARMBuildAttrs::AllowVirtualization);
+
+ ATS.finishAttributeSection();
}
void ARMAsmPrinter::emitARMAttributeSection() {
getModifierVariantKind(ARMCP::ARMCPModifier Modifier) {
switch (Modifier) {
case ARMCP::no_modifier: return MCSymbolRefExpr::VK_None;
- case ARMCP::TLSGD: return MCSymbolRefExpr::VK_ARM_TLSGD;
- case ARMCP::TPOFF: return MCSymbolRefExpr::VK_ARM_TPOFF;
- case ARMCP::GOTTPOFF: return MCSymbolRefExpr::VK_ARM_GOTTPOFF;
- case ARMCP::GOT: return MCSymbolRefExpr::VK_ARM_GOT;
- case ARMCP::GOTOFF: return MCSymbolRefExpr::VK_ARM_GOTOFF;
+ case ARMCP::TLSGD: return MCSymbolRefExpr::VK_TLSGD;
+ case ARMCP::TPOFF: return MCSymbolRefExpr::VK_TPOFF;
+ case ARMCP::GOTTPOFF: return MCSymbolRefExpr::VK_GOTTPOFF;
+ case ARMCP::GOT: return MCSymbolRefExpr::VK_GOT;
+ case ARMCP::GOTOFF: return MCSymbolRefExpr::VK_GOTOFF;
}
llvm_unreachable("Invalid ARMCPModifier!");
}
-MCSymbol *ARMAsmPrinter::GetARMGVSymbol(const GlobalValue *GV) {
- bool isIndirect = Subtarget->isTargetDarwin() &&
+MCSymbol *ARMAsmPrinter::GetARMGVSymbol(const GlobalValue *GV,
+ unsigned char TargetFlags) {
+ bool isIndirect = Subtarget->isTargetMachO() &&
+ (TargetFlags & ARMII::MO_NONLAZY) &&
Subtarget->GVIsIndirectSymbol(GV, TM.getRelocationModel());
if (!isIndirect)
- return Mang->getSymbol(GV);
+ return getSymbol(GV);
// FIXME: Remove this when Darwin transition to @GOT like syntax.
- MCSymbol *MCSym = GetSymbolWithGlobalValueBase(GV, "$non_lazy_ptr");
+ MCSymbol *MCSym = getSymbolWithGlobalValueBase(GV, "$non_lazy_ptr");
MachineModuleInfoMachO &MMIMachO =
MMI->getObjFileInfo<MachineModuleInfoMachO>();
MachineModuleInfoImpl::StubValueTy &StubSym =
MMIMachO.getGVStubEntry(MCSym);
if (StubSym.getPointer() == 0)
StubSym = MachineModuleInfoImpl::
- StubValueTy(Mang->getSymbol(GV), !GV->hasInternalLinkage());
+ StubValueTy(getSymbol(GV), !GV->hasInternalLinkage());
return MCSym;
}
void ARMAsmPrinter::
EmitMachineConstantPoolValue(MachineConstantPoolValue *MCPV) {
+ const DataLayout *DL = TM.getDataLayout();
int Size = TM.getDataLayout()->getTypeAllocSize(MCPV->getType());
ARMConstantPoolValue *ACPV = static_cast<ARMConstantPoolValue*>(MCPV);
if (ACPV->isLSDA()) {
SmallString<128> Str;
raw_svector_ostream OS(Str);
- OS << MAI->getPrivateGlobalPrefix() << "_LSDA_" << getFunctionNumber();
+ OS << DL->getPrivateGlobalPrefix() << "_LSDA_" << getFunctionNumber();
MCSym = OutContext.GetOrCreateSymbol(OS.str());
} else if (ACPV->isBlockAddress()) {
const BlockAddress *BA =
MCSym = GetBlockAddressSymbol(BA);
} else if (ACPV->isGlobalValue()) {
const GlobalValue *GV = cast<ARMConstantPoolConstant>(ACPV)->getGV();
- MCSym = GetARMGVSymbol(GV);
+
+ // On Darwin, const-pool entries may get the "FOO$non_lazy_ptr" mangling, so
+ // flag the global as MO_NONLAZY.
+ unsigned char TF = Subtarget->isTargetMachO() ? ARMII::MO_NONLAZY : 0;
+ MCSym = GetARMGVSymbol(GV, TF);
} else if (ACPV->isMachineBasicBlock()) {
const MachineBasicBlock *MBB = cast<ARMConstantPoolMBB>(ACPV)->getMBB();
MCSym = MBB->getSymbol();
OutContext);
if (ACPV->getPCAdjustment()) {
- MCSymbol *PCLabel = getPICLabel(MAI->getPrivateGlobalPrefix(),
+ MCSymbol *PCLabel = getPICLabel(DL->getPrivateGlobalPrefix(),
getFunctionNumber(),
ACPV->getLabelId(),
OutContext);
assert(MI->getFlag(MachineInstr::FrameSetup) &&
"Only instruction which are involved into frame setup code are allowed");
+ MCTargetStreamer &TS = *OutStreamer.getTargetStreamer();
+ ARMTargetStreamer &ATS = static_cast<ARMTargetStreamer &>(TS);
const MachineFunction &MF = *MI->getParent()->getParent();
const TargetRegisterInfo *RegInfo = MF.getTarget().getRegisterInfo();
const ARMFunctionInfo &AFI = *MF.getInfo<ARMFunctionInfo>();
RegList.push_back(SrcReg);
break;
}
- OutStreamer.EmitRegSave(RegList, Opc == ARM::VSTMDDB_UPD);
+ ATS.emitRegSave(RegList, Opc == ARM::VSTMDDB_UPD);
} else {
// Changes of stack / frame pointer.
if (SrcReg == ARM::SP) {
if (DstReg == FramePtr && FramePtr != ARM::SP)
// Set-up of the frame pointer. Positive values correspond to "add"
// instruction.
- OutStreamer.EmitSetFP(FramePtr, ARM::SP, -Offset);
+ ATS.emitSetFP(FramePtr, ARM::SP, -Offset);
else if (DstReg == ARM::SP) {
// Change of SP by an offset. Positive values correspond to "sub"
// instruction.
- OutStreamer.EmitPad(Offset);
+ ATS.emitPad(Offset);
} else {
MI->dump();
llvm_unreachable("Unsupported opcode for unwinding information");
#include "ARMGenMCPseudoLowering.inc"
void ARMAsmPrinter::EmitInstruction(const MachineInstr *MI) {
+ const DataLayout *DL = TM.getDataLayout();
+
// If we just ended a constant pool, mark it as such.
if (InConstantPool && MI->getOpcode() != ARM::CONSTPOOL_ENTRY) {
OutStreamer.EmitDataRegion(MCDR_DataRegionEnd);
.addReg(0));
const GlobalValue *GV = MI->getOperand(0).getGlobal();
- MCSymbol *GVSym = Mang->getSymbol(GV);
+ MCSymbol *GVSym = getSymbol(GV);
const MCExpr *GVSymExpr = MCSymbolRefExpr::Create(GVSym, OutContext);
OutStreamer.EmitInstruction(MCInstBuilder(ARM::Bcc)
.addExpr(GVSymExpr)
TmpInst.addOperand(MCOperand::CreateReg(MI->getOperand(0).getReg()));
unsigned TF = MI->getOperand(1).getTargetFlags();
- bool isPIC = TF == ARMII::MO_LO16_NONLAZY_PIC;
const GlobalValue *GV = MI->getOperand(1).getGlobal();
- MCSymbol *GVSym = GetARMGVSymbol(GV);
+ MCSymbol *GVSym = GetARMGVSymbol(GV, TF);
const MCExpr *GVSymExpr = MCSymbolRefExpr::Create(GVSym, OutContext);
- if (isPIC) {
- MCSymbol *LabelSym = getPICLabel(MAI->getPrivateGlobalPrefix(),
- getFunctionNumber(),
- MI->getOperand(2).getImm(), OutContext);
- const MCExpr *LabelSymExpr= MCSymbolRefExpr::Create(LabelSym, OutContext);
- unsigned PCAdj = (Opc == ARM::MOVi16_ga_pcrel) ? 8 : 4;
- const MCExpr *PCRelExpr =
- ARMMCExpr::CreateLower16(MCBinaryExpr::CreateSub(GVSymExpr,
- MCBinaryExpr::CreateAdd(LabelSymExpr,
+
+ MCSymbol *LabelSym = getPICLabel(DL->getPrivateGlobalPrefix(),
+ getFunctionNumber(),
+ MI->getOperand(2).getImm(), OutContext);
+ const MCExpr *LabelSymExpr= MCSymbolRefExpr::Create(LabelSym, OutContext);
+ unsigned PCAdj = (Opc == ARM::MOVi16_ga_pcrel) ? 8 : 4;
+ const MCExpr *PCRelExpr =
+ ARMMCExpr::CreateLower16(MCBinaryExpr::CreateSub(GVSymExpr,
+ MCBinaryExpr::CreateAdd(LabelSymExpr,
MCConstantExpr::Create(PCAdj, OutContext),
- OutContext), OutContext), OutContext);
+ OutContext), OutContext), OutContext);
TmpInst.addOperand(MCOperand::CreateExpr(PCRelExpr));
- } else {
- const MCExpr *RefExpr= ARMMCExpr::CreateLower16(GVSymExpr, OutContext);
- TmpInst.addOperand(MCOperand::CreateExpr(RefExpr));
- }
// Add predicate operands.
TmpInst.addOperand(MCOperand::CreateImm(ARMCC::AL));
TmpInst.addOperand(MCOperand::CreateReg(MI->getOperand(1).getReg()));
unsigned TF = MI->getOperand(2).getTargetFlags();
- bool isPIC = TF == ARMII::MO_HI16_NONLAZY_PIC;
const GlobalValue *GV = MI->getOperand(2).getGlobal();
- MCSymbol *GVSym = GetARMGVSymbol(GV);
+ MCSymbol *GVSym = GetARMGVSymbol(GV, TF);
const MCExpr *GVSymExpr = MCSymbolRefExpr::Create(GVSym, OutContext);
- if (isPIC) {
- MCSymbol *LabelSym = getPICLabel(MAI->getPrivateGlobalPrefix(),
- getFunctionNumber(),
- MI->getOperand(3).getImm(), OutContext);
- const MCExpr *LabelSymExpr= MCSymbolRefExpr::Create(LabelSym, OutContext);
- unsigned PCAdj = (Opc == ARM::MOVTi16_ga_pcrel) ? 8 : 4;
- const MCExpr *PCRelExpr =
+
+ MCSymbol *LabelSym = getPICLabel(DL->getPrivateGlobalPrefix(),
+ getFunctionNumber(),
+ MI->getOperand(3).getImm(), OutContext);
+ const MCExpr *LabelSymExpr= MCSymbolRefExpr::Create(LabelSym, OutContext);
+ unsigned PCAdj = (Opc == ARM::MOVTi16_ga_pcrel) ? 8 : 4;
+ const MCExpr *PCRelExpr =
ARMMCExpr::CreateUpper16(MCBinaryExpr::CreateSub(GVSymExpr,
MCBinaryExpr::CreateAdd(LabelSymExpr,
MCConstantExpr::Create(PCAdj, OutContext),
OutContext), OutContext), OutContext);
TmpInst.addOperand(MCOperand::CreateExpr(PCRelExpr));
- } else {
- const MCExpr *RefExpr= ARMMCExpr::CreateUpper16(GVSymExpr, OutContext);
- TmpInst.addOperand(MCOperand::CreateExpr(RefExpr));
- }
// Add predicate operands.
TmpInst.addOperand(MCOperand::CreateImm(ARMCC::AL));
TmpInst.addOperand(MCOperand::CreateReg(0));
// This adds the address of LPC0 to r0.
// Emit the label.
- OutStreamer.EmitLabel(getPICLabel(MAI->getPrivateGlobalPrefix(),
+ OutStreamer.EmitLabel(getPICLabel(DL->getPrivateGlobalPrefix(),
getFunctionNumber(), MI->getOperand(2).getImm(),
OutContext));
// This adds the address of LPC0 to r0.
// Emit the label.
- OutStreamer.EmitLabel(getPICLabel(MAI->getPrivateGlobalPrefix(),
+ OutStreamer.EmitLabel(getPICLabel(DL->getPrivateGlobalPrefix(),
getFunctionNumber(), MI->getOperand(2).getImm(),
OutContext));
// a PC-relative address at the ldr instruction.
// Emit the label.
- OutStreamer.EmitLabel(getPICLabel(MAI->getPrivateGlobalPrefix(),
+ OutStreamer.EmitLabel(getPICLabel(DL->getPrivateGlobalPrefix(),
getFunctionNumber(), MI->getOperand(2).getImm(),
OutContext));
case ARM::TRAP: {
// Non-Darwin binutils don't yet support the "trap" mnemonic.
// FIXME: Remove this special case when they do.
- if (!Subtarget->isTargetDarwin()) {
+ if (!Subtarget->isTargetMachO()) {
//.long 0xe7ffdefe @ trap
uint32_t Val = 0xe7ffdefeUL;
OutStreamer.AddComment("trap");
case ARM::tTRAP: {
// Non-Darwin binutils don't yet support the "trap" mnemonic.
// FIXME: Remove this special case when they do.
- if (!Subtarget->isTargetDarwin()) {
+ if (!Subtarget->isTargetMachO()) {
//.short 57086 @ trap
uint16_t Val = 0xdefe;
OutStreamer.AddComment("trap");