]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/blobdiff - lib/Target/ARM/ARMAsmPrinter.cpp
Debug info: Remove ARMAsmPrinter::EmitDwarfRegOp(). AsmPrinter can now
[opencl/llvm.git] / lib / Target / ARM / ARMAsmPrinter.cpp
index 37cb64638dd245eda376b4393652ff0578ecc13f..b1b1aad2f8c4a4b712b31ebb16e3447524b831d6 100644 (file)
@@ -15,8 +15,8 @@
 #define DEBUG_TYPE "asm-printer"
 #include "ARMAsmPrinter.h"
 #include "ARM.h"
-#include "ARMBuildAttrs.h"
 #include "ARMConstantPoolValue.h"
+#include "ARMFPUName.h"
 #include "ARMMachineFunctionInfo.h"
 #include "ARMTargetMachine.h"
 #include "ARMTargetObjectFile.h"
 #include "MCTargetDesc/ARMMCExpr.h"
 #include "llvm/ADT/SetVector.h"
 #include "llvm/ADT/SmallString.h"
-#include "llvm/Constants.h"
-#include "llvm/DebugInfo.h"
-#include "llvm/Module.h"
-#include "llvm/Type.h"
-#include "llvm/Assembly/Writer.h"
-#include "llvm/CodeGen/MachineModuleInfoImpls.h"
 #include "llvm/CodeGen/MachineFunctionPass.h"
 #include "llvm/CodeGen/MachineJumpTableInfo.h"
+#include "llvm/CodeGen/MachineModuleInfoImpls.h"
+#include "llvm/DebugInfo.h"
+#include "llvm/IR/Constants.h"
+#include "llvm/IR/DataLayout.h"
+#include "llvm/IR/Mangler.h"
+#include "llvm/IR/Module.h"
+#include "llvm/IR/Type.h"
 #include "llvm/MC/MCAsmInfo.h"
 #include "llvm/MC/MCAssembler.h"
 #include "llvm/MC/MCContext.h"
+#include "llvm/MC/MCELFStreamer.h"
 #include "llvm/MC/MCInst.h"
-#include "llvm/MC/MCSectionMachO.h"
+#include "llvm/MC/MCInstBuilder.h"
 #include "llvm/MC/MCObjectStreamer.h"
+#include "llvm/MC/MCSectionMachO.h"
 #include "llvm/MC/MCStreamer.h"
 #include "llvm/MC/MCSymbol.h"
-#include "llvm/Target/Mangler.h"
-#include "llvm/DataLayout.h"
-#include "llvm/Target/TargetMachine.h"
+#include "llvm/Support/ARMBuildAttributes.h"
 #include "llvm/Support/CommandLine.h"
 #include "llvm/Support/Debug.h"
+#include "llvm/Support/ELF.h"
 #include "llvm/Support/ErrorHandling.h"
 #include "llvm/Support/TargetRegistry.h"
 #include "llvm/Support/raw_ostream.h"
+#include "llvm/Target/TargetMachine.h"
 #include <cctype>
 using namespace llvm;
 
-namespace {
-
-  // Per section and per symbol attributes are not supported.
-  // To implement them we would need the ability to delay this emission
-  // until the assembly file is fully parsed/generated as only then do we
-  // know the symbol and section numbers.
-  class AttributeEmitter {
-  public:
-    virtual void MaybeSwitchVendor(StringRef Vendor) = 0;
-    virtual void EmitAttribute(unsigned Attribute, unsigned Value) = 0;
-    virtual void EmitTextAttribute(unsigned Attribute, StringRef String) = 0;
-    virtual void Finish() = 0;
-    virtual ~AttributeEmitter() {}
-  };
-
-  class AsmAttributeEmitter : public AttributeEmitter {
-    MCStreamer &Streamer;
-
-  public:
-    AsmAttributeEmitter(MCStreamer &Streamer_) : Streamer(Streamer_) {}
-    void MaybeSwitchVendor(StringRef Vendor) { }
-
-    void EmitAttribute(unsigned Attribute, unsigned Value) {
-      Streamer.EmitRawText("\t.eabi_attribute " +
-                           Twine(Attribute) + ", " + Twine(Value));
-    }
-
-    void EmitTextAttribute(unsigned Attribute, StringRef String) {
-      switch (Attribute) {
-      default: llvm_unreachable("Unsupported Text attribute in ASM Mode");
-      case ARMBuildAttrs::CPU_name:
-        Streamer.EmitRawText(StringRef("\t.cpu ") + String.lower());
-        break;
-      /* GAS requires .fpu to be emitted regardless of EABI attribute */
-      case ARMBuildAttrs::Advanced_SIMD_arch:
-      case ARMBuildAttrs::VFP_arch:
-        Streamer.EmitRawText(StringRef("\t.fpu ") + String.lower());
-        break;
-      }
-    }
-    void Finish() { }
-  };
-
-  class ObjectAttributeEmitter : public AttributeEmitter {
-    // This structure holds all attributes, accounting for
-    // their string/numeric value, so we can later emmit them
-    // in declaration order, keeping all in the same vector
-    struct AttributeItemType {
-      enum {
-        HiddenAttribute = 0,
-        NumericAttribute,
-        TextAttribute
-      } Type;
-      unsigned Tag;
-      unsigned IntValue;
-      StringRef StringValue;
-    } AttributeItem;
-
-    MCObjectStreamer &Streamer;
-    StringRef CurrentVendor;
-    SmallVector<AttributeItemType, 64> Contents;
-
-    // Account for the ULEB/String size of each item,
-    // not just the number of items
-    size_t ContentsSize;
-    // FIXME: this should be in a more generic place, but
-    // getULEBSize() is in MCAsmInfo and will be moved to MCDwarf
-    size_t getULEBSize(int Value) {
-      size_t Size = 0;
-      do {
-        Value >>= 7;
-        Size += sizeof(int8_t); // Is this really necessary?
-      } while (Value);
-      return Size;
-    }
-
-  public:
-    ObjectAttributeEmitter(MCObjectStreamer &Streamer_) :
-      Streamer(Streamer_), CurrentVendor(""), ContentsSize(0) { }
-
-    void MaybeSwitchVendor(StringRef Vendor) {
-      assert(!Vendor.empty() && "Vendor cannot be empty.");
-
-      if (CurrentVendor.empty())
-        CurrentVendor = Vendor;
-      else if (CurrentVendor == Vendor)
-        return;
-      else
-        Finish();
-
-      CurrentVendor = Vendor;
-
-      assert(Contents.size() == 0);
-    }
-
-    void EmitAttribute(unsigned Attribute, unsigned Value) {
-      AttributeItemType attr = {
-        AttributeItemType::NumericAttribute,
-        Attribute,
-        Value,
-        StringRef("")
-      };
-      ContentsSize += getULEBSize(Attribute);
-      ContentsSize += getULEBSize(Value);
-      Contents.push_back(attr);
-    }
-
-    void EmitTextAttribute(unsigned Attribute, StringRef String) {
-      AttributeItemType attr = {
-        AttributeItemType::TextAttribute,
-        Attribute,
-        0,
-        String
-      };
-      ContentsSize += getULEBSize(Attribute);
-      // String + \0
-      ContentsSize += String.size()+1;
-
-      Contents.push_back(attr);
-    }
-
-    void Finish() {
-      // Vendor size + Vendor name + '\0'
-      const size_t VendorHeaderSize = 4 + CurrentVendor.size() + 1;
-
-      // Tag + Tag Size
-      const size_t TagHeaderSize = 1 + 4;
-
-      Streamer.EmitIntValue(VendorHeaderSize + TagHeaderSize + ContentsSize, 4);
-      Streamer.EmitBytes(CurrentVendor, 0);
-      Streamer.EmitIntValue(0, 1); // '\0'
-
-      Streamer.EmitIntValue(ARMBuildAttrs::File, 1);
-      Streamer.EmitIntValue(TagHeaderSize + ContentsSize, 4);
-
-      // Size should have been accounted for already, now
-      // emit each field as its type (ULEB or String)
-      for (unsigned int i=0; i<Contents.size(); ++i) {
-        AttributeItemType item = Contents[i];
-        Streamer.EmitULEB128IntValue(item.Tag, 0);
-        switch (item.Type) {
-        default: llvm_unreachable("Invalid attribute type");
-        case AttributeItemType::NumericAttribute:
-          Streamer.EmitULEB128IntValue(item.IntValue, 0);
-          break;
-        case AttributeItemType::TextAttribute:
-          Streamer.EmitBytes(item.StringValue.upper(), 0);
-          Streamer.EmitIntValue(0, 1); // '\0'
-          break;
-        }
-      }
-
-      Contents.clear();
-    }
-  };
-
-} // end of anonymous namespace
-
-MachineLocation ARMAsmPrinter::
-getDebugValueLocation(const MachineInstr *MI) const {
-  MachineLocation Location;
-  assert(MI->getNumOperands() == 4 && "Invalid no. of machine operands!");
-  // Frame address.  Currently handles register +- offset only.
-  if (MI->getOperand(0).isReg() && MI->getOperand(1).isImm())
-    Location.set(MI->getOperand(0).getReg(), MI->getOperand(1).getImm());
-  else {
-    DEBUG(dbgs() << "DBG_VALUE instruction ignored! " << *MI << "\n");
-  }
-  return Location;
-}
-
-/// EmitDwarfRegOp - Emit dwarf register operation.
-void ARMAsmPrinter::EmitDwarfRegOp(const MachineLocation &MLoc) const {
-  const TargetRegisterInfo *RI = TM.getRegisterInfo();
-  if (RI->getDwarfRegNum(MLoc.getReg(), false) != -1)
-    AsmPrinter::EmitDwarfRegOp(MLoc);
-  else {
-    unsigned Reg = MLoc.getReg();
-    if (Reg >= ARM::S0 && Reg <= ARM::S31) {
-      assert(ARM::S0 + 31 == ARM::S31 && "Unexpected ARM S register numbering");
-      // S registers are described as bit-pieces of a register
-      // S[2x] = DW_OP_regx(256 + (x>>1)) DW_OP_bit_piece(32, 0)
-      // S[2x+1] = DW_OP_regx(256 + (x>>1)) DW_OP_bit_piece(32, 32)
-
-      unsigned SReg = Reg - ARM::S0;
-      bool odd = SReg & 0x1;
-      unsigned Rx = 256 + (SReg >> 1);
-
-      OutStreamer.AddComment("DW_OP_regx for S register");
-      EmitInt8(dwarf::DW_OP_regx);
-
-      OutStreamer.AddComment(Twine(SReg));
-      EmitULEB128(Rx);
-
-      if (odd) {
-        OutStreamer.AddComment("DW_OP_bit_piece 32 32");
-        EmitInt8(dwarf::DW_OP_bit_piece);
-        EmitULEB128(32);
-        EmitULEB128(32);
-      } else {
-        OutStreamer.AddComment("DW_OP_bit_piece 32 0");
-        EmitInt8(dwarf::DW_OP_bit_piece);
-        EmitULEB128(32);
-        EmitULEB128(0);
-      }
-    } else if (Reg >= ARM::Q0 && Reg <= ARM::Q15) {
-      assert(ARM::Q0 + 15 == ARM::Q15 && "Unexpected ARM Q register numbering");
-      // Q registers Q0-Q15 are described by composing two D registers together.
-      // Qx = DW_OP_regx(256+2x) DW_OP_piece(8) DW_OP_regx(256+2x+1)
-      // DW_OP_piece(8)
-
-      unsigned QReg = Reg - ARM::Q0;
-      unsigned D1 = 256 + 2 * QReg;
-      unsigned D2 = D1 + 1;
-
-      OutStreamer.AddComment("DW_OP_regx for Q register: D1");
-      EmitInt8(dwarf::DW_OP_regx);
-      EmitULEB128(D1);
-      OutStreamer.AddComment("DW_OP_piece 8");
-      EmitInt8(dwarf::DW_OP_piece);
-      EmitULEB128(8);
-
-      OutStreamer.AddComment("DW_OP_regx for Q register: D2");
-      EmitInt8(dwarf::DW_OP_regx);
-      EmitULEB128(D2);
-      OutStreamer.AddComment("DW_OP_piece 8");
-      EmitInt8(dwarf::DW_OP_piece);
-      EmitULEB128(8);
-    }
-  }
-}
-
 void ARMAsmPrinter::EmitFunctionBodyEnd() {
   // Make sure to terminate any constant pools that were at the end
   // of the function.
@@ -309,10 +80,10 @@ void ARMAsmPrinter::EmitXXStructor(const Constant *CV) {
   const GlobalValue *GV = dyn_cast<GlobalValue>(CV->stripPointerCasts());
   assert(GV && "C++ constructor pointer was not a GlobalValue!");
 
-  const MCExpr *E = MCSymbolRefExpr::Create(Mang->getSymbol(GV),
-                                            (Subtarget->isTargetDarwin()
-                                             ? MCSymbolRefExpr::VK_None
-                                             : MCSymbolRefExpr::VK_ARM_TARGET1),
+  const MCExpr *E = MCSymbolRefExpr::Create(getSymbol(GV),
+                                            (Subtarget->isTargetELF()
+                                             ? MCSymbolRefExpr::VK_ARM_TARGET1
+                                             : MCSymbolRefExpr::VK_None),
                                             OutContext);
   
   OutStreamer.EmitValue(E, Size);
@@ -339,6 +110,11 @@ void ARMAsmPrinter::printOperand(const MachineInstr *MI, int OpNum,
     unsigned Reg = MO.getReg();
     assert(TargetRegisterInfo::isPhysicalRegister(Reg));
     assert(!MO.getSubReg() && "Subregs should be eliminated!");
+    if(ARM::GPRPairRegClass.contains(Reg)) {
+      const MachineFunction &MF = *MI->getParent()->getParent();
+      const TargetRegisterInfo *TRI = MF.getTarget().getRegisterInfo();
+      Reg = TRI->getSubReg(Reg, ARM::gsub_0);
+    }
     O << ARMInstPrinter::getRegisterName(Reg);
     break;
   }
@@ -365,25 +141,16 @@ void ARMAsmPrinter::printOperand(const MachineInstr *MI, int OpNum,
     else if ((Modifier && strcmp(Modifier, "hi16") == 0) ||
              (TF & ARMII::MO_HI16))
       O << ":upper16:";
-    O << *Mang->getSymbol(GV);
+    O << *getSymbol(GV);
 
     printOffset(MO.getOffset(), O);
     if (TF == ARMII::MO_PLT)
       O << "(PLT)";
     break;
   }
-  case MachineOperand::MO_ExternalSymbol: {
-    O << *GetExternalSymbolSymbol(MO.getSymbolName());
-    if (TF == ARMII::MO_PLT)
-      O << "(PLT)";
-    break;
-  }
   case MachineOperand::MO_ConstantPoolIndex:
     O << *GetCPISymbol(MO.getIndex());
     break;
-  case MachineOperand::MO_JumpTableIndex:
-    O << *GetJTISymbol(MO.getIndex());
-    break;
   }
 }
 
@@ -391,16 +158,18 @@ void ARMAsmPrinter::printOperand(const MachineInstr *MI, int OpNum,
 
 MCSymbol *ARMAsmPrinter::
 GetARMJTIPICJumpTableLabel2(unsigned uid, unsigned uid2) const {
+  const DataLayout *DL = TM.getDataLayout();
   SmallString<60> Name;
-  raw_svector_ostream(Name) << MAI->getPrivateGlobalPrefix() << "JTI"
+  raw_svector_ostream(Name) << DL->getPrivateGlobalPrefix() << "JTI"
     << getFunctionNumber() << '_' << uid << '_' << uid2;
   return OutContext.GetOrCreateSymbol(Name.str());
 }
 
 
 MCSymbol *ARMAsmPrinter::GetARMSJLJEHLabel() const {
+  const DataLayout *DL = TM.getDataLayout();
   SmallString<60> Name;
-  raw_svector_ostream(Name) << MAI->getPrivateGlobalPrefix() << "SJLJEH"
+  raw_svector_ostream(Name) << DL->getPrivateGlobalPrefix() << "SJLJEH"
     << getFunctionNumber();
   return OutContext.GetOrCreateSymbol(Name.str());
 }
@@ -466,8 +235,14 @@ bool ARMAsmPrinter::PrintAsmOperand(const MachineInstr *MI, unsigned OpNum,
       // This takes advantage of the 2 operand-ness of ldm/stm and that we've
       // already got the operands in registers that are operands to the
       // inline asm statement.
-
-      O << "{" << ARMInstPrinter::getRegisterName(RegBegin);
+      O << "{";
+      if (ARM::GPRPairRegClass.contains(RegBegin)) {
+        const TargetRegisterInfo *TRI = MF->getTarget().getRegisterInfo();
+        unsigned Reg0 = TRI->getSubReg(RegBegin, ARM::gsub_0);
+        O << ARMInstPrinter::getRegisterName(Reg0) << ", ";;
+        RegBegin = TRI->getSubReg(RegBegin, ARM::gsub_1);
+      }
+      O << ARMInstPrinter::getRegisterName(RegBegin);
 
       // FIXME: The register allocator not only may not have given us the
       // registers in sequence, but may not be in ascending registers. This
@@ -492,7 +267,38 @@ bool ARMAsmPrinter::PrintAsmOperand(const MachineInstr *MI, unsigned OpNum,
       if (!FlagsOP.isImm())
         return true;
       unsigned Flags = FlagsOP.getImm();
+
+      // This operand may not be the one that actually provides the register. If
+      // it's tied to a previous one then we should refer instead to that one
+      // for registers and their classes.
+      unsigned TiedIdx;
+      if (InlineAsm::isUseOperandTiedToDef(Flags, TiedIdx)) {
+        for (OpNum = InlineAsm::MIOp_FirstOperand; TiedIdx; --TiedIdx) {
+          unsigned OpFlags = MI->getOperand(OpNum).getImm();
+          OpNum += InlineAsm::getNumOperandRegisters(OpFlags) + 1;
+        }
+        Flags = MI->getOperand(OpNum).getImm();
+
+        // Later code expects OpNum to be pointing at the register rather than
+        // the flags.
+        OpNum += 1;
+      }
+
       unsigned NumVals = InlineAsm::getNumOperandRegisters(Flags);
+      unsigned RC;
+      InlineAsm::hasRegClassConstraint(Flags, RC);
+      if (RC == ARM::GPRPairRegClassID) {
+        if (NumVals != 1)
+          return true;
+        const MachineOperand &MO = MI->getOperand(OpNum);
+        if (!MO.isReg())
+          return true;
+        const TargetRegisterInfo *TRI = MF->getTarget().getRegisterInfo();
+        unsigned Reg = TRI->getSubReg(MO.getReg(), ExtraCode[0] == 'Q' ?
+            ARM::gsub_0 : ARM::gsub_1);
+        O << ARMInstPrinter::getRegisterName(Reg);
+        return false;
+      }
       if (NumVals != 2)
         return true;
       unsigned RegOp = ExtraCode[0] == 'Q' ? OpNum : OpNum + 1;
@@ -527,14 +333,12 @@ bool ARMAsmPrinter::PrintAsmOperand(const MachineInstr *MI, unsigned OpNum,
       const MachineOperand &MO = MI->getOperand(OpNum);
       if (!MO.isReg())
         return true;
-      const TargetRegisterClass &RC = ARM::GPRRegClass;
       const MachineFunction &MF = *MI->getParent()->getParent();
       const TargetRegisterInfo *TRI = MF.getTarget().getRegisterInfo();
-
-      unsigned RegIdx = TRI->getEncodingValue(MO.getReg());
-      RegIdx |= 1; //The odd register is also the higher-numbered one of a pair.
-
-      unsigned Reg = RC.getRegister(RegIdx);
+      unsigned Reg = MO.getReg();
+      if(!ARM::GPRPairRegClass.contains(Reg))
+        return false;
+      Reg = TRI->getSubReg(Reg, ARM::gsub_1);
       O << ARMInstPrinter::getRegisterName(Reg);
       return false;
     }
@@ -570,8 +374,22 @@ bool ARMAsmPrinter::PrintAsmMemoryOperand(const MachineInstr *MI,
   return false;
 }
 
+static bool isThumb(const MCSubtargetInfo& STI) {
+  return (STI.getFeatureBits() & ARM::ModeThumb) != 0;
+}
+
+void ARMAsmPrinter::emitInlineAsmEnd(const MCSubtargetInfo &StartInfo,
+                                     const MCSubtargetInfo *EndInfo) const {
+  // If either end mode is unknown (EndInfo == NULL) or different than
+  // the start mode, then restore the start mode.
+  const bool WasThumb = isThumb(StartInfo);
+  if (EndInfo == NULL || WasThumb != isThumb(*EndInfo)) {
+    OutStreamer.EmitAssemblerFlag(WasThumb ? MCAF_Code16 : MCAF_Code32);
+  }
+}
+
 void ARMAsmPrinter::EmitStartOfAsmFile(Module &M) {
-  if (Subtarget->isTargetDarwin()) {
+  if (Subtarget->isTargetMachO()) {
     Reloc::Model RelocM = TM.getRelocationModel();
     if (RelocM == Reloc::PIC_ || RelocM == Reloc::DynamicNoPIC) {
       // Declare all the text sections up front (before the DWARF sections
@@ -592,7 +410,7 @@ void ARMAsmPrinter::EmitStartOfAsmFile(Module &M) {
       // Now any user defined text sections from function attributes.
       for (Module::iterator F = M.begin(), e = M.end(); F != e; ++F)
         if (!F->isDeclaration() && !F->hasAvailableExternallyLinkage())
-          TextSections.insert(TLOFMacho.SectionForGlobal(F, Mang, TM));
+          TextSections.insert(TLOFMacho.SectionForGlobal(F, *Mang, TM));
       // Now the coalescable sections.
       TextSections.insert(TLOFMacho.getTextCoalSection());
       TextSections.insert(TLOFMacho.getConstTextCoalSection());
@@ -621,6 +439,13 @@ void ARMAsmPrinter::EmitStartOfAsmFile(Module &M) {
                                    SectionKind::getText());
       OutStreamer.SwitchSection(StaticInitSect);
     }
+
+    // Compiling with debug info should not affect the code
+    // generation.  Ensure the cstring section comes before the
+    // optional __DWARF secion. Otherwise, PC-relative loads would
+    // have to use different instruction sequences at "-g" in order to
+    // reach global data in the same object file.
+    OutStreamer.SwitchSection(getObjFileLowering().getCStringSection());
   }
 
   // Use unified assembler syntax.
@@ -633,7 +458,7 @@ void ARMAsmPrinter::EmitStartOfAsmFile(Module &M) {
 
 
 void ARMAsmPrinter::EmitEndOfAsmFile(Module &M) {
-  if (Subtarget->isTargetDarwin()) {
+  if (Subtarget->isTargetMachO()) {
     // All darwin targets use mach-o.
     const TargetLoweringObjectFileMachO &TLOFMacho =
       static_cast<const TargetLoweringObjectFileMachO &>(getObjFileLowering());
@@ -656,7 +481,7 @@ void ARMAsmPrinter::EmitEndOfAsmFile(Module &M) {
 
         if (MCSym.getInt())
           // External to current translation unit.
-          OutStreamer.EmitIntValue(0, 4/*size*/, 0/*addrspace*/);
+          OutStreamer.EmitIntValue(0, 4/*size*/);
         else
           // Internal to current translation unit.
           //
@@ -666,7 +491,7 @@ void ARMAsmPrinter::EmitEndOfAsmFile(Module &M) {
           // We need to fill in the value for the NLP in those cases.
           OutStreamer.EmitValue(MCSymbolRefExpr::Create(MCSym.getPointer(),
                                                         OutContext),
-                                4/*size*/, 0/*addrspace*/);
+                                4/*size*/);
       }
 
       Stubs.clear();
@@ -684,7 +509,7 @@ void ARMAsmPrinter::EmitEndOfAsmFile(Module &M) {
         OutStreamer.EmitValue(MCSymbolRefExpr::
                               Create(Stubs[i].second.getPointer(),
                                      OutContext),
-                              4/*size*/, 0/*addrspace*/);
+                              4/*size*/);
       }
 
       Stubs.clear();
@@ -707,167 +532,157 @@ void ARMAsmPrinter::EmitEndOfAsmFile(Module &M) {
 // to appear in the .ARM.attributes section in ELF.
 // Instead of subclassing the MCELFStreamer, we do the work here.
 
-void ARMAsmPrinter::emitAttributes() {
-
-  emitARMAttributeSection();
-
-  /* GAS expect .fpu to be emitted, regardless of VFP build attribute */
-  bool emitFPU = false;
-  AttributeEmitter *AttrEmitter;
-  if (OutStreamer.hasRawTextSupport()) {
-    AttrEmitter = new AsmAttributeEmitter(OutStreamer);
-    emitFPU = true;
-  } else {
-    MCObjectStreamer &O = static_cast<MCObjectStreamer&>(OutStreamer);
-    AttrEmitter = new ObjectAttributeEmitter(O);
-  }
-
-  AttrEmitter->MaybeSwitchVendor("aeabi");
-
-  std::string CPUString = Subtarget->getCPUString();
-
-  if (CPUString == "cortex-a8" ||
-      Subtarget->isCortexA8()) {
-    AttrEmitter->EmitTextAttribute(ARMBuildAttrs::CPU_name, "cortex-a8");
-    AttrEmitter->EmitAttribute(ARMBuildAttrs::CPU_arch, ARMBuildAttrs::v7);
-    AttrEmitter->EmitAttribute(ARMBuildAttrs::CPU_arch_profile,
-                               ARMBuildAttrs::ApplicationProfile);
-    AttrEmitter->EmitAttribute(ARMBuildAttrs::ARM_ISA_use,
-                               ARMBuildAttrs::Allowed);
-    AttrEmitter->EmitAttribute(ARMBuildAttrs::THUMB_ISA_use,
-                               ARMBuildAttrs::AllowThumb32);
-    // Fixme: figure out when this is emitted.
-    //AttrEmitter->EmitAttribute(ARMBuildAttrs::WMMX_arch,
-    //                           ARMBuildAttrs::AllowWMMXv1);
-    //
-
-    /// ADD additional Else-cases here!
-  } else if (CPUString == "xscale") {
-    AttrEmitter->EmitAttribute(ARMBuildAttrs::CPU_arch, ARMBuildAttrs::v5TEJ);
-    AttrEmitter->EmitAttribute(ARMBuildAttrs::ARM_ISA_use,
-                               ARMBuildAttrs::Allowed);
-    AttrEmitter->EmitAttribute(ARMBuildAttrs::THUMB_ISA_use,
-                               ARMBuildAttrs::Allowed);
-  } else if (CPUString == "generic") {
-    // For a generic CPU, we assume a standard v7a architecture in Subtarget.
-    AttrEmitter->EmitAttribute(ARMBuildAttrs::CPU_arch, ARMBuildAttrs::v7);
-    AttrEmitter->EmitAttribute(ARMBuildAttrs::CPU_arch_profile,
-                               ARMBuildAttrs::ApplicationProfile);
-    AttrEmitter->EmitAttribute(ARMBuildAttrs::ARM_ISA_use,
-                               ARMBuildAttrs::Allowed);
-    AttrEmitter->EmitAttribute(ARMBuildAttrs::THUMB_ISA_use,
-                               ARMBuildAttrs::AllowThumb32);
-  } else if (Subtarget->hasV7Ops()) {
-    AttrEmitter->EmitAttribute(ARMBuildAttrs::CPU_arch, ARMBuildAttrs::v7);
-    AttrEmitter->EmitAttribute(ARMBuildAttrs::THUMB_ISA_use,
-                               ARMBuildAttrs::AllowThumb32);
+static ARMBuildAttrs::CPUArch getArchForCPU(StringRef CPU,
+                                            const ARMSubtarget *Subtarget) {
+  if (CPU == "xscale")
+    return ARMBuildAttrs::v5TEJ;
+
+  if (Subtarget->hasV8Ops())
+    return ARMBuildAttrs::v8;
+  else if (Subtarget->hasV7Ops()) {
+    if (Subtarget->isMClass() && Subtarget->hasThumb2DSP())
+      return ARMBuildAttrs::v7E_M;
+    return ARMBuildAttrs::v7;
   } else if (Subtarget->hasV6T2Ops())
-    AttrEmitter->EmitAttribute(ARMBuildAttrs::CPU_arch, ARMBuildAttrs::v6T2);
+    return ARMBuildAttrs::v6T2;
+  else if (Subtarget->hasV6MOps())
+    return ARMBuildAttrs::v6S_M;
   else if (Subtarget->hasV6Ops())
-    AttrEmitter->EmitAttribute(ARMBuildAttrs::CPU_arch, ARMBuildAttrs::v6);
+    return ARMBuildAttrs::v6;
   else if (Subtarget->hasV5TEOps())
-    AttrEmitter->EmitAttribute(ARMBuildAttrs::CPU_arch, ARMBuildAttrs::v5TE);
+    return ARMBuildAttrs::v5TE;
   else if (Subtarget->hasV5TOps())
-    AttrEmitter->EmitAttribute(ARMBuildAttrs::CPU_arch, ARMBuildAttrs::v5T);
+    return ARMBuildAttrs::v5T;
   else if (Subtarget->hasV4TOps())
-    AttrEmitter->EmitAttribute(ARMBuildAttrs::CPU_arch, ARMBuildAttrs::v4T);
+    return ARMBuildAttrs::v4T;
+  else
+    return ARMBuildAttrs::v4;
+}
 
-  if (Subtarget->hasNEON() && emitFPU) {
-    /* NEON is not exactly a VFP architecture, but GAS emit one of
-     * neon/neon-vfpv4/vfpv3/vfpv2 for .fpu parameters */
-    if (Subtarget->hasVFP4())
-      AttrEmitter->EmitTextAttribute(ARMBuildAttrs::Advanced_SIMD_arch,
-                                     "neon-vfpv4");
-    else
-      AttrEmitter->EmitTextAttribute(ARMBuildAttrs::Advanced_SIMD_arch, "neon");
-    /* If emitted for NEON, omit from VFP below, since you can have both
-     * NEON and VFP in build attributes but only one .fpu */
-    emitFPU = false;
+void ARMAsmPrinter::emitAttributes() {
+  MCTargetStreamer &TS = *OutStreamer.getTargetStreamer();
+  ARMTargetStreamer &ATS = static_cast<ARMTargetStreamer &>(TS);
+
+  ATS.switchVendor("aeabi");
+
+  std::string CPUString = Subtarget->getCPUString();
+
+  // FIXME: remove krait check when GNU tools support krait cpu
+  if (CPUString != "generic" && CPUString != "krait")
+    ATS.emitTextAttribute(ARMBuildAttrs::CPU_name, CPUString);
+
+  ATS.emitAttribute(ARMBuildAttrs::CPU_arch,
+                    getArchForCPU(CPUString, Subtarget));
+
+  // Tag_CPU_arch_profile must have the default value of 0 when "Architecture
+  // profile is not applicable (e.g. pre v7, or cross-profile code)". 
+  if (Subtarget->hasV7Ops()) {
+    if (Subtarget->isAClass()) {
+      ATS.emitAttribute(ARMBuildAttrs::CPU_arch_profile,
+                        ARMBuildAttrs::ApplicationProfile);
+    } else if (Subtarget->isRClass()) {
+      ATS.emitAttribute(ARMBuildAttrs::CPU_arch_profile,
+                        ARMBuildAttrs::RealTimeProfile);
+    } else if (Subtarget->isMClass()) {
+      ATS.emitAttribute(ARMBuildAttrs::CPU_arch_profile,
+                        ARMBuildAttrs::MicroControllerProfile);
+    }
   }
 
-  /* VFPv4 + .fpu */
-  if (Subtarget->hasVFP4()) {
-    AttrEmitter->EmitAttribute(ARMBuildAttrs::VFP_arch,
-                               ARMBuildAttrs::AllowFPv4A);
-    if (emitFPU)
-      AttrEmitter->EmitTextAttribute(ARMBuildAttrs::VFP_arch, "vfpv4");
-
-  /* VFPv3 + .fpu */
-  } else if (Subtarget->hasVFP3()) {
-    AttrEmitter->EmitAttribute(ARMBuildAttrs::VFP_arch,
-                               ARMBuildAttrs::AllowFPv3A);
-    if (emitFPU)
-      AttrEmitter->EmitTextAttribute(ARMBuildAttrs::VFP_arch, "vfpv3");
-
-  /* VFPv2 + .fpu */
-  } else if (Subtarget->hasVFP2()) {
-    AttrEmitter->EmitAttribute(ARMBuildAttrs::VFP_arch,
-                               ARMBuildAttrs::AllowFPv2);
-    if (emitFPU)
-      AttrEmitter->EmitTextAttribute(ARMBuildAttrs::VFP_arch, "vfpv2");
+  ATS.emitAttribute(ARMBuildAttrs::ARM_ISA_use, Subtarget->hasARMOps() ?
+                      ARMBuildAttrs::Allowed : ARMBuildAttrs::Not_Allowed);
+  if (Subtarget->isThumb1Only()) {
+    ATS.emitAttribute(ARMBuildAttrs::THUMB_ISA_use,
+                      ARMBuildAttrs::Allowed);
+  } else if (Subtarget->hasThumb2()) {
+    ATS.emitAttribute(ARMBuildAttrs::THUMB_ISA_use,
+                      ARMBuildAttrs::AllowThumb32);
   }
 
-  /* TODO: ARMBuildAttrs::Allowed is not completely accurate,
-   * since NEON can have 1 (allowed) or 2 (MAC operations) */
   if (Subtarget->hasNEON()) {
-    AttrEmitter->EmitAttribute(ARMBuildAttrs::Advanced_SIMD_arch,
-                               ARMBuildAttrs::Allowed);
+    /* NEON is not exactly a VFP architecture, but GAS emit one of
+     * neon/neon-fp-armv8/neon-vfpv4/vfpv3/vfpv2 for .fpu parameters */
+    if (Subtarget->hasFPARMv8()) {
+      if (Subtarget->hasCrypto())
+        ATS.emitFPU(ARM::CRYPTO_NEON_FP_ARMV8);
+      else
+        ATS.emitFPU(ARM::NEON_FP_ARMV8);
+    }
+    else if (Subtarget->hasVFP4())
+      ATS.emitFPU(ARM::NEON_VFPV4);
+    else
+      ATS.emitFPU(ARM::NEON);
+    // Emit Tag_Advanced_SIMD_arch for ARMv8 architecture
+    if (Subtarget->hasV8Ops())
+      ATS.emitAttribute(ARMBuildAttrs::Advanced_SIMD_arch,
+                        ARMBuildAttrs::AllowNeonARMv8);
+  } else {
+    if (Subtarget->hasFPARMv8())
+      ATS.emitFPU(ARM::FP_ARMV8);
+    else if (Subtarget->hasVFP4())
+      ATS.emitFPU(Subtarget->hasD16() ? ARM::VFPV4_D16 : ARM::VFPV4);
+    else if (Subtarget->hasVFP3())
+      ATS.emitFPU(Subtarget->hasD16() ? ARM::VFPV3_D16 : ARM::VFPV3);
+    else if (Subtarget->hasVFP2())
+      ATS.emitFPU(ARM::VFPV2);
   }
 
   // Signal various FP modes.
   if (!TM.Options.UnsafeFPMath) {
-    AttrEmitter->EmitAttribute(ARMBuildAttrs::ABI_FP_denormal,
-                               ARMBuildAttrs::Allowed);
-    AttrEmitter->EmitAttribute(ARMBuildAttrs::ABI_FP_exceptions,
-                               ARMBuildAttrs::Allowed);
+    ATS.emitAttribute(ARMBuildAttrs::ABI_FP_denormal, ARMBuildAttrs::Allowed);
+    ATS.emitAttribute(ARMBuildAttrs::ABI_FP_exceptions,
+                      ARMBuildAttrs::Allowed);
   }
 
   if (TM.Options.NoInfsFPMath && TM.Options.NoNaNsFPMath)
-    AttrEmitter->EmitAttribute(ARMBuildAttrs::ABI_FP_number_model,
-                               ARMBuildAttrs::Allowed);
+    ATS.emitAttribute(ARMBuildAttrs::ABI_FP_number_model,
+                      ARMBuildAttrs::Allowed);
   else
-    AttrEmitter->EmitAttribute(ARMBuildAttrs::ABI_FP_number_model,
-                               ARMBuildAttrs::AllowIEE754);
+    ATS.emitAttribute(ARMBuildAttrs::ABI_FP_number_model,
+                      ARMBuildAttrs::AllowIEE754);
 
-  // FIXME: add more flags to ARMBuildAttrs.h
+  // FIXME: add more flags to ARMBuildAttributes.h
   // 8-bytes alignment stuff.
-  AttrEmitter->EmitAttribute(ARMBuildAttrs::ABI_align8_needed, 1);
-  AttrEmitter->EmitAttribute(ARMBuildAttrs::ABI_align8_preserved, 1);
+  ATS.emitAttribute(ARMBuildAttrs::ABI_align_needed, 1);
+  ATS.emitAttribute(ARMBuildAttrs::ABI_align_preserved, 1);
 
-  // Hard float.  Use both S and D registers and conform to AAPCS-VFP.
-  if (Subtarget->isAAPCS_ABI() && TM.Options.FloatABIType == FloatABI::Hard) {
-    AttrEmitter->EmitAttribute(ARMBuildAttrs::ABI_HardFP_use, 3);
-    AttrEmitter->EmitAttribute(ARMBuildAttrs::ABI_VFP_args, 1);
-  }
-  // FIXME: Should we signal R9 usage?
-
-  if (Subtarget->hasDivide())
-    AttrEmitter->EmitAttribute(ARMBuildAttrs::DIV_use, 1);
+  // ABI_HardFP_use attribute to indicate single precision FP.
+  if (Subtarget->isFPOnlySP())
+    ATS.emitAttribute(ARMBuildAttrs::ABI_HardFP_use,
+                      ARMBuildAttrs::HardFPSinglePrecision);
 
-  AttrEmitter->Finish();
-  delete AttrEmitter;
-}
-
-void ARMAsmPrinter::emitARMAttributeSection() {
-  // <format-version>
-  // [ <section-length> "vendor-name"
-  // [ <file-tag> <size> <attribute>*
-  //   | <section-tag> <size> <section-number>* 0 <attribute>*
-  //   | <symbol-tag> <size> <symbol-number>* 0 <attribute>*
-  //   ]+
-  // ]*
-
-  if (OutStreamer.hasRawTextSupport())
-    return;
-
-  const ARMElfTargetObjectFile &TLOFELF =
-    static_cast<const ARMElfTargetObjectFile &>
-    (getObjFileLowering());
+  // Hard float.  Use both S and D registers and conform to AAPCS-VFP.
+  if (Subtarget->isAAPCS_ABI() && TM.Options.FloatABIType == FloatABI::Hard)
+    ATS.emitAttribute(ARMBuildAttrs::ABI_VFP_args, ARMBuildAttrs::HardFPAAPCS);
 
-  OutStreamer.SwitchSection(TLOFELF.getAttributesSection());
+  // FIXME: Should we signal R9 usage?
 
-  // Format version
-  OutStreamer.EmitIntValue(0x41, 1);
+  if (Subtarget->hasFP16())
+      ATS.emitAttribute(ARMBuildAttrs::FP_HP_extension, ARMBuildAttrs::AllowHPFP);
+
+  if (Subtarget->hasMPExtension())
+      ATS.emitAttribute(ARMBuildAttrs::MPextension_use, ARMBuildAttrs::AllowMP);
+
+  // Hardware divide in ARM mode is part of base arch, starting from ARMv8.
+  // If only Thumb hwdiv is present, it must also be in base arch (ARMv7-R/M).
+  // It is not possible to produce DisallowDIV: if hwdiv is present in the base
+  // arch, supplying -hwdiv downgrades the effective arch, via ClearImpliedBits.
+  // AllowDIVExt is only emitted if hwdiv isn't available in the base arch;
+  // otherwise, the default value (AllowDIVIfExists) applies.
+  if (Subtarget->hasDivideInARMMode() && !Subtarget->hasV8Ops())
+      ATS.emitAttribute(ARMBuildAttrs::DIV_use, ARMBuildAttrs::AllowDIVExt);
+
+  if (Subtarget->hasTrustZone() && Subtarget->hasVirtualization())
+      ATS.emitAttribute(ARMBuildAttrs::Virtualization_use,
+                        ARMBuildAttrs::AllowTZVirtualization);
+  else if (Subtarget->hasTrustZone())
+      ATS.emitAttribute(ARMBuildAttrs::Virtualization_use,
+                        ARMBuildAttrs::AllowTZ);
+  else if (Subtarget->hasVirtualization())
+      ATS.emitAttribute(ARMBuildAttrs::Virtualization_use,
+                        ARMBuildAttrs::AllowVirtualization);
+
+  ATS.finishAttributeSection();
 }
 
 //===----------------------------------------------------------------------===//
@@ -884,23 +699,25 @@ static MCSymbolRefExpr::VariantKind
 getModifierVariantKind(ARMCP::ARMCPModifier Modifier) {
   switch (Modifier) {
   case ARMCP::no_modifier: return MCSymbolRefExpr::VK_None;
-  case ARMCP::TLSGD:       return MCSymbolRefExpr::VK_ARM_TLSGD;
-  case ARMCP::TPOFF:       return MCSymbolRefExpr::VK_ARM_TPOFF;
-  case ARMCP::GOTTPOFF:    return MCSymbolRefExpr::VK_ARM_GOTTPOFF;
-  case ARMCP::GOT:         return MCSymbolRefExpr::VK_ARM_GOT;
-  case ARMCP::GOTOFF:      return MCSymbolRefExpr::VK_ARM_GOTOFF;
+  case ARMCP::TLSGD:       return MCSymbolRefExpr::VK_TLSGD;
+  case ARMCP::TPOFF:       return MCSymbolRefExpr::VK_TPOFF;
+  case ARMCP::GOTTPOFF:    return MCSymbolRefExpr::VK_GOTTPOFF;
+  case ARMCP::GOT:         return MCSymbolRefExpr::VK_GOT;
+  case ARMCP::GOTOFF:      return MCSymbolRefExpr::VK_GOTOFF;
   }
   llvm_unreachable("Invalid ARMCPModifier!");
 }
 
-MCSymbol *ARMAsmPrinter::GetARMGVSymbol(const GlobalValue *GV) {
-  bool isIndirect = Subtarget->isTargetDarwin() &&
+MCSymbol *ARMAsmPrinter::GetARMGVSymbol(const GlobalValue *GV,
+                                        unsigned char TargetFlags) {
+  bool isIndirect = Subtarget->isTargetMachO() &&
+    (TargetFlags & ARMII::MO_NONLAZY) &&
     Subtarget->GVIsIndirectSymbol(GV, TM.getRelocationModel());
   if (!isIndirect)
-    return Mang->getSymbol(GV);
+    return getSymbol(GV);
 
   // FIXME: Remove this when Darwin transition to @GOT like syntax.
-  MCSymbol *MCSym = GetSymbolWithGlobalValueBase(GV, "$non_lazy_ptr");
+  MCSymbol *MCSym = getSymbolWithGlobalValueBase(GV, "$non_lazy_ptr");
   MachineModuleInfoMachO &MMIMachO =
     MMI->getObjFileInfo<MachineModuleInfoMachO>();
   MachineModuleInfoImpl::StubValueTy &StubSym =
@@ -908,12 +725,13 @@ MCSymbol *ARMAsmPrinter::GetARMGVSymbol(const GlobalValue *GV) {
     MMIMachO.getGVStubEntry(MCSym);
   if (StubSym.getPointer() == 0)
     StubSym = MachineModuleInfoImpl::
-      StubValueTy(Mang->getSymbol(GV), !GV->hasInternalLinkage());
+      StubValueTy(getSymbol(GV), !GV->hasInternalLinkage());
   return MCSym;
 }
 
 void ARMAsmPrinter::
 EmitMachineConstantPoolValue(MachineConstantPoolValue *MCPV) {
+  const DataLayout *DL = TM.getDataLayout();
   int Size = TM.getDataLayout()->getTypeAllocSize(MCPV->getType());
 
   ARMConstantPoolValue *ACPV = static_cast<ARMConstantPoolValue*>(MCPV);
@@ -922,7 +740,7 @@ EmitMachineConstantPoolValue(MachineConstantPoolValue *MCPV) {
   if (ACPV->isLSDA()) {
     SmallString<128> Str;
     raw_svector_ostream OS(Str);
-    OS << MAI->getPrivateGlobalPrefix() << "_LSDA_" << getFunctionNumber();
+    OS << DL->getPrivateGlobalPrefix() << "_LSDA_" << getFunctionNumber();
     MCSym = OutContext.GetOrCreateSymbol(OS.str());
   } else if (ACPV->isBlockAddress()) {
     const BlockAddress *BA =
@@ -930,7 +748,11 @@ EmitMachineConstantPoolValue(MachineConstantPoolValue *MCPV) {
     MCSym = GetBlockAddressSymbol(BA);
   } else if (ACPV->isGlobalValue()) {
     const GlobalValue *GV = cast<ARMConstantPoolConstant>(ACPV)->getGV();
-    MCSym = GetARMGVSymbol(GV);
+
+    // On Darwin, const-pool entries may get the "FOO$non_lazy_ptr" mangling, so
+    // flag the global as MO_NONLAZY.
+    unsigned char TF = Subtarget->isTargetMachO() ? ARMII::MO_NONLAZY : 0;
+    MCSym = GetARMGVSymbol(GV, TF);
   } else if (ACPV->isMachineBasicBlock()) {
     const MachineBasicBlock *MBB = cast<ARMConstantPoolMBB>(ACPV)->getMBB();
     MCSym = MBB->getSymbol();
@@ -946,7 +768,7 @@ EmitMachineConstantPoolValue(MachineConstantPoolValue *MCPV) {
                             OutContext);
 
   if (ACPV->getPCAdjustment()) {
-    MCSymbol *PCLabel = getPICLabel(MAI->getPrivateGlobalPrefix(),
+    MCSymbol *PCLabel = getPICLabel(DL->getPrivateGlobalPrefix(),
                                     getFunctionNumber(),
                                     ACPV->getLabelId(),
                                     OutContext);
@@ -1051,12 +873,10 @@ void ARMAsmPrinter::EmitJump2Table(const MachineInstr *MI) {
                                                       OutContext);
     // If this isn't a TBB or TBH, the entries are direct branch instructions.
     if (OffsetWidth == 4) {
-      MCInst BrInst;
-      BrInst.setOpcode(ARM::t2B);
-      BrInst.addOperand(MCOperand::CreateExpr(MBBSymbolExpr));
-      BrInst.addOperand(MCOperand::CreateImm(ARMCC::AL));
-      BrInst.addOperand(MCOperand::CreateReg(0));
-      OutStreamer.EmitInstruction(BrInst);
+      EmitToStreamer(OutStreamer, MCInstBuilder(ARM::t2B)
+        .addExpr(MBBSymbolExpr)
+        .addImm(ARMCC::AL)
+        .addReg(0));
       continue;
     }
     // Otherwise it's an offset from the dispatch instruction. Construct an
@@ -1083,39 +903,12 @@ void ARMAsmPrinter::EmitJump2Table(const MachineInstr *MI) {
     OutStreamer.EmitDataRegion(MCDR_DataRegionEnd);
 }
 
-void ARMAsmPrinter::PrintDebugValueComment(const MachineInstr *MI,
-                                           raw_ostream &OS) {
-  unsigned NOps = MI->getNumOperands();
-  assert(NOps==4);
-  OS << '\t' << MAI->getCommentString() << "DEBUG_VALUE: ";
-  // cast away const; DIetc do not take const operands for some reason.
-  DIVariable V(const_cast<MDNode *>(MI->getOperand(NOps-1).getMetadata()));
-  OS << V.getName();
-  OS << " <- ";
-  // Frame address.  Currently handles register +- offset only.
-  assert(MI->getOperand(0).isReg() && MI->getOperand(1).isImm());
-  OS << '['; printOperand(MI, 0, OS); OS << '+'; printOperand(MI, 1, OS);
-  OS << ']';
-  OS << "+";
-  printOperand(MI, NOps-2, OS);
-}
-
-static void populateADROperands(MCInst &Inst, unsigned Dest,
-                                const MCSymbol *Label,
-                                unsigned pred, unsigned ccreg,
-                                MCContext &Ctx) {
-  const MCExpr *SymbolExpr = MCSymbolRefExpr::Create(Label, Ctx);
-  Inst.addOperand(MCOperand::CreateReg(Dest));
-  Inst.addOperand(MCOperand::CreateExpr(SymbolExpr));
-  // Add predicate operands.
-  Inst.addOperand(MCOperand::CreateImm(pred));
-  Inst.addOperand(MCOperand::CreateReg(ccreg));
-}
-
 void ARMAsmPrinter::EmitUnwindingInstruction(const MachineInstr *MI) {
   assert(MI->getFlag(MachineInstr::FrameSetup) &&
       "Only instruction which are involved into frame setup code are allowed");
 
+  MCTargetStreamer &TS = *OutStreamer.getTargetStreamer();
+  ARMTargetStreamer &ATS = static_cast<ARMTargetStreamer &>(TS);
   const MachineFunction &MF = *MI->getParent()->getParent();
   const TargetRegisterInfo *RegInfo = MF.getTarget().getRegisterInfo();
   const ARMFunctionInfo &AFI = *MF.getInfo<ARMFunctionInfo>();
@@ -1178,7 +971,7 @@ void ARMAsmPrinter::EmitUnwindingInstruction(const MachineInstr *MI) {
       RegList.push_back(SrcReg);
       break;
     }
-    OutStreamer.EmitRegSave(RegList, Opc == ARM::VSTMDDB_UPD);
+    ATS.emitRegSave(RegList, Opc == ARM::VSTMDDB_UPD);
   } else {
     // Changes of stack / frame pointer.
     if (SrcReg == ARM::SP) {
@@ -1226,17 +1019,17 @@ void ARMAsmPrinter::EmitUnwindingInstruction(const MachineInstr *MI) {
       if (DstReg == FramePtr && FramePtr != ARM::SP)
         // Set-up of the frame pointer. Positive values correspond to "add"
         // instruction.
-        OutStreamer.EmitSetFP(FramePtr, ARM::SP, -Offset);
+        ATS.emitSetFP(FramePtr, ARM::SP, -Offset);
       else if (DstReg == ARM::SP) {
         // Change of SP by an offset. Positive values correspond to "sub"
         // instruction.
-        OutStreamer.EmitPad(Offset);
+        ATS.emitPad(Offset);
       } else {
-        MI->dump();
-        llvm_unreachable("Unsupported opcode for unwinding information");
+        // Move of SP to a register.  Positive values correspond to an "add"
+        // instruction.
+        ATS.emitMovSP(DstReg, -Offset);
       }
     } else if (DstReg == ARM::SP) {
-      // FIXME: .movsp goes here
       MI->dump();
       llvm_unreachable("Unsupported opcode for unwinding information");
     }
@@ -1247,13 +1040,13 @@ void ARMAsmPrinter::EmitUnwindingInstruction(const MachineInstr *MI) {
   }
 }
 
-extern cl::opt<bool> EnableARMEHABI;
-
 // Simple pseudo-instructions have their lowering (with expansion to real
 // instructions) auto-generated.
 #include "ARMGenMCPseudoLowering.inc"
 
 void ARMAsmPrinter::EmitInstruction(const MachineInstr *MI) {
+  const DataLayout *DL = TM.getDataLayout();
+
   // If we just ended a constant pool, mark it as such.
   if (InConstantPool && MI->getOpcode() != ARM::CONSTPOOL_ENTRY) {
     OutStreamer.EmitDataRegion(MCDR_DataRegionEnd);
@@ -1261,7 +1054,8 @@ void ARMAsmPrinter::EmitInstruction(const MachineInstr *MI) {
   }
 
   // Emit unwinding stuff for frame-related instructions
-  if (EnableARMEHABI && MI->getFlag(MachineInstr::FrameSetup))
+  if (Subtarget->isTargetEHABICompatible() &&
+       MI->getFlag(MachineInstr::FrameSetup))
     EmitUnwindingInstruction(MI);
 
   // Do any auto-generated pseudo lowerings.
@@ -1275,142 +1069,109 @@ void ARMAsmPrinter::EmitInstruction(const MachineInstr *MI) {
   unsigned Opc = MI->getOpcode();
   switch (Opc) {
   case ARM::t2MOVi32imm: llvm_unreachable("Should be lowered by thumb2it pass");
-  case ARM::DBG_VALUE: {
-    if (isVerbose() && OutStreamer.hasRawTextSupport()) {
-      SmallString<128> TmpStr;
-      raw_svector_ostream OS(TmpStr);
-      PrintDebugValueComment(MI, OS);
-      OutStreamer.EmitRawText(StringRef(OS.str()));
-    }
-    return;
-  }
+  case ARM::DBG_VALUE: llvm_unreachable("Should be handled by generic printing");
   case ARM::LEApcrel:
   case ARM::tLEApcrel:
   case ARM::t2LEApcrel: {
     // FIXME: Need to also handle globals and externals
-    MCInst TmpInst;
-    TmpInst.setOpcode(MI->getOpcode() == ARM::t2LEApcrel ? ARM::t2ADR
-                      : (MI->getOpcode() == ARM::tLEApcrel ? ARM::tADR
-                         : ARM::ADR));
-    populateADROperands(TmpInst, MI->getOperand(0).getReg(),
-                        GetCPISymbol(MI->getOperand(1).getIndex()),
-                        MI->getOperand(2).getImm(), MI->getOperand(3).getReg(),
-                        OutContext);
-    OutStreamer.EmitInstruction(TmpInst);
+    MCSymbol *CPISymbol = GetCPISymbol(MI->getOperand(1).getIndex());
+    EmitToStreamer(OutStreamer, MCInstBuilder(MI->getOpcode() ==
+                                              ARM::t2LEApcrel ? ARM::t2ADR
+                  : (MI->getOpcode() == ARM::tLEApcrel ? ARM::tADR
+                     : ARM::ADR))
+      .addReg(MI->getOperand(0).getReg())
+      .addExpr(MCSymbolRefExpr::Create(CPISymbol, OutContext))
+      // Add predicate operands.
+      .addImm(MI->getOperand(2).getImm())
+      .addReg(MI->getOperand(3).getReg()));
     return;
   }
   case ARM::LEApcrelJT:
   case ARM::tLEApcrelJT:
   case ARM::t2LEApcrelJT: {
-    MCInst TmpInst;
-    TmpInst.setOpcode(MI->getOpcode() == ARM::t2LEApcrelJT ? ARM::t2ADR
-                      : (MI->getOpcode() == ARM::tLEApcrelJT ? ARM::tADR
-                         : ARM::ADR));
-    populateADROperands(TmpInst, MI->getOperand(0).getReg(),
-                      GetARMJTIPICJumpTableLabel2(MI->getOperand(1).getIndex(),
-                                                  MI->getOperand(2).getImm()),
-                      MI->getOperand(3).getImm(), MI->getOperand(4).getReg(),
-                      OutContext);
-    OutStreamer.EmitInstruction(TmpInst);
+    MCSymbol *JTIPICSymbol =
+      GetARMJTIPICJumpTableLabel2(MI->getOperand(1).getIndex(),
+                                  MI->getOperand(2).getImm());
+    EmitToStreamer(OutStreamer, MCInstBuilder(MI->getOpcode() ==
+                                              ARM::t2LEApcrelJT ? ARM::t2ADR
+                  : (MI->getOpcode() == ARM::tLEApcrelJT ? ARM::tADR
+                     : ARM::ADR))
+      .addReg(MI->getOperand(0).getReg())
+      .addExpr(MCSymbolRefExpr::Create(JTIPICSymbol, OutContext))
+      // Add predicate operands.
+      .addImm(MI->getOperand(3).getImm())
+      .addReg(MI->getOperand(4).getReg()));
     return;
   }
   // Darwin call instructions are just normal call instructions with different
   // clobber semantics (they clobber R9).
   case ARM::BX_CALL: {
-    {
-      MCInst TmpInst;
-      TmpInst.setOpcode(ARM::MOVr);
-      TmpInst.addOperand(MCOperand::CreateReg(ARM::LR));
-      TmpInst.addOperand(MCOperand::CreateReg(ARM::PC));
+    EmitToStreamer(OutStreamer, MCInstBuilder(ARM::MOVr)
+      .addReg(ARM::LR)
+      .addReg(ARM::PC)
       // Add predicate operands.
-      TmpInst.addOperand(MCOperand::CreateImm(ARMCC::AL));
-      TmpInst.addOperand(MCOperand::CreateReg(0));
+      .addImm(ARMCC::AL)
+      .addReg(0)
       // Add 's' bit operand (always reg0 for this)
-      TmpInst.addOperand(MCOperand::CreateReg(0));
-      OutStreamer.EmitInstruction(TmpInst);
-    }
-    {
-      MCInst TmpInst;
-      TmpInst.setOpcode(ARM::BX);
-      TmpInst.addOperand(MCOperand::CreateReg(MI->getOperand(0).getReg()));
-      OutStreamer.EmitInstruction(TmpInst);
-    }
+      .addReg(0));
+
+    EmitToStreamer(OutStreamer, MCInstBuilder(ARM::BX)
+      .addReg(MI->getOperand(0).getReg()));
     return;
   }
   case ARM::tBX_CALL: {
-    {
-      MCInst TmpInst;
-      TmpInst.setOpcode(ARM::tMOVr);
-      TmpInst.addOperand(MCOperand::CreateReg(ARM::LR));
-      TmpInst.addOperand(MCOperand::CreateReg(ARM::PC));
+    EmitToStreamer(OutStreamer, MCInstBuilder(ARM::tMOVr)
+      .addReg(ARM::LR)
+      .addReg(ARM::PC)
       // Add predicate operands.
-      TmpInst.addOperand(MCOperand::CreateImm(ARMCC::AL));
-      TmpInst.addOperand(MCOperand::CreateReg(0));
-      OutStreamer.EmitInstruction(TmpInst);
-    }
-    {
-      MCInst TmpInst;
-      TmpInst.setOpcode(ARM::tBX);
-      TmpInst.addOperand(MCOperand::CreateReg(MI->getOperand(0).getReg()));
+      .addImm(ARMCC::AL)
+      .addReg(0));
+
+    EmitToStreamer(OutStreamer, MCInstBuilder(ARM::tBX)
+      .addReg(MI->getOperand(0).getReg())
       // Add predicate operands.
-      TmpInst.addOperand(MCOperand::CreateImm(ARMCC::AL));
-      TmpInst.addOperand(MCOperand::CreateReg(0));
-      OutStreamer.EmitInstruction(TmpInst);
-    }
+      .addImm(ARMCC::AL)
+      .addReg(0));
     return;
   }
   case ARM::BMOVPCRX_CALL: {
-    {
-      MCInst TmpInst;
-      TmpInst.setOpcode(ARM::MOVr);
-      TmpInst.addOperand(MCOperand::CreateReg(ARM::LR));
-      TmpInst.addOperand(MCOperand::CreateReg(ARM::PC));
+    EmitToStreamer(OutStreamer, MCInstBuilder(ARM::MOVr)
+      .addReg(ARM::LR)
+      .addReg(ARM::PC)
       // Add predicate operands.
-      TmpInst.addOperand(MCOperand::CreateImm(ARMCC::AL));
-      TmpInst.addOperand(MCOperand::CreateReg(0));
+      .addImm(ARMCC::AL)
+      .addReg(0)
       // Add 's' bit operand (always reg0 for this)
-      TmpInst.addOperand(MCOperand::CreateReg(0));
-      OutStreamer.EmitInstruction(TmpInst);
-    }
-    {
-      MCInst TmpInst;
-      TmpInst.setOpcode(ARM::MOVr);
-      TmpInst.addOperand(MCOperand::CreateReg(ARM::PC));
-      TmpInst.addOperand(MCOperand::CreateReg(MI->getOperand(0).getReg()));
+      .addReg(0));
+
+    EmitToStreamer(OutStreamer, MCInstBuilder(ARM::MOVr)
+      .addReg(ARM::PC)
+      .addReg(MI->getOperand(0).getReg())
       // Add predicate operands.
-      TmpInst.addOperand(MCOperand::CreateImm(ARMCC::AL));
-      TmpInst.addOperand(MCOperand::CreateReg(0));
+      .addImm(ARMCC::AL)
+      .addReg(0)
       // Add 's' bit operand (always reg0 for this)
-      TmpInst.addOperand(MCOperand::CreateReg(0));
-      OutStreamer.EmitInstruction(TmpInst);
-    }
+      .addReg(0));
     return;
   }
   case ARM::BMOVPCB_CALL: {
-    {
-      MCInst TmpInst;
-      TmpInst.setOpcode(ARM::MOVr);
-      TmpInst.addOperand(MCOperand::CreateReg(ARM::LR));
-      TmpInst.addOperand(MCOperand::CreateReg(ARM::PC));
+    EmitToStreamer(OutStreamer, MCInstBuilder(ARM::MOVr)
+      .addReg(ARM::LR)
+      .addReg(ARM::PC)
       // Add predicate operands.
-      TmpInst.addOperand(MCOperand::CreateImm(ARMCC::AL));
-      TmpInst.addOperand(MCOperand::CreateReg(0));
+      .addImm(ARMCC::AL)
+      .addReg(0)
       // Add 's' bit operand (always reg0 for this)
-      TmpInst.addOperand(MCOperand::CreateReg(0));
-      OutStreamer.EmitInstruction(TmpInst);
-    }
-    {
-      MCInst TmpInst;
-      TmpInst.setOpcode(ARM::Bcc);
-      const GlobalValue *GV = MI->getOperand(0).getGlobal();
-      MCSymbol *GVSym = Mang->getSymbol(GV);
-      const MCExpr *GVSymExpr = MCSymbolRefExpr::Create(GVSym, OutContext);
-      TmpInst.addOperand(MCOperand::CreateExpr(GVSymExpr));
+      .addReg(0));
+
+    const GlobalValue *GV = MI->getOperand(0).getGlobal();
+    MCSymbol *GVSym = getSymbol(GV);
+    const MCExpr *GVSymExpr = MCSymbolRefExpr::Create(GVSym, OutContext);
+    EmitToStreamer(OutStreamer, MCInstBuilder(ARM::Bcc)
+      .addExpr(GVSymExpr)
       // Add predicate operands.
-      TmpInst.addOperand(MCOperand::CreateImm(ARMCC::AL));
-      TmpInst.addOperand(MCOperand::CreateReg(0));
-      OutStreamer.EmitInstruction(TmpInst);
-    }
+      .addImm(ARMCC::AL)
+      .addReg(0));
     return;
   }
   case ARM::MOVi16_ga_pcrel:
@@ -1420,33 +1181,28 @@ void ARMAsmPrinter::EmitInstruction(const MachineInstr *MI) {
     TmpInst.addOperand(MCOperand::CreateReg(MI->getOperand(0).getReg()));
 
     unsigned TF = MI->getOperand(1).getTargetFlags();
-    bool isPIC = TF == ARMII::MO_LO16_NONLAZY_PIC;
     const GlobalValue *GV = MI->getOperand(1).getGlobal();
-    MCSymbol *GVSym = GetARMGVSymbol(GV);
+    MCSymbol *GVSym = GetARMGVSymbol(GV, TF);
     const MCExpr *GVSymExpr = MCSymbolRefExpr::Create(GVSym, OutContext);
-    if (isPIC) {
-      MCSymbol *LabelSym = getPICLabel(MAI->getPrivateGlobalPrefix(),
-                                       getFunctionNumber(),
-                                       MI->getOperand(2).getImm(), OutContext);
-      const MCExpr *LabelSymExpr= MCSymbolRefExpr::Create(LabelSym, OutContext);
-      unsigned PCAdj = (Opc == ARM::MOVi16_ga_pcrel) ? 8 : 4;
-      const MCExpr *PCRelExpr =
-        ARMMCExpr::CreateLower16(MCBinaryExpr::CreateSub(GVSymExpr,
-                                  MCBinaryExpr::CreateAdd(LabelSymExpr,
+
+    MCSymbol *LabelSym = getPICLabel(DL->getPrivateGlobalPrefix(),
+                                     getFunctionNumber(),
+                                     MI->getOperand(2).getImm(), OutContext);
+    const MCExpr *LabelSymExpr= MCSymbolRefExpr::Create(LabelSym, OutContext);
+    unsigned PCAdj = (Opc == ARM::MOVi16_ga_pcrel) ? 8 : 4;
+    const MCExpr *PCRelExpr =
+      ARMMCExpr::CreateLower16(MCBinaryExpr::CreateSub(GVSymExpr,
+                                      MCBinaryExpr::CreateAdd(LabelSymExpr,
                                       MCConstantExpr::Create(PCAdj, OutContext),
-                                          OutContext), OutContext), OutContext);
+                                      OutContext), OutContext), OutContext);
       TmpInst.addOperand(MCOperand::CreateExpr(PCRelExpr));
-    } else {
-      const MCExpr *RefExpr= ARMMCExpr::CreateLower16(GVSymExpr, OutContext);
-      TmpInst.addOperand(MCOperand::CreateExpr(RefExpr));
-    }
 
     // Add predicate operands.
     TmpInst.addOperand(MCOperand::CreateImm(ARMCC::AL));
     TmpInst.addOperand(MCOperand::CreateReg(0));
     // Add 's' bit operand (always reg0 for this)
     TmpInst.addOperand(MCOperand::CreateReg(0));
-    OutStreamer.EmitInstruction(TmpInst);
+    EmitToStreamer(OutStreamer, TmpInst);
     return;
   }
   case ARM::MOVTi16_ga_pcrel:
@@ -1458,32 +1214,27 @@ void ARMAsmPrinter::EmitInstruction(const MachineInstr *MI) {
     TmpInst.addOperand(MCOperand::CreateReg(MI->getOperand(1).getReg()));
 
     unsigned TF = MI->getOperand(2).getTargetFlags();
-    bool isPIC = TF == ARMII::MO_HI16_NONLAZY_PIC;
     const GlobalValue *GV = MI->getOperand(2).getGlobal();
-    MCSymbol *GVSym = GetARMGVSymbol(GV);
+    MCSymbol *GVSym = GetARMGVSymbol(GV, TF);
     const MCExpr *GVSymExpr = MCSymbolRefExpr::Create(GVSym, OutContext);
-    if (isPIC) {
-      MCSymbol *LabelSym = getPICLabel(MAI->getPrivateGlobalPrefix(),
-                                       getFunctionNumber(),
-                                       MI->getOperand(3).getImm(), OutContext);
-      const MCExpr *LabelSymExpr= MCSymbolRefExpr::Create(LabelSym, OutContext);
-      unsigned PCAdj = (Opc == ARM::MOVTi16_ga_pcrel) ? 8 : 4;
-      const MCExpr *PCRelExpr =
+
+    MCSymbol *LabelSym = getPICLabel(DL->getPrivateGlobalPrefix(),
+                                     getFunctionNumber(),
+                                     MI->getOperand(3).getImm(), OutContext);
+    const MCExpr *LabelSymExpr= MCSymbolRefExpr::Create(LabelSym, OutContext);
+    unsigned PCAdj = (Opc == ARM::MOVTi16_ga_pcrel) ? 8 : 4;
+    const MCExpr *PCRelExpr =
         ARMMCExpr::CreateUpper16(MCBinaryExpr::CreateSub(GVSymExpr,
                                    MCBinaryExpr::CreateAdd(LabelSymExpr,
                                       MCConstantExpr::Create(PCAdj, OutContext),
                                           OutContext), OutContext), OutContext);
       TmpInst.addOperand(MCOperand::CreateExpr(PCRelExpr));
-    } else {
-      const MCExpr *RefExpr= ARMMCExpr::CreateUpper16(GVSymExpr, OutContext);
-      TmpInst.addOperand(MCOperand::CreateExpr(RefExpr));
-    }
     // Add predicate operands.
     TmpInst.addOperand(MCOperand::CreateImm(ARMCC::AL));
     TmpInst.addOperand(MCOperand::CreateReg(0));
     // Add 's' bit operand (always reg0 for this)
     TmpInst.addOperand(MCOperand::CreateReg(0));
-    OutStreamer.EmitInstruction(TmpInst);
+    EmitToStreamer(OutStreamer, TmpInst);
     return;
   }
   case ARM::tPICADD: {
@@ -1493,20 +1244,18 @@ void ARMAsmPrinter::EmitInstruction(const MachineInstr *MI) {
     // This adds the address of LPC0 to r0.
 
     // Emit the label.
-    OutStreamer.EmitLabel(getPICLabel(MAI->getPrivateGlobalPrefix(),
+    OutStreamer.EmitLabel(getPICLabel(DL->getPrivateGlobalPrefix(),
                           getFunctionNumber(), MI->getOperand(2).getImm(),
                           OutContext));
 
     // Form and emit the add.
-    MCInst AddInst;
-    AddInst.setOpcode(ARM::tADDhirr);
-    AddInst.addOperand(MCOperand::CreateReg(MI->getOperand(0).getReg()));
-    AddInst.addOperand(MCOperand::CreateReg(MI->getOperand(0).getReg()));
-    AddInst.addOperand(MCOperand::CreateReg(ARM::PC));
-    // Add predicate operands.
-    AddInst.addOperand(MCOperand::CreateImm(ARMCC::AL));
-    AddInst.addOperand(MCOperand::CreateReg(0));
-    OutStreamer.EmitInstruction(AddInst);
+    EmitToStreamer(OutStreamer, MCInstBuilder(ARM::tADDhirr)
+      .addReg(MI->getOperand(0).getReg())
+      .addReg(MI->getOperand(0).getReg())
+      .addReg(ARM::PC)
+      // Add predicate operands.
+      .addImm(ARMCC::AL)
+      .addReg(0));
     return;
   }
   case ARM::PICADD: {
@@ -1516,22 +1265,20 @@ void ARMAsmPrinter::EmitInstruction(const MachineInstr *MI) {
     // This adds the address of LPC0 to r0.
 
     // Emit the label.
-    OutStreamer.EmitLabel(getPICLabel(MAI->getPrivateGlobalPrefix(),
+    OutStreamer.EmitLabel(getPICLabel(DL->getPrivateGlobalPrefix(),
                           getFunctionNumber(), MI->getOperand(2).getImm(),
                           OutContext));
 
     // Form and emit the add.
-    MCInst AddInst;
-    AddInst.setOpcode(ARM::ADDrr);
-    AddInst.addOperand(MCOperand::CreateReg(MI->getOperand(0).getReg()));
-    AddInst.addOperand(MCOperand::CreateReg(ARM::PC));
-    AddInst.addOperand(MCOperand::CreateReg(MI->getOperand(1).getReg()));
-    // Add predicate operands.
-    AddInst.addOperand(MCOperand::CreateImm(MI->getOperand(3).getImm()));
-    AddInst.addOperand(MCOperand::CreateReg(MI->getOperand(4).getReg()));
-    // Add 's' bit operand (always reg0 for this)
-    AddInst.addOperand(MCOperand::CreateReg(0));
-    OutStreamer.EmitInstruction(AddInst);
+    EmitToStreamer(OutStreamer, MCInstBuilder(ARM::ADDrr)
+      .addReg(MI->getOperand(0).getReg())
+      .addReg(ARM::PC)
+      .addReg(MI->getOperand(1).getReg())
+      // Add predicate operands.
+      .addImm(MI->getOperand(3).getImm())
+      .addReg(MI->getOperand(4).getReg())
+      // Add 's' bit operand (always reg0 for this)
+      .addReg(0));
     return;
   }
   case ARM::PICSTR:
@@ -1549,7 +1296,7 @@ void ARMAsmPrinter::EmitInstruction(const MachineInstr *MI) {
     // a PC-relative address at the ldr instruction.
 
     // Emit the label.
-    OutStreamer.EmitLabel(getPICLabel(MAI->getPrivateGlobalPrefix(),
+    OutStreamer.EmitLabel(getPICLabel(DL->getPrivateGlobalPrefix(),
                           getFunctionNumber(), MI->getOperand(2).getImm(),
                           OutContext));
 
@@ -1567,16 +1314,14 @@ void ARMAsmPrinter::EmitInstruction(const MachineInstr *MI) {
     case ARM::PICLDRSB: Opcode = ARM::LDRSB; break;
     case ARM::PICLDRSH: Opcode = ARM::LDRSH; break;
     }
-    MCInst LdStInst;
-    LdStInst.setOpcode(Opcode);
-    LdStInst.addOperand(MCOperand::CreateReg(MI->getOperand(0).getReg()));
-    LdStInst.addOperand(MCOperand::CreateReg(ARM::PC));
-    LdStInst.addOperand(MCOperand::CreateReg(MI->getOperand(1).getReg()));
-    LdStInst.addOperand(MCOperand::CreateImm(0));
-    // Add predicate operands.
-    LdStInst.addOperand(MCOperand::CreateImm(MI->getOperand(3).getImm()));
-    LdStInst.addOperand(MCOperand::CreateReg(MI->getOperand(4).getReg()));
-    OutStreamer.EmitInstruction(LdStInst);
+    EmitToStreamer(OutStreamer, MCInstBuilder(Opcode)
+      .addReg(MI->getOperand(0).getReg())
+      .addReg(ARM::PC)
+      .addReg(MI->getOperand(1).getReg())
+      .addImm(0)
+      // Add predicate operands.
+      .addImm(MI->getOperand(3).getImm())
+      .addReg(MI->getOperand(4).getReg()));
 
     return;
   }
@@ -1606,29 +1351,26 @@ void ARMAsmPrinter::EmitInstruction(const MachineInstr *MI) {
   }
   case ARM::t2BR_JT: {
     // Lower and emit the instruction itself, then the jump table following it.
-    MCInst TmpInst;
-    TmpInst.setOpcode(ARM::tMOVr);
-    TmpInst.addOperand(MCOperand::CreateReg(ARM::PC));
-    TmpInst.addOperand(MCOperand::CreateReg(MI->getOperand(0).getReg()));
-    // Add predicate operands.
-    TmpInst.addOperand(MCOperand::CreateImm(ARMCC::AL));
-    TmpInst.addOperand(MCOperand::CreateReg(0));
-    OutStreamer.EmitInstruction(TmpInst);
+    EmitToStreamer(OutStreamer, MCInstBuilder(ARM::tMOVr)
+      .addReg(ARM::PC)
+      .addReg(MI->getOperand(0).getReg())
+      // Add predicate operands.
+      .addImm(ARMCC::AL)
+      .addReg(0));
+
     // Output the data for the jump table itself
     EmitJump2Table(MI);
     return;
   }
   case ARM::t2TBB_JT: {
     // Lower and emit the instruction itself, then the jump table following it.
-    MCInst TmpInst;
+    EmitToStreamer(OutStreamer, MCInstBuilder(ARM::t2TBB)
+      .addReg(ARM::PC)
+      .addReg(MI->getOperand(0).getReg())
+      // Add predicate operands.
+      .addImm(ARMCC::AL)
+      .addReg(0));
 
-    TmpInst.setOpcode(ARM::t2TBB);
-    TmpInst.addOperand(MCOperand::CreateReg(ARM::PC));
-    TmpInst.addOperand(MCOperand::CreateReg(MI->getOperand(0).getReg()));
-    // Add predicate operands.
-    TmpInst.addOperand(MCOperand::CreateImm(ARMCC::AL));
-    TmpInst.addOperand(MCOperand::CreateReg(0));
-    OutStreamer.EmitInstruction(TmpInst);
     // Output the data for the jump table itself
     EmitJump2Table(MI);
     // Make sure the next instruction is 2-byte aligned.
@@ -1637,15 +1379,13 @@ void ARMAsmPrinter::EmitInstruction(const MachineInstr *MI) {
   }
   case ARM::t2TBH_JT: {
     // Lower and emit the instruction itself, then the jump table following it.
-    MCInst TmpInst;
+    EmitToStreamer(OutStreamer, MCInstBuilder(ARM::t2TBH)
+      .addReg(ARM::PC)
+      .addReg(MI->getOperand(0).getReg())
+      // Add predicate operands.
+      .addImm(ARMCC::AL)
+      .addReg(0));
 
-    TmpInst.setOpcode(ARM::t2TBH);
-    TmpInst.addOperand(MCOperand::CreateReg(ARM::PC));
-    TmpInst.addOperand(MCOperand::CreateReg(MI->getOperand(0).getReg()));
-    // Add predicate operands.
-    TmpInst.addOperand(MCOperand::CreateImm(ARMCC::AL));
-    TmpInst.addOperand(MCOperand::CreateReg(0));
-    OutStreamer.EmitInstruction(TmpInst);
     // Output the data for the jump table itself
     EmitJump2Table(MI);
     return;
@@ -1666,7 +1406,7 @@ void ARMAsmPrinter::EmitInstruction(const MachineInstr *MI) {
     // Add 's' bit operand (always reg0 for this)
     if (Opc == ARM::MOVr)
       TmpInst.addOperand(MCOperand::CreateReg(0));
-    OutStreamer.EmitInstruction(TmpInst);
+    EmitToStreamer(OutStreamer, TmpInst);
 
     // Make sure the Thumb jump table is 4-byte aligned.
     if (Opc == ARM::tMOVr)
@@ -1696,7 +1436,7 @@ void ARMAsmPrinter::EmitInstruction(const MachineInstr *MI) {
     // Add predicate operands.
     TmpInst.addOperand(MCOperand::CreateImm(ARMCC::AL));
     TmpInst.addOperand(MCOperand::CreateReg(0));
-    OutStreamer.EmitInstruction(TmpInst);
+    EmitToStreamer(OutStreamer, TmpInst);
 
     // Output the data for the jump table itself
     EmitJumpTable(MI);
@@ -1705,17 +1445,15 @@ void ARMAsmPrinter::EmitInstruction(const MachineInstr *MI) {
   case ARM::BR_JTadd: {
     // Lower and emit the instruction itself, then the jump table following it.
     // add pc, target, idx
-    MCInst TmpInst;
-    TmpInst.setOpcode(ARM::ADDrr);
-    TmpInst.addOperand(MCOperand::CreateReg(ARM::PC));
-    TmpInst.addOperand(MCOperand::CreateReg(MI->getOperand(0).getReg()));
-    TmpInst.addOperand(MCOperand::CreateReg(MI->getOperand(1).getReg()));
-    // Add predicate operands.
-    TmpInst.addOperand(MCOperand::CreateImm(ARMCC::AL));
-    TmpInst.addOperand(MCOperand::CreateReg(0));
-    // Add 's' bit operand (always reg0 for this)
-    TmpInst.addOperand(MCOperand::CreateReg(0));
-    OutStreamer.EmitInstruction(TmpInst);
+    EmitToStreamer(OutStreamer, MCInstBuilder(ARM::ADDrr)
+      .addReg(ARM::PC)
+      .addReg(MI->getOperand(0).getReg())
+      .addReg(MI->getOperand(1).getReg())
+      // Add predicate operands.
+      .addImm(ARMCC::AL)
+      .addReg(0)
+      // Add 's' bit operand (always reg0 for this)
+      .addReg(0));
 
     // Output the data for the jump table itself
     EmitJumpTable(MI);
@@ -1724,7 +1462,7 @@ void ARMAsmPrinter::EmitInstruction(const MachineInstr *MI) {
   case ARM::TRAP: {
     // Non-Darwin binutils don't yet support the "trap" mnemonic.
     // FIXME: Remove this special case when they do.
-    if (!Subtarget->isTargetDarwin()) {
+    if (!Subtarget->isTargetMachO()) {
       //.long 0xe7ffdefe @ trap
       uint32_t Val = 0xe7ffdefeUL;
       OutStreamer.AddComment("trap");
@@ -1733,10 +1471,17 @@ void ARMAsmPrinter::EmitInstruction(const MachineInstr *MI) {
     }
     break;
   }
+  case ARM::TRAPNaCl: {
+    //.long 0xe7fedef0 @ trap
+    uint32_t Val = 0xe7fedef0UL;
+    OutStreamer.AddComment("trap");
+    OutStreamer.EmitIntValue(Val, 4);
+    return;
+  }
   case ARM::tTRAP: {
     // Non-Darwin binutils don't yet support the "trap" mnemonic.
     // FIXME: Remove this special case when they do.
-    if (!Subtarget->isTargetDarwin()) {
+    if (!Subtarget->isTargetMachO()) {
       //.short 57086 @ trap
       uint16_t Val = 0xdefe;
       OutStreamer.AddComment("trap");
@@ -1759,75 +1504,57 @@ void ARMAsmPrinter::EmitInstruction(const MachineInstr *MI) {
     unsigned SrcReg = MI->getOperand(0).getReg();
     unsigned ValReg = MI->getOperand(1).getReg();
     MCSymbol *Label = GetARMSJLJEHLabel();
-    {
-      MCInst TmpInst;
-      TmpInst.setOpcode(ARM::tMOVr);
-      TmpInst.addOperand(MCOperand::CreateReg(ValReg));
-      TmpInst.addOperand(MCOperand::CreateReg(ARM::PC));
+    OutStreamer.AddComment("eh_setjmp begin");
+    EmitToStreamer(OutStreamer, MCInstBuilder(ARM::tMOVr)
+      .addReg(ValReg)
+      .addReg(ARM::PC)
       // Predicate.
-      TmpInst.addOperand(MCOperand::CreateImm(ARMCC::AL));
-      TmpInst.addOperand(MCOperand::CreateReg(0));
-      OutStreamer.AddComment("eh_setjmp begin");
-      OutStreamer.EmitInstruction(TmpInst);
-    }
-    {
-      MCInst TmpInst;
-      TmpInst.setOpcode(ARM::tADDi3);
-      TmpInst.addOperand(MCOperand::CreateReg(ValReg));
+      .addImm(ARMCC::AL)
+      .addReg(0));
+
+    EmitToStreamer(OutStreamer, MCInstBuilder(ARM::tADDi3)
+      .addReg(ValReg)
       // 's' bit operand
-      TmpInst.addOperand(MCOperand::CreateReg(ARM::CPSR));
-      TmpInst.addOperand(MCOperand::CreateReg(ValReg));
-      TmpInst.addOperand(MCOperand::CreateImm(7));
+      .addReg(ARM::CPSR)
+      .addReg(ValReg)
+      .addImm(7)
       // Predicate.
-      TmpInst.addOperand(MCOperand::CreateImm(ARMCC::AL));
-      TmpInst.addOperand(MCOperand::CreateReg(0));
-      OutStreamer.EmitInstruction(TmpInst);
-    }
-    {
-      MCInst TmpInst;
-      TmpInst.setOpcode(ARM::tSTRi);
-      TmpInst.addOperand(MCOperand::CreateReg(ValReg));
-      TmpInst.addOperand(MCOperand::CreateReg(SrcReg));
+      .addImm(ARMCC::AL)
+      .addReg(0));
+
+    EmitToStreamer(OutStreamer, MCInstBuilder(ARM::tSTRi)
+      .addReg(ValReg)
+      .addReg(SrcReg)
       // The offset immediate is #4. The operand value is scaled by 4 for the
       // tSTR instruction.
-      TmpInst.addOperand(MCOperand::CreateImm(1));
+      .addImm(1)
       // Predicate.
-      TmpInst.addOperand(MCOperand::CreateImm(ARMCC::AL));
-      TmpInst.addOperand(MCOperand::CreateReg(0));
-      OutStreamer.EmitInstruction(TmpInst);
-    }
-    {
-      MCInst TmpInst;
-      TmpInst.setOpcode(ARM::tMOVi8);
-      TmpInst.addOperand(MCOperand::CreateReg(ARM::R0));
-      TmpInst.addOperand(MCOperand::CreateReg(ARM::CPSR));
-      TmpInst.addOperand(MCOperand::CreateImm(0));
+      .addImm(ARMCC::AL)
+      .addReg(0));
+
+    EmitToStreamer(OutStreamer, MCInstBuilder(ARM::tMOVi8)
+      .addReg(ARM::R0)
+      .addReg(ARM::CPSR)
+      .addImm(0)
       // Predicate.
-      TmpInst.addOperand(MCOperand::CreateImm(ARMCC::AL));
-      TmpInst.addOperand(MCOperand::CreateReg(0));
-      OutStreamer.EmitInstruction(TmpInst);
-    }
-    {
-      const MCExpr *SymbolExpr = MCSymbolRefExpr::Create(Label, OutContext);
-      MCInst TmpInst;
-      TmpInst.setOpcode(ARM::tB);
-      TmpInst.addOperand(MCOperand::CreateExpr(SymbolExpr));
-      TmpInst.addOperand(MCOperand::CreateImm(ARMCC::AL));
-      TmpInst.addOperand(MCOperand::CreateReg(0));
-      OutStreamer.EmitInstruction(TmpInst);
-    }
-    {
-      MCInst TmpInst;
-      TmpInst.setOpcode(ARM::tMOVi8);
-      TmpInst.addOperand(MCOperand::CreateReg(ARM::R0));
-      TmpInst.addOperand(MCOperand::CreateReg(ARM::CPSR));
-      TmpInst.addOperand(MCOperand::CreateImm(1));
+      .addImm(ARMCC::AL)
+      .addReg(0));
+
+    const MCExpr *SymbolExpr = MCSymbolRefExpr::Create(Label, OutContext);
+    EmitToStreamer(OutStreamer, MCInstBuilder(ARM::tB)
+      .addExpr(SymbolExpr)
+      .addImm(ARMCC::AL)
+      .addReg(0));
+
+    OutStreamer.AddComment("eh_setjmp end");
+    EmitToStreamer(OutStreamer, MCInstBuilder(ARM::tMOVi8)
+      .addReg(ARM::R0)
+      .addReg(ARM::CPSR)
+      .addImm(1)
       // Predicate.
-      TmpInst.addOperand(MCOperand::CreateImm(ARMCC::AL));
-      TmpInst.addOperand(MCOperand::CreateReg(0));
-      OutStreamer.AddComment("eh_setjmp end");
-      OutStreamer.EmitInstruction(TmpInst);
-    }
+      .addImm(ARMCC::AL)
+      .addReg(0));
+
     OutStreamer.EmitLabel(Label);
     return;
   }
@@ -1843,69 +1570,53 @@ void ARMAsmPrinter::EmitInstruction(const MachineInstr *MI) {
     unsigned SrcReg = MI->getOperand(0).getReg();
     unsigned ValReg = MI->getOperand(1).getReg();
 
-    {
-      MCInst TmpInst;
-      TmpInst.setOpcode(ARM::ADDri);
-      TmpInst.addOperand(MCOperand::CreateReg(ValReg));
-      TmpInst.addOperand(MCOperand::CreateReg(ARM::PC));
-      TmpInst.addOperand(MCOperand::CreateImm(8));
+    OutStreamer.AddComment("eh_setjmp begin");
+    EmitToStreamer(OutStreamer, MCInstBuilder(ARM::ADDri)
+      .addReg(ValReg)
+      .addReg(ARM::PC)
+      .addImm(8)
       // Predicate.
-      TmpInst.addOperand(MCOperand::CreateImm(ARMCC::AL));
-      TmpInst.addOperand(MCOperand::CreateReg(0));
+      .addImm(ARMCC::AL)
+      .addReg(0)
       // 's' bit operand (always reg0 for this).
-      TmpInst.addOperand(MCOperand::CreateReg(0));
-      OutStreamer.AddComment("eh_setjmp begin");
-      OutStreamer.EmitInstruction(TmpInst);
-    }
-    {
-      MCInst TmpInst;
-      TmpInst.setOpcode(ARM::STRi12);
-      TmpInst.addOperand(MCOperand::CreateReg(ValReg));
-      TmpInst.addOperand(MCOperand::CreateReg(SrcReg));
-      TmpInst.addOperand(MCOperand::CreateImm(4));
+      .addReg(0));
+
+    EmitToStreamer(OutStreamer, MCInstBuilder(ARM::STRi12)
+      .addReg(ValReg)
+      .addReg(SrcReg)
+      .addImm(4)
       // Predicate.
-      TmpInst.addOperand(MCOperand::CreateImm(ARMCC::AL));
-      TmpInst.addOperand(MCOperand::CreateReg(0));
-      OutStreamer.EmitInstruction(TmpInst);
-    }
-    {
-      MCInst TmpInst;
-      TmpInst.setOpcode(ARM::MOVi);
-      TmpInst.addOperand(MCOperand::CreateReg(ARM::R0));
-      TmpInst.addOperand(MCOperand::CreateImm(0));
+      .addImm(ARMCC::AL)
+      .addReg(0));
+
+    EmitToStreamer(OutStreamer, MCInstBuilder(ARM::MOVi)
+      .addReg(ARM::R0)
+      .addImm(0)
       // Predicate.
-      TmpInst.addOperand(MCOperand::CreateImm(ARMCC::AL));
-      TmpInst.addOperand(MCOperand::CreateReg(0));
+      .addImm(ARMCC::AL)
+      .addReg(0)
       // 's' bit operand (always reg0 for this).
-      TmpInst.addOperand(MCOperand::CreateReg(0));
-      OutStreamer.EmitInstruction(TmpInst);
-    }
-    {
-      MCInst TmpInst;
-      TmpInst.setOpcode(ARM::ADDri);
-      TmpInst.addOperand(MCOperand::CreateReg(ARM::PC));
-      TmpInst.addOperand(MCOperand::CreateReg(ARM::PC));
-      TmpInst.addOperand(MCOperand::CreateImm(0));
+      .addReg(0));
+
+    EmitToStreamer(OutStreamer, MCInstBuilder(ARM::ADDri)
+      .addReg(ARM::PC)
+      .addReg(ARM::PC)
+      .addImm(0)
       // Predicate.
-      TmpInst.addOperand(MCOperand::CreateImm(ARMCC::AL));
-      TmpInst.addOperand(MCOperand::CreateReg(0));
+      .addImm(ARMCC::AL)
+      .addReg(0)
       // 's' bit operand (always reg0 for this).
-      TmpInst.addOperand(MCOperand::CreateReg(0));
-      OutStreamer.EmitInstruction(TmpInst);
-    }
-    {
-      MCInst TmpInst;
-      TmpInst.setOpcode(ARM::MOVi);
-      TmpInst.addOperand(MCOperand::CreateReg(ARM::R0));
-      TmpInst.addOperand(MCOperand::CreateImm(1));
+      .addReg(0));
+
+    OutStreamer.AddComment("eh_setjmp end");
+    EmitToStreamer(OutStreamer, MCInstBuilder(ARM::MOVi)
+      .addReg(ARM::R0)
+      .addImm(1)
       // Predicate.
-      TmpInst.addOperand(MCOperand::CreateImm(ARMCC::AL));
-      TmpInst.addOperand(MCOperand::CreateReg(0));
+      .addImm(ARMCC::AL)
+      .addReg(0)
       // 's' bit operand (always reg0 for this).
-      TmpInst.addOperand(MCOperand::CreateReg(0));
-      OutStreamer.AddComment("eh_setjmp end");
-      OutStreamer.EmitInstruction(TmpInst);
-    }
+      .addReg(0));
     return;
   }
   case ARM::Int_eh_sjlj_longjmp: {
@@ -1915,48 +1626,35 @@ void ARMAsmPrinter::EmitInstruction(const MachineInstr *MI) {
     // bx $scratch
     unsigned SrcReg = MI->getOperand(0).getReg();
     unsigned ScratchReg = MI->getOperand(1).getReg();
-    {
-      MCInst TmpInst;
-      TmpInst.setOpcode(ARM::LDRi12);
-      TmpInst.addOperand(MCOperand::CreateReg(ARM::SP));
-      TmpInst.addOperand(MCOperand::CreateReg(SrcReg));
-      TmpInst.addOperand(MCOperand::CreateImm(8));
+    EmitToStreamer(OutStreamer, MCInstBuilder(ARM::LDRi12)
+      .addReg(ARM::SP)
+      .addReg(SrcReg)
+      .addImm(8)
       // Predicate.
-      TmpInst.addOperand(MCOperand::CreateImm(ARMCC::AL));
-      TmpInst.addOperand(MCOperand::CreateReg(0));
-      OutStreamer.EmitInstruction(TmpInst);
-    }
-    {
-      MCInst TmpInst;
-      TmpInst.setOpcode(ARM::LDRi12);
-      TmpInst.addOperand(MCOperand::CreateReg(ScratchReg));
-      TmpInst.addOperand(MCOperand::CreateReg(SrcReg));
-      TmpInst.addOperand(MCOperand::CreateImm(4));
+      .addImm(ARMCC::AL)
+      .addReg(0));
+
+    EmitToStreamer(OutStreamer, MCInstBuilder(ARM::LDRi12)
+      .addReg(ScratchReg)
+      .addReg(SrcReg)
+      .addImm(4)
       // Predicate.
-      TmpInst.addOperand(MCOperand::CreateImm(ARMCC::AL));
-      TmpInst.addOperand(MCOperand::CreateReg(0));
-      OutStreamer.EmitInstruction(TmpInst);
-    }
-    {
-      MCInst TmpInst;
-      TmpInst.setOpcode(ARM::LDRi12);
-      TmpInst.addOperand(MCOperand::CreateReg(ARM::R7));
-      TmpInst.addOperand(MCOperand::CreateReg(SrcReg));
-      TmpInst.addOperand(MCOperand::CreateImm(0));
+      .addImm(ARMCC::AL)
+      .addReg(0));
+
+    EmitToStreamer(OutStreamer, MCInstBuilder(ARM::LDRi12)
+      .addReg(ARM::R7)
+      .addReg(SrcReg)
+      .addImm(0)
       // Predicate.
-      TmpInst.addOperand(MCOperand::CreateImm(ARMCC::AL));
-      TmpInst.addOperand(MCOperand::CreateReg(0));
-      OutStreamer.EmitInstruction(TmpInst);
-    }
-    {
-      MCInst TmpInst;
-      TmpInst.setOpcode(ARM::BX);
-      TmpInst.addOperand(MCOperand::CreateReg(ScratchReg));
+      .addImm(ARMCC::AL)
+      .addReg(0));
+
+    EmitToStreamer(OutStreamer, MCInstBuilder(ARM::BX)
+      .addReg(ScratchReg)
       // Predicate.
-      TmpInst.addOperand(MCOperand::CreateImm(ARMCC::AL));
-      TmpInst.addOperand(MCOperand::CreateReg(0));
-      OutStreamer.EmitInstruction(TmpInst);
-    }
+      .addImm(ARMCC::AL)
+      .addReg(0));
     return;
   }
   case ARM::tInt_eh_sjlj_longjmp: {
@@ -1967,60 +1665,44 @@ void ARMAsmPrinter::EmitInstruction(const MachineInstr *MI) {
     // bx $scratch
     unsigned SrcReg = MI->getOperand(0).getReg();
     unsigned ScratchReg = MI->getOperand(1).getReg();
-    {
-      MCInst TmpInst;
-      TmpInst.setOpcode(ARM::tLDRi);
-      TmpInst.addOperand(MCOperand::CreateReg(ScratchReg));
-      TmpInst.addOperand(MCOperand::CreateReg(SrcReg));
+    EmitToStreamer(OutStreamer, MCInstBuilder(ARM::tLDRi)
+      .addReg(ScratchReg)
+      .addReg(SrcReg)
       // The offset immediate is #8. The operand value is scaled by 4 for the
       // tLDR instruction.
-      TmpInst.addOperand(MCOperand::CreateImm(2));
+      .addImm(2)
       // Predicate.
-      TmpInst.addOperand(MCOperand::CreateImm(ARMCC::AL));
-      TmpInst.addOperand(MCOperand::CreateReg(0));
-      OutStreamer.EmitInstruction(TmpInst);
-    }
-    {
-      MCInst TmpInst;
-      TmpInst.setOpcode(ARM::tMOVr);
-      TmpInst.addOperand(MCOperand::CreateReg(ARM::SP));
-      TmpInst.addOperand(MCOperand::CreateReg(ScratchReg));
+      .addImm(ARMCC::AL)
+      .addReg(0));
+
+    EmitToStreamer(OutStreamer, MCInstBuilder(ARM::tMOVr)
+      .addReg(ARM::SP)
+      .addReg(ScratchReg)
       // Predicate.
-      TmpInst.addOperand(MCOperand::CreateImm(ARMCC::AL));
-      TmpInst.addOperand(MCOperand::CreateReg(0));
-      OutStreamer.EmitInstruction(TmpInst);
-    }
-    {
-      MCInst TmpInst;
-      TmpInst.setOpcode(ARM::tLDRi);
-      TmpInst.addOperand(MCOperand::CreateReg(ScratchReg));
-      TmpInst.addOperand(MCOperand::CreateReg(SrcReg));
-      TmpInst.addOperand(MCOperand::CreateImm(1));
+      .addImm(ARMCC::AL)
+      .addReg(0));
+
+    EmitToStreamer(OutStreamer, MCInstBuilder(ARM::tLDRi)
+      .addReg(ScratchReg)
+      .addReg(SrcReg)
+      .addImm(1)
       // Predicate.
-      TmpInst.addOperand(MCOperand::CreateImm(ARMCC::AL));
-      TmpInst.addOperand(MCOperand::CreateReg(0));
-      OutStreamer.EmitInstruction(TmpInst);
-    }
-    {
-      MCInst TmpInst;
-      TmpInst.setOpcode(ARM::tLDRi);
-      TmpInst.addOperand(MCOperand::CreateReg(ARM::R7));
-      TmpInst.addOperand(MCOperand::CreateReg(SrcReg));
-      TmpInst.addOperand(MCOperand::CreateImm(0));
+      .addImm(ARMCC::AL)
+      .addReg(0));
+
+    EmitToStreamer(OutStreamer, MCInstBuilder(ARM::tLDRi)
+      .addReg(ARM::R7)
+      .addReg(SrcReg)
+      .addImm(0)
       // Predicate.
-      TmpInst.addOperand(MCOperand::CreateImm(ARMCC::AL));
-      TmpInst.addOperand(MCOperand::CreateReg(0));
-      OutStreamer.EmitInstruction(TmpInst);
-    }
-    {
-      MCInst TmpInst;
-      TmpInst.setOpcode(ARM::tBX);
-      TmpInst.addOperand(MCOperand::CreateReg(ScratchReg));
+      .addImm(ARMCC::AL)
+      .addReg(0));
+
+    EmitToStreamer(OutStreamer, MCInstBuilder(ARM::tBX)
+      .addReg(ScratchReg)
       // Predicate.
-      TmpInst.addOperand(MCOperand::CreateImm(ARMCC::AL));
-      TmpInst.addOperand(MCOperand::CreateReg(0));
-      OutStreamer.EmitInstruction(TmpInst);
-    }
+      .addImm(ARMCC::AL)
+      .addReg(0));
     return;
   }
   }
@@ -2028,7 +1710,7 @@ void ARMAsmPrinter::EmitInstruction(const MachineInstr *MI) {
   MCInst TmpInst;
   LowerARMMachineInstrToMCInst(MI, TmpInst, *this);
 
-  OutStreamer.EmitInstruction(TmpInst);
+  EmitToStreamer(OutStreamer, TmpInst);
 }
 
 //===----------------------------------------------------------------------===//