]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/blobdiff - lib/Target/PowerPC/PPCISelLowering.h
[PowerPC] Mark zext of a small scalar load as free
[opencl/llvm.git] / lib / Target / PowerPC / PPCISelLowering.h
index 080ef5d0f76fd77e30496bb30c5565e6b20fe26f..db5a3e42d52fbfae055e1a204d47309fe73bc132 100644 (file)
 //
 //===----------------------------------------------------------------------===//
 
-#ifndef LLVM_TARGET_POWERPC_PPC32ISELLOWERING_H
-#define LLVM_TARGET_POWERPC_PPC32ISELLOWERING_H
+#ifndef LLVM_LIB_TARGET_POWERPC_PPCISELLOWERING_H
+#define LLVM_LIB_TARGET_POWERPC_PPCISELLOWERING_H
 
 #include "PPC.h"
 #include "PPCInstrInfo.h"
 #include "PPCRegisterInfo.h"
-#include "PPCSubtarget.h"
 #include "llvm/CodeGen/CallingConvLower.h"
 #include "llvm/CodeGen/SelectionDAG.h"
 #include "llvm/Target/TargetLowering.h"
@@ -62,6 +61,9 @@ namespace llvm {
       ///
       VPERM,
 
+      /// The CMPB instruction (takes two operands of i32 or i64).
+      CMPB,
+
       /// Hi/Lo - These represent the high and low 16-bit parts of a global
       /// address respectively.  These nodes have two operands, the first of
       /// which must be a TargetGlobalAddress, and the second of which must be a
@@ -71,19 +73,14 @@ namespace llvm {
 
       TOC_ENTRY,
 
-      /// The following three target-specific nodes are used for calls through
+      /// The following two target-specific nodes are used for calls through
       /// function pointers in the 64-bit SVR4 ABI.
 
-      /// Restore the TOC from the TOC save area of the current stack frame.
-      /// This is basically a hard coded load instruction which additionally
-      /// takes/produces a flag.
-      TOC_RESTORE,
-
       /// Like a regular LOAD but additionally taking/producing a flag.
       LOAD,
 
-      /// LOAD into r2 (also taking/producing a flag). Like TOC_RESTORE, this is
-      /// a hard coded load instruction.
+      /// Like LOAD (taking/producing a flag), but using r2 as hard-coded
+      /// destination.
       LOAD_TOC,
 
       /// OPRC, CHAIN = DYNALLOC(CHAIN, NEGSIZE, FRAME_INDEX)
@@ -100,11 +97,21 @@ namespace llvm {
       /// code.
       SRL, SRA, SHL,
 
+      /// The combination of sra[wd]i and addze used to implemented signed
+      /// integer division by a power of 2. The first operand is the dividend,
+      /// and the second is the constant shift amount (representing the
+      /// divisor).
+      SRA_ADDZE,
+
       /// CALL - A direct function call.
       /// CALL_NOP is a call with the special NOP which follows 64-bit
       /// SVR4 calls.
       CALL, CALL_NOP,
 
+      /// CALL_TLS and CALL_NOP_TLS - Versions of CALL and CALL_NOP used
+      /// to access TLS variables.
+      CALL_TLS, CALL_NOP_TLS,
+
       /// CHAIN,FLAG = MTCTR(VAL, CHAIN[, INFLAG]) - Directly corresponds to a
       /// MTCTR instruction.
       MTCTR,
@@ -113,6 +120,10 @@ namespace llvm {
       /// BCTRL instruction.
       BCTRL,
 
+      /// CHAIN,FLAG = BCTRL(CHAIN, ADDR, INFLAG) - The combination of a bctrl
+      /// instruction and the TOC reload required on SVR4 PPC64.
+      BCTRL_LOAD_TOC,
+
       /// Return with a flag operand, matched by 'blr'
       RET_FLAG,
 
@@ -127,6 +138,10 @@ namespace llvm {
       /// implement truncation of i32 or i64 to i1.
       ANDIo_1_EQ_BIT, ANDIo_1_GT_BIT,
 
+      // READ_TIME_BASE - A read of the 64-bit time-base register on a 32-bit
+      // target (returns (Lo, Hi)). It takes a chain operand.
+      READ_TIME_BASE,
+
       // EH_SJLJ_SETJMP - SjLj exception handling setjmp.
       EH_SJLJ_SETJMP,
 
@@ -187,6 +202,10 @@ namespace llvm {
       /// on PPC32.
       PPC32_GOT,
 
+      /// GPRC = address of _GLOBAL_OFFSET_TABLE_. Used by general dynamic and
+      /// local dynamic TLS  on PPC32.
+      PPC32_PICGOT,
+
       /// G8RC = ADDIS_GOT_TPREL_HA %X2, Symbol - Used by the initial-exec
       /// TLS model, produces an ADDIS8 instruction that adds the GOT
       /// base to sym\@got\@tprel\@ha.
@@ -216,10 +235,6 @@ namespace llvm {
       /// sym\@got\@tlsgd\@l.
       ADDI_TLSGD_L,
 
-      /// G8RC = GET_TLS_ADDR %X3, Symbol - For the general-dynamic TLS
-      /// model, produces a call to __tls_get_addr(sym\@tlsgd).
-      GET_TLS_ADDR,
-
       /// G8RC = ADDIS_TLSLD_HA %X2, Symbol - For the local-dynamic TLS
       /// model, produces an ADDIS8 instruction that adds the GOT base
       /// register to sym\@got\@tlsld\@ha.
@@ -230,10 +245,6 @@ namespace llvm {
       /// sym\@got\@tlsld\@l.
       ADDI_TLSLD_L,
 
-      /// G8RC = GET_TLSLD_ADDR %X3, Symbol - For the local-dynamic TLS
-      /// model, produces a call to __tls_get_addr(sym\@tlsld).
-      GET_TLSLD_ADDR,
-
       /// G8RC = ADDIS_DTPREL_HA %X3, Symbol, Chain - For the
       /// local-dynamic TLS model, produces an ADDIS8 instruction
       /// that adds X3 to sym\@dtprel\@ha. The Chain operand is needed
@@ -256,6 +267,13 @@ namespace llvm {
       /// operand identifies the operating system entry point.
       SC,
 
+      /// VSRC, CHAIN = XXSWAPD CHAIN, VSRC - Occurs only for little
+      /// endian.  Maps to an xxswapd instruction that corrects an lxvd2x
+      /// or stxvd2x instruction.  The chain is necessary because the
+      /// sequence replaces a load and needs to provide the same number
+      /// of outputs.
+      XXSWAPD,
+
       /// CHAIN = STBRX CHAIN, GPRC, Ptr, Type - This is a
       /// byte-swapping store instruction.  It byte-swaps the low "Type" bits of
       /// the GPRC input, then stores it through Ptr.  Type can be either i16 or
@@ -295,7 +313,17 @@ namespace llvm {
       /// G8RC = ADDI_TOC_L G8RReg, Symbol - For medium code model, produces
       /// an ADDI8 instruction that adds G8RReg to sym\@toc\@l.
       /// Preceded by an ADDIS_TOC_HA to form a full 32-bit offset.
-      ADDI_TOC_L
+      ADDI_TOC_L,
+
+      /// VSRC, CHAIN = LXVD2X_LE CHAIN, Ptr - Occurs only for little endian.
+      /// Maps directly to an lxvd2x instruction that will be followed by
+      /// an xxswapd.
+      LXVD2X,
+
+      /// CHAIN = STXVD2X CHAIN, VSRC, Ptr - Occurs only for little endian.
+      /// Maps directly to an stxvd2x instruction that will be preceded by
+      /// an xxswapd.
+      STXVD2X
     };
   }
 
@@ -303,25 +331,28 @@ namespace llvm {
   namespace PPC {
     /// isVPKUHUMShuffleMask - Return true if this is the shuffle mask for a
     /// VPKUHUM instruction.
-    bool isVPKUHUMShuffleMask(ShuffleVectorSDNode *N, bool isUnary);
+    bool isVPKUHUMShuffleMask(ShuffleVectorSDNode *N, unsigned ShuffleKind,
+                              SelectionDAG &DAG);
 
     /// isVPKUWUMShuffleMask - Return true if this is the shuffle mask for a
     /// VPKUWUM instruction.
-    bool isVPKUWUMShuffleMask(ShuffleVectorSDNode *N, bool isUnary);
+    bool isVPKUWUMShuffleMask(ShuffleVectorSDNode *N, unsigned ShuffleKind,
+                              SelectionDAG &DAG);
 
     /// isVMRGLShuffleMask - Return true if this is a shuffle mask suitable for
     /// a VRGL* instruction with the specified unit size (1,2 or 4 bytes).
     bool isVMRGLShuffleMask(ShuffleVectorSDNode *N, unsigned UnitSize,
-                            bool isUnary);
+                            unsigned ShuffleKind, SelectionDAG &DAG);
 
     /// isVMRGHShuffleMask - Return true if this is a shuffle mask suitable for
     /// a VRGH* instruction with the specified unit size (1,2 or 4 bytes).
     bool isVMRGHShuffleMask(ShuffleVectorSDNode *N, unsigned UnitSize,
-                            bool isUnary);
+                            unsigned ShuffleKind, SelectionDAG &DAG);
 
-    /// isVSLDOIShuffleMask - If this is a vsldoi shuffle mask, return the shift
-    /// amount, otherwise return -1.
-    int isVSLDOIShuffleMask(SDNode *N, bool isUnary);
+    /// isVSLDOIShuffleMask - If this is a vsldoi shuffle mask, return the
+    /// shift amount, otherwise return -1.
+    int isVSLDOIShuffleMask(SDNode *N, unsigned ShuffleKind,
+                            SelectionDAG &DAG);
 
     /// isSplatShuffleMask - Return true if the specified VECTOR_SHUFFLE operand
     /// specifies a splat of a single element that is suitable for input to
@@ -334,7 +365,7 @@ namespace llvm {
 
     /// getVSPLTImmediate - Return the appropriate VSPLT* immediate to splat the
     /// specified isSplatShuffleMask VECTOR_SHUFFLE mask.
-    unsigned getVSPLTImmediate(SDNode *N, unsigned EltSize);
+    unsigned getVSPLTImmediate(SDNode *N, unsigned EltSize, SelectionDAG &DAG);
 
     /// get_VSPLTI_elt - If this is a build_vector of constants which can be
     /// formed by using a vspltis[bhw] instruction of the specified element
@@ -343,11 +374,12 @@ namespace llvm {
     SDValue get_VSPLTI_elt(SDNode *N, unsigned ByteSize, SelectionDAG &DAG);
   }
 
+  class PPCSubtarget;
   class PPCTargetLowering : public TargetLowering {
-    const PPCSubtarget &PPCSubTarget;
+    const PPCSubtarget &Subtarget;
 
   public:
-    explicit PPCTargetLowering(PPCTargetMachine &TM);
+    explicit PPCTargetLowering(const PPCTargetMachine &TM);
 
     /// getTargetNodeName() - This method returns the name of a target specific
     /// DAG node.
@@ -355,9 +387,22 @@ namespace llvm {
 
     MVT getScalarShiftAmountTy(EVT LHSTy) const override { return MVT::i32; }
 
+    bool isCheapToSpeculateCttz() const override {
+      return true;
+    }
+
+    bool isCheapToSpeculateCtlz() const override {
+      return true;
+    }
+
     /// getSetCCResultType - Return the ISD::SETCC ValueType
     EVT getSetCCResultType(LLVMContext &Context, EVT VT) const override;
 
+    /// Return true if target always beneficiates from combining into FMA for a
+    /// given value type. This must typically return false on targets where FMA
+    /// takes more cycles to execute than FADD.
+    bool enableAggressiveFMAFusion(EVT VT) const override;
+
     /// getPreIndexedAddressParts - returns true by value, base pointer and
     /// offset pointer and addressing mode by reference if the node's address
     /// can be legally represented as pre-indexed load / store address.
@@ -396,8 +441,14 @@ namespace llvm {
     void ReplaceNodeResults(SDNode *N, SmallVectorImpl<SDValue>&Results,
                             SelectionDAG &DAG) const override;
 
+    SDValue expandVSXLoadForLE(SDNode *N, DAGCombinerInfo &DCI) const;
+    SDValue expandVSXStoreForLE(SDNode *N, DAGCombinerInfo &DCI) const;
+
     SDValue PerformDAGCombine(SDNode *N, DAGCombinerInfo &DCI) const override;
 
+    SDValue BuildSDIVPow2(SDNode *N, const APInt &Divisor, SelectionDAG &DAG,
+                          std::vector<SDNode *> *Created) const override;
+
     unsigned getRegisterByName(const char* RegName, EVT VT) const override;
 
     void computeKnownBitsForTargetNode(const SDValue Op,
@@ -406,6 +457,13 @@ namespace llvm {
                                        const SelectionDAG &DAG,
                                        unsigned Depth = 0) const override;
 
+    unsigned getPrefLoopAlignment(MachineLoop *ML) const override;
+
+    Instruction* emitLeadingFence(IRBuilder<> &Builder, AtomicOrdering Ord,
+                                  bool IsStore, bool IsLoad) const override;
+    Instruction* emitTrailingFence(IRBuilder<> &Builder, AtomicOrdering Ord,
+                                   bool IsStore, bool IsLoad) const override;
+
     MachineBasicBlock *
       EmitInstrWithCustomInserter(MachineInstr *MI,
                                   MachineBasicBlock *MBB) const override;
@@ -468,6 +526,8 @@ namespace llvm {
     bool isTruncateFree(Type *Ty1, Type *Ty2) const override;
     bool isTruncateFree(EVT VT1, EVT VT2) const override;
 
+    bool isZExtFree(SDValue Val, EVT VT2) const override;
+
     /// \brief Returns true if it is beneficial to convert a load of a constant
     /// to just the constant itself.
     bool shouldConvertConstantLoadToIntImm(const APInt &Imm,
@@ -475,6 +535,10 @@ namespace llvm {
 
     bool isOffsetFoldingLegal(const GlobalAddressSDNode *GA) const override;
 
+    bool getTgtMemIntrinsic(IntrinsicInfo &Info,
+                            const CallInst &I,
+                            unsigned Intrinsic) const override;
+
     /// getOptimalMemOpType - Returns the target specific optimal type for load
     /// and store operations as a result of memset, memcpy, and memmove
     /// lowering. If DstAlign is zero that means it's safe to destination
@@ -493,9 +557,10 @@ namespace llvm {
 
     /// Is unaligned memory access allowed for the given type, and is it fast
     /// relative to software emulation.
-    bool allowsUnalignedMemoryAccesses(EVT VT,
-                                       unsigned AddrSpace,
-                                       bool *Fast = nullptr) const override;
+    bool allowsMisalignedMemoryAccesses(EVT VT,
+                                        unsigned AddrSpace,
+                                        unsigned Align = 1,
+                                        bool *Fast = nullptr) const override;
 
     /// isFMAFasterThanFMulAndFAdd - Return true if an FMA operation is faster
     /// than a pair of fmul and fadd instructions. fmuladd intrinsics will be
@@ -513,7 +578,44 @@ namespace llvm {
     FastISel *createFastISel(FunctionLoweringInfo &FuncInfo,
                              const TargetLibraryInfo *LibInfo) const override;
 
+    /// \brief Returns true if an argument of type Ty needs to be passed in a
+    /// contiguous block of registers in calling convention CallConv.
+    bool functionArgumentNeedsConsecutiveRegisters(
+      Type *Ty, CallingConv::ID CallConv, bool isVarArg) const override {
+      // We support any array type as "consecutive" block in the parameter
+      // save area.  The element type defines the alignment requirement and
+      // whether the argument should go in GPRs, FPRs, or VRs if available.
+      //
+      // Note that clang uses this capability both to implement the ELFv2
+      // homogeneous float/vector aggregate ABI, and to avoid having to use
+      // "byval" when passing aggregates that might fully fit in registers.
+      return Ty->isArrayTy();
+    }
+
   private:
+
+    struct ReuseLoadInfo {
+      SDValue Ptr;
+      SDValue Chain;
+      SDValue ResChain;
+      MachinePointerInfo MPI;
+      bool IsInvariant;
+      unsigned Alignment;
+      AAMDNodes AAInfo;
+      const MDNode *Ranges;
+
+      ReuseLoadInfo() : IsInvariant(false), Alignment(0), Ranges(nullptr) {}
+    };
+
+    bool canReuseLoadAddress(SDValue Op, EVT MemVT, ReuseLoadInfo &RLI,
+                             SelectionDAG &DAG,
+                             ISD::LoadExtType ET = ISD::NON_EXTLOAD) const;
+    void spliceIntoChain(SDValue ResChain, SDValue NewResChain,
+                         SelectionDAG &DAG) const;
+
+    void LowerFP_TO_INTForReuse(SDValue Op, ReuseLoadInfo &RLI,
+                                SelectionDAG &DAG, SDLoc dl) const;
+
     SDValue getFramePointerFrameIndex(SelectionDAG & DAG) const;
     SDValue getReturnAddrFrameIndex(SelectionDAG & DAG) const;
 
@@ -536,6 +638,8 @@ namespace llvm {
     SDValue LowerFRAMEADDR(SDValue Op, SelectionDAG &DAG) const;
     SDValue LowerConstantPool(SDValue Op, SelectionDAG &DAG) const;
     SDValue LowerBlockAddress(SDValue Op, SelectionDAG &DAG) const;
+    std::pair<SDValue,SDValue> lowerTLSCall(SDValue Op, SDLoc dl,
+                                            SelectionDAG &DAG) const;
     SDValue LowerGlobalTLSAddress(SDValue Op, SelectionDAG &DAG) const;
     SDValue LowerGlobalAddress(SDValue Op, SelectionDAG &DAG) const;
     SDValue LowerJumpTable(SDValue Op, SelectionDAG &DAG) const;
@@ -613,11 +717,6 @@ namespace llvm {
       extendArgForPPC64(ISD::ArgFlagsTy Flags, EVT ObjectVT, SelectionDAG &DAG,
                         SDValue ArgVal, SDLoc dl) const;
 
-    void
-      setMinReservedArea(MachineFunction &MF, SelectionDAG &DAG,
-                         unsigned nAltivecParamsAtEnd,
-                         unsigned MinReservedArea, bool isPPC64) const;
-
     SDValue
       LowerFormalArguments_Darwin(SDValue Chain,
                                   CallingConv::ID CallConv, bool isVarArg,
@@ -674,8 +773,14 @@ namespace llvm {
 
     SDValue DAGCombineExtBoolTrunc(SDNode *N, DAGCombinerInfo &DCI) const;
     SDValue DAGCombineTruncBoolExt(SDNode *N, DAGCombinerInfo &DCI) const;
-    SDValue DAGCombineFastRecip(SDValue Op, DAGCombinerInfo &DCI) const;
-    SDValue DAGCombineFastRecipFSQRT(SDValue Op, DAGCombinerInfo &DCI) const;
+    SDValue combineFPToIntToFP(SDNode *N, DAGCombinerInfo &DCI) const;
+
+    SDValue getRsqrtEstimate(SDValue Operand, DAGCombinerInfo &DCI,
+                             unsigned &RefinementSteps,
+                             bool &UseOneConstNR) const override;
+    SDValue getRecipEstimate(SDValue Operand, DAGCombinerInfo &DCI,
+                             unsigned &RefinementSteps) const override;
+    bool combineRepeatedFPDivisors(unsigned NumUsers) const override;
 
     CCAssignFn *useFastISelCCs(unsigned Flag) const;
   };