index 6296400ec719afcf9dc640c39f6f9b3918595b2a..db5a3e42d52fbfae055e1a204d47309fe73bc132 100644 (file)
//
//===----------------------------------------------------------------------===//
-#ifndef LLVM_TARGET_POWERPC_PPC32ISELLOWERING_H
-#define LLVM_TARGET_POWERPC_PPC32ISELLOWERING_H
+#ifndef LLVM_LIB_TARGET_POWERPC_PPCISELLOWERING_H
+#define LLVM_LIB_TARGET_POWERPC_PPCISELLOWERING_H
#include "PPC.h"
+#include "PPCInstrInfo.h"
#include "PPCRegisterInfo.h"
-#include "PPCSubtarget.h"
+#include "llvm/CodeGen/CallingConvLower.h"
#include "llvm/CodeGen/SelectionDAG.h"
#include "llvm/Target/TargetLowering.h"
/// was temporarily in the f64 operand.
FCFID,
+ /// Newer FCFID[US] integer-to-floating-point conversion instructions for
+ /// unsigned integers and single-precision outputs.
+ FCFIDU, FCFIDS, FCFIDUS,
+
/// FCTI[D,W]Z - The FCTIDZ and FCTIWZ instructions, taking an f32 or f64
/// operand, producing an f64 value containing the integer representation
/// of that FP value.
FCTIDZ, FCTIWZ,
- /// STFIWX - The STFIWX instruction. The first operand is an input token
- /// chain, then an f64 value to store, then an address to store it to.
- STFIWX,
+ /// Newer FCTI[D,W]UZ floating-point-to-integer conversion instructions for
+ /// unsigned integers.
+ FCTIDUZ, FCTIWUZ,
+
+ /// Reciprocal estimate instructions (unary FP ops).
+ FRE, FRSQRTE,
// VMADDFP, VNMSUBFP - The VMADDFP and VNMSUBFP instructions, taking
// three v4f32 operands and producing a v4f32 result.
///
VPERM,
+ /// The CMPB instruction (takes two operands of i32 or i64).
+ CMPB,
+
/// Hi/Lo - These represent the high and low 16-bit parts of a global
/// address respectively. These nodes have two operands, the first of
/// which must be a TargetGlobalAddress, and the second of which must be a
TOC_ENTRY,
- /// The following three target-specific nodes are used for calls through
+ /// The following two target-specific nodes are used for calls through
/// function pointers in the 64-bit SVR4 ABI.
- /// Restore the TOC from the TOC save area of the current stack frame.
- /// This is basically a hard coded load instruction which additionally
- /// takes/produces a flag.
- TOC_RESTORE,
-
/// Like a regular LOAD but additionally taking/producing a flag.
LOAD,
- /// LOAD into r2 (also taking/producing a flag). Like TOC_RESTORE, this is
- /// a hard coded load instruction.
+ /// Like LOAD (taking/producing a flag), but using r2 as hard-coded
+ /// destination.
LOAD_TOC,
/// OPRC, CHAIN = DYNALLOC(CHAIN, NEGSIZE, FRAME_INDEX)
/// code.
SRL, SRA, SHL,
- /// EXTSW_32 - This is the EXTSW instruction for use with "32-bit"
- /// registers.
- EXTSW_32,
+ /// The combination of sra[wd]i and addze used to implemented signed
+ /// integer division by a power of 2. The first operand is the dividend,
+ /// and the second is the constant shift amount (representing the
+ /// divisor).
+ SRA_ADDZE,
/// CALL - A direct function call.
/// CALL_NOP is a call with the special NOP which follows 64-bit
/// SVR4 calls.
CALL, CALL_NOP,
+ /// CALL_TLS and CALL_NOP_TLS - Versions of CALL and CALL_NOP used
+ /// to access TLS variables.
+ CALL_TLS, CALL_NOP_TLS,
+
/// CHAIN,FLAG = MTCTR(VAL, CHAIN[, INFLAG]) - Directly corresponds to a
/// MTCTR instruction.
MTCTR,
/// BCTRL instruction.
BCTRL,
+ /// CHAIN,FLAG = BCTRL(CHAIN, ADDR, INFLAG) - The combination of a bctrl
+ /// instruction and the TOC reload required on SVR4 PPC64.
+ BCTRL_LOAD_TOC,
+
/// Return with a flag operand, matched by 'blr'
RET_FLAG,
- /// R32 = MFCR(CRREG, INFLAG) - Represents the MFCRpseud/MFOCRF
- /// instructions. This copies the bits corresponding to the specified
- /// CRREG into the resultant GPR. Bits corresponding to other CR regs
- /// are undefined.
- MFCR,
+ /// R32 = MFOCRF(CRREG, INFLAG) - Represents the MFOCRF instruction.
+ /// This copies the bits corresponding to the specified CRREG into the
+ /// resultant GPR. Bits corresponding to other CR regs are undefined.
+ MFOCRF,
+
+ // FIXME: Remove these once the ANDI glue bug is fixed:
+ /// i1 = ANDIo_1_[EQ|GT]_BIT(i32 or i64 x) - Represents the result of the
+ /// eq or gt bit of CR0 after executing andi. x, 1. This is used to
+ /// implement truncation of i32 or i64 to i1.
+ ANDIo_1_EQ_BIT, ANDIo_1_GT_BIT,
+
+ // READ_TIME_BASE - A read of the 64-bit time-base register on a 32-bit
+ // target (returns (Lo, Hi)). It takes a chain operand.
+ READ_TIME_BASE,
// EH_SJLJ_SETJMP - SjLj exception handling setjmp.
EH_SJLJ_SETJMP,
/// an optional input flag argument.
COND_BRANCH,
+ /// CHAIN = BDNZ CHAIN, DESTBB - These are used to create counter-based
+ /// loops.
+ BDNZ, BDZ,
+
/// F8RC = FADDRTZ F8RC, F8RC - This is an FADD done with rounding
/// towards zero. Used only as part of the long double-to-int
/// conversion sequence.
CR6SET,
CR6UNSET,
+ /// GPRC = address of _GLOBAL_OFFSET_TABLE_. Used by initial-exec TLS
+ /// on PPC32.
+ PPC32_GOT,
+
+ /// GPRC = address of _GLOBAL_OFFSET_TABLE_. Used by general dynamic and
+ /// local dynamic TLS on PPC32.
+ PPC32_PICGOT,
+
/// G8RC = ADDIS_GOT_TPREL_HA %X2, Symbol - Used by the initial-exec
/// TLS model, produces an ADDIS8 instruction that adds the GOT
- /// base to sym@got@tprel@ha.
+ /// base to sym\@got\@tprel\@ha.
ADDIS_GOT_TPREL_HA,
/// G8RC = LD_GOT_TPREL_L Symbol, G8RReg - Used by the initial-exec
/// TLS model, produces a LD instruction with base register G8RReg
- /// and offset sym@got@tprel@l. This completes the addition that
+ /// and offset sym\@got\@tprel\@l. This completes the addition that
/// finds the offset of "sym" relative to the thread pointer.
LD_GOT_TPREL_L,
/// G8RC = ADD_TLS G8RReg, Symbol - Used by the initial-exec TLS
/// model, produces an ADD instruction that adds the contents of
/// G8RReg to the thread pointer. Symbol contains a relocation
- /// sym@tls which is to be replaced by the thread pointer and
+ /// sym\@tls which is to be replaced by the thread pointer and
/// identifies to the linker that the instruction is part of a
/// TLS sequence.
ADD_TLS,
/// G8RC = ADDIS_TLSGD_HA %X2, Symbol - For the general-dynamic TLS
/// model, produces an ADDIS8 instruction that adds the GOT base
- /// register to sym@got@tlsgd@ha.
+ /// register to sym\@got\@tlsgd\@ha.
ADDIS_TLSGD_HA,
/// G8RC = ADDI_TLSGD_L G8RReg, Symbol - For the general-dynamic TLS
/// model, produces an ADDI8 instruction that adds G8RReg to
- /// sym@got@tlsgd@l.
+ /// sym\@got\@tlsgd\@l.
ADDI_TLSGD_L,
- /// G8RC = GET_TLS_ADDR %X3, Symbol - For the general-dynamic TLS
- /// model, produces a call to __tls_get_addr(sym@tlsgd).
- GET_TLS_ADDR,
-
/// G8RC = ADDIS_TLSLD_HA %X2, Symbol - For the local-dynamic TLS
/// model, produces an ADDIS8 instruction that adds the GOT base
- /// register to sym@got@tlsld@ha.
+ /// register to sym\@got\@tlsld\@ha.
ADDIS_TLSLD_HA,
/// G8RC = ADDI_TLSLD_L G8RReg, Symbol - For the local-dynamic TLS
/// model, produces an ADDI8 instruction that adds G8RReg to
- /// sym@got@tlsld@l.
+ /// sym\@got\@tlsld\@l.
ADDI_TLSLD_L,
- /// G8RC = GET_TLSLD_ADDR %X3, Symbol - For the local-dynamic TLS
- /// model, produces a call to __tls_get_addr(sym@tlsld).
- GET_TLSLD_ADDR,
-
/// G8RC = ADDIS_DTPREL_HA %X3, Symbol, Chain - For the
/// local-dynamic TLS model, produces an ADDIS8 instruction
- /// that adds X3 to sym@dtprel@ha. The Chain operand is needed
+ /// that adds X3 to sym\@dtprel\@ha. The Chain operand is needed
/// to tie this in place following a copy to %X3 from the result
/// of a GET_TLSLD_ADDR.
ADDIS_DTPREL_HA,
/// G8RC = ADDI_DTPREL_L G8RReg, Symbol - For the local-dynamic TLS
/// model, produces an ADDI8 instruction that adds G8RReg to
- /// sym@got@dtprel@l.
+ /// sym\@got\@dtprel\@l.
ADDI_DTPREL_L,
/// VRRC = VADD_SPLAT Elt, EltSize - Temporary node to be expanded
/// optimizations due to constant folding.
VADD_SPLAT,
- /// STD_32 - This is the STD instruction for use with "32-bit" registers.
- STD_32 = ISD::FIRST_TARGET_MEMORY_OPCODE,
+ /// CHAIN = SC CHAIN, Imm128 - System call. The 7-bit unsigned
+ /// operand identifies the operating system entry point.
+ SC,
+
+ /// VSRC, CHAIN = XXSWAPD CHAIN, VSRC - Occurs only for little
+ /// endian. Maps to an xxswapd instruction that corrects an lxvd2x
+ /// or stxvd2x instruction. The chain is necessary because the
+ /// sequence replaces a load and needs to provide the same number
+ /// of outputs.
+ XXSWAPD,
/// CHAIN = STBRX CHAIN, GPRC, Ptr, Type - This is a
/// byte-swapping store instruction. It byte-swaps the low "Type" bits of
/// the GPRC input, then stores it through Ptr. Type can be either i16 or
/// i32.
- STBRX,
+ STBRX = ISD::FIRST_TARGET_MEMORY_OPCODE,
/// GPRC, CHAIN = LBRX CHAIN, Ptr, Type - This is a
/// byte-swapping load instruction. It loads "Type" bits, byte swaps it,
/// or i32.
LBRX,
+ /// STFIWX - The STFIWX instruction. The first operand is an input token
+ /// chain, then an f64 value to store, then an address to store it to.
+ STFIWX,
+
+ /// GPRC, CHAIN = LFIWAX CHAIN, Ptr - This is a floating-point
+ /// load which sign-extends from a 32-bit integer value into the
+ /// destination 64-bit register.
+ LFIWAX,
+
+ /// GPRC, CHAIN = LFIWZX CHAIN, Ptr - This is a floating-point
+ /// load which zero-extends from a 32-bit integer value into the
+ /// destination 64-bit register.
+ LFIWZX,
+
/// G8RC = ADDIS_TOC_HA %X2, Symbol - For medium and large code model,
/// produces an ADDIS8 instruction that adds the TOC base register to
- /// sym@toc@ha.
+ /// sym\@toc\@ha.
ADDIS_TOC_HA,
/// G8RC = LD_TOC_L Symbol, G8RReg - For medium and large code model,
/// produces a LD instruction with base register G8RReg and offset
- /// sym@toc@l. Preceded by an ADDIS_TOC_HA to form a full 32-bit offset.
+ /// sym\@toc\@l. Preceded by an ADDIS_TOC_HA to form a full 32-bit offset.
LD_TOC_L,
/// G8RC = ADDI_TOC_L G8RReg, Symbol - For medium code model, produces
- /// an ADDI8 instruction that adds G8RReg to sym@toc@l.
+ /// an ADDI8 instruction that adds G8RReg to sym\@toc\@l.
/// Preceded by an ADDIS_TOC_HA to form a full 32-bit offset.
- ADDI_TOC_L
+ ADDI_TOC_L,
+
+ /// VSRC, CHAIN = LXVD2X_LE CHAIN, Ptr - Occurs only for little endian.
+ /// Maps directly to an lxvd2x instruction that will be followed by
+ /// an xxswapd.
+ LXVD2X,
+
+ /// CHAIN = STXVD2X CHAIN, VSRC, Ptr - Occurs only for little endian.
+ /// Maps directly to an stxvd2x instruction that will be preceded by
+ /// an xxswapd.
+ STXVD2X
};
}
namespace PPC {
/// isVPKUHUMShuffleMask - Return true if this is the shuffle mask for a
/// VPKUHUM instruction.
- bool isVPKUHUMShuffleMask(ShuffleVectorSDNode *N, bool isUnary);
+ bool isVPKUHUMShuffleMask(ShuffleVectorSDNode *N, unsigned ShuffleKind,
+ SelectionDAG &DAG);
/// isVPKUWUMShuffleMask - Return true if this is the shuffle mask for a
/// VPKUWUM instruction.
- bool isVPKUWUMShuffleMask(ShuffleVectorSDNode *N, bool isUnary);
+ bool isVPKUWUMShuffleMask(ShuffleVectorSDNode *N, unsigned ShuffleKind,
+ SelectionDAG &DAG);
/// isVMRGLShuffleMask - Return true if this is a shuffle mask suitable for
/// a VRGL* instruction with the specified unit size (1,2 or 4 bytes).
bool isVMRGLShuffleMask(ShuffleVectorSDNode *N, unsigned UnitSize,
- bool isUnary);
+ unsigned ShuffleKind, SelectionDAG &DAG);
/// isVMRGHShuffleMask - Return true if this is a shuffle mask suitable for
/// a VRGH* instruction with the specified unit size (1,2 or 4 bytes).
bool isVMRGHShuffleMask(ShuffleVectorSDNode *N, unsigned UnitSize,
- bool isUnary);
+ unsigned ShuffleKind, SelectionDAG &DAG);
- /// isVSLDOIShuffleMask - If this is a vsldoi shuffle mask, return the shift
- /// amount, otherwise return -1.
- int isVSLDOIShuffleMask(SDNode *N, bool isUnary);
+ /// isVSLDOIShuffleMask - If this is a vsldoi shuffle mask, return the
+ /// shift amount, otherwise return -1.
+ int isVSLDOIShuffleMask(SDNode *N, unsigned ShuffleKind,
+ SelectionDAG &DAG);
/// isSplatShuffleMask - Return true if the specified VECTOR_SHUFFLE operand
/// specifies a splat of a single element that is suitable for input to
/// getVSPLTImmediate - Return the appropriate VSPLT* immediate to splat the
/// specified isSplatShuffleMask VECTOR_SHUFFLE mask.
- unsigned getVSPLTImmediate(SDNode *N, unsigned EltSize);
+ unsigned getVSPLTImmediate(SDNode *N, unsigned EltSize, SelectionDAG &DAG);
/// get_VSPLTI_elt - If this is a build_vector of constants which can be
/// formed by using a vspltis[bhw] instruction of the specified element
SDValue get_VSPLTI_elt(SDNode *N, unsigned ByteSize, SelectionDAG &DAG);
}
+ class PPCSubtarget;
class PPCTargetLowering : public TargetLowering {
- const PPCSubtarget &PPCSubTarget;
- const PPCRegisterInfo *PPCRegInfo;
+ const PPCSubtarget &Subtarget;
public:
- explicit PPCTargetLowering(PPCTargetMachine &TM);
+ explicit PPCTargetLowering(const PPCTargetMachine &TM);
/// getTargetNodeName() - This method returns the name of a target specific
/// DAG node.
- virtual const char *getTargetNodeName(unsigned Opcode) const;
+ const char *getTargetNodeName(unsigned Opcode) const override;
+
+ MVT getScalarShiftAmountTy(EVT LHSTy) const override { return MVT::i32; }
- virtual MVT getScalarShiftAmountTy(EVT LHSTy) const { return MVT::i32; }
+ bool isCheapToSpeculateCttz() const override {
+ return true;
+ }
+
+ bool isCheapToSpeculateCtlz() const override {
+ return true;
+ }
/// getSetCCResultType - Return the ISD::SETCC ValueType
- virtual EVT getSetCCResultType(EVT VT) const;
+ EVT getSetCCResultType(LLVMContext &Context, EVT VT) const override;
+
+ /// Return true if target always beneficiates from combining into FMA for a
+ /// given value type. This must typically return false on targets where FMA
+ /// takes more cycles to execute than FADD.
+ bool enableAggressiveFMAFusion(EVT VT) const override;
/// getPreIndexedAddressParts - returns true by value, base pointer and
/// offset pointer and addressing mode by reference if the node's address
/// can be legally represented as pre-indexed load / store address.
- virtual bool getPreIndexedAddressParts(SDNode *N, SDValue &Base,
- SDValue &Offset,
- ISD::MemIndexedMode &AM,
- SelectionDAG &DAG) const;
+ bool getPreIndexedAddressParts(SDNode *N, SDValue &Base,
+ SDValue &Offset,
+ ISD::MemIndexedMode &AM,
+ SelectionDAG &DAG) const override;
/// SelectAddressRegReg - Given the specified addressed, check to see if it
/// can be represented as an indexed [r+r] operation. Returns false if it
/// SelectAddressRegImm - Returns true if the address N can be represented
/// by a base register plus a signed 16-bit displacement [r+imm], and if it
- /// is not better represented as reg+reg.
+ /// is not better represented as reg+reg. If Aligned is true, only accept
+ /// displacements suitable for STD and friends, i.e. multiples of 4.
bool SelectAddressRegImm(SDValue N, SDValue &Disp, SDValue &Base,
- SelectionDAG &DAG) const;
+ SelectionDAG &DAG, bool Aligned) const;
/// SelectAddressRegRegOnly - Given the specified addressed, force it to be
/// represented as an indexed [r+r] operation.
bool SelectAddressRegRegOnly(SDValue N, SDValue &Base, SDValue &Index,
SelectionDAG &DAG) const;
- /// SelectAddressRegImmShift - Returns true if the address N can be
- /// represented by a base register plus a signed 14-bit displacement
- /// [r+imm*4]. Suitable for use by STD and friends.
- bool SelectAddressRegImmShift(SDValue N, SDValue &Disp, SDValue &Base,
- SelectionDAG &DAG) const;
-
- Sched::Preference getSchedulingPreference(SDNode *N) const;
+ Sched::Preference getSchedulingPreference(SDNode *N) const override;
/// LowerOperation - Provide custom lowering hooks for some operations.
///
- virtual SDValue LowerOperation(SDValue Op, SelectionDAG &DAG) const;
+ SDValue LowerOperation(SDValue Op, SelectionDAG &DAG) const override;
/// ReplaceNodeResults - Replace the results of node with an illegal result
/// type with new values built out of custom code.
///
- virtual void ReplaceNodeResults(SDNode *N, SmallVectorImpl<SDValue>&Results,
- SelectionDAG &DAG) const;
+ void ReplaceNodeResults(SDNode *N, SmallVectorImpl<SDValue>&Results,
+ SelectionDAG &DAG) const override;
+
+ SDValue expandVSXLoadForLE(SDNode *N, DAGCombinerInfo &DCI) const;
+ SDValue expandVSXStoreForLE(SDNode *N, DAGCombinerInfo &DCI) const;
+
+ SDValue PerformDAGCombine(SDNode *N, DAGCombinerInfo &DCI) const override;
+
+ SDValue BuildSDIVPow2(SDNode *N, const APInt &Divisor, SelectionDAG &DAG,
+ std::vector<SDNode *> *Created) const override;
- virtual SDValue PerformDAGCombine(SDNode *N, DAGCombinerInfo &DCI) const;
+ unsigned getRegisterByName(const char* RegName, EVT VT) const override;
- virtual void computeMaskedBitsForTargetNode(const SDValue Op,
- APInt &KnownZero,
- APInt &KnownOne,
- const SelectionDAG &DAG,
- unsigned Depth = 0) const;
+ void computeKnownBitsForTargetNode(const SDValue Op,
+ APInt &KnownZero,
+ APInt &KnownOne,
+ const SelectionDAG &DAG,
+ unsigned Depth = 0) const override;
- virtual MachineBasicBlock *
+ unsigned getPrefLoopAlignment(MachineLoop *ML) const override;
+
+ Instruction* emitLeadingFence(IRBuilder<> &Builder, AtomicOrdering Ord,
+ bool IsStore, bool IsLoad) const override;
+ Instruction* emitTrailingFence(IRBuilder<> &Builder, AtomicOrdering Ord,
+ bool IsStore, bool IsLoad) const override;
+
+ MachineBasicBlock *
EmitInstrWithCustomInserter(MachineInstr *MI,
- MachineBasicBlock *MBB) const;
+ MachineBasicBlock *MBB) const override;
MachineBasicBlock *EmitAtomicBinary(MachineInstr *MI,
MachineBasicBlock *MBB, bool is64Bit,
unsigned BinOpcode) const;
MachineBasicBlock *emitEHSjLjLongJmp(MachineInstr *MI,
MachineBasicBlock *MBB) const;
- ConstraintType getConstraintType(const std::string &Constraint) const;
+ ConstraintType
+ getConstraintType(const std::string &Constraint) const override;
/// Examine constraint string and operand type and determine a weight value.
/// The operand object must already have been set up with the operand type.
ConstraintWeight getSingleConstraintMatchWeight(
- AsmOperandInfo &info, const char *constraint) const;
+ AsmOperandInfo &info, const char *constraint) const override;
std::pair<unsigned, const TargetRegisterClass*>
getRegForInlineAsmConstraint(const std::string &Constraint,
- EVT VT) const;
+ MVT VT) const override;
/// getByValTypeAlignment - Return the desired alignment for ByVal aggregate
/// function arguments in the caller parameter area. This is the actual
/// alignment, not its logarithm.
- unsigned getByValTypeAlignment(Type *Ty) const;
+ unsigned getByValTypeAlignment(Type *Ty) const override;
/// LowerAsmOperandForConstraint - Lower the specified operand into the Ops
/// vector. If it is invalid, don't add anything to Ops.
- virtual void LowerAsmOperandForConstraint(SDValue Op,
- std::string &Constraint,
- std::vector<SDValue> &Ops,
- SelectionDAG &DAG) const;
+ void LowerAsmOperandForConstraint(SDValue Op,
+ std::string &Constraint,
+ std::vector<SDValue> &Ops,
+ SelectionDAG &DAG) const override;
/// isLegalAddressingMode - Return true if the addressing mode represented
/// by AM is legal for this target, for a load/store of the specified type.
- virtual bool isLegalAddressingMode(const AddrMode &AM, Type *Ty)const;
+ bool isLegalAddressingMode(const AddrMode &AM, Type *Ty) const override;
+
+ /// isLegalICmpImmediate - Return true if the specified immediate is legal
+ /// icmp immediate, that is the target has icmp instructions which can
+ /// compare a register against the immediate without having to materialize
+ /// the immediate into a register.
+ bool isLegalICmpImmediate(int64_t Imm) const override;
+
+ /// isLegalAddImmediate - Return true if the specified immediate is legal
+ /// add immediate, that is the target has add instructions which can
+ /// add a register and the immediate without having to materialize
+ /// the immediate into a register.
+ bool isLegalAddImmediate(int64_t Imm) const override;
- /// isLegalAddressImmediate - Return true if the integer value can be used
- /// as the offset of the target addressing mode for load / store of the
- /// given type.
- virtual bool isLegalAddressImmediate(int64_t V, Type *Ty) const;
+ /// isTruncateFree - Return true if it's free to truncate a value of
+ /// type Ty1 to type Ty2. e.g. On PPC it's free to truncate a i64 value in
+ /// register X1 to i32 by referencing its sub-register R1.
+ bool isTruncateFree(Type *Ty1, Type *Ty2) const override;
+ bool isTruncateFree(EVT VT1, EVT VT2) const override;
- /// isLegalAddressImmediate - Return true if the GlobalValue can be used as
- /// the offset of the target addressing mode.
- virtual bool isLegalAddressImmediate(GlobalValue *GV) const;
+ bool isZExtFree(SDValue Val, EVT VT2) const override;
- virtual bool isOffsetFoldingLegal(const GlobalAddressSDNode *GA) const;
+ /// \brief Returns true if it is beneficial to convert a load of a constant
+ /// to just the constant itself.
+ bool shouldConvertConstantLoadToIntImm(const APInt &Imm,
+ Type *Ty) const override;
+
+ bool isOffsetFoldingLegal(const GlobalAddressSDNode *GA) const override;
+
+ bool getTgtMemIntrinsic(IntrinsicInfo &Info,
+ const CallInst &I,
+ unsigned Intrinsic) const override;
/// getOptimalMemOpType - Returns the target specific optimal type for load
/// and store operations as a result of memset, memcpy, and memmove
/// source is constant so it does not need to be loaded.
/// It returns EVT::Other if the type should be determined using generic
/// target-independent logic.
- virtual EVT
- getOptimalMemOpType(uint64_t Size, unsigned DstAlign, unsigned SrcAlign,
+ EVT
+ getOptimalMemOpType(uint64_t Size, unsigned DstAlign, unsigned SrcAlign,
bool IsMemset, bool ZeroMemset, bool MemcpyStrSrc,
- MachineFunction &MF) const;
+ MachineFunction &MF) const override;
/// Is unaligned memory access allowed for the given type, and is it fast
/// relative to software emulation.
- virtual bool allowsUnalignedMemoryAccesses(EVT VT, bool *Fast = 0) const;
-
- /// isFMAFasterThanMulAndAdd - Return true if an FMA operation is faster than
- /// a pair of mul and add instructions. fmuladd intrinsics will be expanded to
- /// FMAs when this method returns true (and FMAs are legal), otherwise fmuladd
- /// is expanded to mul + add.
- virtual bool isFMAFasterThanMulAndAdd(EVT VT) const;
+ bool allowsMisalignedMemoryAccesses(EVT VT,
+ unsigned AddrSpace,
+ unsigned Align = 1,
+ bool *Fast = nullptr) const override;
+
+ /// isFMAFasterThanFMulAndFAdd - Return true if an FMA operation is faster
+ /// than a pair of fmul and fadd instructions. fmuladd intrinsics will be
+ /// expanded to FMAs when this method returns true, otherwise fmuladd is
+ /// expanded to fmul + fadd.
+ bool isFMAFasterThanFMulAndFAdd(EVT VT) const override;
+
+ // Should we expand the build vector with shuffles?
+ bool
+ shouldExpandBuildVectorWithShuffles(EVT VT,
+ unsigned DefinedValues) const override;
+
+ /// createFastISel - This method returns a target-specific FastISel object,
+ /// or null if the target does not support "fast" instruction selection.
+ FastISel *createFastISel(FunctionLoweringInfo &FuncInfo,
+ const TargetLibraryInfo *LibInfo) const override;
+
+ /// \brief Returns true if an argument of type Ty needs to be passed in a
+ /// contiguous block of registers in calling convention CallConv.
+ bool functionArgumentNeedsConsecutiveRegisters(
+ Type *Ty, CallingConv::ID CallConv, bool isVarArg) const override {
+ // We support any array type as "consecutive" block in the parameter
+ // save area. The element type defines the alignment requirement and
+ // whether the argument should go in GPRs, FPRs, or VRs if available.
+ //
+ // Note that clang uses this capability both to implement the ELFv2
+ // homogeneous float/vector aggregate ABI, and to avoid having to use
+ // "byval" when passing aggregates that might fully fit in registers.
+ return Ty->isArrayTy();
+ }
private:
+
+ struct ReuseLoadInfo {
+ SDValue Ptr;
+ SDValue Chain;
+ SDValue ResChain;
+ MachinePointerInfo MPI;
+ bool IsInvariant;
+ unsigned Alignment;
+ AAMDNodes AAInfo;
+ const MDNode *Ranges;
+
+ ReuseLoadInfo() : IsInvariant(false), Alignment(0), Ranges(nullptr) {}
+ };
+
+ bool canReuseLoadAddress(SDValue Op, EVT MemVT, ReuseLoadInfo &RLI,
+ SelectionDAG &DAG,
+ ISD::LoadExtType ET = ISD::NON_EXTLOAD) const;
+ void spliceIntoChain(SDValue ResChain, SDValue NewResChain,
+ SelectionDAG &DAG) const;
+
+ void LowerFP_TO_INTForReuse(SDValue Op, ReuseLoadInfo &RLI,
+ SelectionDAG &DAG, SDLoc dl) const;
+
SDValue getFramePointerFrameIndex(SelectionDAG & DAG) const;
SDValue getReturnAddrFrameIndex(SelectionDAG & DAG) const;
SDValue &LROpOut,
SDValue &FPOpOut,
bool isDarwinABI,
- DebugLoc dl) const;
+ SDLoc dl) const;
SDValue LowerRETURNADDR(SDValue Op, SelectionDAG &DAG) const;
SDValue LowerFRAMEADDR(SDValue Op, SelectionDAG &DAG) const;
SDValue LowerConstantPool(SDValue Op, SelectionDAG &DAG) const;
SDValue LowerBlockAddress(SDValue Op, SelectionDAG &DAG) const;
+ std::pair<SDValue,SDValue> lowerTLSCall(SDValue Op, SDLoc dl,
+ SelectionDAG &DAG) const;
SDValue LowerGlobalTLSAddress(SDValue Op, SelectionDAG &DAG) const;
SDValue LowerGlobalAddress(SDValue Op, SelectionDAG &DAG) const;
SDValue LowerJumpTable(SDValue Op, SelectionDAG &DAG) const;
const PPCSubtarget &Subtarget) const;
SDValue LowerVAARG(SDValue Op, SelectionDAG &DAG,
const PPCSubtarget &Subtarget) const;
+ SDValue LowerVACOPY(SDValue Op, SelectionDAG &DAG,
+ const PPCSubtarget &Subtarget) const;
SDValue LowerSTACKRESTORE(SDValue Op, SelectionDAG &DAG,
const PPCSubtarget &Subtarget) const;
SDValue LowerDYNAMIC_STACKALLOC(SDValue Op, SelectionDAG &DAG,
const PPCSubtarget &Subtarget) const;
+ SDValue LowerLOAD(SDValue Op, SelectionDAG &DAG) const;
+ SDValue LowerSTORE(SDValue Op, SelectionDAG &DAG) const;
+ SDValue LowerTRUNCATE(SDValue Op, SelectionDAG &DAG) const;
SDValue LowerSELECT_CC(SDValue Op, SelectionDAG &DAG) const;
- SDValue LowerFP_TO_INT(SDValue Op, SelectionDAG &DAG, DebugLoc dl) const;
- SDValue LowerSINT_TO_FP(SDValue Op, SelectionDAG &DAG) const;
+ SDValue LowerFP_TO_INT(SDValue Op, SelectionDAG &DAG, SDLoc dl) const;
+ SDValue LowerINT_TO_FP(SDValue Op, SelectionDAG &DAG) const;
SDValue LowerFLT_ROUNDS_(SDValue Op, SelectionDAG &DAG) const;
SDValue LowerSHL_PARTS(SDValue Op, SelectionDAG &DAG) const;
SDValue LowerSRL_PARTS(SDValue Op, SelectionDAG &DAG) const;
SDValue LowerVECTOR_SHUFFLE(SDValue Op, SelectionDAG &DAG) const;
SDValue LowerINTRINSIC_WO_CHAIN(SDValue Op, SelectionDAG &DAG) const;
SDValue LowerSCALAR_TO_VECTOR(SDValue Op, SelectionDAG &DAG) const;
+ SDValue LowerSIGN_EXTEND_INREG(SDValue Op, SelectionDAG &DAG) const;
SDValue LowerMUL(SDValue Op, SelectionDAG &DAG) const;
SDValue LowerCallResult(SDValue Chain, SDValue InFlag,
CallingConv::ID CallConv, bool isVarArg,
const SmallVectorImpl<ISD::InputArg> &Ins,
- DebugLoc dl, SelectionDAG &DAG,
+ SDLoc dl, SelectionDAG &DAG,
SmallVectorImpl<SDValue> &InVals) const;
- SDValue FinishCall(CallingConv::ID CallConv, DebugLoc dl, bool isTailCall,
+ SDValue FinishCall(CallingConv::ID CallConv, SDLoc dl, bool isTailCall,
bool isVarArg,
SelectionDAG &DAG,
SmallVector<std::pair<unsigned, SDValue>, 8>
const SmallVectorImpl<ISD::InputArg> &Ins,
SmallVectorImpl<SDValue> &InVals) const;
- virtual SDValue
+ SDValue
LowerFormalArguments(SDValue Chain,
CallingConv::ID CallConv, bool isVarArg,
const SmallVectorImpl<ISD::InputArg> &Ins,
- DebugLoc dl, SelectionDAG &DAG,
- SmallVectorImpl<SDValue> &InVals) const;
+ SDLoc dl, SelectionDAG &DAG,
+ SmallVectorImpl<SDValue> &InVals) const override;
- virtual SDValue
+ SDValue
LowerCall(TargetLowering::CallLoweringInfo &CLI,
- SmallVectorImpl<SDValue> &InVals) const;
+ SmallVectorImpl<SDValue> &InVals) const override;
- virtual bool
+ bool
CanLowerReturn(CallingConv::ID CallConv, MachineFunction &MF,
bool isVarArg,
const SmallVectorImpl<ISD::OutputArg> &Outs,
- LLVMContext &Context) const;
+ LLVMContext &Context) const override;
- virtual SDValue
+ SDValue
LowerReturn(SDValue Chain,
CallingConv::ID CallConv, bool isVarArg,
const SmallVectorImpl<ISD::OutputArg> &Outs,
const SmallVectorImpl<SDValue> &OutVals,
- DebugLoc dl, SelectionDAG &DAG) const;
+ SDLoc dl, SelectionDAG &DAG) const override;
SDValue
extendArgForPPC64(ISD::ArgFlagsTy Flags, EVT ObjectVT, SelectionDAG &DAG,
- SDValue ArgVal, DebugLoc dl) const;
-
- void
- setMinReservedArea(MachineFunction &MF, SelectionDAG &DAG,
- unsigned nAltivecParamsAtEnd,
- unsigned MinReservedArea, bool isPPC64) const;
+ SDValue ArgVal, SDLoc dl) const;
SDValue
LowerFormalArguments_Darwin(SDValue Chain,
CallingConv::ID CallConv, bool isVarArg,
const SmallVectorImpl<ISD::InputArg> &Ins,
- DebugLoc dl, SelectionDAG &DAG,
+ SDLoc dl, SelectionDAG &DAG,
SmallVectorImpl<SDValue> &InVals) const;
SDValue
LowerFormalArguments_64SVR4(SDValue Chain,
CallingConv::ID CallConv, bool isVarArg,
const SmallVectorImpl<ISD::InputArg> &Ins,
- DebugLoc dl, SelectionDAG &DAG,
+ SDLoc dl, SelectionDAG &DAG,
SmallVectorImpl<SDValue> &InVals) const;
SDValue
LowerFormalArguments_32SVR4(SDValue Chain,
CallingConv::ID CallConv, bool isVarArg,
const SmallVectorImpl<ISD::InputArg> &Ins,
- DebugLoc dl, SelectionDAG &DAG,
+ SDLoc dl, SelectionDAG &DAG,
SmallVectorImpl<SDValue> &InVals) const;
SDValue
createMemcpyOutsideCallSeq(SDValue Arg, SDValue PtrOff,
SDValue CallSeqStart, ISD::ArgFlagsTy Flags,
- SelectionDAG &DAG, DebugLoc dl) const;
+ SelectionDAG &DAG, SDLoc dl) const;
SDValue
LowerCall_Darwin(SDValue Chain, SDValue Callee,
const SmallVectorImpl<ISD::OutputArg> &Outs,
const SmallVectorImpl<SDValue> &OutVals,
const SmallVectorImpl<ISD::InputArg> &Ins,
- DebugLoc dl, SelectionDAG &DAG,
+ SDLoc dl, SelectionDAG &DAG,
SmallVectorImpl<SDValue> &InVals) const;
SDValue
LowerCall_64SVR4(SDValue Chain, SDValue Callee,
const SmallVectorImpl<ISD::OutputArg> &Outs,
const SmallVectorImpl<SDValue> &OutVals,
const SmallVectorImpl<ISD::InputArg> &Ins,
- DebugLoc dl, SelectionDAG &DAG,
+ SDLoc dl, SelectionDAG &DAG,
SmallVectorImpl<SDValue> &InVals) const;
SDValue
LowerCall_32SVR4(SDValue Chain, SDValue Callee, CallingConv::ID CallConv,
const SmallVectorImpl<ISD::OutputArg> &Outs,
const SmallVectorImpl<SDValue> &OutVals,
const SmallVectorImpl<ISD::InputArg> &Ins,
- DebugLoc dl, SelectionDAG &DAG,
+ SDLoc dl, SelectionDAG &DAG,
SmallVectorImpl<SDValue> &InVals) const;
SDValue lowerEH_SJLJ_SETJMP(SDValue Op, SelectionDAG &DAG) const;
SDValue lowerEH_SJLJ_LONGJMP(SDValue Op, SelectionDAG &DAG) const;
+
+ SDValue DAGCombineExtBoolTrunc(SDNode *N, DAGCombinerInfo &DCI) const;
+ SDValue DAGCombineTruncBoolExt(SDNode *N, DAGCombinerInfo &DCI) const;
+ SDValue combineFPToIntToFP(SDNode *N, DAGCombinerInfo &DCI) const;
+
+ SDValue getRsqrtEstimate(SDValue Operand, DAGCombinerInfo &DCI,
+ unsigned &RefinementSteps,
+ bool &UseOneConstNR) const override;
+ SDValue getRecipEstimate(SDValue Operand, DAGCombinerInfo &DCI,
+ unsigned &RefinementSteps) const override;
+ bool combineRepeatedFPDivisors(unsigned NumUsers) const override;
+
+ CCAssignFn *useFastISelCCs(unsigned Flag) const;
};
+
+ namespace PPC {
+ FastISel *createFastISel(FunctionLoweringInfo &FuncInfo,
+ const TargetLibraryInfo *LibInfo);
+ }
+
+ bool CC_PPC32_SVR4_Custom_Dummy(unsigned &ValNo, MVT &ValVT, MVT &LocVT,
+ CCValAssign::LocInfo &LocInfo,
+ ISD::ArgFlagsTy &ArgFlags,
+ CCState &State);
+
+ bool CC_PPC32_SVR4_Custom_AlignArgRegs(unsigned &ValNo, MVT &ValVT,
+ MVT &LocVT,
+ CCValAssign::LocInfo &LocInfo,
+ ISD::ArgFlagsTy &ArgFlags,
+ CCState &State);
+
+ bool CC_PPC32_SVR4_Custom_AlignFPArgRegs(unsigned &ValNo, MVT &ValVT,
+ MVT &LocVT,
+ CCValAssign::LocInfo &LocInfo,
+ ISD::ArgFlagsTy &ArgFlags,
+ CCState &State);
}
#endif // LLVM_TARGET_POWERPC_PPC32ISELLOWERING_H