index 98bdf266438b5dbabb5570e2b778e0209eea72f2..db5a3e42d52fbfae055e1a204d47309fe73bc132 100644 (file)
//
//===----------------------------------------------------------------------===//
-#ifndef LLVM_TARGET_POWERPC_PPC32ISELLOWERING_H
-#define LLVM_TARGET_POWERPC_PPC32ISELLOWERING_H
+#ifndef LLVM_LIB_TARGET_POWERPC_PPCISELLOWERING_H
+#define LLVM_LIB_TARGET_POWERPC_PPCISELLOWERING_H
#include "PPC.h"
#include "PPCInstrInfo.h"
#include "PPCRegisterInfo.h"
-#include "PPCSubtarget.h"
#include "llvm/CodeGen/CallingConvLower.h"
#include "llvm/CodeGen/SelectionDAG.h"
#include "llvm/Target/TargetLowering.h"
///
VPERM,
+ /// The CMPB instruction (takes two operands of i32 or i64).
+ CMPB,
+
/// Hi/Lo - These represent the high and low 16-bit parts of a global
/// address respectively. These nodes have two operands, the first of
/// which must be a TargetGlobalAddress, and the second of which must be a
TOC_ENTRY,
- /// The following three target-specific nodes are used for calls through
+ /// The following two target-specific nodes are used for calls through
/// function pointers in the 64-bit SVR4 ABI.
- /// Restore the TOC from the TOC save area of the current stack frame.
- /// This is basically a hard coded load instruction which additionally
- /// takes/produces a flag.
- TOC_RESTORE,
-
/// Like a regular LOAD but additionally taking/producing a flag.
LOAD,
- /// LOAD into r2 (also taking/producing a flag). Like TOC_RESTORE, this is
- /// a hard coded load instruction.
+ /// Like LOAD (taking/producing a flag), but using r2 as hard-coded
+ /// destination.
LOAD_TOC,
/// OPRC, CHAIN = DYNALLOC(CHAIN, NEGSIZE, FRAME_INDEX)
/// code.
SRL, SRA, SHL,
+ /// The combination of sra[wd]i and addze used to implemented signed
+ /// integer division by a power of 2. The first operand is the dividend,
+ /// and the second is the constant shift amount (representing the
+ /// divisor).
+ SRA_ADDZE,
+
/// CALL - A direct function call.
/// CALL_NOP is a call with the special NOP which follows 64-bit
/// SVR4 calls.
CALL, CALL_NOP,
+ /// CALL_TLS and CALL_NOP_TLS - Versions of CALL and CALL_NOP used
+ /// to access TLS variables.
+ CALL_TLS, CALL_NOP_TLS,
+
/// CHAIN,FLAG = MTCTR(VAL, CHAIN[, INFLAG]) - Directly corresponds to a
/// MTCTR instruction.
MTCTR,
/// BCTRL instruction.
BCTRL,
+ /// CHAIN,FLAG = BCTRL(CHAIN, ADDR, INFLAG) - The combination of a bctrl
+ /// instruction and the TOC reload required on SVR4 PPC64.
+ BCTRL_LOAD_TOC,
+
/// Return with a flag operand, matched by 'blr'
RET_FLAG,
/// implement truncation of i32 or i64 to i1.
ANDIo_1_EQ_BIT, ANDIo_1_GT_BIT,
+ // READ_TIME_BASE - A read of the 64-bit time-base register on a 32-bit
+ // target (returns (Lo, Hi)). It takes a chain operand.
+ READ_TIME_BASE,
+
// EH_SJLJ_SETJMP - SjLj exception handling setjmp.
EH_SJLJ_SETJMP,
/// on PPC32.
PPC32_GOT,
+ /// GPRC = address of _GLOBAL_OFFSET_TABLE_. Used by general dynamic and
+ /// local dynamic TLS on PPC32.
+ PPC32_PICGOT,
+
/// G8RC = ADDIS_GOT_TPREL_HA %X2, Symbol - Used by the initial-exec
/// TLS model, produces an ADDIS8 instruction that adds the GOT
/// base to sym\@got\@tprel\@ha.
/// sym\@got\@tlsgd\@l.
ADDI_TLSGD_L,
- /// G8RC = GET_TLS_ADDR %X3, Symbol - For the general-dynamic TLS
- /// model, produces a call to __tls_get_addr(sym\@tlsgd).
- GET_TLS_ADDR,
-
/// G8RC = ADDIS_TLSLD_HA %X2, Symbol - For the local-dynamic TLS
/// model, produces an ADDIS8 instruction that adds the GOT base
/// register to sym\@got\@tlsld\@ha.
/// sym\@got\@tlsld\@l.
ADDI_TLSLD_L,
- /// G8RC = GET_TLSLD_ADDR %X3, Symbol - For the local-dynamic TLS
- /// model, produces a call to __tls_get_addr(sym\@tlsld).
- GET_TLSLD_ADDR,
-
/// G8RC = ADDIS_DTPREL_HA %X3, Symbol, Chain - For the
/// local-dynamic TLS model, produces an ADDIS8 instruction
/// that adds X3 to sym\@dtprel\@ha. The Chain operand is needed
/// operand identifies the operating system entry point.
SC,
+ /// VSRC, CHAIN = XXSWAPD CHAIN, VSRC - Occurs only for little
+ /// endian. Maps to an xxswapd instruction that corrects an lxvd2x
+ /// or stxvd2x instruction. The chain is necessary because the
+ /// sequence replaces a load and needs to provide the same number
+ /// of outputs.
+ XXSWAPD,
+
/// CHAIN = STBRX CHAIN, GPRC, Ptr, Type - This is a
/// byte-swapping store instruction. It byte-swaps the low "Type" bits of
/// the GPRC input, then stores it through Ptr. Type can be either i16 or
/// G8RC = ADDI_TOC_L G8RReg, Symbol - For medium code model, produces
/// an ADDI8 instruction that adds G8RReg to sym\@toc\@l.
/// Preceded by an ADDIS_TOC_HA to form a full 32-bit offset.
- ADDI_TOC_L
+ ADDI_TOC_L,
+
+ /// VSRC, CHAIN = LXVD2X_LE CHAIN, Ptr - Occurs only for little endian.
+ /// Maps directly to an lxvd2x instruction that will be followed by
+ /// an xxswapd.
+ LXVD2X,
+
+ /// CHAIN = STXVD2X CHAIN, VSRC, Ptr - Occurs only for little endian.
+ /// Maps directly to an stxvd2x instruction that will be preceded by
+ /// an xxswapd.
+ STXVD2X
};
}
namespace PPC {
/// isVPKUHUMShuffleMask - Return true if this is the shuffle mask for a
/// VPKUHUM instruction.
- bool isVPKUHUMShuffleMask(ShuffleVectorSDNode *N, bool isUnary);
+ bool isVPKUHUMShuffleMask(ShuffleVectorSDNode *N, unsigned ShuffleKind,
+ SelectionDAG &DAG);
/// isVPKUWUMShuffleMask - Return true if this is the shuffle mask for a
/// VPKUWUM instruction.
- bool isVPKUWUMShuffleMask(ShuffleVectorSDNode *N, bool isUnary);
+ bool isVPKUWUMShuffleMask(ShuffleVectorSDNode *N, unsigned ShuffleKind,
+ SelectionDAG &DAG);
/// isVMRGLShuffleMask - Return true if this is a shuffle mask suitable for
/// a VRGL* instruction with the specified unit size (1,2 or 4 bytes).
bool isVMRGLShuffleMask(ShuffleVectorSDNode *N, unsigned UnitSize,
- bool isUnary);
+ unsigned ShuffleKind, SelectionDAG &DAG);
/// isVMRGHShuffleMask - Return true if this is a shuffle mask suitable for
/// a VRGH* instruction with the specified unit size (1,2 or 4 bytes).
bool isVMRGHShuffleMask(ShuffleVectorSDNode *N, unsigned UnitSize,
- bool isUnary);
+ unsigned ShuffleKind, SelectionDAG &DAG);
- /// isVSLDOIShuffleMask - If this is a vsldoi shuffle mask, return the shift
- /// amount, otherwise return -1.
- int isVSLDOIShuffleMask(SDNode *N, bool isUnary);
+ /// isVSLDOIShuffleMask - If this is a vsldoi shuffle mask, return the
+ /// shift amount, otherwise return -1.
+ int isVSLDOIShuffleMask(SDNode *N, unsigned ShuffleKind,
+ SelectionDAG &DAG);
/// isSplatShuffleMask - Return true if the specified VECTOR_SHUFFLE operand
/// specifies a splat of a single element that is suitable for input to
/// getVSPLTImmediate - Return the appropriate VSPLT* immediate to splat the
/// specified isSplatShuffleMask VECTOR_SHUFFLE mask.
- unsigned getVSPLTImmediate(SDNode *N, unsigned EltSize);
+ unsigned getVSPLTImmediate(SDNode *N, unsigned EltSize, SelectionDAG &DAG);
/// get_VSPLTI_elt - If this is a build_vector of constants which can be
/// formed by using a vspltis[bhw] instruction of the specified element
SDValue get_VSPLTI_elt(SDNode *N, unsigned ByteSize, SelectionDAG &DAG);
}
+ class PPCSubtarget;
class PPCTargetLowering : public TargetLowering {
- const PPCSubtarget &PPCSubTarget;
+ const PPCSubtarget &Subtarget;
public:
- explicit PPCTargetLowering(PPCTargetMachine &TM);
+ explicit PPCTargetLowering(const PPCTargetMachine &TM);
/// getTargetNodeName() - This method returns the name of a target specific
/// DAG node.
MVT getScalarShiftAmountTy(EVT LHSTy) const override { return MVT::i32; }
+ bool isCheapToSpeculateCttz() const override {
+ return true;
+ }
+
+ bool isCheapToSpeculateCtlz() const override {
+ return true;
+ }
+
/// getSetCCResultType - Return the ISD::SETCC ValueType
EVT getSetCCResultType(LLVMContext &Context, EVT VT) const override;
+ /// Return true if target always beneficiates from combining into FMA for a
+ /// given value type. This must typically return false on targets where FMA
+ /// takes more cycles to execute than FADD.
+ bool enableAggressiveFMAFusion(EVT VT) const override;
+
/// getPreIndexedAddressParts - returns true by value, base pointer and
/// offset pointer and addressing mode by reference if the node's address
/// can be legally represented as pre-indexed load / store address.
void ReplaceNodeResults(SDNode *N, SmallVectorImpl<SDValue>&Results,
SelectionDAG &DAG) const override;
+ SDValue expandVSXLoadForLE(SDNode *N, DAGCombinerInfo &DCI) const;
+ SDValue expandVSXStoreForLE(SDNode *N, DAGCombinerInfo &DCI) const;
+
SDValue PerformDAGCombine(SDNode *N, DAGCombinerInfo &DCI) const override;
+ SDValue BuildSDIVPow2(SDNode *N, const APInt &Divisor, SelectionDAG &DAG,
+ std::vector<SDNode *> *Created) const override;
+
unsigned getRegisterByName(const char* RegName, EVT VT) const override;
- void computeMaskedBitsForTargetNode(const SDValue Op,
- APInt &KnownZero,
- APInt &KnownOne,
- const SelectionDAG &DAG,
- unsigned Depth = 0) const override;
+ void computeKnownBitsForTargetNode(const SDValue Op,
+ APInt &KnownZero,
+ APInt &KnownOne,
+ const SelectionDAG &DAG,
+ unsigned Depth = 0) const override;
+
+ unsigned getPrefLoopAlignment(MachineLoop *ML) const override;
+
+ Instruction* emitLeadingFence(IRBuilder<> &Builder, AtomicOrdering Ord,
+ bool IsStore, bool IsLoad) const override;
+ Instruction* emitTrailingFence(IRBuilder<> &Builder, AtomicOrdering Ord,
+ bool IsStore, bool IsLoad) const override;
MachineBasicBlock *
EmitInstrWithCustomInserter(MachineInstr *MI,
bool isTruncateFree(Type *Ty1, Type *Ty2) const override;
bool isTruncateFree(EVT VT1, EVT VT2) const override;
+ bool isZExtFree(SDValue Val, EVT VT2) const override;
+
/// \brief Returns true if it is beneficial to convert a load of a constant
/// to just the constant itself.
bool shouldConvertConstantLoadToIntImm(const APInt &Imm,
bool isOffsetFoldingLegal(const GlobalAddressSDNode *GA) const override;
+ bool getTgtMemIntrinsic(IntrinsicInfo &Info,
+ const CallInst &I,
+ unsigned Intrinsic) const override;
+
/// getOptimalMemOpType - Returns the target specific optimal type for load
/// and store operations as a result of memset, memcpy, and memmove
/// lowering. If DstAlign is zero that means it's safe to destination
/// Is unaligned memory access allowed for the given type, and is it fast
/// relative to software emulation.
- bool allowsUnalignedMemoryAccesses(EVT VT,
- unsigned AddrSpace,
- bool *Fast = nullptr) const override;
+ bool allowsMisalignedMemoryAccesses(EVT VT,
+ unsigned AddrSpace,
+ unsigned Align = 1,
+ bool *Fast = nullptr) const override;
/// isFMAFasterThanFMulAndFAdd - Return true if an FMA operation is faster
/// than a pair of fmul and fadd instructions. fmuladd intrinsics will be
FastISel *createFastISel(FunctionLoweringInfo &FuncInfo,
const TargetLibraryInfo *LibInfo) const override;
+ /// \brief Returns true if an argument of type Ty needs to be passed in a
+ /// contiguous block of registers in calling convention CallConv.
+ bool functionArgumentNeedsConsecutiveRegisters(
+ Type *Ty, CallingConv::ID CallConv, bool isVarArg) const override {
+ // We support any array type as "consecutive" block in the parameter
+ // save area. The element type defines the alignment requirement and
+ // whether the argument should go in GPRs, FPRs, or VRs if available.
+ //
+ // Note that clang uses this capability both to implement the ELFv2
+ // homogeneous float/vector aggregate ABI, and to avoid having to use
+ // "byval" when passing aggregates that might fully fit in registers.
+ return Ty->isArrayTy();
+ }
+
private:
+
+ struct ReuseLoadInfo {
+ SDValue Ptr;
+ SDValue Chain;
+ SDValue ResChain;
+ MachinePointerInfo MPI;
+ bool IsInvariant;
+ unsigned Alignment;
+ AAMDNodes AAInfo;
+ const MDNode *Ranges;
+
+ ReuseLoadInfo() : IsInvariant(false), Alignment(0), Ranges(nullptr) {}
+ };
+
+ bool canReuseLoadAddress(SDValue Op, EVT MemVT, ReuseLoadInfo &RLI,
+ SelectionDAG &DAG,
+ ISD::LoadExtType ET = ISD::NON_EXTLOAD) const;
+ void spliceIntoChain(SDValue ResChain, SDValue NewResChain,
+ SelectionDAG &DAG) const;
+
+ void LowerFP_TO_INTForReuse(SDValue Op, ReuseLoadInfo &RLI,
+ SelectionDAG &DAG, SDLoc dl) const;
+
SDValue getFramePointerFrameIndex(SelectionDAG & DAG) const;
SDValue getReturnAddrFrameIndex(SelectionDAG & DAG) const;
SDValue LowerFRAMEADDR(SDValue Op, SelectionDAG &DAG) const;
SDValue LowerConstantPool(SDValue Op, SelectionDAG &DAG) const;
SDValue LowerBlockAddress(SDValue Op, SelectionDAG &DAG) const;
+ std::pair<SDValue,SDValue> lowerTLSCall(SDValue Op, SDLoc dl,
+ SelectionDAG &DAG) const;
SDValue LowerGlobalTLSAddress(SDValue Op, SelectionDAG &DAG) const;
SDValue LowerGlobalAddress(SDValue Op, SelectionDAG &DAG) const;
SDValue LowerJumpTable(SDValue Op, SelectionDAG &DAG) const;
extendArgForPPC64(ISD::ArgFlagsTy Flags, EVT ObjectVT, SelectionDAG &DAG,
SDValue ArgVal, SDLoc dl) const;
- void
- setMinReservedArea(MachineFunction &MF, SelectionDAG &DAG,
- unsigned nAltivecParamsAtEnd,
- unsigned MinReservedArea, bool isPPC64) const;
-
SDValue
LowerFormalArguments_Darwin(SDValue Chain,
CallingConv::ID CallConv, bool isVarArg,
SDValue DAGCombineExtBoolTrunc(SDNode *N, DAGCombinerInfo &DCI) const;
SDValue DAGCombineTruncBoolExt(SDNode *N, DAGCombinerInfo &DCI) const;
- SDValue DAGCombineFastRecip(SDValue Op, DAGCombinerInfo &DCI) const;
- SDValue DAGCombineFastRecipFSQRT(SDValue Op, DAGCombinerInfo &DCI) const;
+ SDValue combineFPToIntToFP(SDNode *N, DAGCombinerInfo &DCI) const;
+
+ SDValue getRsqrtEstimate(SDValue Operand, DAGCombinerInfo &DCI,
+ unsigned &RefinementSteps,
+ bool &UseOneConstNR) const override;
+ SDValue getRecipEstimate(SDValue Operand, DAGCombinerInfo &DCI,
+ unsigned &RefinementSteps) const override;
+ bool combineRepeatedFPDivisors(unsigned NumUsers) const override;
CCAssignFn *useFastISelCCs(unsigned Flag) const;
};