diff --git a/lib/Target/X86/Disassembler/X86DisassemblerDecoderCommon.h b/lib/Target/X86/Disassembler/X86DisassemblerDecoderCommon.h
index f7fea1d97d829beffca0de9254f2d63474a61be1..51c3232473bfccef6d4623eeb1ad7a6406772337 100644 (file)
-/*===-- X86DisassemblerDecoderCommon.h - Disassembler decoder -----*- C -*-===*
- *
- * The LLVM Compiler Infrastructure
- *
- * This file is distributed under the University of Illinois Open Source
- * License. See LICENSE.TXT for details.
- *
- *===----------------------------------------------------------------------===*
- *
- * This file is part of the X86 Disassembler.
- * It contains common definitions used by both the disassembler and the table
- * generator.
- * Documentation for the disassembler can be found in X86Disassembler.h.
- *
- *===----------------------------------------------------------------------===*/
-
-/*
- * This header file provides those definitions that need to be shared between
- * the decoder and the table generator in a C-friendly manner.
- */
-
-#ifndef X86DISASSEMBLERDECODERCOMMON_H
-#define X86DISASSEMBLERDECODERCOMMON_H
+//===-- X86DisassemblerDecoderCommon.h - Disassembler decoder ---*- C++ -*-===//
+//
+// The LLVM Compiler Infrastructure
+//
+// This file is distributed under the University of Illinois Open Source
+// License. See LICENSE.TXT for details.
+//
+//===----------------------------------------------------------------------===//
+//
+// This file is part of the X86 Disassembler.
+// It contains common definitions used by both the disassembler and the table
+// generator.
+// Documentation for the disassembler can be found in X86Disassembler.h.
+//
+//===----------------------------------------------------------------------===//
+
+#ifndef LLVM_LIB_TARGET_X86_DISASSEMBLER_X86DISASSEMBLERDECODERCOMMON_H
+#define LLVM_LIB_TARGET_X86_DISASSEMBLER_X86DISASSEMBLERDECODERCOMMON_H
#include "llvm/Support/DataTypes.h"
+namespace llvm {
+namespace X86Disassembler {
+
#define INSTRUCTIONS_SYM x86DisassemblerInstrSpecifiers
#define CONTEXTS_SYM x86DisassemblerContexts
#define ONEBYTE_SYM x86DisassemblerOneByteOpcodes
#define TWOBYTE_SYM x86DisassemblerTwoByteOpcodes
#define THREEBYTE38_SYM x86DisassemblerThreeByte38Opcodes
#define THREEBYTE3A_SYM x86DisassemblerThreeByte3AOpcodes
-#define THREEBYTEA6_SYM x86DisassemblerThreeByteA6Opcodes
-#define THREEBYTEA7_SYM x86DisassemblerThreeByteA7Opcodes
+#define XOP8_MAP_SYM x86DisassemblerXOP8Opcodes
+#define XOP9_MAP_SYM x86DisassemblerXOP9Opcodes
+#define XOPA_MAP_SYM x86DisassemblerXOPAOpcodes
#define INSTRUCTIONS_STR "x86DisassemblerInstrSpecifiers"
#define CONTEXTS_STR "x86DisassemblerContexts"
#define TWOBYTE_STR "x86DisassemblerTwoByteOpcodes"
#define THREEBYTE38_STR "x86DisassemblerThreeByte38Opcodes"
#define THREEBYTE3A_STR "x86DisassemblerThreeByte3AOpcodes"
-#define THREEBYTEA6_STR "x86DisassemblerThreeByteA6Opcodes"
-#define THREEBYTEA7_STR "x86DisassemblerThreeByteA7Opcodes"
-
-/*
- * Attributes of an instruction that must be known before the opcode can be
- * processed correctly. Most of these indicate the presence of particular
- * prefixes, but ATTR_64BIT is simply an attribute of the decoding context.
- */
-#define ATTRIBUTE_BITS \
- ENUM_ENTRY(ATTR_NONE, 0x00) \
- ENUM_ENTRY(ATTR_64BIT, 0x01) \
- ENUM_ENTRY(ATTR_XS, 0x02) \
- ENUM_ENTRY(ATTR_XD, 0x04) \
- ENUM_ENTRY(ATTR_REXW, 0x08) \
- ENUM_ENTRY(ATTR_OPSIZE, 0x10) \
- ENUM_ENTRY(ATTR_ADSIZE, 0x20) \
- ENUM_ENTRY(ATTR_VEX, 0x40) \
- ENUM_ENTRY(ATTR_VEXL, 0x80)
+#define XOP8_MAP_STR "x86DisassemblerXOP8Opcodes"
+#define XOP9_MAP_STR "x86DisassemblerXOP9Opcodes"
+#define XOPA_MAP_STR "x86DisassemblerXOPAOpcodes"
+
+// Attributes of an instruction that must be known before the opcode can be
+// processed correctly. Most of these indicate the presence of particular
+// prefixes, but ATTR_64BIT is simply an attribute of the decoding context.
+#define ATTRIBUTE_BITS \
+ ENUM_ENTRY(ATTR_NONE, 0x00) \
+ ENUM_ENTRY(ATTR_64BIT, (0x1 << 0)) \
+ ENUM_ENTRY(ATTR_XS, (0x1 << 1)) \
+ ENUM_ENTRY(ATTR_XD, (0x1 << 2)) \
+ ENUM_ENTRY(ATTR_REXW, (0x1 << 3)) \
+ ENUM_ENTRY(ATTR_OPSIZE, (0x1 << 4)) \
+ ENUM_ENTRY(ATTR_ADSIZE, (0x1 << 5)) \
+ ENUM_ENTRY(ATTR_VEX, (0x1 << 6)) \
+ ENUM_ENTRY(ATTR_VEXL, (0x1 << 7)) \
+ ENUM_ENTRY(ATTR_EVEX, (0x1 << 8)) \
+ ENUM_ENTRY(ATTR_EVEXL, (0x1 << 9)) \
+ ENUM_ENTRY(ATTR_EVEXL2, (0x1 << 10)) \
+ ENUM_ENTRY(ATTR_EVEXK, (0x1 << 11)) \
+ ENUM_ENTRY(ATTR_EVEXKZ, (0x1 << 12)) \
+ ENUM_ENTRY(ATTR_EVEXB, (0x1 << 13))
#define ENUM_ENTRY(n, v) n = v,
enum attributeBits {
};
#undef ENUM_ENTRY
-/*
- * Combinations of the above attributes that are relevant to instruction
- * decode. Although other combinations are possible, they can be reduced to
- * these without affecting the ultimately decoded instruction.
- */
+// Combinations of the above attributes that are relevant to instruction
+// decode. Although other combinations are possible, they can be reduced to
+// these without affecting the ultimately decoded instruction.
-/* Class name Rank Rationale for rank assignment */
+// Class name Rank Rationale for rank assignment
#define INSTRUCTION_CONTEXTS \
ENUM_ENTRY(IC, 0, "says nothing about the instruction") \
ENUM_ENTRY(IC_64BIT, 1, "says the instruction applies in " \
"operands change width") \
ENUM_ENTRY(IC_ADSIZE, 3, "requires an ADSIZE prefix, so " \
"operands change width") \
+ ENUM_ENTRY(IC_OPSIZE_ADSIZE, 4, "requires ADSIZE and OPSIZE prefixes") \
ENUM_ENTRY(IC_XD, 2, "may say something about the opcode " \
"but not the operands") \
ENUM_ENTRY(IC_XS, 2, "may say something about the opcode " \
"operands change width") \
ENUM_ENTRY(IC_XS_OPSIZE, 3, "requires an OPSIZE prefix, so " \
"operands change width") \
- ENUM_ENTRY(IC_64BIT_REXW, 4, "requires a REX.W prefix, so operands "\
+ ENUM_ENTRY(IC_64BIT_REXW, 5, "requires a REX.W prefix, so operands "\
"change width; overrides IC_OPSIZE") \
+ ENUM_ENTRY(IC_64BIT_REXW_ADSIZE, 6, "requires a REX.W prefix and 0x67 " \
+ "prefix") \
ENUM_ENTRY(IC_64BIT_OPSIZE, 3, "Just as meaningful as IC_OPSIZE") \
ENUM_ENTRY(IC_64BIT_ADSIZE, 3, "Just as meaningful as IC_ADSIZE") \
- ENUM_ENTRY(IC_64BIT_XD, 5, "XD instructions are SSE; REX.W is " \
+ ENUM_ENTRY(IC_64BIT_OPSIZE_ADSIZE, 4, "Just as meaningful as IC_OPSIZE/" \
+ "IC_ADSIZE") \
+ ENUM_ENTRY(IC_64BIT_XD, 6, "XD instructions are SSE; REX.W is " \
"secondary") \
- ENUM_ENTRY(IC_64BIT_XS, 5, "Just as meaningful as IC_64BIT_XD") \
+ ENUM_ENTRY(IC_64BIT_XS, 6, "Just as meaningful as IC_64BIT_XD") \
ENUM_ENTRY(IC_64BIT_XD_OPSIZE, 3, "Just as meaningful as IC_XD_OPSIZE") \
ENUM_ENTRY(IC_64BIT_XS_OPSIZE, 3, "Just as meaningful as IC_XS_OPSIZE") \
- ENUM_ENTRY(IC_64BIT_REXW_XS, 6, "OPSIZE could mean a different " \
+ ENUM_ENTRY(IC_64BIT_REXW_XS, 7, "OPSIZE could mean a different " \
"opcode") \
- ENUM_ENTRY(IC_64BIT_REXW_XD, 6, "Just as meaningful as " \
+ ENUM_ENTRY(IC_64BIT_REXW_XD, 7, "Just as meaningful as " \
"IC_64BIT_REXW_XS") \
- ENUM_ENTRY(IC_64BIT_REXW_OPSIZE, 7, "The Dynamic Duo! Prefer over all " \
+ ENUM_ENTRY(IC_64BIT_REXW_OPSIZE, 8, "The Dynamic Duo! Prefer over all " \
"else because this changes most " \
"operands' meaning") \
ENUM_ENTRY(IC_VEX, 1, "requires a VEX prefix") \
ENUM_ENTRY(IC_VEX_L_XS, 4, "requires VEX and the L and XS prefix")\
ENUM_ENTRY(IC_VEX_L_XD, 4, "requires VEX and the L and XD prefix")\
ENUM_ENTRY(IC_VEX_L_OPSIZE, 4, "requires VEX, L, and OpSize") \
- ENUM_ENTRY(IC_VEX_L_W_OPSIZE, 5, "requires VEX, L, W and OpSize")
-
+ ENUM_ENTRY(IC_VEX_L_W, 4, "requires VEX, L and W") \
+ ENUM_ENTRY(IC_VEX_L_W_XS, 5, "requires VEX, L, W and XS prefix") \
+ ENUM_ENTRY(IC_VEX_L_W_XD, 5, "requires VEX, L, W and XD prefix") \
+ ENUM_ENTRY(IC_VEX_L_W_OPSIZE, 5, "requires VEX, L, W and OpSize") \
+ ENUM_ENTRY(IC_EVEX, 1, "requires an EVEX prefix") \
+ ENUM_ENTRY(IC_EVEX_XS, 2, "requires EVEX and the XS prefix") \
+ ENUM_ENTRY(IC_EVEX_XD, 2, "requires EVEX and the XD prefix") \
+ ENUM_ENTRY(IC_EVEX_OPSIZE, 2, "requires EVEX and the OpSize prefix") \
+ ENUM_ENTRY(IC_EVEX_W, 3, "requires EVEX and the W prefix") \
+ ENUM_ENTRY(IC_EVEX_W_XS, 4, "requires EVEX, W, and XS prefix") \
+ ENUM_ENTRY(IC_EVEX_W_XD, 4, "requires EVEX, W, and XD prefix") \
+ ENUM_ENTRY(IC_EVEX_W_OPSIZE, 4, "requires EVEX, W, and OpSize") \
+ ENUM_ENTRY(IC_EVEX_L, 3, "requires EVEX and the L prefix") \
+ ENUM_ENTRY(IC_EVEX_L_XS, 4, "requires EVEX and the L and XS prefix")\
+ ENUM_ENTRY(IC_EVEX_L_XD, 4, "requires EVEX and the L and XD prefix")\
+ ENUM_ENTRY(IC_EVEX_L_OPSIZE, 4, "requires EVEX, L, and OpSize") \
+ ENUM_ENTRY(IC_EVEX_L_W, 3, "requires EVEX, L and W") \
+ ENUM_ENTRY(IC_EVEX_L_W_XS, 4, "requires EVEX, L, W and XS prefix") \
+ ENUM_ENTRY(IC_EVEX_L_W_XD, 4, "requires EVEX, L, W and XD prefix") \
+ ENUM_ENTRY(IC_EVEX_L_W_OPSIZE, 4, "requires EVEX, L, W and OpSize") \
+ ENUM_ENTRY(IC_EVEX_L2, 3, "requires EVEX and the L2 prefix") \
+ ENUM_ENTRY(IC_EVEX_L2_XS, 4, "requires EVEX and the L2 and XS prefix")\
+ ENUM_ENTRY(IC_EVEX_L2_XD, 4, "requires EVEX and the L2 and XD prefix")\
+ ENUM_ENTRY(IC_EVEX_L2_OPSIZE, 4, "requires EVEX, L2, and OpSize") \
+ ENUM_ENTRY(IC_EVEX_L2_W, 3, "requires EVEX, L2 and W") \
+ ENUM_ENTRY(IC_EVEX_L2_W_XS, 4, "requires EVEX, L2, W and XS prefix") \
+ ENUM_ENTRY(IC_EVEX_L2_W_XD, 4, "requires EVEX, L2, W and XD prefix") \
+ ENUM_ENTRY(IC_EVEX_L2_W_OPSIZE, 4, "requires EVEX, L2, W and OpSize") \
+ ENUM_ENTRY(IC_EVEX_K, 1, "requires an EVEX_K prefix") \
+ ENUM_ENTRY(IC_EVEX_XS_K, 2, "requires EVEX_K and the XS prefix") \
+ ENUM_ENTRY(IC_EVEX_XD_K, 2, "requires EVEX_K and the XD prefix") \
+ ENUM_ENTRY(IC_EVEX_OPSIZE_K, 2, "requires EVEX_K and the OpSize prefix") \
+ ENUM_ENTRY(IC_EVEX_W_K, 3, "requires EVEX_K and the W prefix") \
+ ENUM_ENTRY(IC_EVEX_W_XS_K, 4, "requires EVEX_K, W, and XS prefix") \
+ ENUM_ENTRY(IC_EVEX_W_XD_K, 4, "requires EVEX_K, W, and XD prefix") \
+ ENUM_ENTRY(IC_EVEX_W_OPSIZE_K, 4, "requires EVEX_K, W, and OpSize") \
+ ENUM_ENTRY(IC_EVEX_L_K, 3, "requires EVEX_K and the L prefix") \
+ ENUM_ENTRY(IC_EVEX_L_XS_K, 4, "requires EVEX_K and the L and XS prefix")\
+ ENUM_ENTRY(IC_EVEX_L_XD_K, 4, "requires EVEX_K and the L and XD prefix")\
+ ENUM_ENTRY(IC_EVEX_L_OPSIZE_K, 4, "requires EVEX_K, L, and OpSize") \
+ ENUM_ENTRY(IC_EVEX_L_W_K, 3, "requires EVEX_K, L and W") \
+ ENUM_ENTRY(IC_EVEX_L_W_XS_K, 4, "requires EVEX_K, L, W and XS prefix") \
+ ENUM_ENTRY(IC_EVEX_L_W_XD_K, 4, "requires EVEX_K, L, W and XD prefix") \
+ ENUM_ENTRY(IC_EVEX_L_W_OPSIZE_K, 4, "requires EVEX_K, L, W and OpSize") \
+ ENUM_ENTRY(IC_EVEX_L2_K, 3, "requires EVEX_K and the L2 prefix") \
+ ENUM_ENTRY(IC_EVEX_L2_XS_K, 4, "requires EVEX_K and the L2 and XS prefix")\
+ ENUM_ENTRY(IC_EVEX_L2_XD_K, 4, "requires EVEX_K and the L2 and XD prefix")\
+ ENUM_ENTRY(IC_EVEX_L2_OPSIZE_K, 4, "requires EVEX_K, L2, and OpSize") \
+ ENUM_ENTRY(IC_EVEX_L2_W_K, 3, "requires EVEX_K, L2 and W") \
+ ENUM_ENTRY(IC_EVEX_L2_W_XS_K, 4, "requires EVEX_K, L2, W and XS prefix") \
+ ENUM_ENTRY(IC_EVEX_L2_W_XD_K, 4, "requires EVEX_K, L2, W and XD prefix") \
+ ENUM_ENTRY(IC_EVEX_L2_W_OPSIZE_K, 4, "requires EVEX_K, L2, W and OpSize") \
+ ENUM_ENTRY(IC_EVEX_B, 1, "requires an EVEX_B prefix") \
+ ENUM_ENTRY(IC_EVEX_XS_B, 2, "requires EVEX_B and the XS prefix") \
+ ENUM_ENTRY(IC_EVEX_XD_B, 2, "requires EVEX_B and the XD prefix") \
+ ENUM_ENTRY(IC_EVEX_OPSIZE_B, 2, "requires EVEX_B and the OpSize prefix") \
+ ENUM_ENTRY(IC_EVEX_W_B, 3, "requires EVEX_B and the W prefix") \
+ ENUM_ENTRY(IC_EVEX_W_XS_B, 4, "requires EVEX_B, W, and XS prefix") \
+ ENUM_ENTRY(IC_EVEX_W_XD_B, 4, "requires EVEX_B, W, and XD prefix") \
+ ENUM_ENTRY(IC_EVEX_W_OPSIZE_B, 4, "requires EVEX_B, W, and OpSize") \
+ ENUM_ENTRY(IC_EVEX_L_B, 3, "requires EVEX_B and the L prefix") \
+ ENUM_ENTRY(IC_EVEX_L_XS_B, 4, "requires EVEX_B and the L and XS prefix")\
+ ENUM_ENTRY(IC_EVEX_L_XD_B, 4, "requires EVEX_B and the L and XD prefix")\
+ ENUM_ENTRY(IC_EVEX_L_OPSIZE_B, 4, "requires EVEX_B, L, and OpSize") \
+ ENUM_ENTRY(IC_EVEX_L_W_B, 3, "requires EVEX_B, L and W") \
+ ENUM_ENTRY(IC_EVEX_L_W_XS_B, 4, "requires EVEX_B, L, W and XS prefix") \
+ ENUM_ENTRY(IC_EVEX_L_W_XD_B, 4, "requires EVEX_B, L, W and XD prefix") \
+ ENUM_ENTRY(IC_EVEX_L_W_OPSIZE_B, 4, "requires EVEX_B, L, W and OpSize") \
+ ENUM_ENTRY(IC_EVEX_L2_B, 3, "requires EVEX_B and the L2 prefix") \
+ ENUM_ENTRY(IC_EVEX_L2_XS_B, 4, "requires EVEX_B and the L2 and XS prefix")\
+ ENUM_ENTRY(IC_EVEX_L2_XD_B, 4, "requires EVEX_B and the L2 and XD prefix")\
+ ENUM_ENTRY(IC_EVEX_L2_OPSIZE_B, 4, "requires EVEX_B, L2, and OpSize") \
+ ENUM_ENTRY(IC_EVEX_L2_W_B, 3, "requires EVEX_B, L2 and W") \
+ ENUM_ENTRY(IC_EVEX_L2_W_XS_B, 4, "requires EVEX_B, L2, W and XS prefix") \
+ ENUM_ENTRY(IC_EVEX_L2_W_XD_B, 4, "requires EVEX_B, L2, W and XD prefix") \
+ ENUM_ENTRY(IC_EVEX_L2_W_OPSIZE_B, 4, "requires EVEX_B, L2, W and OpSize") \
+ ENUM_ENTRY(IC_EVEX_K_B, 1, "requires EVEX_B and EVEX_K prefix") \
+ ENUM_ENTRY(IC_EVEX_XS_K_B, 2, "requires EVEX_B, EVEX_K and the XS prefix") \
+ ENUM_ENTRY(IC_EVEX_XD_K_B, 2, "requires EVEX_B, EVEX_K and the XD prefix") \
+ ENUM_ENTRY(IC_EVEX_OPSIZE_K_B, 2, "requires EVEX_B, EVEX_K and the OpSize prefix") \
+ ENUM_ENTRY(IC_EVEX_W_K_B, 3, "requires EVEX_B, EVEX_K and the W prefix") \
+ ENUM_ENTRY(IC_EVEX_W_XS_K_B, 4, "requires EVEX_B, EVEX_K, W, and XS prefix") \
+ ENUM_ENTRY(IC_EVEX_W_XD_K_B, 4, "requires EVEX_B, EVEX_K, W, and XD prefix") \
+ ENUM_ENTRY(IC_EVEX_W_OPSIZE_K_B, 4, "requires EVEX_B, EVEX_K, W, and OpSize") \
+ ENUM_ENTRY(IC_EVEX_L_K_B, 3, "requires EVEX_B, EVEX_K and the L prefix") \
+ ENUM_ENTRY(IC_EVEX_L_XS_K_B, 4, "requires EVEX_B, EVEX_K and the L and XS prefix")\
+ ENUM_ENTRY(IC_EVEX_L_XD_K_B, 4, "requires EVEX_B, EVEX_K and the L and XD prefix")\
+ ENUM_ENTRY(IC_EVEX_L_OPSIZE_K_B, 4, "requires EVEX_B, EVEX_K, L, and OpSize") \
+ ENUM_ENTRY(IC_EVEX_L_W_K_B, 3, "requires EVEX_B, EVEX_K, L and W") \
+ ENUM_ENTRY(IC_EVEX_L_W_XS_K_B, 4, "requires EVEX_B, EVEX_K, L, W and XS prefix") \
+ ENUM_ENTRY(IC_EVEX_L_W_XD_K_B, 4, "requires EVEX_B, EVEX_K, L, W and XD prefix") \
+ ENUM_ENTRY(IC_EVEX_L_W_OPSIZE_K_B,4, "requires EVEX_B, EVEX_K, L, W and OpSize") \
+ ENUM_ENTRY(IC_EVEX_L2_K_B, 3, "requires EVEX_B, EVEX_K and the L2 prefix") \
+ ENUM_ENTRY(IC_EVEX_L2_XS_K_B, 4, "requires EVEX_B, EVEX_K and the L2 and XS prefix")\
+ ENUM_ENTRY(IC_EVEX_L2_XD_K_B, 4, "requires EVEX_B, EVEX_K and the L2 and XD prefix")\
+ ENUM_ENTRY(IC_EVEX_L2_OPSIZE_K_B, 4, "requires EVEX_B, EVEX_K, L2, and OpSize") \
+ ENUM_ENTRY(IC_EVEX_L2_W_K_B, 3, "requires EVEX_B, EVEX_K, L2 and W") \
+ ENUM_ENTRY(IC_EVEX_L2_W_XS_K_B, 4, "requires EVEX_B, EVEX_K, L2, W and XS prefix") \
+ ENUM_ENTRY(IC_EVEX_L2_W_XD_K_B, 4, "requires EVEX_B, EVEX_K, L2, W and XD prefix") \
+ ENUM_ENTRY(IC_EVEX_L2_W_OPSIZE_K_B,4, "requires EVEX_B, EVEX_K, L2, W and OpSize") \
+ ENUM_ENTRY(IC_EVEX_KZ_B, 1, "requires EVEX_B and EVEX_KZ prefix") \
+ ENUM_ENTRY(IC_EVEX_XS_KZ_B, 2, "requires EVEX_B, EVEX_KZ and the XS prefix") \
+ ENUM_ENTRY(IC_EVEX_XD_KZ_B, 2, "requires EVEX_B, EVEX_KZ and the XD prefix") \
+ ENUM_ENTRY(IC_EVEX_OPSIZE_KZ_B, 2, "requires EVEX_B, EVEX_KZ and the OpSize prefix") \
+ ENUM_ENTRY(IC_EVEX_W_KZ_B, 3, "requires EVEX_B, EVEX_KZ and the W prefix") \
+ ENUM_ENTRY(IC_EVEX_W_XS_KZ_B, 4, "requires EVEX_B, EVEX_KZ, W, and XS prefix") \
+ ENUM_ENTRY(IC_EVEX_W_XD_KZ_B, 4, "requires EVEX_B, EVEX_KZ, W, and XD prefix") \
+ ENUM_ENTRY(IC_EVEX_W_OPSIZE_KZ_B, 4, "requires EVEX_B, EVEX_KZ, W, and OpSize") \
+ ENUM_ENTRY(IC_EVEX_L_KZ_B, 3, "requires EVEX_B, EVEX_KZ and the L prefix") \
+ ENUM_ENTRY(IC_EVEX_L_XS_KZ_B, 4, "requires EVEX_B, EVEX_KZ and the L and XS prefix")\
+ ENUM_ENTRY(IC_EVEX_L_XD_KZ_B, 4, "requires EVEX_B, EVEX_KZ and the L and XD prefix")\
+ ENUM_ENTRY(IC_EVEX_L_OPSIZE_KZ_B, 4, "requires EVEX_B, EVEX_KZ, L, and OpSize") \
+ ENUM_ENTRY(IC_EVEX_L_W_KZ_B, 3, "requires EVEX_B, EVEX_KZ, L and W") \
+ ENUM_ENTRY(IC_EVEX_L_W_XS_KZ_B, 4, "requires EVEX_B, EVEX_KZ, L, W and XS prefix") \
+ ENUM_ENTRY(IC_EVEX_L_W_XD_KZ_B, 4, "requires EVEX_B, EVEX_KZ, L, W and XD prefix") \
+ ENUM_ENTRY(IC_EVEX_L_W_OPSIZE_KZ_B, 4, "requires EVEX_B, EVEX_KZ, L, W and OpSize") \
+ ENUM_ENTRY(IC_EVEX_L2_KZ_B, 3, "requires EVEX_B, EVEX_KZ and the L2 prefix") \
+ ENUM_ENTRY(IC_EVEX_L2_XS_KZ_B, 4, "requires EVEX_B, EVEX_KZ and the L2 and XS prefix")\
+ ENUM_ENTRY(IC_EVEX_L2_XD_KZ_B, 4, "requires EVEX_B, EVEX_KZ and the L2 and XD prefix")\
+ ENUM_ENTRY(IC_EVEX_L2_OPSIZE_KZ_B, 4, "requires EVEX_B, EVEX_KZ, L2, and OpSize") \
+ ENUM_ENTRY(IC_EVEX_L2_W_KZ_B, 3, "requires EVEX_B, EVEX_KZ, L2 and W") \
+ ENUM_ENTRY(IC_EVEX_L2_W_XS_KZ_B, 4, "requires EVEX_B, EVEX_KZ, L2, W and XS prefix") \
+ ENUM_ENTRY(IC_EVEX_L2_W_XD_KZ_B, 4, "requires EVEX_B, EVEX_KZ, L2, W and XD prefix") \
+ ENUM_ENTRY(IC_EVEX_L2_W_OPSIZE_KZ_B, 4, "requires EVEX_B, EVEX_KZ, L2, W and OpSize") \
+ ENUM_ENTRY(IC_EVEX_KZ, 1, "requires an EVEX_KZ prefix") \
+ ENUM_ENTRY(IC_EVEX_XS_KZ, 2, "requires EVEX_KZ and the XS prefix") \
+ ENUM_ENTRY(IC_EVEX_XD_KZ, 2, "requires EVEX_KZ and the XD prefix") \
+ ENUM_ENTRY(IC_EVEX_OPSIZE_KZ, 2, "requires EVEX_KZ and the OpSize prefix") \
+ ENUM_ENTRY(IC_EVEX_W_KZ, 3, "requires EVEX_KZ and the W prefix") \
+ ENUM_ENTRY(IC_EVEX_W_XS_KZ, 4, "requires EVEX_KZ, W, and XS prefix") \
+ ENUM_ENTRY(IC_EVEX_W_XD_KZ, 4, "requires EVEX_KZ, W, and XD prefix") \
+ ENUM_ENTRY(IC_EVEX_W_OPSIZE_KZ, 4, "requires EVEX_KZ, W, and OpSize") \
+ ENUM_ENTRY(IC_EVEX_L_KZ, 3, "requires EVEX_KZ and the L prefix") \
+ ENUM_ENTRY(IC_EVEX_L_XS_KZ, 4, "requires EVEX_KZ and the L and XS prefix")\
+ ENUM_ENTRY(IC_EVEX_L_XD_KZ, 4, "requires EVEX_KZ and the L and XD prefix")\
+ ENUM_ENTRY(IC_EVEX_L_OPSIZE_KZ, 4, "requires EVEX_KZ, L, and OpSize") \
+ ENUM_ENTRY(IC_EVEX_L_W_KZ, 3, "requires EVEX_KZ, L and W") \
+ ENUM_ENTRY(IC_EVEX_L_W_XS_KZ, 4, "requires EVEX_KZ, L, W and XS prefix") \
+ ENUM_ENTRY(IC_EVEX_L_W_XD_KZ, 4, "requires EVEX_KZ, L, W and XD prefix") \
+ ENUM_ENTRY(IC_EVEX_L_W_OPSIZE_KZ, 4, "requires EVEX_KZ, L, W and OpSize") \
+ ENUM_ENTRY(IC_EVEX_L2_KZ, 3, "requires EVEX_KZ and the L2 prefix") \
+ ENUM_ENTRY(IC_EVEX_L2_XS_KZ, 4, "requires EVEX_KZ and the L2 and XS prefix")\
+ ENUM_ENTRY(IC_EVEX_L2_XD_KZ, 4, "requires EVEX_KZ and the L2 and XD prefix")\
+ ENUM_ENTRY(IC_EVEX_L2_OPSIZE_KZ, 4, "requires EVEX_KZ, L2, and OpSize") \
+ ENUM_ENTRY(IC_EVEX_L2_W_KZ, 3, "requires EVEX_KZ, L2 and W") \
+ ENUM_ENTRY(IC_EVEX_L2_W_XS_KZ, 4, "requires EVEX_KZ, L2, W and XS prefix") \
+ ENUM_ENTRY(IC_EVEX_L2_W_XD_KZ, 4, "requires EVEX_KZ, L2, W and XD prefix") \
+ ENUM_ENTRY(IC_EVEX_L2_W_OPSIZE_KZ, 4, "requires EVEX_KZ, L2, W and OpSize")
#define ENUM_ENTRY(n, r, d) n,
-typedef enum {
+enum InstructionContext {
INSTRUCTION_CONTEXTS
IC_max
-} InstructionContext;
+};
#undef ENUM_ENTRY
-/*
- * Opcode types, which determine which decode table to use, both in the Intel
- * manual and also for the decoder.
- */
-typedef enum {
+// Opcode types, which determine which decode table to use, both in the Intel
+// manual and also for the decoder.
+enum OpcodeType {
ONEBYTE = 0,
TWOBYTE = 1,
THREEBYTE_38 = 2,
THREEBYTE_3A = 3,
- THREEBYTE_A6 = 4,
- THREEBYTE_A7 = 5
-} OpcodeType;
-
-/*
- * The following structs are used for the hierarchical decode table. After
- * determining the instruction's class (i.e., which IC_* constant applies to
- * it), the decoder reads the opcode. Some instructions require specific
- * values of the ModR/M byte, so the ModR/M byte indexes into the final table.
- *
- * If a ModR/M byte is not required, "required" is left unset, and the values
- * for each instructionID are identical.
- */
+ XOP8_MAP = 4,
+ XOP9_MAP = 5,
+ XOPA_MAP = 6
+};
+// The following structs are used for the hierarchical decode table. After
+// determining the instruction's class (i.e., which IC_* constant applies to
+// it), the decoder reads the opcode. Some instructions require specific
+// values of the ModR/M byte, so the ModR/M byte indexes into the final table.
+//
+// If a ModR/M byte is not required, "required" is left unset, and the values
+// for each instructionID are identical.
typedef uint16_t InstrUID;
-/*
- * ModRMDecisionType - describes the type of ModR/M decision, allowing the
- * consumer to determine the number of entries in it.
- *
- * MODRM_ONEENTRY - No matter what the value of the ModR/M byte is, the decoded
- * instruction is the same.
- * MODRM_SPLITRM - If the ModR/M byte is between 0x00 and 0xbf, the opcode
- * corresponds to one instruction; otherwise, it corresponds to
- * a different instruction.
- * MODRM_SPLITREG - ModR/M byte divided by 8 is used to select instruction. This
- corresponds to instructions that use reg field as opcode
- * MODRM_FULL - Potentially, each value of the ModR/M byte could correspond
- * to a different instruction.
- */
-
+// ModRMDecisionType - describes the type of ModR/M decision, allowing the
+// consumer to determine the number of entries in it.
+//
+// MODRM_ONEENTRY - No matter what the value of the ModR/M byte is, the decoded
+// instruction is the same.
+// MODRM_SPLITRM - If the ModR/M byte is between 0x00 and 0xbf, the opcode
+// corresponds to one instruction; otherwise, it corresponds to
+// a different instruction.
+// MODRM_SPLITMISC- If the ModR/M byte is between 0x00 and 0xbf, ModR/M byte
+// divided by 8 is used to select instruction; otherwise, each
+// value of the ModR/M byte could correspond to a different
+// instruction.
+// MODRM_SPLITREG - ModR/M byte divided by 8 is used to select instruction. This
+// corresponds to instructions that use reg field as opcode
+// MODRM_FULL - Potentially, each value of the ModR/M byte could correspond
+// to a different instruction.
#define MODRMTYPES \
ENUM_ENTRY(MODRM_ONEENTRY) \
ENUM_ENTRY(MODRM_SPLITRM) \
+ ENUM_ENTRY(MODRM_SPLITMISC) \
ENUM_ENTRY(MODRM_SPLITREG) \
ENUM_ENTRY(MODRM_FULL)
#define ENUM_ENTRY(n) n,
-typedef enum {
+enum ModRMDecisionType {
MODRMTYPES
MODRM_max
-} ModRMDecisionType;
-#undef ENUM_ENTRY
-
-/*
- * ModRMDecision - Specifies whether a ModR/M byte is needed and (if so) which
- * instruction each possible value of the ModR/M byte corresponds to. Once
- * this information is known, we have narrowed down to a single instruction.
- */
-struct ModRMDecision {
- uint8_t modrm_type;
-
- /* The macro below must be defined wherever this file is included. */
- INSTRUCTION_IDS
-};
-
-/*
- * OpcodeDecision - Specifies which set of ModR/M->instruction tables to look at
- * given a particular opcode.
- */
-struct OpcodeDecision {
- struct ModRMDecision modRMDecisions[256];
-};
-
-/*
- * ContextDecision - Specifies which opcode->instruction tables to look at given
- * a particular context (set of attributes). Since there are many possible
- * contexts, the decoder first uses CONTEXTS_SYM to determine which context
- * applies given a specific set of attributes. Hence there are only IC_max
- * entries in this table, rather than 2^(ATTR_max).
- */
-struct ContextDecision {
- struct OpcodeDecision opcodeDecisions[IC_max];
};
+#undef ENUM_ENTRY
-/*
- * Physical encodings of instruction operands.
- */
+#define CASE_ENCODING_RM \
+ case ENCODING_RM: \
+ case ENCODING_RM_CD2: \
+ case ENCODING_RM_CD4: \
+ case ENCODING_RM_CD8: \
+ case ENCODING_RM_CD16: \
+ case ENCODING_RM_CD32: \
+ case ENCODING_RM_CD64
+// Physical encodings of instruction operands.
#define ENCODINGS \
ENUM_ENTRY(ENCODING_NONE, "") \
ENUM_ENTRY(ENCODING_REG, "Register operand in ModR/M byte.") \
ENUM_ENTRY(ENCODING_RM, "R/M operand in ModR/M byte.") \
+ ENUM_ENTRY(ENCODING_RM_CD2, "R/M operand with CDisp scaling of 2") \
+ ENUM_ENTRY(ENCODING_RM_CD4, "R/M operand with CDisp scaling of 4") \
+ ENUM_ENTRY(ENCODING_RM_CD8, "R/M operand with CDisp scaling of 8") \
+ ENUM_ENTRY(ENCODING_RM_CD16,"R/M operand with CDisp scaling of 16") \
+ ENUM_ENTRY(ENCODING_RM_CD32,"R/M operand with CDisp scaling of 32") \
+ ENUM_ENTRY(ENCODING_RM_CD64,"R/M operand with CDisp scaling of 64") \
ENUM_ENTRY(ENCODING_VVVV, "Register operand in VEX.vvvv byte.") \
+ ENUM_ENTRY(ENCODING_WRITEMASK, "Register operand in EVEX.aaa byte.") \
ENUM_ENTRY(ENCODING_CB, "1-byte code offset (possible new CS value)") \
ENUM_ENTRY(ENCODING_CW, "2-byte") \
ENUM_ENTRY(ENCODING_CD, "4-byte") \
ENUM_ENTRY(ENCODING_RW, "(AX..DI, R8W..R15W)") \
ENUM_ENTRY(ENCODING_RD, "(EAX..EDI, R8D..R15D)") \
ENUM_ENTRY(ENCODING_RO, "(RAX..RDI, R8..R15)") \
- ENUM_ENTRY(ENCODING_I, "Position on floating-point stack added to the " \
- "opcode byte") \
+ ENUM_ENTRY(ENCODING_FP, "Position on floating-point stack in ModR/M " \
+ "byte.") \
\
ENUM_ENTRY(ENCODING_Iv, "Immediate of operand size") \
ENUM_ENTRY(ENCODING_Ia, "Immediate of address size") \
ENUM_ENTRY(ENCODING_Rv, "Register code of operand size added to the " \
"opcode byte") \
ENUM_ENTRY(ENCODING_DUP, "Duplicate of another operand; ID is encoded " \
- "in type")
+ "in type") \
+ ENUM_ENTRY(ENCODING_SI, "Source index; encoded in OpSize/Adsize prefix") \
+ ENUM_ENTRY(ENCODING_DI, "Destination index; encoded in prefixes")
#define ENUM_ENTRY(n, d) n,
- typedef enum {
- ENCODINGS
- ENCODING_max
- } OperandEncoding;
+enum OperandEncoding {
+ ENCODINGS
+ ENCODING_max
+};
#undef ENUM_ENTRY
-/*
- * Semantic interpretations of instruction operands.
- */
-
+// Semantic interpretations of instruction operands.
#define TYPES \
ENUM_ENTRY(TYPE_NONE, "") \
ENUM_ENTRY(TYPE_REL8, "1-byte immediate address") \
ENUM_ENTRY(TYPE_IMM64, "8-byte") \
ENUM_ENTRY(TYPE_IMM3, "1-byte immediate operand between 0 and 7") \
ENUM_ENTRY(TYPE_IMM5, "1-byte immediate operand between 0 and 31") \
+ ENUM_ENTRY(TYPE_UIMM8, "1-byte unsigned immediate operand") \
ENUM_ENTRY(TYPE_RM8, "1-byte register or memory operand") \
ENUM_ENTRY(TYPE_RM16, "2-byte") \
ENUM_ENTRY(TYPE_RM32, "4-byte") \
ENUM_ENTRY(TYPE_M1616, "2+2-byte segment+offset address") \
ENUM_ENTRY(TYPE_M1632, "2+4-byte") \
ENUM_ENTRY(TYPE_M1664, "2+8-byte") \
- ENUM_ENTRY(TYPE_M16_32, "2+4-byte two-part memory operand (LIDT, LGDT)") \
- ENUM_ENTRY(TYPE_M16_16, "2+2-byte (BOUND)") \
- ENUM_ENTRY(TYPE_M32_32, "4+4-byte (BOUND)") \
- ENUM_ENTRY(TYPE_M16_64, "2+8-byte (LIDT, LGDT)") \
+ ENUM_ENTRY(TYPE_SRCIDX8, "1-byte memory at source index") \
+ ENUM_ENTRY(TYPE_SRCIDX16, "2-byte memory at source index") \
+ ENUM_ENTRY(TYPE_SRCIDX32, "4-byte memory at source index") \
+ ENUM_ENTRY(TYPE_SRCIDX64, "8-byte memory at source index") \
+ ENUM_ENTRY(TYPE_DSTIDX8, "1-byte memory at destination index") \
+ ENUM_ENTRY(TYPE_DSTIDX16, "2-byte memory at destination index") \
+ ENUM_ENTRY(TYPE_DSTIDX32, "4-byte memory at destination index") \
+ ENUM_ENTRY(TYPE_DSTIDX64, "8-byte memory at destination index") \
ENUM_ENTRY(TYPE_MOFFS8, "1-byte memory offset (relative to segment " \
"base)") \
ENUM_ENTRY(TYPE_MOFFS16, "2-byte") \
ENUM_ENTRY(TYPE_M32FP, "32-bit IEE754 memory floating-point operand") \
ENUM_ENTRY(TYPE_M64FP, "64-bit") \
ENUM_ENTRY(TYPE_M80FP, "80-bit extended") \
- ENUM_ENTRY(TYPE_M16INT, "2-byte memory integer operand for use in " \
- "floating-point instructions") \
- ENUM_ENTRY(TYPE_M32INT, "4-byte") \
- ENUM_ENTRY(TYPE_M64INT, "8-byte") \
ENUM_ENTRY(TYPE_ST, "Position on the floating-point stack") \
- ENUM_ENTRY(TYPE_MM, "MMX register operand") \
- ENUM_ENTRY(TYPE_MM32, "4-byte MMX register or memory operand") \
- ENUM_ENTRY(TYPE_MM64, "8-byte") \
+ ENUM_ENTRY(TYPE_MM64, "8-byte MMX register") \
ENUM_ENTRY(TYPE_XMM, "XMM register operand") \
ENUM_ENTRY(TYPE_XMM32, "4-byte XMM register or memory operand") \
ENUM_ENTRY(TYPE_XMM64, "8-byte") \
ENUM_ENTRY(TYPE_XMM128, "16-byte") \
ENUM_ENTRY(TYPE_XMM256, "32-byte") \
+ ENUM_ENTRY(TYPE_XMM512, "64-byte") \
+ ENUM_ENTRY(TYPE_VK1, "1-bit") \
+ ENUM_ENTRY(TYPE_VK2, "2-bit") \
+ ENUM_ENTRY(TYPE_VK4, "4-bit") \
+ ENUM_ENTRY(TYPE_VK8, "8-bit") \
+ ENUM_ENTRY(TYPE_VK16, "16-bit") \
+ ENUM_ENTRY(TYPE_VK32, "32-bit") \
+ ENUM_ENTRY(TYPE_VK64, "64-bit") \
ENUM_ENTRY(TYPE_XMM0, "Implicit use of XMM0") \
ENUM_ENTRY(TYPE_SEGMENTREG, "Segment register operand") \
ENUM_ENTRY(TYPE_DEBUGREG, "Debug register operand") \
ENUM_ENTRY(TYPE_M512, "512-bit FPU/MMX/XMM/MXCSR state")
#define ENUM_ENTRY(n, d) n,
-typedef enum {
+enum OperandType {
TYPES
TYPE_max
-} OperandType;
+};
#undef ENUM_ENTRY
-/*
- * OperandSpecifier - The specification for how to extract and interpret one
- * operand.
- */
+/// \brief The specification for how to extract and interpret one operand.
struct OperandSpecifier {
uint8_t encoding;
uint8_t type;
};
-/*
- * Indicates where the opcode modifier (if any) is to be found. Extended
- * opcodes with AddRegFrm have the opcode modifier in the ModR/M byte.
- */
-
+// Indicates where the opcode modifier (if any) is to be found. Extended
+// opcodes with AddRegFrm have the opcode modifier in the ModR/M byte.
#define MODIFIER_TYPES \
- ENUM_ENTRY(MODIFIER_NONE) \
- ENUM_ENTRY(MODIFIER_OPCODE) \
- ENUM_ENTRY(MODIFIER_MODRM)
+ ENUM_ENTRY(MODIFIER_NONE)
#define ENUM_ENTRY(n) n,
-typedef enum {
+enum ModifierType {
MODIFIER_TYPES
MODIFIER_max
-} ModifierType;
+};
#undef ENUM_ENTRY
-#define X86_MAX_OPERANDS 5
+static const unsigned X86_MAX_OPERANDS = 6;
-/*
- * The specification for how to extract and interpret a full instruction and
- * its operands.
- */
-struct InstructionSpecifier {
- uint8_t modifierType;
- uint8_t modifierBase;
- struct OperandSpecifier operands[X86_MAX_OPERANDS];
-
- /* The macro below must be defined wherever this file is included. */
- INSTRUCTION_SPECIFIER_FIELDS
-};
-
-/*
- * Decoding mode for the Intel disassembler. 16-bit, 32-bit, and 64-bit mode
- * are supported, and represent real mode, IA-32e, and IA-32e in 64-bit mode,
- * respectively.
- */
-typedef enum {
+/// Decoding mode for the Intel disassembler. 16-bit, 32-bit, and 64-bit mode
+/// are supported, and represent real mode, IA-32e, and IA-32e in 64-bit mode,
+/// respectively.
+enum DisassemblerMode {
MODE_16BIT,
MODE_32BIT,
MODE_64BIT
-} DisassemblerMode;
+};
+
+} // namespace X86Disassembler
+} // namespace llvm
#endif