index e209c29522d05dbd05f6c2518d2de8eb51eea8d4..450f0771d908a011e02695a5cc64039eee62e8d0 100644 (file)
#include "llvm/CodeGen/SelectionDAGISel.h"
#include "llvm/CodeGen/ValueTypes.h"
#include "llvm/IR/CallingConv.h"
+#include "llvm/IR/Constants.h"
#include "llvm/IR/DerivedTypes.h"
#include "llvm/IR/Function.h"
#include "llvm/IR/GlobalAlias.h"
case XCoreISD::CRC8 : return "XCoreISD::CRC8";
case XCoreISD::BR_JT : return "XCoreISD::BR_JT";
case XCoreISD::BR_JT32 : return "XCoreISD::BR_JT32";
+ case XCoreISD::FRAME_TO_ARGS_OFFSET : return "XCoreISD::FRAME_TO_ARGS_OFFSET";
+ case XCoreISD::EH_RETURN : return "XCoreISD::EH_RETURN";
+ case XCoreISD::MEMBARRIER : return "XCoreISD::MEMBARRIER";
default : return NULL;
}
}
setOperationAction(ISD::STACKRESTORE, MVT::Other, Expand);
setOperationAction(ISD::DYNAMIC_STACKALLOC, MVT::i32, Expand);
+ // Exception handling
+ setOperationAction(ISD::EH_RETURN, MVT::Other, Custom);
+ setExceptionPointerRegister(XCore::R0);
+ setExceptionSelectorRegister(XCore::R1);
+ setOperationAction(ISD::FRAME_TO_ARGS_OFFSET, MVT::i32, Custom);
+
+ // Atomic operations
+ // We request a fence for ATOMIC_* instructions, to reduce them to Monotonic.
+ // As we are always Sequential Consistent, an ATOMIC_FENCE becomes a no OP.
+ setInsertFencesForAtomic(true);
+ setOperationAction(ISD::ATOMIC_FENCE, MVT::Other, Custom);
+ setOperationAction(ISD::ATOMIC_LOAD, MVT::i32, Custom);
+ setOperationAction(ISD::ATOMIC_STORE, MVT::i32, Custom);
+
// TRAMPOLINE is custom lowered.
setOperationAction(ISD::INIT_TRAMPOLINE, MVT::Other, Custom);
setOperationAction(ISD::ADJUST_TRAMPOLINE, MVT::Other, Custom);
// We have target-specific dag combine patterns for the following nodes:
setTargetDAGCombine(ISD::STORE);
setTargetDAGCombine(ISD::ADD);
+ setTargetDAGCombine(ISD::INTRINSIC_VOID);
+ setTargetDAGCombine(ISD::INTRINSIC_W_CHAIN);
setMinFunctionAlignment(1);
+ setPrefFunctionAlignment(2);
+}
+
+bool XCoreTargetLowering::isZExtFree(SDValue Val, EVT VT2) const {
+ if (Val.getOpcode() != ISD::LOAD)
+ return false;
+
+ EVT VT1 = Val.getValueType();
+ if (!VT1.isSimple() || !VT1.isInteger() ||
+ !VT2.isSimple() || !VT2.isInteger())
+ return false;
+
+ switch (VT1.getSimpleVT().SimpleTy) {
+ default: break;
+ case MVT::i8:
+ return true;
+ }
+
+ return false;
}
SDValue XCoreTargetLowering::
LowerOperation(SDValue Op, SelectionDAG &DAG) const {
switch (Op.getOpcode())
{
+ case ISD::EH_RETURN: return LowerEH_RETURN(Op, DAG);
case ISD::GlobalAddress: return LowerGlobalAddress(Op, DAG);
case ISD::BlockAddress: return LowerBlockAddress(Op, DAG);
case ISD::ConstantPool: return LowerConstantPool(Op, DAG);
case ISD::ADD:
case ISD::SUB: return ExpandADDSUB(Op.getNode(), DAG);
case ISD::FRAMEADDR: return LowerFRAMEADDR(Op, DAG);
+ case ISD::RETURNADDR: return LowerRETURNADDR(Op, DAG);
+ case ISD::FRAME_TO_ARGS_OFFSET: return LowerFRAME_TO_ARGS_OFFSET(Op, DAG);
case ISD::INIT_TRAMPOLINE: return LowerINIT_TRAMPOLINE(Op, DAG);
case ISD::ADJUST_TRAMPOLINE: return LowerADJUST_TRAMPOLINE(Op, DAG);
case ISD::INTRINSIC_WO_CHAIN: return LowerINTRINSIC_WO_CHAIN(Op, DAG);
+ case ISD::ATOMIC_FENCE: return LowerATOMIC_FENCE(Op, DAG);
+ case ISD::ATOMIC_LOAD: return LowerATOMIC_LOAD(Op, DAG);
+ case ISD::ATOMIC_STORE: return LowerATOMIC_STORE(Op, DAG);
default:
llvm_unreachable("unimplemented operand");
}
if (const GlobalAlias *GA = dyn_cast<GlobalAlias>(GV))
UnderlyingGV = GA->resolveAliasedGlobal();
if (const GlobalVariable *GVar = dyn_cast<GlobalVariable>(UnderlyingGV)) {
- if (GVar->isConstant())
+ if ( ( GVar->isConstant() &&
+ UnderlyingGV->isLocalLinkage(GV->getLinkage()) )
+ || ( GVar->hasSection() &&
+ StringRef(GVar->getSection()).startswith(".cp.") ) )
return DAG.getNode(XCoreISD::CPRelativeWrapper, dl, MVT::i32, GA);
return DAG.getNode(XCoreISD::DPRelativeWrapper, dl, MVT::i32, GA);
}
return DAG.getNode(XCoreISD::PCRelativeWrapper, dl, MVT::i32, GA);
}
+static bool IsSmallObject(const GlobalValue *GV, const XCoreTargetLowering &XTL) {
+ if (XTL.getTargetMachine().getCodeModel() == CodeModel::Small)
+ return true;
+
+ Type *ObjType = GV->getType()->getPointerElementType();
+ if (!ObjType->isSized())
+ return false;
+
+ unsigned ObjSize = XTL.getDataLayout()->getTypeAllocSize(ObjType);
+ return ObjSize < CodeModelLargeSize && ObjSize != 0;
+}
+
SDValue XCoreTargetLowering::
LowerGlobalAddress(SDValue Op, SelectionDAG &DAG) const
{
- SDLoc DL(Op);
const GlobalAddressSDNode *GN = cast<GlobalAddressSDNode>(Op);
const GlobalValue *GV = GN->getGlobal();
+ SDLoc DL(GN);
int64_t Offset = GN->getOffset();
- // We can only fold positive offsets that are a multiple of the word size.
- int64_t FoldedOffset = std::max(Offset & ~3, (int64_t)0);
- SDValue GA = DAG.getTargetGlobalAddress(GV, DL, MVT::i32, FoldedOffset);
- GA = getGlobalAddressWrapper(GA, GV, DAG);
- // Handle the rest of the offset.
- if (Offset != FoldedOffset) {
- SDValue Remaining = DAG.getConstant(Offset - FoldedOffset, MVT::i32);
- GA = DAG.getNode(ISD::ADD, DL, MVT::i32, GA, Remaining);
+ if (IsSmallObject(GV, *this)) {
+ // We can only fold positive offsets that are a multiple of the word size.
+ int64_t FoldedOffset = std::max(Offset & ~3, (int64_t)0);
+ SDValue GA = DAG.getTargetGlobalAddress(GV, DL, MVT::i32, FoldedOffset);
+ GA = getGlobalAddressWrapper(GA, GV, DAG);
+ // Handle the rest of the offset.
+ if (Offset != FoldedOffset) {
+ SDValue Remaining = DAG.getConstant(Offset - FoldedOffset, MVT::i32);
+ GA = DAG.getNode(ISD::ADD, DL, MVT::i32, GA, Remaining);
+ }
+ return GA;
+ } else {
+ // Ideally we would not fold in offset with an index <= 11.
+ Type *Ty = Type::getInt8PtrTy(*DAG.getContext());
+ Constant *GA = ConstantExpr::getBitCast(const_cast<GlobalValue*>(GV), Ty);
+ Ty = Type::getInt32Ty(*DAG.getContext());
+ Constant *Idx = ConstantInt::get(Ty, Offset);
+ Constant *GAI = ConstantExpr::getGetElementPtr(GA, Idx);
+ SDValue CP = DAG.getConstantPool(GAI, MVT::i32);
+ return DAG.getLoad(getPointerTy(), DL, DAG.getEntryNode(), CP,
+ MachinePointerInfo(), false, false, false, 0);
}
- return GA;
}
SDValue XCoreTargetLowering::
SDValue Res;
if (CP->isMachineConstantPoolEntry()) {
Res = DAG.getTargetConstantPool(CP->getMachineCPVal(), PtrVT,
- CP->getAlignment());
+ CP->getAlignment(), CP->getOffset());
} else {
Res = DAG.getTargetConstantPool(CP->getConstVal(), PtrVT,
- CP->getAlignment());
+ CP->getAlignment(), CP->getOffset());
}
return DAG.getNode(XCoreISD::CPRelativeWrapper, dl, MVT::i32, Res);
}
SDValue XCoreTargetLowering::LowerFRAMEADDR(SDValue Op,
SelectionDAG &DAG) const {
- SDLoc dl(Op);
+ // This nodes represent llvm.frameaddress on the DAG.
+ // It takes one operand, the index of the frame address to return.
+ // An index of zero corresponds to the current function's frame address.
+ // An index of one to the parent's frame address, and so on.
// Depths > 0 not supported yet!
if (cast<ConstantSDNode>(Op.getOperand(0))->getZExtValue() > 0)
return SDValue();
MachineFunction &MF = DAG.getMachineFunction();
const TargetRegisterInfo *RegInfo = getTargetMachine().getRegisterInfo();
- return DAG.getCopyFromReg(DAG.getEntryNode(), dl,
+ return DAG.getCopyFromReg(DAG.getEntryNode(), SDLoc(Op),
RegInfo->getFrameRegister(MF), MVT::i32);
}
+SDValue XCoreTargetLowering::
+LowerRETURNADDR(SDValue Op, SelectionDAG &DAG) const {
+ // This nodes represent llvm.returnaddress on the DAG.
+ // It takes one operand, the index of the return address to return.
+ // An index of zero corresponds to the current function's return address.
+ // An index of one to the parent's return address, and so on.
+ // Depths > 0 not supported yet!
+ if (cast<ConstantSDNode>(Op.getOperand(0))->getZExtValue() > 0)
+ return SDValue();
+
+ MachineFunction &MF = DAG.getMachineFunction();
+ XCoreFunctionInfo *XFI = MF.getInfo<XCoreFunctionInfo>();
+ int FI = XFI->createLRSpillSlot(MF);
+ SDValue FIN = DAG.getFrameIndex(FI, MVT::i32);
+ return DAG.getLoad(getPointerTy(), SDLoc(Op), DAG.getEntryNode(), FIN,
+ MachinePointerInfo::getFixedStack(FI), false, false,
+ false, 0);
+}
+
+SDValue XCoreTargetLowering::
+LowerFRAME_TO_ARGS_OFFSET(SDValue Op, SelectionDAG &DAG) const {
+ // This node represents offset from frame pointer to first on-stack argument.
+ // This is needed for correct stack adjustment during unwind.
+ // However, we don't know the offset until after the frame has be finalised.
+ // This is done during the XCoreFTAOElim pass.
+ return DAG.getNode(XCoreISD::FRAME_TO_ARGS_OFFSET, SDLoc(Op), MVT::i32);
+}
+
+SDValue XCoreTargetLowering::
+LowerEH_RETURN(SDValue Op, SelectionDAG &DAG) const {
+ // OUTCHAIN = EH_RETURN(INCHAIN, OFFSET, HANDLER)
+ // This node represents 'eh_return' gcc dwarf builtin, which is used to
+ // return from exception. The general meaning is: adjust stack by OFFSET and
+ // pass execution to HANDLER.
+ MachineFunction &MF = DAG.getMachineFunction();
+ SDValue Chain = Op.getOperand(0);
+ SDValue Offset = Op.getOperand(1);
+ SDValue Handler = Op.getOperand(2);
+ SDLoc dl(Op);
+
+ // Absolute SP = (FP + FrameToArgs) + Offset
+ const TargetRegisterInfo *RegInfo = getTargetMachine().getRegisterInfo();
+ SDValue Stack = DAG.getCopyFromReg(DAG.getEntryNode(), dl,
+ RegInfo->getFrameRegister(MF), MVT::i32);
+ SDValue FrameToArgs = DAG.getNode(XCoreISD::FRAME_TO_ARGS_OFFSET, dl,
+ MVT::i32);
+ Stack = DAG.getNode(ISD::ADD, dl, MVT::i32, Stack, FrameToArgs);
+ Stack = DAG.getNode(ISD::ADD, dl, MVT::i32, Stack, Offset);
+
+ // R0=ExceptionPointerRegister R1=ExceptionSelectorRegister
+ // which leaves 2 caller saved registers, R2 & R3 for us to use.
+ unsigned StackReg = XCore::R2;
+ unsigned HandlerReg = XCore::R3;
+
+ SDValue OutChains[] = {
+ DAG.getCopyToReg(Chain, dl, StackReg, Stack),
+ DAG.getCopyToReg(Chain, dl, HandlerReg, Handler)
+ };
+
+ Chain = DAG.getNode(ISD::TokenFactor, dl, MVT::Other, OutChains, 2);
+
+ return DAG.getNode(XCoreISD::EH_RETURN, dl, MVT::Other, Chain,
+ DAG.getRegister(StackReg, MVT::i32),
+ DAG.getRegister(HandlerReg, MVT::i32));
+
+}
+
SDValue XCoreTargetLowering::
LowerADJUST_TRAMPOLINE(SDValue Op, SelectionDAG &DAG) const {
return Op.getOperand(0);
return SDValue();
}
+SDValue XCoreTargetLowering::
+LowerATOMIC_FENCE(SDValue Op, SelectionDAG &DAG) const {
+ SDLoc DL(Op);
+ return DAG.getNode(XCoreISD::MEMBARRIER, DL, MVT::Other, Op.getOperand(0));
+}
+
+SDValue XCoreTargetLowering::
+LowerATOMIC_LOAD(SDValue Op, SelectionDAG &DAG) const {
+ AtomicSDNode *N = cast<AtomicSDNode>(Op);
+ assert(N->getOpcode() == ISD::ATOMIC_LOAD && "Bad Atomic OP");
+ assert(N->getOrdering() <= Monotonic &&
+ "setInsertFencesForAtomic(true) and yet greater than Monotonic");
+ if (N->getMemoryVT() == MVT::i32) {
+ if (N->getAlignment() < 4)
+ report_fatal_error("atomic load must be aligned");
+ return DAG.getLoad(getPointerTy(), SDLoc(Op), N->getChain(),
+ N->getBasePtr(), N->getPointerInfo(),
+ N->isVolatile(), N->isNonTemporal(),
+ N->isInvariant(), N->getAlignment(),
+ N->getTBAAInfo(), N->getRanges());
+ }
+ if (N->getMemoryVT() == MVT::i16) {
+ if (N->getAlignment() < 2)
+ report_fatal_error("atomic load must be aligned");
+ return DAG.getExtLoad(ISD::EXTLOAD, SDLoc(Op), MVT::i32, N->getChain(),
+ N->getBasePtr(), N->getPointerInfo(), MVT::i16,
+ N->isVolatile(), N->isNonTemporal(),
+ N->getAlignment(), N->getTBAAInfo());
+ }
+ if (N->getMemoryVT() == MVT::i8)
+ return DAG.getExtLoad(ISD::EXTLOAD, SDLoc(Op), MVT::i32, N->getChain(),
+ N->getBasePtr(), N->getPointerInfo(), MVT::i8,
+ N->isVolatile(), N->isNonTemporal(),
+ N->getAlignment(), N->getTBAAInfo());
+ return SDValue();
+}
+
+SDValue XCoreTargetLowering::
+LowerATOMIC_STORE(SDValue Op, SelectionDAG &DAG) const {
+ AtomicSDNode *N = cast<AtomicSDNode>(Op);
+ assert(N->getOpcode() == ISD::ATOMIC_STORE && "Bad Atomic OP");
+ assert(N->getOrdering() <= Monotonic &&
+ "setInsertFencesForAtomic(true) and yet greater than Monotonic");
+ if (N->getMemoryVT() == MVT::i32) {
+ if (N->getAlignment() < 4)
+ report_fatal_error("atomic store must be aligned");
+ return DAG.getStore(N->getChain(), SDLoc(Op), N->getVal(),
+ N->getBasePtr(), N->getPointerInfo(),
+ N->isVolatile(), N->isNonTemporal(),
+ N->getAlignment(), N->getTBAAInfo());
+ }
+ if (N->getMemoryVT() == MVT::i16) {
+ if (N->getAlignment() < 2)
+ report_fatal_error("atomic store must be aligned");
+ return DAG.getTruncStore(N->getChain(), SDLoc(Op), N->getVal(),
+ N->getBasePtr(), N->getPointerInfo(), MVT::i16,
+ N->isVolatile(), N->isNonTemporal(),
+ N->getAlignment(), N->getTBAAInfo());
+ }
+ if (N->getMemoryVT() == MVT::i8)
+ return DAG.getTruncStore(N->getChain(), SDLoc(Op), N->getVal(),
+ N->getBasePtr(), N->getPointerInfo(), MVT::i8,
+ N->isVolatile(), N->isNonTemporal(),
+ N->getAlignment(), N->getTBAAInfo());
+ return SDValue();
+}
+
//===----------------------------------------------------------------------===//
// Calling Convention Implementation
//===----------------------------------------------------------------------===//
ArgDI != ArgDE; ++ArgDI) {
if (ArgDI->Flags.isByVal() && ArgDI->Flags.getByValSize()) {
unsigned Size = ArgDI->Flags.getByValSize();
- unsigned Align = ArgDI->Flags.getByValAlign();
+ unsigned Align = std::max(StackSlotSize, ArgDI->Flags.getByValAlign());
// Create a new object on the stack and copy the pointee into it.
- int FI = MFI->CreateStackObject(Size, Align, false, false);
+ int FI = MFI->CreateStackObject(Size, Align, false);
SDValue FIN = DAG.getFrameIndex(FI, MVT::i32);
InVals.push_back(FIN);
MemOps.push_back(DAG.getMemcpy(Chain, dl, FIN, ArgDI->SDV,
SDLoc dl(N);
switch (N->getOpcode()) {
default: break;
+ case ISD::INTRINSIC_VOID:
+ switch (cast<ConstantSDNode>(N->getOperand(1))->getZExtValue()) {
+ case Intrinsic::xcore_outt:
+ case Intrinsic::xcore_outct:
+ case Intrinsic::xcore_chkct: {
+ SDValue OutVal = N->getOperand(3);
+ // These instructions ignore the high bits.
+ if (OutVal.hasOneUse()) {
+ unsigned BitWidth = OutVal.getValueSizeInBits();
+ APInt DemandedMask = APInt::getLowBitsSet(BitWidth, 8);
+ APInt KnownZero, KnownOne;
+ TargetLowering::TargetLoweringOpt TLO(DAG, !DCI.isBeforeLegalize(),
+ !DCI.isBeforeLegalizeOps());
+ const TargetLowering &TLI = DAG.getTargetLoweringInfo();
+ if (TLO.ShrinkDemandedConstant(OutVal, DemandedMask) ||
+ TLI.SimplifyDemandedBits(OutVal, DemandedMask, KnownZero, KnownOne,
+ TLO))
+ DCI.CommitTargetLoweringOpt(TLO);
+ }
+ break;
+ }
+ case Intrinsic::xcore_setpt: {
+ SDValue Time = N->getOperand(3);
+ // This instruction ignores the high bits.
+ if (Time.hasOneUse()) {
+ unsigned BitWidth = Time.getValueSizeInBits();
+ APInt DemandedMask = APInt::getLowBitsSet(BitWidth, 16);
+ APInt KnownZero, KnownOne;
+ TargetLowering::TargetLoweringOpt TLO(DAG, !DCI.isBeforeLegalize(),
+ !DCI.isBeforeLegalizeOps());
+ const TargetLowering &TLI = DAG.getTargetLoweringInfo();
+ if (TLO.ShrinkDemandedConstant(Time, DemandedMask) ||
+ TLI.SimplifyDemandedBits(Time, DemandedMask, KnownZero, KnownOne,
+ TLO))
+ DCI.CommitTargetLoweringOpt(TLO);
+ }
+ break;
+ }
+ }
+ break;
case XCoreISD::LADD: {
SDValue N0 = N->getOperand(0);
SDValue N1 = N->getOperand(1);
KnownZero.getBitWidth() - 1);
}
break;
+ case ISD::INTRINSIC_W_CHAIN:
+ {
+ unsigned IntNo = cast<ConstantSDNode>(Op.getOperand(1))->getZExtValue();
+ switch (IntNo) {
+ case Intrinsic::xcore_getts:
+ // High bits are known to be zero.
+ KnownZero = APInt::getHighBitsSet(KnownZero.getBitWidth(),
+ KnownZero.getBitWidth() - 16);
+ break;
+ case Intrinsic::xcore_int:
+ case Intrinsic::xcore_inct:
+ // High bits are known to be zero.
+ KnownZero = APInt::getHighBitsSet(KnownZero.getBitWidth(),
+ KnownZero.getBitWidth() - 8);
+ break;
+ case Intrinsic::xcore_testct:
+ // Result is either 0 or 1.
+ KnownZero = APInt::getHighBitsSet(KnownZero.getBitWidth(),
+ KnownZero.getBitWidth() - 1);
+ break;
+ case Intrinsic::xcore_testwct:
+ // Result is in the range 0 - 4.
+ KnownZero = APInt::getHighBitsSet(KnownZero.getBitWidth(),
+ KnownZero.getBitWidth() - 3);
+ break;
+ }
+ }
+ break;
}
}