]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/blobdiff - lib/Transforms/IPO/ArgumentPromotion.cpp
ArgumentPromotion: Propagate debug locations on calls for which arguments are promoted.
[opencl/llvm.git] / lib / Transforms / IPO / ArgumentPromotion.cpp
index 2132e0a5fe119b341788024333fbcd3a00c18f50..4618c26bc65371a83dfa5c834eef6c885b0034a6 100644 (file)
 //
 //===----------------------------------------------------------------------===//
 
-#define DEBUG_TYPE "argpromotion"
 #include "llvm/Transforms/IPO.h"
 #include "llvm/ADT/DepthFirstIterator.h"
 #include "llvm/ADT/Statistic.h"
 #include "llvm/ADT/StringExtras.h"
 #include "llvm/Analysis/AliasAnalysis.h"
 #include "llvm/Analysis/CallGraph.h"
-#include "llvm/CallGraphSCCPass.h"
-#include "llvm/Constants.h"
-#include "llvm/DerivedTypes.h"
-#include "llvm/Instructions.h"
-#include "llvm/LLVMContext.h"
-#include "llvm/Module.h"
-#include "llvm/Support/CFG.h"
-#include "llvm/Support/CallSite.h"
+#include "llvm/Analysis/CallGraphSCCPass.h"
+#include "llvm/IR/CFG.h"
+#include "llvm/IR/CallSite.h"
+#include "llvm/IR/Constants.h"
+#include "llvm/IR/DerivedTypes.h"
+#include "llvm/IR/Instructions.h"
+#include "llvm/IR/LLVMContext.h"
+#include "llvm/IR/Module.h"
 #include "llvm/Support/Debug.h"
 #include "llvm/Support/raw_ostream.h"
 #include <set>
 using namespace llvm;
 
+#define DEBUG_TYPE "argpromotion"
+
 STATISTIC(NumArgumentsPromoted , "Number of pointer arguments promoted");
 STATISTIC(NumAggregatesPromoted, "Number of aggregate arguments promoted");
 STATISTIC(NumByValArgsPromoted , "Number of byval arguments promoted");
@@ -58,12 +59,12 @@ namespace {
   /// ArgPromotion - The 'by reference' to 'by value' argument promotion pass.
   ///
   struct ArgPromotion : public CallGraphSCCPass {
-    virtual void getAnalysisUsage(AnalysisUsage &AU) const {
+    void getAnalysisUsage(AnalysisUsage &AU) const override {
       AU.addRequired<AliasAnalysis>();
       CallGraphSCCPass::getAnalysisUsage(AU);
     }
 
-    virtual bool runOnSCC(CallGraphSCC &SCC);
+    bool runOnSCC(CallGraphSCC &SCC) override;
     static char ID; // Pass identification, replacement for typeid
     explicit ArgPromotion(unsigned maxElements = 3)
         : CallGraphSCCPass(ID), maxElements(maxElements) {
@@ -88,7 +89,7 @@ char ArgPromotion::ID = 0;
 INITIALIZE_PASS_BEGIN(ArgPromotion, "argpromotion",
                 "Promote 'by reference' arguments to scalars", false, false)
 INITIALIZE_AG_DEPENDENCY(AliasAnalysis)
-INITIALIZE_AG_DEPENDENCY(CallGraph)
+INITIALIZE_PASS_DEPENDENCY(CallGraphWrapperPass)
 INITIALIZE_PASS_END(ArgPromotion, "argpromotion",
                 "Promote 'by reference' arguments to scalars", false, false)
 
@@ -123,26 +124,23 @@ CallGraphNode *ArgPromotion::PromoteArguments(CallGraphNode *CGN) {
   Function *F = CGN->getFunction();
 
   // Make sure that it is local to this module.
-  if (!F || !F->hasLocalLinkage()) return 0;
+  if (!F || !F->hasLocalLinkage()) return nullptr;
 
   // First check: see if there are any pointer arguments!  If not, quick exit.
-  SmallVector<std::pair<Argument*, unsigned>, 16> PointerArgs;
-  unsigned ArgNo = 0;
-  for (Function::arg_iterator I = F->arg_begin(), E = F->arg_end();
-       I != E; ++I, ++ArgNo)
+  SmallVector<Argument*, 16> PointerArgs;
+  for (Function::arg_iterator I = F->arg_begin(), E = F->arg_end(); I != E; ++I)
     if (I->getType()->isPointerTy())
-      PointerArgs.push_back(std::pair<Argument*, unsigned>(I, ArgNo));
-  if (PointerArgs.empty()) return 0;
+      PointerArgs.push_back(I);
+  if (PointerArgs.empty()) return nullptr;
 
   // Second check: make sure that all callers are direct callers.  We can't
   // transform functions that have indirect callers.  Also see if the function
   // is self-recursive.
   bool isSelfRecursive = false;
-  for (Value::use_iterator UI = F->use_begin(), E = F->use_end();
-       UI != E; ++UI) {
-    CallSite CS(*UI);
+  for (Use &U : F->uses()) {
+    CallSite CS(U.getUser());
     // Must be a direct call.
-    if (CS.getInstruction() == 0 || !CS.isCallee(UI)) return 0;
+    if (CS.getInstruction() == nullptr || !CS.isCallee(&U)) return nullptr;
     
     if (CS.getInstruction()->getParent()->getParent() == F)
       isSelfRecursive = true;
@@ -152,15 +150,14 @@ CallGraphNode *ArgPromotion::PromoteArguments(CallGraphNode *CGN) {
   // add it to ArgsToPromote.
   SmallPtrSet<Argument*, 8> ArgsToPromote;
   SmallPtrSet<Argument*, 8> ByValArgsToTransform;
-  for (unsigned i = 0; i != PointerArgs.size(); ++i) {
-    bool isByVal=F->getParamAttributes(PointerArgs[i].second+1).
-      hasAttribute(Attributes::ByVal);
-    Argument *PtrArg = PointerArgs[i].first;
+  for (unsigned i = 0, e = PointerArgs.size(); i != e; ++i) {
+    Argument *PtrArg = PointerArgs[i];
     Type *AgTy = cast<PointerType>(PtrArg->getType())->getElementType();
 
     // If this is a byval argument, and if the aggregate type is small, just
-    // pass the elements, which is always safe.
-    if (isByVal) {
+    // pass the elements, which is always safe.  This does not apply to
+    // inalloca.
+    if (PtrArg->hasByValAttr()) {
       if (StructType *STy = dyn_cast<StructType>(AgTy)) {
         if (maxElements > 0 && STy->getNumElements() > maxElements) {
           DEBUG(dbgs() << "argpromotion disable promoting argument '"
@@ -205,13 +202,13 @@ CallGraphNode *ArgPromotion::PromoteArguments(CallGraphNode *CGN) {
     }
     
     // Otherwise, see if we can promote the pointer to its value.
-    if (isSafeToPromoteArgument(PtrArg, isByVal))
+    if (isSafeToPromoteArgument(PtrArg, PtrArg->hasByValOrInAllocaAttr()))
       ArgsToPromote.insert(PtrArg);
   }
 
   // No promotable pointer arguments.
   if (ArgsToPromote.empty() && ByValArgsToTransform.empty()) 
-    return 0;
+    return nullptr;
 
   return DoPromotion(F, ArgsToPromote, ByValArgsToTransform);
 }
@@ -221,14 +218,12 @@ CallGraphNode *ArgPromotion::PromoteArguments(CallGraphNode *CGN) {
 static bool AllCallersPassInValidPointerForArgument(Argument *Arg) {
   Function *Callee = Arg->getParent();
 
-  unsigned ArgNo = std::distance(Callee->arg_begin(),
-                                 Function::arg_iterator(Arg));
+  unsigned ArgNo = Arg->getArgNo();
 
   // Look at all call sites of the function.  At this pointer we know we only
   // have direct callees.
-  for (Value::use_iterator UI = Callee->use_begin(), E = Callee->use_end();
-       UI != E; ++UI) {
-    CallSite CS(*UI);
+  for (User *U : Callee->users()) {
+    CallSite CS(U);
     assert(CS && "Should only have direct calls!");
 
     if (!CS.getArgument(ArgNo)->isDereferenceablePointer())
@@ -306,7 +301,8 @@ static void MarkIndicesSafe(const ArgPromotion::IndicesVector &ToMark,
 /// This method limits promotion of aggregates to only promote up to three
 /// elements of the aggregate in order to avoid exploding the number of
 /// arguments passed in.
-bool ArgPromotion::isSafeToPromoteArgument(Argument *Arg, bool isByVal) const {
+bool ArgPromotion::isSafeToPromoteArgument(Argument *Arg,
+                                           bool isByValOrInAlloca) const {
   typedef std::set<IndicesVector> GEPIndicesSet;
 
   // Quick exit for unused arguments
@@ -328,6 +324,9 @@ bool ArgPromotion::isSafeToPromoteArgument(Argument *Arg, bool isByVal) const {
   //
   // This set will contain all sets of indices that are loaded in the entry
   // block, and thus are safe to unconditionally load in the caller.
+  //
+  // This optimization is also safe for InAlloca parameters, because it verifies
+  // that the address isn't captured.
   GEPIndicesSet SafeToUnconditionallyLoad;
 
   // This set contains all the sets of indices that we are planning to promote.
@@ -335,7 +334,7 @@ bool ArgPromotion::isSafeToPromoteArgument(Argument *Arg, bool isByVal) const {
   GEPIndicesSet ToPromote;
 
   // If the pointer is always valid, any load with first index 0 is valid.
-  if (isByVal || AllCallersPassInValidPointerForArgument(Arg))
+  if (isByValOrInAlloca || AllCallersPassInValidPointerForArgument(Arg))
     SafeToUnconditionallyLoad.insert(IndicesVector(1, 0));
 
   // First, iterate the entry block and mark loads of (geps of) arguments as
@@ -375,17 +374,16 @@ bool ArgPromotion::isSafeToPromoteArgument(Argument *Arg, bool isByVal) const {
   // not (GEP+)loads, or any (GEP+)loads that are not safe to promote.
   SmallVector<LoadInst*, 16> Loads;
   IndicesVector Operands;
-  for (Value::use_iterator UI = Arg->use_begin(), E = Arg->use_end();
-       UI != E; ++UI) {
-    User *U = *UI;
+  for (Use &U : Arg->uses()) {
+    User *UR = U.getUser();
     Operands.clear();
-    if (LoadInst *LI = dyn_cast<LoadInst>(U)) {
+    if (LoadInst *LI = dyn_cast<LoadInst>(UR)) {
       // Don't hack volatile/atomic loads
       if (!LI->isSimple()) return false;
       Loads.push_back(LI);
       // Direct loads are equivalent to a GEP with a zero index and then a load.
       Operands.push_back(0);
-    } else if (GetElementPtrInst *GEP = dyn_cast<GetElementPtrInst>(U)) {
+    } else if (GetElementPtrInst *GEP = dyn_cast<GetElementPtrInst>(UR)) {
       if (GEP->use_empty()) {
         // Dead GEP's cause trouble later.  Just remove them if we run into
         // them.
@@ -394,7 +392,7 @@ bool ArgPromotion::isSafeToPromoteArgument(Argument *Arg, bool isByVal) const {
         // TODO: This runs the above loop over and over again for dead GEPs
         // Couldn't we just do increment the UI iterator earlier and erase the
         // use?
-        return isSafeToPromoteArgument(Arg, isByVal);
+        return isSafeToPromoteArgument(Arg, isByValOrInAlloca);
       }
 
       // Ensure that all of the indices are constants.
@@ -406,9 +404,8 @@ bool ArgPromotion::isSafeToPromoteArgument(Argument *Arg, bool isByVal) const {
           return false;  // Not a constant operand GEP!
 
       // Ensure that the only users of the GEP are load instructions.
-      for (Value::use_iterator UI = GEP->use_begin(), E = GEP->use_end();
-           UI != E; ++UI)
-        if (LoadInst *LI = dyn_cast<LoadInst>(*UI)) {
+      for (User *GEPU : GEP->users())
+        if (LoadInst *LI = dyn_cast<LoadInst>(GEPU)) {
           // Don't hack volatile/atomic loads
           if (!LI->isSimple()) return false;
           Loads.push_back(LI);
@@ -509,19 +506,20 @@ CallGraphNode *ArgPromotion::DoPromotion(Function *F,
   // OriginalLoads - Keep track of a representative load instruction from the
   // original function so that we can tell the alias analysis implementation
   // what the new GEP/Load instructions we are inserting look like.
-  std::map<IndicesVector, LoadInst*> OriginalLoads;
+  // We need to keep the original loads for each argument and the elements
+  // of the argument that are accessed.
+  std::map<std::pair<Argument*, IndicesVector>, LoadInst*> OriginalLoads;
 
-  // Attributes - Keep track of the parameter attributes for the arguments
+  // Attribute - Keep track of the parameter attributes for the arguments
   // that we are *not* promoting. For the ones that we do promote, the parameter
   // attributes are lost
-  SmallVector<AttributeWithIndex, 8> AttributesVec;
+  SmallVector<AttributeSet, 8> AttributesVec;
   const AttributeSet &PAL = F->getAttributes();
 
   // Add any return attributes.
-  Attributes attrs = PAL.getRetAttributes();
-  if (attrs.hasAttributes())
-    AttributesVec.push_back(AttributeWithIndex::get(AttributeSet::ReturnIndex,
-                                                    attrs));
+  if (PAL.hasAttributes(AttributeSet::ReturnIndex))
+    AttributesVec.push_back(AttributeSet::get(F->getContext(),
+                                              PAL.getRetAttributes()));
 
   // First, determine the new argument list
   unsigned ArgIndex = 1;
@@ -537,9 +535,12 @@ CallGraphNode *ArgPromotion::DoPromotion(Function *F,
     } else if (!ArgsToPromote.count(I)) {
       // Unchanged argument
       Params.push_back(I->getType());
-      Attributes attrs = PAL.getParamAttributes(ArgIndex);
-      if (attrs.hasAttributes())
-        AttributesVec.push_back(AttributeWithIndex::get(Params.size(), attrs));
+      AttributeSet attrs = PAL.getParamAttributes(ArgIndex);
+      if (attrs.hasAttributes(ArgIndex)) {
+        AttrBuilder B(attrs, ArgIndex);
+        AttributesVec.
+          push_back(AttributeSet::get(F->getContext(), Params.size(), B));
+      }
     } else if (I->use_empty()) {
       // Dead argument (which are always marked as promotable)
       ++NumArgumentsDead;
@@ -550,16 +551,15 @@ CallGraphNode *ArgPromotion::DoPromotion(Function *F,
       // In this table, we will track which indices are loaded from the argument
       // (where direct loads are tracked as no indices).
       ScalarizeTable &ArgIndices = ScalarizedElements[I];
-      for (Value::use_iterator UI = I->use_begin(), E = I->use_end(); UI != E;
-           ++UI) {
-        Instruction *User = cast<Instruction>(*UI);
-        assert(isa<LoadInst>(User) || isa<GetElementPtrInst>(User));
+      for (User *U : I->users()) {
+        Instruction *UI = cast<Instruction>(U);
+        assert(isa<LoadInst>(UI) || isa<GetElementPtrInst>(UI));
         IndicesVector Indices;
-        Indices.reserve(User->getNumOperands() - 1);
+        Indices.reserve(UI->getNumOperands() - 1);
         // Since loads will only have a single operand, and GEPs only a single
         // non-index operand, this will record direct loads without any indices,
         // and gep+loads with the GEP indices.
-        for (User::op_iterator II = User->op_begin() + 1, IE = User->op_end();
+        for (User::op_iterator II = UI->op_begin() + 1, IE = UI->op_end();
              II != IE; ++II)
           Indices.push_back(cast<ConstantInt>(*II)->getSExtValue());
         // GEPs with a single 0 index can be merged with direct loads
@@ -567,12 +567,12 @@ CallGraphNode *ArgPromotion::DoPromotion(Function *F,
           Indices.clear();
         ArgIndices.insert(Indices);
         LoadInst *OrigLoad;
-        if (LoadInst *L = dyn_cast<LoadInst>(User))
+        if (LoadInst *L = dyn_cast<LoadInst>(UI))
           OrigLoad = L;
         else
           // Take any load, we will use it only to update Alias Analysis
-          OrigLoad = cast<LoadInst>(User->use_back());
-        OriginalLoads[Indices] = OrigLoad;
+          OrigLoad = cast<LoadInst>(UI->user_back());
+        OriginalLoads[std::make_pair(I, Indices)] = OrigLoad;
       }
 
       // Add a parameter to the function for each element passed in.
@@ -591,10 +591,9 @@ CallGraphNode *ArgPromotion::DoPromotion(Function *F,
   }
 
   // Add any function attributes.
-  attrs = PAL.getFnAttributes();
-  if (attrs.hasAttributes())
-    AttributesVec.push_back(AttributeWithIndex::get(AttributeSet::FunctionIndex,
-                                                    attrs));
+  if (PAL.hasAttributes(AttributeSet::FunctionIndex))
+    AttributesVec.push_back(AttributeSet::get(FTy->getContext(),
+                                              PAL.getFnAttributes()));
 
   Type *RetTy = FTy->getReturnType();
 
@@ -623,8 +622,8 @@ CallGraphNode *ArgPromotion::DoPromotion(Function *F,
 
   // Get the callgraph information that we need to update to reflect our
   // changes.
-  CallGraph &CG = getAnalysis<CallGraph>();
-  
+  CallGraph &CG = getAnalysis<CallGraphWrapperPass>().getCallGraph();
+
   // Get a new callgraph node for NF.
   CallGraphNode *NF_CGN = CG.getOrInsertFunction(NF);
 
@@ -633,16 +632,15 @@ CallGraphNode *ArgPromotion::DoPromotion(Function *F,
   //
   SmallVector<Value*, 16> Args;
   while (!F->use_empty()) {
-    CallSite CS(F->use_back());
+    CallSite CS(F->user_back());
     assert(CS.getCalledFunction() == F);
     Instruction *Call = CS.getInstruction();
     const AttributeSet &CallPAL = CS.getAttributes();
 
     // Add any return attributes.
-    Attributes attrs = CallPAL.getRetAttributes();
-    if (attrs.hasAttributes())
-      AttributesVec.push_back(AttributeWithIndex::get(AttributeSet::ReturnIndex,
-                                                      attrs));
+    if (CallPAL.hasAttributes(AttributeSet::ReturnIndex))
+      AttributesVec.push_back(AttributeSet::get(F->getContext(),
+                                                CallPAL.getRetAttributes()));
 
     // Loop over the operands, inserting GEP and loads in the caller as
     // appropriate.
@@ -653,16 +651,17 @@ CallGraphNode *ArgPromotion::DoPromotion(Function *F,
       if (!ArgsToPromote.count(I) && !ByValArgsToTransform.count(I)) {
         Args.push_back(*AI);          // Unmodified argument
 
-        Attributes Attrs = CallPAL.getParamAttributes(ArgIndex);
-        if (Attrs.hasAttributes())
-          AttributesVec.push_back(AttributeWithIndex::get(Args.size(), Attrs));
-
+        if (CallPAL.hasAttributes(ArgIndex)) {
+          AttrBuilder B(CallPAL, ArgIndex);
+          AttributesVec.
+            push_back(AttributeSet::get(F->getContext(), Args.size(), B));
+        }
       } else if (ByValArgsToTransform.count(I)) {
         // Emit a GEP and load for each element of the struct.
         Type *AgTy = cast<PointerType>(I->getType())->getElementType();
         StructType *STy = cast<StructType>(AgTy);
         Value *Idxs[2] = {
-              ConstantInt::get(Type::getInt32Ty(F->getContext()), 0), 0 };
+              ConstantInt::get(Type::getInt32Ty(F->getContext()), 0), nullptr };
         for (unsigned i = 0, e = STy->getNumElements(); i != e; ++i) {
           Idxs[1] = ConstantInt::get(Type::getInt32Ty(F->getContext()), i);
           Value *Idx = GetElementPtrInst::Create(*AI, Idxs,
@@ -680,7 +679,7 @@ CallGraphNode *ArgPromotion::DoPromotion(Function *F,
         for (ScalarizeTable::iterator SI = ArgIndices.begin(),
                E = ArgIndices.end(); SI != E; ++SI) {
           Value *V = *AI;
-          LoadInst *OrigLoad = OriginalLoads[*SI];
+          LoadInst *OrigLoad = OriginalLoads[std::make_pair(I, *SI)];
           if (!SI->empty()) {
             Ops.reserve(SI->size());
             Type *ElTy = V->getType();
@@ -715,16 +714,17 @@ CallGraphNode *ArgPromotion::DoPromotion(Function *F,
     // Push any varargs arguments on the list.
     for (; AI != CS.arg_end(); ++AI, ++ArgIndex) {
       Args.push_back(*AI);
-      Attributes Attrs = CallPAL.getParamAttributes(ArgIndex);
-      if (Attrs.hasAttributes())
-        AttributesVec.push_back(AttributeWithIndex::get(Args.size(), Attrs));
+      if (CallPAL.hasAttributes(ArgIndex)) {
+        AttrBuilder B(CallPAL, ArgIndex);
+        AttributesVec.
+          push_back(AttributeSet::get(F->getContext(), Args.size(), B));
+      }
     }
 
     // Add any function attributes.
-    attrs = CallPAL.getFnAttributes();
-    if (attrs.hasAttributes())
-      AttributesVec.push_back(AttributeWithIndex::get(AttributeSet::FunctionIndex,
-                                                      attrs));
+    if (CallPAL.hasAttributes(AttributeSet::FunctionIndex))
+      AttributesVec.push_back(AttributeSet::get(Call->getContext(),
+                                                CallPAL.getFnAttributes()));
 
     Instruction *New;
     if (InvokeInst *II = dyn_cast<InvokeInst>(Call)) {
@@ -741,6 +741,7 @@ CallGraphNode *ArgPromotion::DoPromotion(Function *F,
       if (cast<CallInst>(Call)->isTailCall())
         cast<CallInst>(New)->setTailCall();
     }
+    New->setDebugLoc(Call->getDebugLoc());
     Args.clear();
     AttributesVec.clear();
 
@@ -789,10 +790,10 @@ CallGraphNode *ArgPromotion::DoPromotion(Function *F,
 
       // Just add all the struct element types.
       Type *AgTy = cast<PointerType>(I->getType())->getElementType();
-      Value *TheAlloca = new AllocaInst(AgTy, 0, "", InsertPt);
+      Value *TheAlloca = new AllocaInst(AgTy, nullptr, "", InsertPt);
       StructType *STy = cast<StructType>(AgTy);
       Value *Idxs[2] = {
-            ConstantInt::get(Type::getInt32Ty(F->getContext()), 0), 0 };
+            ConstantInt::get(Type::getInt32Ty(F->getContext()), 0), nullptr };
 
       for (unsigned i = 0, e = STy->getNumElements(); i != e; ++i) {
         Idxs[1] = ConstantInt::get(Type::getInt32Ty(F->getContext()), i);
@@ -808,6 +809,15 @@ CallGraphNode *ArgPromotion::DoPromotion(Function *F,
       I->replaceAllUsesWith(TheAlloca);
       TheAlloca->takeName(I);
       AA.replaceWithNewValue(I, TheAlloca);
+
+      // If the alloca is used in a call, we must clear the tail flag since
+      // the callee now uses an alloca from the caller.
+      for (User *U : TheAlloca->users()) {
+        CallInst *Call = dyn_cast<CallInst>(U);
+        if (!Call)
+          continue;
+        Call->setTailCall(false);
+      }
       continue;
     }
 
@@ -822,7 +832,7 @@ CallGraphNode *ArgPromotion::DoPromotion(Function *F,
     ScalarizeTable &ArgIndices = ScalarizedElements[I];
 
     while (!I->use_empty()) {
-      if (LoadInst *LI = dyn_cast<LoadInst>(I->use_back())) {
+      if (LoadInst *LI = dyn_cast<LoadInst>(I->user_back())) {
         assert(ArgIndices.begin()->empty() &&
                "Load element should sort to front!");
         I2->setName(I->getName()+".val");
@@ -832,7 +842,7 @@ CallGraphNode *ArgPromotion::DoPromotion(Function *F,
         DEBUG(dbgs() << "*** Promoted load of argument '" << I->getName()
               << "' in function '" << F->getName() << "'\n");
       } else {
-        GetElementPtrInst *GEP = cast<GetElementPtrInst>(I->use_back());
+        GetElementPtrInst *GEP = cast<GetElementPtrInst>(I->user_back());
         IndicesVector Operands;
         Operands.reserve(GEP->getNumIndices());
         for (User::op_iterator II = GEP->idx_begin(), IE = GEP->idx_end();
@@ -862,7 +872,7 @@ CallGraphNode *ArgPromotion::DoPromotion(Function *F,
         // All of the uses must be load instructions.  Replace them all with
         // the argument specified by ArgNo.
         while (!GEP->use_empty()) {
-          LoadInst *L = cast<LoadInst>(GEP->use_back());
+          LoadInst *L = cast<LoadInst>(GEP->user_back());
           L->replaceAllUsesWith(TheArg);
           AA.replaceWithNewValue(L, TheArg);
           L->eraseFromParent();