diff --git a/lib/Transforms/InstCombine/InstCombineLoadStoreAlloca.cpp b/lib/Transforms/InstCombine/InstCombineLoadStoreAlloca.cpp
index c533d6e5e5f0dd7631024d72d77df953d63142b9..54b1af8ea79199e223bc4bbb449bc0662b3747dc 100644 (file)
//===----------------------------------------------------------------------===//
#include "InstCombine.h"
-#include "llvm/IntrinsicInst.h"
+#include "llvm/ADT/Statistic.h"
#include "llvm/Analysis/Loads.h"
-#include "llvm/Target/TargetData.h"
+#include "llvm/IR/DataLayout.h"
+#include "llvm/IR/LLVMContext.h"
+#include "llvm/IR/IntrinsicInst.h"
#include "llvm/Transforms/Utils/BasicBlockUtils.h"
#include "llvm/Transforms/Utils/Local.h"
-#include "llvm/ADT/Statistic.h"
using namespace llvm;
-STATISTIC(NumDeadStore, "Number of dead stores eliminated");
+#define DEBUG_TYPE "instcombine"
+
+STATISTIC(NumDeadStore, "Number of dead stores eliminated");
+STATISTIC(NumGlobalCopies, "Number of allocas copied from constant global");
+
+/// pointsToConstantGlobal - Return true if V (possibly indirectly) points to
+/// some part of a constant global variable. This intentionally only accepts
+/// constant expressions because we can't rewrite arbitrary instructions.
+static bool pointsToConstantGlobal(Value *V) {
+ if (GlobalVariable *GV = dyn_cast<GlobalVariable>(V))
+ return GV->isConstant();
+
+ if (ConstantExpr *CE = dyn_cast<ConstantExpr>(V)) {
+ if (CE->getOpcode() == Instruction::BitCast ||
+ CE->getOpcode() == Instruction::AddrSpaceCast ||
+ CE->getOpcode() == Instruction::GetElementPtr)
+ return pointsToConstantGlobal(CE->getOperand(0));
+ }
+ return false;
+}
+
+/// isOnlyCopiedFromConstantGlobal - Recursively walk the uses of a (derived)
+/// pointer to an alloca. Ignore any reads of the pointer, return false if we
+/// see any stores or other unknown uses. If we see pointer arithmetic, keep
+/// track of whether it moves the pointer (with IsOffset) but otherwise traverse
+/// the uses. If we see a memcpy/memmove that targets an unoffseted pointer to
+/// the alloca, and if the source pointer is a pointer to a constant global, we
+/// can optimize this.
+static bool
+isOnlyCopiedFromConstantGlobal(Value *V, MemTransferInst *&TheCopy,
+ SmallVectorImpl<Instruction *> &ToDelete) {
+ // We track lifetime intrinsics as we encounter them. If we decide to go
+ // ahead and replace the value with the global, this lets the caller quickly
+ // eliminate the markers.
+
+ SmallVector<std::pair<Value *, bool>, 35> ValuesToInspect;
+ ValuesToInspect.push_back(std::make_pair(V, false));
+ while (!ValuesToInspect.empty()) {
+ auto ValuePair = ValuesToInspect.pop_back_val();
+ const bool IsOffset = ValuePair.second;
+ for (auto &U : ValuePair.first->uses()) {
+ Instruction *I = cast<Instruction>(U.getUser());
+
+ if (LoadInst *LI = dyn_cast<LoadInst>(I)) {
+ // Ignore non-volatile loads, they are always ok.
+ if (!LI->isSimple()) return false;
+ continue;
+ }
+
+ if (isa<BitCastInst>(I) || isa<AddrSpaceCastInst>(I)) {
+ // If uses of the bitcast are ok, we are ok.
+ ValuesToInspect.push_back(std::make_pair(I, IsOffset));
+ continue;
+ }
+ if (GetElementPtrInst *GEP = dyn_cast<GetElementPtrInst>(I)) {
+ // If the GEP has all zero indices, it doesn't offset the pointer. If it
+ // doesn't, it does.
+ ValuesToInspect.push_back(
+ std::make_pair(I, IsOffset || !GEP->hasAllZeroIndices()));
+ continue;
+ }
+
+ if (CallSite CS = I) {
+ // If this is the function being called then we treat it like a load and
+ // ignore it.
+ if (CS.isCallee(&U))
+ continue;
+
+ // Inalloca arguments are clobbered by the call.
+ unsigned ArgNo = CS.getArgumentNo(&U);
+ if (CS.isInAllocaArgument(ArgNo))
+ return false;
+
+ // If this is a readonly/readnone call site, then we know it is just a
+ // load (but one that potentially returns the value itself), so we can
+ // ignore it if we know that the value isn't captured.
+ if (CS.onlyReadsMemory() &&
+ (CS.getInstruction()->use_empty() || CS.doesNotCapture(ArgNo)))
+ continue;
+
+ // If this is being passed as a byval argument, the caller is making a
+ // copy, so it is only a read of the alloca.
+ if (CS.isByValArgument(ArgNo))
+ continue;
+ }
+
+ // Lifetime intrinsics can be handled by the caller.
+ if (IntrinsicInst *II = dyn_cast<IntrinsicInst>(I)) {
+ if (II->getIntrinsicID() == Intrinsic::lifetime_start ||
+ II->getIntrinsicID() == Intrinsic::lifetime_end) {
+ assert(II->use_empty() && "Lifetime markers have no result to use!");
+ ToDelete.push_back(II);
+ continue;
+ }
+ }
+
+ // If this is isn't our memcpy/memmove, reject it as something we can't
+ // handle.
+ MemTransferInst *MI = dyn_cast<MemTransferInst>(I);
+ if (!MI)
+ return false;
+
+ // If the transfer is using the alloca as a source of the transfer, then
+ // ignore it since it is a load (unless the transfer is volatile).
+ if (U.getOperandNo() == 1) {
+ if (MI->isVolatile()) return false;
+ continue;
+ }
+
+ // If we already have seen a copy, reject the second one.
+ if (TheCopy) return false;
+
+ // If the pointer has been offset from the start of the alloca, we can't
+ // safely handle this.
+ if (IsOffset) return false;
+
+ // If the memintrinsic isn't using the alloca as the dest, reject it.
+ if (U.getOperandNo() != 0) return false;
+
+ // If the source of the memcpy/move is not a constant global, reject it.
+ if (!pointsToConstantGlobal(MI->getSource()))
+ return false;
+
+ // Otherwise, the transform is safe. Remember the copy instruction.
+ TheCopy = MI;
+ }
+ }
+ return true;
+}
+
+/// isOnlyCopiedFromConstantGlobal - Return true if the specified alloca is only
+/// modified by a copy from a constant global. If we can prove this, we can
+/// replace any uses of the alloca with uses of the global directly.
+static MemTransferInst *
+isOnlyCopiedFromConstantGlobal(AllocaInst *AI,
+ SmallVectorImpl<Instruction *> &ToDelete) {
+ MemTransferInst *TheCopy = nullptr;
+ if (isOnlyCopiedFromConstantGlobal(AI, TheCopy, ToDelete))
+ return TheCopy;
+ return nullptr;
+}
Instruction *InstCombiner::visitAllocaInst(AllocaInst &AI) {
// Ensure that the alloca array size argument has type intptr_t, so that
// any casting is exposed early.
- if (TD) {
- const Type *IntPtrTy = TD->getIntPtrType(AI.getContext());
+ if (DL) {
+ Type *IntPtrTy = DL->getIntPtrType(AI.getType());
if (AI.getArraySize()->getType() != IntPtrTy) {
Value *V = Builder->CreateIntCast(AI.getArraySize(),
IntPtrTy, false);
// Convert: alloca Ty, C - where C is a constant != 1 into: alloca [C x Ty], 1
if (AI.isArrayAllocation()) { // Check C != 1
if (const ConstantInt *C = dyn_cast<ConstantInt>(AI.getArraySize())) {
- const Type *NewTy =
+ Type *NewTy =
ArrayType::get(AI.getAllocatedType(), C->getZExtValue());
- assert(isa<AllocaInst>(AI) && "Unknown type of allocation inst!");
- AllocaInst *New = Builder->CreateAlloca(NewTy, 0, AI.getName());
+ AllocaInst *New = Builder->CreateAlloca(NewTy, nullptr, AI.getName());
New->setAlignment(AI.getAlignment());
// Scan to the end of the allocation instructions, to skip over a block of
// Now that I is pointing to the first non-allocation-inst in the block,
// insert our getelementptr instruction...
//
- Value *NullIdx =Constant::getNullValue(Type::getInt32Ty(AI.getContext()));
- Value *Idx[2];
- Idx[0] = NullIdx;
- Idx[1] = NullIdx;
- Value *V = GetElementPtrInst::CreateInBounds(New, Idx, Idx + 2,
- New->getName()+".sub", It);
+ Type *IdxTy = DL
+ ? DL->getIntPtrType(AI.getType())
+ : Type::getInt64Ty(AI.getContext());
+ Value *NullIdx = Constant::getNullValue(IdxTy);
+ Value *Idx[2] = { NullIdx, NullIdx };
+ Instruction *GEP =
+ GetElementPtrInst::CreateInBounds(New, Idx, New->getName() + ".sub");
+ InsertNewInstBefore(GEP, *It);
// Now make everything use the getelementptr instead of the original
// allocation.
- return ReplaceInstUsesWith(AI, V);
+ return ReplaceInstUsesWith(AI, GEP);
} else if (isa<UndefValue>(AI.getArraySize())) {
return ReplaceInstUsesWith(AI, Constant::getNullValue(AI.getType()));
}
}
- if (TD && isa<AllocaInst>(AI) && AI.getAllocatedType()->isSized()) {
- // If alloca'ing a zero byte object, replace the alloca with a null pointer.
- // Note that we only do this for alloca's, because malloc should allocate
- // and return a unique pointer, even for a zero byte allocation.
- if (TD->getTypeAllocSize(AI.getAllocatedType()) == 0)
- return ReplaceInstUsesWith(AI, Constant::getNullValue(AI.getType()));
-
+ if (DL && AI.getAllocatedType()->isSized()) {
// If the alignment is 0 (unspecified), assign it the preferred alignment.
if (AI.getAlignment() == 0)
- AI.setAlignment(TD->getPrefTypeAlignment(AI.getAllocatedType()));
+ AI.setAlignment(DL->getPrefTypeAlignment(AI.getAllocatedType()));
+
+ // Move all alloca's of zero byte objects to the entry block and merge them
+ // together. Note that we only do this for alloca's, because malloc should
+ // allocate and return a unique pointer, even for a zero byte allocation.
+ if (DL->getTypeAllocSize(AI.getAllocatedType()) == 0) {
+ // For a zero sized alloca there is no point in doing an array allocation.
+ // This is helpful if the array size is a complicated expression not used
+ // elsewhere.
+ if (AI.isArrayAllocation()) {
+ AI.setOperand(0, ConstantInt::get(AI.getArraySize()->getType(), 1));
+ return &AI;
+ }
+
+ // Get the first instruction in the entry block.
+ BasicBlock &EntryBlock = AI.getParent()->getParent()->getEntryBlock();
+ Instruction *FirstInst = EntryBlock.getFirstNonPHIOrDbg();
+ if (FirstInst != &AI) {
+ // If the entry block doesn't start with a zero-size alloca then move
+ // this one to the start of the entry block. There is no problem with
+ // dominance as the array size was forced to a constant earlier already.
+ AllocaInst *EntryAI = dyn_cast<AllocaInst>(FirstInst);
+ if (!EntryAI || !EntryAI->getAllocatedType()->isSized() ||
+ DL->getTypeAllocSize(EntryAI->getAllocatedType()) != 0) {
+ AI.moveBefore(FirstInst);
+ return &AI;
+ }
+
+ // If the alignment of the entry block alloca is 0 (unspecified),
+ // assign it the preferred alignment.
+ if (EntryAI->getAlignment() == 0)
+ EntryAI->setAlignment(
+ DL->getPrefTypeAlignment(EntryAI->getAllocatedType()));
+ // Replace this zero-sized alloca with the one at the start of the entry
+ // block after ensuring that the address will be aligned enough for both
+ // types.
+ unsigned MaxAlign = std::max(EntryAI->getAlignment(),
+ AI.getAlignment());
+ EntryAI->setAlignment(MaxAlign);
+ if (AI.getType() != EntryAI->getType())
+ return new BitCastInst(EntryAI, AI.getType());
+ return ReplaceInstUsesWith(AI, EntryAI);
+ }
+ }
}
- return 0;
+ if (AI.getAlignment()) {
+ // Check to see if this allocation is only modified by a memcpy/memmove from
+ // a constant global whose alignment is equal to or exceeds that of the
+ // allocation. If this is the case, we can change all users to use
+ // the constant global instead. This is commonly produced by the CFE by
+ // constructs like "void foo() { int A[] = {1,2,3,4,5,6,7,8,9...}; }" if 'A'
+ // is only subsequently read.
+ SmallVector<Instruction *, 4> ToDelete;
+ if (MemTransferInst *Copy = isOnlyCopiedFromConstantGlobal(&AI, ToDelete)) {
+ unsigned SourceAlign = getOrEnforceKnownAlignment(
+ Copy->getSource(), AI.getAlignment(), DL, AC, &AI, DT);
+ if (AI.getAlignment() <= SourceAlign) {
+ DEBUG(dbgs() << "Found alloca equal to global: " << AI << '\n');
+ DEBUG(dbgs() << " memcpy = " << *Copy << '\n');
+ for (unsigned i = 0, e = ToDelete.size(); i != e; ++i)
+ EraseInstFromFunction(*ToDelete[i]);
+ Constant *TheSrc = cast<Constant>(Copy->getSource());
+ Constant *Cast
+ = ConstantExpr::getPointerBitCastOrAddrSpaceCast(TheSrc, AI.getType());
+ Instruction *NewI = ReplaceInstUsesWith(AI, Cast);
+ EraseInstFromFunction(*Copy);
+ ++NumGlobalCopies;
+ return NewI;
+ }
+ }
+ }
+
+ // At last, use the generic allocation site handler to aggressively remove
+ // unused allocas.
+ return visitAllocSite(AI);
+}
+
+/// \brief Helper to combine a load to a new type.
+///
+/// This just does the work of combining a load to a new type. It handles
+/// metadata, etc., and returns the new instruction. The \c NewTy should be the
+/// loaded *value* type. This will convert it to a pointer, cast the operand to
+/// that pointer type, load it, etc.
+///
+/// Note that this will create all of the instructions with whatever insert
+/// point the \c InstCombiner currently is using.
+static LoadInst *combineLoadToNewType(InstCombiner &IC, LoadInst &LI, Type *NewTy) {
+ Value *Ptr = LI.getPointerOperand();
+ unsigned AS = LI.getPointerAddressSpace();
+ SmallVector<std::pair<unsigned, MDNode *>, 8> MD;
+ LI.getAllMetadata(MD);
+
+ LoadInst *NewLoad = IC.Builder->CreateAlignedLoad(
+ IC.Builder->CreateBitCast(Ptr, NewTy->getPointerTo(AS)),
+ LI.getAlignment(), LI.getName());
+ for (const auto &MDPair : MD) {
+ unsigned ID = MDPair.first;
+ MDNode *N = MDPair.second;
+ // Note, essentially every kind of metadata should be preserved here! This
+ // routine is supposed to clone a load instruction changing *only its type*.
+ // The only metadata it makes sense to drop is metadata which is invalidated
+ // when the pointer type changes. This should essentially never be the case
+ // in LLVM, but we explicitly switch over only known metadata to be
+ // conservatively correct. If you are adding metadata to LLVM which pertains
+ // to loads, you almost certainly want to add it here.
+ switch (ID) {
+ case LLVMContext::MD_dbg:
+ case LLVMContext::MD_tbaa:
+ case LLVMContext::MD_prof:
+ case LLVMContext::MD_fpmath:
+ case LLVMContext::MD_tbaa_struct:
+ case LLVMContext::MD_invariant_load:
+ case LLVMContext::MD_alias_scope:
+ case LLVMContext::MD_noalias:
+ case LLVMContext::MD_nontemporal:
+ case LLVMContext::MD_mem_parallel_loop_access:
+ case LLVMContext::MD_nonnull:
+ // All of these directly apply.
+ NewLoad->setMetadata(ID, N);
+ break;
+
+ case LLVMContext::MD_range:
+ // FIXME: It would be nice to propagate this in some way, but the type
+ // conversions make it hard.
+ break;
+ }
+ }
+ return NewLoad;
}
+/// \brief Combine a store to a new type.
+///
+/// Returns the newly created store instruction.
+static StoreInst *combineStoreToNewValue(InstCombiner &IC, StoreInst &SI, Value *V) {
+ Value *Ptr = SI.getPointerOperand();
+ unsigned AS = SI.getPointerAddressSpace();
+ SmallVector<std::pair<unsigned, MDNode *>, 8> MD;
+ SI.getAllMetadata(MD);
+
+ StoreInst *NewStore = IC.Builder->CreateAlignedStore(
+ V, IC.Builder->CreateBitCast(Ptr, V->getType()->getPointerTo(AS)),
+ SI.getAlignment());
+ for (const auto &MDPair : MD) {
+ unsigned ID = MDPair.first;
+ MDNode *N = MDPair.second;
+ // Note, essentially every kind of metadata should be preserved here! This
+ // routine is supposed to clone a store instruction changing *only its
+ // type*. The only metadata it makes sense to drop is metadata which is
+ // invalidated when the pointer type changes. This should essentially
+ // never be the case in LLVM, but we explicitly switch over only known
+ // metadata to be conservatively correct. If you are adding metadata to
+ // LLVM which pertains to stores, you almost certainly want to add it
+ // here.
+ switch (ID) {
+ case LLVMContext::MD_dbg:
+ case LLVMContext::MD_tbaa:
+ case LLVMContext::MD_prof:
+ case LLVMContext::MD_fpmath:
+ case LLVMContext::MD_tbaa_struct:
+ case LLVMContext::MD_alias_scope:
+ case LLVMContext::MD_noalias:
+ case LLVMContext::MD_nontemporal:
+ case LLVMContext::MD_mem_parallel_loop_access:
+ case LLVMContext::MD_nonnull:
+ // All of these directly apply.
+ NewStore->setMetadata(ID, N);
+ break;
+
+ case LLVMContext::MD_invariant_load:
+ case LLVMContext::MD_range:
+ break;
+ }
+ }
+
+ return NewStore;
+}
-/// InstCombineLoadCast - Fold 'load (cast P)' -> cast (load P)' when possible.
-static Instruction *InstCombineLoadCast(InstCombiner &IC, LoadInst &LI,
- const TargetData *TD) {
- User *CI = cast<User>(LI.getOperand(0));
- Value *CastOp = CI->getOperand(0);
-
- const PointerType *DestTy = cast<PointerType>(CI->getType());
- const Type *DestPTy = DestTy->getElementType();
- if (const PointerType *SrcTy = dyn_cast<PointerType>(CastOp->getType())) {
-
- // If the address spaces don't match, don't eliminate the cast.
- if (DestTy->getAddressSpace() != SrcTy->getAddressSpace())
- return 0;
-
- const Type *SrcPTy = SrcTy->getElementType();
-
- if (DestPTy->isIntegerTy() || DestPTy->isPointerTy() ||
- DestPTy->isVectorTy()) {
- // If the source is an array, the code below will not succeed. Check to
- // see if a trivial 'gep P, 0, 0' will help matters. Only do this for
- // constants.
- if (const ArrayType *ASrcTy = dyn_cast<ArrayType>(SrcPTy))
- if (Constant *CSrc = dyn_cast<Constant>(CastOp))
- if (ASrcTy->getNumElements() != 0) {
- Value *Idxs[2];
- Idxs[0] = Constant::getNullValue(Type::getInt32Ty(LI.getContext()));
- Idxs[1] = Idxs[0];
- CastOp = ConstantExpr::getGetElementPtr(CSrc, Idxs, 2);
- SrcTy = cast<PointerType>(CastOp->getType());
- SrcPTy = SrcTy->getElementType();
- }
-
- if (IC.getTargetData() &&
- (SrcPTy->isIntegerTy() || SrcPTy->isPointerTy() ||
- SrcPTy->isVectorTy()) &&
- // Do not allow turning this into a load of an integer, which is then
- // casted to a pointer, this pessimizes pointer analysis a lot.
- (SrcPTy->isPointerTy() == LI.getType()->isPointerTy()) &&
- IC.getTargetData()->getTypeSizeInBits(SrcPTy) ==
- IC.getTargetData()->getTypeSizeInBits(DestPTy)) {
-
- // Okay, we are casting from one integer or pointer type to another of
- // the same size. Instead of casting the pointer before the load, cast
- // the result of the loaded value.
- LoadInst *NewLoad =
- IC.Builder->CreateLoad(CastOp, LI.isVolatile(), CI->getName());
- NewLoad->setAlignment(LI.getAlignment());
- // Now cast the result of the load.
- return new BitCastInst(NewLoad, LI.getType());
+/// \brief Combine loads to match the type of value their uses after looking
+/// through intervening bitcasts.
+///
+/// The core idea here is that if the result of a load is used in an operation,
+/// we should load the type most conducive to that operation. For example, when
+/// loading an integer and converting that immediately to a pointer, we should
+/// instead directly load a pointer.
+///
+/// However, this routine must never change the width of a load or the number of
+/// loads as that would introduce a semantic change. This combine is expected to
+/// be a semantic no-op which just allows loads to more closely model the types
+/// of their consuming operations.
+///
+/// Currently, we also refuse to change the precise type used for an atomic load
+/// or a volatile load. This is debatable, and might be reasonable to change
+/// later. However, it is risky in case some backend or other part of LLVM is
+/// relying on the exact type loaded to select appropriate atomic operations.
+static Instruction *combineLoadToOperationType(InstCombiner &IC, LoadInst &LI) {
+ // FIXME: We could probably with some care handle both volatile and atomic
+ // loads here but it isn't clear that this is important.
+ if (!LI.isSimple())
+ return nullptr;
+
+ if (LI.use_empty())
+ return nullptr;
+
+ Type *Ty = LI.getType();
+
+ // Try to canonicalize loads which are only ever stored to operate over
+ // integers instead of any other type. We only do this when the loaded type
+ // is sized and has a size exactly the same as its store size and the store
+ // size is a legal integer type.
+ const DataLayout *DL = IC.getDataLayout();
+ if (!Ty->isIntegerTy() && Ty->isSized() && DL &&
+ DL->isLegalInteger(DL->getTypeStoreSizeInBits(Ty)) &&
+ DL->getTypeStoreSizeInBits(Ty) == DL->getTypeSizeInBits(Ty)) {
+ if (std::all_of(LI.user_begin(), LI.user_end(), [&LI](User *U) {
+ auto *SI = dyn_cast<StoreInst>(U);
+ return SI && SI->getPointerOperand() != &LI;
+ })) {
+ LoadInst *NewLoad = combineLoadToNewType(
+ IC, LI,
+ Type::getIntNTy(LI.getContext(), DL->getTypeStoreSizeInBits(Ty)));
+ // Replace all the stores with stores of the newly loaded value.
+ for (auto UI = LI.user_begin(), UE = LI.user_end(); UI != UE;) {
+ auto *SI = cast<StoreInst>(*UI++);
+ IC.Builder->SetInsertPoint(SI);
+ combineStoreToNewValue(IC, *SI, NewLoad);
+ IC.EraseInstFromFunction(*SI);
}
+ assert(LI.use_empty() && "Failed to remove all users of the load!");
+ // Return the old load so the combiner can delete it safely.
+ return &LI;
}
}
- return 0;
+
+ // Fold away bit casts of the loaded value by loading the desired type.
+ if (LI.hasOneUse())
+ if (auto *BC = dyn_cast<BitCastInst>(LI.user_back())) {
+ LoadInst *NewLoad = combineLoadToNewType(IC, LI, BC->getDestTy());
+ BC->replaceAllUsesWith(NewLoad);
+ IC.EraseInstFromFunction(*BC);
+ return &LI;
+ }
+
+ // FIXME: We should also canonicalize loads of vectors when their elements are
+ // cast to other types.
+ return nullptr;
}
Instruction *InstCombiner::visitLoadInst(LoadInst &LI) {
Value *Op = LI.getOperand(0);
+ // Try to canonicalize the loaded type.
+ if (Instruction *Res = combineLoadToOperationType(*this, LI))
+ return Res;
+
// Attempt to improve the alignment.
- if (TD) {
- unsigned KnownAlign =
- GetOrEnforceKnownAlignment(Op, TD->getPrefTypeAlignment(LI.getType()));
- if (KnownAlign >
- (LI.getAlignment() == 0 ? TD->getABITypeAlignment(LI.getType()) :
- LI.getAlignment()))
+ if (DL) {
+ unsigned KnownAlign = getOrEnforceKnownAlignment(
+ Op, DL->getPrefTypeAlignment(LI.getType()), DL, AC, &LI, DT);
+ unsigned LoadAlign = LI.getAlignment();
+ unsigned EffectiveLoadAlign = LoadAlign != 0 ? LoadAlign :
+ DL->getABITypeAlignment(LI.getType());
+
+ if (KnownAlign > EffectiveLoadAlign)
LI.setAlignment(KnownAlign);
+ else if (LoadAlign == 0)
+ LI.setAlignment(EffectiveLoadAlign);
}
- // load (cast X) --> cast (load X) iff safe.
- if (isa<CastInst>(Op))
- if (Instruction *Res = InstCombineLoadCast(*this, LI, TD))
- return Res;
+ // None of the following transforms are legal for volatile/atomic loads.
+ // FIXME: Some of it is okay for atomic loads; needs refactoring.
+ if (!LI.isSimple()) return nullptr;
- // None of the following transforms are legal for volatile loads.
- if (LI.isVolatile()) return 0;
-
// Do really simple store-to-load forwarding and load CSE, to catch cases
- // where there are several consequtive memory accesses to the same location,
+ // where there are several consecutive memory accesses to the same location,
// separated by a few arithmetic operations.
BasicBlock::iterator BBI = &LI;
if (Value *AvailableVal = FindAvailableLoadedValue(Op, LI.getParent(), BBI,6))
- return ReplaceInstUsesWith(LI, AvailableVal);
+ return ReplaceInstUsesWith(
+ LI, Builder->CreateBitOrPointerCast(AvailableVal, LI.getType(),
+ LI.getName() + ".cast"));
// load(gep null, ...) -> unreachable
if (GetElementPtrInst *GEPI = dyn_cast<GetElementPtrInst>(Op)) {
Constant::getNullValue(Op->getType()), &LI);
return ReplaceInstUsesWith(LI, UndefValue::get(LI.getType()));
}
- }
+ }
// load null/undef -> unreachable
// TODO: Consider a target hook for valid address spaces for this xform.
return ReplaceInstUsesWith(LI, UndefValue::get(LI.getType()));
}
- // Instcombine load (constantexpr_cast global) -> cast (load global)
- if (ConstantExpr *CE = dyn_cast<ConstantExpr>(Op))
- if (CE->isCast())
- if (Instruction *Res = InstCombineLoadCast(*this, LI, TD))
- return Res;
-
if (Op->hasOneUse()) {
// Change select and PHI nodes to select values instead of addresses: this
// helps alias analysis out a lot, allows many others simplifications, and
if (SelectInst *SI = dyn_cast<SelectInst>(Op)) {
// load (select (Cond, &V1, &V2)) --> select(Cond, load &V1, load &V2).
unsigned Align = LI.getAlignment();
- if (isSafeToLoadUnconditionally(SI->getOperand(1), SI, Align, TD) &&
- isSafeToLoadUnconditionally(SI->getOperand(2), SI, Align, TD)) {
+ if (isSafeToLoadUnconditionally(SI->getOperand(1), SI, Align, DL) &&
+ isSafeToLoadUnconditionally(SI->getOperand(2), SI, Align, DL)) {
LoadInst *V1 = Builder->CreateLoad(SI->getOperand(1),
SI->getOperand(1)->getName()+".val");
LoadInst *V2 = Builder->CreateLoad(SI->getOperand(2),
}
// load (select (cond, null, P)) -> load P
- if (Constant *C = dyn_cast<Constant>(SI->getOperand(1)))
- if (C->isNullValue()) {
- LI.setOperand(0, SI->getOperand(2));
- return &LI;
- }
+ if (isa<ConstantPointerNull>(SI->getOperand(1)) &&
+ LI.getPointerAddressSpace() == 0) {
+ LI.setOperand(0, SI->getOperand(2));
+ return &LI;
+ }
// load (select (cond, P, null)) -> load P
- if (Constant *C = dyn_cast<Constant>(SI->getOperand(2)))
- if (C->isNullValue()) {
- LI.setOperand(0, SI->getOperand(1));
- return &LI;
- }
+ if (isa<ConstantPointerNull>(SI->getOperand(2)) &&
+ LI.getPointerAddressSpace() == 0) {
+ LI.setOperand(0, SI->getOperand(1));
+ return &LI;
+ }
}
}
- return 0;
+ return nullptr;
}
-/// InstCombineStoreToCast - Fold store V, (cast P) -> store (cast V), P
-/// when possible. This makes it generally easy to do alias analysis and/or
-/// SROA/mem2reg of the memory object.
-static Instruction *InstCombineStoreToCast(InstCombiner &IC, StoreInst &SI) {
- User *CI = cast<User>(SI.getOperand(1));
- Value *CastOp = CI->getOperand(0);
-
- const Type *DestPTy = cast<PointerType>(CI->getType())->getElementType();
- const PointerType *SrcTy = dyn_cast<PointerType>(CastOp->getType());
- if (SrcTy == 0) return 0;
-
- const Type *SrcPTy = SrcTy->getElementType();
-
- if (!DestPTy->isIntegerTy() && !DestPTy->isPointerTy())
- return 0;
-
- /// NewGEPIndices - If SrcPTy is an aggregate type, we can emit a "noop gep"
- /// to its first element. This allows us to handle things like:
- /// store i32 xxx, (bitcast {foo*, float}* %P to i32*)
- /// on 32-bit hosts.
- SmallVector<Value*, 4> NewGEPIndices;
-
- // If the source is an array, the code below will not succeed. Check to
- // see if a trivial 'gep P, 0, 0' will help matters. Only do this for
- // constants.
- if (SrcPTy->isArrayTy() || SrcPTy->isStructTy()) {
- // Index through pointer.
- Constant *Zero = Constant::getNullValue(Type::getInt32Ty(SI.getContext()));
- NewGEPIndices.push_back(Zero);
-
- while (1) {
- if (const StructType *STy = dyn_cast<StructType>(SrcPTy)) {
- if (!STy->getNumElements()) /* Struct can be empty {} */
- break;
- NewGEPIndices.push_back(Zero);
- SrcPTy = STy->getElementType(0);
- } else if (const ArrayType *ATy = dyn_cast<ArrayType>(SrcPTy)) {
- NewGEPIndices.push_back(Zero);
- SrcPTy = ATy->getElementType();
- } else {
- break;
- }
- }
-
- SrcTy = PointerType::get(SrcPTy, SrcTy->getAddressSpace());
- }
+/// \brief Combine stores to match the type of value being stored.
+///
+/// The core idea here is that the memory does not have any intrinsic type and
+/// where we can we should match the type of a store to the type of value being
+/// stored.
+///
+/// However, this routine must never change the width of a store or the number of
+/// stores as that would introduce a semantic change. This combine is expected to
+/// be a semantic no-op which just allows stores to more closely model the types
+/// of their incoming values.
+///
+/// Currently, we also refuse to change the precise type used for an atomic or
+/// volatile store. This is debatable, and might be reasonable to change later.
+/// However, it is risky in case some backend or other part of LLVM is relying
+/// on the exact type stored to select appropriate atomic operations.
+///
+/// \returns true if the store was successfully combined away. This indicates
+/// the caller must erase the store instruction. We have to let the caller erase
+/// the store instruction sas otherwise there is no way to signal whether it was
+/// combined or not: IC.EraseInstFromFunction returns a null pointer.
+static bool combineStoreToValueType(InstCombiner &IC, StoreInst &SI) {
+ // FIXME: We could probably with some care handle both volatile and atomic
+ // stores here but it isn't clear that this is important.
+ if (!SI.isSimple())
+ return false;
- if (!SrcPTy->isIntegerTy() && !SrcPTy->isPointerTy())
- return 0;
-
- // If the pointers point into different address spaces or if they point to
- // values with different sizes, we can't do the transformation.
- if (!IC.getTargetData() ||
- SrcTy->getAddressSpace() !=
- cast<PointerType>(CI->getType())->getAddressSpace() ||
- IC.getTargetData()->getTypeSizeInBits(SrcPTy) !=
- IC.getTargetData()->getTypeSizeInBits(DestPTy))
- return 0;
-
- // Okay, we are casting from one integer or pointer type to another of
- // the same size. Instead of casting the pointer before
- // the store, cast the value to be stored.
- Value *NewCast;
- Value *SIOp0 = SI.getOperand(0);
- Instruction::CastOps opcode = Instruction::BitCast;
- const Type* CastSrcTy = SIOp0->getType();
- const Type* CastDstTy = SrcPTy;
- if (CastDstTy->isPointerTy()) {
- if (CastSrcTy->isIntegerTy())
- opcode = Instruction::IntToPtr;
- } else if (CastDstTy->isIntegerTy()) {
- if (SIOp0->getType()->isPointerTy())
- opcode = Instruction::PtrToInt;
+ Value *V = SI.getValueOperand();
+
+ // Fold away bit casts of the stored value by storing the original type.
+ if (auto *BC = dyn_cast<BitCastInst>(V)) {
+ V = BC->getOperand(0);
+ combineStoreToNewValue(IC, SI, V);
+ return true;
}
-
- // SIOp0 is a pointer to aggregate and this is a store to the first field,
- // emit a GEP to index into its first field.
- if (!NewGEPIndices.empty())
- CastOp = IC.Builder->CreateInBoundsGEP(CastOp, NewGEPIndices.begin(),
- NewGEPIndices.end());
-
- NewCast = IC.Builder->CreateCast(opcode, SIOp0, CastDstTy,
- SIOp0->getName()+".c");
- return new StoreInst(NewCast, CastOp);
+
+ // FIXME: We should also canonicalize loads of vectors when their elements are
+ // cast to other types.
+ return false;
}
/// equivalentAddressValues - Test if A and B will obviously have the same
static bool equivalentAddressValues(Value *A, Value *B) {
// Test if the values are trivially equivalent.
if (A == B) return true;
-
+
// Test if the values come form identical arithmetic instructions.
// This uses isIdenticalToWhenDefined instead of isIdenticalTo because
// its only used to compare two uses within the same basic block, which
if (Instruction *BI = dyn_cast<Instruction>(B))
if (cast<Instruction>(A)->isIdenticalToWhenDefined(BI))
return true;
-
+
// Otherwise they may not be equivalent.
return false;
}
-// If this instruction has two uses, one of which is a llvm.dbg.declare,
-// return the llvm.dbg.declare.
-DbgDeclareInst *InstCombiner::hasOneUsePlusDeclare(Value *V) {
- if (!V->hasNUses(2))
- return 0;
- for (Value::use_iterator UI = V->use_begin(), E = V->use_end();
- UI != E; ++UI) {
- if (DbgDeclareInst *DI = dyn_cast<DbgDeclareInst>(UI))
- return DI;
- if (isa<BitCastInst>(UI) && UI->hasOneUse()) {
- if (DbgDeclareInst *DI = dyn_cast<DbgDeclareInst>(UI->use_begin()))
- return DI;
- }
- }
- return 0;
-}
-
Instruction *InstCombiner::visitStoreInst(StoreInst &SI) {
Value *Val = SI.getOperand(0);
Value *Ptr = SI.getOperand(1);
+ // Try to canonicalize the stored type.
+ if (combineStoreToValueType(*this, SI))
+ return EraseInstFromFunction(SI);
+
+ // Attempt to improve the alignment.
+ if (DL) {
+ unsigned KnownAlign = getOrEnforceKnownAlignment(
+ Ptr, DL->getPrefTypeAlignment(Val->getType()), DL, AC, &SI, DT);
+ unsigned StoreAlign = SI.getAlignment();
+ unsigned EffectiveStoreAlign = StoreAlign != 0 ? StoreAlign :
+ DL->getABITypeAlignment(Val->getType());
+
+ if (KnownAlign > EffectiveStoreAlign)
+ SI.setAlignment(KnownAlign);
+ else if (StoreAlign == 0)
+ SI.setAlignment(EffectiveStoreAlign);
+ }
+
+ // Don't hack volatile/atomic stores.
+ // FIXME: Some bits are legal for atomic stores; needs refactoring.
+ if (!SI.isSimple()) return nullptr;
+
// If the RHS is an alloca with a single use, zapify the store, making the
// alloca dead.
- // If the RHS is an alloca with a two uses, the other one being a
- // llvm.dbg.declare, zapify the store and the declare, making the
- // alloca dead. We must do this to prevent declares from affecting
- // codegen.
- if (!SI.isVolatile()) {
- if (Ptr->hasOneUse()) {
- if (isa<AllocaInst>(Ptr))
- return EraseInstFromFunction(SI);
- if (GetElementPtrInst *GEP = dyn_cast<GetElementPtrInst>(Ptr)) {
- if (isa<AllocaInst>(GEP->getOperand(0))) {
- if (GEP->getOperand(0)->hasOneUse())
- return EraseInstFromFunction(SI);
- if (DbgDeclareInst *DI = hasOneUsePlusDeclare(GEP->getOperand(0))) {
- EraseInstFromFunction(*DI);
- return EraseInstFromFunction(SI);
- }
- }
- }
- }
- if (DbgDeclareInst *DI = hasOneUsePlusDeclare(Ptr)) {
- EraseInstFromFunction(*DI);
+ if (Ptr->hasOneUse()) {
+ if (isa<AllocaInst>(Ptr))
return EraseInstFromFunction(SI);
+ if (GetElementPtrInst *GEP = dyn_cast<GetElementPtrInst>(Ptr)) {
+ if (isa<AllocaInst>(GEP->getOperand(0))) {
+ if (GEP->getOperand(0)->hasOneUse())
+ return EraseInstFromFunction(SI);
+ }
}
}
- // Attempt to improve the alignment.
- if (TD) {
- unsigned KnownAlign =
- GetOrEnforceKnownAlignment(Ptr, TD->getPrefTypeAlignment(Val->getType()));
- if (KnownAlign >
- (SI.getAlignment() == 0 ? TD->getABITypeAlignment(Val->getType()) :
- SI.getAlignment()))
- SI.setAlignment(KnownAlign);
- }
-
// Do really simple DSE, to catch cases where there are several consecutive
// stores to the same location, separated by a few arithmetic operations. This
// situation often occurs with bitfield accesses.
(isa<BitCastInst>(BBI) && BBI->getType()->isPointerTy())) {
ScanInsts++;
continue;
- }
-
+ }
+
if (StoreInst *PrevSI = dyn_cast<StoreInst>(BBI)) {
// Prev store isn't volatile, and stores to the same location?
- if (!PrevSI->isVolatile() &&equivalentAddressValues(PrevSI->getOperand(1),
- SI.getOperand(1))) {
+ if (PrevSI->isSimple() && equivalentAddressValues(PrevSI->getOperand(1),
+ SI.getOperand(1))) {
++NumDeadStore;
++BBI;
EraseInstFromFunction(*PrevSI);
}
break;
}
-
+
// If this is a load, we have to stop. However, if the loaded value is from
// the pointer we're loading and is producing the pointer we're storing,
// then *this* store is dead (X = load P; store X -> P).
if (LoadInst *LI = dyn_cast<LoadInst>(BBI)) {
if (LI == Val && equivalentAddressValues(LI->getOperand(0), Ptr) &&
- !SI.isVolatile())
+ LI->isSimple())
return EraseInstFromFunction(SI);
-
+
// Otherwise, this is a load from some other location. Stores before it
// may not be dead.
break;
}
-
+
// Don't skip over loads or things that can modify memory.
if (BBI->mayWriteToMemory() || BBI->mayReadFromMemory())
break;
}
-
-
- if (SI.isVolatile()) return 0; // Don't hack volatile stores.
// store X, null -> turns into 'unreachable' in SimplifyCFG
if (isa<ConstantPointerNull>(Ptr) && SI.getPointerAddressSpace() == 0) {
if (Instruction *U = dyn_cast<Instruction>(Val))
Worklist.Add(U); // Dropped a use.
}
- return 0; // Do not modify these!
+ return nullptr; // Do not modify these!
}
// store undef, Ptr -> noop
if (isa<UndefValue>(Val))
return EraseInstFromFunction(SI);
- // If the pointer destination is a cast, see if we can fold the cast into the
- // source instead.
- if (isa<CastInst>(Ptr))
- if (Instruction *Res = InstCombineStoreToCast(*this, SI))
- return Res;
- if (ConstantExpr *CE = dyn_cast<ConstantExpr>(Ptr))
- if (CE->isCast())
- if (Instruction *Res = InstCombineStoreToCast(*this, SI))
- return Res;
-
-
// If this store is the last instruction in the basic block (possibly
// excepting debug info instructions), and if the block ends with an
// unconditional branch, try to move it to the successor block.
- BBI = &SI;
+ BBI = &SI;
do {
++BBI;
} while (isa<DbgInfoIntrinsic>(BBI) ||
if (BranchInst *BI = dyn_cast<BranchInst>(BBI))
if (BI->isUnconditional())
if (SimplifyStoreAtEndOfBlock(SI))
- return 0; // xform done!
-
- return 0;
+ return nullptr; // xform done!
+
+ return nullptr;
}
/// SimplifyStoreAtEndOfBlock - Turn things like:
///
bool InstCombiner::SimplifyStoreAtEndOfBlock(StoreInst &SI) {
BasicBlock *StoreBB = SI.getParent();
-
+
// Check to see if the successor block has exactly two incoming edges. If
// so, see if the other predecessor contains a store to the same location.
// if so, insert a PHI node (if needed) and move the stores down.
BasicBlock *DestBB = StoreBB->getTerminator()->getSuccessor(0);
-
+
// Determine whether Dest has exactly two predecessors and, if so, compute
// the other predecessor.
pred_iterator PI = pred_begin(DestBB);
- BasicBlock *OtherBB = 0;
- if (*PI != StoreBB)
- OtherBB = *PI;
- ++PI;
- if (PI == pred_end(DestBB))
+ BasicBlock *P = *PI;
+ BasicBlock *OtherBB = nullptr;
+
+ if (P != StoreBB)
+ OtherBB = P;
+
+ if (++PI == pred_end(DestBB))
return false;
-
- if (*PI != StoreBB) {
+
+ P = *PI;
+ if (P != StoreBB) {
if (OtherBB)
return false;
- OtherBB = *PI;
+ OtherBB = P;
}
if (++PI != pred_end(DestBB))
return false;
BranchInst *OtherBr = dyn_cast<BranchInst>(BBI);
if (!OtherBr || BBI == OtherBB->begin())
return false;
-
+
// If the other block ends in an unconditional branch, check for the 'if then
// else' case. there is an instruction before the branch.
- StoreInst *OtherStore = 0;
+ StoreInst *OtherStore = nullptr;
if (OtherBr->isUnconditional()) {
--BBI;
// Skip over debugging info.
return false;
--BBI;
}
- // If this isn't a store, isn't a store to the same location, or if the
- // alignments differ, bail out.
+ // If this isn't a store, isn't a store to the same location, or is not the
+ // right kind of store, bail out.
OtherStore = dyn_cast<StoreInst>(BBI);
if (!OtherStore || OtherStore->getOperand(1) != SI.getOperand(1) ||
- OtherStore->getAlignment() != SI.getAlignment())
+ !SI.isSameOperationAs(OtherStore))
return false;
} else {
// Otherwise, the other block ended with a conditional branch. If one of the
// destinations is StoreBB, then we have the if/then case.
- if (OtherBr->getSuccessor(0) != StoreBB &&
+ if (OtherBr->getSuccessor(0) != StoreBB &&
OtherBr->getSuccessor(1) != StoreBB)
return false;
-
+
// Okay, we know that OtherBr now goes to Dest and StoreBB, so this is an
// if/then triangle. See if there is a store to the same ptr as SI that
// lives in OtherBB.
// Check to see if we find the matching store.
if ((OtherStore = dyn_cast<StoreInst>(BBI))) {
if (OtherStore->getOperand(1) != SI.getOperand(1) ||
- OtherStore->getAlignment() != SI.getAlignment())
+ !SI.isSameOperationAs(OtherStore))
return false;
break;
}
BBI == OtherBB->begin())
return false;
}
-
+
// In order to eliminate the store in OtherBr, we have to
// make sure nothing reads or overwrites the stored value in
// StoreBB.
return false;
}
}
-
+
// Insert a PHI node now if we need it.
Value *MergedVal = OtherStore->getOperand(0);
if (MergedVal != SI.getOperand(0)) {
- PHINode *PN = PHINode::Create(MergedVal->getType(), "storemerge");
- PN->reserveOperandSpace(2);
+ PHINode *PN = PHINode::Create(MergedVal->getType(), 2, "storemerge");
PN->addIncoming(SI.getOperand(0), SI.getParent());
PN->addIncoming(OtherStore->getOperand(0), OtherBB);
MergedVal = InsertNewInstBefore(PN, DestBB->front());
}
-
+
// Advance to a place where it is safe to insert the new store and
// insert it.
- BBI = DestBB->getFirstNonPHI();
- InsertNewInstBefore(new StoreInst(MergedVal, SI.getOperand(1),
- OtherStore->isVolatile(),
- SI.getAlignment()), *BBI);
-
+ BBI = DestBB->getFirstInsertionPt();
+ StoreInst *NewSI = new StoreInst(MergedVal, SI.getOperand(1),
+ SI.isVolatile(),
+ SI.getAlignment(),
+ SI.getOrdering(),
+ SI.getSynchScope());
+ InsertNewInstBefore(NewSI, *BBI);
+ NewSI->setDebugLoc(OtherStore->getDebugLoc());
+
+ // If the two stores had AA tags, merge them.
+ AAMDNodes AATags;
+ SI.getAAMetadata(AATags);
+ if (AATags) {
+ OtherStore->getAAMetadata(AATags, /* Merge = */ true);
+ NewSI->setAAMetadata(AATags);
+ }
+
// Nuke the old stores.
EraseInstFromFunction(SI);
EraseInstFromFunction(*OtherStore);