diff --git a/lib/Transforms/InstCombine/InstructionCombining.cpp b/lib/Transforms/InstCombine/InstructionCombining.cpp
index 0cab81b1bbe3ae1aa5bc6ff790c21c2d90156ee9..33f024b2729fb25882aba3be73de26b610acb1b3 100644 (file)
//
//===----------------------------------------------------------------------===//
-#define DEBUG_TYPE "instcombine"
#include "llvm/Transforms/Scalar.h"
#include "InstCombine.h"
#include "llvm-c/Initialization.h"
#include "llvm/ADT/SmallPtrSet.h"
#include "llvm/ADT/Statistic.h"
#include "llvm/ADT/StringSwitch.h"
+#include "llvm/Analysis/AssumptionCache.h"
+#include "llvm/Analysis/CFG.h"
#include "llvm/Analysis/ConstantFolding.h"
#include "llvm/Analysis/InstructionSimplify.h"
+#include "llvm/Analysis/LoopInfo.h"
#include "llvm/Analysis/MemoryBuiltins.h"
+#include "llvm/Analysis/ValueTracking.h"
#include "llvm/IR/CFG.h"
#include "llvm/IR/DataLayout.h"
+#include "llvm/IR/Dominators.h"
#include "llvm/IR/GetElementPtrTypeIterator.h"
#include "llvm/IR/IntrinsicInst.h"
#include "llvm/IR/PatternMatch.h"
#include "llvm/IR/ValueHandle.h"
#include "llvm/Support/CommandLine.h"
#include "llvm/Support/Debug.h"
-#include "llvm/Target/TargetLibraryInfo.h"
+#include "llvm/Analysis/TargetLibraryInfo.h"
#include "llvm/Transforms/Utils/Local.h"
#include <algorithm>
#include <climits>
using namespace llvm;
using namespace llvm::PatternMatch;
+#define DEBUG_TYPE "instcombine"
+
STATISTIC(NumCombined , "Number of insts combined");
STATISTIC(NumConstProp, "Number of constant folds");
STATISTIC(NumDeadInst , "Number of dead inst eliminated");
STATISTIC(NumFactor , "Number of factorizations");
STATISTIC(NumReassoc , "Number of reassociations");
-static cl::opt<bool> UnsafeFPShrink("enable-double-float-shrink", cl::Hidden,
- cl::init(false),
- cl::desc("Enable unsafe double to float "
- "shrinking for math lib calls"));
-
-// Initialization Routines
-void llvm::initializeInstCombine(PassRegistry &Registry) {
- initializeInstCombinerPass(Registry);
-}
-
-void LLVMInitializeInstCombine(LLVMPassRegistryRef R) {
- initializeInstCombine(*unwrap(R));
-}
-
-char InstCombiner::ID = 0;
-INITIALIZE_PASS_BEGIN(InstCombiner, "instcombine",
- "Combine redundant instructions", false, false)
-INITIALIZE_PASS_DEPENDENCY(TargetLibraryInfo)
-INITIALIZE_PASS_END(InstCombiner, "instcombine",
- "Combine redundant instructions", false, false)
-
-void InstCombiner::getAnalysisUsage(AnalysisUsage &AU) const {
- AU.setPreservesCFG();
- AU.addRequired<TargetLibraryInfo>();
-}
-
-
Value *InstCombiner::EmitGEPOffset(User *GEP) {
return llvm::EmitGEPOffset(Builder, *getDataLayout(), GEP);
}
Instruction::BinaryOps ROp) {
if (Instruction::isCommutative(ROp))
return LeftDistributesOverRight(ROp, LOp);
+
+ switch (LOp) {
+ default:
+ return false;
+ // (X >> Z) & (Y >> Z) -> (X&Y) >> Z for all shifts.
+ // (X >> Z) | (Y >> Z) -> (X|Y) >> Z for all shifts.
+ // (X >> Z) ^ (Y >> Z) -> (X^Y) >> Z for all shifts.
+ case Instruction::And:
+ case Instruction::Or:
+ case Instruction::Xor:
+ switch (ROp) {
+ default:
+ return false;
+ case Instruction::Shl:
+ case Instruction::LShr:
+ case Instruction::AShr:
+ return true;
+ }
+ }
// TODO: It would be nice to handle division, aka "(X + Y)/Z = X/Z + Y/Z",
// but this requires knowing that the addition does not overflow and other
// such subtleties.
return false;
}
+/// This function returns identity value for given opcode, which can be used to
+/// factor patterns like (X * 2) + X ==> (X * 2) + (X * 1) ==> X * (2 + 1).
+static Value *getIdentityValue(Instruction::BinaryOps OpCode, Value *V) {
+ if (isa<Constant>(V))
+ return nullptr;
+
+ if (OpCode == Instruction::Mul)
+ return ConstantInt::get(V->getType(), 1);
+
+ // TODO: We can handle other cases e.g. Instruction::And, Instruction::Or etc.
+
+ return nullptr;
+}
+
+/// This function factors binary ops which can be combined using distributive
+/// laws. This function tries to transform 'Op' based TopLevelOpcode to enable
+/// factorization e.g for ADD(SHL(X , 2), MUL(X, 5)), When this function called
+/// with TopLevelOpcode == Instruction::Add and Op = SHL(X, 2), transforms
+/// SHL(X, 2) to MUL(X, 4) i.e. returns Instruction::Mul with LHS set to 'X' and
+/// RHS to 4.
+static Instruction::BinaryOps
+getBinOpsForFactorization(Instruction::BinaryOps TopLevelOpcode,
+ BinaryOperator *Op, Value *&LHS, Value *&RHS) {
+ if (!Op)
+ return Instruction::BinaryOpsEnd;
+
+ LHS = Op->getOperand(0);
+ RHS = Op->getOperand(1);
+
+ switch (TopLevelOpcode) {
+ default:
+ return Op->getOpcode();
+
+ case Instruction::Add:
+ case Instruction::Sub:
+ if (Op->getOpcode() == Instruction::Shl) {
+ if (Constant *CST = dyn_cast<Constant>(Op->getOperand(1))) {
+ // The multiplier is really 1 << CST.
+ RHS = ConstantExpr::getShl(ConstantInt::get(Op->getType(), 1), CST);
+ return Instruction::Mul;
+ }
+ }
+ return Op->getOpcode();
+ }
+
+ // TODO: We can add other conversions e.g. shr => div etc.
+}
+
+/// This tries to simplify binary operations by factorizing out common terms
+/// (e. g. "(A*B)+(A*C)" -> "A*(B+C)").
+static Value *tryFactorization(InstCombiner::BuilderTy *Builder,
+ const DataLayout *DL, BinaryOperator &I,
+ Instruction::BinaryOps InnerOpcode, Value *A,
+ Value *B, Value *C, Value *D) {
+
+ // If any of A, B, C, D are null, we can not factor I, return early.
+ // Checking A and C should be enough.
+ if (!A || !C || !B || !D)
+ return nullptr;
+
+ Value *SimplifiedInst = nullptr;
+ Value *LHS = I.getOperand(0), *RHS = I.getOperand(1);
+ Instruction::BinaryOps TopLevelOpcode = I.getOpcode();
+
+ // Does "X op' Y" always equal "Y op' X"?
+ bool InnerCommutative = Instruction::isCommutative(InnerOpcode);
+
+ // Does "X op' (Y op Z)" always equal "(X op' Y) op (X op' Z)"?
+ if (LeftDistributesOverRight(InnerOpcode, TopLevelOpcode))
+ // Does the instruction have the form "(A op' B) op (A op' D)" or, in the
+ // commutative case, "(A op' B) op (C op' A)"?
+ if (A == C || (InnerCommutative && A == D)) {
+ if (A != C)
+ std::swap(C, D);
+ // Consider forming "A op' (B op D)".
+ // If "B op D" simplifies then it can be formed with no cost.
+ Value *V = SimplifyBinOp(TopLevelOpcode, B, D, DL);
+ // If "B op D" doesn't simplify then only go on if both of the existing
+ // operations "A op' B" and "C op' D" will be zapped as no longer used.
+ if (!V && LHS->hasOneUse() && RHS->hasOneUse())
+ V = Builder->CreateBinOp(TopLevelOpcode, B, D, RHS->getName());
+ if (V) {
+ SimplifiedInst = Builder->CreateBinOp(InnerOpcode, A, V);
+ }
+ }
+
+ // Does "(X op Y) op' Z" always equal "(X op' Z) op (Y op' Z)"?
+ if (!SimplifiedInst && RightDistributesOverLeft(TopLevelOpcode, InnerOpcode))
+ // Does the instruction have the form "(A op' B) op (C op' B)" or, in the
+ // commutative case, "(A op' B) op (B op' D)"?
+ if (B == D || (InnerCommutative && B == C)) {
+ if (B != D)
+ std::swap(C, D);
+ // Consider forming "(A op C) op' B".
+ // If "A op C" simplifies then it can be formed with no cost.
+ Value *V = SimplifyBinOp(TopLevelOpcode, A, C, DL);
+
+ // If "A op C" doesn't simplify then only go on if both of the existing
+ // operations "A op' B" and "C op' D" will be zapped as no longer used.
+ if (!V && LHS->hasOneUse() && RHS->hasOneUse())
+ V = Builder->CreateBinOp(TopLevelOpcode, A, C, LHS->getName());
+ if (V) {
+ SimplifiedInst = Builder->CreateBinOp(InnerOpcode, V, B);
+ }
+ }
+
+ if (SimplifiedInst) {
+ ++NumFactor;
+ SimplifiedInst->takeName(&I);
+
+ // Check if we can add NSW flag to SimplifiedInst. If so, set NSW flag.
+ // TODO: Check for NUW.
+ if (BinaryOperator *BO = dyn_cast<BinaryOperator>(SimplifiedInst)) {
+ if (isa<OverflowingBinaryOperator>(SimplifiedInst)) {
+ bool HasNSW = false;
+ if (isa<OverflowingBinaryOperator>(&I))
+ HasNSW = I.hasNoSignedWrap();
+
+ if (BinaryOperator *Op0 = dyn_cast<BinaryOperator>(LHS))
+ if (isa<OverflowingBinaryOperator>(Op0))
+ HasNSW &= Op0->hasNoSignedWrap();
+
+ if (BinaryOperator *Op1 = dyn_cast<BinaryOperator>(RHS))
+ if (isa<OverflowingBinaryOperator>(Op1))
+ HasNSW &= Op1->hasNoSignedWrap();
+ BO->setHasNoSignedWrap(HasNSW);
+ }
+ }
+ }
+ return SimplifiedInst;
+}
+
/// SimplifyUsingDistributiveLaws - This tries to simplify binary operations
/// which some other binary operation distributes over either by factorizing
/// out common terms (eg "(A*B)+(A*C)" -> "A*(B+C)") or expanding out if this
Value *LHS = I.getOperand(0), *RHS = I.getOperand(1);
BinaryOperator *Op0 = dyn_cast<BinaryOperator>(LHS);
BinaryOperator *Op1 = dyn_cast<BinaryOperator>(RHS);
- Instruction::BinaryOps TopLevelOpcode = I.getOpcode(); // op
// Factorization.
- if (Op0 && Op1 && Op0->getOpcode() == Op1->getOpcode()) {
- // The instruction has the form "(A op' B) op (C op' D)". Try to factorize
- // a common term.
- Value *A = Op0->getOperand(0), *B = Op0->getOperand(1);
- Value *C = Op1->getOperand(0), *D = Op1->getOperand(1);
- Instruction::BinaryOps InnerOpcode = Op0->getOpcode(); // op'
+ Value *A = nullptr, *B = nullptr, *C = nullptr, *D = nullptr;
+ auto TopLevelOpcode = I.getOpcode();
+ auto LHSOpcode = getBinOpsForFactorization(TopLevelOpcode, Op0, A, B);
+ auto RHSOpcode = getBinOpsForFactorization(TopLevelOpcode, Op1, C, D);
+
+ // The instruction has the form "(A op' B) op (C op' D)". Try to factorize
+ // a common term.
+ if (LHSOpcode == RHSOpcode) {
+ if (Value *V = tryFactorization(Builder, DL, I, LHSOpcode, A, B, C, D))
+ return V;
+ }
- // Does "X op' Y" always equal "Y op' X"?
- bool InnerCommutative = Instruction::isCommutative(InnerOpcode);
-
- // Does "X op' (Y op Z)" always equal "(X op' Y) op (X op' Z)"?
- if (LeftDistributesOverRight(InnerOpcode, TopLevelOpcode))
- // Does the instruction have the form "(A op' B) op (A op' D)" or, in the
- // commutative case, "(A op' B) op (C op' A)"?
- if (A == C || (InnerCommutative && A == D)) {
- if (A != C)
- std::swap(C, D);
- // Consider forming "A op' (B op D)".
- // If "B op D" simplifies then it can be formed with no cost.
- Value *V = SimplifyBinOp(TopLevelOpcode, B, D, DL);
- // If "B op D" doesn't simplify then only go on if both of the existing
- // operations "A op' B" and "C op' D" will be zapped as no longer used.
- if (!V && Op0->hasOneUse() && Op1->hasOneUse())
- V = Builder->CreateBinOp(TopLevelOpcode, B, D, Op1->getName());
- if (V) {
- ++NumFactor;
- V = Builder->CreateBinOp(InnerOpcode, A, V);
- V->takeName(&I);
- return V;
- }
- }
+ // The instruction has the form "(A op' B) op (C)". Try to factorize common
+ // term.
+ if (Value *V = tryFactorization(Builder, DL, I, LHSOpcode, A, B, RHS,
+ getIdentityValue(LHSOpcode, RHS)))
+ return V;
- // Does "(X op Y) op' Z" always equal "(X op' Z) op (Y op' Z)"?
- if (RightDistributesOverLeft(TopLevelOpcode, InnerOpcode))
- // Does the instruction have the form "(A op' B) op (C op' B)" or, in the
- // commutative case, "(A op' B) op (B op' D)"?
- if (B == D || (InnerCommutative && B == C)) {
- if (B != D)
- std::swap(C, D);
- // Consider forming "(A op C) op' B".
- // If "A op C" simplifies then it can be formed with no cost.
- Value *V = SimplifyBinOp(TopLevelOpcode, A, C, DL);
- // If "A op C" doesn't simplify then only go on if both of the existing
- // operations "A op' B" and "C op' D" will be zapped as no longer used.
- if (!V && Op0->hasOneUse() && Op1->hasOneUse())
- V = Builder->CreateBinOp(TopLevelOpcode, A, C, Op0->getName());
- if (V) {
- ++NumFactor;
- V = Builder->CreateBinOp(InnerOpcode, V, B);
- V->takeName(&I);
- return V;
- }
- }
- }
+ // The instruction has the form "(B) op (C op' D)". Try to factorize common
+ // term.
+ if (Value *V = tryFactorization(Builder, DL, I, RHSOpcode, LHS,
+ getIdentityValue(RHSOpcode, LHS), C, D))
+ return V;
// Expansion.
if (Op0 && RightDistributesOverLeft(Op0->getOpcode(), TopLevelOpcode)) {
}
}
- return 0;
+ return nullptr;
}
// dyn_castNegVal - Given a 'sub' instruction, return the RHS of the instruction
if (C->getType()->getElementType()->isIntegerTy())
return ConstantExpr::getNeg(C);
- return 0;
+ return nullptr;
}
// dyn_castFNegVal - Given a 'fsub' instruction, return the RHS of the
if (C->getType()->getElementType()->isFloatingPointTy())
return ConstantExpr::getFNeg(C);
- return 0;
+ return nullptr;
}
static Value *FoldOperationIntoSelectOperand(Instruction &I, Value *SO,
// not have a second operand.
Instruction *InstCombiner::FoldOpIntoSelect(Instruction &Op, SelectInst *SI) {
// Don't modify shared select instructions
- if (!SI->hasOneUse()) return 0;
+ if (!SI->hasOneUse()) return nullptr;
Value *TV = SI->getOperand(1);
Value *FV = SI->getOperand(2);
if (isa<Constant>(TV) || isa<Constant>(FV)) {
// Bool selects with constant operands can be folded to logical ops.
- if (SI->getType()->isIntegerTy(1)) return 0;
+ if (SI->getType()->isIntegerTy(1)) return nullptr;
// If it's a bitcast involving vectors, make sure it has the same number of
// elements on both sides.
@@ -610,10 +708,10 @@ Instruction *InstCombiner::FoldOpIntoSelect(Instruction &Op, SelectInst *SI) {
VectorType *SrcTy = dyn_cast<VectorType>(BC->getSrcTy());
// Verify that either both or neither are vectors.
- if ((SrcTy == NULL) != (DestTy == NULL)) return 0;
+ if ((SrcTy == nullptr) != (DestTy == nullptr)) return nullptr;
// If vectors, verify that they have the same number of elements.
if (SrcTy && SrcTy->getNumElements() != DestTy->getNumElements())
- return 0;
+ return nullptr;
}
Value *SelectTrueVal = FoldOperationIntoSelectOperand(Op, TV, this);
return SelectInst::Create(SI->getCondition(),
SelectTrueVal, SelectFalseVal);
}
- return 0;
+ return nullptr;
}
PHINode *PN = cast<PHINode>(I.getOperand(0));
unsigned NumPHIValues = PN->getNumIncomingValues();
if (NumPHIValues == 0)
- return 0;
+ return nullptr;
// We normally only transform phis with a single use. However, if a PHI has
// multiple uses and they are all the same operation, we can fold *all* of the
for (User *U : PN->users()) {
Instruction *UI = cast<Instruction>(U);
if (UI != &I && !I.isIdenticalTo(UI))
- return 0;
+ return nullptr;
}
// Otherwise, we can replace *all* users with the new PHI we form.
}
// remember the BB it is in. If there is more than one or if *it* is a PHI,
// bail out. We don't do arbitrary constant expressions here because moving
// their computation can be expensive without a cost model.
- BasicBlock *NonConstBB = 0;
+ BasicBlock *NonConstBB = nullptr;
for (unsigned i = 0; i != NumPHIValues; ++i) {
Value *InVal = PN->getIncomingValue(i);
if (isa<Constant>(InVal) && !isa<ConstantExpr>(InVal))
continue;
- if (isa<PHINode>(InVal)) return 0; // Itself a phi.
- if (NonConstBB) return 0; // More than one non-const value.
+ if (isa<PHINode>(InVal)) return nullptr; // Itself a phi.
+ if (NonConstBB) return nullptr; // More than one non-const value.
NonConstBB = PN->getIncomingBlock(i);
// insert a computation after it without breaking the edge.
if (InvokeInst *II = dyn_cast<InvokeInst>(InVal))
if (II->getParent() == NonConstBB)
- return 0;
+ return nullptr;
// If the incoming non-constant value is in I's block, we will remove one
// instruction, but insert another equivalent one, leading to infinite
// instcombine.
- if (NonConstBB == I.getParent())
- return 0;
+ if (isPotentiallyReachable(I.getParent(), NonConstBB, DT, LI))
+ return nullptr;
}
// If there is exactly one non-constant value, we can insert a copy of the
// operation in that block. However, if this is a critical edge, we would be
- // inserting the computation one some other paths (e.g. inside a loop). Only
+ // inserting the computation on some other paths (e.g. inside a loop). Only
// do this if the pred block is unconditionally branching into the phi block.
- if (NonConstBB != 0) {
+ if (NonConstBB != nullptr) {
BranchInst *BI = dyn_cast<BranchInst>(NonConstBB->getTerminator());
- if (!BI || !BI->isUnconditional()) return 0;
+ if (!BI || !BI->isUnconditional()) return nullptr;
}
// Okay, we can do the transformation: create the new PHI node.
BasicBlock *ThisBB = PN->getIncomingBlock(i);
Value *TrueVInPred = TrueV->DoPHITranslation(PhiTransBB, ThisBB);
Value *FalseVInPred = FalseV->DoPHITranslation(PhiTransBB, ThisBB);
- Value *InV = 0;
+ Value *InV = nullptr;
// Beware of ConstantExpr: it may eventually evaluate to getNullValue,
// even if currently isNullValue gives false.
Constant *InC = dyn_cast<Constant>(PN->getIncomingValue(i));
} else if (CmpInst *CI = dyn_cast<CmpInst>(&I)) {
Constant *C = cast<Constant>(I.getOperand(1));
for (unsigned i = 0; i != NumPHIValues; ++i) {
- Value *InV = 0;
+ Value *InV = nullptr;
if (Constant *InC = dyn_cast<Constant>(PN->getIncomingValue(i)))
InV = ConstantExpr::getCompare(CI->getPredicate(), InC, C);
else if (isa<ICmpInst>(CI))
} else if (I.getNumOperands() == 2) {
Constant *C = cast<Constant>(I.getOperand(1));
for (unsigned i = 0; i != NumPHIValues; ++i) {
- Value *InV = 0;
+ Value *InV = nullptr;
if (Constant *InC = dyn_cast<Constant>(PN->getIncomingValue(i)))
InV = ConstantExpr::get(I.getOpcode(), InC, C);
else
assert(PtrTy->isPtrOrPtrVectorTy());
if (!DL)
- return 0;
+ return nullptr;
Type *Ty = PtrTy->getPointerElementType();
if (!Ty->isSized())
- return 0;
+ return nullptr;
// Start with the index over the outer type. Note that the type size
// might be zero (even if the offset isn't zero) if the indexed type
while (Offset) {
// Indexing into tail padding between struct/array elements.
if (uint64_t(Offset*8) >= DL->getTypeSizeInBits(Ty))
- return 0;
+ return nullptr;
if (StructType *STy = dyn_cast<StructType>(Ty)) {
const StructLayout *SL = DL->getStructLayout(STy);
Ty = AT->getElementType();
} else {
// Otherwise, we can't index into the middle of this atomic type, bail.
- return 0;
+ return nullptr;
}
}
// If Scale is zero then it does not divide Val.
if (Scale.isMinValue())
- return 0;
+ return nullptr;
// Look through chains of multiplications, searching for a constant that is
// divisible by Scale. For example, descaling X*(Y*(Z*4)) by a factor of 4
APInt::sdivrem(CI->getValue(), Scale, Quotient, Remainder);
if (!Remainder.isMinValue())
// Not divisible by Scale.
- return 0;
+ return nullptr;
// Replace with the quotient in the parent.
Op = ConstantInt::get(CI->getType(), Quotient);
NoSignedWrap = true;
// Multiplication.
NoSignedWrap = BO->hasNoSignedWrap();
if (RequireNoSignedWrap && !NoSignedWrap)
- return 0;
+ return nullptr;
// There are three cases for multiplication: multiplication by exactly
// the scale, multiplication by a constant different to the scale, and
// Otherwise drill down into the constant.
if (!Op->hasOneUse())
- return 0;
+ return nullptr;
Parent = std::make_pair(BO, 1);
continue;
// Multiplication by something else. Drill down into the left-hand side
// since that's where the reassociate pass puts the good stuff.
if (!Op->hasOneUse())
- return 0;
+ return nullptr;
Parent = std::make_pair(BO, 0);
continue;
// Multiplication by a power of 2.
NoSignedWrap = BO->hasNoSignedWrap();
if (RequireNoSignedWrap && !NoSignedWrap)
- return 0;
+ return nullptr;
Value *LHS = BO->getOperand(0);
int32_t Amt = cast<ConstantInt>(BO->getOperand(1))->
break;
}
if (Amt < logScale || !Op->hasOneUse())
- return 0;
+ return nullptr;
// Multiplication by more than the scale. Reduce the multiplying amount
// by the scale in the parent.
}
if (!Op->hasOneUse())
- return 0;
+ return nullptr;
if (CastInst *Cast = dyn_cast<CastInst>(Op)) {
if (Cast->getOpcode() == Instruction::SExt) {
// Scale and the multiplication Y * SmallScale should not overflow.
if (SmallScale.sext(Scale.getBitWidth()) != Scale)
// SmallScale does not sign-extend to Scale.
- return 0;
+ return nullptr;
assert(SmallScale.exactLogBase2() == logScale);
// Require that Y * SmallScale must not overflow.
RequireNoSignedWrap = true;
// trunc (Y * sext Scale) does not, so nsw flags need to be cleared
// from this point up in the expression (see later).
if (RequireNoSignedWrap)
- return 0;
+ return nullptr;
// Drill down through the cast.
unsigned LargeSize = Cast->getSrcTy()->getPrimitiveSizeInBits();
}
// Unsupported expression, bail out.
- return 0;
+ return nullptr;
+ }
+
+ // If Op is zero then Val = Op * Scale.
+ if (match(Op, m_Zero())) {
+ NoSignedWrap = true;
+ return Op;
}
// We know that we can successfully descale, so from here on we can safely
@@ -1082,10 +1186,112 @@ Value *InstCombiner::Descale(Value *Val, APInt Scale, bool &NoSignedWrap) {
} while (1);
}
+/// \brief Creates node of binary operation with the same attributes as the
+/// specified one but with other operands.
+static Value *CreateBinOpAsGiven(BinaryOperator &Inst, Value *LHS, Value *RHS,
+ InstCombiner::BuilderTy *B) {
+ Value *BORes = B->CreateBinOp(Inst.getOpcode(), LHS, RHS);
+ if (BinaryOperator *NewBO = dyn_cast<BinaryOperator>(BORes)) {
+ if (isa<OverflowingBinaryOperator>(NewBO)) {
+ NewBO->setHasNoSignedWrap(Inst.hasNoSignedWrap());
+ NewBO->setHasNoUnsignedWrap(Inst.hasNoUnsignedWrap());
+ }
+ if (isa<PossiblyExactOperator>(NewBO))
+ NewBO->setIsExact(Inst.isExact());
+ }
+ return BORes;
+}
+
+/// \brief Makes transformation of binary operation specific for vector types.
+/// \param Inst Binary operator to transform.
+/// \return Pointer to node that must replace the original binary operator, or
+/// null pointer if no transformation was made.
+Value *InstCombiner::SimplifyVectorOp(BinaryOperator &Inst) {
+ if (!Inst.getType()->isVectorTy()) return nullptr;
+
+ // It may not be safe to reorder shuffles and things like div, urem, etc.
+ // because we may trap when executing those ops on unknown vector elements.
+ // See PR20059.
+ if (!isSafeToSpeculativelyExecute(&Inst, DL)) return nullptr;
+
+ unsigned VWidth = cast<VectorType>(Inst.getType())->getNumElements();
+ Value *LHS = Inst.getOperand(0), *RHS = Inst.getOperand(1);
+ assert(cast<VectorType>(LHS->getType())->getNumElements() == VWidth);
+ assert(cast<VectorType>(RHS->getType())->getNumElements() == VWidth);
+
+ // If both arguments of binary operation are shuffles, which use the same
+ // mask and shuffle within a single vector, it is worthwhile to move the
+ // shuffle after binary operation:
+ // Op(shuffle(v1, m), shuffle(v2, m)) -> shuffle(Op(v1, v2), m)
+ if (isa<ShuffleVectorInst>(LHS) && isa<ShuffleVectorInst>(RHS)) {
+ ShuffleVectorInst *LShuf = cast<ShuffleVectorInst>(LHS);
+ ShuffleVectorInst *RShuf = cast<ShuffleVectorInst>(RHS);
+ if (isa<UndefValue>(LShuf->getOperand(1)) &&
+ isa<UndefValue>(RShuf->getOperand(1)) &&
+ LShuf->getOperand(0)->getType() == RShuf->getOperand(0)->getType() &&
+ LShuf->getMask() == RShuf->getMask()) {
+ Value *NewBO = CreateBinOpAsGiven(Inst, LShuf->getOperand(0),
+ RShuf->getOperand(0), Builder);
+ Value *Res = Builder->CreateShuffleVector(NewBO,
+ UndefValue::get(NewBO->getType()), LShuf->getMask());
+ return Res;
+ }
+ }
+
+ // If one argument is a shuffle within one vector, the other is a constant,
+ // try moving the shuffle after the binary operation.
+ ShuffleVectorInst *Shuffle = nullptr;
+ Constant *C1 = nullptr;
+ if (isa<ShuffleVectorInst>(LHS)) Shuffle = cast<ShuffleVectorInst>(LHS);
+ if (isa<ShuffleVectorInst>(RHS)) Shuffle = cast<ShuffleVectorInst>(RHS);
+ if (isa<Constant>(LHS)) C1 = cast<Constant>(LHS);
+ if (isa<Constant>(RHS)) C1 = cast<Constant>(RHS);
+ if (Shuffle && C1 &&
+ (isa<ConstantVector>(C1) || isa<ConstantDataVector>(C1)) &&
+ isa<UndefValue>(Shuffle->getOperand(1)) &&
+ Shuffle->getType() == Shuffle->getOperand(0)->getType()) {
+ SmallVector<int, 16> ShMask = Shuffle->getShuffleMask();
+ // Find constant C2 that has property:
+ // shuffle(C2, ShMask) = C1
+ // If such constant does not exist (example: ShMask=<0,0> and C1=<1,2>)
+ // reorder is not possible.
+ SmallVector<Constant*, 16> C2M(VWidth,
+ UndefValue::get(C1->getType()->getScalarType()));
+ bool MayChange = true;
+ for (unsigned I = 0; I < VWidth; ++I) {
+ if (ShMask[I] >= 0) {
+ assert(ShMask[I] < (int)VWidth);
+ if (!isa<UndefValue>(C2M[ShMask[I]])) {
+ MayChange = false;
+ break;
+ }
+ C2M[ShMask[I]] = C1->getAggregateElement(I);
+ }
+ }
+ if (MayChange) {
+ Constant *C2 = ConstantVector::get(C2M);
+ Value *NewLHS, *NewRHS;
+ if (isa<Constant>(LHS)) {
+ NewLHS = C2;
+ NewRHS = Shuffle->getOperand(0);
+ } else {
+ NewLHS = Shuffle->getOperand(0);
+ NewRHS = C2;
+ }
+ Value *NewBO = CreateBinOpAsGiven(Inst, NewLHS, NewRHS, Builder);
+ Value *Res = Builder->CreateShuffleVector(NewBO,
+ UndefValue::get(Inst.getType()), Shuffle->getMask());
+ return Res;
+ }
+ }
+
+ return nullptr;
+}
+
Instruction *InstCombiner::visitGetElementPtrInst(GetElementPtrInst &GEP) {
SmallVector<Value*, 8> Ops(GEP.op_begin(), GEP.op_end());
- if (Value *V = SimplifyGEPInst(Ops, DL))
+ if (Value *V = SimplifyGEPInst(Ops, DL, TLI, DT, AC))
return ReplaceInstUsesWith(GEP, V);
Value *PtrOp = GEP.getOperand(0);
if (MadeChange) return &GEP;
}
+ // Check to see if the inputs to the PHI node are getelementptr instructions.
+ if (PHINode *PN = dyn_cast<PHINode>(PtrOp)) {
+ GetElementPtrInst *Op1 = dyn_cast<GetElementPtrInst>(PN->getOperand(0));
+ if (!Op1)
+ return nullptr;
+
+ signed DI = -1;
+
+ for (auto I = PN->op_begin()+1, E = PN->op_end(); I !=E; ++I) {
+ GetElementPtrInst *Op2 = dyn_cast<GetElementPtrInst>(*I);
+ if (!Op2 || Op1->getNumOperands() != Op2->getNumOperands())
+ return nullptr;
+
+ // Keep track of the type as we walk the GEP.
+ Type *CurTy = Op1->getOperand(0)->getType()->getScalarType();
+
+ for (unsigned J = 0, F = Op1->getNumOperands(); J != F; ++J) {
+ if (Op1->getOperand(J)->getType() != Op2->getOperand(J)->getType())
+ return nullptr;
+
+ if (Op1->getOperand(J) != Op2->getOperand(J)) {
+ if (DI == -1) {
+ // We have not seen any differences yet in the GEPs feeding the
+ // PHI yet, so we record this one if it is allowed to be a
+ // variable.
+
+ // The first two arguments can vary for any GEP, the rest have to be
+ // static for struct slots
+ if (J > 1 && CurTy->isStructTy())
+ return nullptr;
+
+ DI = J;
+ } else {
+ // The GEP is different by more than one input. While this could be
+ // extended to support GEPs that vary by more than one variable it
+ // doesn't make sense since it greatly increases the complexity and
+ // would result in an R+R+R addressing mode which no backend
+ // directly supports and would need to be broken into several
+ // simpler instructions anyway.
+ return nullptr;
+ }
+ }
+
+ // Sink down a layer of the type for the next iteration.
+ if (J > 0) {
+ if (CompositeType *CT = dyn_cast<CompositeType>(CurTy)) {
+ CurTy = CT->getTypeAtIndex(Op1->getOperand(J));
+ } else {
+ CurTy = nullptr;
+ }
+ }
+ }
+ }
+
+ GetElementPtrInst *NewGEP = cast<GetElementPtrInst>(Op1->clone());
+
+ if (DI == -1) {
+ // All the GEPs feeding the PHI are identical. Clone one down into our
+ // BB so that it can be merged with the current GEP.
+ GEP.getParent()->getInstList().insert(GEP.getParent()->getFirstNonPHI(),
+ NewGEP);
+ } else {
+ // All the GEPs feeding the PHI differ at a single offset. Clone a GEP
+ // into the current block so it can be merged, and create a new PHI to
+ // set that index.
+ Instruction *InsertPt = Builder->GetInsertPoint();
+ Builder->SetInsertPoint(PN);
+ PHINode *NewPN = Builder->CreatePHI(Op1->getOperand(DI)->getType(),
+ PN->getNumOperands());
+ Builder->SetInsertPoint(InsertPt);
+
+ for (auto &I : PN->operands())
+ NewPN->addIncoming(cast<GEPOperator>(I)->getOperand(DI),
+ PN->getIncomingBlock(I));
+
+ NewGEP->setOperand(DI, NewPN);
+ GEP.getParent()->getInstList().insert(GEP.getParent()->getFirstNonPHI(),
+ NewGEP);
+ NewGEP->setOperand(DI, NewPN);
+ }
+
+ GEP.setOperand(0, NewGEP);
+ PtrOp = NewGEP;
+ }
+
// Combine Indices - If the source pointer to this getelementptr instruction
// is a getelementptr instruction, combine the indices of the two
// getelementptr instructions into a single instruction.
//
if (GEPOperator *Src = dyn_cast<GEPOperator>(PtrOp)) {
if (!shouldMergeGEPs(*cast<GEPOperator>(&GEP), *Src))
- return 0;
+ return nullptr;
// Note that if our source is a gep chain itself then we wait for that
// chain to be resolved before we perform this transformation. This
if (GEPOperator *SrcGEP =
dyn_cast<GEPOperator>(Src->getOperand(0)))
if (SrcGEP->getNumOperands() == 2 && shouldMergeGEPs(*Src, *SrcGEP))
- return 0; // Wait until our source is folded to completion.
+ return nullptr; // Wait until our source is folded to completion.
SmallVector<Value*, 8> Indices;
// intptr_t). Just avoid transforming this until the input has been
// normalized.
if (SO1->getType() != GO1->getType())
- return 0;
+ return nullptr;
Sum = Builder->CreateAdd(SO1, GO1, PtrOp->getName()+".sum");
}
GetElementPtrInst::Create(Src->getOperand(0), Indices, GEP.getName());
}
- // Canonicalize (gep i8* X, -(ptrtoint Y)) to (sub (ptrtoint X), (ptrtoint Y))
- // The GEP pattern is emitted by the SCEV expander for certain kinds of
- // pointer arithmetic.
- if (DL && GEP.getNumIndices() == 1 &&
- match(GEP.getOperand(1), m_Neg(m_PtrToInt(m_Value())))) {
+ if (DL && GEP.getNumIndices() == 1) {
unsigned AS = GEP.getPointerAddressSpace();
- if (GEP.getType() == Builder->getInt8PtrTy(AS) &&
- GEP.getOperand(1)->getType()->getScalarSizeInBits() ==
+ if (GEP.getOperand(1)->getType()->getScalarSizeInBits() ==
DL->getPointerSizeInBits(AS)) {
- Operator *Index = cast<Operator>(GEP.getOperand(1));
- Value *PtrToInt = Builder->CreatePtrToInt(PtrOp, Index->getType());
- Value *NewSub = Builder->CreateSub(PtrToInt, Index->getOperand(1));
- return CastInst::Create(Instruction::IntToPtr, NewSub, GEP.getType());
+ Type *PtrTy = GEP.getPointerOperandType();
+ Type *Ty = PtrTy->getPointerElementType();
+ uint64_t TyAllocSize = DL->getTypeAllocSize(Ty);
+
+ bool Matched = false;
+ uint64_t C;
+ Value *V = nullptr;
+ if (TyAllocSize == 1) {
+ V = GEP.getOperand(1);
+ Matched = true;
+ } else if (match(GEP.getOperand(1),
+ m_AShr(m_Value(V), m_ConstantInt(C)))) {
+ if (TyAllocSize == 1ULL << C)
+ Matched = true;
+ } else if (match(GEP.getOperand(1),
+ m_SDiv(m_Value(V), m_ConstantInt(C)))) {
+ if (TyAllocSize == C)
+ Matched = true;
+ }
+
+ if (Matched) {
+ // Canonicalize (gep i8* X, -(ptrtoint Y))
+ // to (inttoptr (sub (ptrtoint X), (ptrtoint Y)))
+ // The GEP pattern is emitted by the SCEV expander for certain kinds of
+ // pointer arithmetic.
+ if (match(V, m_Neg(m_PtrToInt(m_Value())))) {
+ Operator *Index = cast<Operator>(V);
+ Value *PtrToInt = Builder->CreatePtrToInt(PtrOp, Index->getType());
+ Value *NewSub = Builder->CreateSub(PtrToInt, Index->getOperand(1));
+ return CastInst::Create(Instruction::IntToPtr, NewSub, GEP.getType());
+ }
+ // Canonicalize (gep i8* X, (ptrtoint Y)-(ptrtoint X))
+ // to (bitcast Y)
+ Value *Y;
+ if (match(V, m_Sub(m_PtrToInt(m_Value(Y)),
+ m_PtrToInt(m_Specific(GEP.getOperand(0)))))) {
+ return CastInst::CreatePointerBitCastOrAddrSpaceCast(Y,
+ GEP.getType());
+ }
+ }
}
}
// We do not handle pointer-vector geps here.
if (!StrippedPtrTy)
- return 0;
+ return nullptr;
if (StrippedPtr != PtrOp) {
bool HasZeroPointerIndex = false;
GetElementPtrInst *Res =
GetElementPtrInst::Create(StrippedPtr, Idx, GEP.getName());
Res->setIsInBounds(GEP.isInBounds());
- return Res;
+ if (StrippedPtrTy->getAddressSpace() == GEP.getAddressSpace())
+ return Res;
+ // Insert Res, and create an addrspacecast.
+ // e.g.,
+ // GEP (addrspacecast i8 addrspace(1)* X to [0 x i8]*), i32 0, ...
+ // ->
+ // %0 = GEP i8 addrspace(1)* X, ...
+ // addrspacecast i8 addrspace(1)* %0 to i8*
+ return new AddrSpaceCastInst(Builder->Insert(Res), GEP.getType());
}
if (ArrayType *XATy =
// to an array of the same type as the destination pointer
// array. Because the array type is never stepped over (there
// is a leading zero) we can fold the cast into this GEP.
- GEP.setOperand(0, StrippedPtr);
- return &GEP;
+ if (StrippedPtrTy->getAddressSpace() == GEP.getAddressSpace()) {
+ GEP.setOperand(0, StrippedPtr);
+ return &GEP;
+ }
+ // Cannot replace the base pointer directly because StrippedPtr's
+ // address space is different. Instead, create a new GEP followed by
+ // an addrspacecast.
+ // e.g.,
+ // GEP (addrspacecast [10 x i8] addrspace(1)* X to [0 x i8]*),
+ // i32 0, ...
+ // ->
+ // %0 = GEP [10 x i8] addrspace(1)* X, ...
+ // addrspacecast i8 addrspace(1)* %0 to i8*
+ SmallVector<Value*, 8> Idx(GEP.idx_begin(), GEP.idx_end());
+ Value *NewGEP = GEP.isInBounds() ?
+ Builder->CreateInBoundsGEP(StrippedPtr, Idx, GEP.getName()) :
+ Builder->CreateGEP(StrippedPtr, Idx, GEP.getName());
+ return new AddrSpaceCastInst(NewGEP, GEP.getType());
}
}
}
Builder->CreateGEP(StrippedPtr, Idx, GEP.getName());
// V and GEP are both pointer types --> BitCast
- if (StrippedPtrTy->getAddressSpace() == GEP.getPointerAddressSpace())
- return new BitCastInst(NewGEP, GEP.getType());
- return new AddrSpaceCastInst(NewGEP, GEP.getType());
+ return CastInst::CreatePointerBitCastOrAddrSpaceCast(NewGEP,
+ GEP.getType());
}
// Transform things like:
Builder->CreateGEP(StrippedPtr, NewIdx, GEP.getName());
// The NewGEP must be pointer typed, so must the old one -> BitCast
- if (StrippedPtrTy->getAddressSpace() == GEP.getPointerAddressSpace())
- return new BitCastInst(NewGEP, GEP.getType());
- return new AddrSpaceCastInst(NewGEP, GEP.getType());
+ return CastInst::CreatePointerBitCastOrAddrSpaceCast(NewGEP,
+ GEP.getType());
}
}
}
Builder->CreateInBoundsGEP(StrippedPtr, Off, GEP.getName()) :
Builder->CreateGEP(StrippedPtr, Off, GEP.getName());
// The NewGEP must be pointer typed, so must the old one -> BitCast
- if (StrippedPtrTy->getAddressSpace() == GEP.getPointerAddressSpace())
- return new BitCastInst(NewGEP, GEP.getType());
- return new AddrSpaceCastInst(NewGEP, GEP.getType());
+ return CastInst::CreatePointerBitCastOrAddrSpaceCast(NewGEP,
+ GEP.getType());
}
}
}
}
if (!DL)
- return 0;
+ return nullptr;
+
+ // addrspacecast between types is canonicalized as a bitcast, then an
+ // addrspacecast. To take advantage of the below bitcast + struct GEP, look
+ // through the addrspacecast.
+ if (AddrSpaceCastInst *ASC = dyn_cast<AddrSpaceCastInst>(PtrOp)) {
+ // X = bitcast A addrspace(1)* to B addrspace(1)*
+ // Y = addrspacecast A addrspace(1)* to B addrspace(2)*
+ // Z = gep Y, <...constant indices...>
+ // Into an addrspacecasted GEP of the struct.
+ if (BitCastInst *BC = dyn_cast<BitCastInst>(ASC->getOperand(0)))
+ PtrOp = BC;
+ }
/// See if we can simplify:
/// X = bitcast A* to B*
if (BitCastInst *BCI = dyn_cast<BitCastInst>(PtrOp)) {
Value *Operand = BCI->getOperand(0);
PointerType *OpType = cast<PointerType>(Operand->getType());
- unsigned OffsetBits = DL->getPointerTypeSizeInBits(OpType);
+ unsigned OffsetBits = DL->getPointerTypeSizeInBits(GEP.getType());
APInt Offset(OffsetBits, 0);
if (!isa<BitCastInst>(Operand) &&
- GEP.accumulateConstantOffset(*DL, Offset) &&
- StrippedPtrTy->getAddressSpace() == GEP.getPointerAddressSpace()) {
+ GEP.accumulateConstantOffset(*DL, Offset)) {
// If this GEP instruction doesn't move the pointer, just replace the GEP
// with a bitcast of the real input to the dest type.
return &GEP;
}
}
+
+ if (Operand->getType()->getPointerAddressSpace() != GEP.getAddressSpace())
+ return new AddrSpaceCastInst(Operand, GEP.getType());
return new BitCastInst(Operand, GEP.getType());
}
if (NGEP->getType() == GEP.getType())
return ReplaceInstUsesWith(GEP, NGEP);
NGEP->takeName(&GEP);
+
+ if (NGEP->getType()->getPointerAddressSpace() != GEP.getAddressSpace())
+ return new AddrSpaceCastInst(NGEP, GEP.getType());
return new BitCastInst(NGEP, GEP.getType());
}
}
}
- return 0;
+ return nullptr;
}
static bool
}
return EraseInstFromFunction(MI);
}
- return 0;
+ return nullptr;
}
/// \brief Move the call to free before a NULL test.
// would duplicate the call to free in each predecessor and it may
// not be profitable even for code size.
if (!PredBB)
- return 0;
+ return nullptr;
// Validate constraint #2: Does this block contains only the call to
// free and an unconditional branch?
// FIXME: We could check if we can speculate everything in the
// predecessor block
if (FreeInstrBB->size() != 2)
- return 0;
+ return nullptr;
BasicBlock *SuccBB;
if (!match(FreeInstrBB->getTerminator(), m_UnconditionalBr(SuccBB)))
- return 0;
+ return nullptr;
// Validate the rest of constraint #1 by matching on the pred branch.
TerminatorInst *TI = PredBB->getTerminator();
BasicBlock *TrueBB, *FalseBB;
ICmpInst::Predicate Pred;
if (!match(TI, m_Br(m_ICmp(Pred, m_Specific(Op), m_Zero()), TrueBB, FalseBB)))
- return 0;
+ return nullptr;
if (Pred != ICmpInst::ICMP_EQ && Pred != ICmpInst::ICMP_NE)
- return 0;
+ return nullptr;
// Validate constraint #3: Ensure the null case just falls through.
if (SuccBB != (Pred == ICmpInst::ICMP_EQ ? TrueBB : FalseBB))
- return 0;
+ return nullptr;
assert(FreeInstrBB == (Pred == ICmpInst::ICMP_EQ ? FalseBB : TrueBB) &&
"Broken CFG: missing edge from predecessor to successor");
if (Instruction *I = tryToMoveFreeBeforeNullTest(FI))
return I;
- return 0;
+ return nullptr;
}
+Instruction *InstCombiner::visitReturnInst(ReturnInst &RI) {
+ if (RI.getNumOperands() == 0) // ret void
+ return nullptr;
+
+ Value *ResultOp = RI.getOperand(0);
+ Type *VTy = ResultOp->getType();
+ if (!VTy->isIntegerTy())
+ return nullptr;
+
+ // There might be assume intrinsics dominating this return that completely
+ // determine the value. If so, constant fold it.
+ unsigned BitWidth = VTy->getPrimitiveSizeInBits();
+ APInt KnownZero(BitWidth, 0), KnownOne(BitWidth, 0);
+ computeKnownBits(ResultOp, KnownZero, KnownOne, 0, &RI);
+ if ((KnownZero|KnownOne).isAllOnesValue())
+ RI.setOperand(0, Constant::getIntegerValue(VTy, KnownOne));
+ return nullptr;
+}
Instruction *InstCombiner::visitBranchInst(BranchInst &BI) {
// Change br (not X), label True, label False to: br X, label False, True
- Value *X = 0;
+ Value *X = nullptr;
BasicBlock *TrueDest;
BasicBlock *FalseDest;
if (match(&BI, m_Br(m_Not(m_Value(X)), TrueDest, FalseDest)) &&
return &BI;
}
- return 0;
+ return nullptr;
}
Instruction *InstCombiner::visitSwitchInst(SwitchInst &SI) {
Value *Cond = SI.getCondition();
+ unsigned BitWidth = cast<IntegerType>(Cond->getType())->getBitWidth();
+ APInt KnownZero(BitWidth, 0), KnownOne(BitWidth, 0);
+ computeKnownBits(Cond, KnownZero, KnownOne);
+ unsigned LeadingKnownZeros = KnownZero.countLeadingOnes();
+ unsigned LeadingKnownOnes = KnownOne.countLeadingOnes();
+
+ // Compute the number of leading bits we can ignore.
+ for (auto &C : SI.cases()) {
+ LeadingKnownZeros = std::min(
+ LeadingKnownZeros, C.getCaseValue()->getValue().countLeadingZeros());
+ LeadingKnownOnes = std::min(
+ LeadingKnownOnes, C.getCaseValue()->getValue().countLeadingOnes());
+ }
+
+ unsigned NewWidth = BitWidth - std::max(LeadingKnownZeros, LeadingKnownOnes);
+
+ // Truncate the condition operand if the new type is equal to or larger than
+ // the largest legal integer type. We need to be conservative here since
+ // x86 generates redundant zero-extenstion instructions if the operand is
+ // truncated to i8 or i16.
+ bool TruncCond = false;
+ if (DL && BitWidth > NewWidth &&
+ NewWidth >= DL->getLargestLegalIntTypeSize()) {
+ TruncCond = true;
+ IntegerType *Ty = IntegerType::get(SI.getContext(), NewWidth);
+ Builder->SetInsertPoint(&SI);
+ Value *NewCond = Builder->CreateTrunc(SI.getCondition(), Ty, "trunc");
+ SI.setCondition(NewCond);
+
+ for (auto &C : SI.cases())
+ static_cast<SwitchInst::CaseIt *>(&C)->setValue(ConstantInt::get(
+ SI.getContext(), C.getCaseValue()->getValue().trunc(NewWidth)));
+ }
+
if (Instruction *I = dyn_cast<Instruction>(Cond)) {
if (I->getOpcode() == Instruction::Add)
if (ConstantInt *AddRHS = dyn_cast<ConstantInt>(I->getOperand(1))) {
for (SwitchInst::CaseIt i = SI.case_begin(), e = SI.case_end();
i != e; ++i) {
ConstantInt* CaseVal = i.getCaseValue();
- Constant* NewCaseVal = ConstantExpr::getSub(cast<Constant>(CaseVal),
- AddRHS);
+ Constant *LHS = CaseVal;
+ if (TruncCond)
+ LHS = LeadingKnownZeros
+ ? ConstantExpr::getZExt(CaseVal, Cond->getType())
+ : ConstantExpr::getSExt(CaseVal, Cond->getType());
+ Constant* NewCaseVal = ConstantExpr::getSub(LHS, AddRHS);
assert(isa<ConstantInt>(NewCaseVal) &&
"Result of expression should be constant");
i.setValue(cast<ConstantInt>(NewCaseVal));
return &SI;
}
}
- return 0;
+
+ return TruncCond ? &SI : nullptr;
}
Instruction *InstCombiner::visitExtractValueInst(ExtractValueInst &EV) {
// first index
return ExtractValueInst::Create(C2, EV.getIndices().slice(1));
}
- return 0; // Can't handle other constants
+ return nullptr; // Can't handle other constants
}
if (InsertValueInst *IV = dyn_cast<InsertValueInst>(Agg)) {
// and if again single-use then via load (gep (gep)) to load (gep).
// However, double extracts from e.g. function arguments or return values
// aren't handled yet.
- return 0;
+ return nullptr;
}
enum Personality_Type {
// Simplify the list of clauses, eg by removing repeated catch clauses
// (these are often created by inlining).
bool MakeNewInstruction = false; // If true, recreate using the following:
- SmallVector<Value *, 16> NewClauses; // - Clauses for the new instruction;
+ SmallVector<Constant *, 16> NewClauses; // - Clauses for the new instruction;
bool CleanupFlag = LI.isCleanup(); // - The new instruction is a cleanup.
SmallPtrSet<Value *, 16> AlreadyCaught; // Typeinfos known caught already.
bool isLastClause = i + 1 == e;
if (LI.isCatch(i)) {
// A catch clause.
- Value *CatchClause = LI.getClause(i);
- Constant *TypeInfo = cast<Constant>(CatchClause->stripPointerCasts());
+ Constant *CatchClause = LI.getClause(i);
+ Constant *TypeInfo = CatchClause->stripPointerCasts();
// If we already saw this clause, there is no point in having a second
// copy of it.
- if (AlreadyCaught.insert(TypeInfo)) {
+ if (AlreadyCaught.insert(TypeInfo).second) {
// This catch clause was not already seen.
NewClauses.push_back(CatchClause);
} else {
// equal (for example if one represents a C++ class, and the other some
// class derived from it).
assert(LI.isFilter(i) && "Unsupported landingpad clause!");
- Value *FilterClause = LI.getClause(i);
+ Constant *FilterClause = LI.getClause(i);
ArrayType *FilterType = cast<ArrayType>(FilterClause->getType());
unsigned NumTypeInfos = FilterType->getNumElements();
// catch-alls. If so, the filter can be discarded.
bool SawCatchAll = false;
for (unsigned j = 0; j != NumTypeInfos; ++j) {
- Value *Elt = Filter->getOperand(j);
- Constant *TypeInfo = cast<Constant>(Elt->stripPointerCasts());
+ Constant *Elt = Filter->getOperand(j);
+ Constant *TypeInfo = Elt->stripPointerCasts();
if (isCatchAll(Personality, TypeInfo)) {
// This element is a catch-all. Bail out, noting this fact.
SawCatchAll = true;
continue;
// There is no point in having multiple copies of the same typeinfo in
// a filter, so only add it if we didn't already.
- if (SeenInFilter.insert(TypeInfo))
+ if (SeenInFilter.insert(TypeInfo).second)
NewFilterElts.push_back(cast<Constant>(Elt));
}
// A filter containing a catch-all cannot match anything by definition.
continue;
// If Filter is a subset of LFilter, i.e. every element of Filter is also
// an element of LFilter, then discard LFilter.
- SmallVectorImpl<Value *>::iterator J = NewClauses.begin() + j;
+ SmallVectorImpl<Constant *>::iterator J = NewClauses.begin() + j;
// If Filter is empty then it is a subset of LFilter.
if (!FElts) {
// Discard LFilter.
return &LI;
}
- return 0;
+ return nullptr;
}
/// whose condition is a known constant, we only visit the reachable successors.
///
static bool AddReachableCodeToWorklist(BasicBlock *BB,
- SmallPtrSet<BasicBlock*, 64> &Visited,
+ SmallPtrSetImpl<BasicBlock*> &Visited,
InstCombiner &IC,
const DataLayout *DL,
const TargetLibraryInfo *TLI) {
BB = Worklist.pop_back_val();
// We have now visited this block! If we've already been here, ignore it.
- if (!Visited.insert(BB)) continue;
+ if (!Visited.insert(BB).second)
+ continue;
for (BasicBlock::iterator BBI = BB->begin(), E = BB->end(); BBI != E; ) {
Instruction *Inst = BBI++;
for (User::op_iterator i = Inst->op_begin(), e = Inst->op_end();
i != e; ++i) {
ConstantExpr *CE = dyn_cast<ConstantExpr>(i);
- if (CE == 0) continue;
+ if (CE == nullptr) continue;
Constant*& FoldRes = FoldedConstants[CE];
if (!FoldRes)
while (!Worklist.isEmpty()) {
Instruction *I = Worklist.RemoveOne();
- if (I == 0) continue; // skip null values.
+ if (I == nullptr) continue; // skip null values.
// Check to see if we can DCE the instruction.
if (isInstructionTriviallyDead(I, TLI)) {
// If the user is one of our immediate successors, and if that successor
// only has us as a predecessors (we'd have to split the critical edge
// otherwise), we can keep going.
- if (UserIsSuccessor && UserParent->getSinglePredecessor())
+ if (UserIsSuccessor && UserParent->getSinglePredecessor()) {
// Okay, the CFG is simple enough, try to sink this instruction.
- MadeIRChange |= TryToSinkInstruction(I, UserParent);
+ if (TryToSinkInstruction(I, UserParent)) {
+ MadeIRChange = true;
+ // We'll add uses of the sunk instruction below, but since sinking
+ // can expose opportunities for it's *operands* add them to the
+ // worklist
+ for (Use &U : I->operands())
+ if (Instruction *OpI = dyn_cast<Instruction>(U.get()))
+ Worklist.Add(OpI);
+ }
+ }
}
}
return MadeIRChange;
}
-namespace {
-class InstCombinerLibCallSimplifier : public LibCallSimplifier {
- InstCombiner *IC;
-public:
- InstCombinerLibCallSimplifier(const DataLayout *DL,
- const TargetLibraryInfo *TLI,
- InstCombiner *IC)
- : LibCallSimplifier(DL, TLI, UnsafeFPShrink) {
- this->IC = IC;
- }
+// FIXME: Passing all of the analyses here in the run method is ugly. We should
+// separate out the worklist from the combiner so that we can construct
+// a combiner once per function while re-using the storage of an external
+// worklist.
+bool InstCombiner::run(Function &F, AssumptionCache *AC, const DataLayout *DL,
+ TargetLibraryInfo *TLI, DominatorTree *DT,
+ LoopInfo *LI) {
+ // Set up our analysis pointers.
+ this->AC = AC;
+ this->DL = DL;
+ this->TLI = TLI;
+ this->DT = DT;
+ this->LI = LI;
- /// replaceAllUsesWith - override so that instruction replacement
- /// can be defined in terms of the instruction combiner framework.
- void replaceAllUsesWith(Instruction *I, Value *With) const override {
- IC->ReplaceInstUsesWith(*I, With);
- }
-};
-}
-
-bool InstCombiner::runOnFunction(Function &F) {
- if (skipOptnoneFunction(F))
- return false;
-
- DataLayoutPass *DLP = getAnalysisIfAvailable<DataLayoutPass>();
- DL = DLP ? &DLP->getDataLayout() : 0;
- TLI = &getAnalysis<TargetLibraryInfo>();
// Minimizing size?
MinimizeSize = F.getAttributes().hasAttribute(AttributeSet::FunctionIndex,
Attribute::MinSize);
/// Builder - This is an IRBuilder that automatically inserts new
/// instructions into the worklist when they are created.
- IRBuilder<true, TargetFolder, InstCombineIRInserter>
- TheBuilder(F.getContext(), TargetFolder(DL),
- InstCombineIRInserter(Worklist));
+ IRBuilder<true, TargetFolder, InstCombineIRInserter> TheBuilder(
+ F.getContext(), TargetFolder(DL), InstCombineIRInserter(Worklist, AC));
Builder = &TheBuilder;
- InstCombinerLibCallSimplifier TheSimplifier(DL, TLI, this);
+ auto InstCombineRAUW = [this](Instruction *From, Value *With) {
+ ReplaceInstUsesWith(*From, With);
+ };
+ LibCallSimplifier TheSimplifier(DL, TLI, InstCombineRAUW);
Simplifier = &TheSimplifier;
bool EverMadeChange = false;
while (DoOneIteration(F, Iteration++))
EverMadeChange = true;
- Builder = 0;
+ Builder = nullptr;
return EverMadeChange;
}
+namespace {
+/// \brief The legacy pass manager's instcombine pass.
+///
+/// This is a basic whole-function wrapper around the instcombine utility. It
+/// will try to combine all instructions in the function.
+class InstructionCombiningPass : public FunctionPass {
+ InstCombiner IC;
+
+public:
+ static char ID; // Pass identification, replacement for typeid
+
+ InstructionCombiningPass() : FunctionPass(ID) {
+ initializeInstructionCombiningPassPass(*PassRegistry::getPassRegistry());
+ }
+
+ void getAnalysisUsage(AnalysisUsage &AU) const override;
+ bool runOnFunction(Function &F) override;
+};
+}
+
+void InstructionCombiningPass::getAnalysisUsage(AnalysisUsage &AU) const {
+ AU.setPreservesCFG();
+ AU.addRequired<AssumptionCacheTracker>();
+ AU.addRequired<TargetLibraryInfoWrapperPass>();
+ AU.addRequired<DominatorTreeWrapperPass>();
+ AU.addPreserved<DominatorTreeWrapperPass>();
+}
+
+bool InstructionCombiningPass::runOnFunction(Function &F) {
+ if (skipOptnoneFunction(F))
+ return false;
+
+ auto &AC = getAnalysis<AssumptionCacheTracker>().getAssumptionCache(F);
+ auto *DLP = getAnalysisIfAvailable<DataLayoutPass>();
+ auto *DL = DLP ? &DLP->getDataLayout() : nullptr;
+ auto &TLI = getAnalysis<TargetLibraryInfoWrapperPass>().getTLI();
+ auto &DT = getAnalysis<DominatorTreeWrapperPass>().getDomTree();
+ auto *LIWP = getAnalysisIfAvailable<LoopInfoWrapperPass>();
+ auto *LI = LIWP ? &LIWP->getLoopInfo() : nullptr;
+
+ return IC.run(F, &AC, DL, &TLI, &DT, LI);
+}
+
+char InstructionCombiningPass::ID = 0;
+INITIALIZE_PASS_BEGIN(InstructionCombiningPass, "instcombine",
+ "Combine redundant instructions", false, false)
+INITIALIZE_PASS_DEPENDENCY(AssumptionCacheTracker)
+INITIALIZE_PASS_DEPENDENCY(TargetLibraryInfoWrapperPass)
+INITIALIZE_PASS_DEPENDENCY(DominatorTreeWrapperPass)
+INITIALIZE_PASS_END(InstructionCombiningPass, "instcombine",
+ "Combine redundant instructions", false, false)
+
+// Initialization Routines
+void llvm::initializeInstCombine(PassRegistry &Registry) {
+ initializeInstructionCombiningPassPass(Registry);
+}
+
+void LLVMInitializeInstCombine(LLVMPassRegistryRef R) {
+ initializeInstructionCombiningPassPass(*unwrap(R));
+}
+
FunctionPass *llvm::createInstructionCombiningPass() {
- return new InstCombiner();
+ return new InstructionCombiningPass();
}