index 6c01826a064109cc53c33a95ad8ee071d2f4ddba..37772277b5888645aa86de667ee82b8456400179 100644 (file)
/// Hidden option to force the pass to not use DomTree and mem2reg, instead
/// forming SSA values through the SSAUpdater infrastructure.
-static cl::opt<bool>
-ForceSSAUpdater("force-ssa-updater", cl::init(false), cl::Hidden);
+static cl::opt<bool> ForceSSAUpdater("force-ssa-updater", cl::init(false),
+ cl::Hidden);
/// Hidden option to enable randomly shuffling the slices to help uncover
/// instability in their order.
/// Hidden option to experiment with completely strict handling of inbounds
/// GEPs.
-static cl::opt<bool> SROAStrictInbounds("sroa-strict-inbounds",
- cl::init(false), cl::Hidden);
+static cl::opt<bool> SROAStrictInbounds("sroa-strict-inbounds", cl::init(false),
+ cl::Hidden);
namespace {
/// \brief A custom IRBuilder inserter which prefixes all names if they are
/// preserved.
template <bool preserveNames = true>
-class IRBuilderPrefixedInserter :
- public IRBuilderDefaultInserter<preserveNames> {
+class IRBuilderPrefixedInserter
+ : public IRBuilderDefaultInserter<preserveNames> {
std::string Prefix;
public:
// Specialization for not preserving the name is trivial.
template <>
-class IRBuilderPrefixedInserter<false> :
- public IRBuilderDefaultInserter<false> {
+class IRBuilderPrefixedInserter<false>
+ : public IRBuilderDefaultInserter<false> {
public:
void SetNamePrefix(const Twine &P) {}
};
/// \brief Provide a typedef for IRBuilder that drops names in release builds.
#ifndef NDEBUG
-typedef llvm::IRBuilder<true, ConstantFolder,
- IRBuilderPrefixedInserter<true> > IRBuilderTy;
+typedef llvm::IRBuilder<true, ConstantFolder, IRBuilderPrefixedInserter<true>>
+ IRBuilderTy;
#else
-typedef llvm::IRBuilder<false, ConstantFolder,
- IRBuilderPrefixedInserter<false> > IRBuilderTy;
+typedef llvm::IRBuilder<false, ConstantFolder, IRBuilderPrefixedInserter<false>>
+ IRBuilderTy;
#endif
}
/// decreasing. Thus the spanning range comes first in a cluster with the
/// same start position.
bool operator<(const Slice &RHS) const {
- if (beginOffset() < RHS.beginOffset()) return true;
- if (beginOffset() > RHS.beginOffset()) return false;
- if (isSplittable() != RHS.isSplittable()) return !isSplittable();
- if (endOffset() > RHS.endOffset()) return true;
+ if (beginOffset() < RHS.beginOffset())
+ return true;
+ if (beginOffset() > RHS.beginOffset())
+ return false;
+ if (isSplittable() != RHS.isSplittable())
+ return !isSplittable();
+ if (endOffset() > RHS.endOffset())
+ return true;
return false;
}
namespace llvm {
template <typename T> struct isPodLike;
-template <> struct isPodLike<Slice> {
- static const bool value = true;
-};
+template <> struct isPodLike<Slice> { static const bool value = true; };
}
namespace {
/// \brief Support for iterating over the slices.
/// @{
typedef SmallVectorImpl<Slice>::iterator iterator;
+ typedef iterator_range<iterator> range;
iterator begin() { return Slices.begin(); }
iterator end() { return Slices.end(); }
typedef SmallVectorImpl<Slice>::const_iterator const_iterator;
+ typedef iterator_range<const_iterator> const_range;
const_iterator begin() const { return Slices.begin(); }
const_iterator end() const { return Slices.end(); }
/// @}
- /// \brief Allow iterating the dead users for this alloca.
- ///
- /// These are instructions which will never actually use the alloca as they
- /// are outside the allocated range. They are safe to replace with undef and
- /// delete.
- /// @{
- typedef SmallVectorImpl<Instruction *>::const_iterator dead_user_iterator;
- dead_user_iterator dead_user_begin() const { return DeadUsers.begin(); }
- dead_user_iterator dead_user_end() const { return DeadUsers.end(); }
- /// @}
+ /// \brief Access the dead users for this alloca.
+ ArrayRef<Instruction *> getDeadUsers() const { return DeadUsers; }
- /// \brief Allow iterating the dead expressions referring to this alloca.
+ /// \brief Access the dead operands referring to this alloca.
///
/// These are operands which have cannot actually be used to refer to the
/// alloca as they are outside its range and the user doesn't correct for
/// that. These mostly consist of PHI node inputs and the like which we just
/// need to replace with undef.
- /// @{
- typedef SmallVectorImpl<Use *>::const_iterator dead_op_iterator;
- dead_op_iterator dead_op_begin() const { return DeadOperands.begin(); }
- dead_op_iterator dead_op_end() const { return DeadOperands.end(); }
- /// @}
+ ArrayRef<Use *> getDeadOperands() const { return DeadOperands; }
#if !defined(NDEBUG) || defined(LLVM_ENABLE_DUMP)
void print(raw_ostream &OS, const_iterator I, StringRef Indent = " ") const;
// being selected between, fold the select. Yes this does (rarely) happen
// early on.
if (ConstantInt *CI = dyn_cast<ConstantInt>(SI.getCondition()))
- return SI.getOperand(1+CI->isZero());
+ return SI.getOperand(1 + CI->isZero());
if (SI.getOperand(1) == SI.getOperand(2))
return SI.getOperand(1);
typedef PtrUseVisitor<SliceBuilder> Base;
const uint64_t AllocSize;
- AllocaSlices &S;
+ AllocaSlices &AS;
SmallDenseMap<Instruction *, unsigned> MemTransferSliceMap;
SmallDenseMap<Instruction *, uint64_t> PHIOrSelectSizes;
SmallPtrSet<Instruction *, 4> VisitedDeadInsts;
public:
- SliceBuilder(const DataLayout &DL, AllocaInst &AI, AllocaSlices &S)
+ SliceBuilder(const DataLayout &DL, AllocaInst &AI, AllocaSlices &AS)
: PtrUseVisitor<SliceBuilder>(DL),
- AllocSize(DL.getTypeAllocSize(AI.getAllocatedType())), S(S) {}
+ AllocSize(DL.getTypeAllocSize(AI.getAllocatedType())), AS(AS) {}
private:
void markAsDead(Instruction &I) {
- if (VisitedDeadInsts.insert(&I))
- S.DeadUsers.push_back(&I);
+ if (VisitedDeadInsts.insert(&I).second)
+ AS.DeadUsers.push_back(&I);
}
void insertUse(Instruction &I, const APInt &Offset, uint64_t Size,
DEBUG(dbgs() << "WARNING: Ignoring " << Size << " byte use @" << Offset
<< " which has zero size or starts outside of the "
<< AllocSize << " byte alloca:\n"
- << " alloca: " << S.AI << "\n"
+ << " alloca: " << AS.AI << "\n"
<< " use: " << I << "\n");
return markAsDead(I);
}
if (Size > AllocSize - BeginOffset) {
DEBUG(dbgs() << "WARNING: Clamping a " << Size << " byte use @" << Offset
<< " to remain within the " << AllocSize << " byte alloca:\n"
- << " alloca: " << S.AI << "\n"
+ << " alloca: " << AS.AI << "\n"
<< " use: " << I << "\n");
EndOffset = AllocSize;
}
- S.Slices.push_back(Slice(BeginOffset, EndOffset, U, IsSplittable));
+ AS.Slices.push_back(Slice(BeginOffset, EndOffset, U, IsSplittable));
}
void visitBitCastInst(BitCastInst &BC) {
GEPOffset +=
APInt(Offset.getBitWidth(), SL->getElementOffset(ElementIdx));
} else {
- // For array or vector indices, scale the index by the size of the type.
+ // For array or vector indices, scale the index by the size of the
+ // type.
APInt Index = OpC->getValue().sextOrTrunc(Offset.getBitWidth());
GEPOffset += Index * APInt(Offset.getBitWidth(),
DL.getTypeAllocSize(GTI.getIndexedType()));
DEBUG(dbgs() << "WARNING: Ignoring " << Size << " byte store @" << Offset
<< " which extends past the end of the " << AllocSize
<< " byte alloca:\n"
- << " alloca: " << S.AI << "\n"
+ << " alloca: " << AS.AI << "\n"
<< " use: " << SI << "\n");
return markAsDead(SI);
}
handleLoadOrStore(ValOp->getType(), SI, Offset, Size, SI.isVolatile());
}
-
void visitMemSetInst(MemSetInst &II) {
assert(II.getRawDest() == *U && "Pointer use is not the destination?");
ConstantInt *Length = dyn_cast<ConstantInt>(II.getLength());
if (!IsOffsetKnown)
return PI.setAborted(&II);
- insertUse(II, Offset,
- Length ? Length->getLimitedValue()
- : AllocSize - Offset.getLimitedValue(),
+ insertUse(II, Offset, Length ? Length->getLimitedValue()
+ : AllocSize - Offset.getLimitedValue(),
(bool)Length);
}
// FIXME: Yet another place we really should bypass this when
// instrumenting for ASan.
if (Offset.uge(AllocSize)) {
- SmallDenseMap<Instruction *, unsigned>::iterator MTPI = MemTransferSliceMap.find(&II);
+ SmallDenseMap<Instruction *, unsigned>::iterator MTPI =
+ MemTransferSliceMap.find(&II);
if (MTPI != MemTransferSliceMap.end())
- S.Slices[MTPI->second].kill();
+ AS.Slices[MTPI->second].kill();
return markAsDead(II);
}
uint64_t RawOffset = Offset.getLimitedValue();
- uint64_t Size = Length ? Length->getLimitedValue()
- : AllocSize - RawOffset;
+ uint64_t Size = Length ? Length->getLimitedValue() : AllocSize - RawOffset;
// Check for the special case where the same exact value is used for both
// source and dest.
bool Inserted;
SmallDenseMap<Instruction *, unsigned>::iterator MTPI;
std::tie(MTPI, Inserted) =
- MemTransferSliceMap.insert(std::make_pair(&II, S.Slices.size()));
+ MemTransferSliceMap.insert(std::make_pair(&II, AS.Slices.size()));
unsigned PrevIdx = MTPI->second;
if (!Inserted) {
- Slice &PrevP = S.Slices[PrevIdx];
+ Slice &PrevP = AS.Slices[PrevIdx];
// Check if the begin offsets match and this is a non-volatile transfer.
// In that case, we can completely elide the transfer.
insertUse(II, Offset, Size, /*IsSplittable=*/Inserted && Length);
// Check that we ended up with a valid index in the map.
- assert(S.Slices[PrevIdx].getUse()->getUser() == &II &&
+ assert(AS.Slices[PrevIdx].getUse()->getUser() == &II &&
"Map index doesn't point back to a slice with this user.");
}
}
for (User *U : I->users())
- if (Visited.insert(cast<Instruction>(U)))
+ if (Visited.insert(cast<Instruction>(U)).second)
Uses.push_back(std::make_pair(I, cast<Instruction>(U)));
} while (!Uses.empty());
else
// Otherwise the operand to the PHI/select is dead, and we can replace
// it with undef.
- S.DeadOperands.push_back(U);
+ AS.DeadOperands.push_back(U);
return;
}
// FIXME: This should instead be escaped in the event we're instrumenting
// for address sanitization.
if (Offset.uge(AllocSize)) {
- S.DeadOperands.push_back(U);
+ AS.DeadOperands.push_back(U);
return;
}
insertUse(I, Offset, Size);
}
- void visitPHINode(PHINode &PN) {
- visitPHINodeOrSelectInst(PN);
- }
+ void visitPHINode(PHINode &PN) { visitPHINodeOrSelectInst(PN); }
- void visitSelectInst(SelectInst &SI) {
- visitPHINodeOrSelectInst(SI);
- }
+ void visitSelectInst(SelectInst &SI) { visitPHINodeOrSelectInst(SI); }
/// \brief Disable SROA entirely if there are unhandled users of the alloca.
- void visitInstruction(Instruction &I) {
- PI.setAborted(&I);
- }
+ void visitInstruction(Instruction &I) { PI.setAborted(&I); }
};
AllocaSlices::AllocaSlices(const DataLayout &DL, AllocaInst &AI)
}
Slices.erase(std::remove_if(Slices.begin(), Slices.end(),
- std::mem_fun_ref(&Slice::isDead)),
+ [](const Slice &S) {
+ return S.isDead();
+ }),
Slices.end());
#if __cplusplus >= 201103L && !defined(NDEBUG)
AllocaInst &AI, DIBuilder &DIB)
: LoadAndStorePromoter(Insts, S), AI(AI), DIB(DIB) {}
- void run(const SmallVectorImpl<Instruction*> &Insts) {
+ void run(const SmallVectorImpl<Instruction *> &Insts) {
// Retain the debug information attached to the alloca for use when
// rewriting loads and stores.
- if (MDNode *DebugNode = MDNode::getIfExists(AI.getContext(), &AI)) {
- for (User *U : DebugNode->users())
- if (DbgDeclareInst *DDI = dyn_cast<DbgDeclareInst>(U))
- DDIs.push_back(DDI);
- else if (DbgValueInst *DVI = dyn_cast<DbgValueInst>(U))
- DVIs.push_back(DVI);
+ if (auto *L = LocalAsMetadata::getIfExists(&AI)) {
+ if (auto *DebugNode = MetadataAsValue::getIfExists(AI.getContext(), L)) {
+ for (User *U : DebugNode->users())
+ if (DbgDeclareInst *DDI = dyn_cast<DbgDeclareInst>(U))
+ DDIs.push_back(DDI);
+ else if (DbgValueInst *DVI = dyn_cast<DbgValueInst>(U))
+ DVIs.push_back(DVI);
+ }
}
LoadAndStorePromoter::run(Insts);
DVIs.pop_back_val()->eraseFromParent();
}
- bool isInstInList(Instruction *I,
- const SmallVectorImpl<Instruction*> &Insts) const override {
+ bool
+ isInstInList(Instruction *I,
+ const SmallVectorImpl<Instruction *> &Insts) const override {
Value *Ptr;
if (LoadInst *LI = dyn_cast<LoadInst>(I))
Ptr = LI->getOperand(0);
else
return false;
- } while (Visited.insert(Ptr));
+ } while (Visited.insert(Ptr).second);
return false;
}
void updateDebugInfo(Instruction *Inst) const override {
- for (SmallVectorImpl<DbgDeclareInst *>::const_iterator I = DDIs.begin(),
- E = DDIs.end(); I != E; ++I) {
- DbgDeclareInst *DDI = *I;
+ for (DbgDeclareInst *DDI : DDIs)
if (StoreInst *SI = dyn_cast<StoreInst>(Inst))
ConvertDebugDeclareToDebugValue(DDI, SI, DIB);
else if (LoadInst *LI = dyn_cast<LoadInst>(Inst))
ConvertDebugDeclareToDebugValue(DDI, LI, DIB);
- }
- for (SmallVectorImpl<DbgValueInst *>::const_iterator I = DVIs.begin(),
- E = DVIs.end(); I != E; ++I) {
- DbgValueInst *DVI = *I;
+ for (DbgValueInst *DVI : DVIs) {
Value *Arg = nullptr;
if (StoreInst *SI = dyn_cast<StoreInst>(Inst)) {
// If an argument is zero extended then use argument directly. The ZExt
};
} // end anon namespace
-
namespace {
/// \brief An optimization pass providing Scalar Replacement of Aggregates.
///
/// directly promoted. Finally, each time we rewrite a use of an alloca other
/// the one being actively rewritten, we add it back onto the list if not
/// already present to ensure it is re-visited.
- SetVector<AllocaInst *, SmallVector<AllocaInst *, 16> > Worklist;
+ SetVector<AllocaInst *, SmallVector<AllocaInst *, 16>> Worklist;
/// \brief A collection of instructions to delete.
/// We try to batch deletions to simplify code and make things a bit more
/// efficient.
- SetVector<Instruction *, SmallVector<Instruction *, 8> > DeadInsts;
+ SetVector<Instruction *, SmallVector<Instruction *, 8>> DeadInsts;
/// \brief Post-promotion worklist.
///
///
/// Note that we have to be very careful to clear allocas out of this list in
/// the event they are deleted.
- SetVector<AllocaInst *, SmallVector<AllocaInst *, 16> > PostPromotionWorklist;
+ SetVector<AllocaInst *, SmallVector<AllocaInst *, 16>> PostPromotionWorklist;
/// \brief A collection of alloca instructions we can directly promote.
std::vector<AllocaInst *> PromotableAllocas;
/// All of these PHIs have been checked for the safety of speculation and by
/// being speculated will allow promoting allocas currently in the promotable
/// queue.
- SetVector<PHINode *, SmallVector<PHINode *, 2> > SpeculatablePHIs;
+ SetVector<PHINode *, SmallVector<PHINode *, 2>> SpeculatablePHIs;
/// \brief A worklist of select instructions to speculate prior to promoting
/// allocas.
/// All of these select instructions have been checked for the safety of
/// speculation and by being speculated will allow promoting allocas
/// currently in the promotable queue.
- SetVector<SelectInst *, SmallVector<SelectInst *, 2> > SpeculatableSelects;
+ SetVector<SelectInst *, SmallVector<SelectInst *, 2>> SpeculatableSelects;
+
+ /// Debug intrinsics do not show up as regular uses in the
+ /// IR. This side-table holds the missing use edges.
+ DenseMap<AllocaInst *, DbgDeclareInst *> DbgDeclares;
public:
SROA(bool RequiresDomTree = true)
- : FunctionPass(ID), RequiresDomTree(RequiresDomTree),
- C(nullptr), DL(nullptr), DT(nullptr) {
+ : FunctionPass(ID), RequiresDomTree(RequiresDomTree), C(nullptr),
+ DL(nullptr), DT(nullptr) {
initializeSROAPass(*PassRegistry::getPassRegistry());
}
bool runOnFunction(Function &F) override;
friend class PHIOrSelectSpeculator;
friend class AllocaSliceRewriter;
- bool rewritePartition(AllocaInst &AI, AllocaSlices &S,
+ bool rewritePartition(AllocaInst &AI, AllocaSlices &AS,
AllocaSlices::iterator B, AllocaSlices::iterator E,
int64_t BeginOffset, int64_t EndOffset,
ArrayRef<AllocaSlices::iterator> SplitUses);
- bool splitAlloca(AllocaInst &AI, AllocaSlices &S);
+ bool splitAlloca(AllocaInst &AI, AllocaSlices &AS);
bool runOnAlloca(AllocaInst &AI);
void clobberUse(Use &U);
void deleteDeadInstructions(SmallPtrSetImpl<AllocaInst *> &DeletedAllocas);
return new SROA(RequiresDomTree);
}
-INITIALIZE_PASS_BEGIN(SROA, "sroa", "Scalar Replacement Of Aggregates",
- false, false)
+INITIALIZE_PASS_BEGIN(SROA, "sroa", "Scalar Replacement Of Aggregates", false,
+ false)
INITIALIZE_PASS_DEPENDENCY(AssumptionTracker)
INITIALIZE_PASS_DEPENDENCY(DominatorTreeWrapperPass)
-INITIALIZE_PASS_END(SROA, "sroa", "Scalar Replacement Of Aggregates",
- false, false)
+INITIALIZE_PASS_END(SROA, "sroa", "Scalar Replacement Of Aggregates", false,
+ false)
/// Walk the range of a partitioning looking for a common type to cover this
/// sequence of slices.
///
/// FIXME: This should be hoisted into a generic utility, likely in
/// Transforms/Util/Local.h
-static bool isSafePHIToSpeculate(PHINode &PN,
- const DataLayout *DL = nullptr) {
+static bool isSafePHIToSpeculate(PHINode &PN, const DataLayout *DL = nullptr) {
// For now, we can only do this promotion if the load is in the same block
// as the PHI, and if there are no stores between the phi and load.
// TODO: Allow recursive phi users.
@@ -1340,7 +1327,8 @@ static Value *getNaturalGEPRecursively(IRBuilderTy &IRB, const DataLayout &DL,
SmallVectorImpl<Value *> &Indices,
Twine NamePrefix) {
if (Offset == 0)
- return getNaturalGEPWithType(IRB, DL, Ptr, Ty, TargetTy, Indices, NamePrefix);
+ return getNaturalGEPWithType(IRB, DL, Ptr, Ty, TargetTy, Indices,
+ NamePrefix);
// We can't recurse through pointer types.
if (Ty->isPointerTy())
/// a single GEP as possible, thus making each GEP more independent of the
/// surrounding code.
static Value *getAdjustedPtr(IRBuilderTy &IRB, const DataLayout &DL, Value *Ptr,
- APInt Offset, Type *PointerTy,
- Twine NamePrefix) {
+ APInt Offset, Type *PointerTy, Twine NamePrefix) {
// Even though we don't look through PHI nodes, we could be called on an
// instruction in an unreachable block, which may be on a cycle.
SmallPtrSet<Value *, 4> Visited;
@@ -1476,7 +1463,7 @@ static Value *getAdjustedPtr(IRBuilderTy &IRB, const DataLayout &DL, Value *Ptr,
break;
Offset += GEPOffset;
Ptr = GEP->getPointerOperand();
- if (!Visited.insert(Ptr))
+ if (!Visited.insert(Ptr).second)
break;
}
@@ -1513,7 +1500,7 @@ static Value *getAdjustedPtr(IRBuilderTy &IRB, const DataLayout &DL, Value *Ptr,
break;
}
assert(Ptr->getType()->isPointerTy() && "Unexpected operand type!");
- } while (Visited.insert(Ptr));
+ } while (Visited.insert(Ptr).second);
if (!OffsetPtr) {
if (!Int8Ptr) {
@@ -1523,9 +1510,10 @@ static Value *getAdjustedPtr(IRBuilderTy &IRB, const DataLayout &DL, Value *Ptr,
Int8PtrOffset = Offset;
}
- OffsetPtr = Int8PtrOffset == 0 ? Int8Ptr :
- IRB.CreateInBoundsGEP(Int8Ptr, IRB.getInt(Int8PtrOffset),
- NamePrefix + "sroa_raw_idx");
+ OffsetPtr = Int8PtrOffset == 0
+ ? Int8Ptr
+ : IRB.CreateInBoundsGEP(Int8Ptr, IRB.getInt(Int8PtrOffset),
+ NamePrefix + "sroa_raw_idx");
}
Ptr = OffsetPtr;
@@ -1629,38 +1617,38 @@ static Value *convertValue(const DataLayout &DL, IRBuilderTy &IRB, Value *V,
///
/// This function is called to test each entry in a partioning which is slated
/// for a single slice.
-static bool isVectorPromotionViableForSlice(
- const DataLayout &DL, AllocaSlices &S, uint64_t SliceBeginOffset,
- uint64_t SliceEndOffset, VectorType *Ty, uint64_t ElementSize,
- AllocaSlices::const_iterator I) {
+static bool
+isVectorPromotionViableForSlice(const DataLayout &DL, uint64_t SliceBeginOffset,
+ uint64_t SliceEndOffset, VectorType *Ty,
+ uint64_t ElementSize, const Slice &S) {
// First validate the slice offsets.
uint64_t BeginOffset =
- std::max(I->beginOffset(), SliceBeginOffset) - SliceBeginOffset;
+ std::max(S.beginOffset(), SliceBeginOffset) - SliceBeginOffset;
uint64_t BeginIndex = BeginOffset / ElementSize;
if (BeginIndex * ElementSize != BeginOffset ||
BeginIndex >= Ty->getNumElements())
return false;
uint64_t EndOffset =
- std::min(I->endOffset(), SliceEndOffset) - SliceBeginOffset;
+ std::min(S.endOffset(), SliceEndOffset) - SliceBeginOffset;
uint64_t EndIndex = EndOffset / ElementSize;
if (EndIndex * ElementSize != EndOffset || EndIndex > Ty->getNumElements())
return false;
assert(EndIndex > BeginIndex && "Empty vector!");
uint64_t NumElements = EndIndex - BeginIndex;
- Type *SliceTy =
- (NumElements == 1) ? Ty->getElementType()
- : VectorType::get(Ty->getElementType(), NumElements);
+ Type *SliceTy = (NumElements == 1)
+ ? Ty->getElementType()
+ : VectorType::get(Ty->getElementType(), NumElements);
Type *SplitIntTy =
Type::getIntNTy(Ty->getContext(), NumElements * ElementSize * 8);
- Use *U = I->getUse();
+ Use *U = S.getUse();
if (MemIntrinsic *MI = dyn_cast<MemIntrinsic>(U->getUser())) {
if (MI->isVolatile())
return false;
- if (!I->isSplittable())
+ if (!S.isSplittable())
return false; // Skip any unsplittable intrinsics.
} else if (IntrinsicInst *II = dyn_cast<IntrinsicInst>(U->getUser())) {
if (II->getIntrinsicID() != Intrinsic::lifetime_start &&
if (LI->isVolatile())
return false;
Type *LTy = LI->getType();
- if (SliceBeginOffset > I->beginOffset() ||
- SliceEndOffset < I->endOffset()) {
+ if (SliceBeginOffset > S.beginOffset() || SliceEndOffset < S.endOffset()) {
assert(LTy->isIntegerTy());
LTy = SplitIntTy;
}
if (SI->isVolatile())
return false;
Type *STy = SI->getValueOperand()->getType();
- if (SliceBeginOffset > I->beginOffset() ||
- SliceEndOffset < I->endOffset()) {
+ if (SliceBeginOffset > S.beginOffset() || SliceEndOffset < S.endOffset()) {
assert(STy->isIntegerTy());
STy = SplitIntTy;
}
/// SSA value. We only can ensure this for a limited set of operations, and we
/// don't want to do the rewrites unless we are confident that the result will
/// be promotable, so we have an early test here.
-static bool
-isVectorPromotionViable(const DataLayout &DL, Type *AllocaTy, AllocaSlices &S,
- uint64_t SliceBeginOffset, uint64_t SliceEndOffset,
- AllocaSlices::const_iterator I,
- AllocaSlices::const_iterator E,
+static VectorType *
+isVectorPromotionViable(const DataLayout &DL, uint64_t SliceBeginOffset,
+ uint64_t SliceEndOffset,
+ AllocaSlices::const_range Slices,
ArrayRef<AllocaSlices::iterator> SplitUses) {
- VectorType *Ty = dyn_cast<VectorType>(AllocaTy);
- if (!Ty)
- return false;
+ // Collect the candidate types for vector-based promotion. Also track whether
+ // we have different element types.
+ SmallVector<VectorType *, 4> CandidateTys;
+ Type *CommonEltTy = nullptr;
+ bool HaveCommonEltTy = true;
+ auto CheckCandidateType = [&](Type *Ty) {
+ if (auto *VTy = dyn_cast<VectorType>(Ty)) {
+ CandidateTys.push_back(VTy);
+ if (!CommonEltTy)
+ CommonEltTy = VTy->getElementType();
+ else if (CommonEltTy != VTy->getElementType())
+ HaveCommonEltTy = false;
+ }
+ };
+ // Consider any loads or stores that are the exact size of the slice.
+ for (const auto &S : Slices)
+ if (S.beginOffset() == SliceBeginOffset &&
+ S.endOffset() == SliceEndOffset) {
+ if (auto *LI = dyn_cast<LoadInst>(S.getUse()->getUser()))
+ CheckCandidateType(LI->getType());
+ else if (auto *SI = dyn_cast<StoreInst>(S.getUse()->getUser()))
+ CheckCandidateType(SI->getValueOperand()->getType());
+ }
+
+ // If we didn't find a vector type, nothing to do here.
+ if (CandidateTys.empty())
+ return nullptr;
- uint64_t ElementSize = DL.getTypeSizeInBits(Ty->getScalarType());
+ // Remove non-integer vector types if we had multiple common element types.
+ // FIXME: It'd be nice to replace them with integer vector types, but we can't
+ // do that until all the backends are known to produce good code for all
+ // integer vector types.
+ if (!HaveCommonEltTy) {
+ CandidateTys.erase(std::remove_if(CandidateTys.begin(), CandidateTys.end(),
+ [](VectorType *VTy) {
+ return !VTy->getElementType()->isIntegerTy();
+ }),
+ CandidateTys.end());
+
+ // If there were no integer vector types, give up.
+ if (CandidateTys.empty())
+ return nullptr;
- // While the definition of LLVM vectors is bitpacked, we don't support sizes
- // that aren't byte sized.
- if (ElementSize % 8)
- return false;
- assert((DL.getTypeSizeInBits(Ty) % 8) == 0 &&
- "vector size not a multiple of element size?");
- ElementSize /= 8;
+ // Rank the remaining candidate vector types. This is easy because we know
+ // they're all integer vectors. We sort by ascending number of elements.
+ auto RankVectorTypes = [&DL](VectorType *RHSTy, VectorType *LHSTy) {
+ assert(DL.getTypeSizeInBits(RHSTy) == DL.getTypeSizeInBits(LHSTy) &&
+ "Cannot have vector types of different sizes!");
+ assert(RHSTy->getElementType()->isIntegerTy() &&
+ "All non-integer types eliminated!");
+ assert(LHSTy->getElementType()->isIntegerTy() &&
+ "All non-integer types eliminated!");
+ return RHSTy->getNumElements() < LHSTy->getNumElements();
+ };
+ std::sort(CandidateTys.begin(), CandidateTys.end(), RankVectorTypes);
+ CandidateTys.erase(
+ std::unique(CandidateTys.begin(), CandidateTys.end(), RankVectorTypes),
+ CandidateTys.end());
+ } else {
+// The only way to have the same element type in every vector type is to
+// have the same vector type. Check that and remove all but one.
+#ifndef NDEBUG
+ for (VectorType *VTy : CandidateTys) {
+ assert(VTy->getElementType() == CommonEltTy &&
+ "Unaccounted for element type!");
+ assert(VTy == CandidateTys[0] &&
+ "Different vector types with the same element type!");
+ }
+#endif
+ CandidateTys.resize(1);
+ }
- for (; I != E; ++I)
- if (!isVectorPromotionViableForSlice(DL, S, SliceBeginOffset,
- SliceEndOffset, Ty, ElementSize, I))
- return false;
+ // Try each vector type, and return the one which works.
+ auto CheckVectorTypeForPromotion = [&](VectorType *VTy) {
+ uint64_t ElementSize = DL.getTypeSizeInBits(VTy->getElementType());
- for (ArrayRef<AllocaSlices::iterator>::const_iterator SUI = SplitUses.begin(),
- SUE = SplitUses.end();
- SUI != SUE; ++SUI)
- if (!isVectorPromotionViableForSlice(DL, S, SliceBeginOffset,
- SliceEndOffset, Ty, ElementSize, *SUI))
+ // While the definition of LLVM vectors is bitpacked, we don't support sizes
+ // that aren't byte sized.
+ if (ElementSize % 8)
return false;
+ assert((DL.getTypeSizeInBits(VTy) % 8) == 0 &&
+ "vector size not a multiple of element size?");
+ ElementSize /= 8;
- return true;
+ for (const auto &S : Slices)
+ if (!isVectorPromotionViableForSlice(DL, SliceBeginOffset, SliceEndOffset,
+ VTy, ElementSize, S))
+ return false;
+
+ for (const auto &SI : SplitUses)
+ if (!isVectorPromotionViableForSlice(DL, SliceBeginOffset, SliceEndOffset,
+ VTy, ElementSize, *SI))
+ return false;
+
+ return true;
+ };
+ for (VectorType *VTy : CandidateTys)
+ if (CheckVectorTypeForPromotion(VTy))
+ return VTy;
+
+ return nullptr;
}
/// \brief Test whether a slice of an alloca is valid for integer widening.
@@ -1749,23 +1808,25 @@ isVectorPromotionViable(const DataLayout &DL, Type *AllocaTy, AllocaSlices &S,
static bool isIntegerWideningViableForSlice(const DataLayout &DL,
Type *AllocaTy,
uint64_t AllocBeginOffset,
- uint64_t Size, AllocaSlices &S,
- AllocaSlices::const_iterator I,
+ uint64_t Size, const Slice &S,
bool &WholeAllocaOp) {
- uint64_t RelBegin = I->beginOffset() - AllocBeginOffset;
- uint64_t RelEnd = I->endOffset() - AllocBeginOffset;
+ uint64_t RelBegin = S.beginOffset() - AllocBeginOffset;
+ uint64_t RelEnd = S.endOffset() - AllocBeginOffset;
// We can't reasonably handle cases where the load or store extends past
// the end of the aloca's type and into its padding.
if (RelEnd > Size)
return false;
- Use *U = I->getUse();
+ Use *U = S.getUse();
if (LoadInst *LI = dyn_cast<LoadInst>(U->getUser())) {
if (LI->isVolatile())
return false;
- if (RelBegin == 0 && RelEnd == Size)
+ // Note that we don't count vector loads or stores as whole-alloca
+ // operations which enable integer widening because we would prefer to use
+ // vector widening instead.
+ if (!isa<VectorType>(LI->getType()) && RelBegin == 0 && RelEnd == Size)
WholeAllocaOp = true;
if (IntegerType *ITy = dyn_cast<IntegerType>(LI->getType())) {
if (ITy->getBitWidth() < DL.getTypeStoreSizeInBits(ITy))
Type *ValueTy = SI->getValueOperand()->getType();
if (SI->isVolatile())
return false;
- if (RelBegin == 0 && RelEnd == Size)
+ // Note that we don't count vector loads or stores as whole-alloca
+ // operations which enable integer widening because we would prefer to use
+ // vector widening instead.
+ if (!isa<VectorType>(ValueTy) && RelBegin == 0 && RelEnd == Size)
WholeAllocaOp = true;
if (IntegerType *ITy = dyn_cast<IntegerType>(ValueTy)) {
if (ITy->getBitWidth() < DL.getTypeStoreSizeInBits(ITy))
} else if (MemIntrinsic *MI = dyn_cast<MemIntrinsic>(U->getUser())) {
if (MI->isVolatile() || !isa<Constant>(MI->getLength()))
return false;
- if (!I->isSplittable())
+ if (!S.isSplittable())
return false; // Skip any unsplittable intrinsics.
} else if (IntrinsicInst *II = dyn_cast<IntrinsicInst>(U->getUser())) {
if (II->getIntrinsicID() != Intrinsic::lifetime_start &&
/// promote the resulting alloca.
static bool
isIntegerWideningViable(const DataLayout &DL, Type *AllocaTy,
- uint64_t AllocBeginOffset, AllocaSlices &S,
- AllocaSlices::const_iterator I,
- AllocaSlices::const_iterator E,
+ uint64_t AllocBeginOffset,
+ AllocaSlices::const_range Slices,
ArrayRef<AllocaSlices::iterator> SplitUses) {
uint64_t SizeInBits = DL.getTypeSizeInBits(AllocaTy);
// Don't create integer types larger than the maximum bitwidth.
// promote due to some other unsplittable entry (which we may make splittable
// later). However, if there are only splittable uses, go ahead and assume
// that we cover the alloca.
- bool WholeAllocaOp = (I != E) ? false : DL.isLegalInteger(SizeInBits);
+ bool WholeAllocaOp =
+ Slices.begin() != Slices.end() ? false : DL.isLegalInteger(SizeInBits);
- for (; I != E; ++I)
+ for (const auto &S : Slices)
if (!isIntegerWideningViableForSlice(DL, AllocaTy, AllocBeginOffset, Size,
- S, I, WholeAllocaOp))
+ S, WholeAllocaOp))
return false;
- for (ArrayRef<AllocaSlices::iterator>::const_iterator SUI = SplitUses.begin(),
- SUE = SplitUses.end();
- SUI != SUE; ++SUI)
+ for (const auto &SI : SplitUses)
if (!isIntegerWideningViableForSlice(DL, AllocaTy, AllocBeginOffset, Size,
- S, *SUI, WholeAllocaOp))
+ *SI, WholeAllocaOp))
return false;
return WholeAllocaOp;
@@ -1867,9 +1929,9 @@ static Value *extractInteger(const DataLayout &DL, IRBuilderTy &IRB, Value *V,
IntegerType *IntTy = cast<IntegerType>(V->getType());
assert(DL.getTypeStoreSize(Ty) + Offset <= DL.getTypeStoreSize(IntTy) &&
"Element extends past full value");
- uint64_t ShAmt = 8*Offset;
+ uint64_t ShAmt = 8 * Offset;
if (DL.isBigEndian())
- ShAmt = 8*(DL.getTypeStoreSize(IntTy) - DL.getTypeStoreSize(Ty) - Offset);
+ ShAmt = 8 * (DL.getTypeStoreSize(IntTy) - DL.getTypeStoreSize(Ty) - Offset);
if (ShAmt) {
V = IRB.CreateLShr(V, ShAmt, Name + ".shift");
DEBUG(dbgs() << " shifted: " << *V << "\n");
@@ -1896,9 +1958,9 @@ static Value *insertInteger(const DataLayout &DL, IRBuilderTy &IRB, Value *Old,
}
assert(DL.getTypeStoreSize(Ty) + Offset <= DL.getTypeStoreSize(IntTy) &&
"Element store outside of alloca store");
- uint64_t ShAmt = 8*Offset;
+ uint64_t ShAmt = 8 * Offset;
if (DL.isBigEndian())
- ShAmt = 8*(DL.getTypeStoreSize(IntTy) - DL.getTypeStoreSize(Ty) - Offset);
+ ShAmt = 8 * (DL.getTypeStoreSize(IntTy) - DL.getTypeStoreSize(Ty) - Offset);
if (ShAmt) {
V = IRB.CreateShl(V, ShAmt, Name + ".shift");
DEBUG(dbgs() << " shifted: " << *V << "\n");
@@ -1914,9 +1976,8 @@ static Value *insertInteger(const DataLayout &DL, IRBuilderTy &IRB, Value *Old,
return V;
}
-static Value *extractVector(IRBuilderTy &IRB, Value *V,
- unsigned BeginIndex, unsigned EndIndex,
- const Twine &Name) {
+static Value *extractVector(IRBuilderTy &IRB, Value *V, unsigned BeginIndex,
+ unsigned EndIndex, const Twine &Name) {
VectorType *VecTy = cast<VectorType>(V->getType());
unsigned NumElements = EndIndex - BeginIndex;
assert(NumElements <= VecTy->getNumElements() && "Too many elements!");
return V;
}
- SmallVector<Constant*, 8> Mask;
+ SmallVector<Constant *, 8> Mask;
Mask.reserve(NumElements);
for (unsigned i = BeginIndex; i != EndIndex; ++i)
Mask.push_back(IRB.getInt32(i));
V = IRB.CreateShuffleVector(V, UndefValue::get(V->getType()),
- ConstantVector::get(Mask),
- Name + ".extract");
+ ConstantVector::get(Mask), Name + ".extract");
DEBUG(dbgs() << " shuffle: " << *V << "\n");
return V;
}
// Single element to insert.
V = IRB.CreateInsertElement(Old, V, IRB.getInt32(BeginIndex),
Name + ".insert");
- DEBUG(dbgs() << " insert: " << *V << "\n");
+ DEBUG(dbgs() << " insert: " << *V << "\n");
return V;
}
// use a shuffle vector to widen it with undef elements, and then
// a second shuffle vector to select between the loaded vector and the
// incoming vector.
- SmallVector<Constant*, 8> Mask;
+ SmallVector<Constant *, 8> Mask;
Mask.reserve(VecTy->getNumElements());
for (unsigned i = 0; i != VecTy->getNumElements(); ++i)
if (i >= BeginIndex && i < EndIndex)
else
Mask.push_back(UndefValue::get(IRB.getInt32Ty()));
V = IRB.CreateShuffleVector(V, UndefValue::get(V->getType()),
- ConstantVector::get(Mask),
- Name + ".expand");
+ ConstantVector::get(Mask), Name + ".expand");
DEBUG(dbgs() << " shuffle: " << *V << "\n");
Mask.clear();
typedef llvm::InstVisitor<AllocaSliceRewriter, bool> Base;
const DataLayout &DL;
- AllocaSlices &S;
+ AllocaSlices &AS;
SROA &Pass;
AllocaInst &OldAI, &NewAI;
const uint64_t NewAllocaBeginOffset, NewAllocaEndOffset;
Type *NewAllocaTy;
+ // This is a convenience and flag variable that will be null unless the new
+ // alloca's integer operations should be widened to this integer type due to
+ // passing isIntegerWideningViable above. If it is non-null, the desired
+ // integer type will be stored here for easy access during rewriting.
+ IntegerType *IntTy;
+
// If we are rewriting an alloca partition which can be written as pure
// vector operations, we stash extra information here. When VecTy is
// non-null, we have some strict guarantees about the rewritten alloca:
Type *ElementTy;
uint64_t ElementSize;
- // This is a convenience and flag variable that will be null unless the new
- // alloca's integer operations should be widened to this integer type due to
- // passing isIntegerWideningViable above. If it is non-null, the desired
- // integer type will be stored here for easy access during rewriting.
- IntegerType *IntTy;
-
// The original offset of the slice currently being rewritten relative to
// the original alloca.
uint64_t BeginOffset, EndOffset;
IRBuilderTy IRB;
public:
- AllocaSliceRewriter(const DataLayout &DL, AllocaSlices &S, SROA &Pass,
+ AllocaSliceRewriter(const DataLayout &DL, AllocaSlices &AS, SROA &Pass,
AllocaInst &OldAI, AllocaInst &NewAI,
uint64_t NewAllocaBeginOffset,
- uint64_t NewAllocaEndOffset, bool IsVectorPromotable,
- bool IsIntegerPromotable,
+ uint64_t NewAllocaEndOffset, bool IsIntegerPromotable,
+ VectorType *PromotableVecTy,
SmallPtrSetImpl<PHINode *> &PHIUsers,
SmallPtrSetImpl<SelectInst *> &SelectUsers)
- : DL(DL), S(S), Pass(Pass), OldAI(OldAI), NewAI(NewAI),
+ : DL(DL), AS(AS), Pass(Pass), OldAI(OldAI), NewAI(NewAI),
NewAllocaBeginOffset(NewAllocaBeginOffset),
NewAllocaEndOffset(NewAllocaEndOffset),
NewAllocaTy(NewAI.getAllocatedType()),
- VecTy(IsVectorPromotable ? cast<VectorType>(NewAllocaTy) : nullptr),
- ElementTy(VecTy ? VecTy->getElementType() : nullptr),
- ElementSize(VecTy ? DL.getTypeSizeInBits(ElementTy) / 8 : 0),
IntTy(IsIntegerPromotable
? Type::getIntNTy(
NewAI.getContext(),
DL.getTypeSizeInBits(NewAI.getAllocatedType()))
: nullptr),
+ VecTy(PromotableVecTy),
+ ElementTy(VecTy ? VecTy->getElementType() : nullptr),
+ ElementSize(VecTy ? DL.getTypeSizeInBits(ElementTy) / 8 : 0),
BeginOffset(), EndOffset(), IsSplittable(), IsSplit(), OldUse(),
OldPtr(), PHIUsers(PHIUsers), SelectUsers(SelectUsers),
IRB(NewAI.getContext(), ConstantFolder()) {
"Only multiple-of-8 sized vector elements are viable");
++NumVectorized;
}
- assert((!IsVectorPromotable && !IsIntegerPromotable) ||
- IsVectorPromotable != IsIntegerPromotable);
+ assert((!IntTy && !VecTy) || (IntTy && !VecTy) || (!IntTy && VecTy));
}
bool visit(AllocaSlices::const_iterator I) {
);
}
- /// \brief Compute suitable alignment to access this slice of the *new* alloca.
+ /// \brief Compute suitable alignment to access this slice of the *new*
+ /// alloca.
///
/// You can optionally pass a type to this routine and if that type's ABI
/// alignment is itself suitable, this will return zero.
unsigned NewAIAlign = NewAI.getAlignment();
if (!NewAIAlign)
NewAIAlign = DL.getABITypeAlignment(NewAI.getAllocatedType());
- unsigned Align = MinAlign(NewAIAlign, NewBeginOffset - NewAllocaBeginOffset);
+ unsigned Align =
+ MinAlign(NewAIAlign, NewBeginOffset - NewAllocaBeginOffset);
return (Ty && Align == DL.getABITypeAlignment(Ty)) ? 0 : Align;
}
unsigned EndIndex = getIndex(NewEndOffset);
assert(EndIndex > BeginIndex && "Empty vector!");
- Value *V = IRB.CreateAlignedLoad(&NewAI, NewAI.getAlignment(),
- "load");
+ Value *V = IRB.CreateAlignedLoad(&NewAI, NewAI.getAlignment(), "load");
return extractVector(IRB, V, BeginIndex, EndIndex, "vec");
}
Value *rewriteIntegerLoad(LoadInst &LI) {
assert(IntTy && "We cannot insert an integer to the alloca");
assert(!LI.isVolatile());
- Value *V = IRB.CreateAlignedLoad(&NewAI, NewAI.getAlignment(),
- "load");
+ Value *V = IRB.CreateAlignedLoad(&NewAI, NewAI.getAlignment(), "load");
V = convertValue(DL, IRB, V, IntTy);
assert(NewBeginOffset >= NewAllocaBeginOffset && "Out of bounds offset");
uint64_t Offset = NewBeginOffset - NewAllocaBeginOffset;
V = rewriteIntegerLoad(LI);
} else if (NewBeginOffset == NewAllocaBeginOffset &&
canConvertValue(DL, NewAllocaTy, LI.getType())) {
- V = IRB.CreateAlignedLoad(&NewAI, NewAI.getAlignment(),
- LI.isVolatile(), LI.getName());
+ V = IRB.CreateAlignedLoad(&NewAI, NewAI.getAlignment(), LI.isVolatile(),
+ LI.getName());
} else {
Type *LTy = TargetTy->getPointerTo();
V = IRB.CreateAlignedLoad(getNewAllocaSlicePtr(IRB, LTy),
assert(SliceSize < DL.getTypeStoreSize(LI.getType()) &&
"Split load isn't smaller than original load");
assert(LI.getType()->getIntegerBitWidth() ==
- DL.getTypeStoreSizeInBits(LI.getType()) &&
+ DL.getTypeStoreSizeInBits(LI.getType()) &&
"Non-byte-multiple bit width");
// Move the insertion point just past the load so that we can refer to it.
IRB.SetInsertPoint(std::next(BasicBlock::iterator(&LI)));
// basis for the new value. This allows us to replace the uses of LI with
// the computed value, and then replace the placeholder with LI, leaving
// LI only used for this computation.
- Value *Placeholder
- = new LoadInst(UndefValue::get(LI.getType()->getPointerTo()));
- V = insertInteger(DL, IRB, Placeholder, V, NewBeginOffset,
- "insert");
+ Value *Placeholder =
+ new LoadInst(UndefValue::get(LI.getType()->getPointerTo()));
+ V = insertInteger(DL, IRB, Placeholder, V, NewBeginOffset, "insert");
LI.replaceAllUsesWith(V);
Placeholder->replaceAllUsesWith(&LI);
delete Placeholder;
assert(EndIndex > BeginIndex && "Empty vector!");
unsigned NumElements = EndIndex - BeginIndex;
assert(NumElements <= VecTy->getNumElements() && "Too many elements!");
- Type *SliceTy =
- (NumElements == 1) ? ElementTy
- : VectorType::get(ElementTy, NumElements);
+ Type *SliceTy = (NumElements == 1)
+ ? ElementTy
+ : VectorType::get(ElementTy, NumElements);
if (V->getType() != SliceTy)
V = convertValue(DL, IRB, V, SliceTy);
// Mix in the existing elements.
- Value *Old = IRB.CreateAlignedLoad(&NewAI, NewAI.getAlignment(),
- "load");
+ Value *Old = IRB.CreateAlignedLoad(&NewAI, NewAI.getAlignment(), "load");
V = insertVector(IRB, Old, V, BeginIndex, "vec");
}
StoreInst *Store = IRB.CreateAlignedStore(V, &NewAI, NewAI.getAlignment());
assert(IntTy && "We cannot extract an integer from the alloca");
assert(!SI.isVolatile());
if (DL.getTypeSizeInBits(V->getType()) != IntTy->getBitWidth()) {
- Value *Old = IRB.CreateAlignedLoad(&NewAI, NewAI.getAlignment(),
- "oldload");
+ Value *Old =
+ IRB.CreateAlignedLoad(&NewAI, NewAI.getAlignment(), "oldload");
Old = convertValue(DL, IRB, Old, IntTy);
assert(BeginOffset >= NewAllocaBeginOffset && "Out of bounds offset");
uint64_t Offset = BeginOffset - NewAllocaBeginOffset;
- V = insertInteger(DL, IRB, Old, SI.getValueOperand(), Offset,
- "insert");
+ V = insertInteger(DL, IRB, Old, SI.getValueOperand(), Offset, "insert");
}
V = convertValue(DL, IRB, V, NewAllocaTy);
StoreInst *Store = IRB.CreateAlignedStore(V, &NewAI, NewAI.getAlignment());
assert(V->getType()->isIntegerTy() &&
"Only integer type loads and stores are split");
assert(V->getType()->getIntegerBitWidth() ==
- DL.getTypeStoreSizeInBits(V->getType()) &&
+ DL.getTypeStoreSizeInBits(V->getType()) &&
"Non-byte-multiple bit width");
IntegerType *NarrowTy = Type::getIntNTy(SI.getContext(), SliceSize * 8);
- V = extractInteger(DL, IRB, V, NarrowTy, NewBeginOffset,
- "extract");
+ V = extractInteger(DL, IRB, V, NarrowTy, NewBeginOffset, "extract");
}
if (VecTy)
if (Size == 1)
return V;
- Type *SplatIntTy = Type::getIntNTy(VTy->getContext(), Size*8);
- V = IRB.CreateMul(IRB.CreateZExt(V, SplatIntTy, "zext"),
- ConstantExpr::getUDiv(
- Constant::getAllOnesValue(SplatIntTy),
- ConstantExpr::getZExt(
- Constant::getAllOnesValue(V->getType()),
- SplatIntTy)),
- "isplat");
+ Type *SplatIntTy = Type::getIntNTy(VTy->getContext(), Size * 8);
+ V = IRB.CreateMul(
+ IRB.CreateZExt(V, SplatIntTy, "zext"),
+ ConstantExpr::getUDiv(
+ Constant::getAllOnesValue(SplatIntTy),
+ ConstantExpr::getZExt(Constant::getAllOnesValue(V->getType()),
+ SplatIntTy)),
+ "isplat");
return V;
}
// If this doesn't map cleanly onto the alloca type, and that type isn't
// a single value type, just emit a memset.
if (!VecTy && !IntTy &&
- (BeginOffset > NewAllocaBeginOffset ||
- EndOffset < NewAllocaEndOffset ||
+ (BeginOffset > NewAllocaBeginOffset || EndOffset < NewAllocaEndOffset ||
SliceSize != DL.getTypeStoreSize(AllocaTy) ||
!AllocaTy->isSingleValueType() ||
!DL.isLegalInteger(DL.getTypeSizeInBits(ScalarTy)) ||
- DL.getTypeSizeInBits(ScalarTy)%8 != 0)) {
+ DL.getTypeSizeInBits(ScalarTy) % 8 != 0)) {
Type *SizeTy = II.getLength()->getType();
Constant *Size = ConstantInt::get(SizeTy, NewEndOffset - NewBeginOffset);
CallInst *New = IRB.CreateMemSet(
if (NumElements > 1)
Splat = getVectorSplat(Splat, NumElements);
- Value *Old = IRB.CreateAlignedLoad(&NewAI, NewAI.getAlignment(),
- "oldload");
+ Value *Old =
+ IRB.CreateAlignedLoad(&NewAI, NewAI.getAlignment(), "oldload");
V = insertVector(IRB, Old, Splat, BeginIndex, "vec");
} else if (IntTy) {
// If this is a memset on an alloca where we can widen stores, insert the
if (IntTy && (BeginOffset != NewAllocaBeginOffset ||
EndOffset != NewAllocaBeginOffset)) {
- Value *Old = IRB.CreateAlignedLoad(&NewAI, NewAI.getAlignment(),
- "oldload");
+ Value *Old =
+ IRB.CreateAlignedLoad(&NewAI, NewAI.getAlignment(), "oldload");
Old = convertValue(DL, IRB, Old, IntTy);
uint64_t Offset = NewBeginOffset - NewAllocaBeginOffset;
V = insertInteger(DL, IRB, Old, V, Offset, "insert");
// Strip all inbounds GEPs and pointer casts to try to dig out any root
// alloca that should be re-examined after rewriting this instruction.
Value *OtherPtr = IsDest ? II.getRawSource() : II.getRawDest();
- if (AllocaInst *AI
- = dyn_cast<AllocaInst>(OtherPtr->stripInBoundsOffsets())) {
+ if (AllocaInst *AI =
+ dyn_cast<AllocaInst>(OtherPtr->stripInBoundsOffsets())) {
assert(AI != &OldAI && AI != &NewAI &&
"Splittable transfers cannot reach the same alloca on both ends.");
Pass.Worklist.insert(AI);
unsigned BeginIndex = VecTy ? getIndex(NewBeginOffset) : 0;
unsigned EndIndex = VecTy ? getIndex(NewEndOffset) : 0;
unsigned NumElements = EndIndex - BeginIndex;
- IntegerType *SubIntTy
- = IntTy ? Type::getIntNTy(IntTy->getContext(), Size*8) : nullptr;
+ IntegerType *SubIntTy =
+ IntTy ? Type::getIntNTy(IntTy->getContext(), Size * 8) : nullptr;
// Reset the other pointer type to match the register type we're going to
// use, but using the address space of the original other pointer.
Value *Src;
if (VecTy && !IsWholeAlloca && !IsDest) {
- Src = IRB.CreateAlignedLoad(&NewAI, NewAI.getAlignment(),
- "load");
+ Src = IRB.CreateAlignedLoad(&NewAI, NewAI.getAlignment(), "load");
Src = extractVector(IRB, Src, BeginIndex, EndIndex, "vec");
} else if (IntTy && !IsWholeAlloca && !IsDest) {
- Src = IRB.CreateAlignedLoad(&NewAI, NewAI.getAlignment(),
- "load");
+ Src = IRB.CreateAlignedLoad(&NewAI, NewAI.getAlignment(), "load");
Src = convertValue(DL, IRB, Src, IntTy);
uint64_t Offset = NewBeginOffset - NewAllocaBeginOffset;
Src = extractInteger(DL, IRB, Src, SubIntTy, Offset, "extract");
} else {
- Src = IRB.CreateAlignedLoad(SrcPtr, SrcAlign, II.isVolatile(),
- "copyload");
+ Src =
+ IRB.CreateAlignedLoad(SrcPtr, SrcAlign, II.isVolatile(), "copyload");
}
if (VecTy && !IsWholeAlloca && IsDest) {
- Value *Old = IRB.CreateAlignedLoad(&NewAI, NewAI.getAlignment(),
- "oldload");
+ Value *Old =
+ IRB.CreateAlignedLoad(&NewAI, NewAI.getAlignment(), "oldload");
Src = insertVector(IRB, Old, Src, BeginIndex, "vec");
} else if (IntTy && !IsWholeAlloca && IsDest) {
- Value *Old = IRB.CreateAlignedLoad(&NewAI, NewAI.getAlignment(),
- "oldload");
+ Value *Old =
+ IRB.CreateAlignedLoad(&NewAI, NewAI.getAlignment(), "oldload");
Old = convertValue(DL, IRB, Old, IntTy);
uint64_t Offset = NewBeginOffset - NewAllocaBeginOffset;
Src = insertInteger(DL, IRB, Old, Src, Offset, "insert");
// Record this instruction for deletion.
Pass.DeadInsts.insert(&II);
- ConstantInt *Size
- = ConstantInt::get(cast<IntegerType>(II.getArgOperand(0)->getType()),
+ ConstantInt *Size =
+ ConstantInt::get(cast<IntegerType>(II.getArgOperand(0)->getType()),
NewEndOffset - NewBeginOffset);
Value *Ptr = getNewAllocaSlicePtr(IRB, OldPtr->getType());
Value *New;
SelectUsers.insert(&SI);
return true;
}
-
};
}
/// This uses a set to de-duplicate users.
void enqueueUsers(Instruction &I) {
for (Use &U : I.uses())
- if (Visited.insert(U.getUser()))
+ if (Visited.insert(U.getUser()).second)
Queue.push_back(&U);
}
bool visitInstruction(Instruction &I) { return false; }
/// \brief Generic recursive split emission class.
- template <typename Derived>
- class OpSplitter {
+ template <typename Derived> class OpSplitter {
protected:
/// The builder used to form new instructions.
IRBuilderTy IRB;
/// Initialize the splitter with an insertion point, Ptr and start with a
/// single zero GEP index.
OpSplitter(Instruction *InsertionPoint, Value *Ptr)
- : IRB(InsertionPoint), GEPIndices(1, IRB.getInt32(0)), Ptr(Ptr) {}
+ : IRB(InsertionPoint), GEPIndices(1, IRB.getInt32(0)), Ptr(Ptr) {}
public:
/// \brief Generic recursive split emission routine.
struct LoadOpSplitter : public OpSplitter<LoadOpSplitter> {
LoadOpSplitter(Instruction *InsertionPoint, Value *Ptr)
- : OpSplitter<LoadOpSplitter>(InsertionPoint, Ptr) {}
+ : OpSplitter<LoadOpSplitter>(InsertionPoint, Ptr) {}
/// Emit a leaf load of a single value. This is called at the leaves of the
/// recursive emission to actually load values.
struct StoreOpSplitter : public OpSplitter<StoreOpSplitter> {
StoreOpSplitter(Instruction *InsertionPoint, Value *Ptr)
- : OpSplitter<StoreOpSplitter>(InsertionPoint, Ptr) {}
+ : OpSplitter<StoreOpSplitter>(InsertionPoint, Ptr) {}
/// Emit a leaf store of a single value. This is called at the leaves of the
/// recursive emission to actually produce stores.
assert(Ty->isSingleValueType());
// Extract the single value and store it using the indices.
Value *Store = IRB.CreateStore(
- IRB.CreateExtractValue(Agg, Indices, Name + ".extract"),
- IRB.CreateInBoundsGEP(Ptr, GEPIndices, Name + ".gep"));
+ IRB.CreateExtractValue(Agg, Indices, Name + ".extract"),
+ IRB.CreateInBoundsGEP(Ptr, GEPIndices, Name + ".gep"));
(void)Store;
DEBUG(dbgs() << " to: " << *Store << "\n");
}
/// when the size or offset cause either end of type-based partition to be off.
/// Also, this is a best-effort routine. It is reasonable to give up and not
/// return a type if necessary.
-static Type *getTypePartition(const DataLayout &DL, Type *Ty,
- uint64_t Offset, uint64_t Size) {
+static Type *getTypePartition(const DataLayout &DL, Type *Ty, uint64_t Offset,
+ uint64_t Size) {
if (Offset == 0 && DL.getTypeAllocSize(Ty) == Size)
return stripAggregateTypeWrapping(DL, Ty);
if (Offset > DL.getTypeAllocSize(Ty) ||
}
// Try to build up a sub-structure.
- StructType *SubTy = StructType::get(STy->getContext(), makeArrayRef(EI, EE),
- STy->isPacked());
+ StructType *SubTy =
+ StructType::get(STy->getContext(), makeArrayRef(EI, EE), STy->isPacked());
const StructLayout *SubSL = DL.getStructLayout(SubTy);
if (Size != SubSL->getSizeInBytes())
return nullptr; // The sub-struct doesn't have quite the size needed.
/// appropriate new offsets. It also evaluates how successful the rewrite was
/// at enabling promotion and if it was successful queues the alloca to be
/// promoted.
-bool SROA::rewritePartition(AllocaInst &AI, AllocaSlices &S,
+bool SROA::rewritePartition(AllocaInst &AI, AllocaSlices &AS,
AllocaSlices::iterator B, AllocaSlices::iterator E,
int64_t BeginOffset, int64_t EndOffset,
ArrayRef<AllocaSlices::iterator> SplitUses) {
SliceTy = ArrayType::get(Type::getInt8Ty(*C), SliceSize);
assert(DL->getTypeAllocSize(SliceTy) >= SliceSize);
- bool IsVectorPromotable = isVectorPromotionViable(
- *DL, SliceTy, S, BeginOffset, EndOffset, B, E, SplitUses);
+ bool IsIntegerPromotable = isIntegerWideningViable(
+ *DL, SliceTy, BeginOffset, AllocaSlices::const_range(B, E), SplitUses);
- bool IsIntegerPromotable =
- !IsVectorPromotable &&
- isIntegerWideningViable(*DL, SliceTy, BeginOffset, S, B, E, SplitUses);
+ VectorType *VecTy =
+ IsIntegerPromotable
+ ? nullptr
+ : isVectorPromotionViable(*DL, BeginOffset, EndOffset,
+ AllocaSlices::const_range(B, E), SplitUses);
+ if (VecTy)
+ SliceTy = VecTy;
// Check for the case where we're going to rewrite to a new alloca of the
// exact same type as the original, and with the same access offsets. In that
// perform phi and select speculation.
AllocaInst *NewAI;
if (SliceTy == AI.getAllocatedType()) {
- assert(BeginOffset == 0 &&
- "Non-zero begin offset but same alloca type");
+ assert(BeginOffset == 0 && "Non-zero begin offset but same alloca type");
NewAI = &AI;
// FIXME: We should be able to bail at this point with "nothing changed".
// FIXME: We might want to defer PHI speculation until after here.
// the alloca's alignment unconstrained.
if (Alignment <= DL->getABITypeAlignment(SliceTy))
Alignment = 0;
- NewAI = new AllocaInst(SliceTy, nullptr, Alignment,
- AI.getName() + ".sroa." + Twine(B - S.begin()), &AI);
+ NewAI =
+ new AllocaInst(SliceTy, nullptr, Alignment,
+ AI.getName() + ".sroa." + Twine(B - AS.begin()), &AI);
++NumNewAllocas;
+
+ // Migrate debug information from the old alloca to the new alloca
+ // and the individial slices.
+ if (DbgDeclareInst *DbgDecl = DbgDeclares.lookup(&AI)) {
+ DIVariable Var(DbgDecl->getVariable());
+ DIExpression Piece;
+ DIBuilder DIB(*AI.getParent()->getParent()->getParent(),
+ /*AllowUnresolved*/ false);
+ // Create a piece expression describing the slice, if the new slize is
+ // smaller than the old alloca or the old alloca already was described
+ // with a piece. It would be even better to just compare against the size
+ // of the type described in the debug info, but then we would need to
+ // build an expensive DIRefMap.
+ if (SliceSize < DL->getTypeAllocSize(AI.getAllocatedType()) ||
+ DIExpression(DbgDecl->getExpression()).isVariablePiece())
+ Piece = DIB.createPieceExpression(BeginOffset, SliceSize);
+ Instruction *NewDDI = DIB.insertDeclare(NewAI, Var, Piece, &AI);
+ NewDDI->setDebugLoc(DbgDecl->getDebugLoc());
+ DbgDeclares.insert(std::make_pair(NewAI, cast<DbgDeclareInst>(NewDDI)));
+ DeadInsts.insert(DbgDecl);
+ }
}
DEBUG(dbgs() << "Rewriting alloca partition "
SmallPtrSet<PHINode *, 8> PHIUsers;
SmallPtrSet<SelectInst *, 8> SelectUsers;
- AllocaSliceRewriter Rewriter(*DL, S, *this, AI, *NewAI, BeginOffset,
- EndOffset, IsVectorPromotable,
- IsIntegerPromotable, PHIUsers, SelectUsers);
+ AllocaSliceRewriter Rewriter(*DL, AS, *this, AI, *NewAI, BeginOffset,
+ EndOffset, IsIntegerPromotable, VecTy, PHIUsers,
+ SelectUsers);
bool Promotable = true;
- for (ArrayRef<AllocaSlices::iterator>::const_iterator SUI = SplitUses.begin(),
- SUE = SplitUses.end();
- SUI != SUE; ++SUI) {
+ for (auto &SplitUse : SplitUses) {
DEBUG(dbgs() << " rewriting split ");
- DEBUG(S.printSlice(dbgs(), *SUI, ""));
- Promotable &= Rewriter.visit(*SUI);
+ DEBUG(AS.printSlice(dbgs(), SplitUse, ""));
+ Promotable &= Rewriter.visit(SplitUse);
++NumUses;
}
for (AllocaSlices::iterator I = B; I != E; ++I) {
DEBUG(dbgs() << " rewriting ");
- DEBUG(S.printSlice(dbgs(), I, ""));
+ DEBUG(AS.printSlice(dbgs(), I, ""));
Promotable &= Rewriter.visit(I);
++NumUses;
}
// If we have either PHIs or Selects to speculate, add them to those
// worklists and re-queue the new alloca so that we promote in on the
// next iteration.
- for (SmallPtrSetImpl<PHINode *>::iterator I = PHIUsers.begin(),
- E = PHIUsers.end();
- I != E; ++I)
- SpeculatablePHIs.insert(*I);
- for (SmallPtrSetImpl<SelectInst *>::iterator I = SelectUsers.begin(),
- E = SelectUsers.end();
- I != E; ++I)
- SpeculatableSelects.insert(*I);
+ for (PHINode *PHIUser : PHIUsers)
+ SpeculatablePHIs.insert(PHIUser);
+ for (SelectInst *SelectUser : SelectUsers)
+ SpeculatableSelects.insert(SelectUser);
Worklist.insert(NewAI);
}
} else {
}
size_t SplitUsesOldSize = SplitUses.size();
- SplitUses.erase(std::remove_if(SplitUses.begin(), SplitUses.end(),
- [Offset](const AllocaSlices::iterator &I) {
- return I->endOffset() <= Offset;
- }),
+ SplitUses.erase(std::remove_if(
+ SplitUses.begin(), SplitUses.end(),
+ [Offset](const AllocaSlices::iterator &I) {
+ return I->endOffset() <= Offset;
+ }),
SplitUses.end());
if (SplitUsesOldSize == SplitUses.size())
return;
// Recompute the max. While this is linear, so is remove_if.
MaxSplitUseEndOffset = 0;
- for (SmallVectorImpl<AllocaSlices::iterator>::iterator
- SUI = SplitUses.begin(),
- SUE = SplitUses.end();
- SUI != SUE; ++SUI)
- MaxSplitUseEndOffset = std::max((*SUI)->endOffset(), MaxSplitUseEndOffset);
+ for (AllocaSlices::iterator SplitUse : SplitUses)
+ MaxSplitUseEndOffset =
+ std::max(SplitUse->endOffset(), MaxSplitUseEndOffset);
}
/// \brief Walks the slices of an alloca and form partitions based on them,
/// rewriting each of their uses.
-bool SROA::splitAlloca(AllocaInst &AI, AllocaSlices &S) {
- if (S.begin() == S.end())
+bool SROA::splitAlloca(AllocaInst &AI, AllocaSlices &AS) {
+ if (AS.begin() == AS.end())
return false;
unsigned NumPartitions = 0;
SmallVector<AllocaSlices::iterator, 4> SplitUses;
uint64_t MaxSplitUseEndOffset = 0;
- uint64_t BeginOffset = S.begin()->beginOffset();
+ uint64_t BeginOffset = AS.begin()->beginOffset();
- for (AllocaSlices::iterator SI = S.begin(), SJ = std::next(SI), SE = S.end();
+ for (AllocaSlices::iterator SI = AS.begin(), SJ = std::next(SI),
+ SE = AS.end();
SI != SE; SI = SJ) {
uint64_t MaxEndOffset = SI->endOffset();
// we'll have to rewrite uses and erase old split uses.
if (BeginOffset < MaxEndOffset) {
// Rewrite a sequence of overlapping slices.
- Changed |=
- rewritePartition(AI, S, SI, SJ, BeginOffset, MaxEndOffset, SplitUses);
+ Changed |= rewritePartition(AI, AS, SI, SJ, BeginOffset, MaxEndOffset,
+ SplitUses);
++NumPartitions;
removeFinishedSplitUses(SplitUses, MaxSplitUseEndOffset, MaxEndOffset);
uint64_t PostSplitEndOffset =
SJ == SE ? MaxSplitUseEndOffset : SJ->beginOffset();
- Changed |= rewritePartition(AI, S, SJ, SJ, MaxEndOffset, PostSplitEndOffset,
- SplitUses);
+ Changed |= rewritePartition(AI, AS, SJ, SJ, MaxEndOffset,
+ PostSplitEndOffset, SplitUses);
++NumPartitions;
if (SJ == SE)
Changed |= AggRewriter.rewrite(AI);
// Build the slices using a recursive instruction-visiting builder.
- AllocaSlices S(*DL, AI);
- DEBUG(S.print(dbgs()));
- if (S.isEscaped())
+ AllocaSlices AS(*DL, AI);
+ DEBUG(AS.print(dbgs()));
+ if (AS.isEscaped())
return Changed;
// Delete all the dead users of this alloca before splitting and rewriting it.
- for (AllocaSlices::dead_user_iterator DI = S.dead_user_begin(),
- DE = S.dead_user_end();
- DI != DE; ++DI) {
+ for (Instruction *DeadUser : AS.getDeadUsers()) {
// Free up everything used by this instruction.
- for (Use &DeadOp : (*DI)->operands())
+ for (Use &DeadOp : DeadUser->operands())
clobberUse(DeadOp);
// Now replace the uses of this instruction.
- (*DI)->replaceAllUsesWith(UndefValue::get((*DI)->getType()));
+ DeadUser->replaceAllUsesWith(UndefValue::get(DeadUser->getType()));
// And mark it for deletion.
- DeadInsts.insert(*DI);
+ DeadInsts.insert(DeadUser);
Changed = true;
}
- for (AllocaSlices::dead_op_iterator DO = S.dead_op_begin(),
- DE = S.dead_op_end();
- DO != DE; ++DO) {
- clobberUse(**DO);
+ for (Use *DeadOp : AS.getDeadOperands()) {
+ clobberUse(*DeadOp);
Changed = true;
}
// No slices to split. Leave the dead alloca for a later pass to clean up.
- if (S.begin() == S.end())
+ if (AS.begin() == AS.end())
return Changed;
- Changed |= splitAlloca(AI, S);
+ Changed |= splitAlloca(AI, AS);
DEBUG(dbgs() << " Speculating PHIs\n");
while (!SpeculatablePHIs.empty())
///
/// We also record the alloca instructions deleted here so that they aren't
/// subsequently handed to mem2reg to promote.
-void SROA::deleteDeadInstructions(SmallPtrSetImpl<AllocaInst*> &DeletedAllocas) {
+void SROA::deleteDeadInstructions(
+ SmallPtrSetImpl<AllocaInst *> &DeletedAllocas) {
while (!DeadInsts.empty()) {
Instruction *I = DeadInsts.pop_back_val();
DEBUG(dbgs() << "Deleting dead instruction: " << *I << "\n");
SmallVectorImpl<Instruction *> &Worklist,
SmallPtrSetImpl<Instruction *> &Visited) {
for (User *U : I.users())
- if (Visited.insert(cast<Instruction>(U)))
+ if (Visited.insert(cast<Instruction>(U)).second)
Worklist.push_back(cast<Instruction>(U));
}
DEBUG(dbgs() << "Promoting allocas with SSAUpdater...\n");
SSAUpdater SSA;
- DIBuilder DIB(*F.getParent());
+ DIBuilder DIB(*F.getParent(), /*AllowUnresolved*/ false);
SmallVector<Instruction *, 64> Insts;
// We need a worklist to walk the uses of each alloca.
BasicBlock &EntryBB = F.getEntryBlock();
for (BasicBlock::iterator I = EntryBB.begin(), E = std::prev(EntryBB.end());
- I != E; ++I)
+ I != E; ++I) {
if (AllocaInst *AI = dyn_cast<AllocaInst>(I))
Worklist.insert(AI);
+ else if (DbgDeclareInst *DDI = dyn_cast<DbgDeclareInst>(I))
+ if (auto AI = dyn_cast_or_null<AllocaInst>(DDI->getAddress()))
+ DbgDeclares.insert(std::make_pair(AI, DDI));
+ }
bool Changed = false;
// A set of deleted alloca instruction pointers which should be removed from
// Remove the deleted allocas from various lists so that we don't try to
// continue processing them.
if (!DeletedAllocas.empty()) {
- auto IsInSet = [&](AllocaInst *AI) {
- return DeletedAllocas.count(AI);
- };
+ auto IsInSet = [&](AllocaInst *AI) { return DeletedAllocas.count(AI); };
Worklist.remove_if(IsInSet);
PostPromotionWorklist.remove_if(IsInSet);
PromotableAllocas.erase(std::remove_if(PromotableAllocas.begin(),