index 147237edbcb586ba224d83c4650627c95eafcde7..73861866956df2ce1c37a0f3ea88f4a8717fd06b 100644 (file)
#include "llvm/ADT/SetVector.h"
#include "llvm/ADT/StringExtras.h"
#include "llvm/Analysis/AliasAnalysis.h"
-#include "llvm/Analysis/AssumptionTracker.h"
+#include "llvm/Analysis/AssumptionCache.h"
#include "llvm/Analysis/CallGraph.h"
#include "llvm/Analysis/CaptureTracking.h"
#include "llvm/Analysis/InstructionSimplify.h"
// Now we have a complete set of all metadata in the chains used to specify
// the noalias scopes and the lists of those scopes.
- SmallVector<MDNode *, 16> DummyNodes;
+ SmallVector<TempMDTuple, 16> DummyNodes;
DenseMap<const MDNode *, TrackingMDNodeRef> MDMap;
for (SetVector<const MDNode *>::iterator I = MD.begin(), IE = MD.end();
I != IE; ++I) {
- MDNode *Dummy = MDNode::getTemporary(CalledFunc->getContext(), None);
- DummyNodes.push_back(Dummy);
- MDMap[*I].reset(Dummy);
+ DummyNodes.push_back(MDTuple::getTemporary(CalledFunc->getContext(), None));
+ MDMap[*I].reset(DummyNodes.back().get());
}
// Create new metadata nodes to replace the dummy nodes, replacing old
}
MDNode *NewM = MDNode::get(CalledFunc->getContext(), NewOps);
- MDNodeFwdDecl *TempM = cast<MDNodeFwdDecl>(MDMap[*I]);
+ MDTuple *TempM = cast<MDTuple>(MDMap[*I]);
+ assert(TempM->isTemporary() && "Expected temporary node");
TempM->replaceAllUsesWith(NewM);
}
NI->setMetadata(LLVMContext::MD_noalias, M);
}
}
-
- // Now that everything has been replaced, delete the dummy nodes.
- for (unsigned i = 0, ie = DummyNodes.size(); i != ie; ++i)
- MDNode::deleteTemporary(DummyNodes[i]);
}
/// AddAliasScopeMetadata - If the inlined function has noalias arguments, then
DominatorTree DT;
bool DTCalculated = false;
- const Function *CalledFunc = CS.getCalledFunction();
- for (Function::const_arg_iterator I = CalledFunc->arg_begin(),
- E = CalledFunc->arg_end(); I != E; ++I) {
+ Function *CalledFunc = CS.getCalledFunction();
+ for (Function::arg_iterator I = CalledFunc->arg_begin(),
+ E = CalledFunc->arg_end();
+ I != E; ++I) {
unsigned Align = I->getType()->isPointerTy() ? I->getParamAlignment() : 0;
if (Align && !I->hasByValOrInAllocaAttr() && !I->hasNUses(0)) {
if (!DTCalculated) {
// If we can already prove the asserted alignment in the context of the
// caller, then don't bother inserting the assumption.
Value *Arg = CS.getArgument(I->getArgNo());
- if (getKnownAlignment(Arg, IFI.DL, IFI.AT, CS.getInstruction(),
- &DT) >= Align)
+ if (getKnownAlignment(Arg, IFI.DL,
+ &IFI.ACT->getAssumptionCache(*CalledFunc),
+ CS.getInstruction(), &DT) >= Align)
continue;
IRBuilder<>(CS.getInstruction()).CreateAlignmentAssumption(*IFI.DL, Arg,
PointerType *ArgTy = cast<PointerType>(Arg->getType());
Type *AggTy = ArgTy->getElementType();
+ Function *Caller = TheCall->getParent()->getParent();
+
// If the called function is readonly, then it could not mutate the caller's
// copy of the byval'd memory. In this case, it is safe to elide the copy and
// temporary.
// If the pointer is already known to be sufficiently aligned, or if we can
// round it up to a larger alignment, then we don't need a temporary.
- if (getOrEnforceKnownAlignment(Arg, ByValAlignment,
- IFI.DL, IFI.AT, TheCall) >= ByValAlignment)
+ if (getOrEnforceKnownAlignment(Arg, ByValAlignment, IFI.DL,
+ &IFI.ACT->getAssumptionCache(*Caller),
+ TheCall) >= ByValAlignment)
return Arg;
// Otherwise, we have to make a memcpy to get a safe alignment. This is bad
// pointer inside the callee).
Align = std::max(Align, ByValAlignment);
- Function *Caller = TheCall->getParent()->getParent();
-
Value *NewAlloca = new AllocaInst(AggTy, nullptr, Align, Arg->getName(),
&*Caller->begin()->begin());
IFI.StaticAllocas.push_back(cast<AllocaInst>(NewAlloca));
return false;
}
-/// updateInlinedAtInfo - Helper function used by fixupLineNumbers to
-/// recursively update InlinedAtEntry of a DebugLoc.
-static DebugLoc updateInlinedAtInfo(const DebugLoc &DL,
- const DebugLoc &InlinedAtDL,
- LLVMContext &Ctx) {
- if (MDNode *IA = DL.getInlinedAt(Ctx)) {
- DebugLoc NewInlinedAtDL
- = updateInlinedAtInfo(DebugLoc::getFromDILocation(IA), InlinedAtDL, Ctx);
- return DebugLoc::get(DL.getLine(), DL.getCol(), DL.getScope(Ctx),
- NewInlinedAtDL.getAsMDNode(Ctx));
+/// Rebuild the entire inlined-at chain for this instruction so that the top of
+/// the chain now is inlined-at the new call site.
+static DebugLoc
+updateInlinedAtInfo(DebugLoc DL, MDLocation *InlinedAtNode,
+ LLVMContext &Ctx,
+ DenseMap<const MDLocation *, MDLocation *> &IANodes) {
+ SmallVector<MDLocation*, 3> InlinedAtLocations;
+ MDLocation *Last = InlinedAtNode;
+ DebugLoc CurInlinedAt = DL;
+
+ // Gather all the inlined-at nodes
+ while (MDLocation *IA =
+ cast_or_null<MDLocation>(CurInlinedAt.getInlinedAt(Ctx))) {
+ // Skip any we've already built nodes for
+ if (MDLocation *Found = IANodes[IA]) {
+ Last = Found;
+ break;
+ }
+
+ InlinedAtLocations.push_back(IA);
+ CurInlinedAt = DebugLoc::getFromDILocation(IA);
}
- return DebugLoc::get(DL.getLine(), DL.getCol(), DL.getScope(Ctx),
- InlinedAtDL.getAsMDNode(Ctx));
+ // Starting from the top, rebuild the nodes to point to the new inlined-at
+ // location (then rebuilding the rest of the chain behind it) and update the
+ // map of already-constructed inlined-at nodes.
+ for (auto I = InlinedAtLocations.rbegin(), E = InlinedAtLocations.rend();
+ I != E; ++I) {
+ const MDLocation *MD = *I;
+ Last = IANodes[MD] = MDLocation::getDistinct(
+ Ctx, MD->getLine(), MD->getColumn(), MD->getScope(), Last);
+ }
+
+ // And finally create the normal location for this instruction, referring to
+ // the new inlined-at chain.
+ return DebugLoc::get(DL.getLine(), DL.getCol(), DL.getScope(Ctx), Last);
}
/// fixupLineNumbers - Update inlined instructions' line numbers to
if (TheCallDL.isUnknown())
return;
+ auto &Ctx = Fn->getContext();
+ auto *InlinedAtNode = cast<MDLocation>(TheCallDL.getAsMDNode(Ctx));
+
+ // Create a unique call site, not to be confused with any other call from the
+ // same location.
+ InlinedAtNode = MDLocation::getDistinct(
+ Ctx, InlinedAtNode->getLine(), InlinedAtNode->getColumn(),
+ InlinedAtNode->getScope(), InlinedAtNode->getInlinedAt());
+
+ // Cache the inlined-at nodes as they're built so they are reused, without
+ // this every instruction's inlined-at chain would become distinct from each
+ // other.
+ DenseMap<const MDLocation *, MDLocation *> IANodes;
+
for (; FI != Fn->end(); ++FI) {
for (BasicBlock::iterator BI = FI->begin(), BE = FI->end();
BI != BE; ++BI) {
BI->setDebugLoc(TheCallDL);
} else {
- BI->setDebugLoc(updateInlinedAtInfo(DL, TheCallDL, BI->getContext()));
+ BI->setDebugLoc(updateInlinedAtInfo(DL, InlinedAtNode, BI->getContext(), IANodes));
if (DbgValueInst *DVI = dyn_cast<DbgValueInst>(BI)) {
LLVMContext &Ctx = BI->getContext();
MDNode *InlinedAt = BI->getDebugLoc().getInlinedAt(Ctx);
DVI->setOperand(2, MetadataAsValue::get(
Ctx, createInlinedVariable(DVI->getVariable(),
InlinedAt, Ctx)));
+ } else if (DbgDeclareInst *DDI = dyn_cast<DbgDeclareInst>(BI)) {
+ LLVMContext &Ctx = BI->getContext();
+ MDNode *InlinedAt = BI->getDebugLoc().getInlinedAt(Ctx);
+ DDI->setOperand(1, MetadataAsValue::get(
+ Ctx, createInlinedVariable(DDI->getVariable(),
+ InlinedAt, Ctx)));
}
}
}
// FIXME: We could register any cloned assumptions instead of clearing the
// whole function's cache.
- if (IFI.AT)
- IFI.AT->forgetCachedAssumptions(Caller);
+ if (IFI.ACT)
+ IFI.ACT->getAssumptionCache(*Caller).clear();
}
// If there are any alloca instructions in the block that used to be the entry
// the entries are the same or undef). If so, remove the PHI so it doesn't
// block other optimizations.
if (PHI) {
- if (Value *V = SimplifyInstruction(PHI, IFI.DL, nullptr, nullptr, IFI.AT)) {
+ if (Value *V = SimplifyInstruction(PHI, IFI.DL, nullptr, nullptr,
+ &IFI.ACT->getAssumptionCache(*Caller))) {
PHI->replaceAllUsesWith(V);
PHI->eraseFromParent();
}