index 5464dbc4a8308b7608166037fe7a89e2426c625f..f0a9f2b1fcb354dc088555c534ab4cdb51100f90 100644 (file)
// This file implements inlining of a function into a call site, resolving
// parameters and the return value as appropriate.
//
-// The code in this file for handling inlines through invoke
-// instructions preserves semantics only under some assumptions about
-// the behavior of unwinders which correspond to gcc-style libUnwind
-// exception personality functions. Eventually the IR will be
-// improved to make this unnecessary, but until then, this code is
-// marked [LIBUNWIND].
-//
//===----------------------------------------------------------------------===//
#include "llvm/Transforms/Utils/Cloning.h"
-#include "llvm/Constants.h"
-#include "llvm/DerivedTypes.h"
-#include "llvm/Module.h"
-#include "llvm/Instructions.h"
-#include "llvm/IntrinsicInst.h"
-#include "llvm/Intrinsics.h"
-#include "llvm/Attributes.h"
+#include "llvm/ADT/SmallVector.h"
+#include "llvm/ADT/StringExtras.h"
#include "llvm/Analysis/CallGraph.h"
-#include "llvm/Analysis/DebugInfo.h"
#include "llvm/Analysis/InstructionSimplify.h"
-#include "llvm/Target/TargetData.h"
+#include "llvm/IR/Attributes.h"
+#include "llvm/IR/CallSite.h"
+#include "llvm/IR/CFG.h"
+#include "llvm/IR/Constants.h"
+#include "llvm/IR/DataLayout.h"
+#include "llvm/IR/DebugInfo.h"
+#include "llvm/IR/DerivedTypes.h"
+#include "llvm/IR/IRBuilder.h"
+#include "llvm/IR/Instructions.h"
+#include "llvm/IR/IntrinsicInst.h"
+#include "llvm/IR/Intrinsics.h"
+#include "llvm/IR/Module.h"
#include "llvm/Transforms/Utils/Local.h"
-#include "llvm/ADT/SmallVector.h"
-#include "llvm/ADT/StringExtras.h"
-#include "llvm/Support/CallSite.h"
-#include "llvm/Support/IRBuilder.h"
using namespace llvm;
-bool llvm::InlineFunction(CallInst *CI, InlineFunctionInfo &IFI) {
- return InlineFunction(CallSite(CI), IFI);
-}
-bool llvm::InlineFunction(InvokeInst *II, InlineFunctionInfo &IFI) {
- return InlineFunction(CallSite(II), IFI);
+bool llvm::InlineFunction(CallInst *CI, InlineFunctionInfo &IFI,
+ bool InsertLifetime) {
+ return InlineFunction(CallSite(CI), IFI, InsertLifetime);
}
-
-// FIXME: New EH - Remove the functions marked [LIBUNWIND] when new EH is
-// turned on.
-
-/// [LIBUNWIND] Look for an llvm.eh.exception call in the given block.
-static EHExceptionInst *findExceptionInBlock(BasicBlock *bb) {
- for (BasicBlock::iterator i = bb->begin(), e = bb->end(); i != e; i++) {
- EHExceptionInst *exn = dyn_cast<EHExceptionInst>(i);
- if (exn) return exn;
- }
-
- return 0;
-}
-
-/// [LIBUNWIND] Look for the 'best' llvm.eh.selector instruction for
-/// the given llvm.eh.exception call.
-static EHSelectorInst *findSelectorForException(EHExceptionInst *exn) {
- BasicBlock *exnBlock = exn->getParent();
-
- EHSelectorInst *outOfBlockSelector = 0;
- for (Instruction::use_iterator
- ui = exn->use_begin(), ue = exn->use_end(); ui != ue; ++ui) {
- EHSelectorInst *sel = dyn_cast<EHSelectorInst>(*ui);
- if (!sel) continue;
-
- // Immediately accept an eh.selector in the same block as the
- // excepton call.
- if (sel->getParent() == exnBlock) return sel;
-
- // Otherwise, use the first selector we see.
- if (!outOfBlockSelector) outOfBlockSelector = sel;
- }
-
- return outOfBlockSelector;
-}
-
-/// [LIBUNWIND] Find the (possibly absent) call to @llvm.eh.selector
-/// in the given landing pad. In principle, llvm.eh.exception is
-/// required to be in the landing pad; in practice, SplitCriticalEdge
-/// can break that invariant, and then inlining can break it further.
-/// There's a real need for a reliable solution here, but until that
-/// happens, we have some fragile workarounds here.
-static EHSelectorInst *findSelectorForLandingPad(BasicBlock *lpad) {
- // Look for an exception call in the actual landing pad.
- EHExceptionInst *exn = findExceptionInBlock(lpad);
- if (exn) return findSelectorForException(exn);
-
- // Okay, if that failed, look for one in an obvious successor. If
- // we find one, we'll fix the IR by moving things back to the
- // landing pad.
-
- bool dominates = true; // does the lpad dominate the exn call
- BasicBlock *nonDominated = 0; // if not, the first non-dominated block
- BasicBlock *lastDominated = 0; // and the block which branched to it
-
- BasicBlock *exnBlock = lpad;
-
- // We need to protect against lpads that lead into infinite loops.
- SmallPtrSet<BasicBlock*,4> visited;
- visited.insert(exnBlock);
-
- do {
- // We're not going to apply this hack to anything more complicated
- // than a series of unconditional branches, so if the block
- // doesn't terminate in an unconditional branch, just fail. More
- // complicated cases can arise when, say, sinking a call into a
- // split unwind edge and then inlining it; but that can do almost
- // *anything* to the CFG, including leaving the selector
- // completely unreachable. The only way to fix that properly is
- // to (1) prohibit transforms which move the exception or selector
- // values away from the landing pad, e.g. by producing them with
- // instructions that are pinned to an edge like a phi, or
- // producing them with not-really-instructions, and (2) making
- // transforms which split edges deal with that.
- BranchInst *branch = dyn_cast<BranchInst>(&exnBlock->back());
- if (!branch || branch->isConditional()) return 0;
-
- BasicBlock *successor = branch->getSuccessor(0);
-
- // Fail if we found an infinite loop.
- if (!visited.insert(successor)) return 0;
-
- // If the successor isn't dominated by exnBlock:
- if (!successor->getSinglePredecessor()) {
- // We don't want to have to deal with threading the exception
- // through multiple levels of phi, so give up if we've already
- // followed a non-dominating edge.
- if (!dominates) return 0;
-
- // Otherwise, remember this as a non-dominating edge.
- dominates = false;
- nonDominated = successor;
- lastDominated = exnBlock;
- }
-
- exnBlock = successor;
-
- // Can we stop here?
- exn = findExceptionInBlock(exnBlock);
- } while (!exn);
-
- // Look for a selector call for the exception we found.
- EHSelectorInst *selector = findSelectorForException(exn);
- if (!selector) return 0;
-
- // The easy case is when the landing pad still dominates the
- // exception call, in which case we can just move both calls back to
- // the landing pad.
- if (dominates) {
- selector->moveBefore(lpad->getFirstNonPHI());
- exn->moveBefore(selector);
- return selector;
- }
-
- // Otherwise, we have to split at the first non-dominating block.
- // The CFG looks basically like this:
- // lpad:
- // phis_0
- // insnsAndBranches_1
- // br label %nonDominated
- // nonDominated:
- // phis_2
- // insns_3
- // %exn = call i8* @llvm.eh.exception()
- // insnsAndBranches_4
- // %selector = call @llvm.eh.selector(i8* %exn, ...
- // We need to turn this into:
- // lpad:
- // phis_0
- // %exn0 = call i8* @llvm.eh.exception()
- // %selector0 = call @llvm.eh.selector(i8* %exn0, ...
- // insnsAndBranches_1
- // br label %split // from lastDominated
- // nonDominated:
- // phis_2 (without edge from lastDominated)
- // %exn1 = call i8* @llvm.eh.exception()
- // %selector1 = call i8* @llvm.eh.selector(i8* %exn1, ...
- // br label %split
- // split:
- // phis_2 (edge from lastDominated, edge from split)
- // %exn = phi ...
- // %selector = phi ...
- // insns_3
- // insnsAndBranches_4
-
- assert(nonDominated);
- assert(lastDominated);
-
- // First, make clones of the intrinsics to go in lpad.
- EHExceptionInst *lpadExn = cast<EHExceptionInst>(exn->clone());
- EHSelectorInst *lpadSelector = cast<EHSelectorInst>(selector->clone());
- lpadSelector->setArgOperand(0, lpadExn);
- lpadSelector->insertBefore(lpad->getFirstNonPHI());
- lpadExn->insertBefore(lpadSelector);
-
- // Split the non-dominated block.
- BasicBlock *split =
- nonDominated->splitBasicBlock(nonDominated->getFirstNonPHI(),
- nonDominated->getName() + ".lpad-fix");
-
- // Redirect the last dominated branch there.
- cast<BranchInst>(lastDominated->back()).setSuccessor(0, split);
-
- // Move the existing intrinsics to the end of the old block.
- selector->moveBefore(&nonDominated->back());
- exn->moveBefore(selector);
-
- Instruction *splitIP = &split->front();
-
- // For all the phis in nonDominated, make a new phi in split to join
- // that phi with the edge from lastDominated.
- for (BasicBlock::iterator
- i = nonDominated->begin(), e = nonDominated->end(); i != e; ++i) {
- PHINode *phi = dyn_cast<PHINode>(i);
- if (!phi) break;
-
- PHINode *splitPhi = PHINode::Create(phi->getType(), 2, phi->getName(),
- splitIP);
- phi->replaceAllUsesWith(splitPhi);
- splitPhi->addIncoming(phi, nonDominated);
- splitPhi->addIncoming(phi->removeIncomingValue(lastDominated),
- lastDominated);
- }
-
- // Make new phis for the exception and selector.
- PHINode *exnPhi = PHINode::Create(exn->getType(), 2, "", splitIP);
- exn->replaceAllUsesWith(exnPhi);
- selector->setArgOperand(0, exn); // except for this use
- exnPhi->addIncoming(exn, nonDominated);
- exnPhi->addIncoming(lpadExn, lastDominated);
-
- PHINode *selectorPhi = PHINode::Create(selector->getType(), 2, "", splitIP);
- selector->replaceAllUsesWith(selectorPhi);
- selectorPhi->addIncoming(selector, nonDominated);
- selectorPhi->addIncoming(lpadSelector, lastDominated);
-
- return lpadSelector;
+bool llvm::InlineFunction(InvokeInst *II, InlineFunctionInfo &IFI,
+ bool InsertLifetime) {
+ return InlineFunction(CallSite(II), IFI, InsertLifetime);
}
namespace {
/// A class for recording information about inlining through an invoke.
class InvokeInliningInfo {
- BasicBlock *OuterUnwindDest;
- EHSelectorInst *OuterSelector;
- BasicBlock *InnerUnwindDest;
- PHINode *InnerExceptionPHI;
- PHINode *InnerSelectorPHI;
+ BasicBlock *OuterResumeDest; ///< Destination of the invoke's unwind.
+ BasicBlock *InnerResumeDest; ///< Destination for the callee's resume.
+ LandingPadInst *CallerLPad; ///< LandingPadInst associated with the invoke.
+ PHINode *InnerEHValuesPHI; ///< PHI for EH values from landingpad insts.
SmallVector<Value*, 8> UnwindDestPHIValues;
- // FIXME: New EH - These will replace the analogous ones above.
- BasicBlock *OuterResumeDest; //< Destination of the invoke's unwind.
- BasicBlock *InnerResumeDest; //< Destination for the callee's resume.
- LandingPadInst *CallerLPad; //< LandingPadInst associated with the invoke.
- PHINode *InnerEHValuesPHI; //< PHI for EH values from landingpad insts.
-
public:
InvokeInliningInfo(InvokeInst *II)
- : OuterUnwindDest(II->getUnwindDest()), OuterSelector(0),
- InnerUnwindDest(0), InnerExceptionPHI(0), InnerSelectorPHI(0),
- OuterResumeDest(II->getUnwindDest()), InnerResumeDest(0),
- CallerLPad(0), InnerEHValuesPHI(0) {
+ : OuterResumeDest(II->getUnwindDest()), InnerResumeDest(nullptr),
+ CallerLPad(nullptr), InnerEHValuesPHI(nullptr) {
// If there are PHI nodes in the unwind destination block, we need to keep
// track of which values came into them from the invoke before removing
// the edge from this block.
llvm::BasicBlock *InvokeBB = II->getParent();
- BasicBlock::iterator I = OuterUnwindDest->begin();
+ BasicBlock::iterator I = OuterResumeDest->begin();
for (; isa<PHINode>(I); ++I) {
// Save the value to use for this edge.
PHINode *PHI = cast<PHINode>(I);
UnwindDestPHIValues.push_back(PHI->getIncomingValueForBlock(InvokeBB));
}
- // FIXME: With the new EH, this if/dyn_cast should be a 'cast'.
- if (LandingPadInst *LPI = dyn_cast<LandingPadInst>(I)) {
- CallerLPad = LPI;
- }
- }
-
- /// The outer unwind destination is the target of unwind edges
- /// introduced for calls within the inlined function.
- BasicBlock *getOuterUnwindDest() const {
- return OuterUnwindDest;
+ CallerLPad = cast<LandingPadInst>(I);
}
- EHSelectorInst *getOuterSelector() {
- if (!OuterSelector)
- OuterSelector = findSelectorForLandingPad(OuterUnwindDest);
- return OuterSelector;
+ /// getOuterResumeDest - The outer unwind destination is the target of
+ /// unwind edges introduced for calls within the inlined function.
+ BasicBlock *getOuterResumeDest() const {
+ return OuterResumeDest;
}
- BasicBlock *getInnerUnwindDest();
-
- // FIXME: New EH - Rename when new EH is turned on.
- BasicBlock *getInnerUnwindDestNewEH();
+ BasicBlock *getInnerResumeDest();
LandingPadInst *getLandingPadInst() const { return CallerLPad; }
- bool forwardEHResume(CallInst *call, BasicBlock *src);
-
/// forwardResume - Forward the 'resume' instruction to the caller's landing
/// pad block. When the landing pad block has only one predecessor, this is
/// a simple branch. When there is more than one predecessor, we need to
/// split the landing pad block after the landingpad instruction and jump
/// to there.
- void forwardResume(ResumeInst *RI);
+ void forwardResume(ResumeInst *RI,
+ SmallPtrSet<LandingPadInst*, 16> &InlinedLPads);
/// addIncomingPHIValuesFor - Add incoming-PHI values to the unwind
/// destination block for the given basic block, using the values for the
/// original invoke's source block.
void addIncomingPHIValuesFor(BasicBlock *BB) const {
- addIncomingPHIValuesForInto(BB, OuterUnwindDest);
+ addIncomingPHIValuesForInto(BB, OuterResumeDest);
}
void addIncomingPHIValuesForInto(BasicBlock *src, BasicBlock *dest) const {
};
}
-/// [LIBUNWIND] Get or create a target for the branch out of rewritten calls to
-/// llvm.eh.resume.
-BasicBlock *InvokeInliningInfo::getInnerUnwindDest() {
- if (InnerUnwindDest) return InnerUnwindDest;
-
- // Find and hoist the llvm.eh.exception and llvm.eh.selector calls
- // in the outer landing pad to immediately following the phis.
- EHSelectorInst *selector = getOuterSelector();
- if (!selector) return 0;
-
- // The call to llvm.eh.exception *must* be in the landing pad.
- Instruction *exn = cast<Instruction>(selector->getArgOperand(0));
- assert(exn->getParent() == OuterUnwindDest);
-
- // TODO: recognize when we've already done this, so that we don't
- // get a linear number of these when inlining calls into lots of
- // invokes with the same landing pad.
-
- // Do the hoisting.
- Instruction *splitPoint = exn->getParent()->getFirstNonPHI();
- assert(splitPoint != selector && "selector-on-exception dominance broken!");
- if (splitPoint == exn) {
- selector->removeFromParent();
- selector->insertAfter(exn);
- splitPoint = selector->getNextNode();
- } else {
- exn->moveBefore(splitPoint);
- selector->moveBefore(splitPoint);
- }
-
- // Split the landing pad.
- InnerUnwindDest = OuterUnwindDest->splitBasicBlock(splitPoint,
- OuterUnwindDest->getName() + ".body");
-
- // The number of incoming edges we expect to the inner landing pad.
- const unsigned phiCapacity = 2;
-
- // Create corresponding new phis for all the phis in the outer landing pad.
- BasicBlock::iterator insertPoint = InnerUnwindDest->begin();
- BasicBlock::iterator I = OuterUnwindDest->begin();
- for (unsigned i = 0, e = UnwindDestPHIValues.size(); i != e; ++i, ++I) {
- PHINode *outerPhi = cast<PHINode>(I);
- PHINode *innerPhi = PHINode::Create(outerPhi->getType(), phiCapacity,
- outerPhi->getName() + ".lpad-body",
- insertPoint);
- outerPhi->replaceAllUsesWith(innerPhi);
- innerPhi->addIncoming(outerPhi, OuterUnwindDest);
- }
-
- // Create a phi for the exception value...
- InnerExceptionPHI = PHINode::Create(exn->getType(), phiCapacity,
- "exn.lpad-body", insertPoint);
- exn->replaceAllUsesWith(InnerExceptionPHI);
- selector->setArgOperand(0, exn); // restore this use
- InnerExceptionPHI->addIncoming(exn, OuterUnwindDest);
-
- // ...and the selector.
- InnerSelectorPHI = PHINode::Create(selector->getType(), phiCapacity,
- "selector.lpad-body", insertPoint);
- selector->replaceAllUsesWith(InnerSelectorPHI);
- InnerSelectorPHI->addIncoming(selector, OuterUnwindDest);
-
- // All done.
- return InnerUnwindDest;
-}
-
-/// [LIBUNWIND] Try to forward the given call, which logically occurs
-/// at the end of the given block, as a branch to the inner unwind
-/// block. Returns true if the call was forwarded.
-bool InvokeInliningInfo::forwardEHResume(CallInst *call, BasicBlock *src) {
- // First, check whether this is a call to the intrinsic.
- Function *fn = dyn_cast<Function>(call->getCalledValue());
- if (!fn || fn->getName() != "llvm.eh.resume")
- return false;
-
- // At this point, we need to return true on all paths, because
- // otherwise we'll construct an invoke of the intrinsic, which is
- // not well-formed.
-
- // Try to find or make an inner unwind dest, which will fail if we
- // can't find a selector call for the outer unwind dest.
- BasicBlock *dest = getInnerUnwindDest();
- bool hasSelector = (dest != 0);
-
- // If we failed, just use the outer unwind dest, dropping the
- // exception and selector on the floor.
- if (!hasSelector)
- dest = OuterUnwindDest;
-
- // Make a branch.
- BranchInst::Create(dest, src);
-
- // Update the phis in the destination. They were inserted in an
- // order which makes this work.
- addIncomingPHIValuesForInto(src, dest);
-
- if (hasSelector) {
- InnerExceptionPHI->addIncoming(call->getArgOperand(0), src);
- InnerSelectorPHI->addIncoming(call->getArgOperand(1), src);
- }
-
- return true;
-}
-
-/// Get or create a target for the branch from ResumeInsts.
-BasicBlock *InvokeInliningInfo::getInnerUnwindDestNewEH() {
- // FIXME: New EH - rename this function when new EH is turned on.
+/// getInnerResumeDest - Get or create a target for the branch from ResumeInsts.
+BasicBlock *InvokeInliningInfo::getInnerResumeDest() {
if (InnerResumeDest) return InnerResumeDest;
// Split the landing pad.
/// block. When the landing pad block has only one predecessor, this is a simple
/// branch. When there is more than one predecessor, we need to split the
/// landing pad block after the landingpad instruction and jump to there.
-void InvokeInliningInfo::forwardResume(ResumeInst *RI) {
- BasicBlock *Dest = getInnerUnwindDestNewEH();
+void InvokeInliningInfo::forwardResume(ResumeInst *RI,
+ SmallPtrSet<LandingPadInst*, 16> &InlinedLPads) {
+ BasicBlock *Dest = getInnerResumeDest();
BasicBlock *Src = RI->getParent();
BranchInst::Create(Dest, Src);
RI->eraseFromParent();
}
-/// [LIBUNWIND] Check whether this selector is "only cleanups":
-/// call i32 @llvm.eh.selector(blah, blah, i32 0)
-static bool isCleanupOnlySelector(EHSelectorInst *selector) {
- if (selector->getNumArgOperands() != 3) return false;
- ConstantInt *val = dyn_cast<ConstantInt>(selector->getArgOperand(2));
- return (val && val->isZero());
-}
-
/// HandleCallsInBlockInlinedThroughInvoke - When we inline a basic block into
/// an invoke, we have to turn all of the calls that can throw into
/// invokes. This function analyze BB to see if there are any calls, and if so,
/// it rewrites them to be invokes that jump to InvokeDest and fills in the PHI
/// nodes in that block with the values specified in InvokeDestPHIValues.
-///
-/// Returns true to indicate that the next block should be skipped.
-static bool HandleCallsInBlockInlinedThroughInvoke(BasicBlock *BB,
+static void HandleCallsInBlockInlinedThroughInvoke(BasicBlock *BB,
InvokeInliningInfo &Invoke) {
- LandingPadInst *LPI = Invoke.getLandingPadInst();
-
for (BasicBlock::iterator BBI = BB->begin(), E = BB->end(); BBI != E; ) {
Instruction *I = BBI++;
- if (LPI) // FIXME: New EH - This won't be NULL in the new EH.
- if (LandingPadInst *L = dyn_cast<LandingPadInst>(I)) {
- unsigned NumClauses = LPI->getNumClauses();
- L->reserveClauses(NumClauses);
- for (unsigned i = 0; i != NumClauses; ++i)
- L->addClause(LPI->getClause(i));
- }
-
// We only need to check for function calls: inlined invoke
// instructions require no special handling.
CallInst *CI = dyn_cast<CallInst>(I);
- if (CI == 0) continue;
-
- // LIBUNWIND: merge selector instructions.
- if (EHSelectorInst *Inner = dyn_cast<EHSelectorInst>(CI)) {
- EHSelectorInst *Outer = Invoke.getOuterSelector();
- if (!Outer) continue;
-
- bool innerIsOnlyCleanup = isCleanupOnlySelector(Inner);
- bool outerIsOnlyCleanup = isCleanupOnlySelector(Outer);
-
- // If both selectors contain only cleanups, we don't need to do
- // anything. TODO: this is really just a very specific instance
- // of a much more general optimization.
- if (innerIsOnlyCleanup && outerIsOnlyCleanup) continue;
-
- // Otherwise, we just append the outer selector to the inner selector.
- SmallVector<Value*, 16> NewSelector;
- for (unsigned i = 0, e = Inner->getNumArgOperands(); i != e; ++i)
- NewSelector.push_back(Inner->getArgOperand(i));
- for (unsigned i = 2, e = Outer->getNumArgOperands(); i != e; ++i)
- NewSelector.push_back(Outer->getArgOperand(i));
-
- CallInst *NewInner =
- IRBuilder<>(Inner).CreateCall(Inner->getCalledValue(), NewSelector);
- // No need to copy attributes, calling convention, etc.
- NewInner->takeName(Inner);
- Inner->replaceAllUsesWith(NewInner);
- Inner->eraseFromParent();
- continue;
- }
-
+
// If this call cannot unwind, don't convert it to an invoke.
- if (CI->doesNotThrow())
+ // Inline asm calls cannot throw.
+ if (!CI || CI->doesNotThrow() || isa<InlineAsm>(CI->getCalledValue()))
continue;
-
- // Convert this function call into an invoke instruction.
- // First, split the basic block.
+
+ // Convert this function call into an invoke instruction. First, split the
+ // basic block.
BasicBlock *Split = BB->splitBasicBlock(CI, CI->getName()+".noexc");
// Delete the unconditional branch inserted by splitBasicBlock
BB->getInstList().pop_back();
- // LIBUNWIND: If this is a call to @llvm.eh.resume, just branch
- // directly to the new landing pad.
- if (Invoke.forwardEHResume(CI, BB)) {
- // TODO: 'Split' is now unreachable; clean it up.
-
- // We want to leave the original call intact so that the call
- // graph and other structures won't get misled. We also have to
- // avoid processing the next block, or we'll iterate here forever.
- return true;
- }
-
- // Otherwise, create the new invoke instruction.
+ // Create the new invoke instruction.
ImmutableCallSite CS(CI);
SmallVector<Value*, 8> InvokeArgs(CS.arg_begin(), CS.arg_end());
- InvokeInst *II =
- InvokeInst::Create(CI->getCalledValue(), Split,
- Invoke.getOuterUnwindDest(),
- InvokeArgs, CI->getName(), BB);
+ InvokeInst *II = InvokeInst::Create(CI->getCalledValue(), Split,
+ Invoke.getOuterResumeDest(),
+ InvokeArgs, CI->getName(), BB);
+ II->setDebugLoc(CI->getDebugLoc());
II->setCallingConv(CI->getCallingConv());
II->setAttributes(CI->getAttributes());
// updates the CallGraph if present, because it uses a WeakVH.
CI->replaceAllUsesWith(II);
- Split->getInstList().pop_front(); // Delete the original call
+ // Delete the original call
+ Split->getInstList().pop_front();
- // Update any PHI nodes in the exceptional block to indicate that
- // there is now a new entry in them.
+ // Update any PHI nodes in the exceptional block to indicate that there is
+ // now a new entry in them.
Invoke.addIncomingPHIValuesFor(BB);
- return false;
+ return;
}
-
- return false;
}
-
/// HandleInlinedInvoke - If we inlined an invoke site, we need to convert calls
-/// in the body of the inlined function into invokes and turn unwind
-/// instructions into branches to the invoke unwind dest.
+/// in the body of the inlined function into invokes.
///
/// II is the invoke instruction being inlined. FirstNewBlock is the first
/// block of the inlined code (the last block is the end of the function),
// The inlined code is currently at the end of the function, scan from the
// start of the inlined code to its end, checking for stuff we need to
- // rewrite. If the code doesn't have calls or unwinds, we know there is
- // nothing to rewrite.
- if (!InlinedCodeInfo.ContainsCalls && !InlinedCodeInfo.ContainsUnwinds) {
- // Now that everything is happy, we have one final detail. The PHI nodes in
- // the exception destination block still have entries due to the original
- // invoke instruction. Eliminate these entries (which might even delete the
- // PHI node) now.
- InvokeDest->removePredecessor(II->getParent());
- return;
+ // rewrite.
+ InvokeInliningInfo Invoke(II);
+
+ // Get all of the inlined landing pad instructions.
+ SmallPtrSet<LandingPadInst*, 16> InlinedLPads;
+ for (Function::iterator I = FirstNewBlock, E = Caller->end(); I != E; ++I)
+ if (InvokeInst *II = dyn_cast<InvokeInst>(I->getTerminator()))
+ InlinedLPads.insert(II->getLandingPadInst());
+
+ // Append the clauses from the outer landing pad instruction into the inlined
+ // landing pad instructions.
+ LandingPadInst *OuterLPad = Invoke.getLandingPadInst();
+ for (SmallPtrSet<LandingPadInst*, 16>::iterator I = InlinedLPads.begin(),
+ E = InlinedLPads.end(); I != E; ++I) {
+ LandingPadInst *InlinedLPad = *I;
+ unsigned OuterNum = OuterLPad->getNumClauses();
+ InlinedLPad->reserveClauses(OuterNum);
+ for (unsigned OuterIdx = 0; OuterIdx != OuterNum; ++OuterIdx)
+ InlinedLPad->addClause(OuterLPad->getClause(OuterIdx));
+ if (OuterLPad->isCleanup())
+ InlinedLPad->setCleanup(true);
}
- InvokeInliningInfo Invoke(II);
-
for (Function::iterator BB = FirstNewBlock, E = Caller->end(); BB != E; ++BB){
if (InlinedCodeInfo.ContainsCalls)
- if (HandleCallsInBlockInlinedThroughInvoke(BB, Invoke)) {
- // Honor a request to skip the next block. We don't need to
- // consider UnwindInsts in this case either.
- ++BB;
- continue;
- }
-
- if (UnwindInst *UI = dyn_cast<UnwindInst>(BB->getTerminator())) {
- // An UnwindInst requires special handling when it gets inlined into an
- // invoke site. Once this happens, we know that the unwind would cause
- // a control transfer to the invoke exception destination, so we can
- // transform it into a direct branch to the exception destination.
- BranchInst::Create(InvokeDest, UI);
+ HandleCallsInBlockInlinedThroughInvoke(BB, Invoke);
- // Delete the unwind instruction!
- UI->eraseFromParent();
-
- // Update any PHI nodes in the exceptional block to indicate that
- // there is now a new entry in them.
- Invoke.addIncomingPHIValuesFor(BB);
- }
-
- if (ResumeInst *RI = dyn_cast<ResumeInst>(BB->getTerminator())) {
- Invoke.forwardResume(RI);
- }
+ // Forward any resumes that are remaining here.
+ if (ResumeInst *RI = dyn_cast<ResumeInst>(BB->getTerminator()))
+ Invoke.forwardResume(RI, InlinedLPads);
}
// Now that everything is happy, we have one final detail. The PHI nodes in
// the exception destination block still have entries due to the original
- // invoke instruction. Eliminate these entries (which might even delete the
+ // invoke instruction. Eliminate these entries (which might even delete the
// PHI node) now.
InvokeDest->removePredecessor(II->getParent());
}
ValueToValueMapTy::iterator VMI = VMap.find(OrigCall);
// Only copy the edge if the call was inlined!
- if (VMI == VMap.end() || VMI->second == 0)
+ if (VMI == VMap.end() || VMI->second == nullptr)
continue;
// If the call was inlined, but then constant folded, there is no edge to
// add. Check for this case.
Instruction *NewCall = dyn_cast<Instruction>(VMI->second);
- if (NewCall == 0) continue;
+ if (!NewCall) continue;
// Remember that this call site got inlined for the client of
// InlineFunction.
// happens, set the callee of the new call site to a more precise
// destination. This can also happen if the call graph node of the caller
// was just unnecessarily imprecise.
- if (I->second->getFunction() == 0)
+ if (!I->second->getFunction())
if (Function *F = CallSite(NewCall).getCalledFunction()) {
// Indirect call site resolved to direct call.
CallerNode->addCalledFunction(CallSite(NewCall), CG[F]);
CallerNode->removeCallEdgeFor(CS);
}
+static void HandleByValArgumentInit(Value *Dst, Value *Src, Module *M,
+ BasicBlock *InsertBlock,
+ InlineFunctionInfo &IFI) {
+ LLVMContext &Context = Src->getContext();
+ Type *VoidPtrTy = Type::getInt8PtrTy(Context);
+ Type *AggTy = cast<PointerType>(Src->getType())->getElementType();
+ Type *Tys[3] = { VoidPtrTy, VoidPtrTy, Type::getInt64Ty(Context) };
+ Function *MemCpyFn = Intrinsic::getDeclaration(M, Intrinsic::memcpy, Tys);
+ IRBuilder<> builder(InsertBlock->begin());
+ Value *DstCast = builder.CreateBitCast(Dst, VoidPtrTy, "tmp");
+ Value *SrcCast = builder.CreateBitCast(Src, VoidPtrTy, "tmp");
+
+ Value *Size;
+ if (IFI.DL == nullptr)
+ Size = ConstantExpr::getSizeOf(AggTy);
+ else
+ Size = ConstantInt::get(Type::getInt64Ty(Context),
+ IFI.DL->getTypeStoreSize(AggTy));
+
+ // Always generate a memcpy of alignment 1 here because we don't know
+ // the alignment of the src pointer. Other optimizations can infer
+ // better alignment.
+ Value *CallArgs[] = {
+ DstCast, SrcCast, Size,
+ ConstantInt::get(Type::getInt32Ty(Context), 1),
+ ConstantInt::getFalse(Context) // isVolatile
+ };
+ builder.CreateCall(MemCpyFn, CallArgs);
+}
+
/// HandleByValArgument - When inlining a call site that has a byval argument,
/// we have to make the implicit memcpy explicit by adding it.
static Value *HandleByValArgument(Value *Arg, Instruction *TheCall,
const Function *CalledFunc,
InlineFunctionInfo &IFI,
unsigned ByValAlignment) {
- Type *AggTy = cast<PointerType>(Arg->getType())->getElementType();
+ PointerType *ArgTy = cast<PointerType>(Arg->getType());
+ Type *AggTy = ArgTy->getElementType();
// If the called function is readonly, then it could not mutate the caller's
// copy of the byval'd memory. In this case, it is safe to elide the copy and
// If the pointer is already known to be sufficiently aligned, or if we can
// round it up to a larger alignment, then we don't need a temporary.
if (getOrEnforceKnownAlignment(Arg, ByValAlignment,
- IFI.TD) >= ByValAlignment)
+ IFI.DL) >= ByValAlignment)
return Arg;
// Otherwise, we have to make a memcpy to get a safe alignment. This is bad
// for code quality, but rarely happens and is required for correctness.
}
-
- LLVMContext &Context = Arg->getContext();
- Type *VoidPtrTy = Type::getInt8PtrTy(Context);
-
- // Create the alloca. If we have TargetData, use nice alignment.
+ // Create the alloca. If we have DataLayout, use nice alignment.
unsigned Align = 1;
- if (IFI.TD)
- Align = IFI.TD->getPrefTypeAlignment(AggTy);
+ if (IFI.DL)
+ Align = IFI.DL->getPrefTypeAlignment(AggTy);
// If the byval had an alignment specified, we *must* use at least that
// alignment, as it is required by the byval argument (and uses of the
Function *Caller = TheCall->getParent()->getParent();
- Value *NewAlloca = new AllocaInst(AggTy, 0, Align, Arg->getName(),
+ Value *NewAlloca = new AllocaInst(AggTy, nullptr, Align, Arg->getName(),
&*Caller->begin()->begin());
- // Emit a memcpy.
- Type *Tys[3] = {VoidPtrTy, VoidPtrTy, Type::getInt64Ty(Context)};
- Function *MemCpyFn = Intrinsic::getDeclaration(Caller->getParent(),
- Intrinsic::memcpy,
- Tys);
- Value *DestCast = new BitCastInst(NewAlloca, VoidPtrTy, "tmp", TheCall);
- Value *SrcCast = new BitCastInst(Arg, VoidPtrTy, "tmp", TheCall);
-
- Value *Size;
- if (IFI.TD == 0)
- Size = ConstantExpr::getSizeOf(AggTy);
- else
- Size = ConstantInt::get(Type::getInt64Ty(Context),
- IFI.TD->getTypeStoreSize(AggTy));
-
- // Always generate a memcpy of alignment 1 here because we don't know
- // the alignment of the src pointer. Other optimizations can infer
- // better alignment.
- Value *CallArgs[] = {
- DestCast, SrcCast, Size,
- ConstantInt::get(Type::getInt32Ty(Context), 1),
- ConstantInt::getFalse(Context) // isVolatile
- };
- IRBuilder<>(TheCall).CreateCall(MemCpyFn, CallArgs);
+ IFI.StaticAllocas.push_back(cast<AllocaInst>(NewAlloca));
// Uses of the argument in the function should use our new alloca
// instead.
// isUsedByLifetimeMarker - Check whether this Value is used by a lifetime
// intrinsic.
static bool isUsedByLifetimeMarker(Value *V) {
- for (Value::use_iterator UI = V->use_begin(), UE = V->use_end(); UI != UE;
- ++UI) {
- if (IntrinsicInst *II = dyn_cast<IntrinsicInst>(*UI)) {
+ for (User *U : V->users()) {
+ if (IntrinsicInst *II = dyn_cast<IntrinsicInst>(U)) {
switch (II->getIntrinsicID()) {
default: break;
case Intrinsic::lifetime_start:
// hasLifetimeMarkers - Check whether the given alloca already has
// lifetime.start or lifetime.end intrinsics.
static bool hasLifetimeMarkers(AllocaInst *AI) {
- Type *Int8PtrTy = Type::getInt8PtrTy(AI->getType()->getContext());
- if (AI->getType() == Int8PtrTy)
+ Type *Ty = AI->getType();
+ Type *Int8PtrTy = Type::getInt8PtrTy(Ty->getContext(),
+ Ty->getPointerAddressSpace());
+ if (Ty == Int8PtrTy)
return isUsedByLifetimeMarker(AI);
// Do a scan to find all the casts to i8*.
- for (Value::use_iterator I = AI->use_begin(), E = AI->use_end(); I != E;
- ++I) {
- if (I->getType() != Int8PtrTy) continue;
- if (I->stripPointerCasts() != AI) continue;
- if (isUsedByLifetimeMarker(*I))
+ for (User *U : AI->users()) {
+ if (U->getType() != Int8PtrTy) continue;
+ if (U->stripPointerCasts() != AI) continue;
+ if (isUsedByLifetimeMarker(U))
return true;
}
return false;
}
-/// updateInlinedAtInfo - Helper function used by fixupLineNumbers to recursively
-/// update InlinedAtEntry of a DebugLoc.
+/// updateInlinedAtInfo - Helper function used by fixupLineNumbers to
+/// recursively update InlinedAtEntry of a DebugLoc.
static DebugLoc updateInlinedAtInfo(const DebugLoc &DL,
const DebugLoc &InlinedAtDL,
LLVMContext &Ctx) {
return DebugLoc::get(DL.getLine(), DL.getCol(), DL.getScope(Ctx),
NewInlinedAtDL.getAsMDNode(Ctx));
}
-
+
return DebugLoc::get(DL.getLine(), DL.getCol(), DL.getScope(Ctx),
InlinedAtDL.getAsMDNode(Ctx));
}
-
/// fixupLineNumbers - Update inlined instructions' line numbers to
/// to encode location where these instructions are inlined.
static void fixupLineNumbers(Function *Fn, Function::iterator FI,
- Instruction *TheCall) {
+ Instruction *TheCall) {
DebugLoc TheCallDL = TheCall->getDebugLoc();
if (TheCallDL.isUnknown())
return;
for (BasicBlock::iterator BI = FI->begin(), BE = FI->end();
BI != BE; ++BI) {
DebugLoc DL = BI->getDebugLoc();
- if (!DL.isUnknown()) {
+ if (DL.isUnknown()) {
+ // If the inlined instruction has no line number, make it look as if it
+ // originates from the call location. This is important for
+ // ((__always_inline__, __nodebug__)) functions which must use caller
+ // location for all instructions in their function body.
+ BI->setDebugLoc(TheCallDL);
+ } else {
BI->setDebugLoc(updateInlinedAtInfo(DL, TheCallDL, BI->getContext()));
if (DbgValueInst *DVI = dyn_cast<DbgValueInst>(BI)) {
LLVMContext &Ctx = BI->getContext();
}
}
-// InlineFunction - This function inlines the called function into the basic
-// block of the caller. This returns false if it is not possible to inline this
-// call. The program is still in a well defined state if this occurs though.
-//
-// Note that this only does one level of inlining. For example, if the
-// instruction 'call B' is inlined, and 'B' calls 'C', then the call to 'C' now
-// exists in the instruction stream. Similarly this will inline a recursive
-// function by one level.
-//
-bool llvm::InlineFunction(CallSite CS, InlineFunctionInfo &IFI) {
+/// Returns a musttail call instruction if one immediately precedes the given
+/// return instruction with an optional bitcast instruction between them.
+static CallInst *getPrecedingMustTailCall(ReturnInst *RI) {
+ Instruction *Prev = RI->getPrevNode();
+ if (!Prev)
+ return nullptr;
+
+ if (Value *RV = RI->getReturnValue()) {
+ if (RV != Prev)
+ return nullptr;
+
+ // Look through the optional bitcast.
+ if (auto *BI = dyn_cast<BitCastInst>(Prev)) {
+ RV = BI->getOperand(0);
+ Prev = BI->getPrevNode();
+ if (!Prev || RV != Prev)
+ return nullptr;
+ }
+ }
+
+ if (auto *CI = dyn_cast<CallInst>(Prev)) {
+ if (CI->isMustTailCall())
+ return CI;
+ }
+ return nullptr;
+}
+
+/// InlineFunction - This function inlines the called function into the basic
+/// block of the caller. This returns false if it is not possible to inline
+/// this call. The program is still in a well defined state if this occurs
+/// though.
+///
+/// Note that this only does one level of inlining. For example, if the
+/// instruction 'call B' is inlined, and 'B' calls 'C', then the call to 'C' now
+/// exists in the instruction stream. Similarly this will inline a recursive
+/// function by one level.
+bool llvm::InlineFunction(CallSite CS, InlineFunctionInfo &IFI,
+ bool InsertLifetime) {
Instruction *TheCall = CS.getInstruction();
- LLVMContext &Context = TheCall->getContext();
assert(TheCall->getParent() && TheCall->getParent()->getParent() &&
"Instruction not in function!");
IFI.reset();
const Function *CalledFunc = CS.getCalledFunction();
- if (CalledFunc == 0 || // Can't inline external function or indirect
+ if (!CalledFunc || // Can't inline external function or indirect
CalledFunc->isDeclaration() || // call, or call to a vararg function!
CalledFunc->getFunctionType()->isVarArg()) return false;
- // If the call to the callee is not a tail call, we must clear the 'tail'
- // flags on any calls that we inline.
- bool MustClearTailCallFlags =
- !(isa<CallInst>(TheCall) && cast<CallInst>(TheCall)->isTailCall());
-
// If the call to the callee cannot throw, set the 'nounwind' flag on any
// calls that we inline.
bool MarkNoUnwind = CS.doesNotThrow();
return false;
}
- // Find the personality function used by the landing pads of the caller. If it
- // exists, then check to see that it matches the personality function used in
- // the callee.
- for (Function::const_iterator
- I = Caller->begin(), E = Caller->end(); I != E; ++I)
+ // Get the personality function from the callee if it contains a landing pad.
+ Value *CalleePersonality = nullptr;
+ for (Function::const_iterator I = CalledFunc->begin(), E = CalledFunc->end();
+ I != E; ++I)
if (const InvokeInst *II = dyn_cast<InvokeInst>(I->getTerminator())) {
const BasicBlock *BB = II->getUnwindDest();
- // FIXME: This 'isa' here should become go away once the new EH system is
- // in place.
- if (!isa<LandingPadInst>(BB->getFirstNonPHI()))
- continue;
- const LandingPadInst *LP = cast<LandingPadInst>(BB->getFirstNonPHI());
- const Value *CallerPersFn = LP->getPersonalityFn();
-
- // If the personality functions match, then we can perform the
- // inlining. Otherwise, we can't inline.
- // TODO: This isn't 100% true. Some personality functions are proper
- // supersets of others and can be used in place of the other.
- for (Function::const_iterator
- I = CalledFunc->begin(), E = CalledFunc->end(); I != E; ++I)
- if (const InvokeInst *II = dyn_cast<InvokeInst>(I->getTerminator())) {
- const BasicBlock *BB = II->getUnwindDest();
- // FIXME: This 'if/dyn_cast' here should become a normal 'cast' once
- // the new EH system is in place.
- if (const LandingPadInst *LP =
- dyn_cast<LandingPadInst>(BB->getFirstNonPHI()))
- if (CallerPersFn != LP->getPersonalityFn())
- return false;
- break;
- }
-
+ const LandingPadInst *LP = BB->getLandingPadInst();
+ CalleePersonality = LP->getPersonalityFn();
break;
}
+ // Find the personality function used by the landing pads of the caller. If it
+ // exists, then check to see that it matches the personality function used in
+ // the callee.
+ if (CalleePersonality) {
+ for (Function::const_iterator I = Caller->begin(), E = Caller->end();
+ I != E; ++I)
+ if (const InvokeInst *II = dyn_cast<InvokeInst>(I->getTerminator())) {
+ const BasicBlock *BB = II->getUnwindDest();
+ const LandingPadInst *LP = BB->getLandingPadInst();
+
+ // If the personality functions match, then we can perform the
+ // inlining. Otherwise, we can't inline.
+ // TODO: This isn't 100% true. Some personality functions are proper
+ // supersets of others and can be used in place of the other.
+ if (LP->getPersonalityFn() != CalleePersonality)
+ return false;
+
+ break;
+ }
+ }
+
// Get an iterator to the last basic block in the function, which will have
// the new function inlined after it.
- //
Function::iterator LastBlock = &Caller->back();
// Make sure to capture all of the return instructions from the cloned
{ // Scope to destroy VMap after cloning.
ValueToValueMapTy VMap;
+ // Keep a list of pair (dst, src) to emit byval initializations.
+ SmallVector<std::pair<Value*, Value*>, 4> ByValInit;
assert(CalledFunc->arg_size() == CS.arg_size() &&
"No varargs calls can be inlined!");
// by them explicit. However, we don't do this if the callee is readonly
// or readnone, because the copy would be unneeded: the callee doesn't
// modify the struct.
- if (CalledFunc->paramHasAttr(ArgNo+1, Attribute::ByVal)) {
+ if (CS.isByValArgument(ArgNo)) {
ActualArg = HandleByValArgument(ActualArg, TheCall, CalledFunc, IFI,
CalledFunc->getParamAlignment(ArgNo+1));
-
- // Calls that we inline may use the new alloca, so we need to clear
- // their 'tail' flags if HandleByValArgument introduced a new alloca and
- // the callee has calls.
- MustClearTailCallFlags |= ActualArg != *AI;
+ if (ActualArg != *AI)
+ ByValInit.push_back(std::make_pair(ActualArg, (Value*) *AI));
}
VMap[I] = ActualArg;
// happy with whatever the cloner can do.
CloneAndPruneFunctionInto(Caller, CalledFunc, VMap,
/*ModuleLevelChanges=*/false, Returns, ".i",
- &InlinedFunctionInfo, IFI.TD, TheCall);
+ &InlinedFunctionInfo, IFI.DL, TheCall);
// Remember the first block that is newly cloned over.
FirstNewBlock = LastBlock; ++FirstNewBlock;
+ // Inject byval arguments initialization.
+ for (std::pair<Value*, Value*> &Init : ByValInit)
+ HandleByValArgumentInit(Init.first, Init.second, Caller->getParent(),
+ FirstNewBlock, IFI);
+
// Update the callgraph if requested.
if (IFI.CG)
UpdateCallGraphAfterInlining(CS, FirstNewBlock, VMap, IFI);
// block for the callee, move them to the entry block of the caller. First
// calculate which instruction they should be inserted before. We insert the
// instructions at the end of the current alloca list.
- //
{
BasicBlock::iterator InsertPoint = Caller->begin()->begin();
for (BasicBlock::iterator I = FirstNewBlock->begin(),
E = FirstNewBlock->end(); I != E; ) {
AllocaInst *AI = dyn_cast<AllocaInst>(I++);
- if (AI == 0) continue;
+ if (!AI) continue;
// If the alloca is now dead, remove it. This often occurs due to code
// specialization.
}
}
+ bool InlinedMustTailCalls = false;
+ if (InlinedFunctionInfo.ContainsCalls) {
+ CallInst::TailCallKind CallSiteTailKind = CallInst::TCK_None;
+ if (CallInst *CI = dyn_cast<CallInst>(TheCall))
+ CallSiteTailKind = CI->getTailCallKind();
+
+ for (Function::iterator BB = FirstNewBlock, E = Caller->end(); BB != E;
+ ++BB) {
+ for (Instruction &I : *BB) {
+ CallInst *CI = dyn_cast<CallInst>(&I);
+ if (!CI)
+ continue;
+
+ // We need to reduce the strength of any inlined tail calls. For
+ // musttail, we have to avoid introducing potential unbounded stack
+ // growth. For example, if functions 'f' and 'g' are mutually recursive
+ // with musttail, we can inline 'g' into 'f' so long as we preserve
+ // musttail on the cloned call to 'f'. If either the inlined call site
+ // or the cloned call site is *not* musttail, the program already has
+ // one frame of stack growth, so it's safe to remove musttail. Here is
+ // a table of example transformations:
+ //
+ // f -> musttail g -> musttail f ==> f -> musttail f
+ // f -> musttail g -> tail f ==> f -> tail f
+ // f -> g -> musttail f ==> f -> f
+ // f -> g -> tail f ==> f -> f
+ CallInst::TailCallKind ChildTCK = CI->getTailCallKind();
+ ChildTCK = std::min(CallSiteTailKind, ChildTCK);
+ CI->setTailCallKind(ChildTCK);
+ InlinedMustTailCalls |= CI->isMustTailCall();
+
+ // Calls inlined through a 'nounwind' call site should be marked
+ // 'nounwind'.
+ if (MarkNoUnwind)
+ CI->setDoesNotThrow();
+ }
+ }
+ }
+
// Leave lifetime markers for the static alloca's, scoping them to the
// function we just inlined.
- if (!IFI.StaticAllocas.empty()) {
+ if (InsertLifetime && !IFI.StaticAllocas.empty()) {
IRBuilder<> builder(FirstNewBlock->begin());
for (unsigned ai = 0, ae = IFI.StaticAllocas.size(); ai != ae; ++ai) {
AllocaInst *AI = IFI.StaticAllocas[ai];
if (hasLifetimeMarkers(AI))
continue;
- builder.CreateLifetimeStart(AI);
- for (unsigned ri = 0, re = Returns.size(); ri != re; ++ri) {
- IRBuilder<> builder(Returns[ri]);
- builder.CreateLifetimeEnd(AI);
+ // Try to determine the size of the allocation.
+ ConstantInt *AllocaSize = nullptr;
+ if (ConstantInt *AIArraySize =
+ dyn_cast<ConstantInt>(AI->getArraySize())) {
+ if (IFI.DL) {
+ Type *AllocaType = AI->getAllocatedType();
+ uint64_t AllocaTypeSize = IFI.DL->getTypeAllocSize(AllocaType);
+ uint64_t AllocaArraySize = AIArraySize->getLimitedValue();
+ assert(AllocaArraySize > 0 && "array size of AllocaInst is zero");
+ // Check that array size doesn't saturate uint64_t and doesn't
+ // overflow when it's multiplied by type size.
+ if (AllocaArraySize != ~0ULL &&
+ UINT64_MAX / AllocaArraySize >= AllocaTypeSize) {
+ AllocaSize = ConstantInt::get(Type::getInt64Ty(AI->getContext()),
+ AllocaArraySize * AllocaTypeSize);
+ }
+ }
+ }
+
+ builder.CreateLifetimeStart(AI, AllocaSize);
+ for (ReturnInst *RI : Returns) {
+ // Don't insert llvm.lifetime.end calls between a musttail call and a
+ // return. The return kills all local allocas.
+ if (InlinedMustTailCalls && getPrecedingMustTailCall(RI))
+ continue;
+ IRBuilder<>(RI).CreateLifetimeEnd(AI, AllocaSize);
}
}
}
// Insert a call to llvm.stackrestore before any return instructions in the
// inlined function.
- for (unsigned i = 0, e = Returns.size(); i != e; ++i) {
- IRBuilder<>(Returns[i]).CreateCall(StackRestore, SavedPtr);
- }
-
- // Count the number of StackRestore calls we insert.
- unsigned NumStackRestores = Returns.size();
-
- // If we are inlining an invoke instruction, insert restores before each
- // unwind. These unwinds will be rewritten into branches later.
- if (InlinedFunctionInfo.ContainsUnwinds && isa<InvokeInst>(TheCall)) {
- for (Function::iterator BB = FirstNewBlock, E = Caller->end();
- BB != E; ++BB)
- if (UnwindInst *UI = dyn_cast<UnwindInst>(BB->getTerminator())) {
- IRBuilder<>(UI).CreateCall(StackRestore, SavedPtr);
- ++NumStackRestores;
- }
+ for (ReturnInst *RI : Returns) {
+ // Don't insert llvm.stackrestore calls between a musttail call and a
+ // return. The return will restore the stack pointer.
+ if (InlinedMustTailCalls && getPrecedingMustTailCall(RI))
+ continue;
+ IRBuilder<>(RI).CreateCall(StackRestore, SavedPtr);
}
}
- // If we are inlining tail call instruction through a call site that isn't
- // marked 'tail', we must remove the tail marker for any calls in the inlined
- // code. Also, calls inlined through a 'nounwind' call site should be marked
- // 'nounwind'.
- if (InlinedFunctionInfo.ContainsCalls &&
- (MustClearTailCallFlags || MarkNoUnwind)) {
- for (Function::iterator BB = FirstNewBlock, E = Caller->end();
- BB != E; ++BB)
- for (BasicBlock::iterator I = BB->begin(), E = BB->end(); I != E; ++I)
- if (CallInst *CI = dyn_cast<CallInst>(I)) {
- if (MustClearTailCallFlags)
- CI->setTailCall(false);
- if (MarkNoUnwind)
- CI->setDoesNotThrow();
- }
- }
+ // If we are inlining for an invoke instruction, we must make sure to rewrite
+ // any call instructions into invoke instructions.
+ if (InvokeInst *II = dyn_cast<InvokeInst>(TheCall))
+ HandleInlinedInvoke(II, FirstNewBlock, InlinedFunctionInfo);
- // If we are inlining through a 'nounwind' call site then any inlined 'unwind'
- // instructions are unreachable.
- if (InlinedFunctionInfo.ContainsUnwinds && MarkNoUnwind)
- for (Function::iterator BB = FirstNewBlock, E = Caller->end();
- BB != E; ++BB) {
- TerminatorInst *Term = BB->getTerminator();
- if (isa<UnwindInst>(Term)) {
- new UnreachableInst(Context, Term);
- BB->getInstList().erase(Term);
+ // Handle any inlined musttail call sites. In order for a new call site to be
+ // musttail, the source of the clone and the inlined call site must have been
+ // musttail. Therefore it's safe to return without merging control into the
+ // phi below.
+ if (InlinedMustTailCalls) {
+ // Check if we need to bitcast the result of any musttail calls.
+ Type *NewRetTy = Caller->getReturnType();
+ bool NeedBitCast = !TheCall->use_empty() && TheCall->getType() != NewRetTy;
+
+ // Handle the returns preceded by musttail calls separately.
+ SmallVector<ReturnInst *, 8> NormalReturns;
+ for (ReturnInst *RI : Returns) {
+ CallInst *ReturnedMustTail = getPrecedingMustTailCall(RI);
+ if (!ReturnedMustTail) {
+ NormalReturns.push_back(RI);
+ continue;
}
+ if (!NeedBitCast)
+ continue;
+
+ // Delete the old return and any preceding bitcast.
+ BasicBlock *CurBB = RI->getParent();
+ auto *OldCast = dyn_cast_or_null<BitCastInst>(RI->getReturnValue());
+ RI->eraseFromParent();
+ if (OldCast)
+ OldCast->eraseFromParent();
+
+ // Insert a new bitcast and return with the right type.
+ IRBuilder<> Builder(CurBB);
+ Builder.CreateRet(Builder.CreateBitCast(ReturnedMustTail, NewRetTy));
}
- // If we are inlining for an invoke instruction, we must make sure to rewrite
- // any inlined 'unwind' instructions into branches to the invoke exception
- // destination, and call instructions into invoke instructions.
- if (InvokeInst *II = dyn_cast<InvokeInst>(TheCall))
- HandleInlinedInvoke(II, FirstNewBlock, InlinedFunctionInfo);
+ // Leave behind the normal returns so we can merge control flow.
+ std::swap(Returns, NormalReturns);
+ }
// If we cloned in _exactly one_ basic block, and if that block ends in a
// return instruction, we splice the body of the inlined callee directly into
// If the call site was an invoke instruction, add a branch to the normal
// destination.
- if (InvokeInst *II = dyn_cast<InvokeInst>(TheCall))
- BranchInst::Create(II->getNormalDest(), TheCall);
+ if (InvokeInst *II = dyn_cast<InvokeInst>(TheCall)) {
+ BranchInst *NewBr = BranchInst::Create(II->getNormalDest(), TheCall);
+ NewBr->setDebugLoc(Returns[0]->getDebugLoc());
+ }
// If the return instruction returned a value, replace uses of the call with
// uses of the returned value.
// "starter" and "ender" blocks. How we accomplish this depends on whether
// this is an invoke instruction or a call instruction.
BasicBlock *AfterCallBB;
+ BranchInst *CreatedBranchToNormalDest = nullptr;
if (InvokeInst *II = dyn_cast<InvokeInst>(TheCall)) {
// Add an unconditional branch to make this look like the CallInst case...
- BranchInst *NewBr = BranchInst::Create(II->getNormalDest(), TheCall);
+ CreatedBranchToNormalDest = BranchInst::Create(II->getNormalDest(), TheCall);
// Split the basic block. This guarantees that no PHI nodes will have to be
// updated due to new incoming edges, and make the invoke case more
// symmetric to the call case.
- AfterCallBB = OrigBB->splitBasicBlock(NewBr,
+ AfterCallBB = OrigBB->splitBasicBlock(CreatedBranchToNormalDest,
CalledFunc->getName()+".exit");
} else { // It's a call
// any users of the original call/invoke instruction.
Type *RTy = CalledFunc->getReturnType();
- PHINode *PHI = 0;
+ PHINode *PHI = nullptr;
if (Returns.size() > 1) {
// The PHI node should go at the front of the new basic block to merge all
// possible incoming values.
// Add a branch to the merge points and remove return instructions.
+ DebugLoc Loc;
for (unsigned i = 0, e = Returns.size(); i != e; ++i) {
ReturnInst *RI = Returns[i];
- BranchInst::Create(AfterCallBB, RI);
+ BranchInst* BI = BranchInst::Create(AfterCallBB, RI);
+ Loc = RI->getDebugLoc();
+ BI->setDebugLoc(Loc);
RI->eraseFromParent();
}
+ // We need to set the debug location to *somewhere* inside the
+ // inlined function. The line number may be nonsensical, but the
+ // instruction will at least be associated with the right
+ // function.
+ if (CreatedBranchToNormalDest)
+ CreatedBranchToNormalDest->setDebugLoc(Loc);
} else if (!Returns.empty()) {
// Otherwise, if there is exactly one return value, just replace anything
// using the return value of the call with the computed value.
AfterCallBB->getInstList().splice(AfterCallBB->begin(),
ReturnBB->getInstList());
+ if (CreatedBranchToNormalDest)
+ CreatedBranchToNormalDest->setDebugLoc(Returns[0]->getDebugLoc());
+
// Delete the return instruction now and empty ReturnBB now.
Returns[0]->eraseFromParent();
ReturnBB->eraseFromParent();
// Since we are now done with the Call/Invoke, we can delete it.
TheCall->eraseFromParent();
+ // If we inlined any musttail calls and the original return is now
+ // unreachable, delete it. It can only contain a bitcast and ret.
+ if (InlinedMustTailCalls && pred_begin(AfterCallBB) == pred_end(AfterCallBB))
+ AfterCallBB->eraseFromParent();
+
// We should always be able to fold the entry block of the function into the
// single predecessor of the block...
assert(cast<BranchInst>(Br)->isUnconditional() && "splitBasicBlock broken!");
// If we inserted a phi node, check to see if it has a single value (e.g. all
// the entries are the same or undef). If so, remove the PHI so it doesn't
// block other optimizations.
- if (PHI)
- if (Value *V = SimplifyInstruction(PHI, IFI.TD)) {
+ if (PHI) {
+ if (Value *V = SimplifyInstruction(PHI, IFI.DL)) {
PHI->replaceAllUsesWith(V);
PHI->eraseFromParent();
}
+ }
return true;
}