]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/blobdiff - lib/Transforms/Utils/InlineFunction.cpp
DebugInfo: Preserve debug location information when transforming a call into an invok...
[opencl/llvm.git] / lib / Transforms / Utils / InlineFunction.cpp
index 6d8a319635c272b36a80b12ae84a7dfa3c9b8926..f0a9f2b1fcb354dc088555c534ab4cdb51100f90 100644 (file)
 // This file implements inlining of a function into a call site, resolving
 // parameters and the return value as appropriate.
 //
-// The code in this file for handling inlines through invoke
-// instructions preserves semantics only under some assumptions about
-// the behavior of unwinders which correspond to gcc-style libUnwind
-// exception personality functions.  Eventually the IR will be
-// improved to make this unnecessary, but until then, this code is
-// marked [LIBUNWIND].
-//
 //===----------------------------------------------------------------------===//
 
 #include "llvm/Transforms/Utils/Cloning.h"
-#include "llvm/Constants.h"
-#include "llvm/DerivedTypes.h"
-#include "llvm/Module.h"
-#include "llvm/Instructions.h"
-#include "llvm/IntrinsicInst.h"
-#include "llvm/Intrinsics.h"
-#include "llvm/Attributes.h"
+#include "llvm/ADT/SmallVector.h"
+#include "llvm/ADT/StringExtras.h"
 #include "llvm/Analysis/CallGraph.h"
-#include "llvm/Analysis/DebugInfo.h"
 #include "llvm/Analysis/InstructionSimplify.h"
-#include "llvm/Target/TargetData.h"
+#include "llvm/IR/Attributes.h"
+#include "llvm/IR/CallSite.h"
+#include "llvm/IR/CFG.h"
+#include "llvm/IR/Constants.h"
+#include "llvm/IR/DataLayout.h"
+#include "llvm/IR/DebugInfo.h"
+#include "llvm/IR/DerivedTypes.h"
+#include "llvm/IR/IRBuilder.h"
+#include "llvm/IR/Instructions.h"
+#include "llvm/IR/IntrinsicInst.h"
+#include "llvm/IR/Intrinsics.h"
+#include "llvm/IR/Module.h"
 #include "llvm/Transforms/Utils/Local.h"
-#include "llvm/ADT/SmallVector.h"
-#include "llvm/ADT/StringExtras.h"
-#include "llvm/Support/CallSite.h"
-#include "llvm/Support/IRBuilder.h"
 using namespace llvm;
 
-bool llvm::InlineFunction(CallInst *CI, InlineFunctionInfo &IFI) {
-  return InlineFunction(CallSite(CI), IFI);
-}
-bool llvm::InlineFunction(InvokeInst *II, InlineFunctionInfo &IFI) {
-  return InlineFunction(CallSite(II), IFI);
-}
-
-/// [LIBUNWIND] Look for an llvm.eh.exception call in the given block.
-static EHExceptionInst *findExceptionInBlock(BasicBlock *bb) {
-  for (BasicBlock::iterator i = bb->begin(), e = bb->end(); i != e; i++) {
-    EHExceptionInst *exn = dyn_cast<EHExceptionInst>(i);
-    if (exn) return exn;
-  }
-
-  return 0;
+bool llvm::InlineFunction(CallInst *CI, InlineFunctionInfo &IFI,
+                          bool InsertLifetime) {
+  return InlineFunction(CallSite(CI), IFI, InsertLifetime);
 }
-
-/// [LIBUNWIND] Look for the 'best' llvm.eh.selector instruction for
-/// the given llvm.eh.exception call.
-static EHSelectorInst *findSelectorForException(EHExceptionInst *exn) {
-  BasicBlock *exnBlock = exn->getParent();
-
-  EHSelectorInst *outOfBlockSelector = 0;
-  for (Instruction::use_iterator
-         ui = exn->use_begin(), ue = exn->use_end(); ui != ue; ++ui) {
-    EHSelectorInst *sel = dyn_cast<EHSelectorInst>(*ui);
-    if (!sel) continue;
-
-    // Immediately accept an eh.selector in the same block as the
-    // excepton call.
-    if (sel->getParent() == exnBlock) return sel;
-
-    // Otherwise, use the first selector we see.
-    if (!outOfBlockSelector) outOfBlockSelector = sel;
-  }
-
-  return outOfBlockSelector;
-}
-
-/// [LIBUNWIND] Find the (possibly absent) call to @llvm.eh.selector
-/// in the given landing pad.  In principle, llvm.eh.exception is
-/// required to be in the landing pad; in practice, SplitCriticalEdge
-/// can break that invariant, and then inlining can break it further.
-/// There's a real need for a reliable solution here, but until that
-/// happens, we have some fragile workarounds here.
-static EHSelectorInst *findSelectorForLandingPad(BasicBlock *lpad) {
-  // Look for an exception call in the actual landing pad.
-  EHExceptionInst *exn = findExceptionInBlock(lpad);
-  if (exn) return findSelectorForException(exn);
-
-  // Okay, if that failed, look for one in an obvious successor.  If
-  // we find one, we'll fix the IR by moving things back to the
-  // landing pad.
-
-  bool dominates = true; // does the lpad dominate the exn call
-  BasicBlock *nonDominated = 0; // if not, the first non-dominated block
-  BasicBlock *lastDominated = 0; // and the block which branched to it
-
-  BasicBlock *exnBlock = lpad;
-
-  // We need to protect against lpads that lead into infinite loops.
-  SmallPtrSet<BasicBlock*,4> visited;
-  visited.insert(exnBlock);
-
-  do {
-    // We're not going to apply this hack to anything more complicated
-    // than a series of unconditional branches, so if the block
-    // doesn't terminate in an unconditional branch, just fail.  More
-    // complicated cases can arise when, say, sinking a call into a
-    // split unwind edge and then inlining it; but that can do almost
-    // *anything* to the CFG, including leaving the selector
-    // completely unreachable.  The only way to fix that properly is
-    // to (1) prohibit transforms which move the exception or selector
-    // values away from the landing pad, e.g. by producing them with
-    // instructions that are pinned to an edge like a phi, or
-    // producing them with not-really-instructions, and (2) making
-    // transforms which split edges deal with that.
-    BranchInst *branch = dyn_cast<BranchInst>(&exnBlock->back());
-    if (!branch || branch->isConditional()) return 0;
-
-    BasicBlock *successor = branch->getSuccessor(0);
-
-    // Fail if we found an infinite loop.
-    if (!visited.insert(successor)) return 0;
-
-    // If the successor isn't dominated by exnBlock:
-    if (!successor->getSinglePredecessor()) {
-      // We don't want to have to deal with threading the exception
-      // through multiple levels of phi, so give up if we've already
-      // followed a non-dominating edge.
-      if (!dominates) return 0;
-
-      // Otherwise, remember this as a non-dominating edge.
-      dominates = false;
-      nonDominated = successor;
-      lastDominated = exnBlock;
-    }
-
-    exnBlock = successor;
-
-    // Can we stop here?
-    exn = findExceptionInBlock(exnBlock);
-  } while (!exn);
-
-  // Look for a selector call for the exception we found.
-  EHSelectorInst *selector = findSelectorForException(exn);
-  if (!selector) return 0;
-
-  // The easy case is when the landing pad still dominates the
-  // exception call, in which case we can just move both calls back to
-  // the landing pad.
-  if (dominates) {
-    selector->moveBefore(lpad->getFirstNonPHI());
-    exn->moveBefore(selector);
-    return selector;
-  }
-
-  // Otherwise, we have to split at the first non-dominating block.
-  // The CFG looks basically like this:
-  //    lpad:
-  //      phis_0
-  //      insnsAndBranches_1
-  //      br label %nonDominated
-  //    nonDominated:
-  //      phis_2
-  //      insns_3
-  //      %exn = call i8* @llvm.eh.exception()
-  //      insnsAndBranches_4
-  //      %selector = call @llvm.eh.selector(i8* %exn, ...
-  // We need to turn this into:
-  //    lpad:
-  //      phis_0
-  //      %exn0 = call i8* @llvm.eh.exception()
-  //      %selector0 = call @llvm.eh.selector(i8* %exn0, ...
-  //      insnsAndBranches_1
-  //      br label %split // from lastDominated
-  //    nonDominated:
-  //      phis_2 (without edge from lastDominated)
-  //      %exn1 = call i8* @llvm.eh.exception()
-  //      %selector1 = call i8* @llvm.eh.selector(i8* %exn1, ...
-  //      br label %split
-  //    split:
-  //      phis_2 (edge from lastDominated, edge from split)
-  //      %exn = phi ...
-  //      %selector = phi ...
-  //      insns_3
-  //      insnsAndBranches_4
-
-  assert(nonDominated);
-  assert(lastDominated);
-
-  // First, make clones of the intrinsics to go in lpad.
-  EHExceptionInst *lpadExn = cast<EHExceptionInst>(exn->clone());
-  EHSelectorInst *lpadSelector = cast<EHSelectorInst>(selector->clone());
-  lpadSelector->setArgOperand(0, lpadExn);
-  lpadSelector->insertBefore(lpad->getFirstNonPHI());
-  lpadExn->insertBefore(lpadSelector);
-
-  // Split the non-dominated block.
-  BasicBlock *split =
-    nonDominated->splitBasicBlock(nonDominated->getFirstNonPHI(),
-                                  nonDominated->getName() + ".lpad-fix");
-
-  // Redirect the last dominated branch there.
-  cast<BranchInst>(lastDominated->back()).setSuccessor(0, split);
-
-  // Move the existing intrinsics to the end of the old block.
-  selector->moveBefore(&nonDominated->back());
-  exn->moveBefore(selector);
-
-  Instruction *splitIP = &split->front();
-
-  // For all the phis in nonDominated, make a new phi in split to join
-  // that phi with the edge from lastDominated.
-  for (BasicBlock::iterator
-         i = nonDominated->begin(), e = nonDominated->end(); i != e; ++i) {
-    PHINode *phi = dyn_cast<PHINode>(i);
-    if (!phi) break;
-
-    PHINode *splitPhi = PHINode::Create(phi->getType(), 2, phi->getName(),
-                                        splitIP);
-    phi->replaceAllUsesWith(splitPhi);
-    splitPhi->addIncoming(phi, nonDominated);
-    splitPhi->addIncoming(phi->removeIncomingValue(lastDominated),
-                          lastDominated);
-  }
-
-  // Make new phis for the exception and selector.
-  PHINode *exnPhi = PHINode::Create(exn->getType(), 2, "", splitIP);
-  exn->replaceAllUsesWith(exnPhi);
-  selector->setArgOperand(0, exn); // except for this use
-  exnPhi->addIncoming(exn, nonDominated);
-  exnPhi->addIncoming(lpadExn, lastDominated);
-
-  PHINode *selectorPhi = PHINode::Create(selector->getType(), 2, "", splitIP);
-  selector->replaceAllUsesWith(selectorPhi);
-  selectorPhi->addIncoming(selector, nonDominated);
-  selectorPhi->addIncoming(lpadSelector, lastDominated);
-
-  return lpadSelector;
+bool llvm::InlineFunction(InvokeInst *II, InlineFunctionInfo &IFI,
+                          bool InsertLifetime) {
+  return InlineFunction(CallSite(II), IFI, InsertLifetime);
 }
 
 namespace {
   /// A class for recording information about inlining through an invoke.
   class InvokeInliningInfo {
-    BasicBlock *OuterUnwindDest;
-    EHSelectorInst *OuterSelector;
-    BasicBlock *InnerUnwindDest;
-    PHINode *InnerExceptionPHI;
-    PHINode *InnerSelectorPHI;
+    BasicBlock *OuterResumeDest; ///< Destination of the invoke's unwind.
+    BasicBlock *InnerResumeDest; ///< Destination for the callee's resume.
+    LandingPadInst *CallerLPad;  ///< LandingPadInst associated with the invoke.
+    PHINode *InnerEHValuesPHI;   ///< PHI for EH values from landingpad insts.
     SmallVector<Value*, 8> UnwindDestPHIValues;
 
   public:
-    InvokeInliningInfo(InvokeInst *II) :
-      OuterUnwindDest(II->getUnwindDest()), OuterSelector(0),
-      InnerUnwindDest(0), InnerExceptionPHI(0), InnerSelectorPHI(0) {
-
-      // If there are PHI nodes in the unwind destination block, we
-      // need to keep track of which values came into them from the
-      // invoke before removing the edge from this block.
-      llvm::BasicBlock *invokeBB = II->getParent();
-      for (BasicBlock::iterator I = OuterUnwindDest->begin();
-             isa<PHINode>(I); ++I) {
+    InvokeInliningInfo(InvokeInst *II)
+      : OuterResumeDest(II->getUnwindDest()), InnerResumeDest(nullptr),
+        CallerLPad(nullptr), InnerEHValuesPHI(nullptr) {
+      // If there are PHI nodes in the unwind destination block, we need to keep
+      // track of which values came into them from the invoke before removing
+      // the edge from this block.
+      llvm::BasicBlock *InvokeBB = II->getParent();
+      BasicBlock::iterator I = OuterResumeDest->begin();
+      for (; isa<PHINode>(I); ++I) {
         // Save the value to use for this edge.
-        PHINode *phi = cast<PHINode>(I);
-        UnwindDestPHIValues.push_back(phi->getIncomingValueForBlock(invokeBB));
+        PHINode *PHI = cast<PHINode>(I);
+        UnwindDestPHIValues.push_back(PHI->getIncomingValueForBlock(InvokeBB));
       }
-    }
 
-    /// The outer unwind destination is the target of unwind edges
-    /// introduced for calls within the inlined function.
-    BasicBlock *getOuterUnwindDest() const {
-      return OuterUnwindDest;
+      CallerLPad = cast<LandingPadInst>(I);
     }
 
-    EHSelectorInst *getOuterSelector() {
-      if (!OuterSelector)
-        OuterSelector = findSelectorForLandingPad(OuterUnwindDest);
-      return OuterSelector;
+    /// getOuterResumeDest - The outer unwind destination is the target of
+    /// unwind edges introduced for calls within the inlined function.
+    BasicBlock *getOuterResumeDest() const {
+      return OuterResumeDest;
     }
 
-    BasicBlock *getInnerUnwindDest();
+    BasicBlock *getInnerResumeDest();
+
+    LandingPadInst *getLandingPadInst() const { return CallerLPad; }
 
-    bool forwardEHResume(CallInst *call, BasicBlock *src);
+    /// forwardResume - Forward the 'resume' instruction to the caller's landing
+    /// pad block. When the landing pad block has only one predecessor, this is
+    /// a simple branch. When there is more than one predecessor, we need to
+    /// split the landing pad block after the landingpad instruction and jump
+    /// to there.
+    void forwardResume(ResumeInst *RI,
+                       SmallPtrSet<LandingPadInst*, 16> &InlinedLPads);
 
-    /// Add incoming-PHI values to the unwind destination block for
-    /// the given basic block, using the values for the original
-    /// invoke's source block.
+    /// addIncomingPHIValuesFor - Add incoming-PHI values to the unwind
+    /// destination block for the given basic block, using the values for the
+    /// original invoke's source block.
     void addIncomingPHIValuesFor(BasicBlock *BB) const {
-      addIncomingPHIValuesForInto(BB, OuterUnwindDest);
+      addIncomingPHIValuesForInto(BB, OuterResumeDest);
     }
 
     void addIncomingPHIValuesForInto(BasicBlock *src, BasicBlock *dest) const {
@@ -300,116 +103,58 @@ namespace {
   };
 }
 
-/// Get or create a target for the branch out of rewritten calls to
-/// llvm.eh.resume.
-BasicBlock *InvokeInliningInfo::getInnerUnwindDest() {
-  if (InnerUnwindDest) return InnerUnwindDest;
-
-  // Find and hoist the llvm.eh.exception and llvm.eh.selector calls
-  // in the outer landing pad to immediately following the phis.
-  EHSelectorInst *selector = getOuterSelector();
-  if (!selector) return 0;
-
-  // The call to llvm.eh.exception *must* be in the landing pad.
-  Instruction *exn = cast<Instruction>(selector->getArgOperand(0));
-  assert(exn->getParent() == OuterUnwindDest);
-
-  // TODO: recognize when we've already done this, so that we don't
-  // get a linear number of these when inlining calls into lots of
-  // invokes with the same landing pad.
-
-  // Do the hoisting.
-  Instruction *splitPoint = exn->getParent()->getFirstNonPHI();
-  assert(splitPoint != selector && "selector-on-exception dominance broken!");
-  if (splitPoint == exn) {
-    selector->removeFromParent();
-    selector->insertAfter(exn);
-    splitPoint = selector->getNextNode();
-  } else {
-    exn->moveBefore(splitPoint);
-    selector->moveBefore(splitPoint);
-  }
+/// getInnerResumeDest - Get or create a target for the branch from ResumeInsts.
+BasicBlock *InvokeInliningInfo::getInnerResumeDest() {
+  if (InnerResumeDest) return InnerResumeDest;
 
   // Split the landing pad.
-  InnerUnwindDest = OuterUnwindDest->splitBasicBlock(splitPoint,
-                                        OuterUnwindDest->getName() + ".body");
+  BasicBlock::iterator SplitPoint = CallerLPad; ++SplitPoint;
+  InnerResumeDest =
+    OuterResumeDest->splitBasicBlock(SplitPoint,
+                                     OuterResumeDest->getName() + ".body");
 
   // The number of incoming edges we expect to the inner landing pad.
-  const unsigned phiCapacity = 2;
+  const unsigned PHICapacity = 2;
 
-  // Create corresponding new phis for all the phis in the outer landing pad.
-  BasicBlock::iterator insertPoint = InnerUnwindDest->begin();
-  BasicBlock::iterator I = OuterUnwindDest->begin();
+  // Create corresponding new PHIs for all the PHIs in the outer landing pad.
+  BasicBlock::iterator InsertPoint = InnerResumeDest->begin();
+  BasicBlock::iterator I = OuterResumeDest->begin();
   for (unsigned i = 0, e = UnwindDestPHIValues.size(); i != e; ++i, ++I) {
-    PHINode *outerPhi = cast<PHINode>(I);
-    PHINode *innerPhi = PHINode::Create(outerPhi->getType(), phiCapacity,
-                                        outerPhi->getName() + ".lpad-body",
-                                        insertPoint);
-    outerPhi->replaceAllUsesWith(innerPhi);
-    innerPhi->addIncoming(outerPhi, OuterUnwindDest);
+    PHINode *OuterPHI = cast<PHINode>(I);
+    PHINode *InnerPHI = PHINode::Create(OuterPHI->getType(), PHICapacity,
+                                        OuterPHI->getName() + ".lpad-body",
+                                        InsertPoint);
+    OuterPHI->replaceAllUsesWith(InnerPHI);
+    InnerPHI->addIncoming(OuterPHI, OuterResumeDest);
   }
 
-  // Create a phi for the exception value...
-  InnerExceptionPHI = PHINode::Create(exn->getType(), phiCapacity,
-                                      "exn.lpad-body", insertPoint);
-  exn->replaceAllUsesWith(InnerExceptionPHI);
-  selector->setArgOperand(0, exn); // restore this use
-  InnerExceptionPHI->addIncoming(exn, OuterUnwindDest);
-
-  // ...and the selector.
-  InnerSelectorPHI = PHINode::Create(selector->getType(), phiCapacity,
-                                     "selector.lpad-body", insertPoint);
-  selector->replaceAllUsesWith(InnerSelectorPHI);
-  InnerSelectorPHI->addIncoming(selector, OuterUnwindDest);
+  // Create a PHI for the exception values.
+  InnerEHValuesPHI = PHINode::Create(CallerLPad->getType(), PHICapacity,
+                                     "eh.lpad-body", InsertPoint);
+  CallerLPad->replaceAllUsesWith(InnerEHValuesPHI);
+  InnerEHValuesPHI->addIncoming(CallerLPad, OuterResumeDest);
 
   // All done.
-  return InnerUnwindDest;
+  return InnerResumeDest;
 }
 
-/// [LIBUNWIND] Try to forward the given call, which logically occurs
-/// at the end of the given block, as a branch to the inner unwind
-/// block.  Returns true if the call was forwarded.
-bool InvokeInliningInfo::forwardEHResume(CallInst *call, BasicBlock *src) {
-  // First, check whether this is a call to the intrinsic.
-  Function *fn = dyn_cast<Function>(call->getCalledValue());
-  if (!fn || fn->getName() != "llvm.eh.resume")
-    return false;
-  
-  // At this point, we need to return true on all paths, because
-  // otherwise we'll construct an invoke of the intrinsic, which is
-  // not well-formed.
-
-  // Try to find or make an inner unwind dest, which will fail if we
-  // can't find a selector call for the outer unwind dest.
-  BasicBlock *dest = getInnerUnwindDest();
-  bool hasSelector = (dest != 0);
-
-  // If we failed, just use the outer unwind dest, dropping the
-  // exception and selector on the floor.
-  if (!hasSelector)
-    dest = OuterUnwindDest;
-
-  // Make a branch.
-  BranchInst::Create(dest, src);
-
-  // Update the phis in the destination.  They were inserted in an
-  // order which makes this work.
-  addIncomingPHIValuesForInto(src, dest);
-
-  if (hasSelector) {
-    InnerExceptionPHI->addIncoming(call->getArgOperand(0), src);
-    InnerSelectorPHI->addIncoming(call->getArgOperand(1), src);
-  }
+/// forwardResume - Forward the 'resume' instruction to the caller's landing pad
+/// block. When the landing pad block has only one predecessor, this is a simple
+/// branch. When there is more than one predecessor, we need to split the
+/// landing pad block after the landingpad instruction and jump to there.
+void InvokeInliningInfo::forwardResume(ResumeInst *RI,
+                               SmallPtrSet<LandingPadInst*, 16> &InlinedLPads) {
+  BasicBlock *Dest = getInnerResumeDest();
+  BasicBlock *Src = RI->getParent();
 
-  return true;
-}
+  BranchInst::Create(Dest, Src);
 
-/// [LIBUNWIND] Check whether this selector is "only cleanups":
-///   call i32 @llvm.eh.selector(blah, blah, i32 0)
-static bool isCleanupOnlySelector(EHSelectorInst *selector) {
-  if (selector->getNumArgOperands() != 3) return false;
-  ConstantInt *val = dyn_cast<ConstantInt>(selector->getArgOperand(2));
-  return (val && val->isZero());
+  // Update the PHIs in the destination. They were inserted in an order which
+  // makes this work.
+  addIncomingPHIValuesForInto(Src, Dest);
+
+  InnerEHValuesPHI->addIncoming(RI->getOperand(0), Src);
+  RI->eraseFromParent();
 }
 
 /// HandleCallsInBlockInlinedThroughInvoke - When we inline a basic block into
@@ -417,76 +162,34 @@ static bool isCleanupOnlySelector(EHSelectorInst *selector) {
 /// invokes.  This function analyze BB to see if there are any calls, and if so,
 /// it rewrites them to be invokes that jump to InvokeDest and fills in the PHI
 /// nodes in that block with the values specified in InvokeDestPHIValues.
-///
-/// Returns true to indicate that the next block should be skipped.
-static bool HandleCallsInBlockInlinedThroughInvoke(BasicBlock *BB,
+static void HandleCallsInBlockInlinedThroughInvoke(BasicBlock *BB,
                                                    InvokeInliningInfo &Invoke) {
   for (BasicBlock::iterator BBI = BB->begin(), E = BB->end(); BBI != E; ) {
     Instruction *I = BBI++;
-    
+
     // We only need to check for function calls: inlined invoke
     // instructions require no special handling.
     CallInst *CI = dyn_cast<CallInst>(I);
-    if (CI == 0) continue;
-
-    // LIBUNWIND: merge selector instructions.
-    if (EHSelectorInst *Inner = dyn_cast<EHSelectorInst>(CI)) {
-      EHSelectorInst *Outer = Invoke.getOuterSelector();
-      if (!Outer) continue;
-
-      bool innerIsOnlyCleanup = isCleanupOnlySelector(Inner);
-      bool outerIsOnlyCleanup = isCleanupOnlySelector(Outer);
-
-      // If both selectors contain only cleanups, we don't need to do
-      // anything.  TODO: this is really just a very specific instance
-      // of a much more general optimization.
-      if (innerIsOnlyCleanup && outerIsOnlyCleanup) continue;
-
-      // Otherwise, we just append the outer selector to the inner selector.
-      SmallVector<Value*, 16> NewSelector;
-      for (unsigned i = 0, e = Inner->getNumArgOperands(); i != e; ++i)
-        NewSelector.push_back(Inner->getArgOperand(i));
-      for (unsigned i = 2, e = Outer->getNumArgOperands(); i != e; ++i)
-        NewSelector.push_back(Outer->getArgOperand(i));
-
-      CallInst *NewInner =
-        IRBuilder<>(Inner).CreateCall(Inner->getCalledValue(), NewSelector);
-      // No need to copy attributes, calling convention, etc.
-      NewInner->takeName(Inner);
-      Inner->replaceAllUsesWith(NewInner);
-      Inner->eraseFromParent();
-      continue;
-    }
-    
+
     // If this call cannot unwind, don't convert it to an invoke.
-    if (CI->doesNotThrow())
+    // Inline asm calls cannot throw.
+    if (!CI || CI->doesNotThrow() || isa<InlineAsm>(CI->getCalledValue()))
       continue;
-    
-    // Convert this function call into an invoke instruction.
-    // First, split the basic block.
+
+    // Convert this function call into an invoke instruction.  First, split the
+    // basic block.
     BasicBlock *Split = BB->splitBasicBlock(CI, CI->getName()+".noexc");
 
     // Delete the unconditional branch inserted by splitBasicBlock
     BB->getInstList().pop_back();
 
-    // LIBUNWIND: If this is a call to @llvm.eh.resume, just branch
-    // directly to the new landing pad.
-    if (Invoke.forwardEHResume(CI, BB)) {
-      // TODO: 'Split' is now unreachable; clean it up.
-
-      // We want to leave the original call intact so that the call
-      // graph and other structures won't get misled.  We also have to
-      // avoid processing the next block, or we'll iterate here forever.
-      return true;
-    }
-
-    // Otherwise, create the new invoke instruction.
+    // Create the new invoke instruction.
     ImmutableCallSite CS(CI);
     SmallVector<Value*, 8> InvokeArgs(CS.arg_begin(), CS.arg_end());
-    InvokeInst *II =
-      InvokeInst::Create(CI->getCalledValue(), Split,
-                         Invoke.getOuterUnwindDest(),
-                         InvokeArgs, CI->getName(), BB);
+    InvokeInst *II = InvokeInst::Create(CI->getCalledValue(), Split,
+                                        Invoke.getOuterResumeDest(),
+                                        InvokeArgs, CI->getName(), BB);
+    II->setDebugLoc(CI->getDebugLoc());
     II->setCallingConv(CI->getCallingConv());
     II->setAttributes(CI->getAttributes());
     
@@ -494,21 +197,18 @@ static bool HandleCallsInBlockInlinedThroughInvoke(BasicBlock *BB,
     // updates the CallGraph if present, because it uses a WeakVH.
     CI->replaceAllUsesWith(II);
 
-    Split->getInstList().pop_front();  // Delete the original call
+    // Delete the original call
+    Split->getInstList().pop_front();
 
-    // Update any PHI nodes in the exceptional block to indicate that
-    // there is now a new entry in them.
+    // Update any PHI nodes in the exceptional block to indicate that there is
+    // now a new entry in them.
     Invoke.addIncomingPHIValuesFor(BB);
-    return false;
+    return;
   }
-
-  return false;
 }
-  
 
 /// HandleInlinedInvoke - If we inlined an invoke site, we need to convert calls
-/// in the body of the inlined function into invokes and turn unwind
-/// instructions into branches to the invoke unwind dest.
+/// in the body of the inlined function into invokes.
 ///
 /// II is the invoke instruction being inlined.  FirstNewBlock is the first
 /// block of the inlined code (the last block is the end of the function),
@@ -521,47 +221,41 @@ static void HandleInlinedInvoke(InvokeInst *II, BasicBlock *FirstNewBlock,
 
   // The inlined code is currently at the end of the function, scan from the
   // start of the inlined code to its end, checking for stuff we need to
-  // rewrite.  If the code doesn't have calls or unwinds, we know there is
-  // nothing to rewrite.
-  if (!InlinedCodeInfo.ContainsCalls && !InlinedCodeInfo.ContainsUnwinds) {
-    // Now that everything is happy, we have one final detail.  The PHI nodes in
-    // the exception destination block still have entries due to the original
-    // invoke instruction.  Eliminate these entries (which might even delete the
-    // PHI node) now.
-    InvokeDest->removePredecessor(II->getParent());
-    return;
+  // rewrite.
+  InvokeInliningInfo Invoke(II);
+
+  // Get all of the inlined landing pad instructions.
+  SmallPtrSet<LandingPadInst*, 16> InlinedLPads;
+  for (Function::iterator I = FirstNewBlock, E = Caller->end(); I != E; ++I)
+    if (InvokeInst *II = dyn_cast<InvokeInst>(I->getTerminator()))
+      InlinedLPads.insert(II->getLandingPadInst());
+
+  // Append the clauses from the outer landing pad instruction into the inlined
+  // landing pad instructions.
+  LandingPadInst *OuterLPad = Invoke.getLandingPadInst();
+  for (SmallPtrSet<LandingPadInst*, 16>::iterator I = InlinedLPads.begin(),
+         E = InlinedLPads.end(); I != E; ++I) {
+    LandingPadInst *InlinedLPad = *I;
+    unsigned OuterNum = OuterLPad->getNumClauses();
+    InlinedLPad->reserveClauses(OuterNum);
+    for (unsigned OuterIdx = 0; OuterIdx != OuterNum; ++OuterIdx)
+      InlinedLPad->addClause(OuterLPad->getClause(OuterIdx));
+    if (OuterLPad->isCleanup())
+      InlinedLPad->setCleanup(true);
   }
 
-  InvokeInliningInfo Invoke(II);
-  
   for (Function::iterator BB = FirstNewBlock, E = Caller->end(); BB != E; ++BB){
     if (InlinedCodeInfo.ContainsCalls)
-      if (HandleCallsInBlockInlinedThroughInvoke(BB, Invoke)) {
-        // Honor a request to skip the next block.  We don't need to
-        // consider UnwindInsts in this case either.
-        ++BB;
-        continue;
-      }
-
-    if (UnwindInst *UI = dyn_cast<UnwindInst>(BB->getTerminator())) {
-      // An UnwindInst requires special handling when it gets inlined into an
-      // invoke site.  Once this happens, we know that the unwind would cause
-      // a control transfer to the invoke exception destination, so we can
-      // transform it into a direct branch to the exception destination.
-      BranchInst::Create(InvokeDest, UI);
+      HandleCallsInBlockInlinedThroughInvoke(BB, Invoke);
 
-      // Delete the unwind instruction!
-      UI->eraseFromParent();
-
-      // Update any PHI nodes in the exceptional block to indicate that
-      // there is now a new entry in them.
-      Invoke.addIncomingPHIValuesFor(BB);
-    }
+    // Forward any resumes that are remaining here.
+    if (ResumeInst *RI = dyn_cast<ResumeInst>(BB->getTerminator()))
+      Invoke.forwardResume(RI, InlinedLPads);
   }
 
   // Now that everything is happy, we have one final detail.  The PHI nodes in
   // the exception destination block still have entries due to the original
-  // invoke instruction.  Eliminate these entries (which might even delete the
+  // invoke instruction. Eliminate these entries (which might even delete the
   // PHI node) now.
   InvokeDest->removePredecessor(II->getParent());
 }
@@ -597,13 +291,13 @@ static void UpdateCallGraphAfterInlining(CallSite CS,
 
     ValueToValueMapTy::iterator VMI = VMap.find(OrigCall);
     // Only copy the edge if the call was inlined!
-    if (VMI == VMap.end() || VMI->second == 0)
+    if (VMI == VMap.end() || VMI->second == nullptr)
       continue;
     
     // If the call was inlined, but then constant folded, there is no edge to
     // add.  Check for this case.
     Instruction *NewCall = dyn_cast<Instruction>(VMI->second);
-    if (NewCall == 0) continue;
+    if (!NewCall) continue;
 
     // Remember that this call site got inlined for the client of
     // InlineFunction.
@@ -614,7 +308,7 @@ static void UpdateCallGraphAfterInlining(CallSite CS,
     // happens, set the callee of the new call site to a more precise
     // destination.  This can also happen if the call graph node of the caller
     // was just unnecessarily imprecise.
-    if (I->second->getFunction() == 0)
+    if (!I->second->getFunction())
       if (Function *F = CallSite(NewCall).getCalledFunction()) {
         // Indirect call site resolved to direct call.
         CallerNode->addCalledFunction(CallSite(NewCall), CG[F]);
@@ -630,13 +324,44 @@ static void UpdateCallGraphAfterInlining(CallSite CS,
   CallerNode->removeCallEdgeFor(CS);
 }
 
+static void HandleByValArgumentInit(Value *Dst, Value *Src, Module *M,
+                                    BasicBlock *InsertBlock,
+                                    InlineFunctionInfo &IFI) {
+  LLVMContext &Context = Src->getContext();
+  Type *VoidPtrTy = Type::getInt8PtrTy(Context);
+  Type *AggTy = cast<PointerType>(Src->getType())->getElementType();
+  Type *Tys[3] = { VoidPtrTy, VoidPtrTy, Type::getInt64Ty(Context) };
+  Function *MemCpyFn = Intrinsic::getDeclaration(M, Intrinsic::memcpy, Tys);
+  IRBuilder<> builder(InsertBlock->begin());
+  Value *DstCast = builder.CreateBitCast(Dst, VoidPtrTy, "tmp");
+  Value *SrcCast = builder.CreateBitCast(Src, VoidPtrTy, "tmp");
+
+  Value *Size;
+  if (IFI.DL == nullptr)
+    Size = ConstantExpr::getSizeOf(AggTy);
+  else
+    Size = ConstantInt::get(Type::getInt64Ty(Context),
+                            IFI.DL->getTypeStoreSize(AggTy));
+
+  // Always generate a memcpy of alignment 1 here because we don't know
+  // the alignment of the src pointer.  Other optimizations can infer
+  // better alignment.
+  Value *CallArgs[] = {
+    DstCast, SrcCast, Size,
+    ConstantInt::get(Type::getInt32Ty(Context), 1),
+    ConstantInt::getFalse(Context) // isVolatile
+  };
+  builder.CreateCall(MemCpyFn, CallArgs);
+}
+
 /// HandleByValArgument - When inlining a call site that has a byval argument,
 /// we have to make the implicit memcpy explicit by adding it.
 static Value *HandleByValArgument(Value *Arg, Instruction *TheCall,
                                   const Function *CalledFunc,
                                   InlineFunctionInfo &IFI,
                                   unsigned ByValAlignment) {
-  Type *AggTy = cast<PointerType>(Arg->getType())->getElementType();
+  PointerType *ArgTy = cast<PointerType>(Arg->getType());
+  Type *AggTy = ArgTy->getElementType();
 
   // If the called function is readonly, then it could not mutate the caller's
   // copy of the byval'd memory.  In this case, it is safe to elide the copy and
@@ -651,21 +376,17 @@ static Value *HandleByValArgument(Value *Arg, Instruction *TheCall,
     // If the pointer is already known to be sufficiently aligned, or if we can
     // round it up to a larger alignment, then we don't need a temporary.
     if (getOrEnforceKnownAlignment(Arg, ByValAlignment,
-                                   IFI.TD) >= ByValAlignment)
+                                   IFI.DL) >= ByValAlignment)
       return Arg;
     
     // Otherwise, we have to make a memcpy to get a safe alignment.  This is bad
     // for code quality, but rarely happens and is required for correctness.
   }
-  
-  LLVMContext &Context = Arg->getContext();
 
-  Type *VoidPtrTy = Type::getInt8PtrTy(Context);
-  
-  // Create the alloca.  If we have TargetData, use nice alignment.
+  // Create the alloca.  If we have DataLayout, use nice alignment.
   unsigned Align = 1;
-  if (IFI.TD)
-    Align = IFI.TD->getPrefTypeAlignment(AggTy);
+  if (IFI.DL)
+    Align = IFI.DL->getPrefTypeAlignment(AggTy);
   
   // If the byval had an alignment specified, we *must* use at least that
   // alignment, as it is required by the byval argument (and uses of the
@@ -674,32 +395,9 @@ static Value *HandleByValArgument(Value *Arg, Instruction *TheCall,
   
   Function *Caller = TheCall->getParent()->getParent(); 
   
-  Value *NewAlloca = new AllocaInst(AggTy, 0, Align, Arg->getName(), 
+  Value *NewAlloca = new AllocaInst(AggTy, nullptr, Align, Arg->getName(), 
                                     &*Caller->begin()->begin());
-  // Emit a memcpy.
-  Type *Tys[3] = {VoidPtrTy, VoidPtrTy, Type::getInt64Ty(Context)};
-  Function *MemCpyFn = Intrinsic::getDeclaration(Caller->getParent(),
-                                                 Intrinsic::memcpy, 
-                                                 Tys);
-  Value *DestCast = new BitCastInst(NewAlloca, VoidPtrTy, "tmp", TheCall);
-  Value *SrcCast = new BitCastInst(Arg, VoidPtrTy, "tmp", TheCall);
-  
-  Value *Size;
-  if (IFI.TD == 0)
-    Size = ConstantExpr::getSizeOf(AggTy);
-  else
-    Size = ConstantInt::get(Type::getInt64Ty(Context),
-                            IFI.TD->getTypeStoreSize(AggTy));
-  
-  // Always generate a memcpy of alignment 1 here because we don't know
-  // the alignment of the src pointer.  Other optimizations can infer
-  // better alignment.
-  Value *CallArgs[] = {
-    DestCast, SrcCast, Size,
-    ConstantInt::get(Type::getInt32Ty(Context), 1),
-    ConstantInt::getFalse(Context) // isVolatile
-  };
-  IRBuilder<>(TheCall).CreateCall(MemCpyFn, CallArgs);
+  IFI.StaticAllocas.push_back(cast<AllocaInst>(NewAlloca));
   
   // Uses of the argument in the function should use our new alloca
   // instead.
@@ -709,9 +407,8 @@ static Value *HandleByValArgument(Value *Arg, Instruction *TheCall,
 // isUsedByLifetimeMarker - Check whether this Value is used by a lifetime
 // intrinsic.
 static bool isUsedByLifetimeMarker(Value *V) {
-  for (Value::use_iterator UI = V->use_begin(), UE = V->use_end(); UI != UE;
-       ++UI) {
-    if (IntrinsicInst *II = dyn_cast<IntrinsicInst>(*UI)) {
+  for (User *U : V->users()) {
+    if (IntrinsicInst *II = dyn_cast<IntrinsicInst>(U)) {
       switch (II->getIntrinsicID()) {
       default: break;
       case Intrinsic::lifetime_start:
@@ -726,23 +423,24 @@ static bool isUsedByLifetimeMarker(Value *V) {
 // hasLifetimeMarkers - Check whether the given alloca already has
 // lifetime.start or lifetime.end intrinsics.
 static bool hasLifetimeMarkers(AllocaInst *AI) {
-  Type *Int8PtrTy = Type::getInt8PtrTy(AI->getType()->getContext());
-  if (AI->getType() == Int8PtrTy)
+  Type *Ty = AI->getType();
+  Type *Int8PtrTy = Type::getInt8PtrTy(Ty->getContext(),
+                                       Ty->getPointerAddressSpace());
+  if (Ty == Int8PtrTy)
     return isUsedByLifetimeMarker(AI);
 
   // Do a scan to find all the casts to i8*.
-  for (Value::use_iterator I = AI->use_begin(), E = AI->use_end(); I != E;
-       ++I) {
-    if (I->getType() != Int8PtrTy) continue;
-    if (I->stripPointerCasts() != AI) continue;
-    if (isUsedByLifetimeMarker(*I))
+  for (User *U : AI->users()) {
+    if (U->getType() != Int8PtrTy) continue;
+    if (U->stripPointerCasts() != AI) continue;
+    if (isUsedByLifetimeMarker(U))
       return true;
   }
   return false;
 }
 
-/// updateInlinedAtInfo - Helper function used by fixupLineNumbers to recursively
-/// update InlinedAtEntry of a DebugLoc.
+/// updateInlinedAtInfo - Helper function used by fixupLineNumbers to
+/// recursively update InlinedAtEntry of a DebugLoc.
 static DebugLoc updateInlinedAtInfo(const DebugLoc &DL, 
                                     const DebugLoc &InlinedAtDL,
                                     LLVMContext &Ctx) {
@@ -752,16 +450,15 @@ static DebugLoc updateInlinedAtInfo(const DebugLoc &DL,
     return DebugLoc::get(DL.getLine(), DL.getCol(), DL.getScope(Ctx),
                          NewInlinedAtDL.getAsMDNode(Ctx));
   }
-                                             
+
   return DebugLoc::get(DL.getLine(), DL.getCol(), DL.getScope(Ctx),
                        InlinedAtDL.getAsMDNode(Ctx));
 }
 
-
 /// fixupLineNumbers - Update inlined instructions' line numbers to 
 /// to encode location where these instructions are inlined.
 static void fixupLineNumbers(Function *Fn, Function::iterator FI,
-                              Instruction *TheCall) {
+                             Instruction *TheCall) {
   DebugLoc TheCallDL = TheCall->getDebugLoc();
   if (TheCallDL.isUnknown())
     return;
@@ -770,24 +467,64 @@ static void fixupLineNumbers(Function *Fn, Function::iterator FI,
     for (BasicBlock::iterator BI = FI->begin(), BE = FI->end();
          BI != BE; ++BI) {
       DebugLoc DL = BI->getDebugLoc();
-      if (!DL.isUnknown())
+      if (DL.isUnknown()) {
+        // If the inlined instruction has no line number, make it look as if it
+        // originates from the call location. This is important for
+        // ((__always_inline__, __nodebug__)) functions which must use caller
+        // location for all instructions in their function body.
+        BI->setDebugLoc(TheCallDL);
+      } else {
         BI->setDebugLoc(updateInlinedAtInfo(DL, TheCallDL, BI->getContext()));
+        if (DbgValueInst *DVI = dyn_cast<DbgValueInst>(BI)) {
+          LLVMContext &Ctx = BI->getContext();
+          MDNode *InlinedAt = BI->getDebugLoc().getInlinedAt(Ctx);
+          DVI->setOperand(2, createInlinedVariable(DVI->getVariable(), 
+                                                   InlinedAt, Ctx));
+        }
+      }
     }
   }
 }
 
-// InlineFunction - This function inlines the called function into the basic
-// block of the caller.  This returns false if it is not possible to inline this
-// call.  The program is still in a well defined state if this occurs though.
-//
-// Note that this only does one level of inlining.  For example, if the
-// instruction 'call B' is inlined, and 'B' calls 'C', then the call to 'C' now
-// exists in the instruction stream.  Similarly this will inline a recursive
-// function by one level.
-//
-bool llvm::InlineFunction(CallSite CS, InlineFunctionInfo &IFI) {
+/// Returns a musttail call instruction if one immediately precedes the given
+/// return instruction with an optional bitcast instruction between them.
+static CallInst *getPrecedingMustTailCall(ReturnInst *RI) {
+  Instruction *Prev = RI->getPrevNode();
+  if (!Prev)
+    return nullptr;
+
+  if (Value *RV = RI->getReturnValue()) {
+    if (RV != Prev)
+      return nullptr;
+
+    // Look through the optional bitcast.
+    if (auto *BI = dyn_cast<BitCastInst>(Prev)) {
+      RV = BI->getOperand(0);
+      Prev = BI->getPrevNode();
+      if (!Prev || RV != Prev)
+        return nullptr;
+    }
+  }
+
+  if (auto *CI = dyn_cast<CallInst>(Prev)) {
+    if (CI->isMustTailCall())
+      return CI;
+  }
+  return nullptr;
+}
+
+/// InlineFunction - This function inlines the called function into the basic
+/// block of the caller.  This returns false if it is not possible to inline
+/// this call.  The program is still in a well defined state if this occurs
+/// though.
+///
+/// Note that this only does one level of inlining.  For example, if the
+/// instruction 'call B' is inlined, and 'B' calls 'C', then the call to 'C' now
+/// exists in the instruction stream.  Similarly this will inline a recursive
+/// function by one level.
+bool llvm::InlineFunction(CallSite CS, InlineFunctionInfo &IFI,
+                          bool InsertLifetime) {
   Instruction *TheCall = CS.getInstruction();
-  LLVMContext &Context = TheCall->getContext();
   assert(TheCall->getParent() && TheCall->getParent()->getParent() &&
          "Instruction not in function!");
 
@@ -795,15 +532,10 @@ bool llvm::InlineFunction(CallSite CS, InlineFunctionInfo &IFI) {
   IFI.reset();
   
   const Function *CalledFunc = CS.getCalledFunction();
-  if (CalledFunc == 0 ||          // Can't inline external function or indirect
+  if (!CalledFunc ||              // Can't inline external function or indirect
       CalledFunc->isDeclaration() || // call, or call to a vararg function!
       CalledFunc->getFunctionType()->isVarArg()) return false;
 
-  // If the call to the callee is not a tail call, we must clear the 'tail'
-  // flags on any calls that we inline.
-  bool MustClearTailCallFlags =
-    !(isa<CallInst>(TheCall) && cast<CallInst>(TheCall)->isTailCall());
-
   // If the call to the callee cannot throw, set the 'nounwind' flag on any
   // calls that we inline.
   bool MarkNoUnwind = CS.doesNotThrow();
@@ -822,9 +554,40 @@ bool llvm::InlineFunction(CallSite CS, InlineFunctionInfo &IFI) {
       return false;
   }
 
+  // Get the personality function from the callee if it contains a landing pad.
+  Value *CalleePersonality = nullptr;
+  for (Function::const_iterator I = CalledFunc->begin(), E = CalledFunc->end();
+       I != E; ++I)
+    if (const InvokeInst *II = dyn_cast<InvokeInst>(I->getTerminator())) {
+      const BasicBlock *BB = II->getUnwindDest();
+      const LandingPadInst *LP = BB->getLandingPadInst();
+      CalleePersonality = LP->getPersonalityFn();
+      break;
+    }
+
+  // Find the personality function used by the landing pads of the caller. If it
+  // exists, then check to see that it matches the personality function used in
+  // the callee.
+  if (CalleePersonality) {
+    for (Function::const_iterator I = Caller->begin(), E = Caller->end();
+         I != E; ++I)
+      if (const InvokeInst *II = dyn_cast<InvokeInst>(I->getTerminator())) {
+        const BasicBlock *BB = II->getUnwindDest();
+        const LandingPadInst *LP = BB->getLandingPadInst();
+
+        // If the personality functions match, then we can perform the
+        // inlining. Otherwise, we can't inline.
+        // TODO: This isn't 100% true. Some personality functions are proper
+        //       supersets of others and can be used in place of the other.
+        if (LP->getPersonalityFn() != CalleePersonality)
+          return false;
+
+        break;
+      }
+  }
+
   // Get an iterator to the last basic block in the function, which will have
   // the new function inlined after it.
-  //
   Function::iterator LastBlock = &Caller->back();
 
   // Make sure to capture all of the return instructions from the cloned
@@ -835,6 +598,8 @@ bool llvm::InlineFunction(CallSite CS, InlineFunctionInfo &IFI) {
 
   { // Scope to destroy VMap after cloning.
     ValueToValueMapTy VMap;
+    // Keep a list of pair (dst, src) to emit byval initializations.
+    SmallVector<std::pair<Value*, Value*>, 4> ByValInit;
 
     assert(CalledFunc->arg_size() == CS.arg_size() &&
            "No varargs calls can be inlined!");
@@ -851,14 +616,11 @@ bool llvm::InlineFunction(CallSite CS, InlineFunctionInfo &IFI) {
       // by them explicit.  However, we don't do this if the callee is readonly
       // or readnone, because the copy would be unneeded: the callee doesn't
       // modify the struct.
-      if (CalledFunc->paramHasAttr(ArgNo+1, Attribute::ByVal)) {
+      if (CS.isByValArgument(ArgNo)) {
         ActualArg = HandleByValArgument(ActualArg, TheCall, CalledFunc, IFI,
                                         CalledFunc->getParamAlignment(ArgNo+1));
-        // Calls that we inline may use the new alloca, so we need to clear
-        // their 'tail' flags if HandleByValArgument introduced a new alloca and
-        // the callee has calls.
-        MustClearTailCallFlags |= ActualArg != *AI;
+        if (ActualArg != *AI)
+          ByValInit.push_back(std::make_pair(ActualArg, (Value*) *AI));
       }
 
       VMap[I] = ActualArg;
@@ -870,11 +632,16 @@ bool llvm::InlineFunction(CallSite CS, InlineFunctionInfo &IFI) {
     // happy with whatever the cloner can do.
     CloneAndPruneFunctionInto(Caller, CalledFunc, VMap, 
                               /*ModuleLevelChanges=*/false, Returns, ".i",
-                              &InlinedFunctionInfo, IFI.TD, TheCall);
+                              &InlinedFunctionInfo, IFI.DL, TheCall);
 
     // Remember the first block that is newly cloned over.
     FirstNewBlock = LastBlock; ++FirstNewBlock;
 
+    // Inject byval arguments initialization.
+    for (std::pair<Value*, Value*> &Init : ByValInit)
+      HandleByValArgumentInit(Init.first, Init.second, Caller->getParent(),
+                              FirstNewBlock, IFI);
+
     // Update the callgraph if requested.
     if (IFI.CG)
       UpdateCallGraphAfterInlining(CS, FirstNewBlock, VMap, IFI);
@@ -887,13 +654,12 @@ bool llvm::InlineFunction(CallSite CS, InlineFunctionInfo &IFI) {
   // block for the callee, move them to the entry block of the caller.  First
   // calculate which instruction they should be inserted before.  We insert the
   // instructions at the end of the current alloca list.
-  //
   {
     BasicBlock::iterator InsertPoint = Caller->begin()->begin();
     for (BasicBlock::iterator I = FirstNewBlock->begin(),
          E = FirstNewBlock->end(); I != E; ) {
       AllocaInst *AI = dyn_cast<AllocaInst>(I++);
-      if (AI == 0) continue;
+      if (!AI) continue;
       
       // If the alloca is now dead, remove it.  This often occurs due to code
       // specialization.
@@ -925,9 +691,48 @@ bool llvm::InlineFunction(CallSite CS, InlineFunctionInfo &IFI) {
     }
   }
 
+  bool InlinedMustTailCalls = false;
+  if (InlinedFunctionInfo.ContainsCalls) {
+    CallInst::TailCallKind CallSiteTailKind = CallInst::TCK_None;
+    if (CallInst *CI = dyn_cast<CallInst>(TheCall))
+      CallSiteTailKind = CI->getTailCallKind();
+
+    for (Function::iterator BB = FirstNewBlock, E = Caller->end(); BB != E;
+         ++BB) {
+      for (Instruction &I : *BB) {
+        CallInst *CI = dyn_cast<CallInst>(&I);
+        if (!CI)
+          continue;
+
+        // We need to reduce the strength of any inlined tail calls.  For
+        // musttail, we have to avoid introducing potential unbounded stack
+        // growth.  For example, if functions 'f' and 'g' are mutually recursive
+        // with musttail, we can inline 'g' into 'f' so long as we preserve
+        // musttail on the cloned call to 'f'.  If either the inlined call site
+        // or the cloned call site is *not* musttail, the program already has
+        // one frame of stack growth, so it's safe to remove musttail.  Here is
+        // a table of example transformations:
+        //
+        //    f -> musttail g -> musttail f  ==>  f -> musttail f
+        //    f -> musttail g ->     tail f  ==>  f ->     tail f
+        //    f ->          g -> musttail f  ==>  f ->          f
+        //    f ->          g ->     tail f  ==>  f ->          f
+        CallInst::TailCallKind ChildTCK = CI->getTailCallKind();
+        ChildTCK = std::min(CallSiteTailKind, ChildTCK);
+        CI->setTailCallKind(ChildTCK);
+        InlinedMustTailCalls |= CI->isMustTailCall();
+
+        // Calls inlined through a 'nounwind' call site should be marked
+        // 'nounwind'.
+        if (MarkNoUnwind)
+          CI->setDoesNotThrow();
+      }
+    }
+  }
+
   // Leave lifetime markers for the static alloca's, scoping them to the
   // function we just inlined.
-  if (!IFI.StaticAllocas.empty()) {
+  if (InsertLifetime && !IFI.StaticAllocas.empty()) {
     IRBuilder<> builder(FirstNewBlock->begin());
     for (unsigned ai = 0, ae = IFI.StaticAllocas.size(); ai != ae; ++ai) {
       AllocaInst *AI = IFI.StaticAllocas[ai];
@@ -937,10 +742,32 @@ bool llvm::InlineFunction(CallSite CS, InlineFunctionInfo &IFI) {
       if (hasLifetimeMarkers(AI))
         continue;
 
-      builder.CreateLifetimeStart(AI);
-      for (unsigned ri = 0, re = Returns.size(); ri != re; ++ri) {
-        IRBuilder<> builder(Returns[ri]);
-        builder.CreateLifetimeEnd(AI);
+      // Try to determine the size of the allocation.
+      ConstantInt *AllocaSize = nullptr;
+      if (ConstantInt *AIArraySize =
+          dyn_cast<ConstantInt>(AI->getArraySize())) {
+        if (IFI.DL) {
+          Type *AllocaType = AI->getAllocatedType();
+          uint64_t AllocaTypeSize = IFI.DL->getTypeAllocSize(AllocaType);
+          uint64_t AllocaArraySize = AIArraySize->getLimitedValue();
+          assert(AllocaArraySize > 0 && "array size of AllocaInst is zero");
+          // Check that array size doesn't saturate uint64_t and doesn't
+          // overflow when it's multiplied by type size.
+          if (AllocaArraySize != ~0ULL &&
+              UINT64_MAX / AllocaArraySize >= AllocaTypeSize) {
+            AllocaSize = ConstantInt::get(Type::getInt64Ty(AI->getContext()),
+                                          AllocaArraySize * AllocaTypeSize);
+          }
+        }
+      }
+
+      builder.CreateLifetimeStart(AI, AllocaSize);
+      for (ReturnInst *RI : Returns) {
+        // Don't insert llvm.lifetime.end calls between a musttail call and a
+        // return.  The return kills all local allocas.
+        if (InlinedMustTailCalls && getPrecedingMustTailCall(RI))
+          continue;
+        IRBuilder<>(RI).CreateLifetimeEnd(AI, AllocaSize);
       }
     }
   }
@@ -959,59 +786,55 @@ bool llvm::InlineFunction(CallSite CS, InlineFunctionInfo &IFI) {
 
     // Insert a call to llvm.stackrestore before any return instructions in the
     // inlined function.
-    for (unsigned i = 0, e = Returns.size(); i != e; ++i) {
-      IRBuilder<>(Returns[i]).CreateCall(StackRestore, SavedPtr);
-    }
-
-    // Count the number of StackRestore calls we insert.
-    unsigned NumStackRestores = Returns.size();
-
-    // If we are inlining an invoke instruction, insert restores before each
-    // unwind.  These unwinds will be rewritten into branches later.
-    if (InlinedFunctionInfo.ContainsUnwinds && isa<InvokeInst>(TheCall)) {
-      for (Function::iterator BB = FirstNewBlock, E = Caller->end();
-           BB != E; ++BB)
-        if (UnwindInst *UI = dyn_cast<UnwindInst>(BB->getTerminator())) {
-          IRBuilder<>(UI).CreateCall(StackRestore, SavedPtr);
-          ++NumStackRestores;
-        }
+    for (ReturnInst *RI : Returns) {
+      // Don't insert llvm.stackrestore calls between a musttail call and a
+      // return.  The return will restore the stack pointer.
+      if (InlinedMustTailCalls && getPrecedingMustTailCall(RI))
+        continue;
+      IRBuilder<>(RI).CreateCall(StackRestore, SavedPtr);
     }
   }
 
-  // If we are inlining tail call instruction through a call site that isn't
-  // marked 'tail', we must remove the tail marker for any calls in the inlined
-  // code.  Also, calls inlined through a 'nounwind' call site should be marked
-  // 'nounwind'.
-  if (InlinedFunctionInfo.ContainsCalls &&
-      (MustClearTailCallFlags || MarkNoUnwind)) {
-    for (Function::iterator BB = FirstNewBlock, E = Caller->end();
-         BB != E; ++BB)
-      for (BasicBlock::iterator I = BB->begin(), E = BB->end(); I != E; ++I)
-        if (CallInst *CI = dyn_cast<CallInst>(I)) {
-          if (MustClearTailCallFlags)
-            CI->setTailCall(false);
-          if (MarkNoUnwind)
-            CI->setDoesNotThrow();
-        }
-  }
+  // If we are inlining for an invoke instruction, we must make sure to rewrite
+  // any call instructions into invoke instructions.
+  if (InvokeInst *II = dyn_cast<InvokeInst>(TheCall))
+    HandleInlinedInvoke(II, FirstNewBlock, InlinedFunctionInfo);
 
-  // If we are inlining through a 'nounwind' call site then any inlined 'unwind'
-  // instructions are unreachable.
-  if (InlinedFunctionInfo.ContainsUnwinds && MarkNoUnwind)
-    for (Function::iterator BB = FirstNewBlock, E = Caller->end();
-         BB != E; ++BB) {
-      TerminatorInst *Term = BB->getTerminator();
-      if (isa<UnwindInst>(Term)) {
-        new UnreachableInst(Context, Term);
-        BB->getInstList().erase(Term);
+  // Handle any inlined musttail call sites.  In order for a new call site to be
+  // musttail, the source of the clone and the inlined call site must have been
+  // musttail.  Therefore it's safe to return without merging control into the
+  // phi below.
+  if (InlinedMustTailCalls) {
+    // Check if we need to bitcast the result of any musttail calls.
+    Type *NewRetTy = Caller->getReturnType();
+    bool NeedBitCast = !TheCall->use_empty() && TheCall->getType() != NewRetTy;
+
+    // Handle the returns preceded by musttail calls separately.
+    SmallVector<ReturnInst *, 8> NormalReturns;
+    for (ReturnInst *RI : Returns) {
+      CallInst *ReturnedMustTail = getPrecedingMustTailCall(RI);
+      if (!ReturnedMustTail) {
+        NormalReturns.push_back(RI);
+        continue;
       }
+      if (!NeedBitCast)
+        continue;
+
+      // Delete the old return and any preceding bitcast.
+      BasicBlock *CurBB = RI->getParent();
+      auto *OldCast = dyn_cast_or_null<BitCastInst>(RI->getReturnValue());
+      RI->eraseFromParent();
+      if (OldCast)
+        OldCast->eraseFromParent();
+
+      // Insert a new bitcast and return with the right type.
+      IRBuilder<> Builder(CurBB);
+      Builder.CreateRet(Builder.CreateBitCast(ReturnedMustTail, NewRetTy));
     }
 
-  // If we are inlining for an invoke instruction, we must make sure to rewrite
-  // any inlined 'unwind' instructions into branches to the invoke exception
-  // destination, and call instructions into invoke instructions.
-  if (InvokeInst *II = dyn_cast<InvokeInst>(TheCall))
-    HandleInlinedInvoke(II, FirstNewBlock, InlinedFunctionInfo);
+    // Leave behind the normal returns so we can merge control flow.
+    std::swap(Returns, NormalReturns);
+  }
 
   // If we cloned in _exactly one_ basic block, and if that block ends in a
   // return instruction, we splice the body of the inlined callee directly into
@@ -1025,8 +848,10 @@ bool llvm::InlineFunction(CallSite CS, InlineFunctionInfo &IFI) {
 
     // If the call site was an invoke instruction, add a branch to the normal
     // destination.
-    if (InvokeInst *II = dyn_cast<InvokeInst>(TheCall))
-      BranchInst::Create(II->getNormalDest(), TheCall);
+    if (InvokeInst *II = dyn_cast<InvokeInst>(TheCall)) {
+      BranchInst *NewBr = BranchInst::Create(II->getNormalDest(), TheCall);
+      NewBr->setDebugLoc(Returns[0]->getDebugLoc());
+    }
 
     // If the return instruction returned a value, replace uses of the call with
     // uses of the returned value.
@@ -1054,15 +879,16 @@ bool llvm::InlineFunction(CallSite CS, InlineFunctionInfo &IFI) {
   // "starter" and "ender" blocks.  How we accomplish this depends on whether
   // this is an invoke instruction or a call instruction.
   BasicBlock *AfterCallBB;
+  BranchInst *CreatedBranchToNormalDest = nullptr;
   if (InvokeInst *II = dyn_cast<InvokeInst>(TheCall)) {
 
     // Add an unconditional branch to make this look like the CallInst case...
-    BranchInst *NewBr = BranchInst::Create(II->getNormalDest(), TheCall);
+    CreatedBranchToNormalDest = BranchInst::Create(II->getNormalDest(), TheCall);
 
     // Split the basic block.  This guarantees that no PHI nodes will have to be
     // updated due to new incoming edges, and make the invoke case more
     // symmetric to the call case.
-    AfterCallBB = OrigBB->splitBasicBlock(NewBr,
+    AfterCallBB = OrigBB->splitBasicBlock(CreatedBranchToNormalDest,
                                           CalledFunc->getName()+".exit");
 
   } else {  // It's a call
@@ -1092,7 +918,7 @@ bool llvm::InlineFunction(CallSite CS, InlineFunctionInfo &IFI) {
   // any users of the original call/invoke instruction.
   Type *RTy = CalledFunc->getReturnType();
 
-  PHINode *PHI = 0;
+  PHINode *PHI = nullptr;
   if (Returns.size() > 1) {
     // The PHI node should go at the front of the new basic block to merge all
     // possible incoming values.
@@ -1117,11 +943,20 @@ bool llvm::InlineFunction(CallSite CS, InlineFunctionInfo &IFI) {
 
 
     // Add a branch to the merge points and remove return instructions.
+    DebugLoc Loc;
     for (unsigned i = 0, e = Returns.size(); i != e; ++i) {
       ReturnInst *RI = Returns[i];
-      BranchInst::Create(AfterCallBB, RI);
+      BranchInst* BI = BranchInst::Create(AfterCallBB, RI);
+      Loc = RI->getDebugLoc();
+      BI->setDebugLoc(Loc);
       RI->eraseFromParent();
     }
+    // We need to set the debug location to *somewhere* inside the
+    // inlined function. The line number may be nonsensical, but the
+    // instruction will at least be associated with the right
+    // function.
+    if (CreatedBranchToNormalDest)
+      CreatedBranchToNormalDest->setDebugLoc(Loc);
   } else if (!Returns.empty()) {
     // Otherwise, if there is exactly one return value, just replace anything
     // using the return value of the call with the computed value.
@@ -1141,6 +976,9 @@ bool llvm::InlineFunction(CallSite CS, InlineFunctionInfo &IFI) {
     AfterCallBB->getInstList().splice(AfterCallBB->begin(),
                                       ReturnBB->getInstList());
 
+    if (CreatedBranchToNormalDest)
+      CreatedBranchToNormalDest->setDebugLoc(Returns[0]->getDebugLoc());
+
     // Delete the return instruction now and empty ReturnBB now.
     Returns[0]->eraseFromParent();
     ReturnBB->eraseFromParent();
@@ -1153,6 +991,11 @@ bool llvm::InlineFunction(CallSite CS, InlineFunctionInfo &IFI) {
   // Since we are now done with the Call/Invoke, we can delete it.
   TheCall->eraseFromParent();
 
+  // If we inlined any musttail calls and the original return is now
+  // unreachable, delete it.  It can only contain a bitcast and ret.
+  if (InlinedMustTailCalls && pred_begin(AfterCallBB) == pred_end(AfterCallBB))
+    AfterCallBB->eraseFromParent();
+
   // We should always be able to fold the entry block of the function into the
   // single predecessor of the block...
   assert(cast<BranchInst>(Br)->isUnconditional() && "splitBasicBlock broken!");
@@ -1172,11 +1015,12 @@ bool llvm::InlineFunction(CallSite CS, InlineFunctionInfo &IFI) {
   // If we inserted a phi node, check to see if it has a single value (e.g. all
   // the entries are the same or undef).  If so, remove the PHI so it doesn't
   // block other optimizations.
-  if (PHI)
-    if (Value *V = SimplifyInstruction(PHI, IFI.TD)) {
+  if (PHI) {
+    if (Value *V = SimplifyInstruction(PHI, IFI.DL)) {
       PHI->replaceAllUsesWith(V);
       PHI->eraseFromParent();
     }
+  }
 
   return true;
 }