index 9729687a83eff584d3aaf1d630ef2ef4ac6c2382..e2ba0473fd15a161cc89d1c7976ab9c56160a65b 100644 (file)
//===----------------------------------------------------------------------===//
#include "llvm/Transforms/Utils/Local.h"
-#include "llvm/Constants.h"
-#include "llvm/DIBuilder.h"
-#include "llvm/DebugInfo.h"
-#include "llvm/DerivedTypes.h"
-#include "llvm/GlobalAlias.h"
-#include "llvm/GlobalVariable.h"
-#include "llvm/IRBuilder.h"
-#include "llvm/Instructions.h"
-#include "llvm/IntrinsicInst.h"
-#include "llvm/Intrinsics.h"
-#include "llvm/MDBuilder.h"
-#include "llvm/Metadata.h"
-#include "llvm/Operator.h"
#include "llvm/ADT/DenseMap.h"
+#include "llvm/ADT/STLExtras.h"
#include "llvm/ADT/SmallPtrSet.h"
-#include "llvm/Analysis/Dominators.h"
+#include "llvm/ADT/Statistic.h"
#include "llvm/Analysis/InstructionSimplify.h"
#include "llvm/Analysis/MemoryBuiltins.h"
-#include "llvm/Analysis/ProfileInfo.h"
#include "llvm/Analysis/ValueTracking.h"
-#include "llvm/Support/CFG.h"
+#include "llvm/IR/CFG.h"
+#include "llvm/IR/Constants.h"
+#include "llvm/IR/DIBuilder.h"
+#include "llvm/IR/DataLayout.h"
+#include "llvm/IR/DebugInfo.h"
+#include "llvm/IR/DerivedTypes.h"
+#include "llvm/IR/Dominators.h"
+#include "llvm/IR/GetElementPtrTypeIterator.h"
+#include "llvm/IR/GlobalAlias.h"
+#include "llvm/IR/GlobalVariable.h"
+#include "llvm/IR/IRBuilder.h"
+#include "llvm/IR/Instructions.h"
+#include "llvm/IR/IntrinsicInst.h"
+#include "llvm/IR/Intrinsics.h"
+#include "llvm/IR/MDBuilder.h"
+#include "llvm/IR/Metadata.h"
+#include "llvm/IR/Operator.h"
+#include "llvm/IR/ValueHandle.h"
#include "llvm/Support/Debug.h"
-#include "llvm/Support/GetElementPtrTypeIterator.h"
#include "llvm/Support/MathExtras.h"
-#include "llvm/Support/ValueHandle.h"
#include "llvm/Support/raw_ostream.h"
-#include "llvm/DataLayout.h"
using namespace llvm;
+#define DEBUG_TYPE "local"
+
+STATISTIC(NumRemoved, "Number of unreachable basic blocks removed");
+
//===----------------------------------------------------------------------===//
// Local constant propagation.
//
BI->eraseFromParent();
return true;
}
-
+
if (Dest2 == Dest1) { // Conditional branch to same location?
// This branch matches something like this:
// br bool %cond, label %Dest, label %Dest
}
return false;
}
-
+
if (SwitchInst *SI = dyn_cast<SwitchInst>(T)) {
// If we are switching on a constant, we can convert the switch into a
// single branch instruction!
// dest. If so, eliminate it as an explicit compare.
if (i.getCaseSuccessor() == DefaultDest) {
MDNode* MD = SI->getMetadata(LLVMContext::MD_prof);
- // MD should have 2 + NumCases operands.
- if (MD && MD->getNumOperands() == 2 + SI->getNumCases()) {
+ unsigned NCases = SI->getNumCases();
+ // Fold the case metadata into the default if there will be any branches
+ // left, unless the metadata doesn't match the switch.
+ if (NCases > 1 && MD && MD->getNumOperands() == 2 + NCases) {
// Collect branch weights into a vector.
SmallVector<uint32_t, 8> Weights;
for (unsigned MD_i = 1, MD_e = MD->getNumOperands(); MD_i < MD_e;
RecursivelyDeleteTriviallyDeadInstructions(Cond, TLI);
return true;
}
-
+
if (SI->getNumCases() == 1) {
// Otherwise, we can fold this switch into a conditional branch
// instruction if it has only one non-default destination.
SwitchInst::CaseIt FirstCase = SI->case_begin();
- IntegersSubset& Case = FirstCase.getCaseValueEx();
- if (Case.isSingleNumber()) {
- // FIXME: Currently work with ConstantInt based numbers.
- Value *Cond = Builder.CreateICmpEQ(SI->getCondition(),
- Case.getSingleNumber(0).toConstantInt(),
- "cond");
-
- // Insert the new branch.
- BranchInst *NewBr = Builder.CreateCondBr(Cond,
- FirstCase.getCaseSuccessor(),
- SI->getDefaultDest());
- MDNode* MD = SI->getMetadata(LLVMContext::MD_prof);
- if (MD && MD->getNumOperands() == 3) {
- ConstantInt *SICase = dyn_cast<ConstantInt>(MD->getOperand(2));
- ConstantInt *SIDef = dyn_cast<ConstantInt>(MD->getOperand(1));
- assert(SICase && SIDef);
- // The TrueWeight should be the weight for the single case of SI.
- NewBr->setMetadata(LLVMContext::MD_prof,
- MDBuilder(BB->getContext()).
- createBranchWeights(SICase->getValue().getZExtValue(),
- SIDef->getValue().getZExtValue()));
- }
+ Value *Cond = Builder.CreateICmpEQ(SI->getCondition(),
+ FirstCase.getCaseValue(), "cond");
- // Delete the old switch.
- SI->eraseFromParent();
- return true;
+ // Insert the new branch.
+ BranchInst *NewBr = Builder.CreateCondBr(Cond,
+ FirstCase.getCaseSuccessor(),
+ SI->getDefaultDest());
+ MDNode* MD = SI->getMetadata(LLVMContext::MD_prof);
+ if (MD && MD->getNumOperands() == 3) {
+ ConstantInt *SICase = dyn_cast<ConstantInt>(MD->getOperand(2));
+ ConstantInt *SIDef = dyn_cast<ConstantInt>(MD->getOperand(1));
+ assert(SICase && SIDef);
+ // The TrueWeight should be the weight for the single case of SI.
+ NewBr->setMetadata(LLVMContext::MD_prof,
+ MDBuilder(BB->getContext()).
+ createBranchWeights(SICase->getValue().getZExtValue(),
+ SIDef->getValue().getZExtValue()));
}
+
+ // Delete the old switch.
+ SI->eraseFromParent();
+ return true;
}
return false;
}
BasicBlock *TheOnlyDest = BA->getBasicBlock();
// Insert the new branch.
Builder.CreateBr(TheOnlyDest);
-
+
for (unsigned i = 0, e = IBI->getNumDestinations(); i != e; ++i) {
if (IBI->getDestination(i) == TheOnlyDest)
TheOnlyDest = 0;
IBI->eraseFromParent();
if (DeleteDeadConditions)
RecursivelyDeleteTriviallyDeadInstructions(Address, TLI);
-
+
// If we didn't find our destination in the IBI successor list, then we
// have undefined behavior. Replace the unconditional branch with an
// 'unreachable' instruction.
BB->getTerminator()->eraseFromParent();
new UnreachableInst(BB->getContext(), BB);
}
-
+
return true;
}
}
-
+
return false;
}
Instruction *I = dyn_cast<Instruction>(V);
if (!I || !I->use_empty() || !isInstructionTriviallyDead(I, TLI))
return false;
-
+
SmallVector<Instruction*, 16> DeadInsts;
DeadInsts.push_back(I);
-
+
do {
I = DeadInsts.pop_back_val();
for (unsigned i = 0, e = I->getNumOperands(); i != e; ++i) {
Value *OpV = I->getOperand(i);
I->setOperand(i, 0);
-
+
if (!OpV->use_empty()) continue;
-
+
// If the operand is an instruction that became dead as we nulled out the
// operand, and if it is 'trivially' dead, delete it in a future loop
// iteration.
if (isInstructionTriviallyDead(OpI, TLI))
DeadInsts.push_back(OpI);
}
-
+
I->eraseFromParent();
} while (!DeadInsts.empty());
/// true when there are no uses or multiple uses that all refer to the same
/// value.
static bool areAllUsesEqual(Instruction *I) {
- Value::use_iterator UI = I->use_begin();
- Value::use_iterator UE = I->use_end();
+ Value::user_iterator UI = I->user_begin();
+ Value::user_iterator UE = I->user_end();
if (UI == UE)
return true;
const TargetLibraryInfo *TLI) {
SmallPtrSet<Instruction*, 4> Visited;
for (Instruction *I = PN; areAllUsesEqual(I) && !I->mayHaveSideEffects();
- I = cast<Instruction>(*I->use_begin())) {
+ I = cast<Instruction>(*I->user_begin())) {
if (I->use_empty())
return RecursivelyDeleteTriviallyDeadInstructions(I, TLI);
Instruction *Inst = BI++;
WeakVH BIHandle(BI);
- if (recursivelySimplifyInstruction(Inst, TD)) {
+ if (recursivelySimplifyInstruction(Inst, TD, TLI)) {
MadeChange = true;
if (BIHandle != BI)
BI = BB->begin();
// This only adjusts blocks with PHI nodes.
if (!isa<PHINode>(BB->begin()))
return;
-
+
// Remove the entries for Pred from the PHI nodes in BB, but do not simplify
// them down. This will leave us with single entry phi nodes and other phis
// that can be removed.
BB->removePredecessor(Pred, true);
-
+
WeakVH PhiIt = &BB->front();
while (PHINode *PN = dyn_cast<PHINode>(PhiIt)) {
PhiIt = &*++BasicBlock::iterator(cast<Instruction>(PhiIt));
PN->replaceAllUsesWith(NewVal);
PN->eraseFromParent();
}
-
+
BasicBlock *PredBB = DestBB->getSinglePredecessor();
assert(PredBB && "Block doesn't have a single predecessor!");
-
+
// Zap anything that took the address of DestBB. Not doing this will give the
// address an invalid value.
if (DestBB->hasAddressTaken()) {
BA->getType()));
BA->destroyConstant();
}
-
+
// Anything that branched to PredBB now branches to DestBB.
PredBB->replaceAllUsesWith(DestBB);
-
+
// Splice all the instructions from PredBB to DestBB.
PredBB->getTerminator()->eraseFromParent();
DestBB->getInstList().splice(DestBB->begin(), PredBB->getInstList());
if (P) {
- DominatorTree *DT = P->getAnalysisIfAvailable<DominatorTree>();
- if (DT) {
- BasicBlock *PredBBIDom = DT->getNode(PredBB)->getIDom()->getBlock();
- DT->changeImmediateDominator(DestBB, PredBBIDom);
- DT->eraseNode(PredBB);
- }
- ProfileInfo *PI = P->getAnalysisIfAvailable<ProfileInfo>();
- if (PI) {
- PI->replaceAllUses(PredBB, DestBB);
- PI->removeEdge(ProfileInfo::getEdge(PredBB, DestBB));
+ if (DominatorTreeWrapperPass *DTWP =
+ P->getAnalysisIfAvailable<DominatorTreeWrapperPass>()) {
+ DominatorTree &DT = DTWP->getDomTree();
+ BasicBlock *PredBBIDom = DT.getNode(PredBB)->getIDom()->getBlock();
+ DT.changeImmediateDominator(DestBB, PredBBIDom);
+ DT.eraseNode(PredBB);
}
}
// Nuke BB.
PredBB->eraseFromParent();
}
+/// CanMergeValues - Return true if we can choose one of these values to use
+/// in place of the other. Note that we will always choose the non-undef
+/// value to keep.
+static bool CanMergeValues(Value *First, Value *Second) {
+ return First == Second || isa<UndefValue>(First) || isa<UndefValue>(Second);
+}
+
/// CanPropagatePredecessorsForPHIs - Return true if we can fold BB, an
-/// almost-empty BB ending in an unconditional branch to Succ, into succ.
+/// almost-empty BB ending in an unconditional branch to Succ, into Succ.
///
/// Assumption: Succ is the single successor for BB.
///
static bool CanPropagatePredecessorsForPHIs(BasicBlock *BB, BasicBlock *Succ) {
assert(*succ_begin(BB) == Succ && "Succ is not successor of BB!");
- DEBUG(dbgs() << "Looking to fold " << BB->getName() << " into "
+ DEBUG(dbgs() << "Looking to fold " << BB->getName() << " into "
<< Succ->getName() << "\n");
// Shortcut, if there is only a single predecessor it must be BB and merging
// is always safe
@@ -554,9 +559,10 @@ static bool CanPropagatePredecessorsForPHIs(BasicBlock *BB, BasicBlock *Succ) {
for (unsigned PI = 0, PE = PN->getNumIncomingValues(); PI != PE; ++PI) {
BasicBlock *IBB = PN->getIncomingBlock(PI);
if (BBPreds.count(IBB) &&
- BBPN->getIncomingValueForBlock(IBB) != PN->getIncomingValue(PI)) {
- DEBUG(dbgs() << "Can't fold, phi node " << PN->getName() << " in "
- << Succ->getName() << " is conflicting with "
+ !CanMergeValues(BBPN->getIncomingValueForBlock(IBB),
+ PN->getIncomingValue(PI))) {
+ DEBUG(dbgs() << "Can't fold, phi node " << PN->getName() << " in "
+ << Succ->getName() << " is conflicting with "
<< BBPN->getName() << " with regard to common predecessor "
<< IBB->getName() << "\n");
return false;
// one for BB, in which case this phi node will not prevent the merging
// of the block.
BasicBlock *IBB = PN->getIncomingBlock(PI);
- if (BBPreds.count(IBB) && Val != PN->getIncomingValue(PI)) {
- DEBUG(dbgs() << "Can't fold, phi node " << PN->getName() << " in "
+ if (BBPreds.count(IBB) &&
+ !CanMergeValues(Val, PN->getIncomingValue(PI))) {
+ DEBUG(dbgs() << "Can't fold, phi node " << PN->getName() << " in "
<< Succ->getName() << " is conflicting with regard to common "
<< "predecessor " << IBB->getName() << "\n");
return false;
@@ -582,6 +589,139 @@ static bool CanPropagatePredecessorsForPHIs(BasicBlock *BB, BasicBlock *Succ) {
return true;
}
+typedef SmallVector<BasicBlock *, 16> PredBlockVector;
+typedef DenseMap<BasicBlock *, Value *> IncomingValueMap;
+
+/// \brief Determines the value to use as the phi node input for a block.
+///
+/// Select between \p OldVal any value that we know flows from \p BB
+/// to a particular phi on the basis of which one (if either) is not
+/// undef. Update IncomingValues based on the selected value.
+///
+/// \param OldVal The value we are considering selecting.
+/// \param BB The block that the value flows in from.
+/// \param IncomingValues A map from block-to-value for other phi inputs
+/// that we have examined.
+///
+/// \returns the selected value.
+static Value *selectIncomingValueForBlock(Value *OldVal, BasicBlock *BB,
+ IncomingValueMap &IncomingValues) {
+ if (!isa<UndefValue>(OldVal)) {
+ assert((!IncomingValues.count(BB) ||
+ IncomingValues.find(BB)->second == OldVal) &&
+ "Expected OldVal to match incoming value from BB!");
+
+ IncomingValues.insert(std::make_pair(BB, OldVal));
+ return OldVal;
+ }
+
+ IncomingValueMap::const_iterator It = IncomingValues.find(BB);
+ if (It != IncomingValues.end()) return It->second;
+
+ return OldVal;
+}
+
+/// \brief Create a map from block to value for the operands of a
+/// given phi.
+///
+/// Create a map from block to value for each non-undef value flowing
+/// into \p PN.
+///
+/// \param PN The phi we are collecting the map for.
+/// \param IncomingValues [out] The map from block to value for this phi.
+static void gatherIncomingValuesToPhi(PHINode *PN,
+ IncomingValueMap &IncomingValues) {
+ for (unsigned i = 0, e = PN->getNumIncomingValues(); i != e; ++i) {
+ BasicBlock *BB = PN->getIncomingBlock(i);
+ Value *V = PN->getIncomingValue(i);
+
+ if (!isa<UndefValue>(V))
+ IncomingValues.insert(std::make_pair(BB, V));
+ }
+}
+
+/// \brief Replace the incoming undef values to a phi with the values
+/// from a block-to-value map.
+///
+/// \param PN The phi we are replacing the undefs in.
+/// \param IncomingValues A map from block to value.
+static void replaceUndefValuesInPhi(PHINode *PN,
+ const IncomingValueMap &IncomingValues) {
+ for (unsigned i = 0, e = PN->getNumIncomingValues(); i != e; ++i) {
+ Value *V = PN->getIncomingValue(i);
+
+ if (!isa<UndefValue>(V)) continue;
+
+ BasicBlock *BB = PN->getIncomingBlock(i);
+ IncomingValueMap::const_iterator It = IncomingValues.find(BB);
+ if (It == IncomingValues.end()) continue;
+
+ PN->setIncomingValue(i, It->second);
+ }
+}
+
+/// \brief Replace a value flowing from a block to a phi with
+/// potentially multiple instances of that value flowing from the
+/// block's predecessors to the phi.
+///
+/// \param BB The block with the value flowing into the phi.
+/// \param BBPreds The predecessors of BB.
+/// \param PN The phi that we are updating.
+static void redirectValuesFromPredecessorsToPhi(BasicBlock *BB,
+ const PredBlockVector &BBPreds,
+ PHINode *PN) {
+ Value *OldVal = PN->removeIncomingValue(BB, false);
+ assert(OldVal && "No entry in PHI for Pred BB!");
+
+ IncomingValueMap IncomingValues;
+
+ // We are merging two blocks - BB, and the block containing PN - and
+ // as a result we need to redirect edges from the predecessors of BB
+ // to go to the block containing PN, and update PN
+ // accordingly. Since we allow merging blocks in the case where the
+ // predecessor and successor blocks both share some predecessors,
+ // and where some of those common predecessors might have undef
+ // values flowing into PN, we want to rewrite those values to be
+ // consistent with the non-undef values.
+
+ gatherIncomingValuesToPhi(PN, IncomingValues);
+
+ // If this incoming value is one of the PHI nodes in BB, the new entries
+ // in the PHI node are the entries from the old PHI.
+ if (isa<PHINode>(OldVal) && cast<PHINode>(OldVal)->getParent() == BB) {
+ PHINode *OldValPN = cast<PHINode>(OldVal);
+ for (unsigned i = 0, e = OldValPN->getNumIncomingValues(); i != e; ++i) {
+ // Note that, since we are merging phi nodes and BB and Succ might
+ // have common predecessors, we could end up with a phi node with
+ // identical incoming branches. This will be cleaned up later (and
+ // will trigger asserts if we try to clean it up now, without also
+ // simplifying the corresponding conditional branch).
+ BasicBlock *PredBB = OldValPN->getIncomingBlock(i);
+ Value *PredVal = OldValPN->getIncomingValue(i);
+ Value *Selected = selectIncomingValueForBlock(PredVal, PredBB,
+ IncomingValues);
+
+ // And add a new incoming value for this predecessor for the
+ // newly retargeted branch.
+ PN->addIncoming(Selected, PredBB);
+ }
+ } else {
+ for (unsigned i = 0, e = BBPreds.size(); i != e; ++i) {
+ // Update existing incoming values in PN for this
+ // predecessor of BB.
+ BasicBlock *PredBB = BBPreds[i];
+ Value *Selected = selectIncomingValueForBlock(OldVal, PredBB,
+ IncomingValues);
+
+ // And add a new incoming value for this predecessor for the
+ // newly retargeted branch.
+ PN->addIncoming(Selected, PredBB);
+ }
+ }
+
+ replaceUndefValuesInPhi(PN, IncomingValues);
+}
+
/// TryToSimplifyUncondBranchFromEmptyBlock - BB is known to contain an
/// unconditional branch, and contains no instructions other than PHI nodes,
/// potential side-effect free intrinsics and the branch. If possible,
// We can't eliminate infinite loops.
BasicBlock *Succ = cast<BranchInst>(BB->getTerminator())->getSuccessor(0);
if (BB == Succ) return false;
-
+
// Check to see if merging these blocks would cause conflicts for any of the
// phi nodes in BB or Succ. If not, we can safely merge.
if (!CanPropagatePredecessorsForPHIs(BB, Succ)) return false;
// possible to handle such cases, but difficult: it requires checking whether
// BB dominates Succ, which is non-trivial to calculate in the case where
// Succ has multiple predecessors. Also, it requires checking whether
- // constructing the necessary self-referential PHI node doesn't intoduce any
+ // constructing the necessary self-referential PHI node doesn't introduce any
// conflicts; this isn't too difficult, but the previous code for doing this
// was incorrect.
//
if (!Succ->getSinglePredecessor()) {
BasicBlock::iterator BBI = BB->begin();
while (isa<PHINode>(*BBI)) {
- for (Value::use_iterator UI = BBI->use_begin(), E = BBI->use_end();
- UI != E; ++UI) {
- if (PHINode* PN = dyn_cast<PHINode>(*UI)) {
- if (PN->getIncomingBlock(UI) != BB)
+ for (Use &U : BBI->uses()) {
+ if (PHINode* PN = dyn_cast<PHINode>(U.getUser())) {
+ if (PN->getIncomingBlock(U) != BB)
return false;
} else {
return false;
}
DEBUG(dbgs() << "Killing Trivial BB: \n" << *BB);
-
+
if (isa<PHINode>(Succ->begin())) {
// If there is more than one pred of succ, and there are PHI nodes in
// the successor, then we need to add incoming edges for the PHI nodes
//
- const SmallVector<BasicBlock*, 16> BBPreds(pred_begin(BB), pred_end(BB));
-
+ const PredBlockVector BBPreds(pred_begin(BB), pred_end(BB));
+
// Loop over all of the PHI nodes in the successor of BB.
for (BasicBlock::iterator I = Succ->begin(); isa<PHINode>(I); ++I) {
PHINode *PN = cast<PHINode>(I);
- Value *OldVal = PN->removeIncomingValue(BB, false);
- assert(OldVal && "No entry in PHI for Pred BB!");
-
- // If this incoming value is one of the PHI nodes in BB, the new entries
- // in the PHI node are the entries from the old PHI.
- if (isa<PHINode>(OldVal) && cast<PHINode>(OldVal)->getParent() == BB) {
- PHINode *OldValPN = cast<PHINode>(OldVal);
- for (unsigned i = 0, e = OldValPN->getNumIncomingValues(); i != e; ++i)
- // Note that, since we are merging phi nodes and BB and Succ might
- // have common predecessors, we could end up with a phi node with
- // identical incoming branches. This will be cleaned up later (and
- // will trigger asserts if we try to clean it up now, without also
- // simplifying the corresponding conditional branch).
- PN->addIncoming(OldValPN->getIncomingValue(i),
- OldValPN->getIncomingBlock(i));
- } else {
- // Add an incoming value for each of the new incoming values.
- for (unsigned i = 0, e = BBPreds.size(); i != e; ++i)
- PN->addIncoming(OldVal, BBPreds[i]);
- }
+
+ redirectValuesFromPredecessorsToPhi(BB, BBPreds, PN);
}
}
-
+
if (Succ->getSinglePredecessor()) {
// BB is the only predecessor of Succ, so Succ will end up with exactly
// the same predecessors BB had.
PN->eraseFromParent();
}
}
-
+
// Everything that jumped to BB now goes to Succ.
BB->replaceAllUsesWith(Succ);
if (!Succ->hasName()) Succ->takeName(BB);
// the final program then it is impossible for us to reliably enforce the
// preferred alignment.
if (GV->isWeakForLinker()) return Align;
-
+
if (GV->getAlignment() >= PrefAlign)
return GV->getAlignment();
// We can only increase the alignment of the global if it has no alignment
/// and it is more than the alignment of the ultimate object, see if we can
/// increase the alignment of the ultimate object, making this check succeed.
unsigned llvm::getOrEnforceKnownAlignment(Value *V, unsigned PrefAlign,
- const DataLayout *TD) {
+ const DataLayout *DL) {
assert(V->getType()->isPointerTy() &&
"getOrEnforceKnownAlignment expects a pointer!");
- unsigned AS = cast<PointerType>(V->getType())->getAddressSpace();
- unsigned BitWidth = TD ? TD->getPointerSizeInBits(AS) : 64;
+ unsigned BitWidth = DL ? DL->getPointerTypeSizeInBits(V->getType()) : 64;
+
APInt KnownZero(BitWidth, 0), KnownOne(BitWidth, 0);
- ComputeMaskedBits(V, KnownZero, KnownOne, TD);
+ ComputeMaskedBits(V, KnownZero, KnownOne, DL);
unsigned TrailZ = KnownZero.countTrailingOnes();
-
- // Avoid trouble with rediculously large TrailZ values, such as
+
+ // Avoid trouble with ridiculously large TrailZ values, such as
// those computed from a null pointer.
TrailZ = std::min(TrailZ, unsigned(sizeof(unsigned) * CHAR_BIT - 1));
-
+
unsigned Align = 1u << std::min(BitWidth - 1, TrailZ);
-
+
// LLVM doesn't support alignments larger than this currently.
Align = std::min(Align, +Value::MaximumAlignment);
-
+
if (PrefAlign > Align)
- Align = enforceKnownAlignment(V, Align, PrefAlign, TD);
-
+ Align = enforceKnownAlignment(V, Align, PrefAlign, DL);
+
// We don't need to make any adjustment.
return Align;
}
/// Dbg Intrinsic utilities
///
-/// Inserts a llvm.dbg.value instrinsic before the stores to an alloca'd value
+/// See if there is a dbg.value intrinsic for DIVar before I.
+static bool LdStHasDebugValue(DIVariable &DIVar, Instruction *I) {
+ // Since we can't guarantee that the original dbg.declare instrinsic
+ // is removed by LowerDbgDeclare(), we need to make sure that we are
+ // not inserting the same dbg.value intrinsic over and over.
+ llvm::BasicBlock::InstListType::iterator PrevI(I);
+ if (PrevI != I->getParent()->getInstList().begin()) {
+ --PrevI;
+ if (DbgValueInst *DVI = dyn_cast<DbgValueInst>(PrevI))
+ if (DVI->getValue() == I->getOperand(0) &&
+ DVI->getOffset() == 0 &&
+ DVI->getVariable() == DIVar)
+ return true;
+ }
+ return false;
+}
+
+/// Inserts a llvm.dbg.value intrinsic before a store to an alloca'd value
/// that has an associated llvm.dbg.decl intrinsic.
bool llvm::ConvertDebugDeclareToDebugValue(DbgDeclareInst *DDI,
StoreInst *SI, DIBuilder &Builder) {
DIVariable DIVar(DDI->getVariable());
- if (!DIVar.Verify())
+ assert((!DIVar || DIVar.isVariable()) &&
+ "Variable in DbgDeclareInst should be either null or a DIVariable.");
+ if (!DIVar)
return false;
+ if (LdStHasDebugValue(DIVar, SI))
+ return true;
+
Instruction *DbgVal = NULL;
// If an argument is zero extended then use argument directly. The ZExt
// may be zapped by an optimization pass in future.
return true;
}
-/// Inserts a llvm.dbg.value instrinsic before the stores to an alloca'd value
+/// Inserts a llvm.dbg.value intrinsic before a load of an alloca'd value
/// that has an associated llvm.dbg.decl intrinsic.
bool llvm::ConvertDebugDeclareToDebugValue(DbgDeclareInst *DDI,
LoadInst *LI, DIBuilder &Builder) {
DIVariable DIVar(DDI->getVariable());
- if (!DIVar.Verify())
+ assert((!DIVar || DIVar.isVariable()) &&
+ "Variable in DbgDeclareInst should be either null or a DIVariable.");
+ if (!DIVar)
return false;
- Instruction *DbgVal =
+ if (LdStHasDebugValue(DIVar, LI))
+ return true;
+
+ Instruction *DbgVal =
Builder.insertDbgValueIntrinsic(LI->getOperand(0), 0,
DIVar, LI);
-
+
// Propagate any debug metadata from the store onto the dbg.value.
DebugLoc LIDL = LI->getDebugLoc();
if (!LIDL.isUnknown())
bool llvm::LowerDbgDeclare(Function &F) {
DIBuilder DIB(*F.getParent());
SmallVector<DbgDeclareInst *, 4> Dbgs;
- for (Function::iterator FI = F.begin(), FE = F.end(); FI != FE; ++FI)
- for (BasicBlock::iterator BI = FI->begin(), BE = FI->end(); BI != BE; ++BI) {
- if (DbgDeclareInst *DDI = dyn_cast<DbgDeclareInst>(BI))
+ for (auto &FI : F)
+ for (BasicBlock::iterator BI : FI)
+ if (auto DDI = dyn_cast<DbgDeclareInst>(BI))
Dbgs.push_back(DDI);
- }
+
if (Dbgs.empty())
return false;
- for (SmallVector<DbgDeclareInst *, 4>::iterator I = Dbgs.begin(),
- E = Dbgs.end(); I != E; ++I) {
- DbgDeclareInst *DDI = *I;
- if (AllocaInst *AI = dyn_cast_or_null<AllocaInst>(DDI->getAddress())) {
- bool RemoveDDI = true;
- for (Value::use_iterator UI = AI->use_begin(), E = AI->use_end();
- UI != E; ++UI)
- if (StoreInst *SI = dyn_cast<StoreInst>(*UI))
+ for (auto &I : Dbgs) {
+ DbgDeclareInst *DDI = I;
+ AllocaInst *AI = dyn_cast_or_null<AllocaInst>(DDI->getAddress());
+ // If this is an alloca for a scalar variable, insert a dbg.value
+ // at each load and store to the alloca and erase the dbg.declare.
+ // The dbg.values allow tracking a variable even if it is not
+ // stored on the stack, while the dbg.declare can only describe
+ // the stack slot (and at a lexical-scope granularity). Later
+ // passes will attempt to elide the stack slot.
+ if (AI && !AI->isArrayAllocation()) {
+ for (User *U : AI->users())
+ if (StoreInst *SI = dyn_cast<StoreInst>(U))
ConvertDebugDeclareToDebugValue(DDI, SI, DIB);
- else if (LoadInst *LI = dyn_cast<LoadInst>(*UI))
+ else if (LoadInst *LI = dyn_cast<LoadInst>(U))
ConvertDebugDeclareToDebugValue(DDI, LI, DIB);
- else
- RemoveDDI = false;
- if (RemoveDDI)
- DDI->eraseFromParent();
+ else if (Instruction *I = dyn_cast<Instruction>(U)) {
+ // This is a call by-value or some other instruction that
+ // takes a pointer to the variable. Insert a *value*
+ // intrinsic that describes the alloca.
+ auto DbgVal =
+ DIB.insertDbgValueIntrinsic(AI, 0,
+ DIVariable(DDI->getVariable()), I);
+ DbgVal->setDebugLoc(I->getDebugLoc());
+ }
+ DDI->eraseFromParent();
}
}
return true;
/// alloca 'V', if any.
DbgDeclareInst *llvm::FindAllocaDbgDeclare(Value *V) {
if (MDNode *DebugNode = MDNode::getIfExists(V->getContext(), V))
- for (Value::use_iterator UI = DebugNode->use_begin(),
- E = DebugNode->use_end(); UI != E; ++UI)
- if (DbgDeclareInst *DDI = dyn_cast<DbgDeclareInst>(*UI))
+ for (User *U : DebugNode->users())
+ if (DbgDeclareInst *DDI = dyn_cast<DbgDeclareInst>(U))
return DDI;
return 0;
}
+
+bool llvm::replaceDbgDeclareForAlloca(AllocaInst *AI, Value *NewAllocaAddress,
+ DIBuilder &Builder) {
+ DbgDeclareInst *DDI = FindAllocaDbgDeclare(AI);
+ if (!DDI)
+ return false;
+ DIVariable DIVar(DDI->getVariable());
+ assert((!DIVar || DIVar.isVariable()) &&
+ "Variable in DbgDeclareInst should be either null or a DIVariable.");
+ if (!DIVar)
+ return false;
+
+ // Create a copy of the original DIDescriptor for user variable, appending
+ // "deref" operation to a list of address elements, as new llvm.dbg.declare
+ // will take a value storing address of the memory for variable, not
+ // alloca itself.
+ Type *Int64Ty = Type::getInt64Ty(AI->getContext());
+ SmallVector<Value*, 4> NewDIVarAddress;
+ if (DIVar.hasComplexAddress()) {
+ for (unsigned i = 0, n = DIVar.getNumAddrElements(); i < n; ++i) {
+ NewDIVarAddress.push_back(
+ ConstantInt::get(Int64Ty, DIVar.getAddrElement(i)));
+ }
+ }
+ NewDIVarAddress.push_back(ConstantInt::get(Int64Ty, DIBuilder::OpDeref));
+ DIVariable NewDIVar = Builder.createComplexVariable(
+ DIVar.getTag(), DIVar.getContext(), DIVar.getName(),
+ DIVar.getFile(), DIVar.getLineNumber(), DIVar.getType(),
+ NewDIVarAddress, DIVar.getArgNumber());
+
+ // Insert llvm.dbg.declare in the same basic block as the original alloca,
+ // and remove old llvm.dbg.declare.
+ BasicBlock *BB = AI->getParent();
+ Builder.insertDeclare(NewAllocaAddress, NewDIVar, BB);
+ DDI->eraseFromParent();
+ return true;
+}
+
+/// changeToUnreachable - Insert an unreachable instruction before the specified
+/// instruction, making it and the rest of the code in the block dead.
+static void changeToUnreachable(Instruction *I, bool UseLLVMTrap) {
+ BasicBlock *BB = I->getParent();
+ // Loop over all of the successors, removing BB's entry from any PHI
+ // nodes.
+ for (succ_iterator SI = succ_begin(BB), SE = succ_end(BB); SI != SE; ++SI)
+ (*SI)->removePredecessor(BB);
+
+ // Insert a call to llvm.trap right before this. This turns the undefined
+ // behavior into a hard fail instead of falling through into random code.
+ if (UseLLVMTrap) {
+ Function *TrapFn =
+ Intrinsic::getDeclaration(BB->getParent()->getParent(), Intrinsic::trap);
+ CallInst *CallTrap = CallInst::Create(TrapFn, "", I);
+ CallTrap->setDebugLoc(I->getDebugLoc());
+ }
+ new UnreachableInst(I->getContext(), I);
+
+ // All instructions after this are dead.
+ BasicBlock::iterator BBI = I, BBE = BB->end();
+ while (BBI != BBE) {
+ if (!BBI->use_empty())
+ BBI->replaceAllUsesWith(UndefValue::get(BBI->getType()));
+ BB->getInstList().erase(BBI++);
+ }
+}
+
+/// changeToCall - Convert the specified invoke into a normal call.
+static void changeToCall(InvokeInst *II) {
+ SmallVector<Value*, 8> Args(II->op_begin(), II->op_end() - 3);
+ CallInst *NewCall = CallInst::Create(II->getCalledValue(), Args, "", II);
+ NewCall->takeName(II);
+ NewCall->setCallingConv(II->getCallingConv());
+ NewCall->setAttributes(II->getAttributes());
+ NewCall->setDebugLoc(II->getDebugLoc());
+ II->replaceAllUsesWith(NewCall);
+
+ // Follow the call by a branch to the normal destination.
+ BranchInst::Create(II->getNormalDest(), II);
+
+ // Update PHI nodes in the unwind destination
+ II->getUnwindDest()->removePredecessor(II->getParent());
+ II->eraseFromParent();
+}
+
+static bool markAliveBlocks(BasicBlock *BB,
+ SmallPtrSet<BasicBlock*, 128> &Reachable) {
+
+ SmallVector<BasicBlock*, 128> Worklist;
+ Worklist.push_back(BB);
+ Reachable.insert(BB);
+ bool Changed = false;
+ do {
+ BB = Worklist.pop_back_val();
+
+ // Do a quick scan of the basic block, turning any obviously unreachable
+ // instructions into LLVM unreachable insts. The instruction combining pass
+ // canonicalizes unreachable insts into stores to null or undef.
+ for (BasicBlock::iterator BBI = BB->begin(), E = BB->end(); BBI != E;++BBI){
+ if (CallInst *CI = dyn_cast<CallInst>(BBI)) {
+ if (CI->doesNotReturn()) {
+ // If we found a call to a no-return function, insert an unreachable
+ // instruction after it. Make sure there isn't *already* one there
+ // though.
+ ++BBI;
+ if (!isa<UnreachableInst>(BBI)) {
+ // Don't insert a call to llvm.trap right before the unreachable.
+ changeToUnreachable(BBI, false);
+ Changed = true;
+ }
+ break;
+ }
+ }
+
+ // Store to undef and store to null are undefined and used to signal that
+ // they should be changed to unreachable by passes that can't modify the
+ // CFG.
+ if (StoreInst *SI = dyn_cast<StoreInst>(BBI)) {
+ // Don't touch volatile stores.
+ if (SI->isVolatile()) continue;
+
+ Value *Ptr = SI->getOperand(1);
+
+ if (isa<UndefValue>(Ptr) ||
+ (isa<ConstantPointerNull>(Ptr) &&
+ SI->getPointerAddressSpace() == 0)) {
+ changeToUnreachable(SI, true);
+ Changed = true;
+ break;
+ }
+ }
+ }
+
+ // Turn invokes that call 'nounwind' functions into ordinary calls.
+ if (InvokeInst *II = dyn_cast<InvokeInst>(BB->getTerminator())) {
+ Value *Callee = II->getCalledValue();
+ if (isa<ConstantPointerNull>(Callee) || isa<UndefValue>(Callee)) {
+ changeToUnreachable(II, true);
+ Changed = true;
+ } else if (II->doesNotThrow()) {
+ if (II->use_empty() && II->onlyReadsMemory()) {
+ // jump to the normal destination branch.
+ BranchInst::Create(II->getNormalDest(), II);
+ II->getUnwindDest()->removePredecessor(II->getParent());
+ II->eraseFromParent();
+ } else
+ changeToCall(II);
+ Changed = true;
+ }
+ }
+
+ Changed |= ConstantFoldTerminator(BB, true);
+ for (succ_iterator SI = succ_begin(BB), SE = succ_end(BB); SI != SE; ++SI)
+ if (Reachable.insert(*SI))
+ Worklist.push_back(*SI);
+ } while (!Worklist.empty());
+ return Changed;
+}
+
+/// removeUnreachableBlocksFromFn - Remove blocks that are not reachable, even
+/// if they are in a dead cycle. Return true if a change was made, false
+/// otherwise.
+bool llvm::removeUnreachableBlocks(Function &F) {
+ SmallPtrSet<BasicBlock*, 128> Reachable;
+ bool Changed = markAliveBlocks(F.begin(), Reachable);
+
+ // If there are unreachable blocks in the CFG...
+ if (Reachable.size() == F.size())
+ return Changed;
+
+ assert(Reachable.size() < F.size());
+ NumRemoved += F.size()-Reachable.size();
+
+ // Loop over all of the basic blocks that are not reachable, dropping all of
+ // their internal references...
+ for (Function::iterator BB = ++F.begin(), E = F.end(); BB != E; ++BB) {
+ if (Reachable.count(BB))
+ continue;
+
+ for (succ_iterator SI = succ_begin(BB), SE = succ_end(BB); SI != SE; ++SI)
+ if (Reachable.count(*SI))
+ (*SI)->removePredecessor(BB);
+ BB->dropAllReferences();
+ }
+
+ for (Function::iterator I = ++F.begin(); I != F.end();)
+ if (!Reachable.count(I))
+ I = F.getBasicBlockList().erase(I);
+ else
+ ++I;
+
+ return true;
+}