index 5b3bdbe4be2ca62d136f28b7e0d81f0a7835492d..f6867c24ee58da885da49e31e74a0017e5275728 100644 (file)
//
//===----------------------------------------------------------------------===//
-#define DEBUG_TYPE "simplifycfg"
#include "llvm/Transforms/Utils/Local.h"
#include "llvm/ADT/DenseMap.h"
#include "llvm/ADT/STLExtras.h"
#include "llvm/Support/Debug.h"
#include "llvm/Support/raw_ostream.h"
#include "llvm/Transforms/Utils/BasicBlockUtils.h"
+#include "llvm/Transforms/Utils/Local.h"
+#include "llvm/Transforms/Utils/ValueMapper.h"
#include <algorithm>
#include <map>
#include <set>
using namespace llvm;
using namespace PatternMatch;
+#define DEBUG_TYPE "simplifycfg"
+
static cl::opt<unsigned>
PHINodeFoldingThreshold("phi-node-folding-threshold", cl::Hidden, cl::init(1),
cl::desc("Control the amount of phi node folding to perform (default = 1)"));
cl::desc("Hoist conditional stores if an unconditional store precedes"));
STATISTIC(NumBitMaps, "Number of switch instructions turned into bitmaps");
+STATISTIC(NumLinearMaps, "Number of switch instructions turned into linear mapping");
STATISTIC(NumLookupTables, "Number of switch instructions turned into lookup tables");
+STATISTIC(NumLookupTablesHoles, "Number of switch instructions turned into lookup tables (holes checked)");
+STATISTIC(NumTableCmpReuses, "Number of reused switch table lookup compares");
STATISTIC(NumSinkCommons, "Number of common instructions sunk down to the end block");
STATISTIC(NumSpeculations, "Number of speculative executed instructions");
namespace {
+ // The first field contains the value that the switch produces when a certain
+ // case group is selected, and the second field is a vector containing the cases
+ // composing the case group.
+ typedef SmallVector<std::pair<Constant *, SmallVector<ConstantInt *, 4>>, 2>
+ SwitchCaseResultVectorTy;
+ // The first field contains the phi node that generates a result of the switch
+ // and the second field contains the value generated for a certain case in the switch
+ // for that PHI.
+ typedef SmallVector<std::pair<PHINode *, Constant *>, 4> SwitchCaseResultsTy;
+
/// ValueEqualityComparisonCase - Represents a case of a switch.
struct ValueEqualityComparisonCase {
ConstantInt *Value;
class SimplifyCFGOpt {
const TargetTransformInfo &TTI;
+ unsigned BonusInstThreshold;
const DataLayout *const DL;
+ AssumptionCache *AC;
Value *isValueEqualityComparison(TerminatorInst *TI);
BasicBlock *GetValueEqualityComparisonCases(TerminatorInst *TI,
std::vector<ValueEqualityComparisonCase> &Cases);
bool SimplifyCondBranch(BranchInst *BI, IRBuilder <>&Builder);
public:
- SimplifyCFGOpt(const TargetTransformInfo &TTI, const DataLayout *DL)
- : TTI(TTI), DL(DL) {}
+ SimplifyCFGOpt(const TargetTransformInfo &TTI, unsigned BonusInstThreshold,
+ const DataLayout *DL, AssumptionCache *AC)
+ : TTI(TTI), BonusInstThreshold(BonusInstThreshold), DL(DL), AC(AC) {}
bool run(BasicBlock *BB);
};
}
/// ComputeSpeculationCost - Compute an abstract "cost" of speculating the
/// given instruction, which is assumed to be safe to speculate. 1 means
/// cheap, 2 means less cheap, and UINT_MAX means prohibitively expensive.
-static unsigned ComputeSpeculationCost(const User *I) {
- assert(isSafeToSpeculativelyExecute(I) &&
+static unsigned ComputeSpeculationCost(const User *I, const DataLayout *DL) {
+ assert(isSafeToSpeculativelyExecute(I, DL) &&
"Instruction is not safe to speculatively execute!");
switch (Operator::getOpcode(I)) {
default:
if (!cast<GEPOperator>(I)->hasAllConstantIndices())
return UINT_MAX;
return 1;
+ case Instruction::ExtractValue:
case Instruction::Load:
case Instruction::Add:
case Instruction::Sub:
case Instruction::Trunc:
case Instruction::ZExt:
case Instruction::SExt:
+ case Instruction::BitCast:
+ case Instruction::ExtractElement:
+ case Instruction::InsertElement:
return 1; // These are all cheap.
case Instruction::Call:
/// V plus its non-dominating operands. If that cost is greater than
/// CostRemaining, false is returned and CostRemaining is undefined.
static bool DominatesMergePoint(Value *V, BasicBlock *BB,
- SmallPtrSet<Instruction*, 4> *AggressiveInsts,
- unsigned &CostRemaining) {
+ SmallPtrSetImpl<Instruction*> *AggressiveInsts,
+ unsigned &CostRemaining,
+ const DataLayout *DL) {
Instruction *I = dyn_cast<Instruction>(V);
if (!I) {
// Non-instructions all dominate instructions, but not all constantexprs
// branch to BB, then it must be in the 'conditional' part of the "if
// statement". If not, it definitely dominates the region.
BranchInst *BI = dyn_cast<BranchInst>(PBB->getTerminator());
- if (BI == 0 || BI->isConditional() || BI->getSuccessor(0) != BB)
+ if (!BI || BI->isConditional() || BI->getSuccessor(0) != BB)
return true;
// If we aren't allowing aggressive promotion anymore, then don't consider
// instructions in the 'if region'.
- if (AggressiveInsts == 0) return false;
+ if (!AggressiveInsts) return false;
// If we have seen this instruction before, don't count it again.
if (AggressiveInsts->count(I)) return true;
// Okay, it looks like the instruction IS in the "condition". Check to
// see if it's a cheap instruction to unconditionally compute, and if it
// only uses stuff defined outside of the condition. If so, hoist it out.
- if (!isSafeToSpeculativelyExecute(I))
+ if (!isSafeToSpeculativelyExecute(I, DL))
return false;
- unsigned Cost = ComputeSpeculationCost(I);
+ unsigned Cost = ComputeSpeculationCost(I, DL);
if (Cost > CostRemaining)
return false;
// Okay, we can only really hoist these out if their operands do
// not take us over the cost threshold.
for (User::op_iterator i = I->op_begin(), e = I->op_end(); i != e; ++i)
- if (!DominatesMergePoint(*i, BB, AggressiveInsts, CostRemaining))
+ if (!DominatesMergePoint(*i, BB, AggressiveInsts, CostRemaining, DL))
return false;
// Okay, it's safe to do this! Remember this instruction.
AggressiveInsts->insert(I);
return cast<ConstantInt>
(ConstantExpr::getIntegerCast(CI, PtrTy, /*isSigned=*/false));
}
- return 0;
+ return nullptr;
}
-/// GatherConstantCompares - Given a potentially 'or'd or 'and'd together
-/// collection of icmp eq/ne instructions that compare a value against a
-/// constant, return the value being compared, and stick the constant into the
-/// Values vector.
-static Value *
-GatherConstantCompares(Value *V, std::vector<ConstantInt*> &Vals, Value *&Extra,
- const DataLayout *DL, bool isEQ, unsigned &UsedICmps) {
- Instruction *I = dyn_cast<Instruction>(V);
- if (I == 0) return 0;
-
- // If this is an icmp against a constant, handle this as one of the cases.
- if (ICmpInst *ICI = dyn_cast<ICmpInst>(I)) {
- if (ConstantInt *C = GetConstantInt(I->getOperand(1), DL)) {
- Value *RHSVal;
- ConstantInt *RHSC;
-
- if (ICI->getPredicate() == (isEQ ? ICmpInst::ICMP_EQ:ICmpInst::ICMP_NE)) {
- // (x & ~2^x) == y --> x == y || x == y|2^x
- // This undoes a transformation done by instcombine to fuse 2 compares.
- if (match(ICI->getOperand(0),
- m_And(m_Value(RHSVal), m_ConstantInt(RHSC)))) {
- APInt Not = ~RHSC->getValue();
- if (Not.isPowerOf2()) {
- Vals.push_back(C);
- Vals.push_back(
- ConstantInt::get(C->getContext(), C->getValue() | Not));
- UsedICmps++;
- return RHSVal;
- }
- }
+namespace {
+
+/// Given a chain of or (||) or and (&&) comparison of a value against a
+/// constant, this will try to recover the information required for a switch
+/// structure.
+/// It will depth-first traverse the chain of comparison, seeking for patterns
+/// like %a == 12 or %a < 4 and combine them to produce a set of integer
+/// representing the different cases for the switch.
+/// Note that if the chain is composed of '||' it will build the set of elements
+/// that matches the comparisons (i.e. any of this value validate the chain)
+/// while for a chain of '&&' it will build the set elements that make the test
+/// fail.
+struct ConstantComparesGatherer {
+
+ Value *CompValue; /// Value found for the switch comparison
+ Value *Extra; /// Extra clause to be checked before the switch
+ SmallVector<ConstantInt *, 8> Vals; /// Set of integers to match in switch
+ unsigned UsedICmps; /// Number of comparisons matched in the and/or chain
+
+ /// Construct and compute the result for the comparison instruction Cond
+ ConstantComparesGatherer(Instruction *Cond, const DataLayout *DL)
+ : CompValue(nullptr), Extra(nullptr), UsedICmps(0) {
+ gather(Cond, DL);
+ }
+
+ /// Prevent copy
+ ConstantComparesGatherer(const ConstantComparesGatherer &)
+ LLVM_DELETED_FUNCTION;
+ ConstantComparesGatherer &
+ operator=(const ConstantComparesGatherer &) LLVM_DELETED_FUNCTION;
- UsedICmps++;
- Vals.push_back(C);
- return I->getOperand(0);
+private:
+
+ /// Try to set the current value used for the comparison, it succeeds only if
+ /// it wasn't set before or if the new value is the same as the old one
+ bool setValueOnce(Value *NewVal) {
+ if(CompValue && CompValue != NewVal) return false;
+ CompValue = NewVal;
+ return (CompValue != nullptr);
+ }
+
+ /// Try to match Instruction "I" as a comparison against a constant and
+ /// populates the array Vals with the set of values that match (or do not
+ /// match depending on isEQ).
+ /// Return false on failure. On success, the Value the comparison matched
+ /// against is placed in CompValue.
+ /// If CompValue is already set, the function is expected to fail if a match
+ /// is found but the value compared to is different.
+ bool matchInstruction(Instruction *I, const DataLayout *DL, bool isEQ) {
+ // If this is an icmp against a constant, handle this as one of the cases.
+ ICmpInst *ICI;
+ ConstantInt *C;
+ if (!((ICI = dyn_cast<ICmpInst>(I)) &&
+ (C = GetConstantInt(I->getOperand(1), DL)))) {
+ return false;
+ }
+
+ Value *RHSVal;
+ ConstantInt *RHSC;
+
+ // Pattern match a special case
+ // (x & ~2^x) == y --> x == y || x == y|2^x
+ // This undoes a transformation done by instcombine to fuse 2 compares.
+ if (ICI->getPredicate() == (isEQ ? ICmpInst::ICMP_EQ:ICmpInst::ICMP_NE)) {
+ if (match(ICI->getOperand(0),
+ m_And(m_Value(RHSVal), m_ConstantInt(RHSC)))) {
+ APInt Not = ~RHSC->getValue();
+ if (Not.isPowerOf2()) {
+ // If we already have a value for the switch, it has to match!
+ if(!setValueOnce(RHSVal))
+ return false;
+
+ Vals.push_back(C);
+ Vals.push_back(ConstantInt::get(C->getContext(),
+ C->getValue() | Not));
+ UsedICmps++;
+ return true;
+ }
}
- // If we have "x ult 3" comparison, for example, then we can add 0,1,2 to
- // the set.
- ConstantRange Span =
- ConstantRange::makeICmpRegion(ICI->getPredicate(), C->getValue());
-
- // Shift the range if the compare is fed by an add. This is the range
- // compare idiom as emitted by instcombine.
- bool hasAdd =
- match(I->getOperand(0), m_Add(m_Value(RHSVal), m_ConstantInt(RHSC)));
- if (hasAdd)
- Span = Span.subtract(RHSC->getValue());
-
- // If this is an and/!= check then we want to optimize "x ugt 2" into
- // x != 0 && x != 1.
- if (!isEQ)
- Span = Span.inverse();
-
- // If there are a ton of values, we don't want to make a ginormous switch.
- if (Span.getSetSize().ugt(8) || Span.isEmptySet())
- return 0;
-
- for (APInt Tmp = Span.getLower(); Tmp != Span.getUpper(); ++Tmp)
- Vals.push_back(ConstantInt::get(V->getContext(), Tmp));
+ // If we already have a value for the switch, it has to match!
+ if(!setValueOnce(ICI->getOperand(0)))
+ return false;
+
UsedICmps++;
- return hasAdd ? RHSVal : I->getOperand(0);
+ Vals.push_back(C);
+ return ICI->getOperand(0);
}
- return 0;
- }
- // Otherwise, we can only handle an | or &, depending on isEQ.
- if (I->getOpcode() != (isEQ ? Instruction::Or : Instruction::And))
- return 0;
+ // If we have "x ult 3", for example, then we can add 0,1,2 to the set.
+ ConstantRange Span = ConstantRange::makeICmpRegion(ICI->getPredicate(),
+ C->getValue());
- unsigned NumValsBeforeLHS = Vals.size();
- unsigned UsedICmpsBeforeLHS = UsedICmps;
- if (Value *LHS = GatherConstantCompares(I->getOperand(0), Vals, Extra, DL,
- isEQ, UsedICmps)) {
- unsigned NumVals = Vals.size();
- unsigned UsedICmpsBeforeRHS = UsedICmps;
- if (Value *RHS = GatherConstantCompares(I->getOperand(1), Vals, Extra, DL,
- isEQ, UsedICmps)) {
- if (LHS == RHS)
- return LHS;
- Vals.resize(NumVals);
- UsedICmps = UsedICmpsBeforeRHS;
+ // Shift the range if the compare is fed by an add. This is the range
+ // compare idiom as emitted by instcombine.
+ Value *CandidateVal = I->getOperand(0);
+ if(match(I->getOperand(0), m_Add(m_Value(RHSVal), m_ConstantInt(RHSC)))) {
+ Span = Span.subtract(RHSC->getValue());
+ CandidateVal = RHSVal;
}
- // The RHS of the or/and can't be folded in and we haven't used "Extra" yet,
- // set it and return success.
- if (Extra == 0 || Extra == I->getOperand(1)) {
- Extra = I->getOperand(1);
- return LHS;
+ // If this is an and/!= check, then we are looking to build the set of
+ // value that *don't* pass the and chain. I.e. to turn "x ugt 2" into
+ // x != 0 && x != 1.
+ if (!isEQ)
+ Span = Span.inverse();
+
+ // If there are a ton of values, we don't want to make a ginormous switch.
+ if (Span.getSetSize().ugt(8) || Span.isEmptySet()) {
+ return false;
}
- Vals.resize(NumValsBeforeLHS);
- UsedICmps = UsedICmpsBeforeLHS;
- return 0;
+ // If we already have a value for the switch, it has to match!
+ if(!setValueOnce(CandidateVal))
+ return false;
+
+ // Add all values from the range to the set
+ for (APInt Tmp = Span.getLower(); Tmp != Span.getUpper(); ++Tmp)
+ Vals.push_back(ConstantInt::get(I->getContext(), Tmp));
+
+ UsedICmps++;
+ return true;
+
}
- // If the LHS can't be folded in, but Extra is available and RHS can, try to
- // use LHS as Extra.
- if (Extra == 0 || Extra == I->getOperand(0)) {
- Value *OldExtra = Extra;
- Extra = I->getOperand(0);
- if (Value *RHS = GatherConstantCompares(I->getOperand(1), Vals, Extra, DL,
- isEQ, UsedICmps))
- return RHS;
- assert(Vals.size() == NumValsBeforeLHS);
- Extra = OldExtra;
+ /// gather - Given a potentially 'or'd or 'and'd together collection of icmp
+ /// eq/ne/lt/gt instructions that compare a value against a constant, extract
+ /// the value being compared, and stick the list constants into the Vals
+ /// vector.
+ /// One "Extra" case is allowed to differ from the other.
+ void gather(Value *V, const DataLayout *DL) {
+ Instruction *I = dyn_cast<Instruction>(V);
+ bool isEQ = (I->getOpcode() == Instruction::Or);
+
+ // Keep a stack (SmallVector for efficiency) for depth-first traversal
+ SmallVector<Value *, 8> DFT;
+
+ // Initialize
+ DFT.push_back(V);
+
+ while(!DFT.empty()) {
+ V = DFT.pop_back_val();
+
+ if (Instruction *I = dyn_cast<Instruction>(V)) {
+ // If it is a || (or && depending on isEQ), process the operands.
+ if (I->getOpcode() == (isEQ ? Instruction::Or : Instruction::And)) {
+ DFT.push_back(I->getOperand(1));
+ DFT.push_back(I->getOperand(0));
+ continue;
+ }
+
+ // Try to match the current instruction
+ if (matchInstruction(I, DL, isEQ))
+ // Match succeed, continue the loop
+ continue;
+ }
+
+ // One element of the sequence of || (or &&) could not be match as a
+ // comparison against the same value as the others.
+ // We allow only one "Extra" case to be checked before the switch
+ if (!Extra) {
+ Extra = V;
+ continue;
+ }
+ // Failed to parse a proper sequence, abort now
+ CompValue = nullptr;
+ break;
+ }
}
+};
- return 0;
}
static void EraseTerminatorInstAndDCECond(TerminatorInst *TI) {
- Instruction *Cond = 0;
+ Instruction *Cond = nullptr;
if (SwitchInst *SI = dyn_cast<SwitchInst>(TI)) {
Cond = dyn_cast<Instruction>(SI->getCondition());
} else if (BranchInst *BI = dyn_cast<BranchInst>(TI)) {
/// isValueEqualityComparison - Return true if the specified terminator checks
/// to see if a value is equal to constant integer value.
Value *SimplifyCFGOpt::isValueEqualityComparison(TerminatorInst *TI) {
- Value *CV = 0;
+ Value *CV = nullptr;
if (SwitchInst *SI = dyn_cast<SwitchInst>(TI)) {
// Do not permit merging of large switch instructions into their
// predecessors unless there is only one predecessor.
// Collect branch weights into a vector.
SmallVector<uint32_t, 8> Weights;
- MDNode* MD = SI->getMetadata(LLVMContext::MD_prof);
+ MDNode *MD = SI->getMetadata(LLVMContext::MD_prof);
bool HasWeight = MD && (MD->getNumOperands() == 2 + SI->getNumCases());
if (HasWeight)
for (unsigned MD_i = 1, MD_e = MD->getNumOperands(); MD_i < MD_e;
++MD_i) {
- ConstantInt* CI = dyn_cast<ConstantInt>(MD->getOperand(MD_i));
- assert(CI);
+ ConstantInt *CI = mdconst::extract<ConstantInt>(MD->getOperand(MD_i));
Weights.push_back(CI->getValue().getZExtValue());
}
for (SwitchInst::CaseIt i = SI->case_end(), e = SI->case_begin(); i != e;) {
// Otherwise, TI's block must correspond to some matched value. Find out
// which value (or set of values) this is.
- ConstantInt *TIV = 0;
+ ConstantInt *TIV = nullptr;
BasicBlock *TIBB = TI->getParent();
for (unsigned i = 0, e = PredCases.size(); i != e; ++i)
if (PredCases[i].Dest == TIBB) {
- if (TIV != 0)
+ if (TIV)
return false; // Cannot handle multiple values coming to this block.
TIV = PredCases[i].Value;
}
// Okay, we found the one constant that our value can be if we get into TI's
// BB. Find out which successor will unconditionally be branched to.
- BasicBlock *TheRealDest = 0;
+ BasicBlock *TheRealDest = nullptr;
for (unsigned i = 0, e = ThisCases.size(); i != e; ++i)
if (ThisCases[i].Value == TIV) {
TheRealDest = ThisCases[i].Dest;
}
// If not handled by any explicit cases, it is handled by the default case.
- if (TheRealDest == 0) TheRealDest = ThisDef;
+ if (!TheRealDest) TheRealDest = ThisDef;
// Remove PHI node entries for dead edges.
BasicBlock *CheckEdge = TheRealDest;
if (*SI != CheckEdge)
(*SI)->removePredecessor(TIBB);
else
- CheckEdge = 0;
+ CheckEdge = nullptr;
// Insert the new branch.
Instruction *NI = Builder.CreateBr(TheRealDest);
}
static inline bool HasBranchWeights(const Instruction* I) {
- MDNode* ProfMD = I->getMetadata(LLVMContext::MD_prof);
+ MDNode *ProfMD = I->getMetadata(LLVMContext::MD_prof);
if (ProfMD && ProfMD->getOperand(0))
if (MDString* MDS = dyn_cast<MDString>(ProfMD->getOperand(0)))
return MDS->getString().equals("branch_weights");
/// metadata.
static void GetBranchWeights(TerminatorInst *TI,
SmallVectorImpl<uint64_t> &Weights) {
- MDNode* MD = TI->getMetadata(LLVMContext::MD_prof);
+ MDNode *MD = TI->getMetadata(LLVMContext::MD_prof);
assert(MD);
for (unsigned i = 1, e = MD->getNumOperands(); i < e; ++i) {
- ConstantInt *CI = cast<ConstantInt>(MD->getOperand(i));
+ ConstantInt *CI = mdconst::extract<ConstantInt>(MD->getOperand(i));
Weights.push_back(CI->getValue().getZExtValue());
}
// Okay, last check. If BB is still a successor of PSI, then we must
// have an infinite loop case. If so, add an infinitely looping block
// to handle the case to preserve the behavior of the code.
- BasicBlock *InfLoopBlock = 0;
+ BasicBlock *InfLoopBlock = nullptr;
for (unsigned i = 0, e = NewSI->getNumSuccessors(); i != e; ++i)
if (NewSI->getSuccessor(i) == BB) {
- if (InfLoopBlock == 0) {
+ if (!InfLoopBlock) {
// Insert it at the end of the function, because it's either code,
// or it won't matter if it's hot. :)
InfLoopBlock = BasicBlock::Create(BB->getContext(),
return true;
}
+static bool passingValueIsAlwaysUndefined(Value *V, Instruction *I);
+
/// HoistThenElseCodeToIf - Given a conditional branch that goes to BB1 and
/// BB2, hoist any common code in the two blocks up into the branch block. The
/// caller of this function guarantees that BI's block dominates BB1 and BB2.
-static bool HoistThenElseCodeToIf(BranchInst *BI) {
+static bool HoistThenElseCodeToIf(BranchInst *BI, const DataLayout *DL) {
// This does very trivial matching, with limited scanning, to find identical
// instructions in the two blocks. In particular, we don't want to get into
// O(M*N) situations here where M and N are the sizes of BB1 and BB2. As
if (!I2->use_empty())
I2->replaceAllUsesWith(I1);
I1->intersectOptionalDataWith(I2);
+ unsigned KnownIDs[] = {
+ LLVMContext::MD_tbaa,
+ LLVMContext::MD_range,
+ LLVMContext::MD_fpmath,
+ LLVMContext::MD_invariant_load,
+ LLVMContext::MD_nonnull
+ };
+ combineMetadata(I1, I2, KnownIDs);
I2->eraseFromParent();
Changed = true;
if (BB1V == BB2V)
continue;
- if (isa<ConstantExpr>(BB1V) && !isSafeToSpeculativelyExecute(BB1V))
+ // Check for passingValueIsAlwaysUndefined here because we would rather
+ // eliminate undefined control flow then converting it to a select.
+ if (passingValueIsAlwaysUndefined(BB1V, PN) ||
+ passingValueIsAlwaysUndefined(BB2V, PN))
+ return Changed;
+
+ if (isa<ConstantExpr>(BB1V) && !isSafeToSpeculativelyExecute(BB1V, DL))
return Changed;
- if (isa<ConstantExpr>(BB2V) && !isSafeToSpeculativelyExecute(BB2V))
+ if (isa<ConstantExpr>(BB2V) && !isSafeToSpeculativelyExecute(BB2V, DL))
return Changed;
}
}
// These values do not agree. Insert a select instruction before NT
// that determines the right value.
SelectInst *&SI = InsertedSelects[std::make_pair(BB1V, BB2V)];
- if (SI == 0)
+ if (!SI)
SI = cast<SelectInst>
(Builder.CreateSelect(BI->getCondition(), BB1V, BB2V,
BB1V->getName()+"."+BB2V->getName()));
return false;
// Gather the PHI nodes in BBEnd.
- std::map<Value*, std::pair<Value*, PHINode*> > MapValueFromBB1ToBB2;
- Instruction *FirstNonPhiInBBEnd = 0;
- for (BasicBlock::iterator I = BBEnd->begin(), E = BBEnd->end();
- I != E; ++I) {
+ SmallDenseMap<std::pair<Value *, Value *>, PHINode *> JointValueMap;
+ Instruction *FirstNonPhiInBBEnd = nullptr;
+ for (BasicBlock::iterator I = BBEnd->begin(), E = BBEnd->end(); I != E; ++I) {
if (PHINode *PN = dyn_cast<PHINode>(I)) {
Value *BB1V = PN->getIncomingValueForBlock(BB1);
Value *BB2V = PN->getIncomingValueForBlock(BB2);
- MapValueFromBB1ToBB2[BB1V] = std::make_pair(BB2V, PN);
+ JointValueMap[std::make_pair(BB1V, BB2V)] = PN;
} else {
FirstNonPhiInBBEnd = &*I;
break;
if (!FirstNonPhiInBBEnd)
return false;
-
// This does very trivial matching, with limited scanning, to find identical
// instructions in the two blocks. We scan backward for obviously identical
// instructions in an identical order.
BasicBlock::InstListType::reverse_iterator RI1 = BB1->getInstList().rbegin(),
- RE1 = BB1->getInstList().rend(), RI2 = BB2->getInstList().rbegin(),
- RE2 = BB2->getInstList().rend();
+ RE1 = BB1->getInstList().rend(),
+ RI2 = BB2->getInstList().rbegin(),
+ RE2 = BB2->getInstList().rend();
// Skip debug info.
while (RI1 != RE1 && isa<DbgInfoIntrinsic>(&*RI1)) ++RI1;
if (RI1 == RE1)
return Changed;
Instruction *I1 = &*RI1, *I2 = &*RI2;
+ auto InstPair = std::make_pair(I1, I2);
// I1 and I2 should have a single use in the same PHI node, and they
// perform the same operation.
// Cannot move control-flow-involving, volatile loads, vaarg, etc.
I1->mayHaveSideEffects() || I2->mayHaveSideEffects() ||
I1->mayReadOrWriteMemory() || I2->mayReadOrWriteMemory() ||
!I1->hasOneUse() || !I2->hasOneUse() ||
- MapValueFromBB1ToBB2.find(I1) == MapValueFromBB1ToBB2.end() ||
- MapValueFromBB1ToBB2[I1].first != I2)
+ !JointValueMap.count(InstPair))
return Changed;
// Check whether we should swap the operands of ICmpInst.
+ // TODO: Add support of communativity.
ICmpInst *ICmp1 = dyn_cast<ICmpInst>(I1), *ICmp2 = dyn_cast<ICmpInst>(I2);
bool SwapOpnds = false;
if (ICmp1 && ICmp2 &&
// The operands should be either the same or they need to be generated
// with a PHI node after sinking. We only handle the case where there is
// a single pair of different operands.
- Value *DifferentOp1 = 0, *DifferentOp2 = 0;
- unsigned Op1Idx = 0;
+ Value *DifferentOp1 = nullptr, *DifferentOp2 = nullptr;
+ unsigned Op1Idx = ~0U;
for (unsigned I = 0, E = I1->getNumOperands(); I != E; ++I) {
if (I1->getOperand(I) == I2->getOperand(I))
continue;
- // Early exit if we have more-than one pair of different operands or
- // the different operand is already in MapValueFromBB1ToBB2.
- // Early exit if we need a PHI node to replace a constant.
- if (DifferentOp1 ||
- MapValueFromBB1ToBB2.find(I1->getOperand(I)) !=
- MapValueFromBB1ToBB2.end() ||
+ // Early exit if we have more-than one pair of different operands or if
+ // we need a PHI node to replace a constant.
+ if (Op1Idx != ~0U ||
isa<Constant>(I1->getOperand(I)) ||
isa<Constant>(I2->getOperand(I))) {
// If we can't sink the instructions, undo the swapping.
DifferentOp2 = I2->getOperand(I);
}
- // We insert the pair of different operands to MapValueFromBB1ToBB2 and
- // remove (I1, I2) from MapValueFromBB1ToBB2.
- if (DifferentOp1) {
- PHINode *NewPN = PHINode::Create(DifferentOp1->getType(), 2,
- DifferentOp1->getName() + ".sink",
- BBEnd->begin());
- MapValueFromBB1ToBB2[DifferentOp1] = std::make_pair(DifferentOp2, NewPN);
+ DEBUG(dbgs() << "SINK common instructions " << *I1 << "\n");
+ DEBUG(dbgs() << " " << *I2 << "\n");
+
+ // We insert the pair of different operands to JointValueMap and
+ // remove (I1, I2) from JointValueMap.
+ if (Op1Idx != ~0U) {
+ auto &NewPN = JointValueMap[std::make_pair(DifferentOp1, DifferentOp2)];
+ if (!NewPN) {
+ NewPN =
+ PHINode::Create(DifferentOp1->getType(), 2,
+ DifferentOp1->getName() + ".sink", BBEnd->begin());
+ NewPN->addIncoming(DifferentOp1, BB1);
+ NewPN->addIncoming(DifferentOp2, BB2);
+ DEBUG(dbgs() << "Create PHI node " << *NewPN << "\n";);
+ }
// I1 should use NewPN instead of DifferentOp1.
I1->setOperand(Op1Idx, NewPN);
- NewPN->addIncoming(DifferentOp1, BB1);
- NewPN->addIncoming(DifferentOp2, BB2);
- DEBUG(dbgs() << "Create PHI node " << *NewPN << "\n";);
}
- PHINode *OldPN = MapValueFromBB1ToBB2[I1].second;
- MapValueFromBB1ToBB2.erase(I1);
+ PHINode *OldPN = JointValueMap[InstPair];
+ JointValueMap.erase(InstPair);
- DEBUG(dbgs() << "SINK common instructions " << *I1 << "\n";);
- DEBUG(dbgs() << " " << *I2 << "\n";);
// We need to update RE1 and RE2 if we are going to sink the first
// instruction in the basic block down.
bool UpdateRE1 = (I1 == BB1->begin()), UpdateRE2 = (I2 == BB2->begin());
if (!I2->use_empty())
I2->replaceAllUsesWith(I1);
I1->intersectOptionalDataWith(I2);
+ // TODO: Use combineMetadata here to preserve what metadata we can
+ // (analogous to the hoisting case above).
I2->eraseFromParent();
if (UpdateRE1)
BasicBlock *StoreBB, BasicBlock *EndBB) {
StoreInst *StoreToHoist = dyn_cast<StoreInst>(I);
if (!StoreToHoist)
- return 0;
+ return nullptr;
// Volatile or atomic.
if (!StoreToHoist->isSimple())
- return 0;
+ return nullptr;
Value *StorePtr = StoreToHoist->getPointerOperand();
// Could be calling an instruction that effects memory like free().
if (CurI->mayHaveSideEffects() && !isa<StoreInst>(CurI))
- return 0;
+ return nullptr;
StoreInst *SI = dyn_cast<StoreInst>(CurI);
// Found the previous store make sure it stores to the same location.
// Found the previous store, return its value operand.
return SI->getValueOperand();
else if (SI)
- return 0; // Unknown store.
+ return nullptr; // Unknown store.
}
- return 0;
+ return nullptr;
}
/// \brief Speculate a conditional basic block flattening the CFG.
/// \endcode
///
/// \returns true if the conditional block is removed.
-static bool SpeculativelyExecuteBB(BranchInst *BI, BasicBlock *ThenBB) {
+static bool SpeculativelyExecuteBB(BranchInst *BI, BasicBlock *ThenBB,
+ const DataLayout *DL) {
// Be conservative for now. FP select instruction can often be expensive.
Value *BrCond = BI->getCondition();
if (isa<FCmpInst>(BrCond))
SmallDenseMap<Instruction *, unsigned, 4> SinkCandidateUseCounts;
unsigned SpeculationCost = 0;
- Value *SpeculatedStoreValue = 0;
- StoreInst *SpeculatedStore = 0;
+ Value *SpeculatedStoreValue = nullptr;
+ StoreInst *SpeculatedStore = nullptr;
for (BasicBlock::iterator BBI = ThenBB->begin(),
BBE = std::prev(ThenBB->end());
BBI != BBE; ++BBI) {
return false;
// Don't hoist the instruction if it's unsafe or expensive.
- if (!isSafeToSpeculativelyExecute(I) &&
+ if (!isSafeToSpeculativelyExecute(I, DL) &&
!(HoistCondStores &&
(SpeculatedStoreValue = isSafeToSpeculateStore(I, BB, ThenBB,
EndBB))))
return false;
if (!SpeculatedStoreValue &&
- ComputeSpeculationCost(I) > PHINodeFoldingThreshold)
+ ComputeSpeculationCost(I, DL) > PHINodeFoldingThreshold)
return false;
// Store the store speculation candidate.
if (ThenV == OrigV)
continue;
+ // Don't convert to selects if we could remove undefined behavior instead.
+ if (passingValueIsAlwaysUndefined(OrigV, PN) ||
+ passingValueIsAlwaysUndefined(ThenV, PN))
+ return false;
+
HaveRewritablePHIs = true;
ConstantExpr *OrigCE = dyn_cast<ConstantExpr>(OrigV);
ConstantExpr *ThenCE = dyn_cast<ConstantExpr>(ThenV);
if (!OrigCE && !ThenCE)
continue; // Known safe and cheap.
- if ((ThenCE && !isSafeToSpeculativelyExecute(ThenCE)) ||
- (OrigCE && !isSafeToSpeculativelyExecute(OrigCE)))
+ if ((ThenCE && !isSafeToSpeculativelyExecute(ThenCE, DL)) ||
+ (OrigCE && !isSafeToSpeculativelyExecute(OrigCE, DL)))
return false;
- unsigned OrigCost = OrigCE ? ComputeSpeculationCost(OrigCE) : 0;
- unsigned ThenCost = ThenCE ? ComputeSpeculationCost(ThenCE) : 0;
+ unsigned OrigCost = OrigCE ? ComputeSpeculationCost(OrigCE, DL) : 0;
+ unsigned ThenCost = ThenCE ? ComputeSpeculationCost(ThenCE, DL) : 0;
if (OrigCost + ThenCost > 2 * PHINodeFoldingThreshold)
return false;
// constants.
for (unsigned i = 0, e = PN->getNumIncomingValues(); i != e; ++i) {
ConstantInt *CB = dyn_cast<ConstantInt>(PN->getIncomingValue(i));
- if (CB == 0 || !CB->getType()->isIntegerTy(1)) continue;
+ if (!CB || !CB->getType()->isIntegerTy(1)) continue;
// Okay, we now know that all edges from PredBB should be revectored to
// branch to RealDest.
}
if (!DominatesMergePoint(PN->getIncomingValue(0), BB, &AggressiveInsts,
- MaxCostVal0) ||
+ MaxCostVal0, DL) ||
!DominatesMergePoint(PN->getIncomingValue(1), BB, &AggressiveInsts,
- MaxCostVal1))
+ MaxCostVal1, DL))
return false;
}
// If we folded the first phi, PN dangles at this point. Refresh it. If
// we ran out of PHIs then we simplified them all.
PN = dyn_cast<PHINode>(BB->begin());
- if (PN == 0) return true;
+ if (!PN) return true;
// Don't fold i1 branches on PHIs which contain binary operators. These can
// often be turned into switches and other things.
// instructions in the predecessor blocks can be promoted as well. If
// not, we won't be able to get rid of the control flow, so it's not
// worth promoting to select instructions.
- BasicBlock *DomBlock = 0;
+ BasicBlock *DomBlock = nullptr;
BasicBlock *IfBlock1 = PN->getIncomingBlock(0);
BasicBlock *IfBlock2 = PN->getIncomingBlock(1);
if (cast<BranchInst>(IfBlock1->getTerminator())->isConditional()) {
- IfBlock1 = 0;
+ IfBlock1 = nullptr;
} else {
DomBlock = *pred_begin(IfBlock1);
for (BasicBlock::iterator I = IfBlock1->begin();!isa<TerminatorInst>(I);++I)
}
if (cast<BranchInst>(IfBlock2->getTerminator())->isConditional()) {
- IfBlock2 = 0;
+ IfBlock2 = nullptr;
} else {
DomBlock = *pred_begin(IfBlock2);
for (BasicBlock::iterator I = IfBlock2->begin();!isa<TerminatorInst>(I);++I)
"Looking for probabilities on unconditional branch?");
MDNode *ProfileData = BI->getMetadata(LLVMContext::MD_prof);
if (!ProfileData || ProfileData->getNumOperands() != 3) return false;
- ConstantInt *CITrue = dyn_cast<ConstantInt>(ProfileData->getOperand(1));
- ConstantInt *CIFalse = dyn_cast<ConstantInt>(ProfileData->getOperand(2));
+ ConstantInt *CITrue =
+ mdconst::dyn_extract<ConstantInt>(ProfileData->getOperand(1));
+ ConstantInt *CIFalse =
+ mdconst::dyn_extract<ConstantInt>(ProfileData->getOperand(2));
if (!CITrue || !CIFalse) return false;
ProbTrue = CITrue->getValue().getZExtValue();
ProbFalse = CIFalse->getValue().getZExtValue();
/// FoldBranchToCommonDest - If this basic block is simple enough, and if a
/// predecessor branches to us and one of our successors, fold the block into
/// the predecessor and use logical operations to pick the right destination.
-bool llvm::FoldBranchToCommonDest(BranchInst *BI) {
+bool llvm::FoldBranchToCommonDest(BranchInst *BI, const DataLayout *DL,
+ unsigned BonusInstThreshold) {
BasicBlock *BB = BI->getParent();
- Instruction *Cond = 0;
+ Instruction *Cond = nullptr;
if (BI->isConditional())
Cond = dyn_cast<Instruction>(BI->getCondition());
else {
}
}
- if (Cond == 0)
+ if (!Cond)
return false;
}
- if (Cond == 0 || (!isa<CmpInst>(Cond) && !isa<BinaryOperator>(Cond)) ||
- Cond->getParent() != BB || !Cond->hasOneUse())
+ if (!Cond || (!isa<CmpInst>(Cond) && !isa<BinaryOperator>(Cond)) ||
+ Cond->getParent() != BB || !Cond->hasOneUse())
return false;
- // Only allow this if the condition is a simple instruction that can be
- // executed unconditionally. It must be in the same block as the branch, and
- // must be at the front of the block.
- BasicBlock::iterator FrontIt = BB->front();
-
- // Ignore dbg intrinsics.
- while (isa<DbgInfoIntrinsic>(FrontIt)) ++FrontIt;
-
- // Allow a single instruction to be hoisted in addition to the compare
- // that feeds the branch. We later ensure that any values that _it_ uses
- // were also live in the predecessor, so that we don't unnecessarily create
- // register pressure or inhibit out-of-order execution.
- Instruction *BonusInst = 0;
- if (&*FrontIt != Cond &&
- FrontIt->hasOneUse() && FrontIt->user_back() == Cond &&
- isSafeToSpeculativelyExecute(FrontIt)) {
- BonusInst = &*FrontIt;
- ++FrontIt;
-
- // Ignore dbg intrinsics.
- while (isa<DbgInfoIntrinsic>(FrontIt)) ++FrontIt;
- }
-
- // Only a single bonus inst is allowed.
- if (&*FrontIt != Cond)
- return false;
-
// Make sure the instruction after the condition is the cond branch.
BasicBlock::iterator CondIt = Cond; ++CondIt;
- // Ingore dbg intrinsics.
+ // Ignore dbg intrinsics.
while (isa<DbgInfoIntrinsic>(CondIt)) ++CondIt;
if (&*CondIt != BI)
return false;
+ // Only allow this transformation if computing the condition doesn't involve
+ // too many instructions and these involved instructions can be executed
+ // unconditionally. We denote all involved instructions except the condition
+ // as "bonus instructions", and only allow this transformation when the
+ // number of the bonus instructions does not exceed a certain threshold.
+ unsigned NumBonusInsts = 0;
+ for (auto I = BB->begin(); Cond != I; ++I) {
+ // Ignore dbg intrinsics.
+ if (isa<DbgInfoIntrinsic>(I))
+ continue;
+ if (!I->hasOneUse() || !isSafeToSpeculativelyExecute(I, DL))
+ return false;
+ // I has only one use and can be executed unconditionally.
+ Instruction *User = dyn_cast<Instruction>(I->user_back());
+ if (User == nullptr || User->getParent() != BB)
+ return false;
+ // I is used in the same BB. Since BI uses Cond and doesn't have more slots
+ // to use any other instruction, User must be an instruction between next(I)
+ // and Cond.
+ ++NumBonusInsts;
+ // Early exits once we reach the limit.
+ if (NumBonusInsts > BonusInstThreshold)
+ return false;
+ }
+
// Cond is known to be a compare or binary operator. Check to make sure that
// neither operand is a potentially-trapping constant expression.
if (ConstantExpr *CE = dyn_cast<ConstantExpr>(Cond->getOperand(0)))
// Finally, don't infinitely unroll conditional loops.
BasicBlock *TrueDest = BI->getSuccessor(0);
- BasicBlock *FalseDest = (BI->isConditional()) ? BI->getSuccessor(1) : 0;
+ BasicBlock *FalseDest = (BI->isConditional()) ? BI->getSuccessor(1) : nullptr;
if (TrueDest == BB || FalseDest == BB)
return false;
// the common successor, verify that the same value flows in from both
// blocks.
SmallVector<PHINode*, 4> PHIs;
- if (PBI == 0 || PBI->isUnconditional() ||
+ if (!PBI || PBI->isUnconditional() ||
(BI->isConditional() &&
!SafeToMergeTerminators(BI, PBI)) ||
(!BI->isConditional() &&
continue;
}
- // Ensure that any values used in the bonus instruction are also used
- // by the terminator of the predecessor. This means that those values
- // must already have been resolved, so we won't be inhibiting the
- // out-of-order core by speculating them earlier. We also allow
- // instructions that are used by the terminator's condition because it
- // exposes more merging opportunities.
- bool UsedByBranch = (BonusInst && BonusInst->hasOneUse() &&
- BonusInst->user_back() == Cond);
-
- if (BonusInst && !UsedByBranch) {
- // Collect the values used by the bonus inst
- SmallPtrSet<Value*, 4> UsedValues;
- for (Instruction::op_iterator OI = BonusInst->op_begin(),
- OE = BonusInst->op_end(); OI != OE; ++OI) {
- Value *V = *OI;
- if (!isa<Constant>(V) && !isa<Argument>(V))
- UsedValues.insert(V);
- }
-
- SmallVector<std::pair<Value*, unsigned>, 4> Worklist;
- Worklist.push_back(std::make_pair(PBI->getOperand(0), 0));
-
- // Walk up to four levels back up the use-def chain of the predecessor's
- // terminator to see if all those values were used. The choice of four
- // levels is arbitrary, to provide a compile-time-cost bound.
- while (!Worklist.empty()) {
- std::pair<Value*, unsigned> Pair = Worklist.back();
- Worklist.pop_back();
-
- if (Pair.second >= 4) continue;
- UsedValues.erase(Pair.first);
- if (UsedValues.empty()) break;
-
- if (Instruction *I = dyn_cast<Instruction>(Pair.first)) {
- for (Instruction::op_iterator OI = I->op_begin(), OE = I->op_end();
- OI != OE; ++OI)
- Worklist.push_back(std::make_pair(OI->get(), Pair.second+1));
- }
- }
-
- if (!UsedValues.empty()) return false;
- }
-
DEBUG(dbgs() << "FOLDING BRANCH TO COMMON DEST:\n" << *PBI << *BB);
IRBuilder<> Builder(PBI);
PBI->swapSuccessors();
}
- // If we have a bonus inst, clone it into the predecessor block.
- Instruction *NewBonus = 0;
- if (BonusInst) {
- NewBonus = BonusInst->clone();
+ // If we have bonus instructions, clone them into the predecessor block.
+ // Note that there may be mutliple predecessor blocks, so we cannot move
+ // bonus instructions to a predecessor block.
+ ValueToValueMapTy VMap; // maps original values to cloned values
+ // We already make sure Cond is the last instruction before BI. Therefore,
+ // every instructions before Cond other than DbgInfoIntrinsic are bonus
+ // instructions.
+ for (auto BonusInst = BB->begin(); Cond != BonusInst; ++BonusInst) {
+ if (isa<DbgInfoIntrinsic>(BonusInst))
+ continue;
+ Instruction *NewBonusInst = BonusInst->clone();
+ RemapInstruction(NewBonusInst, VMap,
+ RF_NoModuleLevelChanges | RF_IgnoreMissingEntries);
+ VMap[BonusInst] = NewBonusInst;
// If we moved a load, we cannot any longer claim any knowledge about
// its potential value. The previous information might have been valid
// only given the branch precondition.
// For an analogous reason, we must also drop all the metadata whose
// semantics we don't understand.
- NewBonus->dropUnknownMetadata(LLVMContext::MD_dbg);
+ NewBonusInst->dropUnknownMetadata(LLVMContext::MD_dbg);
- PredBlock->getInstList().insert(PBI, NewBonus);
- NewBonus->takeName(BonusInst);
- BonusInst->setName(BonusInst->getName()+".old");
+ PredBlock->getInstList().insert(PBI, NewBonusInst);
+ NewBonusInst->takeName(BonusInst);
+ BonusInst->setName(BonusInst->getName() + ".old");
}
// Clone Cond into the predecessor basic block, and or/and the
// two conditions together.
Instruction *New = Cond->clone();
- if (BonusInst) New->replaceUsesOfWith(BonusInst, NewBonus);
+ RemapInstruction(New, VMap,
+ RF_NoModuleLevelChanges | RF_IgnoreMissingEntries);
PredBlock->getInstList().insert(PBI, New);
New->takeName(Cond);
- Cond->setName(New->getName()+".old");
+ Cond->setName(New->getName() + ".old");
if (BI->isConditional()) {
Instruction *NewCond =
MDBuilder(BI->getContext()).
createBranchWeights(MDWeights));
} else
- PBI->setMetadata(LLVMContext::MD_prof, NULL);
+ PBI->setMetadata(LLVMContext::MD_prof, nullptr);
} else {
// Update PHI nodes in the common successors.
for (unsigned i = 0, e = PHIs.size(); i != e; ++i) {
ConstantInt *PBI_C = cast<ConstantInt>(
PHIs[i]->getIncomingValueForBlock(PBI->getParent()));
assert(PBI_C->getType()->isIntegerTy(1));
- Instruction *MergedCond = 0;
+ Instruction *MergedCond = nullptr;
if (PBI->getSuccessor(0) == TrueDest) {
// Create (PBI_Cond and PBI_C) or (!PBI_Cond and BI_Value)
// PBI_C is true: PBI_Cond or (!PBI_Cond and BI_Value)
}
// If this is a conditional branch in an empty block, and if any
- // predecessors is a conditional branch to one of our destinations,
+ // predecessors are a conditional branch to one of our destinations,
// fold the conditions into logical ops and one cond br.
BasicBlock::iterator BBI = BB->begin();
// Ignore dbg intrinsics.
@@ -2372,16 +2451,33 @@ static bool SimplifyCondBranchToCondBranch(BranchInst *PBI, BranchInst *BI) {
// Do not perform this transformation if it would require
// insertion of a large number of select instructions. For targets
// without predication/cmovs, this is a big pessimization.
- BasicBlock *CommonDest = PBI->getSuccessor(PBIOp);
+ // Also do not perform this transformation if any phi node in the common
+ // destination block can trap when reached by BB or PBB (PR17073). In that
+ // case, it would be unsafe to hoist the operation into a select instruction.
+
+ BasicBlock *CommonDest = PBI->getSuccessor(PBIOp);
unsigned NumPhis = 0;
for (BasicBlock::iterator II = CommonDest->begin();
- isa<PHINode>(II); ++II, ++NumPhis)
+ isa<PHINode>(II); ++II, ++NumPhis) {
if (NumPhis > 2) // Disable this xform.
return false;
+ PHINode *PN = cast<PHINode>(II);
+ Value *BIV = PN->getIncomingValueForBlock(BB);
+ if (ConstantExpr *CE = dyn_cast<ConstantExpr>(BIV))
+ if (CE->canTrap())
+ return false;
+
+ unsigned PBBIdx = PN->getBasicBlockIndex(PBI->getParent());
+ Value *PBIV = PN->getIncomingValue(PBBIdx);
+ if (ConstantExpr *CE = dyn_cast<ConstantExpr>(PBIV))
+ if (CE->canTrap())
+ return false;
+ }
+
// Finally, if everything is ok, fold the branches to logical ops.
- BasicBlock *OtherDest = BI->getSuccessor(BIOp ^ 1);
+ BasicBlock *OtherDest = BI->getSuccessor(BIOp ^ 1);
DEBUG(dbgs() << "FOLDING BRs:" << *PBI->getParent()
<< "AND: " << *BI->getParent());
@@ -2497,16 +2593,16 @@ static bool SimplifyTerminatorOnSelect(TerminatorInst *OldTerm, Value *Cond,
// If TrueBB and FalseBB are equal, only try to preserve one copy of that
// successor.
BasicBlock *KeepEdge1 = TrueBB;
- BasicBlock *KeepEdge2 = TrueBB != FalseBB ? FalseBB : 0;
+ BasicBlock *KeepEdge2 = TrueBB != FalseBB ? FalseBB : nullptr;
// Then remove the rest.
for (unsigned I = 0, E = OldTerm->getNumSuccessors(); I != E; ++I) {
BasicBlock *Succ = OldTerm->getSuccessor(I);
// Make sure only to keep exactly one copy of each edge.
if (Succ == KeepEdge1)
- KeepEdge1 = 0;
+ KeepEdge1 = nullptr;
else if (Succ == KeepEdge2)
- KeepEdge2 = 0;
+ KeepEdge2 = nullptr;
else
Succ->removePredecessor(OldTerm->getParent());
}
Builder.SetCurrentDebugLocation(OldTerm->getDebugLoc());
// Insert an appropriate new terminator.
- if ((KeepEdge1 == 0) && (KeepEdge2 == 0)) {
+ if (!KeepEdge1 && !KeepEdge2) {
if (TrueBB == FalseBB)
// We were only looking for one successor, and it was present.
// Create an unconditional branch to it.
// One of the selected values was a successor, but the other wasn't.
// Insert an unconditional branch to the one that was found;
// the edge to the one that wasn't must be unreachable.
- if (KeepEdge1 == 0)
+ if (!KeepEdge1)
// Only TrueBB was found.
Builder.CreateBr(TrueBB);
else
/// the PHI, merging the third icmp into the switch.
static bool TryToSimplifyUncondBranchWithICmpInIt(
ICmpInst *ICI, IRBuilder<> &Builder, const TargetTransformInfo &TTI,
- const DataLayout *DL) {
+ unsigned BonusInstThreshold, const DataLayout *DL, AssumptionCache *AC) {
BasicBlock *BB = ICI->getParent();
// If the block has any PHIs in it or the icmp has multiple uses, it is too
// 'V' and this block is the default case for the switch. In this case we can
// fold the compared value into the switch to simplify things.
BasicBlock *Pred = BB->getSinglePredecessor();
- if (Pred == 0 || !isa<SwitchInst>(Pred->getTerminator())) return false;
+ if (!Pred || !isa<SwitchInst>(Pred->getTerminator())) return false;
SwitchInst *SI = cast<SwitchInst>(Pred->getTerminator());
if (SI->getCondition() != V)
ICI->eraseFromParent();
}
// BB is now empty, so it is likely to simplify away.
- return SimplifyCFG(BB, TTI, DL) | true;
+ return SimplifyCFG(BB, TTI, BonusInstThreshold, DL, AC) | true;
}
// Ok, the block is reachable from the default dest. If the constant we're
ICI->replaceAllUsesWith(V);
ICI->eraseFromParent();
// BB is now empty, so it is likely to simplify away.
- return SimplifyCFG(BB, TTI, DL) | true;
+ return SimplifyCFG(BB, TTI, BonusInstThreshold, DL, AC) | true;
}
// The use of the icmp has to be in the 'end' block, by the only PHI node in
// the block.
BasicBlock *SuccBlock = BB->getTerminator()->getSuccessor(0);
PHINode *PHIUse = dyn_cast<PHINode>(ICI->user_back());
- if (PHIUse == 0 || PHIUse != &SuccBlock->front() ||
+ if (PHIUse == nullptr || PHIUse != &SuccBlock->front() ||
isa<PHINode>(++BasicBlock::iterator(PHIUse)))
return false;
static bool SimplifyBranchOnICmpChain(BranchInst *BI, const DataLayout *DL,
IRBuilder<> &Builder) {
Instruction *Cond = dyn_cast<Instruction>(BI->getCondition());
- if (Cond == 0) return false;
-
+ if (!Cond) return false;
// Change br (X == 0 | X == 1), T, F into a switch instruction.
// If this is a bunch of seteq's or'd together, or if it's a bunch of
// 'setne's and'ed together, collect them.
- Value *CompVal = 0;
- std::vector<ConstantInt*> Values;
- bool TrueWhenEqual = true;
- Value *ExtraCase = 0;
- unsigned UsedICmps = 0;
-
- if (Cond->getOpcode() == Instruction::Or) {
- CompVal = GatherConstantCompares(Cond, Values, ExtraCase, DL, true,
- UsedICmps);
- } else if (Cond->getOpcode() == Instruction::And) {
- CompVal = GatherConstantCompares(Cond, Values, ExtraCase, DL, false,
- UsedICmps);
- TrueWhenEqual = false;
- }
+
+ // Try to gather values from a chain of and/or to be turned into a switch
+ ConstantComparesGatherer ConstantCompare(Cond, DL);
+ // Unpack the result
+ SmallVectorImpl<ConstantInt*> &Values = ConstantCompare.Vals;
+ Value *CompVal = ConstantCompare.CompValue;
+ unsigned UsedICmps = ConstantCompare.UsedICmps;
+ Value *ExtraCase = ConstantCompare.Extra;
// If we didn't have a multiply compared value, fail.
- if (CompVal == 0) return false;
+ if (!CompVal) return false;
// Avoid turning single icmps into a switch.
if (UsedICmps <= 1)
return false;
+ bool TrueWhenEqual = (Cond->getOpcode() == Instruction::Or);
+
// There might be duplicate constants in the list, which the switch
// instruction can't handle, remove them now.
array_pod_sort(Values.begin(), Values.end(), ConstantIntSortPredicate);
}
// If we eliminated all predecessors of the block, delete the block now.
- if (pred_begin(BB) == pred_end(BB))
+ if (pred_empty(BB))
// We know there are no successors, so just nuke the block.
BB->eraseFromParent();
// Find the most popular block.
unsigned MaxPop = 0;
unsigned MaxIndex = 0;
- BasicBlock *MaxBlock = 0;
+ BasicBlock *MaxBlock = nullptr;
for (std::map<BasicBlock*, std::pair<unsigned, unsigned> >::iterator
I = Popularity.begin(), E = Popularity.end(); I != E; ++I) {
if (I->second.first > MaxPop ||
}
// If this block is now dead, remove it.
- if (pred_begin(BB) == pred_end(BB) &&
+ if (pred_empty(BB) &&
BB != &BB->getParent()->getEntryBlock()) {
// We know there are no successors, so just nuke the block.
BB->eraseFromParent();
/// EliminateDeadSwitchCases - Compute masked bits for the condition of a switch
/// and use it to remove dead cases.
-static bool EliminateDeadSwitchCases(SwitchInst *SI) {
+static bool EliminateDeadSwitchCases(SwitchInst *SI, const DataLayout *DL,
+ AssumptionCache *AC) {
Value *Cond = SI->getCondition();
unsigned Bits = Cond->getType()->getIntegerBitWidth();
APInt KnownZero(Bits, 0), KnownOne(Bits, 0);
- ComputeMaskedBits(Cond, KnownZero, KnownOne);
+ computeKnownBits(Cond, KnownZero, KnownOne, DL, 0, AC, SI);
// Gather dead cases.
SmallVector<ConstantInt*, 8> DeadCases;
BasicBlock *BB,
int *PhiIndex) {
if (BB->getFirstNonPHIOrDbg() != BB->getTerminator())
- return NULL; // BB must be empty to be a candidate for simplification.
+ return nullptr; // BB must be empty to be a candidate for simplification.
if (!BB->getSinglePredecessor())
- return NULL; // BB must be dominated by the switch.
+ return nullptr; // BB must be dominated by the switch.
BranchInst *Branch = dyn_cast<BranchInst>(BB->getTerminator());
if (!Branch || !Branch->isUnconditional())
- return NULL; // Terminator must be unconditional branch.
+ return nullptr; // Terminator must be unconditional branch.
BasicBlock *Succ = Branch->getSuccessor(0);
return PHI;
}
- return NULL;
+ return nullptr;
}
/// ForwardSwitchConditionToPHI - Try to forward the condition of a switch
/// ValidLookupTableConstant - Return true if the backend will be able to handle
/// initializing an array of constants like C.
static bool ValidLookupTableConstant(Constant *C) {
+ if (C->isThreadDependent())
+ return false;
+ if (C->isDLLImportDependent())
+ return false;
+
if (ConstantExpr *CE = dyn_cast<ConstantExpr>(C))
return CE->isGEPWithNoNotionalOverIndexing();
if (SelectInst *Select = dyn_cast<SelectInst>(I)) {
Constant *A = LookupConstant(Select->getCondition(), ConstantPool);
if (!A)
- return 0;
+ return nullptr;
if (A->isAllOnesValue())
return LookupConstant(Select->getTrueValue(), ConstantPool);
if (A->isNullValue())
return LookupConstant(Select->getFalseValue(), ConstantPool);
- return 0;
+ return nullptr;
}
SmallVector<Constant *, 4> COps;
if (Constant *A = LookupConstant(I->getOperand(N), ConstantPool))
COps.push_back(A);
else
- return 0;
+ return nullptr;
}
if (CmpInst *Cmp = dyn_cast<CmpInst>(I))
continue;
} else if (Constant *C = ConstantFold(I, ConstantPool, DL)) {
// Instruction is side-effect free and constant.
+
+ // If the instruction has uses outside this block or a phi node slot for
+ // the block, it is not safe to bypass the instruction since it would then
+ // no longer dominate all its uses.
+ for (auto &Use : I->uses()) {
+ User *User = Use.getUser();
+ if (Instruction *I = dyn_cast<Instruction>(User))
+ if (I->getParent() == CaseDest)
+ continue;
+ if (PHINode *Phi = dyn_cast<PHINode>(User))
+ if (Phi->getIncomingBlock(Use) == CaseDest)
+ continue;
+ return false;
+ }
+
ConstantPool.insert(std::make_pair(I, C));
} else {
break;
if (!ConstVal)
return false;
- // Note: If the constant comes from constant-propagating the case value
- // through the CaseDest basic block, it will be safe to remove the
- // instructions in that block. They cannot be used (except in the phi nodes
- // we visit) outside CaseDest, because that block does not dominate its
- // successor. If it did, we would not be in this phi node.
-
// Be conservative about which kinds of constants we support.
if (!ValidLookupTableConstant(ConstVal))
return false;
return Res.size() > 0;
}
+// MapCaseToResult - Helper function used to
+// add CaseVal to the list of cases that generate Result.
+static void MapCaseToResult(ConstantInt *CaseVal,
+ SwitchCaseResultVectorTy &UniqueResults,
+ Constant *Result) {
+ for (auto &I : UniqueResults) {
+ if (I.first == Result) {
+ I.second.push_back(CaseVal);
+ return;
+ }
+ }
+ UniqueResults.push_back(std::make_pair(Result,
+ SmallVector<ConstantInt*, 4>(1, CaseVal)));
+}
+
+// InitializeUniqueCases - Helper function that initializes a map containing
+// results for the PHI node of the common destination block for a switch
+// instruction. Returns false if multiple PHI nodes have been found or if
+// there is not a common destination block for the switch.
+static bool InitializeUniqueCases(
+ SwitchInst *SI, const DataLayout *DL, PHINode *&PHI,
+ BasicBlock *&CommonDest,
+ SwitchCaseResultVectorTy &UniqueResults,
+ Constant *&DefaultResult) {
+ for (auto &I : SI->cases()) {
+ ConstantInt *CaseVal = I.getCaseValue();
+
+ // Resulting value at phi nodes for this case value.
+ SwitchCaseResultsTy Results;
+ if (!GetCaseResults(SI, CaseVal, I.getCaseSuccessor(), &CommonDest, Results,
+ DL))
+ return false;
+
+ // Only one value per case is permitted
+ if (Results.size() > 1)
+ return false;
+ MapCaseToResult(CaseVal, UniqueResults, Results.begin()->second);
+
+ // Check the PHI consistency.
+ if (!PHI)
+ PHI = Results[0].first;
+ else if (PHI != Results[0].first)
+ return false;
+ }
+ // Find the default result value.
+ SmallVector<std::pair<PHINode *, Constant *>, 1> DefaultResults;
+ BasicBlock *DefaultDest = SI->getDefaultDest();
+ GetCaseResults(SI, nullptr, SI->getDefaultDest(), &CommonDest, DefaultResults,
+ DL);
+ // If the default value is not found abort unless the default destination
+ // is unreachable.
+ DefaultResult =
+ DefaultResults.size() == 1 ? DefaultResults.begin()->second : nullptr;
+ if ((!DefaultResult &&
+ !isa<UnreachableInst>(DefaultDest->getFirstNonPHIOrDbg())))
+ return false;
+
+ return true;
+}
+
+// ConvertTwoCaseSwitch - Helper function that checks if it is possible to
+// transform a switch with only two cases (or two cases + default)
+// that produces a result into a value select.
+// Example:
+// switch (a) {
+// case 10: %0 = icmp eq i32 %a, 10
+// return 10; %1 = select i1 %0, i32 10, i32 4
+// case 20: ----> %2 = icmp eq i32 %a, 20
+// return 2; %3 = select i1 %2, i32 2, i32 %1
+// default:
+// return 4;
+// }
+static Value *
+ConvertTwoCaseSwitch(const SwitchCaseResultVectorTy &ResultVector,
+ Constant *DefaultResult, Value *Condition,
+ IRBuilder<> &Builder) {
+ assert(ResultVector.size() == 2 &&
+ "We should have exactly two unique results at this point");
+ // If we are selecting between only two cases transform into a simple
+ // select or a two-way select if default is possible.
+ if (ResultVector[0].second.size() == 1 &&
+ ResultVector[1].second.size() == 1) {
+ ConstantInt *const FirstCase = ResultVector[0].second[0];
+ ConstantInt *const SecondCase = ResultVector[1].second[0];
+
+ bool DefaultCanTrigger = DefaultResult;
+ Value *SelectValue = ResultVector[1].first;
+ if (DefaultCanTrigger) {
+ Value *const ValueCompare =
+ Builder.CreateICmpEQ(Condition, SecondCase, "switch.selectcmp");
+ SelectValue = Builder.CreateSelect(ValueCompare, ResultVector[1].first,
+ DefaultResult, "switch.select");
+ }
+ Value *const ValueCompare =
+ Builder.CreateICmpEQ(Condition, FirstCase, "switch.selectcmp");
+ return Builder.CreateSelect(ValueCompare, ResultVector[0].first, SelectValue,
+ "switch.select");
+ }
+
+ return nullptr;
+}
+
+// RemoveSwitchAfterSelectConversion - Helper function to cleanup a switch
+// instruction that has been converted into a select, fixing up PHI nodes and
+// basic blocks.
+static void RemoveSwitchAfterSelectConversion(SwitchInst *SI, PHINode *PHI,
+ Value *SelectValue,
+ IRBuilder<> &Builder) {
+ BasicBlock *SelectBB = SI->getParent();
+ while (PHI->getBasicBlockIndex(SelectBB) >= 0)
+ PHI->removeIncomingValue(SelectBB);
+ PHI->addIncoming(SelectValue, SelectBB);
+
+ Builder.CreateBr(PHI->getParent());
+
+ // Remove the switch.
+ for (unsigned i = 0, e = SI->getNumSuccessors(); i < e; ++i) {
+ BasicBlock *Succ = SI->getSuccessor(i);
+
+ if (Succ == PHI->getParent())
+ continue;
+ Succ->removePredecessor(SelectBB);
+ }
+ SI->eraseFromParent();
+}
+
+/// SwitchToSelect - If the switch is only used to initialize one or more
+/// phi nodes in a common successor block with only two different
+/// constant values, replace the switch with select.
+static bool SwitchToSelect(SwitchInst *SI, IRBuilder<> &Builder,
+ const DataLayout *DL, AssumptionCache *AC) {
+ Value *const Cond = SI->getCondition();
+ PHINode *PHI = nullptr;
+ BasicBlock *CommonDest = nullptr;
+ Constant *DefaultResult;
+ SwitchCaseResultVectorTy UniqueResults;
+ // Collect all the cases that will deliver the same value from the switch.
+ if (!InitializeUniqueCases(SI, DL, PHI, CommonDest, UniqueResults,
+ DefaultResult))
+ return false;
+ // Selects choose between maximum two values.
+ if (UniqueResults.size() != 2)
+ return false;
+ assert(PHI != nullptr && "PHI for value select not found");
+
+ Builder.SetInsertPoint(SI);
+ Value *SelectValue = ConvertTwoCaseSwitch(
+ UniqueResults,
+ DefaultResult, Cond, Builder);
+ if (SelectValue) {
+ RemoveSwitchAfterSelectConversion(SI, PHI, SelectValue, Builder);
+ return true;
+ }
+ // The switch couldn't be converted into a select.
+ return false;
+}
+
namespace {
/// SwitchLookupTable - This class represents a lookup table that can be used
/// to replace a switch.
// store that single value and return it for each lookup.
SingleValueKind,
+ // For tables where there is a linear relationship between table index
+ // and values. We calculate the result with a simple multiplication
+ // and addition instead of a table lookup.
+ LinearMapKind,
+
// For small tables with integer elements, we can pack them into a bitmap
// that fits into a target-legal register. Values are retrieved by
// shift and mask operations.
ConstantInt *BitMap;
IntegerType *BitMapElementTy;
+ // For LinearMapKind, these are the constants used to derive the value.
+ ConstantInt *LinearOffset;
+ ConstantInt *LinearMultiplier;
+
// For ArrayKind, this is the array.
GlobalVariable *Array;
};
const SmallVectorImpl<std::pair<ConstantInt*, Constant*> >& Values,
Constant *DefaultValue,
const DataLayout *DL)
- : SingleValue(0), BitMap(0), BitMapElementTy(0), Array(0) {
+ : SingleValue(nullptr), BitMap(nullptr), BitMapElementTy(nullptr),
+ LinearOffset(nullptr), LinearMultiplier(nullptr), Array(nullptr) {
assert(Values.size() && "Can't build lookup table without values!");
assert(TableSize >= Values.size() && "Can't fit values in table!");
TableContents[Idx] = CaseRes;
if (CaseRes != SingleValue)
- SingleValue = 0;
+ SingleValue = nullptr;
}
// Fill in any holes in the table with the default result.
if (Values.size() < TableSize) {
- assert(DefaultValue && "Need a default value to fill the lookup table holes.");
+ assert(DefaultValue &&
+ "Need a default value to fill the lookup table holes.");
assert(DefaultValue->getType() == ValueType);
for (uint64_t I = 0; I < TableSize; ++I) {
if (!TableContents[I])
}
if (DefaultValue != SingleValue)
- SingleValue = 0;
+ SingleValue = nullptr;
}
// If each element in the table contains the same value, we only need to store
return;
}
+ // Check if we can derive the value with a linear transformation from the
+ // table index.
+ if (isa<IntegerType>(ValueType)) {
+ bool LinearMappingPossible = true;
+ APInt PrevVal;
+ APInt DistToPrev;
+ assert(TableSize >= 2 && "Should be a SingleValue table.");
+ // Check if there is the same distance between two consecutive values.
+ for (uint64_t I = 0; I < TableSize; ++I) {
+ ConstantInt *ConstVal = dyn_cast<ConstantInt>(TableContents[I]);
+ if (!ConstVal) {
+ // This is an undef. We could deal with it, but undefs in lookup tables
+ // are very seldom. It's probably not worth the additional complexity.
+ LinearMappingPossible = false;
+ break;
+ }
+ APInt Val = ConstVal->getValue();
+ if (I != 0) {
+ APInt Dist = Val - PrevVal;
+ if (I == 1) {
+ DistToPrev = Dist;
+ } else if (Dist != DistToPrev) {
+ LinearMappingPossible = false;
+ break;
+ }
+ }
+ PrevVal = Val;
+ }
+ if (LinearMappingPossible) {
+ LinearOffset = cast<ConstantInt>(TableContents[0]);
+ LinearMultiplier = ConstantInt::get(M.getContext(), DistToPrev);
+ Kind = LinearMapKind;
+ ++NumLinearMaps;
+ return;
+ }
+ }
+
// If the type is integer and the table fits in a register, build a bitmap.
if (WouldFitInRegister(DL, TableSize, ValueType)) {
IntegerType *IT = cast<IntegerType>(ValueType);
switch (Kind) {
case SingleValueKind:
return SingleValue;
+ case LinearMapKind: {
+ // Derive the result value from the input value.
+ Value *Result = Builder.CreateIntCast(Index, LinearMultiplier->getType(),
+ false, "switch.idx.cast");
+ if (!LinearMultiplier->isOne())
+ Result = Builder.CreateMul(Result, LinearMultiplier, "switch.idx.mult");
+ if (!LinearOffset->isZero())
+ Result = Builder.CreateAdd(Result, LinearOffset, "switch.offset");
+ return Result;
+ }
case BitMapKind: {
// Type of the bitmap (e.g. i59).
IntegerType *MapTy = BitMap->getType();
"switch.masked");
}
case ArrayKind: {
+ // Make sure the table index will not overflow when treated as signed.
+ IntegerType *IT = cast<IntegerType>(Index->getType());
+ uint64_t TableSize = Array->getInitializer()->getType()
+ ->getArrayNumElements();
+ if (TableSize > (1ULL << (IT->getBitWidth() - 1)))
+ Index = Builder.CreateZExt(Index,
+ IntegerType::get(IT->getContext(),
+ IT->getBitWidth() + 1),
+ "switch.tableidx.zext");
+
Value *GEPIndices[] = { Builder.getInt32(0), Index };
Value *GEP = Builder.CreateInBoundsGEP(Array, GEPIndices,
"switch.gep");
bool AllTablesFitInRegister = true;
bool HasIllegalType = false;
- for (SmallDenseMap<PHINode*, Type*>::const_iterator I = ResultTypes.begin(),
- E = ResultTypes.end(); I != E; ++I) {
- Type *Ty = I->second;
+ for (const auto &I : ResultTypes) {
+ Type *Ty = I.second;
// Saturate this flag to true.
HasIllegalType = HasIllegalType || !TTI.isTypeLegal(Ty);
return SI->getNumCases() * 10 >= TableSize * 4;
}
+/// Try to reuse the switch table index compare. Following pattern:
+/// \code
+/// if (idx < tablesize)
+/// r = table[idx]; // table does not contain default_value
+/// else
+/// r = default_value;
+/// if (r != default_value)
+/// ...
+/// \endcode
+/// Is optimized to:
+/// \code
+/// cond = idx < tablesize;
+/// if (cond)
+/// r = table[idx];
+/// else
+/// r = default_value;
+/// if (cond)
+/// ...
+/// \endcode
+/// Jump threading will then eliminate the second if(cond).
+static void reuseTableCompare(User *PhiUser, BasicBlock *PhiBlock,
+ BranchInst *RangeCheckBranch, Constant *DefaultValue,
+ const SmallVectorImpl<std::pair<ConstantInt*, Constant*> >& Values) {
+
+ ICmpInst *CmpInst = dyn_cast<ICmpInst>(PhiUser);
+ if (!CmpInst)
+ return;
+
+ // We require that the compare is in the same block as the phi so that jump
+ // threading can do its work afterwards.
+ if (CmpInst->getParent() != PhiBlock)
+ return;
+
+ Constant *CmpOp1 = dyn_cast<Constant>(CmpInst->getOperand(1));
+ if (!CmpOp1)
+ return;
+
+ Value *RangeCmp = RangeCheckBranch->getCondition();
+ Constant *TrueConst = ConstantInt::getTrue(RangeCmp->getType());
+ Constant *FalseConst = ConstantInt::getFalse(RangeCmp->getType());
+
+ // Check if the compare with the default value is constant true or false.
+ Constant *DefaultConst = ConstantExpr::getICmp(CmpInst->getPredicate(),
+ DefaultValue, CmpOp1, true);
+ if (DefaultConst != TrueConst && DefaultConst != FalseConst)
+ return;
+
+ // Check if the compare with the case values is distinct from the default
+ // compare result.
+ for (auto ValuePair : Values) {
+ Constant *CaseConst = ConstantExpr::getICmp(CmpInst->getPredicate(),
+ ValuePair.second, CmpOp1, true);
+ if (!CaseConst || CaseConst == DefaultConst)
+ return;
+ assert((CaseConst == TrueConst || CaseConst == FalseConst) &&
+ "Expect true or false as compare result.");
+ }
+
+ // Check if the branch instruction dominates the phi node. It's a simple
+ // dominance check, but sufficient for our needs.
+ // Although this check is invariant in the calling loops, it's better to do it
+ // at this late stage. Practically we do it at most once for a switch.
+ BasicBlock *BranchBlock = RangeCheckBranch->getParent();
+ for (auto PI = pred_begin(PhiBlock), E = pred_end(PhiBlock); PI != E; ++PI) {
+ BasicBlock *Pred = *PI;
+ if (Pred != BranchBlock && Pred->getUniquePredecessor() != BranchBlock)
+ return;
+ }
+
+ if (DefaultConst == FalseConst) {
+ // The compare yields the same result. We can replace it.
+ CmpInst->replaceAllUsesWith(RangeCmp);
+ ++NumTableCmpReuses;
+ } else {
+ // The compare yields the same result, just inverted. We can replace it.
+ Value *InvertedTableCmp = BinaryOperator::CreateXor(RangeCmp,
+ ConstantInt::get(RangeCmp->getType(), 1), "inverted.cmp",
+ RangeCheckBranch);
+ CmpInst->replaceAllUsesWith(InvertedTableCmp);
+ ++NumTableCmpReuses;
+ }
+}
+
/// SwitchToLookupTable - If the switch is only used to initialize one or more
/// phi nodes in a common successor block with different constant values,
/// replace the switch with lookup tables.
ConstantInt *MinCaseVal = CI.getCaseValue();
ConstantInt *MaxCaseVal = CI.getCaseValue();
- BasicBlock *CommonDest = 0;
+ BasicBlock *CommonDest = nullptr;
typedef SmallVector<std::pair<ConstantInt*, Constant*>, 4> ResultListTy;
SmallDenseMap<PHINode*, ResultListTy> ResultLists;
SmallDenseMap<PHINode*, Constant*> DefaultResults;
return false;
// Append the result from this case to the list for each phi.
- for (ResultsTy::iterator I = Results.begin(), E = Results.end(); I!=E; ++I) {
- if (!ResultLists.count(I->first))
- PHIs.push_back(I->first);
- ResultLists[I->first].push_back(std::make_pair(CaseVal, I->second));
+ for (const auto &I : Results) {
+ PHINode *PHI = I.first;
+ Constant *Value = I.second;
+ if (!ResultLists.count(PHI))
+ PHIs.push_back(PHI);
+ ResultLists[PHI].push_back(std::make_pair(CaseVal, Value));
}
}
// Keep track of the result types.
- for (size_t I = 0, E = PHIs.size(); I != E; ++I) {
- PHINode *PHI = PHIs[I];
+ for (PHINode *PHI : PHIs) {
ResultTypes[PHI] = ResultLists[PHI][0].second->getType();
}
uint64_t TableSize = RangeSpread.getLimitedValue() + 1;
bool TableHasHoles = (NumResults < TableSize);
- // If the table has holes, we need a constant result for the default case.
+ // If the table has holes, we need a constant result for the default case
+ // or a bitmask that fits in a register.
SmallVector<std::pair<PHINode*, Constant*>, 4> DefaultResultsList;
- if (TableHasHoles && !GetCaseResults(SI, 0, SI->getDefaultDest(), &CommonDest,
- DefaultResultsList, DL))
- return false;
+ bool HasDefaultResults = GetCaseResults(SI, nullptr, SI->getDefaultDest(),
+ &CommonDest, DefaultResultsList, DL);
+
+ bool NeedMask = (TableHasHoles && !HasDefaultResults);
+ if (NeedMask) {
+ // As an extra penalty for the validity test we require more cases.
+ if (SI->getNumCases() < 4) // FIXME: Find best threshold value (benchmark).
+ return false;
+ if (!(DL && DL->fitsInLegalInteger(TableSize)))
+ return false;
+ }
- for (size_t I = 0, E = DefaultResultsList.size(); I != E; ++I) {
- PHINode *PHI = DefaultResultsList[I].first;
- Constant *Result = DefaultResultsList[I].second;
+ for (const auto &I : DefaultResultsList) {
+ PHINode *PHI = I.first;
+ Constant *Result = I.second;
DefaultResults[PHI] = Result;
}
// lookup table BB. Otherwise, check if the condition value is within the case
// range. If it is so, branch to the new BB. Otherwise branch to SI's default
// destination.
+ BranchInst *RangeCheckBranch = nullptr;
+
const bool GeneratingCoveredLookupTable = MaxTableSize == TableSize;
if (GeneratingCoveredLookupTable) {
Builder.CreateBr(LookupBB);
- SI->getDefaultDest()->removePredecessor(SI->getParent());
+ // We cached PHINodes in PHIs, to avoid accessing deleted PHINodes later,
+ // do not delete PHINodes here.
+ SI->getDefaultDest()->removePredecessor(SI->getParent(),
+ true/*DontDeleteUselessPHIs*/);
} else {
Value *Cmp = Builder.CreateICmpULT(TableIndex, ConstantInt::get(
- MinCaseVal->getType(), TableSize));
- Builder.CreateCondBr(Cmp, LookupBB, SI->getDefaultDest());
+ MinCaseVal->getType(), TableSize));
+ RangeCheckBranch = Builder.CreateCondBr(Cmp, LookupBB, SI->getDefaultDest());
}
// Populate the BB that does the lookups.
Builder.SetInsertPoint(LookupBB);
+
+ if (NeedMask) {
+ // Before doing the lookup we do the hole check.
+ // The LookupBB is therefore re-purposed to do the hole check
+ // and we create a new LookupBB.
+ BasicBlock *MaskBB = LookupBB;
+ MaskBB->setName("switch.hole_check");
+ LookupBB = BasicBlock::Create(Mod.getContext(),
+ "switch.lookup",
+ CommonDest->getParent(),
+ CommonDest);
+
+ // Make the mask's bitwidth at least 8bit and a power-of-2 to avoid
+ // unnecessary illegal types.
+ uint64_t TableSizePowOf2 = NextPowerOf2(std::max(7ULL, TableSize - 1ULL));
+ APInt MaskInt(TableSizePowOf2, 0);
+ APInt One(TableSizePowOf2, 1);
+ // Build bitmask; fill in a 1 bit for every case.
+ const ResultListTy &ResultList = ResultLists[PHIs[0]];
+ for (size_t I = 0, E = ResultList.size(); I != E; ++I) {
+ uint64_t Idx = (ResultList[I].first->getValue() -
+ MinCaseVal->getValue()).getLimitedValue();
+ MaskInt |= One << Idx;
+ }
+ ConstantInt *TableMask = ConstantInt::get(Mod.getContext(), MaskInt);
+
+ // Get the TableIndex'th bit of the bitmask.
+ // If this bit is 0 (meaning hole) jump to the default destination,
+ // else continue with table lookup.
+ IntegerType *MapTy = TableMask->getType();
+ Value *MaskIndex = Builder.CreateZExtOrTrunc(TableIndex, MapTy,
+ "switch.maskindex");
+ Value *Shifted = Builder.CreateLShr(TableMask, MaskIndex,
+ "switch.shifted");
+ Value *LoBit = Builder.CreateTrunc(Shifted,
+ Type::getInt1Ty(Mod.getContext()),
+ "switch.lobit");
+ Builder.CreateCondBr(LoBit, LookupBB, SI->getDefaultDest());
+
+ Builder.SetInsertPoint(LookupBB);
+ AddPredecessorToBlock(SI->getDefaultDest(), MaskBB, SI->getParent());
+ }
+
bool ReturnedEarly = false;
for (size_t I = 0, E = PHIs.size(); I != E; ++I) {
PHINode *PHI = PHIs[I];
+ const ResultListTy &ResultList = ResultLists[PHI];
- SwitchLookupTable Table(Mod, TableSize, MinCaseVal, ResultLists[PHI],
- DefaultResults[PHI], DL);
+ // If using a bitmask, use any value to fill the lookup table holes.
+ Constant *DV = NeedMask ? ResultLists[PHI][0].second : DefaultResults[PHI];
+ SwitchLookupTable Table(Mod, TableSize, MinCaseVal, ResultList, DV, DL);
Value *Result = Table.BuildLookup(TableIndex, Builder);
break;
}
+ // Do a small peephole optimization: re-use the switch table compare if
+ // possible.
+ if (!TableHasHoles && HasDefaultResults && RangeCheckBranch) {
+ BasicBlock *PhiBlock = PHI->getParent();
+ // Search for compare instructions which use the phi.
+ for (auto *User : PHI->users()) {
+ reuseTableCompare(User, PhiBlock, RangeCheckBranch, DV, ResultList);
+ }
+ }
+
PHI->addIncoming(Result, LookupBB);
}
SI->eraseFromParent();
++NumLookupTables;
+ if (NeedMask)
+ ++NumLookupTablesHoles;
return true;
}
// see if that predecessor totally determines the outcome of this switch.
if (BasicBlock *OnlyPred = BB->getSinglePredecessor())
if (SimplifyEqualityComparisonWithOnlyPredecessor(SI, OnlyPred, Builder))
- return SimplifyCFG(BB, TTI, DL) | true;
+ return SimplifyCFG(BB, TTI, BonusInstThreshold, DL, AC) | true;
Value *Cond = SI->getCondition();
if (SelectInst *Select = dyn_cast<SelectInst>(Cond))
if (SimplifySwitchOnSelect(SI, Select))
- return SimplifyCFG(BB, TTI, DL) | true;
+ return SimplifyCFG(BB, TTI, BonusInstThreshold, DL, AC) | true;
// If the block only contains the switch, see if we can fold the block
// away into any preds.
++BBI;
if (SI == &*BBI)
if (FoldValueComparisonIntoPredecessors(SI, Builder))
- return SimplifyCFG(BB, TTI, DL) | true;
+ return SimplifyCFG(BB, TTI, BonusInstThreshold, DL, AC) | true;
}
// Try to transform the switch into an icmp and a branch.
if (TurnSwitchRangeIntoICmp(SI, Builder))
- return SimplifyCFG(BB, TTI, DL) | true;
+ return SimplifyCFG(BB, TTI, BonusInstThreshold, DL, AC) | true;
// Remove unreachable cases.
- if (EliminateDeadSwitchCases(SI))
- return SimplifyCFG(BB, TTI, DL) | true;
+ if (EliminateDeadSwitchCases(SI, DL, AC))
+ return SimplifyCFG(BB, TTI, BonusInstThreshold, DL, AC) | true;
+
+ if (SwitchToSelect(SI, Builder, DL, AC))
+ return SimplifyCFG(BB, TTI, BonusInstThreshold, DL, AC) | true;
if (ForwardSwitchConditionToPHI(SI))
- return SimplifyCFG(BB, TTI, DL) | true;
+ return SimplifyCFG(BB, TTI, BonusInstThreshold, DL, AC) | true;
if (SwitchToLookupTable(SI, Builder, TTI, DL))
- return SimplifyCFG(BB, TTI, DL) | true;
+ return SimplifyCFG(BB, TTI, BonusInstThreshold, DL, AC) | true;
return false;
}
SmallPtrSet<Value *, 8> Succs;
for (unsigned i = 0, e = IBI->getNumDestinations(); i != e; ++i) {
BasicBlock *Dest = IBI->getDestination(i);
- if (!Dest->hasAddressTaken() || !Succs.insert(Dest)) {
+ if (!Dest->hasAddressTaken() || !Succs.insert(Dest).second) {
Dest->removePredecessor(BB);
IBI->removeDestination(i);
--i; --e;
if (SelectInst *SI = dyn_cast<SelectInst>(IBI->getAddress())) {
if (SimplifyIndirectBrOnSelect(IBI, SI))
- return SimplifyCFG(BB, TTI, DL) | true;
+ return SimplifyCFG(BB, TTI, BonusInstThreshold, DL, AC) | true;
}
return Changed;
}
@@ -3911,7 +4399,7 @@ bool SimplifyCFGOpt::SimplifyUncondBranch(BranchInst *BI, IRBuilder<> &Builder){
return true;
// If the Terminator is the only non-phi instruction, simplify the block.
- BasicBlock::iterator I = BB->getFirstNonPHIOrDbgOrLifetime();
+ BasicBlock::iterator I = BB->getFirstNonPHIOrDbg();
if (I->isTerminator() && BB != &BB->getParent()->getEntryBlock() &&
TryToSimplifyUncondBranchFromEmptyBlock(BB))
return true;
@@ -3923,7 +4411,8 @@ bool SimplifyCFGOpt::SimplifyUncondBranch(BranchInst *BI, IRBuilder<> &Builder){
for (++I; isa<DbgInfoIntrinsic>(I); ++I)
;
if (I->isTerminator() &&
- TryToSimplifyUncondBranchWithICmpInIt(ICI, Builder, TTI, DL))
+ TryToSimplifyUncondBranchWithICmpInIt(ICI, Builder, TTI,
+ BonusInstThreshold, DL, AC))
return true;
}
@@ -3931,8 +4420,8 @@ bool SimplifyCFGOpt::SimplifyUncondBranch(BranchInst *BI, IRBuilder<> &Builder){
// branches to us and our successor, fold the comparison into the
// predecessor and use logical operations to update the incoming value
// for PHI nodes in common successor.
- if (FoldBranchToCommonDest(BI))
- return SimplifyCFG(BB, TTI, DL) | true;
+ if (FoldBranchToCommonDest(BI, DL, BonusInstThreshold))
+ return SimplifyCFG(BB, TTI, BonusInstThreshold, DL, AC) | true;
return false;
}
@@ -3947,7 +4436,7 @@ bool SimplifyCFGOpt::SimplifyCondBranch(BranchInst *BI, IRBuilder<> &Builder) {
// switch.
if (BasicBlock *OnlyPred = BB->getSinglePredecessor())
if (SimplifyEqualityComparisonWithOnlyPredecessor(BI, OnlyPred, Builder))
- return SimplifyCFG(BB, TTI, DL) | true;
+ return SimplifyCFG(BB, TTI, BonusInstThreshold, DL, AC) | true;
// This block must be empty, except for the setcond inst, if it exists.
// Ignore dbg intrinsics.
@@ -3957,14 +4446,14 @@ bool SimplifyCFGOpt::SimplifyCondBranch(BranchInst *BI, IRBuilder<> &Builder) {
++I;
if (&*I == BI) {
if (FoldValueComparisonIntoPredecessors(BI, Builder))
- return SimplifyCFG(BB, TTI, DL) | true;
+ return SimplifyCFG(BB, TTI, BonusInstThreshold, DL, AC) | true;
} else if (&*I == cast<Instruction>(BI->getCondition())){
++I;
// Ignore dbg intrinsics.
while (isa<DbgInfoIntrinsic>(I))
++I;
if (&*I == BI && FoldValueComparisonIntoPredecessors(BI, Builder))
- return SimplifyCFG(BB, TTI, DL) | true;
+ return SimplifyCFG(BB, TTI, BonusInstThreshold, DL, AC) | true;
}
}
@@ -3975,34 +4464,34 @@ bool SimplifyCFGOpt::SimplifyCondBranch(BranchInst *BI, IRBuilder<> &Builder) {
// If this basic block is ONLY a compare and a branch, and if a predecessor
// branches to us and one of our successors, fold the comparison into the
// predecessor and use logical operations to pick the right destination.
- if (FoldBranchToCommonDest(BI))
- return SimplifyCFG(BB, TTI, DL) | true;
+ if (FoldBranchToCommonDest(BI, DL, BonusInstThreshold))
+ return SimplifyCFG(BB, TTI, BonusInstThreshold, DL, AC) | true;
// We have a conditional branch to two blocks that are only reachable
// from BI. We know that the condbr dominates the two blocks, so see if
// there is any identical code in the "then" and "else" blocks. If so, we
// can hoist it up to the branching block.
- if (BI->getSuccessor(0)->getSinglePredecessor() != 0) {
- if (BI->getSuccessor(1)->getSinglePredecessor() != 0) {
- if (HoistThenElseCodeToIf(BI))
- return SimplifyCFG(BB, TTI, DL) | true;
+ if (BI->getSuccessor(0)->getSinglePredecessor()) {
+ if (BI->getSuccessor(1)->getSinglePredecessor()) {
+ if (HoistThenElseCodeToIf(BI, DL))
+ return SimplifyCFG(BB, TTI, BonusInstThreshold, DL, AC) | true;
} else {
// If Successor #1 has multiple preds, we may be able to conditionally
- // execute Successor #0 if it branches to successor #1.
+ // execute Successor #0 if it branches to Successor #1.
TerminatorInst *Succ0TI = BI->getSuccessor(0)->getTerminator();
if (Succ0TI->getNumSuccessors() == 1 &&
Succ0TI->getSuccessor(0) == BI->getSuccessor(1))
- if (SpeculativelyExecuteBB(BI, BI->getSuccessor(0)))
- return SimplifyCFG(BB, TTI, DL) | true;
+ if (SpeculativelyExecuteBB(BI, BI->getSuccessor(0), DL))
+ return SimplifyCFG(BB, TTI, BonusInstThreshold, DL, AC) | true;
}
- } else if (BI->getSuccessor(1)->getSinglePredecessor() != 0) {
+ } else if (BI->getSuccessor(1)->getSinglePredecessor()) {
// If Successor #0 has multiple preds, we may be able to conditionally
- // execute Successor #1 if it branches to successor #0.
+ // execute Successor #1 if it branches to Successor #0.
TerminatorInst *Succ1TI = BI->getSuccessor(1)->getTerminator();
if (Succ1TI->getNumSuccessors() == 1 &&
Succ1TI->getSuccessor(0) == BI->getSuccessor(0))
- if (SpeculativelyExecuteBB(BI, BI->getSuccessor(1)))
- return SimplifyCFG(BB, TTI, DL) | true;
+ if (SpeculativelyExecuteBB(BI, BI->getSuccessor(1), DL))
+ return SimplifyCFG(BB, TTI, BonusInstThreshold, DL, AC) | true;
}
// If this is a branch on a phi node in the current block, thread control
@@ -4010,14 +4499,14 @@ bool SimplifyCFGOpt::SimplifyCondBranch(BranchInst *BI, IRBuilder<> &Builder) {
if (PHINode *PN = dyn_cast<PHINode>(BI->getCondition()))
if (PN->getParent() == BI->getParent())
if (FoldCondBranchOnPHI(BI, DL))
- return SimplifyCFG(BB, TTI, DL) | true;
+ return SimplifyCFG(BB, TTI, BonusInstThreshold, DL, AC) | true;
// Scan predecessor blocks for conditional branches.
for (pred_iterator PI = pred_begin(BB), E = pred_end(BB); PI != E; ++PI)
if (BranchInst *PBI = dyn_cast<BranchInst>((*PI)->getTerminator()))
if (PBI != BI && PBI->isConditional())
if (SimplifyCondBranchToCondBranch(PBI, BI))
- return SimplifyCFG(BB, TTI, DL) | true;
+ return SimplifyCFG(BB, TTI, BonusInstThreshold, DL, AC) | true;
return false;
}
// Remove basic blocks that have no predecessors (except the entry block)...
// or that just have themself as a predecessor. These are unreachable.
- if ((pred_begin(BB) == pred_end(BB) &&
+ if ((pred_empty(BB) &&
BB != &BB->getParent()->getEntryBlock()) ||
BB->getSinglePredecessor() == BB) {
DEBUG(dbgs() << "Removing BB: \n" << *BB);
/// of the CFG. It returns true if a modification was made.
///
bool llvm::SimplifyCFG(BasicBlock *BB, const TargetTransformInfo &TTI,
- const DataLayout *DL) {
- return SimplifyCFGOpt(TTI, DL).run(BB);
+ unsigned BonusInstThreshold, const DataLayout *DL,
+ AssumptionCache *AC) {
+ return SimplifyCFGOpt(TTI, BonusInstThreshold, DL, AC).run(BB);
}