index c4b45ed147363aa443899440d547cc9211a34f9a..f6867c24ee58da885da49e31e74a0017e5275728 100644 (file)
const TargetTransformInfo &TTI;
unsigned BonusInstThreshold;
const DataLayout *const DL;
- AssumptionTracker *AT;
+ AssumptionCache *AC;
Value *isValueEqualityComparison(TerminatorInst *TI);
BasicBlock *GetValueEqualityComparisonCases(TerminatorInst *TI,
std::vector<ValueEqualityComparisonCase> &Cases);
public:
SimplifyCFGOpt(const TargetTransformInfo &TTI, unsigned BonusInstThreshold,
- const DataLayout *DL, AssumptionTracker *AT)
- : TTI(TTI), BonusInstThreshold(BonusInstThreshold), DL(DL), AT(AT) {}
+ const DataLayout *DL, AssumptionCache *AC)
+ : TTI(TTI), BonusInstThreshold(BonusInstThreshold), DL(DL), AC(AC) {}
bool run(BasicBlock *BB);
};
}
if (HasWeight)
for (unsigned MD_i = 1, MD_e = MD->getNumOperands(); MD_i < MD_e;
++MD_i) {
- ConstantInt* CI = dyn_cast<ConstantInt>(MD->getOperand(MD_i));
- assert(CI);
+ ConstantInt *CI = mdconst::extract<ConstantInt>(MD->getOperand(MD_i));
Weights.push_back(CI->getValue().getZExtValue());
}
for (SwitchInst::CaseIt i = SI->case_end(), e = SI->case_begin(); i != e;) {
MDNode *MD = TI->getMetadata(LLVMContext::MD_prof);
assert(MD);
for (unsigned i = 1, e = MD->getNumOperands(); i < e; ++i) {
- ConstantInt *CI = cast<ConstantInt>(MD->getOperand(i));
+ ConstantInt *CI = mdconst::extract<ConstantInt>(MD->getOperand(i));
Weights.push_back(CI->getValue().getZExtValue());
}
return false;
// Gather the PHI nodes in BBEnd.
- std::map<Value*, std::pair<Value*, PHINode*> > MapValueFromBB1ToBB2;
+ SmallDenseMap<std::pair<Value *, Value *>, PHINode *> JointValueMap;
Instruction *FirstNonPhiInBBEnd = nullptr;
- for (BasicBlock::iterator I = BBEnd->begin(), E = BBEnd->end();
- I != E; ++I) {
+ for (BasicBlock::iterator I = BBEnd->begin(), E = BBEnd->end(); I != E; ++I) {
if (PHINode *PN = dyn_cast<PHINode>(I)) {
Value *BB1V = PN->getIncomingValueForBlock(BB1);
Value *BB2V = PN->getIncomingValueForBlock(BB2);
- MapValueFromBB1ToBB2[BB1V] = std::make_pair(BB2V, PN);
+ JointValueMap[std::make_pair(BB1V, BB2V)] = PN;
} else {
FirstNonPhiInBBEnd = &*I;
break;
if (!FirstNonPhiInBBEnd)
return false;
-
// This does very trivial matching, with limited scanning, to find identical
// instructions in the two blocks. We scan backward for obviously identical
// instructions in an identical order.
BasicBlock::InstListType::reverse_iterator RI1 = BB1->getInstList().rbegin(),
- RE1 = BB1->getInstList().rend(), RI2 = BB2->getInstList().rbegin(),
- RE2 = BB2->getInstList().rend();
+ RE1 = BB1->getInstList().rend(),
+ RI2 = BB2->getInstList().rbegin(),
+ RE2 = BB2->getInstList().rend();
// Skip debug info.
while (RI1 != RE1 && isa<DbgInfoIntrinsic>(&*RI1)) ++RI1;
if (RI1 == RE1)
return Changed;
Instruction *I1 = &*RI1, *I2 = &*RI2;
+ auto InstPair = std::make_pair(I1, I2);
// I1 and I2 should have a single use in the same PHI node, and they
// perform the same operation.
// Cannot move control-flow-involving, volatile loads, vaarg, etc.
I1->mayHaveSideEffects() || I2->mayHaveSideEffects() ||
I1->mayReadOrWriteMemory() || I2->mayReadOrWriteMemory() ||
!I1->hasOneUse() || !I2->hasOneUse() ||
- MapValueFromBB1ToBB2.find(I1) == MapValueFromBB1ToBB2.end() ||
- MapValueFromBB1ToBB2[I1].first != I2)
+ !JointValueMap.count(InstPair))
return Changed;
// Check whether we should swap the operands of ICmpInst.
+ // TODO: Add support of communativity.
ICmpInst *ICmp1 = dyn_cast<ICmpInst>(I1), *ICmp2 = dyn_cast<ICmpInst>(I2);
bool SwapOpnds = false;
if (ICmp1 && ICmp2 &&
// with a PHI node after sinking. We only handle the case where there is
// a single pair of different operands.
Value *DifferentOp1 = nullptr, *DifferentOp2 = nullptr;
- unsigned Op1Idx = 0;
+ unsigned Op1Idx = ~0U;
for (unsigned I = 0, E = I1->getNumOperands(); I != E; ++I) {
if (I1->getOperand(I) == I2->getOperand(I))
continue;
- // Early exit if we have more-than one pair of different operands or
- // the different operand is already in MapValueFromBB1ToBB2.
- // Early exit if we need a PHI node to replace a constant.
- if (DifferentOp1 ||
- MapValueFromBB1ToBB2.find(I1->getOperand(I)) !=
- MapValueFromBB1ToBB2.end() ||
+ // Early exit if we have more-than one pair of different operands or if
+ // we need a PHI node to replace a constant.
+ if (Op1Idx != ~0U ||
isa<Constant>(I1->getOperand(I)) ||
isa<Constant>(I2->getOperand(I))) {
// If we can't sink the instructions, undo the swapping.
DifferentOp2 = I2->getOperand(I);
}
- // We insert the pair of different operands to MapValueFromBB1ToBB2 and
- // remove (I1, I2) from MapValueFromBB1ToBB2.
- if (DifferentOp1) {
- PHINode *NewPN = PHINode::Create(DifferentOp1->getType(), 2,
- DifferentOp1->getName() + ".sink",
- BBEnd->begin());
- MapValueFromBB1ToBB2[DifferentOp1] = std::make_pair(DifferentOp2, NewPN);
+ DEBUG(dbgs() << "SINK common instructions " << *I1 << "\n");
+ DEBUG(dbgs() << " " << *I2 << "\n");
+
+ // We insert the pair of different operands to JointValueMap and
+ // remove (I1, I2) from JointValueMap.
+ if (Op1Idx != ~0U) {
+ auto &NewPN = JointValueMap[std::make_pair(DifferentOp1, DifferentOp2)];
+ if (!NewPN) {
+ NewPN =
+ PHINode::Create(DifferentOp1->getType(), 2,
+ DifferentOp1->getName() + ".sink", BBEnd->begin());
+ NewPN->addIncoming(DifferentOp1, BB1);
+ NewPN->addIncoming(DifferentOp2, BB2);
+ DEBUG(dbgs() << "Create PHI node " << *NewPN << "\n";);
+ }
// I1 should use NewPN instead of DifferentOp1.
I1->setOperand(Op1Idx, NewPN);
- NewPN->addIncoming(DifferentOp1, BB1);
- NewPN->addIncoming(DifferentOp2, BB2);
- DEBUG(dbgs() << "Create PHI node " << *NewPN << "\n";);
}
- PHINode *OldPN = MapValueFromBB1ToBB2[I1].second;
- MapValueFromBB1ToBB2.erase(I1);
+ PHINode *OldPN = JointValueMap[InstPair];
+ JointValueMap.erase(InstPair);
- DEBUG(dbgs() << "SINK common instructions " << *I1 << "\n";);
- DEBUG(dbgs() << " " << *I2 << "\n";);
// We need to update RE1 and RE2 if we are going to sink the first
// instruction in the basic block down.
bool UpdateRE1 = (I1 == BB1->begin()), UpdateRE2 = (I2 == BB2->begin());
"Looking for probabilities on unconditional branch?");
MDNode *ProfileData = BI->getMetadata(LLVMContext::MD_prof);
if (!ProfileData || ProfileData->getNumOperands() != 3) return false;
- ConstantInt *CITrue = dyn_cast<ConstantInt>(ProfileData->getOperand(1));
- ConstantInt *CIFalse = dyn_cast<ConstantInt>(ProfileData->getOperand(2));
+ ConstantInt *CITrue =
+ mdconst::dyn_extract<ConstantInt>(ProfileData->getOperand(1));
+ ConstantInt *CIFalse =
+ mdconst::dyn_extract<ConstantInt>(ProfileData->getOperand(2));
if (!CITrue || !CIFalse) return false;
ProbTrue = CITrue->getValue().getZExtValue();
ProbFalse = CIFalse->getValue().getZExtValue();
/// the PHI, merging the third icmp into the switch.
static bool TryToSimplifyUncondBranchWithICmpInIt(
ICmpInst *ICI, IRBuilder<> &Builder, const TargetTransformInfo &TTI,
- unsigned BonusInstThreshold, const DataLayout *DL, AssumptionTracker *AT) {
+ unsigned BonusInstThreshold, const DataLayout *DL, AssumptionCache *AC) {
BasicBlock *BB = ICI->getParent();
// If the block has any PHIs in it or the icmp has multiple uses, it is too
ICI->eraseFromParent();
}
// BB is now empty, so it is likely to simplify away.
- return SimplifyCFG(BB, TTI, BonusInstThreshold, DL, AT) | true;
+ return SimplifyCFG(BB, TTI, BonusInstThreshold, DL, AC) | true;
}
// Ok, the block is reachable from the default dest. If the constant we're
ICI->replaceAllUsesWith(V);
ICI->eraseFromParent();
// BB is now empty, so it is likely to simplify away.
- return SimplifyCFG(BB, TTI, BonusInstThreshold, DL, AT) | true;
+ return SimplifyCFG(BB, TTI, BonusInstThreshold, DL, AC) | true;
}
// The use of the icmp has to be in the 'end' block, by the only PHI node in
}
// If we eliminated all predecessors of the block, delete the block now.
- if (pred_begin(BB) == pred_end(BB))
+ if (pred_empty(BB))
// We know there are no successors, so just nuke the block.
BB->eraseFromParent();
}
// If this block is now dead, remove it.
- if (pred_begin(BB) == pred_end(BB) &&
+ if (pred_empty(BB) &&
BB != &BB->getParent()->getEntryBlock()) {
// We know there are no successors, so just nuke the block.
BB->eraseFromParent();
/// EliminateDeadSwitchCases - Compute masked bits for the condition of a switch
/// and use it to remove dead cases.
static bool EliminateDeadSwitchCases(SwitchInst *SI, const DataLayout *DL,
- AssumptionTracker *AT) {
+ AssumptionCache *AC) {
Value *Cond = SI->getCondition();
unsigned Bits = Cond->getType()->getIntegerBitWidth();
APInt KnownZero(Bits, 0), KnownOne(Bits, 0);
- computeKnownBits(Cond, KnownZero, KnownOne, DL, 0, AT, SI);
+ computeKnownBits(Cond, KnownZero, KnownOne, DL, 0, AC, SI);
// Gather dead cases.
SmallVector<ConstantInt*, 8> DeadCases;
continue;
} else if (Constant *C = ConstantFold(I, ConstantPool, DL)) {
// Instruction is side-effect free and constant.
+
+ // If the instruction has uses outside this block or a phi node slot for
+ // the block, it is not safe to bypass the instruction since it would then
+ // no longer dominate all its uses.
+ for (auto &Use : I->uses()) {
+ User *User = Use.getUser();
+ if (Instruction *I = dyn_cast<Instruction>(User))
+ if (I->getParent() == CaseDest)
+ continue;
+ if (PHINode *Phi = dyn_cast<PHINode>(User))
+ if (Phi->getIncomingBlock(Use) == CaseDest)
+ continue;
+ return false;
+ }
+
ConstantPool.insert(std::make_pair(I, C));
} else {
break;
if (!ConstVal)
return false;
- // Note: If the constant comes from constant-propagating the case value
- // through the CaseDest basic block, it will be safe to remove the
- // instructions in that block. They cannot be used (except in the phi nodes
- // we visit) outside CaseDest, because that block does not dominate its
- // successor. If it did, we would not be in this phi node.
-
// Be conservative about which kinds of constants we support.
if (!ValidLookupTableConstant(ConstVal))
return false;
/// phi nodes in a common successor block with only two different
/// constant values, replace the switch with select.
static bool SwitchToSelect(SwitchInst *SI, IRBuilder<> &Builder,
- const DataLayout *DL, AssumptionTracker *AT) {
+ const DataLayout *DL, AssumptionCache *AC) {
Value *const Cond = SI->getCondition();
PHINode *PHI = nullptr;
BasicBlock *CommonDest = nullptr;
assert((CaseConst == TrueConst || CaseConst == FalseConst) &&
"Expect true or false as compare result.");
}
+
+ // Check if the branch instruction dominates the phi node. It's a simple
+ // dominance check, but sufficient for our needs.
+ // Although this check is invariant in the calling loops, it's better to do it
+ // at this late stage. Practically we do it at most once for a switch.
+ BasicBlock *BranchBlock = RangeCheckBranch->getParent();
+ for (auto PI = pred_begin(PhiBlock), E = pred_end(PhiBlock); PI != E; ++PI) {
+ BasicBlock *Pred = *PI;
+ if (Pred != BranchBlock && Pred->getUniquePredecessor() != BranchBlock)
+ return;
+ }
if (DefaultConst == FalseConst) {
// The compare yields the same result. We can replace it.
// see if that predecessor totally determines the outcome of this switch.
if (BasicBlock *OnlyPred = BB->getSinglePredecessor())
if (SimplifyEqualityComparisonWithOnlyPredecessor(SI, OnlyPred, Builder))
- return SimplifyCFG(BB, TTI, BonusInstThreshold, DL, AT) | true;
+ return SimplifyCFG(BB, TTI, BonusInstThreshold, DL, AC) | true;
Value *Cond = SI->getCondition();
if (SelectInst *Select = dyn_cast<SelectInst>(Cond))
if (SimplifySwitchOnSelect(SI, Select))
- return SimplifyCFG(BB, TTI, BonusInstThreshold, DL, AT) | true;
+ return SimplifyCFG(BB, TTI, BonusInstThreshold, DL, AC) | true;
// If the block only contains the switch, see if we can fold the block
// away into any preds.
++BBI;
if (SI == &*BBI)
if (FoldValueComparisonIntoPredecessors(SI, Builder))
- return SimplifyCFG(BB, TTI, BonusInstThreshold, DL, AT) | true;
+ return SimplifyCFG(BB, TTI, BonusInstThreshold, DL, AC) | true;
}
// Try to transform the switch into an icmp and a branch.
if (TurnSwitchRangeIntoICmp(SI, Builder))
- return SimplifyCFG(BB, TTI, BonusInstThreshold, DL, AT) | true;
+ return SimplifyCFG(BB, TTI, BonusInstThreshold, DL, AC) | true;
// Remove unreachable cases.
- if (EliminateDeadSwitchCases(SI, DL, AT))
- return SimplifyCFG(BB, TTI, BonusInstThreshold, DL, AT) | true;
+ if (EliminateDeadSwitchCases(SI, DL, AC))
+ return SimplifyCFG(BB, TTI, BonusInstThreshold, DL, AC) | true;
- if (SwitchToSelect(SI, Builder, DL, AT))
- return SimplifyCFG(BB, TTI, BonusInstThreshold, DL, AT) | true;
+ if (SwitchToSelect(SI, Builder, DL, AC))
+ return SimplifyCFG(BB, TTI, BonusInstThreshold, DL, AC) | true;
if (ForwardSwitchConditionToPHI(SI))
- return SimplifyCFG(BB, TTI, BonusInstThreshold, DL, AT) | true;
+ return SimplifyCFG(BB, TTI, BonusInstThreshold, DL, AC) | true;
if (SwitchToLookupTable(SI, Builder, TTI, DL))
- return SimplifyCFG(BB, TTI, BonusInstThreshold, DL, AT) | true;
+ return SimplifyCFG(BB, TTI, BonusInstThreshold, DL, AC) | true;
return false;
}
if (SelectInst *SI = dyn_cast<SelectInst>(IBI->getAddress())) {
if (SimplifyIndirectBrOnSelect(IBI, SI))
- return SimplifyCFG(BB, TTI, BonusInstThreshold, DL, AT) | true;
+ return SimplifyCFG(BB, TTI, BonusInstThreshold, DL, AC) | true;
}
return Changed;
}
@@ -4391,7 +4412,7 @@ bool SimplifyCFGOpt::SimplifyUncondBranch(BranchInst *BI, IRBuilder<> &Builder){
;
if (I->isTerminator() &&
TryToSimplifyUncondBranchWithICmpInIt(ICI, Builder, TTI,
- BonusInstThreshold, DL, AT))
+ BonusInstThreshold, DL, AC))
return true;
}
@@ -4400,7 +4421,7 @@ bool SimplifyCFGOpt::SimplifyUncondBranch(BranchInst *BI, IRBuilder<> &Builder){
// predecessor and use logical operations to update the incoming value
// for PHI nodes in common successor.
if (FoldBranchToCommonDest(BI, DL, BonusInstThreshold))
- return SimplifyCFG(BB, TTI, BonusInstThreshold, DL, AT) | true;
+ return SimplifyCFG(BB, TTI, BonusInstThreshold, DL, AC) | true;
return false;
}
@@ -4415,7 +4436,7 @@ bool SimplifyCFGOpt::SimplifyCondBranch(BranchInst *BI, IRBuilder<> &Builder) {
// switch.
if (BasicBlock *OnlyPred = BB->getSinglePredecessor())
if (SimplifyEqualityComparisonWithOnlyPredecessor(BI, OnlyPred, Builder))
- return SimplifyCFG(BB, TTI, BonusInstThreshold, DL, AT) | true;
+ return SimplifyCFG(BB, TTI, BonusInstThreshold, DL, AC) | true;
// This block must be empty, except for the setcond inst, if it exists.
// Ignore dbg intrinsics.
@@ -4425,14 +4446,14 @@ bool SimplifyCFGOpt::SimplifyCondBranch(BranchInst *BI, IRBuilder<> &Builder) {
++I;
if (&*I == BI) {
if (FoldValueComparisonIntoPredecessors(BI, Builder))
- return SimplifyCFG(BB, TTI, BonusInstThreshold, DL, AT) | true;
+ return SimplifyCFG(BB, TTI, BonusInstThreshold, DL, AC) | true;
} else if (&*I == cast<Instruction>(BI->getCondition())){
++I;
// Ignore dbg intrinsics.
while (isa<DbgInfoIntrinsic>(I))
++I;
if (&*I == BI && FoldValueComparisonIntoPredecessors(BI, Builder))
- return SimplifyCFG(BB, TTI, BonusInstThreshold, DL, AT) | true;
+ return SimplifyCFG(BB, TTI, BonusInstThreshold, DL, AC) | true;
}
}
@@ -4444,7 +4465,7 @@ bool SimplifyCFGOpt::SimplifyCondBranch(BranchInst *BI, IRBuilder<> &Builder) {
// branches to us and one of our successors, fold the comparison into the
// predecessor and use logical operations to pick the right destination.
if (FoldBranchToCommonDest(BI, DL, BonusInstThreshold))
- return SimplifyCFG(BB, TTI, BonusInstThreshold, DL, AT) | true;
+ return SimplifyCFG(BB, TTI, BonusInstThreshold, DL, AC) | true;
// We have a conditional branch to two blocks that are only reachable
// from BI. We know that the condbr dominates the two blocks, so see if
@@ -4453,7 +4474,7 @@ bool SimplifyCFGOpt::SimplifyCondBranch(BranchInst *BI, IRBuilder<> &Builder) {
if (BI->getSuccessor(0)->getSinglePredecessor()) {
if (BI->getSuccessor(1)->getSinglePredecessor()) {
if (HoistThenElseCodeToIf(BI, DL))
- return SimplifyCFG(BB, TTI, BonusInstThreshold, DL, AT) | true;
+ return SimplifyCFG(BB, TTI, BonusInstThreshold, DL, AC) | true;
} else {
// If Successor #1 has multiple preds, we may be able to conditionally
// execute Successor #0 if it branches to Successor #1.
@@ -4461,7 +4482,7 @@ bool SimplifyCFGOpt::SimplifyCondBranch(BranchInst *BI, IRBuilder<> &Builder) {
if (Succ0TI->getNumSuccessors() == 1 &&
Succ0TI->getSuccessor(0) == BI->getSuccessor(1))
if (SpeculativelyExecuteBB(BI, BI->getSuccessor(0), DL))
- return SimplifyCFG(BB, TTI, BonusInstThreshold, DL, AT) | true;
+ return SimplifyCFG(BB, TTI, BonusInstThreshold, DL, AC) | true;
}
} else if (BI->getSuccessor(1)->getSinglePredecessor()) {
// If Successor #0 has multiple preds, we may be able to conditionally
@@ -4470,7 +4491,7 @@ bool SimplifyCFGOpt::SimplifyCondBranch(BranchInst *BI, IRBuilder<> &Builder) {
if (Succ1TI->getNumSuccessors() == 1 &&
Succ1TI->getSuccessor(0) == BI->getSuccessor(0))
if (SpeculativelyExecuteBB(BI, BI->getSuccessor(1), DL))
- return SimplifyCFG(BB, TTI, BonusInstThreshold, DL, AT) | true;
+ return SimplifyCFG(BB, TTI, BonusInstThreshold, DL, AC) | true;
}
// If this is a branch on a phi node in the current block, thread control
@@ -4478,14 +4499,14 @@ bool SimplifyCFGOpt::SimplifyCondBranch(BranchInst *BI, IRBuilder<> &Builder) {
if (PHINode *PN = dyn_cast<PHINode>(BI->getCondition()))
if (PN->getParent() == BI->getParent())
if (FoldCondBranchOnPHI(BI, DL))
- return SimplifyCFG(BB, TTI, BonusInstThreshold, DL, AT) | true;
+ return SimplifyCFG(BB, TTI, BonusInstThreshold, DL, AC) | true;
// Scan predecessor blocks for conditional branches.
for (pred_iterator PI = pred_begin(BB), E = pred_end(BB); PI != E; ++PI)
if (BranchInst *PBI = dyn_cast<BranchInst>((*PI)->getTerminator()))
if (PBI != BI && PBI->isConditional())
if (SimplifyCondBranchToCondBranch(PBI, BI))
- return SimplifyCFG(BB, TTI, BonusInstThreshold, DL, AT) | true;
+ return SimplifyCFG(BB, TTI, BonusInstThreshold, DL, AC) | true;
return false;
}
// Remove basic blocks that have no predecessors (except the entry block)...
// or that just have themself as a predecessor. These are unreachable.
- if ((pred_begin(BB) == pred_end(BB) &&
+ if ((pred_empty(BB) &&
BB != &BB->getParent()->getEntryBlock()) ||
BB->getSinglePredecessor() == BB) {
DEBUG(dbgs() << "Removing BB: \n" << *BB);
/// of the CFG. It returns true if a modification was made.
///
bool llvm::SimplifyCFG(BasicBlock *BB, const TargetTransformInfo &TTI,
- unsigned BonusInstThreshold,
- const DataLayout *DL, AssumptionTracker *AT) {
- return SimplifyCFGOpt(TTI, BonusInstThreshold, DL, AT).run(BB);
+ unsigned BonusInstThreshold, const DataLayout *DL,
+ AssumptionCache *AC) {
+ return SimplifyCFGOpt(TTI, BonusInstThreshold, DL, AC).run(BB);
}