]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/blobdiff - test/Transforms/InstCombine/load.ll
[canonicalize] Teach InstCombine to canonicalize loads which are only
[opencl/llvm.git] / test / Transforms / InstCombine / load.ll
index f085346597bab92e4a7669a5bf812f59defaa9bd..700797ab22cf6da9dfebef535e406ace8d785fb7 100644 (file)
+; RUN: opt -instcombine -S < %s | FileCheck %s
+
 ; This test makes sure that these instructions are properly eliminated.
-;
 
-; RUN: as < %s | opt -instcombine | dis | not grep load
+target datalayout = "e-m:e-p:64:64:64-i64:64-f80:128-n8:16:32:64-S128"
+
+@X = constant i32 42           ; <i32*> [#uses=2]
+@X2 = constant i32 47          ; <i32*> [#uses=1]
+@Y = constant [2 x { i32, float }] [ { i32, float } { i32 12, float 1.000000e+00 }, { i32, float } { i32 37, float 0x3FF3B2FEC0000000 } ]              ; <[2 x { i32, float }]*> [#uses=2]
+@Z = constant [2 x { i32, float }] zeroinitializer             ; <[2 x { i32, float }]*> [#uses=1]
+
+@GLOBAL = internal constant [4 x i32] zeroinitializer
+
 
-%X = constant int 42
-%Y = constant [2 x { int, float }] [ { int, float } { int 12, float 1.0 }, 
-                                     { int, float } { int 37, float 1.2312 } ]
-int %test1() {
-       %B = load int* %X
-       ret int %B
+; CHECK-LABEL: @test1(
+; CHECK-NOT: load
+define i32 @test1() {
+       %B = load i32* @X               ; <i32> [#uses=1]
+       ret i32 %B
 }
 
-float %test2() {
-       %A = getelementptr [2 x { int, float}]* %Y, long 0, long 1, ubyte 1
-       %B = load float* %A
+; CHECK-LABEL: @test2(
+; CHECK-NOT: load
+define float @test2() {
+       %A = getelementptr [2 x { i32, float }]* @Y, i64 0, i64 1, i32 1                ; <float*> [#uses=1]
+       %B = load float* %A             ; <float> [#uses=1]
        ret float %B
 }
 
-int %test3() {
-       %A = getelementptr [2 x { int, float}]* %Y, long 0, long 0, ubyte 0
-       %B = load int* %A
-       ret int %B
+; CHECK-LABEL: @test3(
+; CHECK-NOT: load
+define i32 @test3() {
+       %A = getelementptr [2 x { i32, float }]* @Y, i64 0, i64 0, i32 0                ; <i32*> [#uses=1]
+       %B = load i32* %A               ; <i32> [#uses=1]
+       ret i32 %B
 }
 
+; CHECK-LABEL: @test4(
+; CHECK-NOT: load
+define i32 @test4() {
+       %A = getelementptr [2 x { i32, float }]* @Z, i64 0, i64 1, i32 0                ; <i32*> [#uses=1]
+       %B = load i32* %A               ; <i32> [#uses=1]
+       ret i32 %B
+}
+
+; CHECK-LABEL: @test5(
+; CHECK-NOT: load
+define i32 @test5(i1 %C) {
+       %Y = select i1 %C, i32* @X, i32* @X2            ; <i32*> [#uses=1]
+       %Z = load i32* %Y               ; <i32> [#uses=1]
+       ret i32 %Z
+}
+
+; CHECK-LABEL: @test7(
+; CHECK-NOT: load
+define i32 @test7(i32 %X) {
+       %V = getelementptr i32* null, i32 %X            ; <i32*> [#uses=1]
+       %R = load i32* %V               ; <i32> [#uses=1]
+       ret i32 %R
+}
 
+; CHECK-LABEL: @test8(
+; CHECK-NOT: load
+define i32 @test8(i32* %P) {
+       store i32 1, i32* %P
+       %X = load i32* %P               ; <i32> [#uses=1]
+       ret i32 %X
+}
+
+; CHECK-LABEL: @test9(
+; CHECK-NOT: load
+define i32 @test9(i32* %P) {
+       %X = load i32* %P               ; <i32> [#uses=1]
+       %Y = load i32* %P               ; <i32> [#uses=1]
+       %Z = sub i32 %X, %Y             ; <i32> [#uses=1]
+       ret i32 %Z
+}
+
+; CHECK-LABEL: @test10(
+; CHECK-NOT: load
+define i32 @test10(i1 %C.upgrd.1, i32* %P, i32* %Q) {
+       br i1 %C.upgrd.1, label %T, label %F
+T:             ; preds = %0
+       store i32 1, i32* %Q
+       store i32 0, i32* %P
+       br label %C
+F:             ; preds = %0
+       store i32 0, i32* %P
+       br label %C
+C:             ; preds = %F, %T
+       %V = load i32* %P               ; <i32> [#uses=1]
+       ret i32 %V
+}
+
+; CHECK-LABEL: @test11(
+; CHECK-NOT: load
+define double @test11(double* %p) {
+  %t0 = getelementptr double* %p, i32 1
+  store double 2.0, double* %t0
+  %t1 = getelementptr double* %p, i32 1
+  %x = load double* %t1
+  ret double %x
+}
+
+; CHECK-LABEL: @test12(
+; CHECK-NOT: load
+define i32 @test12(i32* %P) {
+  %A = alloca i32
+  store i32 123, i32* %A
+  ; Cast the result of the load not the source
+  %Q = bitcast i32* %A to i32*
+  %V = load i32* %Q
+  ret i32 %V
+}
+
+; CHECK-LABEL: @test13(
+; CHECK-NOT: load
+define <16 x i8> @test13(<2 x i64> %x) {
+  %tmp = load <16 x i8>* bitcast ([4 x i32]* @GLOBAL to <16 x i8>*)
+  ret <16 x i8> %tmp
+}
+
+define i8 @test14(i8 %x, i32 %y) {
+; This test must not have the store of %x forwarded to the load -- there is an
+; intervening store if %y. However, the intervening store occurs with a different
+; type and size and to a different pointer value. This is ensuring that none of
+; those confuse the analysis into thinking that the second store does not alias
+; the first.
+; CHECK-LABEL: @test14(
+; CHECK:         %[[R:.*]] = load i8*
+; CHECK-NEXT:    ret i8 %[[R]]
+  %a = alloca i32
+  %a.i8 = bitcast i32* %a to i8*
+  store i8 %x, i8* %a.i8
+  store i32 %y, i32* %a
+  %r = load i8* %a.i8
+  ret i8 %r
+}
+
+@test15_global = external global i32
+
+define i8 @test15(i8 %x, i32 %y) {
+; Same test as @test14 essentially, but using a global instead of an alloca.
+; CHECK-LABEL: @test15(
+; CHECK:         %[[R:.*]] = load i8*
+; CHECK-NEXT:    ret i8 %[[R]]
+  %g.i8 = bitcast i32* @test15_global to i8*
+  store i8 %x, i8* %g.i8
+  store i32 %y, i32* @test15_global
+  %r = load i8* %g.i8
+  ret i8 %r
+}
+
+define void @test16(i8* %x, i8* %a, i8* %b, i8* %c) {
+; Check that we canonicalize loads which are only stored to use integer types
+; when there is a valid integer type.
+; CHECK-LABEL: @test16(
+; CHECK: %[[L1:.*]] = load i32*
+; CHECK-NOT: load
+; CHECK: store i32 %[[L1]], i32*
+; CHECK: store i32 %[[L1]], i32*
+; CHECK-NOT: store
+; CHECK: %[[L1:.*]] = load i32*
+; CHECK-NOT: load
+; CHECK: store i32 %[[L1]], i32*
+; CHECK: store i32 %[[L1]], i32*
+; CHECK-NOT: store
+; CHECK: ret
+
+entry:
+  %x.cast = bitcast i8* %x to float*
+  %a.cast = bitcast i8* %a to float*
+  %b.cast = bitcast i8* %b to float*
+  %c.cast = bitcast i8* %c to i32*
+
+  %x1 = load float* %x.cast
+  store float %x1, float* %a.cast
+  store float %x1, float* %b.cast
+
+  %x2 = load float* %x.cast
+  store float %x2, float* %b.cast
+  %x2.cast = bitcast float %x2 to i32
+  store i32 %x2.cast, i32* %c.cast
+
+  ret void
+}
+
+define void @test17(i8** %x, i8 %y) {
+; Check that in cases similar to @test16 we don't try to rewrite a load when
+; its only use is a store but it is used as the pointer to that store rather
+; than the value.
+;
+; CHECK-LABEL: @test17(
+; CHECK: %[[L:.*]] = load i8**
+; CHECK: store i8 %y, i8* %[[L]]
+
+entry:
+  %x.load = load i8** %x
+  store i8 %y, i8* %x.load
+
+  ret void
+}