index 2fa5a127a233b0efae0ef59986f5e98bdbf741e0..4f23db0908da7c00f01994de743b997c44973c3d 100644 (file)
using namespace llvm;
#define MRM_MAPPING \
+ MAP(C0, 32) \
MAP(C1, 33) \
MAP(C2, 34) \
MAP(C3, 35) \
MAP(C9, 38) \
MAP(CA, 39) \
MAP(CB, 40) \
- MAP(E8, 41) \
- MAP(F0, 42) \
- MAP(F8, 45) \
- MAP(F9, 46) \
- MAP(D0, 47) \
- MAP(D1, 48) \
- MAP(D4, 49) \
- MAP(D5, 50) \
- MAP(D6, 51) \
- MAP(D8, 52) \
- MAP(D9, 53) \
- MAP(DA, 54) \
- MAP(DB, 55) \
- MAP(DC, 56) \
- MAP(DD, 57) \
- MAP(DE, 58) \
- MAP(DF, 59)
+ MAP(CF, 41) \
+ MAP(D0, 42) \
+ MAP(D1, 43) \
+ MAP(D4, 44) \
+ MAP(D5, 45) \
+ MAP(D6, 46) \
+ MAP(D7, 47) \
+ MAP(D8, 48) \
+ MAP(D9, 49) \
+ MAP(DA, 50) \
+ MAP(DB, 51) \
+ MAP(DC, 52) \
+ MAP(DD, 53) \
+ MAP(DE, 54) \
+ MAP(DF, 55) \
+ MAP(E0, 56) \
+ MAP(E1, 57) \
+ MAP(E2, 58) \
+ MAP(E3, 59) \
+ MAP(E4, 60) \
+ MAP(E5, 61) \
+ MAP(E8, 62) \
+ MAP(E9, 63) \
+ MAP(EA, 64) \
+ MAP(EB, 65) \
+ MAP(EC, 66) \
+ MAP(ED, 67) \
+ MAP(EE, 68) \
+ MAP(F0, 69) \
+ MAP(F1, 70) \
+ MAP(F2, 71) \
+ MAP(F3, 72) \
+ MAP(F4, 73) \
+ MAP(F5, 74) \
+ MAP(F6, 75) \
+ MAP(F7, 76) \
+ MAP(F8, 77) \
+ MAP(F9, 78) \
+ MAP(FA, 79) \
+ MAP(FB, 80) \
+ MAP(FC, 81) \
+ MAP(FD, 82) \
+ MAP(FE, 83) \
+ MAP(FF, 84)
// A clone of X86 since we can't depend on something that is generated.
namespace X86Local {
MRMDestMem = 4,
MRMSrcReg = 5,
MRMSrcMem = 6,
+ RawFrmMemOffs = 7,
+ RawFrmSrc = 8,
+ RawFrmDst = 9,
+ RawFrmDstSrc = 10,
+ RawFrmImm8 = 11,
+ RawFrmImm16 = 12,
+ MRMXr = 14, MRMXm = 15,
MRM0r = 16, MRM1r = 17, MRM2r = 18, MRM3r = 19,
MRM4r = 20, MRM5r = 21, MRM6r = 22, MRM7r = 23,
MRM0m = 24, MRM1m = 25, MRM2m = 26, MRM3m = 27,
MRM4m = 28, MRM5m = 29, MRM6m = 30, MRM7m = 31,
- MRMInitReg = 32,
- RawFrmImm8 = 43,
- RawFrmImm16 = 44,
#define MAP(from, to) MRM_##from = to,
MRM_MAPPING
#undef MAP
};
enum {
- TB = 1,
- REP = 2,
- D8 = 3, D9 = 4, DA = 5, DB = 6,
- DC = 7, DD = 8, DE = 9, DF = 10,
- XD = 11, XS = 12,
- T8 = 13, P_TA = 14,
- A6 = 15, A7 = 16, T8XD = 17, T8XS = 18, TAXD = 19,
- XOP8 = 20, XOP9 = 21, XOPA = 22
+ OB = 0, TB = 1, T8 = 2, TA = 3, XOP8 = 4, XOP9 = 5, XOPA = 6
};
-}
-// If rows are added to the opcode extension tables, then corresponding entries
-// must be added here.
-//
-// If the row corresponds to a single byte (i.e., 8f), then add an entry for
-// that byte to ONE_BYTE_EXTENSION_TABLES.
-//
-// If the row corresponds to two bytes where the first is 0f, add an entry for
-// the second byte to TWO_BYTE_EXTENSION_TABLES.
-//
-// If the row corresponds to some other set of bytes, you will need to modify
-// the code in RecognizableInstr::emitDecodePath() as well, and add new prefixes
-// to the X86 TD files, except in two cases: if the first two bytes of such a
-// new combination are 0f 38 or 0f 3a, you just have to add maps called
-// THREE_BYTE_38_EXTENSION_TABLES and THREE_BYTE_3A_EXTENSION_TABLES and add a
-// switch(Opcode) just below the case X86Local::T8: or case X86Local::TA: line
-// in RecognizableInstr::emitDecodePath().
-
-#define ONE_BYTE_EXTENSION_TABLES \
- EXTENSION_TABLE(80) \
- EXTENSION_TABLE(81) \
- EXTENSION_TABLE(82) \
- EXTENSION_TABLE(83) \
- EXTENSION_TABLE(8f) \
- EXTENSION_TABLE(c0) \
- EXTENSION_TABLE(c1) \
- EXTENSION_TABLE(c6) \
- EXTENSION_TABLE(c7) \
- EXTENSION_TABLE(d0) \
- EXTENSION_TABLE(d1) \
- EXTENSION_TABLE(d2) \
- EXTENSION_TABLE(d3) \
- EXTENSION_TABLE(f6) \
- EXTENSION_TABLE(f7) \
- EXTENSION_TABLE(fe) \
- EXTENSION_TABLE(ff)
-
-#define TWO_BYTE_EXTENSION_TABLES \
- EXTENSION_TABLE(00) \
- EXTENSION_TABLE(01) \
- EXTENSION_TABLE(0d) \
- EXTENSION_TABLE(18) \
- EXTENSION_TABLE(71) \
- EXTENSION_TABLE(72) \
- EXTENSION_TABLE(73) \
- EXTENSION_TABLE(ae) \
- EXTENSION_TABLE(ba) \
- EXTENSION_TABLE(c7)
-
-#define THREE_BYTE_38_EXTENSION_TABLES \
- EXTENSION_TABLE(F3)
-
-#define XOP9_MAP_EXTENSION_TABLES \
- EXTENSION_TABLE(01) \
- EXTENSION_TABLE(02)
+ enum {
+ PS = 1, PD = 2, XS = 3, XD = 4
+ };
-using namespace X86Disassembler;
+ enum {
+ VEX = 1, XOP = 2, EVEX = 3
+ };
-/// needsModRMForDecode - Indicates whether a particular instruction requires a
-/// ModR/M byte for the instruction to be properly decoded. For example, a
-/// MRMDestReg instruction needs the Mod field in the ModR/M byte to be set to
-/// 0b11.
-///
-/// @param form - The form of the instruction.
-/// @return - true if the form implies that a ModR/M byte is required, false
-/// otherwise.
-static bool needsModRMForDecode(uint8_t form) {
- if (form == X86Local::MRMDestReg ||
- form == X86Local::MRMDestMem ||
- form == X86Local::MRMSrcReg ||
- form == X86Local::MRMSrcMem ||
- (form >= X86Local::MRM0r && form <= X86Local::MRM7r) ||
- (form >= X86Local::MRM0m && form <= X86Local::MRM7m))
- return true;
- else
- return false;
+ enum {
+ OpSize16 = 1, OpSize32 = 2
+ };
+
+ enum {
+ AdSize16 = 1, AdSize32 = 2, AdSize64 = 3
+ };
}
+using namespace X86Disassembler;
+
/// isRegFormat - Indicates whether a particular form requires the Mod field of
/// the ModR/M byte to be 0b11.
///
/// @return - true if the form implies that Mod must be 0b11, false
/// otherwise.
static bool isRegFormat(uint8_t form) {
- if (form == X86Local::MRMDestReg ||
- form == X86Local::MRMSrcReg ||
- (form >= X86Local::MRM0r && form <= X86Local::MRM7r))
- return true;
- else
- return false;
+ return (form == X86Local::MRMDestReg ||
+ form == X86Local::MRMSrcReg ||
+ form == X86Local::MRMXr ||
+ (form >= X86Local::MRM0r && form <= X86Local::MRM7r));
}
/// byteFromBitsInit - Extracts a value at most 8 bits in width from a BitsInit.
return;
}
- Prefix = byteFromRec(Rec, "Prefix");
+ OpPrefix = byteFromRec(Rec, "OpPrefixBits");
+ OpMap = byteFromRec(Rec, "OpMapBits");
Opcode = byteFromRec(Rec, "Opcode");
Form = byteFromRec(Rec, "FormBits");
- SegOvr = byteFromRec(Rec, "SegOvrBits");
+ Encoding = byteFromRec(Rec, "OpEncBits");
- HasOpSizePrefix = Rec->getValueAsBit("hasOpSizePrefix");
- HasAdSizePrefix = Rec->getValueAsBit("hasAdSizePrefix");
+ OpSize = byteFromRec(Rec, "OpSizeBits");
+ AdSize = byteFromRec(Rec, "AdSizeBits");
HasREX_WPrefix = Rec->getValueAsBit("hasREX_WPrefix");
- HasVEXPrefix = Rec->getValueAsBit("hasVEXPrefix");
- HasVEX_4VPrefix = Rec->getValueAsBit("hasVEX_4VPrefix");
- HasVEX_4VOp3Prefix = Rec->getValueAsBit("hasVEX_4VOp3Prefix");
+ HasVEX_4V = Rec->getValueAsBit("hasVEX_4V");
+ HasVEX_4VOp3 = Rec->getValueAsBit("hasVEX_4VOp3");
HasVEX_WPrefix = Rec->getValueAsBit("hasVEX_WPrefix");
HasMemOp4Prefix = Rec->getValueAsBit("hasMemOp4Prefix");
IgnoresVEX_L = Rec->getValueAsBit("ignoresVEX_L");
- HasEVEXPrefix = Rec->getValueAsBit("hasEVEXPrefix");
HasEVEX_L2Prefix = Rec->getValueAsBit("hasEVEX_L2");
HasEVEX_K = Rec->getValueAsBit("hasEVEX_K");
HasEVEX_KZ = Rec->getValueAsBit("hasEVEX_Z");
HasEVEX_B = Rec->getValueAsBit("hasEVEX_B");
- HasLockPrefix = Rec->getValueAsBit("hasLockPrefix");
IsCodeGenOnly = Rec->getValueAsBit("isCodeGenOnly");
+ ForceDisassemble = Rec->getValueAsBit("ForceDisassemble");
+ CD8_Scale = byteFromRec(Rec, "CD8_Scale");
Name = Rec->getName();
AsmString = Rec->getValueAsString("AsmString");
Operands = &insn.Operands.OperandList;
- IsSSE = (HasOpSizePrefix && (Name.find("16") == Name.npos)) ||
- (Name.find("CRC32") != Name.npos);
HasVEX_LPrefix = Rec->getValueAsBit("hasVEX_L");
// Check for 64-bit inst which does not require REX
break;
}
}
- // FIXME: These instructions aren't marked as 64-bit in any way
- Is64Bit |= Rec->getName().find("MOV64") != Name.npos ||
- Rec->getName().find("PUSH64") != Name.npos ||
- Rec->getName().find("POP64") != Name.npos;
+
+ if (Form == X86Local::Pseudo || (IsCodeGenOnly && !ForceDisassemble)) {
+ ShouldBeEmitted = false;
+ return;
+ }
+
+ // Special case since there is no attribute class for 64-bit and VEX
+ if (Name == "VMASKMOVDQU64") {
+ ShouldBeEmitted = false;
+ return;
+ }
ShouldBeEmitted = true;
}
RecognizableInstr recogInstr(tables, insn, uid);
- recogInstr.emitInstructionSpecifier();
-
- if (recogInstr.shouldBeEmitted())
+ if (recogInstr.shouldBeEmitted()) {
+ recogInstr.emitInstructionSpecifier();
recogInstr.emitDecodePath(tables);
+ }
}
#define EVEX_KB(n) (HasEVEX_KZ && HasEVEX_B ? n##_KZ_B : \
InstructionContext RecognizableInstr::insnContext() const {
InstructionContext insnContext;
- if (HasEVEXPrefix) {
+ if (Encoding == X86Local::EVEX) {
if (HasVEX_LPrefix && HasEVEX_L2Prefix) {
errs() << "Don't support VEX.L if EVEX_L2 is enabled: " << Name << "\n";
llvm_unreachable("Don't support VEX.L if EVEX_L2 is enabled");
}
// VEX_L & VEX_W
if (HasVEX_LPrefix && HasVEX_WPrefix) {
- if (HasOpSizePrefix)
+ if (OpPrefix == X86Local::PD)
insnContext = EVEX_KB(IC_EVEX_L_W_OPSIZE);
- else if (Prefix == X86Local::XS || Prefix == X86Local::T8XS)
+ else if (OpPrefix == X86Local::XS)
insnContext = EVEX_KB(IC_EVEX_L_W_XS);
- else if (Prefix == X86Local::XD || Prefix == X86Local::T8XD ||
- Prefix == X86Local::TAXD)
+ else if (OpPrefix == X86Local::XD)
insnContext = EVEX_KB(IC_EVEX_L_W_XD);
- else
+ else if (OpPrefix == X86Local::PS)
insnContext = EVEX_KB(IC_EVEX_L_W);
+ else {
+ errs() << "Instruction does not use a prefix: " << Name << "\n";
+ llvm_unreachable("Invalid prefix");
+ }
} else if (HasVEX_LPrefix) {
// VEX_L
- if (HasOpSizePrefix)
+ if (OpPrefix == X86Local::PD)
insnContext = EVEX_KB(IC_EVEX_L_OPSIZE);
- else if (Prefix == X86Local::XS || Prefix == X86Local::T8XS)
+ else if (OpPrefix == X86Local::XS)
insnContext = EVEX_KB(IC_EVEX_L_XS);
- else if (Prefix == X86Local::XD || Prefix == X86Local::T8XD ||
- Prefix == X86Local::TAXD)
+ else if (OpPrefix == X86Local::XD)
insnContext = EVEX_KB(IC_EVEX_L_XD);
- else
+ else if (OpPrefix == X86Local::PS)
insnContext = EVEX_KB(IC_EVEX_L);
+ else {
+ errs() << "Instruction does not use a prefix: " << Name << "\n";
+ llvm_unreachable("Invalid prefix");
+ }
}
else if (HasEVEX_L2Prefix && HasVEX_WPrefix) {
// EVEX_L2 & VEX_W
- if (HasOpSizePrefix)
+ if (OpPrefix == X86Local::PD)
insnContext = EVEX_KB(IC_EVEX_L2_W_OPSIZE);
- else if (Prefix == X86Local::XS || Prefix == X86Local::T8XS)
+ else if (OpPrefix == X86Local::XS)
insnContext = EVEX_KB(IC_EVEX_L2_W_XS);
- else if (Prefix == X86Local::XD || Prefix == X86Local::T8XD ||
- Prefix == X86Local::TAXD)
+ else if (OpPrefix == X86Local::XD)
insnContext = EVEX_KB(IC_EVEX_L2_W_XD);
- else
+ else if (OpPrefix == X86Local::PS)
insnContext = EVEX_KB(IC_EVEX_L2_W);
+ else {
+ errs() << "Instruction does not use a prefix: " << Name << "\n";
+ llvm_unreachable("Invalid prefix");
+ }
} else if (HasEVEX_L2Prefix) {
// EVEX_L2
- if (HasOpSizePrefix)
+ if (OpPrefix == X86Local::PD)
insnContext = EVEX_KB(IC_EVEX_L2_OPSIZE);
- else if (Prefix == X86Local::XD || Prefix == X86Local::T8XD ||
- Prefix == X86Local::TAXD)
+ else if (OpPrefix == X86Local::XD)
insnContext = EVEX_KB(IC_EVEX_L2_XD);
- else if (Prefix == X86Local::XS || Prefix == X86Local::T8XS)
+ else if (OpPrefix == X86Local::XS)
insnContext = EVEX_KB(IC_EVEX_L2_XS);
- else
+ else if (OpPrefix == X86Local::PS)
insnContext = EVEX_KB(IC_EVEX_L2);
+ else {
+ errs() << "Instruction does not use a prefix: " << Name << "\n";
+ llvm_unreachable("Invalid prefix");
+ }
}
else if (HasVEX_WPrefix) {
// VEX_W
- if (HasOpSizePrefix)
+ if (OpPrefix == X86Local::PD)
insnContext = EVEX_KB(IC_EVEX_W_OPSIZE);
- else if (Prefix == X86Local::XS || Prefix == X86Local::T8XS)
+ else if (OpPrefix == X86Local::XS)
insnContext = EVEX_KB(IC_EVEX_W_XS);
- else if (Prefix == X86Local::XD || Prefix == X86Local::T8XD ||
- Prefix == X86Local::TAXD)
+ else if (OpPrefix == X86Local::XD)
insnContext = EVEX_KB(IC_EVEX_W_XD);
- else
+ else if (OpPrefix == X86Local::PS)
insnContext = EVEX_KB(IC_EVEX_W);
+ else {
+ errs() << "Instruction does not use a prefix: " << Name << "\n";
+ llvm_unreachable("Invalid prefix");
+ }
}
// No L, no W
- else if (HasOpSizePrefix)
+ else if (OpPrefix == X86Local::PD)
insnContext = EVEX_KB(IC_EVEX_OPSIZE);
- else if (Prefix == X86Local::XD || Prefix == X86Local::T8XD ||
- Prefix == X86Local::TAXD)
+ else if (OpPrefix == X86Local::XD)
insnContext = EVEX_KB(IC_EVEX_XD);
- else if (Prefix == X86Local::XS || Prefix == X86Local::T8XS)
+ else if (OpPrefix == X86Local::XS)
insnContext = EVEX_KB(IC_EVEX_XS);
else
insnContext = EVEX_KB(IC_EVEX);
/// eof EVEX
- } else if (HasVEX_4VPrefix || HasVEX_4VOp3Prefix|| HasVEXPrefix) {
+ } else if (Encoding == X86Local::VEX || Encoding == X86Local::XOP) {
if (HasVEX_LPrefix && HasVEX_WPrefix) {
- if (HasOpSizePrefix)
+ if (OpPrefix == X86Local::PD)
insnContext = IC_VEX_L_W_OPSIZE;
- else if (Prefix == X86Local::XS || Prefix == X86Local::T8XS)
+ else if (OpPrefix == X86Local::XS)
insnContext = IC_VEX_L_W_XS;
- else if (Prefix == X86Local::XD || Prefix == X86Local::T8XD ||
- Prefix == X86Local::TAXD)
+ else if (OpPrefix == X86Local::XD)
insnContext = IC_VEX_L_W_XD;
- else
+ else if (OpPrefix == X86Local::PS)
insnContext = IC_VEX_L_W;
- } else if (HasOpSizePrefix && HasVEX_LPrefix)
+ else {
+ errs() << "Instruction does not use a prefix: " << Name << "\n";
+ llvm_unreachable("Invalid prefix");
+ }
+ } else if (OpPrefix == X86Local::PD && HasVEX_LPrefix)
insnContext = IC_VEX_L_OPSIZE;
- else if (HasOpSizePrefix && HasVEX_WPrefix)
+ else if (OpPrefix == X86Local::PD && HasVEX_WPrefix)
insnContext = IC_VEX_W_OPSIZE;
- else if (HasOpSizePrefix)
+ else if (OpPrefix == X86Local::PD)
insnContext = IC_VEX_OPSIZE;
- else if (HasVEX_LPrefix &&
- (Prefix == X86Local::XS || Prefix == X86Local::T8XS))
+ else if (HasVEX_LPrefix && OpPrefix == X86Local::XS)
insnContext = IC_VEX_L_XS;
- else if (HasVEX_LPrefix && (Prefix == X86Local::XD ||
- Prefix == X86Local::T8XD ||
- Prefix == X86Local::TAXD))
+ else if (HasVEX_LPrefix && OpPrefix == X86Local::XD)
insnContext = IC_VEX_L_XD;
- else if (HasVEX_WPrefix &&
- (Prefix == X86Local::XS || Prefix == X86Local::T8XS))
+ else if (HasVEX_WPrefix && OpPrefix == X86Local::XS)
insnContext = IC_VEX_W_XS;
- else if (HasVEX_WPrefix && (Prefix == X86Local::XD ||
- Prefix == X86Local::T8XD ||
- Prefix == X86Local::TAXD))
+ else if (HasVEX_WPrefix && OpPrefix == X86Local::XD)
insnContext = IC_VEX_W_XD;
- else if (HasVEX_WPrefix)
+ else if (HasVEX_WPrefix && OpPrefix == X86Local::PS)
insnContext = IC_VEX_W;
- else if (HasVEX_LPrefix)
+ else if (HasVEX_LPrefix && OpPrefix == X86Local::PS)
insnContext = IC_VEX_L;
- else if (Prefix == X86Local::XD || Prefix == X86Local::T8XD ||
- Prefix == X86Local::TAXD)
+ else if (OpPrefix == X86Local::XD)
insnContext = IC_VEX_XD;
- else if (Prefix == X86Local::XS || Prefix == X86Local::T8XS)
+ else if (OpPrefix == X86Local::XS)
insnContext = IC_VEX_XS;
- else
+ else if (OpPrefix == X86Local::PS)
insnContext = IC_VEX;
- } else if (Is64Bit || HasREX_WPrefix) {
- if (HasREX_WPrefix && HasOpSizePrefix)
+ else {
+ errs() << "Instruction does not use a prefix: " << Name << "\n";
+ llvm_unreachable("Invalid prefix");
+ }
+ } else if (Is64Bit || HasREX_WPrefix || AdSize == X86Local::AdSize64) {
+ if (HasREX_WPrefix && (OpSize == X86Local::OpSize16 || OpPrefix == X86Local::PD))
insnContext = IC_64BIT_REXW_OPSIZE;
- else if (HasOpSizePrefix && (Prefix == X86Local::XD ||
- Prefix == X86Local::T8XD ||
- Prefix == X86Local::TAXD))
+ else if (HasREX_WPrefix && AdSize == X86Local::AdSize32)
+ insnContext = IC_64BIT_REXW_ADSIZE;
+ else if (OpSize == X86Local::OpSize16 && OpPrefix == X86Local::XD)
insnContext = IC_64BIT_XD_OPSIZE;
- else if (HasOpSizePrefix &&
- (Prefix == X86Local::XS || Prefix == X86Local::T8XS))
+ else if (OpSize == X86Local::OpSize16 && OpPrefix == X86Local::XS)
insnContext = IC_64BIT_XS_OPSIZE;
- else if (HasOpSizePrefix)
+ else if (OpSize == X86Local::OpSize16 && AdSize == X86Local::AdSize32)
+ insnContext = IC_64BIT_OPSIZE_ADSIZE;
+ else if (OpSize == X86Local::OpSize16 || OpPrefix == X86Local::PD)
insnContext = IC_64BIT_OPSIZE;
- else if (HasAdSizePrefix)
+ else if (AdSize == X86Local::AdSize32)
insnContext = IC_64BIT_ADSIZE;
- else if (HasREX_WPrefix &&
- (Prefix == X86Local::XS || Prefix == X86Local::T8XS))
+ else if (HasREX_WPrefix && OpPrefix == X86Local::XS)
insnContext = IC_64BIT_REXW_XS;
- else if (HasREX_WPrefix && (Prefix == X86Local::XD ||
- Prefix == X86Local::T8XD ||
- Prefix == X86Local::TAXD))
+ else if (HasREX_WPrefix && OpPrefix == X86Local::XD)
insnContext = IC_64BIT_REXW_XD;
- else if (Prefix == X86Local::XD || Prefix == X86Local::T8XD ||
- Prefix == X86Local::TAXD)
+ else if (OpPrefix == X86Local::XD)
insnContext = IC_64BIT_XD;
- else if (Prefix == X86Local::XS || Prefix == X86Local::T8XS)
+ else if (OpPrefix == X86Local::XS)
insnContext = IC_64BIT_XS;
else if (HasREX_WPrefix)
insnContext = IC_64BIT_REXW;
else
insnContext = IC_64BIT;
} else {
- if (HasOpSizePrefix && (Prefix == X86Local::XD ||
- Prefix == X86Local::T8XD ||
- Prefix == X86Local::TAXD))
+ if (OpSize == X86Local::OpSize16 && OpPrefix == X86Local::XD)
insnContext = IC_XD_OPSIZE;
- else if (HasOpSizePrefix &&
- (Prefix == X86Local::XS || Prefix == X86Local::T8XS))
+ else if (OpSize == X86Local::OpSize16 && OpPrefix == X86Local::XS)
insnContext = IC_XS_OPSIZE;
- else if (HasOpSizePrefix)
+ else if (OpSize == X86Local::OpSize16 && AdSize == X86Local::AdSize16)
+ insnContext = IC_OPSIZE_ADSIZE;
+ else if (OpSize == X86Local::OpSize16 || OpPrefix == X86Local::PD)
insnContext = IC_OPSIZE;
- else if (HasAdSizePrefix)
+ else if (AdSize == X86Local::AdSize16)
insnContext = IC_ADSIZE;
- else if (Prefix == X86Local::XD || Prefix == X86Local::T8XD ||
- Prefix == X86Local::TAXD)
+ else if (OpPrefix == X86Local::XD)
insnContext = IC_XD;
- else if (Prefix == X86Local::XS || Prefix == X86Local::T8XS ||
- Prefix == X86Local::REP)
+ else if (OpPrefix == X86Local::XS)
insnContext = IC_XS;
else
insnContext = IC;
return insnContext;
}
-RecognizableInstr::filter_ret RecognizableInstr::filter() const {
- ///////////////////
- // FILTER_STRONG
- //
-
- // Filter out intrinsics
-
- assert(Rec->isSubClassOf("X86Inst") && "Can only filter X86 instructions");
-
- if (Form == X86Local::Pseudo ||
- (IsCodeGenOnly && Name.find("_REV") == Name.npos &&
- Name.find("INC32") == Name.npos && Name.find("DEC32") == Name.npos))
- return FILTER_STRONG;
-
-
- // Filter out artificial instructions but leave in the LOCK_PREFIX so it is
- // printed as a separate "instruction".
-
- // Filter out instructions with segment override prefixes.
- // They're too messy to handle now and we'll special case them if needed.
-
- if (SegOvr)
- return FILTER_STRONG;
-
-
- /////////////////
- // FILTER_WEAK
- //
-
-
- // Filter out instructions with a LOCK prefix;
- // prefer forms that do not have the prefix
- if (HasLockPrefix)
- return FILTER_WEAK;
-
- // Filter out alternate forms of AVX instructions
- if (Name.find("_alt") != Name.npos ||
- (Name.find("r64r") != Name.npos && Name.find("r64r64") == Name.npos && Name.find("r64r8") == Name.npos) ||
- Name.find("_64mr") != Name.npos ||
- Name.find("rr64") != Name.npos)
- return FILTER_WEAK;
-
- // Special cases.
-
- if (Name == "PUSH64i16" ||
- Name == "MOVPQI2QImr" ||
- Name == "VMOVPQI2QImr" ||
- Name == "VMASKMOVDQU64")
- return FILTER_WEAK;
-
- // XACQUIRE and XRELEASE reuse REPNE and REP respectively.
- // For now, just prefer the REP versions.
- if (Name == "XACQUIRE_PREFIX" ||
- Name == "XRELEASE_PREFIX")
- return FILTER_WEAK;
-
- return FILTER_NORMAL;
+void RecognizableInstr::adjustOperandEncoding(OperandEncoding &encoding) {
+ // The scaling factor for AVX512 compressed displacement encoding is an
+ // instruction attribute. Adjust the ModRM encoding type to include the
+ // scale for compressed displacement.
+ if (encoding != ENCODING_RM || CD8_Scale == 0)
+ return;
+ encoding = (OperandEncoding)(encoding + Log2_32(CD8_Scale));
+ assert(encoding <= ENCODING_RM_CD64 && "Invalid CDisp scaling");
}
void RecognizableInstr::handleOperand(bool optional, unsigned &operandIndex,
const unsigned *operandMapping,
OperandEncoding (*encodingFromString)
(const std::string&,
- bool hasOpSizePrefix)) {
+ uint8_t OpSize)) {
if (optional) {
if (physicalOperandIndex >= numPhysicalOperands)
return;
const std::string &typeName = (*Operands)[operandIndex].Rec->getName();
- Spec->operands[operandIndex].encoding = encodingFromString(typeName,
- HasOpSizePrefix);
+ OperandEncoding encoding = encodingFromString(typeName, OpSize);
+ // Adjust the encoding type for an operand based on the instruction.
+ adjustOperandEncoding(encoding);
+ Spec->operands[operandIndex].encoding = encoding;
Spec->operands[operandIndex].type = typeFromString(typeName,
- IsSSE,
- HasREX_WPrefix,
- HasOpSizePrefix);
+ HasREX_WPrefix, OpSize);
++operandIndex;
++physicalOperandIndex;
void RecognizableInstr::emitInstructionSpecifier() {
Spec->name = Name;
- if (!ShouldBeEmitted)
- return;
-
- switch (filter()) {
- case FILTER_WEAK:
- Spec->filtered = true;
- break;
- case FILTER_STRONG:
- ShouldBeEmitted = false;
- return;
- case FILTER_NORMAL:
- break;
- }
-
Spec->insnContext = insnContext();
const std::vector<CGIOperandList::OperandInfo> &OperandList = *Operands;
assert(numOperands <= X86_MAX_OPERANDS && "X86_MAX_OPERANDS is not large enough");
for (unsigned operandIndex = 0; operandIndex < numOperands; ++operandIndex) {
- if (OperandList[operandIndex].Constraints.size()) {
+ if (!OperandList[operandIndex].Constraints.empty()) {
const CGIOperandList::ConstraintInfo &Constraint =
OperandList[operandIndex].Constraints[0];
if (Constraint.isTied()) {
// physicalOperandIndex should always be < numPhysicalOperands
unsigned physicalOperandIndex = 0;
+ // Given the set of prefix bits, how many additional operands does the
+ // instruction have?
+ unsigned additionalOperands = 0;
+ if (HasVEX_4V || HasVEX_4VOp3)
+ ++additionalOperands;
+ if (HasEVEX_K)
+ ++additionalOperands;
+
switch (Form) {
+ default: llvm_unreachable("Unhandled form");
+ case X86Local::RawFrmSrc:
+ HANDLE_OPERAND(relocation);
+ return;
+ case X86Local::RawFrmDst:
+ HANDLE_OPERAND(relocation);
+ return;
+ case X86Local::RawFrmDstSrc:
+ HANDLE_OPERAND(relocation);
+ HANDLE_OPERAND(relocation);
+ return;
case X86Local::RawFrm:
// Operand 1 (optional) is an address or immediate.
// Operand 2 (optional) is an immediate.
HANDLE_OPTIONAL(relocation)
HANDLE_OPTIONAL(immediate)
break;
+ case X86Local::RawFrmMemOffs:
+ // Operand 1 is an address.
+ HANDLE_OPERAND(relocation);
+ break;
case X86Local::AddRegFrm:
// Operand 1 is added to the opcode.
// Operand 2 (optional) is an address.
break;
case X86Local::MRMDestReg:
// Operand 1 is a register operand in the R/M field.
+ // - In AVX512 there may be a mask operand here -
// Operand 2 is a register operand in the Reg/Opcode field.
// - In AVX, there is a register operand in the VEX.vvvv field here -
// Operand 3 (optional) is an immediate.
- if (HasVEX_4VPrefix)
- assert(numPhysicalOperands >= 3 && numPhysicalOperands <= 4 &&
- "Unexpected number of operands for MRMDestRegFrm with VEX_4V");
- else
- assert(numPhysicalOperands >= 2 && numPhysicalOperands <= 3 &&
- "Unexpected number of operands for MRMDestRegFrm");
+ assert(numPhysicalOperands >= 2 + additionalOperands &&
+ numPhysicalOperands <= 3 + additionalOperands &&
+ "Unexpected number of operands for MRMDestRegFrm");
HANDLE_OPERAND(rmRegister)
+ if (HasEVEX_K)
+ HANDLE_OPERAND(writemaskRegister)
- if (HasVEX_4VPrefix)
+ if (HasVEX_4V)
// FIXME: In AVX, the register below becomes the one encoded
// in ModRMVEX and the one above the one in the VEX.VVVV field
HANDLE_OPERAND(vvvvRegister)
// Operand 2 is a register operand in the Reg/Opcode field.
// - In AVX, there is a register operand in the VEX.vvvv field here -
// Operand 3 (optional) is an immediate.
- if (HasVEX_4VPrefix)
- assert(numPhysicalOperands >= 3 && numPhysicalOperands <= 4 &&
- "Unexpected number of operands for MRMDestMemFrm with VEX_4V");
- else
- assert(numPhysicalOperands >= 2 && numPhysicalOperands <= 3 &&
- "Unexpected number of operands for MRMDestMemFrm");
+ assert(numPhysicalOperands >= 2 + additionalOperands &&
+ numPhysicalOperands <= 3 + additionalOperands &&
+ "Unexpected number of operands for MRMDestMemFrm with VEX_4V");
+
HANDLE_OPERAND(memory)
if (HasEVEX_K)
HANDLE_OPERAND(writemaskRegister)
- if (HasVEX_4VPrefix)
+ if (HasVEX_4V)
// FIXME: In AVX, the register below becomes the one encoded
// in ModRMVEX and the one above the one in the VEX.VVVV field
HANDLE_OPERAND(vvvvRegister)
// Operand 3 (optional) is an immediate.
// Operand 4 (optional) is an immediate.
- if (HasVEX_4VPrefix || HasVEX_4VOp3Prefix)
- assert(numPhysicalOperands >= 3 && numPhysicalOperands <= 5 &&
- "Unexpected number of operands for MRMSrcRegFrm with VEX_4V");
- else
- assert(numPhysicalOperands >= 2 && numPhysicalOperands <= 4 &&
- "Unexpected number of operands for MRMSrcRegFrm");
+ assert(numPhysicalOperands >= 2 + additionalOperands &&
+ numPhysicalOperands <= 4 + additionalOperands &&
+ "Unexpected number of operands for MRMSrcRegFrm");
HANDLE_OPERAND(roRegister)
if (HasEVEX_K)
HANDLE_OPERAND(writemaskRegister)
- if (HasVEX_4VPrefix)
+ if (HasVEX_4V)
// FIXME: In AVX, the register below becomes the one encoded
// in ModRMVEX and the one above the one in the VEX.VVVV field
HANDLE_OPERAND(vvvvRegister)
HANDLE_OPERAND(rmRegister)
- if (HasVEX_4VOp3Prefix)
+ if (HasVEX_4VOp3)
HANDLE_OPERAND(vvvvRegister)
if (!HasMemOp4Prefix)
// - In AVX, there is a register operand in the VEX.vvvv field here -
// Operand 3 (optional) is an immediate.
- if (HasVEX_4VPrefix || HasVEX_4VOp3Prefix)
- assert(numPhysicalOperands >= 3 && numPhysicalOperands <= 5 &&
- "Unexpected number of operands for MRMSrcMemFrm with VEX_4V");
- else
- assert(numPhysicalOperands >= 2 && numPhysicalOperands <= 3 &&
- "Unexpected number of operands for MRMSrcMemFrm");
+ assert(numPhysicalOperands >= 2 + additionalOperands &&
+ numPhysicalOperands <= 4 + additionalOperands &&
+ "Unexpected number of operands for MRMSrcMemFrm");
HANDLE_OPERAND(roRegister)
if (HasEVEX_K)
HANDLE_OPERAND(writemaskRegister)
- if (HasVEX_4VPrefix)
+ if (HasVEX_4V)
// FIXME: In AVX, the register below becomes the one encoded
// in ModRMVEX and the one above the one in the VEX.VVVV field
HANDLE_OPERAND(vvvvRegister)
HANDLE_OPERAND(memory)
- if (HasVEX_4VOp3Prefix)
+ if (HasVEX_4VOp3)
HANDLE_OPERAND(vvvvRegister)
if (!HasMemOp4Prefix)
HANDLE_OPTIONAL(immediate)
HANDLE_OPTIONAL(immediate) // above might be a register in 7:4
break;
+ case X86Local::MRMXr:
case X86Local::MRM0r:
case X86Local::MRM1r:
case X86Local::MRM2r:
case X86Local::MRM5r:
case X86Local::MRM6r:
case X86Local::MRM7r:
- {
- // Operand 1 is a register operand in the R/M field.
- // Operand 2 (optional) is an immediate or relocation.
- // Operand 3 (optional) is an immediate.
- unsigned kOp = (HasEVEX_K) ? 1:0;
- unsigned Op4v = (HasVEX_4VPrefix) ? 1:0;
- if (numPhysicalOperands > 3 + kOp + Op4v)
- llvm_unreachable("Unexpected number of operands for MRMnr");
- }
- if (HasVEX_4VPrefix)
+ // Operand 1 is a register operand in the R/M field.
+ // Operand 2 (optional) is an immediate or relocation.
+ // Operand 3 (optional) is an immediate.
+ assert(numPhysicalOperands >= 0 + additionalOperands &&
+ numPhysicalOperands <= 3 + additionalOperands &&
+ "Unexpected number of operands for MRMnr");
+
+ if (HasVEX_4V)
HANDLE_OPERAND(vvvvRegister)
if (HasEVEX_K)
HANDLE_OPTIONAL(relocation)
HANDLE_OPTIONAL(immediate)
break;
+ case X86Local::MRMXm:
case X86Local::MRM0m:
case X86Local::MRM1m:
case X86Local::MRM2m:
case X86Local::MRM5m:
case X86Local::MRM6m:
case X86Local::MRM7m:
- {
- // Operand 1 is a memory operand (possibly SIB-extended)
- // Operand 2 (optional) is an immediate or relocation.
- unsigned kOp = (HasEVEX_K) ? 1:0;
- unsigned Op4v = (HasVEX_4VPrefix) ? 1:0;
- if (numPhysicalOperands < 1 + kOp + Op4v ||
- numPhysicalOperands > 2 + kOp + Op4v)
- llvm_unreachable("Unexpected number of operands for MRMnm");
- }
- if (HasVEX_4VPrefix)
+ // Operand 1 is a memory operand (possibly SIB-extended)
+ // Operand 2 (optional) is an immediate or relocation.
+ assert(numPhysicalOperands >= 1 + additionalOperands &&
+ numPhysicalOperands <= 2 + additionalOperands &&
+ "Unexpected number of operands for MRMnm");
+
+ if (HasVEX_4V)
HANDLE_OPERAND(vvvvRegister)
if (HasEVEX_K)
HANDLE_OPERAND(writemaskRegister)
HANDLE_OPERAND(relocation)
}
break;
- case X86Local::MRMInitReg:
+ case X86Local::MRM_C0: case X86Local::MRM_C1: case X86Local::MRM_C2:
+ case X86Local::MRM_C3: case X86Local::MRM_C4: case X86Local::MRM_C8:
+ case X86Local::MRM_C9: case X86Local::MRM_CA: case X86Local::MRM_CB:
+ case X86Local::MRM_CF: case X86Local::MRM_D0: case X86Local::MRM_D1:
+ case X86Local::MRM_D4: case X86Local::MRM_D5: case X86Local::MRM_D6:
+ case X86Local::MRM_D7: case X86Local::MRM_D8: case X86Local::MRM_D9:
+ case X86Local::MRM_DA: case X86Local::MRM_DB: case X86Local::MRM_DC:
+ case X86Local::MRM_DD: case X86Local::MRM_DE: case X86Local::MRM_DF:
+ case X86Local::MRM_E0: case X86Local::MRM_E1: case X86Local::MRM_E2:
+ case X86Local::MRM_E3: case X86Local::MRM_E4: case X86Local::MRM_E5:
+ case X86Local::MRM_E8: case X86Local::MRM_E9: case X86Local::MRM_EA:
+ case X86Local::MRM_EB: case X86Local::MRM_EC: case X86Local::MRM_ED:
+ case X86Local::MRM_EE: case X86Local::MRM_F0: case X86Local::MRM_F1:
+ case X86Local::MRM_F2: case X86Local::MRM_F3: case X86Local::MRM_F4:
+ case X86Local::MRM_F5: case X86Local::MRM_F6: case X86Local::MRM_F7:
+ case X86Local::MRM_F9: case X86Local::MRM_FA: case X86Local::MRM_FB:
+ case X86Local::MRM_FC: case X86Local::MRM_FD: case X86Local::MRM_FE:
+ case X86Local::MRM_FF:
// Ignored.
break;
}
OpcodeType opcodeType = (OpcodeType)-1;
- ModRMFilter* filter = NULL;
+ ModRMFilter* filter = nullptr;
uint8_t opcodeToSet = 0;
- switch (Prefix) {
- default: llvm_unreachable("Invalid prefix!");
- // Extended two-byte opcodes can start with f2 0f, f3 0f, or 0f
- case X86Local::XD:
- case X86Local::XS:
+ switch (OpMap) {
+ default: llvm_unreachable("Invalid map!");
+ case X86Local::OB:
case X86Local::TB:
- opcodeType = TWOBYTE;
-
- switch (Opcode) {
- default:
- if (needsModRMForDecode(Form))
- filter = new ModFilter(isRegFormat(Form));
- else
- filter = new DumbFilter();
- break;
-#define EXTENSION_TABLE(n) case 0x##n:
- TWO_BYTE_EXTENSION_TABLES
-#undef EXTENSION_TABLE
- switch (Form) {
- default:
- llvm_unreachable("Unhandled two-byte extended opcode");
- case X86Local::MRM0r:
- case X86Local::MRM1r:
- case X86Local::MRM2r:
- case X86Local::MRM3r:
- case X86Local::MRM4r:
- case X86Local::MRM5r:
- case X86Local::MRM6r:
- case X86Local::MRM7r:
- filter = new ExtendedFilter(true, Form - X86Local::MRM0r);
- break;
- case X86Local::MRM0m:
- case X86Local::MRM1m:
- case X86Local::MRM2m:
- case X86Local::MRM3m:
- case X86Local::MRM4m:
- case X86Local::MRM5m:
- case X86Local::MRM6m:
- case X86Local::MRM7m:
- filter = new ExtendedFilter(false, Form - X86Local::MRM0m);
- break;
- MRM_MAPPING
- } // switch (Form)
- break;
- } // switch (Opcode)
- opcodeToSet = Opcode;
- break;
case X86Local::T8:
- case X86Local::T8XD:
- case X86Local::T8XS:
- opcodeType = THREEBYTE_38;
- switch (Opcode) {
- default:
- if (needsModRMForDecode(Form))
- filter = new ModFilter(isRegFormat(Form));
- else
- filter = new DumbFilter();
- break;
-#define EXTENSION_TABLE(n) case 0x##n:
- THREE_BYTE_38_EXTENSION_TABLES
-#undef EXTENSION_TABLE
- switch (Form) {
- default:
- llvm_unreachable("Unhandled two-byte extended opcode");
- case X86Local::MRM0r:
- case X86Local::MRM1r:
- case X86Local::MRM2r:
- case X86Local::MRM3r:
- case X86Local::MRM4r:
- case X86Local::MRM5r:
- case X86Local::MRM6r:
- case X86Local::MRM7r:
- filter = new ExtendedFilter(true, Form - X86Local::MRM0r);
- break;
- case X86Local::MRM0m:
- case X86Local::MRM1m:
- case X86Local::MRM2m:
- case X86Local::MRM3m:
- case X86Local::MRM4m:
- case X86Local::MRM5m:
- case X86Local::MRM6m:
- case X86Local::MRM7m:
- filter = new ExtendedFilter(false, Form - X86Local::MRM0m);
- break;
- MRM_MAPPING
- } // switch (Form)
- break;
- } // switch (Opcode)
- opcodeToSet = Opcode;
- break;
- case X86Local::P_TA:
- case X86Local::TAXD:
- opcodeType = THREEBYTE_3A;
- if (needsModRMForDecode(Form))
- filter = new ModFilter(isRegFormat(Form));
- else
- filter = new DumbFilter();
- opcodeToSet = Opcode;
- break;
- case X86Local::A6:
- opcodeType = THREEBYTE_A6;
- if (needsModRMForDecode(Form))
- filter = new ModFilter(isRegFormat(Form));
- else
- filter = new DumbFilter();
- opcodeToSet = Opcode;
- break;
- case X86Local::A7:
- opcodeType = THREEBYTE_A7;
- if (needsModRMForDecode(Form))
- filter = new ModFilter(isRegFormat(Form));
- else
- filter = new DumbFilter();
- opcodeToSet = Opcode;
- break;
+ case X86Local::TA:
case X86Local::XOP8:
- opcodeType = XOP8_MAP;
- if (needsModRMForDecode(Form))
- filter = new ModFilter(isRegFormat(Form));
- else
- filter = new DumbFilter();
- opcodeToSet = Opcode;
- break;
case X86Local::XOP9:
- opcodeType = XOP9_MAP;
- switch (Opcode) {
+ case X86Local::XOPA:
+ switch (OpMap) {
+ default: llvm_unreachable("Unexpected map!");
+ case X86Local::OB: opcodeType = ONEBYTE; break;
+ case X86Local::TB: opcodeType = TWOBYTE; break;
+ case X86Local::T8: opcodeType = THREEBYTE_38; break;
+ case X86Local::TA: opcodeType = THREEBYTE_3A; break;
+ case X86Local::XOP8: opcodeType = XOP8_MAP; break;
+ case X86Local::XOP9: opcodeType = XOP9_MAP; break;
+ case X86Local::XOPA: opcodeType = XOPA_MAP; break;
+ }
+
+ switch (Form) {
default:
- if (needsModRMForDecode(Form))
- filter = new ModFilter(isRegFormat(Form));
- else
- filter = new DumbFilter();
- break;
-#define EXTENSION_TABLE(n) case 0x##n:
- XOP9_MAP_EXTENSION_TABLES
-#undef EXTENSION_TABLE
- switch (Form) {
- default:
- llvm_unreachable("Unhandled XOP9 extended opcode");
- case X86Local::MRM0r:
- case X86Local::MRM1r:
- case X86Local::MRM2r:
- case X86Local::MRM3r:
- case X86Local::MRM4r:
- case X86Local::MRM5r:
- case X86Local::MRM6r:
- case X86Local::MRM7r:
- filter = new ExtendedFilter(true, Form - X86Local::MRM0r);
- break;
- case X86Local::MRM0m:
- case X86Local::MRM1m:
- case X86Local::MRM2m:
- case X86Local::MRM3m:
- case X86Local::MRM4m:
- case X86Local::MRM5m:
- case X86Local::MRM6m:
- case X86Local::MRM7m:
- filter = new ExtendedFilter(false, Form - X86Local::MRM0m);
- break;
- MRM_MAPPING
- } // switch (Form)
+ filter = new DumbFilter();
break;
- } // switch (Opcode)
- opcodeToSet = Opcode;
- break;
- case X86Local::XOPA:
- opcodeType = XOPA_MAP;
- if (needsModRMForDecode(Form))
+ case X86Local::MRMDestReg: case X86Local::MRMDestMem:
+ case X86Local::MRMSrcReg: case X86Local::MRMSrcMem:
+ case X86Local::MRMXr: case X86Local::MRMXm:
filter = new ModFilter(isRegFormat(Form));
- else
- filter = new DumbFilter();
- opcodeToSet = Opcode;
- break;
- case X86Local::D8:
- case X86Local::D9:
- case X86Local::DA:
- case X86Local::DB:
- case X86Local::DC:
- case X86Local::DD:
- case X86Local::DE:
- case X86Local::DF:
- assert(Opcode >= 0xc0 && "Unexpected opcode for an escape opcode");
- assert(Form == X86Local::RawFrm);
- opcodeType = ONEBYTE;
- filter = new ExactFilter(Opcode);
- opcodeToSet = 0xd8 + (Prefix - X86Local::D8);
- break;
- case X86Local::REP:
- case 0:
- opcodeType = ONEBYTE;
- switch (Opcode) {
-#define EXTENSION_TABLE(n) case 0x##n:
- ONE_BYTE_EXTENSION_TABLES
-#undef EXTENSION_TABLE
- switch (Form) {
- default:
- llvm_unreachable("Fell through the cracks of a single-byte "
- "extended opcode");
- case X86Local::MRM0r:
- case X86Local::MRM1r:
- case X86Local::MRM2r:
- case X86Local::MRM3r:
- case X86Local::MRM4r:
- case X86Local::MRM5r:
- case X86Local::MRM6r:
- case X86Local::MRM7r:
- filter = new ExtendedFilter(true, Form - X86Local::MRM0r);
- break;
- case X86Local::MRM0m:
- case X86Local::MRM1m:
- case X86Local::MRM2m:
- case X86Local::MRM3m:
- case X86Local::MRM4m:
- case X86Local::MRM5m:
- case X86Local::MRM6m:
- case X86Local::MRM7m:
- filter = new ExtendedFilter(false, Form - X86Local::MRM0m);
- break;
- MRM_MAPPING
- } // switch (Form)
break;
- case 0xd8:
- case 0xd9:
- case 0xda:
- case 0xdb:
- case 0xdc:
- case 0xdd:
- case 0xde:
- case 0xdf:
- switch (Form) {
- default:
- llvm_unreachable("Unhandled escape opcode form");
- case X86Local::MRM0r:
- case X86Local::MRM1r:
- case X86Local::MRM2r:
- case X86Local::MRM3r:
- case X86Local::MRM4r:
- case X86Local::MRM5r:
- case X86Local::MRM6r:
- case X86Local::MRM7r:
- filter = new ExtendedFilter(true, Form - X86Local::MRM0r);
- break;
- case X86Local::MRM0m:
- case X86Local::MRM1m:
- case X86Local::MRM2m:
- case X86Local::MRM3m:
- case X86Local::MRM4m:
- case X86Local::MRM5m:
- case X86Local::MRM6m:
- case X86Local::MRM7m:
- filter = new ExtendedFilter(false, Form - X86Local::MRM0m);
- break;
- } // switch (Form)
+ case X86Local::MRM0r: case X86Local::MRM1r:
+ case X86Local::MRM2r: case X86Local::MRM3r:
+ case X86Local::MRM4r: case X86Local::MRM5r:
+ case X86Local::MRM6r: case X86Local::MRM7r:
+ filter = new ExtendedFilter(true, Form - X86Local::MRM0r);
break;
- default:
- if (needsModRMForDecode(Form))
- filter = new ModFilter(isRegFormat(Form));
- else
- filter = new DumbFilter();
+ case X86Local::MRM0m: case X86Local::MRM1m:
+ case X86Local::MRM2m: case X86Local::MRM3m:
+ case X86Local::MRM4m: case X86Local::MRM5m:
+ case X86Local::MRM6m: case X86Local::MRM7m:
+ filter = new ExtendedFilter(false, Form - X86Local::MRM0m);
break;
- } // switch (Opcode)
+ MRM_MAPPING
+ } // switch (Form)
+
opcodeToSet = Opcode;
- } // switch (Prefix)
+ break;
+ } // switch (OpMap)
+
+ unsigned AddressSize = 0;
+ switch (AdSize) {
+ case X86Local::AdSize16: AddressSize = 16; break;
+ case X86Local::AdSize32: AddressSize = 32; break;
+ case X86Local::AdSize64: AddressSize = 64; break;
+ }
assert(opcodeType != (OpcodeType)-1 &&
"Opcode type not set");
insnContext(),
currentOpcode,
*filter,
- UID, Is32Bit, IgnoresVEX_L);
+ UID, Is32Bit, IgnoresVEX_L, AddressSize);
} else {
tables.setTableFields(opcodeType,
insnContext(),
opcodeToSet,
*filter,
- UID, Is32Bit, IgnoresVEX_L);
+ UID, Is32Bit, IgnoresVEX_L, AddressSize);
}
delete filter;
#define TYPE(str, type) if (s == str) return type;
OperandType RecognizableInstr::typeFromString(const std::string &s,
- bool isSSE,
bool hasREX_WPrefix,
- bool hasOpSizePrefix) {
- if (isSSE) {
- // For SSE instructions, we ignore the OpSize prefix and force operand
- // sizes.
- TYPE("GR16", TYPE_R16)
- TYPE("GR32", TYPE_R32)
- TYPE("GR64", TYPE_R64)
- }
+ uint8_t OpSize) {
if(hasREX_WPrefix) {
// For instructions with a REX_W prefix, a declared 32-bit register encoding
// is special.
TYPE("GR32", TYPE_R32)
}
- if(!hasOpSizePrefix) {
- // For instructions without an OpSize prefix, a declared 16-bit register or
+ if(OpSize == X86Local::OpSize16) {
+ // For OpSize16 instructions, a declared 16-bit register or
+ // immediate encoding is special.
+ TYPE("GR16", TYPE_Rv)
+ TYPE("i16imm", TYPE_IMMv)
+ } else if(OpSize == X86Local::OpSize32) {
+ // For OpSize32 instructions, a declared 32-bit register or
// immediate encoding is special.
- TYPE("GR16", TYPE_R16)
- TYPE("i16imm", TYPE_IMM16)
+ TYPE("GR32", TYPE_Rv)
}
TYPE("i16mem", TYPE_Mv)
- TYPE("i16imm", TYPE_IMMv)
+ TYPE("i16imm", TYPE_IMM16)
TYPE("i16i8imm", TYPE_IMMv)
- TYPE("GR16", TYPE_Rv)
+ TYPE("GR16", TYPE_R16)
TYPE("i32mem", TYPE_Mv)
TYPE("i32imm", TYPE_IMMv)
TYPE("i32i8imm", TYPE_IMM32)
- TYPE("u32u8imm", TYPE_IMM32)
- TYPE("GR32", TYPE_Rv)
+ TYPE("GR32", TYPE_R32)
TYPE("GR32orGR64", TYPE_R32)
TYPE("i64mem", TYPE_Mv)
TYPE("i64i32imm", TYPE_IMM64)
TYPE("GR64", TYPE_R64)
TYPE("i8mem", TYPE_M8)
TYPE("i8imm", TYPE_IMM8)
+ TYPE("u8imm", TYPE_UIMM8)
TYPE("GR8", TYPE_R8)
TYPE("VR128", TYPE_XMM128)
TYPE("VR128X", TYPE_XMM128)
TYPE("SSECC", TYPE_IMM3)
TYPE("AVXCC", TYPE_IMM5)
TYPE("AVX512RC", TYPE_IMM32)
- TYPE("brtarget", TYPE_RELv)
- TYPE("uncondbrtarget", TYPE_RELv)
+ TYPE("brtarget32", TYPE_RELv)
+ TYPE("brtarget16", TYPE_RELv)
TYPE("brtarget8", TYPE_REL8)
TYPE("f80mem", TYPE_M80FP)
- TYPE("lea32mem", TYPE_LEA)
TYPE("lea64_32mem", TYPE_LEA)
TYPE("lea64mem", TYPE_LEA)
TYPE("VR64", TYPE_MM64)
TYPE("i64imm", TYPE_IMMv)
+ TYPE("anymem", TYPE_M)
TYPE("opaque32mem", TYPE_M1616)
TYPE("opaque48mem", TYPE_M1632)
TYPE("opaque80mem", TYPE_M1664)
TYPE("SEGMENT_REG", TYPE_SEGMENTREG)
TYPE("DEBUG_REG", TYPE_DEBUGREG)
TYPE("CONTROL_REG", TYPE_CONTROLREG)
- TYPE("offset8", TYPE_MOFFS8)
- TYPE("offset16", TYPE_MOFFS16)
- TYPE("offset32", TYPE_MOFFS32)
- TYPE("offset64", TYPE_MOFFS64)
+ TYPE("srcidx8", TYPE_SRCIDX8)
+ TYPE("srcidx16", TYPE_SRCIDX16)
+ TYPE("srcidx32", TYPE_SRCIDX32)
+ TYPE("srcidx64", TYPE_SRCIDX64)
+ TYPE("dstidx8", TYPE_DSTIDX8)
+ TYPE("dstidx16", TYPE_DSTIDX16)
+ TYPE("dstidx32", TYPE_DSTIDX32)
+ TYPE("dstidx64", TYPE_DSTIDX64)
+ TYPE("offset16_8", TYPE_MOFFS8)
+ TYPE("offset16_16", TYPE_MOFFS16)
+ TYPE("offset16_32", TYPE_MOFFS32)
+ TYPE("offset32_8", TYPE_MOFFS8)
+ TYPE("offset32_16", TYPE_MOFFS16)
+ TYPE("offset32_32", TYPE_MOFFS32)
+ TYPE("offset32_64", TYPE_MOFFS64)
+ TYPE("offset64_8", TYPE_MOFFS8)
+ TYPE("offset64_16", TYPE_MOFFS16)
+ TYPE("offset64_32", TYPE_MOFFS32)
+ TYPE("offset64_64", TYPE_MOFFS64)
TYPE("VR256", TYPE_XMM256)
TYPE("VR256X", TYPE_XMM256)
TYPE("VR512", TYPE_XMM512)
TYPE("VK1", TYPE_VK1)
TYPE("VK1WM", TYPE_VK1)
+ TYPE("VK2", TYPE_VK2)
+ TYPE("VK2WM", TYPE_VK2)
+ TYPE("VK4", TYPE_VK4)
+ TYPE("VK4WM", TYPE_VK4)
TYPE("VK8", TYPE_VK8)
TYPE("VK8WM", TYPE_VK8)
TYPE("VK16", TYPE_VK16)
TYPE("VK16WM", TYPE_VK16)
+ TYPE("VK32", TYPE_VK32)
+ TYPE("VK32WM", TYPE_VK32)
+ TYPE("VK64", TYPE_VK64)
+ TYPE("VK64WM", TYPE_VK64)
TYPE("GR16_NOAX", TYPE_Rv)
TYPE("GR32_NOAX", TYPE_Rv)
TYPE("GR64_NOAX", TYPE_R64)
#undef TYPE
#define ENCODING(str, encoding) if (s == str) return encoding;
-OperandEncoding RecognizableInstr::immediateEncodingFromString
- (const std::string &s,
- bool hasOpSizePrefix) {
- if(!hasOpSizePrefix) {
+OperandEncoding
+RecognizableInstr::immediateEncodingFromString(const std::string &s,
+ uint8_t OpSize) {
+ if(OpSize != X86Local::OpSize16) {
// For instructions without an OpSize prefix, a declared 16-bit register or
// immediate encoding is special.
ENCODING("i16imm", ENCODING_IW)
}
ENCODING("i32i8imm", ENCODING_IB)
- ENCODING("u32u8imm", ENCODING_IB)
ENCODING("SSECC", ENCODING_IB)
ENCODING("AVXCC", ENCODING_IB)
ENCODING("AVX512RC", ENCODING_IB)
ENCODING("i64i32imm", ENCODING_ID)
ENCODING("i64i8imm", ENCODING_IB)
ENCODING("i8imm", ENCODING_IB)
+ ENCODING("u8imm", ENCODING_IB)
// This is not a typo. Instructions like BLENDVPD put
// register IDs in 8-bit immediates nowadays.
ENCODING("FR32", ENCODING_IB)
llvm_unreachable("Unhandled immediate encoding");
}
-OperandEncoding RecognizableInstr::rmRegisterEncodingFromString
- (const std::string &s,
- bool hasOpSizePrefix) {
+OperandEncoding
+RecognizableInstr::rmRegisterEncodingFromString(const std::string &s,
+ uint8_t OpSize) {
ENCODING("RST", ENCODING_FP)
ENCODING("GR16", ENCODING_RM)
ENCODING("GR32", ENCODING_RM)
ENCODING("VK1", ENCODING_RM)
ENCODING("VK8", ENCODING_RM)
ENCODING("VK16", ENCODING_RM)
+ ENCODING("VK32", ENCODING_RM)
+ ENCODING("VK64", ENCODING_RM)
errs() << "Unhandled R/M register encoding " << s << "\n";
llvm_unreachable("Unhandled R/M register encoding");
}
-OperandEncoding RecognizableInstr::roRegisterEncodingFromString
- (const std::string &s,
- bool hasOpSizePrefix) {
+OperandEncoding
+RecognizableInstr::roRegisterEncodingFromString(const std::string &s,
+ uint8_t OpSize) {
ENCODING("GR16", ENCODING_REG)
ENCODING("GR32", ENCODING_REG)
ENCODING("GR32orGR64", ENCODING_REG)
ENCODING("FR32X", ENCODING_REG)
ENCODING("VR512", ENCODING_REG)
ENCODING("VK1", ENCODING_REG)
+ ENCODING("VK2", ENCODING_REG)
+ ENCODING("VK4", ENCODING_REG)
ENCODING("VK8", ENCODING_REG)
ENCODING("VK16", ENCODING_REG)
+ ENCODING("VK32", ENCODING_REG)
+ ENCODING("VK64", ENCODING_REG)
ENCODING("VK1WM", ENCODING_REG)
ENCODING("VK8WM", ENCODING_REG)
ENCODING("VK16WM", ENCODING_REG)
llvm_unreachable("Unhandled reg/opcode register encoding");
}
-OperandEncoding RecognizableInstr::vvvvRegisterEncodingFromString
- (const std::string &s,
- bool hasOpSizePrefix) {
+OperandEncoding
+RecognizableInstr::vvvvRegisterEncodingFromString(const std::string &s,
+ uint8_t OpSize) {
ENCODING("GR32", ENCODING_VVVV)
ENCODING("GR64", ENCODING_VVVV)
ENCODING("FR32", ENCODING_VVVV)
ENCODING("VR256X", ENCODING_VVVV)
ENCODING("VR512", ENCODING_VVVV)
ENCODING("VK1", ENCODING_VVVV)
+ ENCODING("VK2", ENCODING_VVVV)
+ ENCODING("VK4", ENCODING_VVVV)
ENCODING("VK8", ENCODING_VVVV)
ENCODING("VK16", ENCODING_VVVV)
+ ENCODING("VK32", ENCODING_VVVV)
+ ENCODING("VK64", ENCODING_VVVV)
errs() << "Unhandled VEX.vvvv register encoding " << s << "\n";
llvm_unreachable("Unhandled VEX.vvvv register encoding");
}
-OperandEncoding RecognizableInstr::writemaskRegisterEncodingFromString
- (const std::string &s,
- bool hasOpSizePrefix) {
+OperandEncoding
+RecognizableInstr::writemaskRegisterEncodingFromString(const std::string &s,
+ uint8_t OpSize) {
ENCODING("VK1WM", ENCODING_WRITEMASK)
+ ENCODING("VK2WM", ENCODING_WRITEMASK)
+ ENCODING("VK4WM", ENCODING_WRITEMASK)
ENCODING("VK8WM", ENCODING_WRITEMASK)
ENCODING("VK16WM", ENCODING_WRITEMASK)
+ ENCODING("VK32WM", ENCODING_WRITEMASK)
+ ENCODING("VK64WM", ENCODING_WRITEMASK)
errs() << "Unhandled mask register encoding " << s << "\n";
llvm_unreachable("Unhandled mask register encoding");
}
-OperandEncoding RecognizableInstr::memoryEncodingFromString
- (const std::string &s,
- bool hasOpSizePrefix) {
+OperandEncoding
+RecognizableInstr::memoryEncodingFromString(const std::string &s,
+ uint8_t OpSize) {
ENCODING("i16mem", ENCODING_RM)
ENCODING("i32mem", ENCODING_RM)
ENCODING("i64mem", ENCODING_RM)
ENCODING("i256mem", ENCODING_RM)
ENCODING("i512mem", ENCODING_RM)
ENCODING("f80mem", ENCODING_RM)
- ENCODING("lea32mem", ENCODING_RM)
ENCODING("lea64_32mem", ENCODING_RM)
ENCODING("lea64mem", ENCODING_RM)
+ ENCODING("anymem", ENCODING_RM)
ENCODING("opaque32mem", ENCODING_RM)
ENCODING("opaque48mem", ENCODING_RM)
ENCODING("opaque80mem", ENCODING_RM)
llvm_unreachable("Unhandled memory encoding");
}
-OperandEncoding RecognizableInstr::relocationEncodingFromString
- (const std::string &s,
- bool hasOpSizePrefix) {
- if(!hasOpSizePrefix) {
+OperandEncoding
+RecognizableInstr::relocationEncodingFromString(const std::string &s,
+ uint8_t OpSize) {
+ if(OpSize != X86Local::OpSize16) {
// For instructions without an OpSize prefix, a declared 16-bit register or
// immediate encoding is special.
ENCODING("i16imm", ENCODING_IW)
ENCODING("i64i32imm", ENCODING_ID)
ENCODING("i64i8imm", ENCODING_IB)
ENCODING("i8imm", ENCODING_IB)
+ ENCODING("u8imm", ENCODING_IB)
ENCODING("i64i32imm_pcrel", ENCODING_ID)
ENCODING("i16imm_pcrel", ENCODING_IW)
ENCODING("i32imm_pcrel", ENCODING_ID)
- ENCODING("brtarget", ENCODING_Iv)
+ ENCODING("brtarget32", ENCODING_Iv)
+ ENCODING("brtarget16", ENCODING_Iv)
ENCODING("brtarget8", ENCODING_IB)
ENCODING("i64imm", ENCODING_IO)
- ENCODING("offset8", ENCODING_Ia)
- ENCODING("offset16", ENCODING_Ia)
- ENCODING("offset32", ENCODING_Ia)
- ENCODING("offset64", ENCODING_Ia)
+ ENCODING("offset16_8", ENCODING_Ia)
+ ENCODING("offset16_16", ENCODING_Ia)
+ ENCODING("offset16_32", ENCODING_Ia)
+ ENCODING("offset32_8", ENCODING_Ia)
+ ENCODING("offset32_16", ENCODING_Ia)
+ ENCODING("offset32_32", ENCODING_Ia)
+ ENCODING("offset32_64", ENCODING_Ia)
+ ENCODING("offset64_8", ENCODING_Ia)
+ ENCODING("offset64_16", ENCODING_Ia)
+ ENCODING("offset64_32", ENCODING_Ia)
+ ENCODING("offset64_64", ENCODING_Ia)
+ ENCODING("srcidx8", ENCODING_SI)
+ ENCODING("srcidx16", ENCODING_SI)
+ ENCODING("srcidx32", ENCODING_SI)
+ ENCODING("srcidx64", ENCODING_SI)
+ ENCODING("dstidx8", ENCODING_DI)
+ ENCODING("dstidx16", ENCODING_DI)
+ ENCODING("dstidx32", ENCODING_DI)
+ ENCODING("dstidx64", ENCODING_DI)
errs() << "Unhandled relocation encoding " << s << "\n";
llvm_unreachable("Unhandled relocation encoding");
}
-OperandEncoding RecognizableInstr::opcodeModifierEncodingFromString
- (const std::string &s,
- bool hasOpSizePrefix) {
+OperandEncoding
+RecognizableInstr::opcodeModifierEncodingFromString(const std::string &s,
+ uint8_t OpSize) {
ENCODING("GR32", ENCODING_Rv)
ENCODING("GR64", ENCODING_RO)
ENCODING("GR16", ENCODING_Rv)