author | Bill Schmidt <wschmidt@linux.vnet.ibm.com> | |
Tue, 27 May 2014 15:57:51 +0000 (15:57 +0000) | ||
committer | Bill Schmidt <wschmidt@linux.vnet.ibm.com> | |
Tue, 27 May 2014 15:57:51 +0000 (15:57 +0000) | ||
commit | 3f01f5296ec2d146f92bcc479a5bade9e898fc40 | |
tree | 49fd56349563075e6e8deb968aff93337a87565c | tree | snapshot (tar.xz tar.gz zip) |
parent | 61e341e0bfcc83ec865fe763759e66ab3c2feba5 | commit | diff |
[PATCH] Correct type used for VADD_SPLAT optimization on PowerPC
In PPCISelLowering.cpp: PPCTargetLowering::LowerBUILD_VECTOR(), there
is an optimization for certain patterns to generate one or two vector
splats followed by a vector add or subtract. This operation is
represented by a VADD_SPLAT in the selection DAG. Prior to this
patch, it was possible for the VADD_SPLAT to be assigned the wrong
data type, causing incorrect code generation. This patch corrects the
problem.
Specifically, the code previously assigned the value type of the
BUILD_VECTOR node to the newly generated VADD_SPLAT node. This is
correct much of the time, but not always. The problem is that the
call to isConstantSplat() may return a SplatBitSize that is not the
same as the number of bits in the original element vector type. The
correct type to assign is a vector type with the same element bit size
as SplatBitSize.
The included test case shows an example of this, where the
BUILD_VECTOR node has a type of v16i8. The vector to be built is {0,
16, 0, 16, 0, 16, 0, 16, 0, 16, 0, 16, 0, 16, 0, 16}. isConstantSplat
detects that we can generate a splat of 16 for type v8i16, which is
the type we must assign to the VADD_SPLAT node. If we do not, we
generate a vspltisb of 8 and a vaddubm, which generates the incorrect
result {16, 16, 16, 16, 16, 16, 16, 16, 16, 16, 16, 16, 16, 16, 16,
16}. The correct code generation is a vspltish of 8 and a vadduhm.
This patch also corrected code generation for
CodeGen/PowerPC/2008-07-10-SplatMiscompile.ll, which had been marked
as an XFAIL, so we can remove the XFAIL from the test case.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209662 91177308-0d34-0410-b5e6-96231b3b80d8
In PPCISelLowering.cpp: PPCTargetLowering::LowerBUILD_VECTOR(), there
is an optimization for certain patterns to generate one or two vector
splats followed by a vector add or subtract. This operation is
represented by a VADD_SPLAT in the selection DAG. Prior to this
patch, it was possible for the VADD_SPLAT to be assigned the wrong
data type, causing incorrect code generation. This patch corrects the
problem.
Specifically, the code previously assigned the value type of the
BUILD_VECTOR node to the newly generated VADD_SPLAT node. This is
correct much of the time, but not always. The problem is that the
call to isConstantSplat() may return a SplatBitSize that is not the
same as the number of bits in the original element vector type. The
correct type to assign is a vector type with the same element bit size
as SplatBitSize.
The included test case shows an example of this, where the
BUILD_VECTOR node has a type of v16i8. The vector to be built is {0,
16, 0, 16, 0, 16, 0, 16, 0, 16, 0, 16, 0, 16, 0, 16}. isConstantSplat
detects that we can generate a splat of 16 for type v8i16, which is
the type we must assign to the VADD_SPLAT node. If we do not, we
generate a vspltisb of 8 and a vaddubm, which generates the incorrect
result {16, 16, 16, 16, 16, 16, 16, 16, 16, 16, 16, 16, 16, 16, 16,
16}. The correct code generation is a vspltish of 8 and a vadduhm.
This patch also corrected code generation for
CodeGen/PowerPC/2008-07-10-SplatMiscompile.ll, which had been marked
as an XFAIL, so we can remove the XFAIL from the test case.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209662 91177308-0d34-0410-b5e6-96231b3b80d8
lib/Target/PowerPC/PPCISelLowering.cpp | diff | blob | history | |
test/CodeGen/PowerPC/2008-07-10-SplatMiscompile.ll | diff | blob | history | |
test/CodeGen/PowerPC/splat-bug.ll | [new file with mode: 0644] | blob |