author | Rafael Espindola <rafael.espindola@gmail.com> | |
Wed, 31 Dec 2014 17:19:34 +0000 (17:19 +0000) | ||
committer | Rafael Espindola <rafael.espindola@gmail.com> | |
Wed, 31 Dec 2014 17:19:34 +0000 (17:19 +0000) | ||
commit | 8093abb7454e5419e121bd105487dfa231f35b37 | |
tree | 5284288d6b5cd44998a2d322bcbec27cdb263f52 | tree | snapshot (tar.xz tar.gz zip) |
parent | f5943bd9a9749ff73256634d14c258264b72c7dc | commit | diff |
Add r224985 back with a fix.
The issues was that AArch64 has additional restrictions on when local
relocations can be used. We have to take those into consideration when
deciding to put a L symbol in the symbol table or not.
Original message:
Remove doesSectionRequireSymbols.
In an assembly expression like
bar:
.long L0 + 1
the intended semantics is that bar will contain a pointer one byte past L0.
In sections that are merged by content (strings, 4 byte constants, etc), a
single position in the section doesn't give the linker enough information.
For example, it would not be able to tell a relocation must point to the
end of a string, since that would look just like the start of the next.
The solution used in ELF to use relocation with symbols if there is a non-zero
addend.
In MachO before this patch we would just keep all symbols in some sections.
This would miss some cases (only cstrings on x86_64 were implemented) and was
inefficient since most relocations have an addend of 0 and can be represented
without the symbol.
This patch implements the non-zero addend logic for MachO too.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225048 91177308-0d34-0410-b5e6-96231b3b80d8
The issues was that AArch64 has additional restrictions on when local
relocations can be used. We have to take those into consideration when
deciding to put a L symbol in the symbol table or not.
Original message:
Remove doesSectionRequireSymbols.
In an assembly expression like
bar:
.long L0 + 1
the intended semantics is that bar will contain a pointer one byte past L0.
In sections that are merged by content (strings, 4 byte constants, etc), a
single position in the section doesn't give the linker enough information.
For example, it would not be able to tell a relocation must point to the
end of a string, since that would look just like the start of the next.
The solution used in ELF to use relocation with symbols if there is a non-zero
addend.
In MachO before this patch we would just keep all symbols in some sections.
This would miss some cases (only cstrings on x86_64 were implemented) and was
inefficient since most relocations have an addend of 0 and can be represented
without the symbol.
This patch implements the non-zero addend logic for MachO too.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225048 91177308-0d34-0410-b5e6-96231b3b80d8
19 files changed: