]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/commit
Change how dbg_value sdnodes are converted into machine instructions. Their placement...
authorEvan Cheng <evan.cheng@apple.com>
Thu, 25 Mar 2010 01:38:16 +0000 (01:38 +0000)
committerEvan Cheng <evan.cheng@apple.com>
Thu, 25 Mar 2010 01:38:16 +0000 (01:38 +0000)
commitbfcb3051899b7141a946d769fcf6e8a8453bc530
tree558cf199676b89de5e3152b585acf3e13c51544b
parent7c3d45a03e64ac1b5b2ecdb7153989fd7cebfd2c
Change how dbg_value sdnodes are converted into machine instructions. Their placement should be determined by the relative order of incoming llvm instructions. The scheduler will now use the SDNode ordering information to determine where to insert them. A dbg_value instruction is inserted after the instruction with the last highest source order and before the instruction with the next highest source order. It will optimize the placement by inserting right after the instruction that produces the value if they have consecutive order numbers.

Here is a theoretical example that illustrates why the placement is important.

tmp1 =
store tmp1 -> x
...
tmp2 = add ...
...
call
...
store tmp2 -> x

Now mem2reg comes along:

tmp1 =
dbg_value (tmp1 -> x)
...
tmp2 = add ...
...
call
...
dbg_value (tmp2 -> x)

When the debugger examine the value of x after the add instruction but before the call, it should have the value of tmp1.

Furthermore, for dbg_value's that reference constants, they should not be emitted at the beginning of the block (since they do not have "producers").

This patch also cleans up how SDISel manages DbgValue nodes. It allow a SDNode to be referenced by multiple SDDbgValue nodes. When a SDNode is deleted, it uses the information to find the SDDbgValues and invalidate them. They are not deleted until the corresponding SelectionDAG is destroyed.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@99469 91177308-0d34-0410-b5e6-96231b3b80d8
include/llvm/CodeGen/MachineOperand.h
include/llvm/CodeGen/SelectionDAG.h
lib/CodeGen/SelectionDAG/InstrEmitter.cpp
lib/CodeGen/SelectionDAG/InstrEmitter.h
lib/CodeGen/SelectionDAG/SDNodeDbgValue.h
lib/CodeGen/SelectionDAG/ScheduleDAGSDNodes.cpp
lib/CodeGen/SelectionDAG/SelectionDAG.cpp
lib/CodeGen/SelectionDAG/SelectionDAGBuilder.cpp