]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/commit
[SROA] Fix two total think-os in r225061 that should have been caught on
authorChandler Carruth <chandlerc@gmail.com>
Thu, 1 Jan 2015 23:26:16 +0000 (23:26 +0000)
committerChandler Carruth <chandlerc@gmail.com>
Thu, 1 Jan 2015 23:26:16 +0000 (23:26 +0000)
commited3f2c6761806946c94431e7628cc6a59fe058f8
treec74a7b812dc5cf036d7b0f8d2298c6454808383f
parent32399786f9d34ae55a1dbebcf7be4c630f51503f
[SROA] Fix two total think-os in r225061 that should have been caught on
a +asserts bootstrap, but my bootstrap had asserts off. Oops.

Anyways, in some places it is reasonable to cast (as a sanity check) the
pointer operand to a load or store to an instruction within SROA --
namely when the pointer operand is expected to be derived from an
alloca, and thus always an instruction. However, the pre-splitting code
also deals with loads and stores to non-alloca pointers and there we
need to just use the Value*. Nothing about the code relied on the
instruction cast, it was only there essentially as an invariant
assertion. Remove the two that don't actually hold.

This should fix the proximate issue in PR22080, but I'm also doing an
asserts bootstrap myself to see if there are other issues lurking.

I'll craft a reduced test case in a moment, but I wanted to get the tree
healthy as quickly as possible.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225068 91177308-0d34-0410-b5e6-96231b3b80d8
lib/Transforms/Scalar/SROA.cpp