summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 4dc6aa2)
raw | patch | inline | side by side (parent: 4dc6aa2)
author | Reid Kleckner <reid@kleckner.net> | |
Thu, 13 Nov 2014 23:32:52 +0000 (23:32 +0000) | ||
committer | Reid Kleckner <reid@kleckner.net> | |
Thu, 13 Nov 2014 23:32:52 +0000 (23:32 +0000) |
Fix for LLI failure on Windows\X86: http://llvm.org/PR5053
LLI.exe crashes on Windows\X86 when single precession floating point
intrinsics like the following are used: acos, asin, atan, atan2, ceil,
copysign, cos, cosh, exp, floor, fmin, fmax, fmod, log, pow, sin, sinh,
sqrt, tan, tanh
The above intrinsics are defined as inline-expansions in math.h, and are
not exported by msvcr120.dll (Win32 API GetProcAddress returns null).
For an FREM instruction, the JIT compiler generates a call to a stub for
the fmodf() intrinsic, and adds a relocation to fixup at load time. The
loader searches the libraries for the function, but fails because the
symbol is not exported. So, the call target remains NULL and the
execution crashes.
Since the math functions are loaded at JIT/runtime, the JIT can patch
CALL instruction directly instead of the searching the libraries'
exported symbols. However, this fix caused build failures due to
unresolved symbols like _fmodf at link time.
Therefore, the current fix defines helper functions in the Runtime
link/load library to perform the above operations. The address of these
helper functions are used to patch up the CALL instruction at load time.
Reviewers: lhames, rnk
Reviewed By: rnk
Differential Revision: http://reviews.llvm.org/D5387
Patch by Swaroop Sridhar!
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@221947 91177308-0d34-0410-b5e6-96231b3b80d8
LLI.exe crashes on Windows\X86 when single precession floating point
intrinsics like the following are used: acos, asin, atan, atan2, ceil,
copysign, cos, cosh, exp, floor, fmin, fmax, fmod, log, pow, sin, sinh,
sqrt, tan, tanh
The above intrinsics are defined as inline-expansions in math.h, and are
not exported by msvcr120.dll (Win32 API GetProcAddress returns null).
For an FREM instruction, the JIT compiler generates a call to a stub for
the fmodf() intrinsic, and adds a relocation to fixup at load time. The
loader searches the libraries for the function, but fails because the
symbol is not exported. So, the call target remains NULL and the
execution crashes.
Since the math functions are loaded at JIT/runtime, the JIT can patch
CALL instruction directly instead of the searching the libraries'
exported symbols. However, this fix caused build failures due to
unresolved symbols like _fmodf at link time.
Therefore, the current fix defines helper functions in the Runtime
link/load library to perform the above operations. The address of these
helper functions are used to patch up the CALL instruction at load time.
Reviewers: lhames, rnk
Reviewed By: rnk
Differential Revision: http://reviews.llvm.org/D5387
Patch by Swaroop Sridhar!
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@221947 91177308-0d34-0410-b5e6-96231b3b80d8
lib/Support/Windows/DynamicLibrary.inc | patch | blob | history | |
lib/Support/Windows/explicit_symbols.inc | patch | blob | history | |
test/ExecutionEngine/frem.ll | [new file with mode: 0644] | patch | blob |
index 241f95d55a97ce774862933134af7403f9aace3f..79d5f79afa9722c7215d155c265e9432e42afcba 100644 (file)
extern "C" { extern void *SYM; }
#define EXPLICIT_SYMBOL2(SYMFROM, SYMTO) EXPLICIT_SYMBOL(SYMTO)
+#ifdef _M_IX86
+// Win32 on x86 implements certain single-precision math functions as macros.
+// These functions are not exported by the DLL, but will still be needed
+// for symbol-resolution by the JIT loader. Therefore, this Support libray
+// provides helper functions with the same implementation.
+
+#define INLINE_DEF_SYMBOL1(TYP, SYM) \
+ extern "C" TYP inline_##SYM(TYP _X) { return SYM(_X); }
+#define INLINE_DEF_SYMBOL2(TYP, SYM) \
+ extern "C" TYP inline_##SYM(TYP _X, TYP _Y) { return SYM(_X, _Y); }
+#endif
+
#include "explicit_symbols.inc"
#undef EXPLICIT_SYMBOL
#undef EXPLICIT_SYMBOL2
+#undef INLINE_DEF_SYMBOL1
+#undef INLINE_DEF_SYMBOL2
void* DynamicLibrary::SearchForAddressOfSymbol(const char* symbolName) {
SmartScopedLock<true> Lock(*SymbolsMutex);
}
}
- #define EXPLICIT_SYMBOL(SYM) \
- if (!strcmp(symbolName, #SYM)) return (void*)&SYM;
- #define EXPLICIT_SYMBOL2(SYMFROM, SYMTO) \
- if (!strcmp(symbolName, #SYMFROM)) return (void*)&SYMTO;
+#define EXPLICIT_SYMBOL(SYM) \
+ if (!strcmp(symbolName, #SYM)) \
+ return (void *)&SYM;
+#define EXPLICIT_SYMBOL2(SYMFROM, SYMTO) \
+ if (!strcmp(symbolName, #SYMFROM)) \
+ return (void *)&SYMTO;
+
+#ifdef _M_IX86
+#define INLINE_DEF_SYMBOL1(TYP, SYM) \
+ if (!strcmp(symbolName, #SYM)) \
+ return (void *)&inline_##SYM;
+#define INLINE_DEF_SYMBOL2(TYP, SYM) INLINE_DEF_SYMBOL1(TYP, SYM)
+#endif
{
- #include "explicit_symbols.inc"
+#include "explicit_symbols.inc"
}
- #undef EXPLICIT_SYMBOL
- #undef EXPLICIT_SYMBOL2
+#undef EXPLICIT_SYMBOL
+#undef EXPLICIT_SYMBOL2
+#undef INLINE_DEF_SYMBOL1
+#undef INLINE_DEF_SYMBOL2
return 0;
}
-
void *DynamicLibrary::getAddressOfSymbol(const char *symbolName) {
if (!isValid())
return NULL;
return (void *)(intptr_t)GetProcAddress((HMODULE)Data, symbolName);
}
-
}
index 379645d2ff6074faab2d57315c7409879107091c..5f3818919d203ea07f0c85e7b2efce36e7d18c39 100644 (file)
/* msvcrt */
#if defined(_MSC_VER)
EXPLICIT_SYMBOL2(alloca, _alloca_probe)
+
+#ifdef _M_IX86
+#define INLINE_DEF_FLOAT_SYMBOL(SYM, ARGC) INLINE_DEF_SYMBOL##ARGC(float, SYM)
+ INLINE_DEF_FLOAT_SYMBOL(acosf, 1)
+ INLINE_DEF_FLOAT_SYMBOL(asinf, 1)
+ INLINE_DEF_FLOAT_SYMBOL(atanf, 1)
+ INLINE_DEF_FLOAT_SYMBOL(atan2f, 2)
+ INLINE_DEF_FLOAT_SYMBOL(ceilf, 1)
+#if (_MSC_VER==1800)
+ INLINE_DEF_FLOAT_SYMBOL(copysignf, 2)
+#endif
+ INLINE_DEF_FLOAT_SYMBOL(cosf, 1)
+ INLINE_DEF_FLOAT_SYMBOL(coshf, 1)
+ INLINE_DEF_FLOAT_SYMBOL(expf, 1)
+ INLINE_DEF_FLOAT_SYMBOL(floorf, 1)
+ INLINE_DEF_FLOAT_SYMBOL(fminf, 2)
+ INLINE_DEF_FLOAT_SYMBOL(fmaxf, 2)
+ INLINE_DEF_FLOAT_SYMBOL(fmodf, 2)
+ INLINE_DEF_FLOAT_SYMBOL(logf, 1)
+ INLINE_DEF_FLOAT_SYMBOL(powf, 2)
+ INLINE_DEF_FLOAT_SYMBOL(sinf, 1)
+ INLINE_DEF_FLOAT_SYMBOL(sinhf, 1)
+ INLINE_DEF_FLOAT_SYMBOL(sqrtf, 1)
+ INLINE_DEF_FLOAT_SYMBOL(tanf, 1)
+ INLINE_DEF_FLOAT_SYMBOL(tanhf, 1)
+#undef INLINE_DEF_FLOAT_SYMBOL
+#endif
+
#endif
diff --git a/test/ExecutionEngine/frem.ll b/test/ExecutionEngine/frem.ll
--- /dev/null
@@ -0,0 +1,20 @@
+; LLI.exe used to crash on Windows\X86 when certain single precession
+; floating point intrinsics (defined as macros) are used.
+; This unit test guards against the failure.
+;
+; RUN: %lli %s | FileCheck %s
+
+@flt = internal global float 12.0e+0
+@str = internal constant [18 x i8] c"Double value: %f\0A\00"
+
+declare i32 @printf(i8* nocapture, ...) nounwind
+
+define i32 @main() {
+ %flt = load float* @flt
+ %float2 = frem float %flt, 5.0
+ %double1 = fpext float %float2 to double
+ call i32 (i8*, ...)* @printf(i8* getelementptr ([18 x i8]* @str, i32 0, i64 0), double %double1)
+ ret i32 0
+}
+
+; CHECK: Double value: 2.0