summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 5723359)
raw | patch | inline | side by side (parent: 5723359)
author | Chris Lattner <sabre@nondot.org> | |
Mon, 20 Dec 2010 07:45:28 +0000 (07:45 +0000) | ||
committer | Chris Lattner <sabre@nondot.org> | |
Mon, 20 Dec 2010 07:45:28 +0000 (07:45 +0000) |
argument. The generated alloca has to have at least the alignment of the
byval, if not, the client may be making assumptions that the new alloca won't
satisfy.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@122234 91177308-0d34-0410-b5e6-96231b3b80d8
byval, if not, the client may be making assumptions that the new alloca won't
satisfy.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@122234 91177308-0d34-0410-b5e6-96231b3b80d8
lib/Transforms/Utils/InlineFunction.cpp | patch | blob | history | |
test/Transforms/Inline/byval.ll | patch | blob | history |
index 5cf0fed19f478626724fa128fee1ff870844cc56..3f50ccdaf5ad77c5637d30249d2088cc00099591 100644 (file)
CalledFunc->isDeclaration() || // call, or call to a vararg function!
CalledFunc->getFunctionType()->isVarArg()) return false;
-
// If the call to the callee is not a tail call, we must clear the 'tail'
// flags on any calls that we inline.
bool MustClearTailCallFlags =
if (CalledFunc->paramHasAttr(ArgNo+1, Attribute::ByVal) &&
!CalledFunc->onlyReadsMemory()) {
const Type *AggTy = cast<PointerType>(I->getType())->getElementType();
- const Type *VoidPtrTy =
- Type::getInt8PtrTy(Context);
+ const Type *VoidPtrTy = Type::getInt8PtrTy(Context);
// Create the alloca. If we have TargetData, use nice alignment.
unsigned Align = 1;
- if (IFI.TD) Align = IFI.TD->getPrefTypeAlignment(AggTy);
- Value *NewAlloca = new AllocaInst(AggTy, 0, Align,
- I->getName(),
+ if (IFI.TD)
+ Align = IFI.TD->getPrefTypeAlignment(AggTy);
+
+ // If the byval had an alignment specified, we *must* use at least that
+ // alignment, as it is required by the byval argument (and uses of the
+ // pointer inside the callee).
+ Align = std::max(Align, CalledFunc->getParamAlignment(ArgNo+1));
+
+ Value *NewAlloca = new AllocaInst(AggTy, 0, Align, I->getName(),
&*Caller->begin()->begin());
// Emit a memcpy.
const Type *Tys[3] = {VoidPtrTy, VoidPtrTy, Type::getInt64Ty(Context)};
index 00686341cb279eabd02b89123cb9d4bd5f674cf1..da0beab9dc7a762edac46e171bb5b365c98fc432 100644 (file)
; CHECK-NOT: call void @llvm.memcpy
; CHECK: ret i32
}
+
+
+; Inlining a byval with an explicit alignment needs to use *at least* that
+; alignment on the generated alloca.
+; PR8769
+declare void @g3(%struct.ss* %p)
+
+define internal void @f3(%struct.ss* byval align 64 %b) nounwind {
+ call void @g3(%struct.ss* %b) ;; Could make alignment assumptions!
+ ret void
+}
+
+define void @test3() nounwind {
+entry:
+ %S = alloca %struct.ss, align 1 ;; May not be aligned.
+ call void @f3( %struct.ss* byval align 64 %S) nounwind
+ ret void
+; CHECK: @test3()
+; CHECK: %b = alloca %struct.ss, align 64
+; CHECK: %S = alloca %struct.ss
+; CHECK: call void @llvm.memcpy
+; CHECK: call void @g3(%struct.ss* %b)
+; CHECK: ret void
+}