summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 2dade43)
raw | patch | inline | side by side (parent: 2dade43)
author | Chris Bieneman <beanz@apple.com> | |
Tue, 15 Jul 2014 17:18:41 +0000 (17:18 +0000) | ||
committer | Chris Bieneman <beanz@apple.com> | |
Tue, 15 Jul 2014 17:18:41 +0000 (17:18 +0000) |
The coalescer is very aggressive at propagating constraints on the register classes, and the register allocator doesn’t know how to split sub-registers later to recover. This patch provides an escape valve for targets that encounter this problem to limit coalescing.
This patch also implements such for ARM to lower register pressure when using lots of large register classes. This works around PR18825.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@213078 91177308-0d34-0410-b5e6-96231b3b80d8
This patch also implements such for ARM to lower register pressure when using lots of large register classes. This works around PR18825.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@213078 91177308-0d34-0410-b5e6-96231b3b80d8
include/llvm/Target/TargetSubtargetInfo.h | patch | blob | history | |
lib/CodeGen/RegisterCoalescer.cpp | patch | blob | history | |
lib/Target/ARM/ARMMachineFunctionInfo.h | patch | blob | history | |
lib/Target/ARM/ARMSubtarget.cpp | patch | blob | history | |
lib/Target/ARM/ARMSubtarget.h | patch | blob | history | |
test/CodeGen/ARM/out-of-registers.ll | [new file with mode: 0644] | patch | blob |
test/CodeGen/ARM/vector-spilling.ll | [new file with mode: 0644] | patch | blob |
test/CodeGen/ARM/vldm-sched-a9.ll | patch | blob | history |
index bbb83efc780bc25049f82334af2051d9ec220df8..e2aea45f4c1d8d2a7c050945138960f398543250 100644 (file)
/// \brief Reset the features for the subtarget.
virtual void resetSubtargetFeatures(const MachineFunction *MF) { }
+
+ /// \brief SrcRC and DstRC will be morphed into NewRC if this returns true.
+ virtual bool shouldCoalesce(MachineInstr *MI,
+ const TargetRegisterClass *SrcRC,
+ unsigned SubReg,
+ const TargetRegisterClass *DstRC,
+ unsigned DstSubReg,
+ const TargetRegisterClass *NewRC) const
+ { return true; }
+
};
} // End llvm namespace
index 5aaeb874d68cbf8df74113d6488a86ab8ce6e684..0bda4c7998717a419428987128081d6fd4ea88cf 100644 (file)
return false;
}
+ if (CP.getNewRC()) {
+ const TargetSubtargetInfo &ST = TM->getSubtarget<TargetSubtargetInfo>();
+ auto SrcRC = MRI->getRegClass(CP.getSrcReg());
+ auto DstRC = MRI->getRegClass(CP.getDstReg());
+ unsigned SrcIdx = CP.getSrcIdx();
+ unsigned DstIdx = CP.getDstIdx();
+ if (CP.isFlipped()) {
+ std::swap(SrcIdx, DstIdx);
+ std::swap(SrcRC, DstRC);
+ }
+ if (!ST.shouldCoalesce(CopyMI, SrcRC, SrcIdx, DstRC, DstIdx,
+ CP.getNewRC())) {
+ DEBUG(dbgs() << "\tSubtarget bailed on coalescing.\n");
+ return false;
+ }
+ }
+
// Dead code elimination. This really should be handled by MachineDCE, but
// sometimes dead copies slip through, and we can't generate invalid live
// ranges.
index 44a9e3495b90169304c5b603bb967d8997b76bd4..d3fabc3ebb0401e4e0648eed19a3fff9fdc8bee6 100644 (file)
#include "llvm/CodeGen/MachineFunction.h"
#include "llvm/Target/TargetMachine.h"
#include "llvm/Target/TargetRegisterInfo.h"
+#include "llvm/ADT/DenseMap.h"
namespace llvm {
/// being passed on the stack
unsigned ArgumentStackSize;
+ /// CoalescedWeights - mapping of basic blocks to the rolling counter of
+ /// coalesced weights.
+ DenseMap<const MachineBasicBlock*, unsigned> CoalescedWeights;
+
public:
ARMFunctionInfo() :
isThumb(false),
else
return -1U;
}
+
+ DenseMap<const MachineBasicBlock*, unsigned>::iterator getCoalescedWeight(
+ MachineBasicBlock* MBB) {
+ auto It = CoalescedWeights.find(MBB);
+ if (It == CoalescedWeights.end()) {
+ It = CoalescedWeights.insert(std::make_pair(MBB, 0)).first;
+ }
+ return It;
+ }
};
} // End llvm namespace
index f21413b33ef3190549fbc96635e5f943a033aff8..0c6ff529653f2161bc29ad9b5f5d280c0398a36b 100644 (file)
#include "ARMJITInfo.h"
#include "ARMSelectionDAGInfo.h"
#include "ARMSubtarget.h"
+#include "ARMMachineFunctionInfo.h"
#include "Thumb1FrameLowering.h"
#include "Thumb1InstrInfo.h"
#include "Thumb2InstrInfo.h"
#include "llvm/Support/CommandLine.h"
#include "llvm/Target/TargetInstrInfo.h"
#include "llvm/Target/TargetOptions.h"
+#include "llvm/Target/TargetRegisterInfo.h"
+#include "llvm/CodeGen/MachineRegisterInfo.h"
using namespace llvm;
!MF.getFunction()->getAttributes().hasAttribute(
AttributeSet::FunctionIndex, Attribute::MinSize));
}
+
+bool ARMSubtarget::shouldCoalesce(MachineInstr *MI,
+ const TargetRegisterClass *SrcRC,
+ unsigned SubReg,
+ const TargetRegisterClass *DstRC,
+ unsigned DstSubReg,
+ const TargetRegisterClass *NewRC) const {
+ auto MBB = MI->getParent();
+ auto MF = MBB->getParent();
+ const MachineRegisterInfo &MRI = MF->getRegInfo();
+ // If not copying into a sub-register this should be ok because we shouldn't
+ // need to split the reg.
+ if (!DstSubReg)
+ return true;
+ // Small registers don't frequently cause a problem, so we can coalesce them.
+ if (NewRC->getSize() < 32 && DstRC->getSize() < 32 && SrcRC->getSize() < 32)
+ return true;
+
+ auto NewRCWeight =
+ MRI.getTargetRegisterInfo()->getRegClassWeight(NewRC);
+ auto SrcRCWeight =
+ MRI.getTargetRegisterInfo()->getRegClassWeight(SrcRC);
+ auto DstRCWeight =
+ MRI.getTargetRegisterInfo()->getRegClassWeight(DstRC);
+ // If the source register class is more expensive than the destination, the
+ // coalescing is probably profitable.
+ if (SrcRCWeight.RegWeight > NewRCWeight.RegWeight)
+ return true;
+ if (DstRCWeight.RegWeight > NewRCWeight.RegWeight)
+ return true;
+
+ // If the register allocator isn't constrained, we can always allow coalescing
+ // unfortunately we don't know yet if we will be constrained.
+ // The goal of this heuristic is to restrict how many expensive registers
+ // we allow to coalesce in a given basic block.
+ auto AFI = MF->getInfo<ARMFunctionInfo>();
+ auto It = AFI->getCoalescedWeight(MBB);
+
+ DEBUG(dbgs() << "\tARM::shouldCoalesce - Coalesced Weight: " << It->second << "\n");
+ DEBUG(dbgs() << "\tARM::shouldCoalesce - Reg Weight: " << NewRCWeight.RegWeight << "\n");
+ unsigned SizeMultiplier = MBB->size()/100;
+ SizeMultiplier = SizeMultiplier ? SizeMultiplier : 1;
+ if (It->second < NewRCWeight.WeightLimit * SizeMultiplier) {
+ It->second += NewRCWeight.RegWeight;
+ return true;
+ }
+ return false;
+}
index 44d2159cb548c54bf6be436ccde773e127db9fc8..626bb0e7860946af3602526d2861a766537ca4d3 100644 (file)
/// GVIsIndirectSymbol - true if the GV will be accessed via an indirect
/// symbol.
bool GVIsIndirectSymbol(const GlobalValue *GV, Reloc::Model RelocM) const;
+
+ /// \brief SrcRC and DstRC will be morphed into NewRC if this returns true
+ bool shouldCoalesce(MachineInstr *MI,
+ const TargetRegisterClass *SrcRC,
+ unsigned SubReg,
+ const TargetRegisterClass *DstRC,
+ unsigned DstSubReg,
+ const TargetRegisterClass *NewRC) const override;
};
} // End llvm namespace
diff --git a/test/CodeGen/ARM/out-of-registers.ll b/test/CodeGen/ARM/out-of-registers.ll
--- /dev/null
@@ -0,0 +1,42 @@
+; RUN: llc -O3 %s -o - | FileCheck %s
+; ModuleID = 'fo.c'
+target datalayout = "e-p:32:32:32-i1:8:32-i8:8:32-i16:16:32-i32:32:32-i64:64:64-f32:32:32-f64:64:64-v64:64:64-v128:64:128-a0:0:32-n8:16:32-S64"
+target triple = "thumbv7-none-linux-gnueabi"
+
+; CHECK: vpush
+; CHECK: vpop
+
+define void @foo(float* nocapture %A) #0 {
+ %1= bitcast float* %A to i8*
+ %2 = tail call { <4 x float>, <4 x float>, <4 x float>, <4 x float> } @llvm.arm.neon.vld4.v4f32(i8* %1, i32 4)
+ %3 = extractvalue { <4 x float>, <4 x float>, <4 x float>, <4 x float> } %2, 0
+ %divp_vec = fdiv <4 x float> <float 1.000000e+00, float 1.000000e+00, float 1.000000e+00, float 1.000000e+00>, %3
+ %4 = extractvalue { <4 x float>, <4 x float>, <4 x float>, <4 x float> } %2, 1
+ %div3p_vec = fdiv <4 x float> <float 1.000000e+00, float 1.000000e+00, float 1.000000e+00, float 1.000000e+00>, %4
+ %5 = extractvalue { <4 x float>, <4 x float>, <4 x float>, <4 x float> } %2, 2
+ %div8p_vec = fdiv <4 x float> <float 1.000000e+00, float 1.000000e+00, float 1.000000e+00, float 1.000000e+00>, %5
+ %6 = extractvalue { <4 x float>, <4 x float>, <4 x float>, <4 x float> } %2, 3
+ %div13p_vec = fdiv <4 x float> <float 1.000000e+00, float 1.000000e+00, float 1.000000e+00, float 1.000000e+00>, %6
+ tail call void @llvm.arm.neon.vst4.v4f32(i8* %1, <4 x float> %divp_vec, <4 x float> %div3p_vec, <4 x float> %div8p_vec, <4 x float> %div13p_vec, i32 4)
+ ret void
+}
+
+; Function Attrs: nounwind
+declare i32 @llvm.annotation.i32(i32, i8*, i8*, i32) #1
+
+; Function Attrs: nounwind readonly
+
+; Function Attrs: nounwind
+declare void @llvm.arm.neon.vst4.v4f32(i8*, <4 x float>, <4 x float>, <4 x float>, <4 x float>, i32) #1
+declare { <4 x float>, <4 x float>, <4 x float>, <4 x float> } @llvm.arm.neon.vld4.v4f32(i8*, i32) #2
+
+; Function Attrs: nounwind
+
+attributes #0 = { nounwind "less-precise-fpmad"="false" "no-frame-pointer-elim"="false" "no-infs-fp-math"="true" "no-nans-fp-math"="true" "stack-protector-buffer-size"="8" "unsafe-fp-math"="true" "use-soft-float"="false" }
+attributes #1 = { nounwind }
+attributes #2 = { nounwind readonly }
+
+!llvm.ident = !{!0}
+
+!0 = metadata !{metadata !"Snapdragon LLVM ARM Compiler 3.4"}
+!1 = metadata !{metadata !1}
diff --git a/test/CodeGen/ARM/vector-spilling.ll b/test/CodeGen/ARM/vector-spilling.ll
--- /dev/null
@@ -0,0 +1,34 @@
+; RUN: llc < %s -march=arm -mtriple=armv7-linux-gnueabihf -arm-atomic-cfg-tidy=0 -float-abi=hard -mcpu=cortex-a9 -O3 | FileCheck %s
+
+target datalayout = "e-p:32:32:32-i1:8:8-i8:8:8-i16:16:16-i32:32:32-i64:64:64-f32:32:32-f64:64:64-v64:64:64-v128:128:128-a0:0:64-n32-S64"
+
+; This test will generate spills/fills using vldmia instructions that access 24 bytes of memory.
+; Check that we don't crash when we generate these instructions on Cortex-A9.
+
+; CHECK: test:
+; CHECK: vstmia
+; CHECK: vldmia
+define void @test(<8 x i64>* %src) #0 {
+entry:
+ %0 = getelementptr inbounds <8 x i64>* %src, i32 0
+ %1 = load <8 x i64>* %0, align 8
+
+ %2 = getelementptr inbounds <8 x i64>* %src, i32 1
+ %3 = load <8 x i64>* %2, align 8
+
+ %4 = getelementptr inbounds <8 x i64>* %src, i32 2
+ %5 = load <8 x i64>* %4, align 8
+
+ %6 = getelementptr inbounds <8 x i64>* %src, i32 3
+ %7 = load <8 x i64>* %6, align 8
+
+ %8 = shufflevector <8 x i64> %1, <8 x i64> %3, <8 x i32> <i32 0, i32 8, i32 1, i32 9, i32 2, i32 10, i32 3, i32 11>
+ %9 = shufflevector <8 x i64> %1, <8 x i64> %3, <8 x i32> <i32 4, i32 12, i32 5, i32 13, i32 6, i32 14, i32 7, i32 15>
+
+ tail call void(<8 x i64>, <8 x i64>, <8 x i64>, <8 x i64>, <8 x i64>, <8 x i64>)* @foo(<8 x i64> %1, <8 x i64> %3, <8 x i64> %5, <8 x i64> %7, <8 x i64> %8, <8 x i64> %9)
+ ret void
+}
+
+declare void @foo(<8 x i64>, <8 x i64>, <8 x i64>, <8 x i64>, <8 x i64>, <8 x i64>)
+
+attributes #0 = { noredzone "less-precise-fpmad"="false" "no-frame-pointer-elim"="false" "no-frame-pointer-elim-non-leaf"="false" "no-infs-fp-math"="false" "no-nans-fp-math"="false" "unsafe-fp-math"="false" "use-soft-float"="false" }
index f2e5eb9b7e035086f36ea12a2f670527b4dcbef3..64f3770e3d21272fba75df6c19419198f976b356 100644 (file)
target datalayout = "e-p:32:32:32-i1:8:8-i8:8:8-i16:16:16-i32:32:32-i64:64:64-f32:32:32-f64:64:64-v64:64:64-v128:128:128-a0:0:64-n32-S64"
-; This test will generate spills/fills using vldmia instructions that access 64 bytes of memory.
-; Check that we don't crash when we generate these instructions on Cortex-A9.
+; This test used to test vector spilling using vstmia/vldmia instructions, but
+; the changes for PR:18825 prevent that spilling.
; CHECK: test:
-; CHECK: vstmia
-; CHECK: vldmia
+; CHECK-NOT: vstmia
+; CHECK-NOT: vldmia
define void @test(i64* %src) #0 {
entry:
%arrayidx39 = getelementptr inbounds i64* %src, i32 13