summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: b05ad79)
raw | patch | inline | side by side (parent: b05ad79)
author | Rui Ueyama <ruiu@google.com> | |
Thu, 18 Jul 2013 22:44:20 +0000 (22:44 +0000) | ||
committer | Rui Ueyama <ruiu@google.com> | |
Thu, 18 Jul 2013 22:44:20 +0000 (22:44 +0000) |
Summary:
Dump optional data directory entries in the PE/COFF header, so that
we can test the output of LLD linker. This patch updates the test binary
file, but the source of the binary is the same. I just re-linked the file.
I don't know how the previous file was linked, but the previous file did
not have any data directory entries for some reason.
Reviewers: rafael
CC: llvm-commits
Differential Revision: http://llvm-reviews.chandlerc.com/D1148
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@186623 91177308-0d34-0410-b5e6-96231b3b80d8
Dump optional data directory entries in the PE/COFF header, so that
we can test the output of LLD linker. This patch updates the test binary
file, but the source of the binary is the same. I just re-linked the file.
I don't know how the previous file was linked, but the previous file did
not have any data directory entries for some reason.
Reviewers: rafael
CC: llvm-commits
Differential Revision: http://llvm-reviews.chandlerc.com/D1148
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@186623 91177308-0d34-0410-b5e6-96231b3b80d8
index c7c5c7f118d4b5523cdd4c9ef5c41cdebf05d28a..21900675ffdb341ae5a78d4e9c52a0bf81ac428c 100644 (file)
private:
const coff_file_header *COFFHeader;
const pe32_header *PE32Header;
+ const data_directory *DataDirectory;
const coff_section *SectionTable;
const coff_symbol *SymbolTable;
const char *StringTable;
error_code getHeader(const coff_file_header *&Res) const;
error_code getCOFFHeader(const coff_file_header *&Res) const;
error_code getPE32Header(const pe32_header *&Res) const;
+ error_code getDataDirectory(uint32_t index, const data_directory *&Res) const;
error_code getSection(int32_t index, const coff_section *&Res) const;
error_code getSymbol(uint32_t index, const coff_symbol *&Res) const;
template <typename T>
index 49317e905142d2115bfd09f5e17efd9e48c7f074..c66a1e044b5eaff9f37947ef7c6fbb3454ffcbc8 100644 (file)
return true;
}
-// Returns false if any bytes in [addr, addr + size) fall outsize of m.
-bool checkAddr(const MemoryBuffer *m,
- error_code &ec,
- uintptr_t addr,
- uint64_t size) {
- if (addr + size < addr ||
- addr + size < size ||
- addr + size > uintptr_t(m->getBufferEnd())) {
- ec = object_error::unexpected_eof;
- return false;
+// Sets Obj unless any bytes in [addr, addr + size) fall outsize of m.
+// Returns unexpected_eof if error.
+template<typename T>
+error_code getObject(const T *&Obj, const MemoryBuffer *M, const uint8_t *Ptr,
+ const size_t Size = sizeof(T)) {
+ uintptr_t Addr = uintptr_t(Ptr);
+ if (Addr + Size < Addr ||
+ Addr + Size < Size ||
+ Addr + Size > uintptr_t(M->getBufferEnd())) {
+ return object_error::unexpected_eof;
}
- return true;
+ Obj = reinterpret_cast<const T *>(Addr);
+ return object_error::success;
}
}
: ObjectFile(Binary::ID_COFF, Object)
, COFFHeader(0)
, PE32Header(0)
+ , DataDirectory(0)
, SectionTable(0)
, SymbolTable(0)
, StringTable(0)
hasPEHeader = true;
}
- COFFHeader = reinterpret_cast<const coff_file_header *>(base() + CurPtr);
- if (!checkAddr(Data, ec, uintptr_t(COFFHeader), sizeof(coff_file_header)))
+ if ((ec = getObject(COFFHeader, Data, base() + CurPtr)))
return;
CurPtr += sizeof(coff_file_header);
if (hasPEHeader) {
- PE32Header = reinterpret_cast<const pe32_header *>(base() + CurPtr);
- if (!checkAddr(Data, ec, uintptr_t(PE32Header), sizeof(pe32_header)))
+ if ((ec = getObject(PE32Header, Data, base() + CurPtr)))
return;
- // We only support PE32. If this is PE32 (not PE32+), the magic byte
- // should be 0x10b. If this is not PE32, continue as if there's no PE
- // header in this file.
- if (PE32Header->Magic != 0x10b)
+ if (PE32Header->Magic != 0x10b) {
+ // We only support PE32. If this is PE32 (not PE32+), the magic byte
+ // should be 0x10b. If this is not PE32, continue as if there's no PE
+ // header in this file.
PE32Header = 0;
- // There may be optional data directory after PE header. Skip them.
+ } else if (PE32Header->NumberOfRvaAndSize > 0) {
+ const uint8_t *addr = base() + CurPtr + sizeof(pe32_header);
+ uint64_t size = sizeof(data_directory) * PE32Header->NumberOfRvaAndSize;
+ if ((ec = getObject(DataDirectory, Data, addr, size)))
+ return;
+ }
CurPtr += COFFHeader->SizeOfOptionalHeader;
}
- SectionTable =
- reinterpret_cast<const coff_section *>(base() + CurPtr);
- if (!checkAddr(Data, ec, uintptr_t(SectionTable),
- COFFHeader->NumberOfSections * sizeof(coff_section)))
+ if ((ec = getObject(SectionTable, Data, base() + CurPtr,
+ COFFHeader->NumberOfSections * sizeof(coff_section))))
return;
if (COFFHeader->PointerToSymbolTable != 0) {
- SymbolTable =
- reinterpret_cast<const coff_symbol *>(base()
- + COFFHeader->PointerToSymbolTable);
- if (!checkAddr(Data, ec, uintptr_t(SymbolTable),
- COFFHeader->NumberOfSymbols * sizeof(coff_symbol)))
+ if ((ec = getObject(SymbolTable, Data,
+ base() + COFFHeader->PointerToSymbolTable,
+ COFFHeader->NumberOfSymbols * sizeof(coff_symbol))))
return;
// Find string table.
- StringTable = reinterpret_cast<const char *>(base())
- + COFFHeader->PointerToSymbolTable
- + COFFHeader->NumberOfSymbols * sizeof(coff_symbol);
- if (!checkAddr(Data, ec, uintptr_t(StringTable), sizeof(ulittle32_t)))
+ const uint8_t *StringTableAddr = base() + COFFHeader->PointerToSymbolTable
+ + COFFHeader->NumberOfSymbols * sizeof(coff_symbol);
+ const uint32_t *StringTableSizePtr;
+ if ((ec = getObject(StringTableSizePtr, Data, StringTableAddr)))
return;
-
- StringTableSize = *reinterpret_cast<const ulittle32_t *>(StringTable);
- if (!checkAddr(Data, ec, uintptr_t(StringTable), StringTableSize))
+ StringTableSize = *StringTableSizePtr;
+ if ((ec = getObject(StringTable, Data, StringTableAddr, StringTableSize)))
return;
+
// Check that the string table is null terminated if has any in it.
if (StringTableSize < 4
|| (StringTableSize > 4 && StringTable[StringTableSize - 1] != 0)) {
return object_error::success;
}
+error_code COFFObjectFile::getDataDirectory(uint32_t index,
+ const data_directory *&Res) const {
+ // Error if if there's no data directory or the index is out of range.
+ if (!DataDirectory || index > PE32Header->NumberOfRvaAndSize)
+ return object_error::parse_failed;
+ Res = &DataDirectory[index];
+ return object_error::success;
+}
+
error_code COFFObjectFile::getSection(int32_t index,
const coff_section *&Result) const {
// Check for special index values.
diff --git a/test/tools/llvm-readobj/Inputs/trivial.exe.coff-i386 b/test/tools/llvm-readobj/Inputs/trivial.exe.coff-i386
index 3009f90da08e8951d5d1898c1381e980840a8c6d..1558d2452ecc19dbaa4f2384bb205dd5a6b53d62 100644 (file)
Binary files a/test/tools/llvm-readobj/Inputs/trivial.exe.coff-i386 and b/test/tools/llvm-readobj/Inputs/trivial.exe.coff-i386 differ
Binary files a/test/tools/llvm-readobj/Inputs/trivial.exe.coff-i386 and b/test/tools/llvm-readobj/Inputs/trivial.exe.coff-i386 differ
index 1082dccd4c9ca308b66a9428663156ff60292994..b900e365f202442a6492318cfefefd2f45c45c51 100644 (file)
PE32-NEXT: AddressSize: 32bit
PE32-NEXT: ImageFileHeader {
PE32-NEXT: Machine: IMAGE_FILE_MACHINE_I386 (0x14C)
-PE32-NEXT: SectionCount: 1
-PE32-NEXT: TimeDateStamp: 2013-05-24 21:24:34 (0x519FDA92)
+PE32-NEXT: SectionCount: 3
+PE32-NEXT: TimeDateStamp: 2013-07-16 00:39:15 (0x51E49633)
PE32-NEXT: PointerToSymbolTable: 0x0
PE32-NEXT: SymbolCount: 0
PE32-NEXT: OptionalHeaderSize: 224
PE32-NEXT: ]
PE32-NEXT: }
PE32-NEXT: ImageOptionalHeader {
-PE32-NEXT: MajorLinkerVersion: 10
+PE32-NEXT: MajorLinkerVersion: 11
PE32-NEXT: MinorLinkerVersion: 0
PE32-NEXT: SizeOfCode: 512
-PE32-NEXT: SizeOfInitializedData: 0
+PE32-NEXT: SizeOfInitializedData: 1024
PE32-NEXT: SizeOfUninitializedData: 0
PE32-NEXT: AddressOfEntryPoint: 0x1000
PE32-NEXT: BaseOfCode: 0x1000
PE32-NEXT: ImageBase: 0x400000
PE32-NEXT: SectionAlignment: 4096
PE32-NEXT: FileAlignment: 512
-PE32-NEXT: MajorOperatingSystemVersion: 5
-PE32-NEXT: MinorOperatingSystemVersion: 1
+PE32-NEXT: MajorOperatingSystemVersion: 6
+PE32-NEXT: MinorOperatingSystemVersion: 0
PE32-NEXT: MajorImageVersion: 0
PE32-NEXT: MinorImageVersion: 0
-PE32-NEXT: MajorSubsystemVersion: 5
-PE32-NEXT: MinorSubsystemVersion: 1
-PE32-NEXT: SizeOfImage: 8192
-PE32-NEXT: SizeOfHeaders: 512
-PE32-NEXT: Subsystem: IMAGE_SUBSYSTEM_WINDOWS_GUI (0x2)
+PE32-NEXT: MajorSubsystemVersion: 6
+PE32-NEXT: MinorSubsystemVersion: 0
+PE32-NEXT: SizeOfImage: 16384
+PE32-NEXT: SizeOfHeaders: 1024
+PE32-NEXT: Subsystem: IMAGE_SUBSYSTEM_WINDOWS_CUI (0x3)
PE32-NEXT: Subsystem [ (0x8140)
PE32-NEXT: IMAGE_DLL_CHARACTERISTICS_DYNAMIC_BASE (0x40)
PE32-NEXT: IMAGE_DLL_CHARACTERISTICS_NX_COMPAT (0x100)
PE32-NEXT: SizeOfHeapReserve: 1048576
PE32-NEXT: SizeOfHeapCommit: 4096
PE32-NEXT: NumberOfRvaAndSize: 16
+PE32-NEXT: DataDirectory {
+PE32-NEXT: ExportTableRVA: 0x0
+PE32-NEXT: ExportTableSize: 0x0
+PE32-NEXT: ImportTableRVA: 0x0
+PE32-NEXT: ImportTableSize: 0x0
+PE32-NEXT: ResourceTableRVA: 0x0
+PE32-NEXT: ResourceTableSize: 0x0
+PE32-NEXT: ExceptionTableRVA: 0x0
+PE32-NEXT: ExceptionTableSize: 0x0
+PE32-NEXT: CertificateTableRVA: 0x0
+PE32-NEXT: CertificateTableSize: 0x0
+PE32-NEXT: BaseRelocationTableRVA: 0x3000
+PE32-NEXT: BaseRelocationTableSize: 0xC
+PE32-NEXT: DebugRVA: 0x0
+PE32-NEXT: DebugSize: 0x0
+PE32-NEXT: ArchitectureRVA: 0x0
+PE32-NEXT: ArchitectureSize: 0x0
+PE32-NEXT: GlobalPtrRVA: 0x0
+PE32-NEXT: GlobalPtrSize: 0x0
+PE32-NEXT: TLSTableRVA: 0x0
+PE32-NEXT: TLSTableSize: 0x0
+PE32-NEXT: LoadConfigTableRVA: 0x0
+PE32-NEXT: LoadConfigTableSize: 0x0
+PE32-NEXT: BoundImportRVA: 0x0
+PE32-NEXT: BoundImportSize: 0x0
+PE32-NEXT: IATRVA: 0x0
+PE32-NEXT: IATSize: 0x0
+PE32-NEXT: DelayImportDescriptorRVA: 0x0
+PE32-NEXT: DelayImportDescriptorSize: 0x0
+PE32-NEXT: CLRRuntimeHeaderRVA: 0x0
+PE32-NEXT: CLRRuntimeHeaderSize: 0x0
+PE32-NEXT: ReservedRVA: 0x0
+PE32-NEXT: ReservedSize: 0x0
+PE32-NEXT: }
PE32-NEXT: }
index 1ceb8fcd316dcc2f6111c12d84674a5d530bd9d4..2f309e30ec22b7dd8f50a656afb92b029353935a 100644 (file)
void printRelocation(section_iterator SecI, relocation_iterator RelI);
+ void printDataDirectory(uint32_t Index, const std::string &FieldName);
+
void printX64UnwindInfo();
void printRuntimeFunction(
}
}
+void COFFDumper::printDataDirectory(uint32_t Index, const std::string &FieldName) {
+ const data_directory *Data;
+ if (Obj->getDataDirectory(Index, Data))
+ return;
+ W.printHex(FieldName + "RVA", Data->RelativeVirtualAddress);
+ W.printHex(FieldName + "Size", Data->Size);
+}
+
void COFFDumper::printFileHeaders() {
// Print COFF header
const coff_file_header *COFFHeader = 0;
W.printNumber("SizeOfHeapReserve", PEHeader->SizeOfHeapReserve);
W.printNumber("SizeOfHeapCommit", PEHeader->SizeOfHeapCommit);
W.printNumber("NumberOfRvaAndSize", PEHeader->NumberOfRvaAndSize);
+
+ if (PEHeader->NumberOfRvaAndSize > 0) {
+ DictScope D(W, "DataDirectory");
+ static const char * const directory[] = {
+ "ExportTable", "ImportTable", "ResourceTable", "ExceptionTable",
+ "CertificateTable", "BaseRelocationTable", "Debug", "Architecture",
+ "GlobalPtr", "TLSTable", "LoadConfigTable", "BoundImport", "IAT",
+ "DelayImportDescriptor", "CLRRuntimeHeader", "Reserved"
+ };
+
+ for (uint32_t i = 0; i < PEHeader->NumberOfRvaAndSize; ++i) {
+ printDataDirectory(i, directory[i]);
+ }
+ }
}
}