]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/commitdiff
Use the paths to libffi's header and library even when no custom
authorOscar Fuentes <ofv@wanadoo.es>
Thu, 27 Jan 2011 22:58:34 +0000 (22:58 +0000)
committerOscar Fuentes <ofv@wanadoo.es>
Thu, 27 Jan 2011 22:58:34 +0000 (22:58 +0000)
location was stated with FFI_INCLUDE_DIR/FFI_LIBRARY_DIR.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@124449 91177308-0d34-0410-b5e6-96231b3b80d8

lib/ExecutionEngine/Interpreter/CMakeLists.txt

index 39df555d5e294c38afca882c20a4d6f042854790..c8e4b6eedcd79ca71d9276e59967c99f6b3bbaf3 100644 (file)
@@ -1,12 +1,16 @@
-# If the user required a custom path for ffi headers, use it on its
-# abolute form (see config-ix.cmake):
-if( FFI_INCLUDE_DIR )
+# Make sure that the path to libffi headers is on the command
+# line. That path can be a compiler's non-default path even when
+# FFI_INCLUDE_DIR was not used, because cmake has its own paths for
+# searching for headers (CMAKE_SYSTEM_INCLUDE_PATH, for instance):
+if( FFI_INCLUDE_PATH )
   include_directories( ${FFI_INCLUDE_PATH} )
 endif()
 
-# If the user required a custom path for libffi, use it on its abolute
-# form (see config-ix.cmake):
-if( FFI_LIBRARY_DIR )
+# Make sure that the path to libffi archive is on the command
+# line. That path can be a linker's non-default path even when
+# FFI_LIBRARY_DIR was not used, because cmake has its own paths for
+# searching for libraries (CMAKE_SYSTEM_LIBRARY_PATH, for instance):
+if( FFI_LIBRARY_PATH )
   link_directories( ${FFI_LIBRARY_PATH} )
 endif()