summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: bf93354)
raw | patch | inline | side by side (parent: bf93354)
author | Michael J. Spencer <bigcheesegs@gmail.com> | |
Thu, 29 May 2014 01:42:45 +0000 (01:42 +0000) | ||
committer | Michael J. Spencer <bigcheesegs@gmail.com> | |
Thu, 29 May 2014 01:42:45 +0000 (01:42 +0000) |
An address only use of an extract element of a load can be simplified to a
load. Without this the result of the extract element is spilled to the
stack so that an address is available.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209788 91177308-0d34-0410-b5e6-96231b3b80d8
load. Without this the result of the extract element is spilled to the
stack so that an address is available.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209788 91177308-0d34-0410-b5e6-96231b3b80d8
lib/CodeGen/SelectionDAG/DAGCombiner.cpp | patch | blob | history | |
test/CodeGen/X86/vec_splat.ll | patch | blob | history |
index c4089446f08df75f53c38c7431d479e4c0e2f327..f346dcfcddd91f9cc53a7040a3abc7dae2c327f5 100644 (file)
bool CombineToPostIndexedLoadStore(SDNode *N);
bool SliceUpLoad(SDNode *N);
+ /// \brief Replace an ISD::EXTRACT_VECTOR_ELT of a load with a narrowed
+ /// load.
+ ///
+ /// \param EVE ISD::EXTRACT_VECTOR_ELT to be replaced.
+ /// \param InVecVT type of the input vector to EVE with bitcasts resolved.
+ /// \param EltNo index of the vector element to load.
+ /// \param OriginalLoad load that EVE came from to be replaced.
+ /// \returns EVE on success SDValue() on failure.
+ SDValue ReplaceExtractVectorEltOfLoadWithNarrowedLoad(
+ SDNode *EVE, EVT InVecVT, SDValue EltNo, LoadSDNode *OriginalLoad);
void ReplaceLoadWithPromotedLoad(SDNode *Load, SDNode *ExtLoad);
SDValue PromoteOperand(SDValue Op, EVT PVT, bool &Replace);
SDValue SExtPromoteOperand(SDValue Op, EVT PVT);
return DAG.getNode(ISD::BUILD_VECTOR, dl, VT, Ops);
}
+SDValue DAGCombiner::ReplaceExtractVectorEltOfLoadWithNarrowedLoad(
+ SDNode *EVE, EVT InVecVT, SDValue EltNo, LoadSDNode *OriginalLoad) {
+ EVT ResultVT = EVE->getValueType(0);
+ EVT VecEltVT = InVecVT.getVectorElementType();
+ unsigned Align = OriginalLoad->getAlignment();
+ unsigned NewAlign = TLI.getDataLayout()->getABITypeAlignment(
+ VecEltVT.getTypeForEVT(*DAG.getContext()));
+
+ if (NewAlign > Align || !TLI.isOperationLegalOrCustom(ISD::LOAD, VecEltVT))
+ return SDValue();
+
+ Align = NewAlign;
+
+ SDValue NewPtr = OriginalLoad->getBasePtr();
+ SDValue Offset;
+ EVT PtrType = NewPtr.getValueType();
+ MachinePointerInfo MPI;
+ if (auto *ConstEltNo = dyn_cast<ConstantSDNode>(EltNo)) {
+ int Elt = ConstEltNo->getZExtValue();
+ unsigned PtrOff = VecEltVT.getSizeInBits() * Elt / 8;
+ if (TLI.isBigEndian())
+ PtrOff = InVecVT.getSizeInBits() / 8 - PtrOff;
+ Offset = DAG.getConstant(PtrOff, PtrType);
+ MPI = OriginalLoad->getPointerInfo().getWithOffset(PtrOff);
+ } else {
+ Offset = DAG.getNode(
+ ISD::MUL, SDLoc(EVE), EltNo.getValueType(), EltNo,
+ DAG.getConstant(VecEltVT.getStoreSize(), EltNo.getValueType()));
+ if (TLI.isBigEndian())
+ Offset = DAG.getNode(
+ ISD::SUB, SDLoc(EVE), EltNo.getValueType(),
+ DAG.getConstant(InVecVT.getStoreSize(), EltNo.getValueType()), Offset);
+ MPI = OriginalLoad->getPointerInfo();
+ }
+ NewPtr = DAG.getNode(ISD::ADD, SDLoc(EVE), PtrType, NewPtr, Offset);
+
+ // The replacement we need to do here is a little tricky: we need to
+ // replace an extractelement of a load with a load.
+ // Use ReplaceAllUsesOfValuesWith to do the replacement.
+ // Note that this replacement assumes that the extractvalue is the only
+ // use of the load; that's okay because we don't want to perform this
+ // transformation in other cases anyway.
+ SDValue Load;
+ SDValue Chain;
+ if (ResultVT.bitsGT(VecEltVT)) {
+ // If the result type of vextract is wider than the load, then issue an
+ // extending load instead.
+ ISD::LoadExtType ExtType = TLI.isLoadExtLegal(ISD::ZEXTLOAD, VecEltVT)
+ ? ISD::ZEXTLOAD
+ : ISD::EXTLOAD;
+ Load = DAG.getExtLoad(ExtType, SDLoc(EVE), ResultVT, OriginalLoad->getChain(),
+ NewPtr, MPI, VecEltVT, OriginalLoad->isVolatile(),
+ OriginalLoad->isNonTemporal(), Align,
+ OriginalLoad->getTBAAInfo());
+ Chain = Load.getValue(1);
+ } else {
+ Load = DAG.getLoad(
+ VecEltVT, SDLoc(EVE), OriginalLoad->getChain(), NewPtr, MPI,
+ OriginalLoad->isVolatile(), OriginalLoad->isNonTemporal(),
+ OriginalLoad->isInvariant(), Align, OriginalLoad->getTBAAInfo());
+ Chain = Load.getValue(1);
+ if (ResultVT.bitsLT(VecEltVT))
+ Load = DAG.getNode(ISD::TRUNCATE, SDLoc(EVE), ResultVT, Load);
+ else
+ Load = DAG.getNode(ISD::BITCAST, SDLoc(EVE), ResultVT, Load);
+ }
+ WorkListRemover DeadNodes(*this);
+ SDValue From[] = { SDValue(EVE, 0), SDValue(OriginalLoad, 1) };
+ SDValue To[] = { Load, Chain };
+ DAG.ReplaceAllUsesOfValuesWith(From, To, 2);
+ // Since we're explicitly calling ReplaceAllUses, add the new node to the
+ // worklist explicitly as well.
+ AddToWorkList(Load.getNode());
+ AddUsersToWorkList(Load.getNode()); // Add users too
+ // Make sure to revisit this node to clean it up; it will usually be dead.
+ AddToWorkList(EVE);
+ ++OpsNarrowed;
+ return SDValue(EVE, 0);
+}
+
SDValue DAGCombiner::visitEXTRACT_VECTOR_ELT(SDNode *N) {
// (vextract (scalar_to_vector val, 0) -> val
SDValue InVec = N->getOperand(0);
}
}
+ bool BCNumEltsChanged = false;
+ EVT ExtVT = VT.getVectorElementType();
+ EVT LVT = ExtVT;
+
+ // If the result of load has to be truncated, then it's not necessarily
+ // profitable.
+ if (NVT.bitsLT(LVT) && !TLI.isTruncateFree(LVT, NVT))
+ return SDValue();
+
+ if (InVec.getOpcode() == ISD::BITCAST) {
+ // Don't duplicate a load with other uses.
+ if (!InVec.hasOneUse())
+ return SDValue();
+
+ EVT BCVT = InVec.getOperand(0).getValueType();
+ if (!BCVT.isVector() || ExtVT.bitsGT(BCVT.getVectorElementType()))
+ return SDValue();
+ if (VT.getVectorNumElements() != BCVT.getVectorNumElements())
+ BCNumEltsChanged = true;
+ InVec = InVec.getOperand(0);
+ ExtVT = BCVT.getVectorElementType();
+ }
+
+ // (vextract (vN[if]M load $addr), i) -> ([if]M load $addr + i * size)
+ if (!LegalOperations && !ConstEltNo && InVec.hasOneUse() &&
+ ISD::isNormalLoad(InVec.getNode())) {
+ SDValue Index = N->getOperand(1);
+ if (LoadSDNode *OrigLoad = dyn_cast<LoadSDNode>(InVec))
+ return ReplaceExtractVectorEltOfLoadWithNarrowedLoad(N, VT, Index,
+ OrigLoad);
+ }
+
// Perform only after legalization to ensure build_vector / vector_shuffle
// optimizations have already been done.
if (!LegalOperations) return SDValue();
if (ConstEltNo) {
int Elt = cast<ConstantSDNode>(EltNo)->getZExtValue();
- bool NewLoad = false;
- bool BCNumEltsChanged = false;
- EVT ExtVT = VT.getVectorElementType();
- EVT LVT = ExtVT;
-
- // If the result of load has to be truncated, then it's not necessarily
- // profitable.
- if (NVT.bitsLT(LVT) && !TLI.isTruncateFree(LVT, NVT))
- return SDValue();
-
- if (InVec.getOpcode() == ISD::BITCAST) {
- // Don't duplicate a load with other uses.
- if (!InVec.hasOneUse())
- return SDValue();
-
- EVT BCVT = InVec.getOperand(0).getValueType();
- if (!BCVT.isVector() || ExtVT.bitsGT(BCVT.getVectorElementType()))
- return SDValue();
- if (VT.getVectorNumElements() != BCVT.getVectorNumElements())
- BCNumEltsChanged = true;
- InVec = InVec.getOperand(0);
- ExtVT = BCVT.getVectorElementType();
- NewLoad = true;
- }
LoadSDNode *LN0 = nullptr;
const ShuffleVectorSDNode *SVN = nullptr;
if (ISD::isNormalLoad(InVec.getNode())) {
LN0 = cast<LoadSDNode>(InVec);
Elt = (Idx < (int)NumElems) ? Idx : Idx - (int)NumElems;
+ EltNo = DAG.getConstant(Elt, EltNo.getValueType());
}
}
if (Elt == -1)
return DAG.getUNDEF(LVT);
- unsigned Align = LN0->getAlignment();
- if (NewLoad) {
- // Check the resultant load doesn't need a higher alignment than the
- // original load.
- unsigned NewAlign =
- TLI.getDataLayout()
- ->getABITypeAlignment(LVT.getTypeForEVT(*DAG.getContext()));
-
- if (NewAlign > Align || !TLI.isOperationLegalOrCustom(ISD::LOAD, LVT))
- return SDValue();
-
- Align = NewAlign;
- }
-
- SDValue NewPtr = LN0->getBasePtr();
- unsigned PtrOff = 0;
-
- if (Elt) {
- PtrOff = LVT.getSizeInBits() * Elt / 8;
- EVT PtrType = NewPtr.getValueType();
- if (TLI.isBigEndian())
- PtrOff = VT.getSizeInBits() / 8 - PtrOff;
- NewPtr = DAG.getNode(ISD::ADD, SDLoc(N), PtrType, NewPtr,
- DAG.getConstant(PtrOff, PtrType));
- }
-
- // The replacement we need to do here is a little tricky: we need to
- // replace an extractelement of a load with a load.
- // Use ReplaceAllUsesOfValuesWith to do the replacement.
- // Note that this replacement assumes that the extractvalue is the only
- // use of the load; that's okay because we don't want to perform this
- // transformation in other cases anyway.
- SDValue Load;
- SDValue Chain;
- if (NVT.bitsGT(LVT)) {
- // If the result type of vextract is wider than the load, then issue an
- // extending load instead.
- ISD::LoadExtType ExtType = TLI.isLoadExtLegal(ISD::ZEXTLOAD, LVT)
- ? ISD::ZEXTLOAD : ISD::EXTLOAD;
- Load = DAG.getExtLoad(ExtType, SDLoc(N), NVT, LN0->getChain(),
- NewPtr, LN0->getPointerInfo().getWithOffset(PtrOff),
- LVT, LN0->isVolatile(), LN0->isNonTemporal(),
- Align, LN0->getTBAAInfo());
- Chain = Load.getValue(1);
- } else {
- Load = DAG.getLoad(LVT, SDLoc(N), LN0->getChain(), NewPtr,
- LN0->getPointerInfo().getWithOffset(PtrOff),
- LN0->isVolatile(), LN0->isNonTemporal(),
- LN0->isInvariant(), Align, LN0->getTBAAInfo());
- Chain = Load.getValue(1);
- if (NVT.bitsLT(LVT))
- Load = DAG.getNode(ISD::TRUNCATE, SDLoc(N), NVT, Load);
- else
- Load = DAG.getNode(ISD::BITCAST, SDLoc(N), NVT, Load);
- }
- WorkListRemover DeadNodes(*this);
- SDValue From[] = { SDValue(N, 0), SDValue(LN0,1) };
- SDValue To[] = { Load, Chain };
- DAG.ReplaceAllUsesOfValuesWith(From, To, 2);
- // Since we're explcitly calling ReplaceAllUses, add the new node to the
- // worklist explicitly as well.
- AddToWorkList(Load.getNode());
- AddUsersToWorkList(Load.getNode()); // Add users too
- // Make sure to revisit this node to clean it up; it will usually be dead.
- AddToWorkList(N);
- return SDValue(N, 0);
+ return ReplaceExtractVectorEltOfLoadWithNarrowedLoad(N, VT, EltNo, LN0);
}
return SDValue();
index a02e3836078c6779ef5be476cdad90df7fb494f0..28f2a9074cb841def9eafefbb988226e8dbe5c92 100644 (file)
; RUN: llc < %s -march=x86 -mcpu=pentium4 -mattr=+sse2 | FileCheck %s -check-prefix=SSE2
; RUN: llc < %s -march=x86 -mcpu=pentium4 -mattr=+sse3 | FileCheck %s -check-prefix=SSE3
+; RUN: llc < %s -march=x86-64 -mattr=+avx | FileCheck %s -check-prefix=AVX
define void @test_v4sf(<4 x float>* %P, <4 x float>* %Q, float %X) nounwind {
%tmp = insertelement <4 x float> zeroinitializer, float %X, i32 0 ; <<4 x float>> [#uses=1]
; Fold extract of a load into the load's address computation. This avoids spilling to the stack.
define <4 x float> @load_extract_splat(<4 x float>* nocapture readonly %ptr, i64 %i, i64 %j) nounwind {
+ %1 = getelementptr inbounds <4 x float>* %ptr, i64 %i
+ %2 = load <4 x float>* %1, align 16
+ %3 = trunc i64 %j to i32
+ %4 = extractelement <4 x float> %2, i32 %3
+ %5 = insertelement <4 x float> undef, float %4, i32 0
+ %6 = insertelement <4 x float> %5, float %4, i32 1
+ %7 = insertelement <4 x float> %6, float %4, i32 2
+ %8 = insertelement <4 x float> %7, float %4, i32 3
+ ret <4 x float> %8
+
+; AVX-LABEL: load_extract_splat
+; AVX-NOT: rsp
+; AVX: vbroadcastss
+}
+
+; Fold extract of a load into the load's address computation. This avoids spilling to the stack.
+define <4 x float> @load_extract_splat1(<4 x float>* nocapture readonly %ptr, i64 %i, i64 %j) nounwind {
%1 = getelementptr inbounds <4 x float>* %ptr, i64 %i
%2 = load <4 x float>* %1, align 16
%3 = extractelement <4 x float> %2, i64 %j
%7 = insertelement <4 x float> %6, float %3, i32 3
ret <4 x float> %7
-; AVX-LABEL: load_extract_splat
+; AVX-LABEL: load_extract_splat1
; AVX-NOT: movs
; AVX: vbroadcastss
}