summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: d1fc0f8)
raw | patch | inline | side by side (parent: d1fc0f8)
author | Alexey Samsonov <samsonov@google.com> | |
Tue, 1 Oct 2013 16:25:14 +0000 (16:25 +0000) | ||
committer | Alexey Samsonov <samsonov@google.com> | |
Tue, 1 Oct 2013 16:25:14 +0000 (16:25 +0000) |
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@191779 91177308-0d34-0410-b5e6-96231b3b80d8
lib/DebugInfo/DWARFDebugAranges.cpp | patch | blob | history | |
lib/DebugInfo/DWARFDebugAranges.h | patch | blob | history |
index e2dfd30bed9f2ff1049af420956924669523f35e..6aa40b3d27ae12a3dc7d8c958e207c40649749ac 100644 (file)
#include <cassert>
using namespace llvm;
-// Compare function DWARFDebugAranges::Range structures
-static bool RangeLessThan(const DWARFDebugAranges::Range &range1,
- const DWARFDebugAranges::Range &range2) {
- return range1.LoPC < range2.LoPC;
-}
-
namespace {
class CountArangeDescriptors {
public:
CUOffsetCollection(CUOffsets) {}
void operator()(const DWARFDebugArangeSet &Set) {
DWARFDebugAranges::Range Range;
- Range.Offset = Set.getCompileUnitDIEOffset();
- CUOffsetCollection.insert(Range.Offset);
+ Range.CUOffset = Set.getCompileUnitDIEOffset();
+ CUOffsetCollection.insert(Range.CUOffset);
for (uint32_t i = 0, n = Set.getNumDescriptors(); i < n; ++i) {
const DWARFDebugArangeSet::Descriptor *ArangeDescPtr =
Set.getDescriptor(i);
- Range.LoPC = ArangeDescPtr->Address;
+ Range.LowPC = ArangeDescPtr->Address;
Range.Length = ArangeDescPtr->Length;
// Insert each item in increasing address order so binary searching
// can later be done!
DWARFDebugAranges::RangeColl::iterator InsertPos =
std::lower_bound(RangeCollection.begin(), RangeCollection.end(),
- Range, RangeLessThan);
+ Range);
RangeCollection.insert(InsertPos, Range);
}
}
}
}
- sort(true, /* overlap size */ 0);
+ sortAndMinimize();
}
void DWARFDebugAranges::dump(raw_ostream &OS) const {
void DWARFDebugAranges::Range::dump(raw_ostream &OS) const {
OS << format("{0x%8.8x}: [0x%8.8" PRIx64 " - 0x%8.8" PRIx64 ")\n",
- Offset, LoPC, HiPC());
+ CUOffset, LowPC, HighPC());
}
void DWARFDebugAranges::appendRange(uint32_t CUOffset, uint64_t LowPC,
uint64_t HighPC) {
if (!Aranges.empty()) {
- if (Aranges.back().Offset == CUOffset && Aranges.back().HiPC() == LowPC) {
- Aranges.back().setHiPC(HighPC);
+ if (Aranges.back().CUOffset == CUOffset &&
+ Aranges.back().HighPC() == LowPC) {
+ Aranges.back().setHighPC(HighPC);
return;
}
}
Aranges.push_back(Range(LowPC, HighPC, CUOffset));
}
-void DWARFDebugAranges::sort(bool Minimize, uint32_t OverlapSize) {
+void DWARFDebugAranges::sortAndMinimize() {
const size_t orig_arange_size = Aranges.size();
// Size of one? If so, no sorting is needed
if (orig_arange_size <= 1)
return;
// Sort our address range entries
- std::stable_sort(Aranges.begin(), Aranges.end(), RangeLessThan);
-
- if (!Minimize)
- return;
+ std::stable_sort(Aranges.begin(), Aranges.end());
// Most address ranges are contiguous from function to function
// so our new ranges will likely be smaller. We calculate the size
// copy the new minimal stuff over to the new collection.
size_t minimal_size = 1;
for (size_t i = 1; i < orig_arange_size; ++i) {
- if (!Range::SortedOverlapCheck(Aranges[i-1], Aranges[i], OverlapSize))
+ if (!Range::SortedOverlapCheck(Aranges[i-1], Aranges[i]))
++minimal_size;
}
uint32_t j = 0;
minimal_aranges[j] = Aranges[0];
for (size_t i = 1; i < orig_arange_size; ++i) {
- if (Range::SortedOverlapCheck(minimal_aranges[j], Aranges[i],
- OverlapSize)) {
- minimal_aranges[j].setHiPC (Aranges[i].HiPC());
+ if (Range::SortedOverlapCheck(minimal_aranges[j], Aranges[i])) {
+ minimal_aranges[j].setHighPC(Aranges[i].HighPC());
} else {
// Only increment j if we aren't merging
minimal_aranges[++j] = Aranges[i];
}
}
- assert (j+1 == minimal_size);
+ assert(j+1 == minimal_size);
// Now swap our new minimal aranges into place. The local
// minimal_aranges will then contian the old big collection
Range range(Address);
RangeCollIterator begin = Aranges.begin();
RangeCollIterator end = Aranges.end();
- RangeCollIterator pos = std::lower_bound(begin, end, range, RangeLessThan);
+ RangeCollIterator pos =
+ std::lower_bound(begin, end, range);
- if (pos != end && pos->LoPC <= Address && Address < pos->HiPC()) {
- return pos->Offset;
+ if (pos != end && pos->containsAddress(Address)) {
+ return pos->CUOffset;
} else if (pos != begin) {
--pos;
- if (pos->LoPC <= Address && Address < pos->HiPC())
- return (*pos).Offset;
+ if (pos->containsAddress(Address))
+ return pos->CUOffset;
}
}
return -1U;
index a5da2137ef445eab937bede9dbd5bc08ca0448fb..cbd7d53ab63d51f7f80d7ce0b382432a4e599f64 100644 (file)
class DWARFDebugAranges {
public:
struct Range {
- explicit Range(uint64_t lo = -1ULL, uint64_t hi = -1ULL,
- uint32_t off = -1U)
- : LoPC(lo), Length(hi-lo), Offset(off) {}
-
- void clear() {
- LoPC = -1ULL;
- Length = 0;
- Offset = -1U;
- }
+ explicit Range(uint64_t LowPC = -1ULL, uint64_t HighPC = -1ULL,
+ uint32_t CUOffset = -1U)
+ : LowPC(LowPC), Length(HighPC - LowPC), CUOffset(CUOffset) {}
- void setHiPC(uint64_t HiPC) {
- if (HiPC == -1ULL || HiPC <= LoPC)
+ void setHighPC(uint64_t HighPC) {
+ if (HighPC == -1ULL || HighPC <= LowPC)
Length = 0;
else
- Length = HiPC - LoPC;
+ Length = HighPC - LowPC;
}
- uint64_t HiPC() const {
+ uint64_t HighPC() const {
if (Length)
- return LoPC + Length;
+ return LowPC + Length;
return -1ULL;
}
- bool isValidRange() const { return Length > 0; }
+ bool containsAddress(uint64_t Address) const {
+ return LowPC <= Address && Address < HighPC();
+ }
- static bool SortedOverlapCheck(const Range &curr_range,
- const Range &next_range, uint32_t n) {
- if (curr_range.Offset != next_range.Offset)
- return false;
- return curr_range.HiPC() + n >= next_range.LoPC;
+ bool operator <(const Range &other) const {
+ return LowPC < other.LowPC;
}
- bool contains(const Range &range) const {
- return LoPC <= range.LoPC && range.HiPC() <= HiPC();
+ static bool SortedOverlapCheck(const Range &Left, const Range &Right) {
+ if (Left.CUOffset != Right.CUOffset)
+ return false;
+ return Left.HighPC() >= Right.LowPC;
}
void dump(raw_ostream &OS) const;
- uint64_t LoPC; // Start of address range
- uint32_t Length; // End of address range (not including this address)
- uint32_t Offset; // Offset of the compile unit or die
+ uint64_t LowPC; // Start of address range.
+ uint32_t Length; // End of address range (not including this address).
+ uint32_t CUOffset; // Offset of the compile unit or die.
};
void clear() {
void extract(DataExtractor DebugArangesData);
void generate(DWARFContext *CTX);
- // Use appendRange multiple times and then call sort.
+ // Use appendRange multiple times and then call sortAndMinimize.
void appendRange(uint32_t CUOffset, uint64_t LowPC, uint64_t HighPC);
- void sort(bool Minimize, uint32_t OverlapSize);
+ void sortAndMinimize();
void dump(raw_ostream &OS) const;
uint32_t findAddress(uint64_t Address) const;