summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 83d886d)
raw | patch | inline | side by side (parent: 83d886d)
author | Hal Finkel <hfinkel@anl.gov> | |
Sun, 7 Sep 2014 20:05:11 +0000 (20:05 +0000) | ||
committer | Hal Finkel <hfinkel@anl.gov> | |
Sun, 7 Sep 2014 20:05:11 +0000 (20:05 +0000) |
This adds a ScalarEvolution-powered transformation that updates load, store and
memory intrinsic pointer alignments based on invariant((a+q) & b == 0)
expressions. Many of the simple cases we can get with ValueTracking, but we
still need something like this for the more complicated cases (such as those
with an offset) that require some algebra. Note that gcc's
__builtin_assume_aligned's optional third argument provides exactly for this
kind of 'misalignment' offset for which this kind of logic is necessary.
The primary motivation is to fixup alignments for vector loads/stores after
vectorization (and unrolling). This pass is added to the optimization pipeline
just after the SLP vectorizer runs (which, admittedly, does not preserve SE,
although I imagine it could). Regardless, I actually don't think that the
preservation matters too much in this case: SE computes lazily, and this pass
won't issue any SE queries unless there are any assume intrinsics, so there
should be no real additional cost in the common case (SLP does preserve DT and
LoopInfo).
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@217344 91177308-0d34-0410-b5e6-96231b3b80d8
memory intrinsic pointer alignments based on invariant((a+q) & b == 0)
expressions. Many of the simple cases we can get with ValueTracking, but we
still need something like this for the more complicated cases (such as those
with an offset) that require some algebra. Note that gcc's
__builtin_assume_aligned's optional third argument provides exactly for this
kind of 'misalignment' offset for which this kind of logic is necessary.
The primary motivation is to fixup alignments for vector loads/stores after
vectorization (and unrolling). This pass is added to the optimization pipeline
just after the SLP vectorizer runs (which, admittedly, does not preserve SE,
although I imagine it could). Regardless, I actually don't think that the
preservation matters too much in this case: SE computes lazily, and this pass
won't issue any SE queries unless there are any assume intrinsics, so there
should be no real additional cost in the common case (SLP does preserve DT and
LoopInfo).
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@217344 91177308-0d34-0410-b5e6-96231b3b80d8
include/llvm-c/Transforms/Scalar.h | patch | blob | history | |
include/llvm/InitializePasses.h | patch | blob | history | |
include/llvm/LinkAllPasses.h | patch | blob | history | |
include/llvm/Transforms/Scalar.h | patch | blob | history | |
lib/Transforms/IPO/PassManagerBuilder.cpp | patch | blob | history | |
lib/Transforms/Scalar/AlignmentFromAssumptions.cpp | [new file with mode: 0644] | patch | blob |
lib/Transforms/Scalar/CMakeLists.txt | patch | blob | history | |
lib/Transforms/Scalar/Scalar.cpp | patch | blob | history | |
test/Transforms/AlignmentFromAssumptions/simple.ll | [new file with mode: 0644] | patch | blob |
index c0d670e30507ae5d83fa83dcca9f2e826ba8230a..a8ad772624b300bc83da448345fec38b7bc3598f 100644 (file)
/** See llvm::createAggressiveDCEPass function. */
void LLVMAddAggressiveDCEPass(LLVMPassManagerRef PM);
+/** See llvm::createAlignmentFromAssumptionsPass function. */
+void LLVMAddAlignmentFromAssumptionsPass(LLVMPassManagerRef PM);
+
/** See llvm::createCFGSimplificationPass function. */
void LLVMAddCFGSimplificationPass(LLVMPassManagerRef PM);
index b1dea4fa19f36fcda26ed41524f489aa222e4dbe..b0ec376267e31648cf3705edf48e17e3dcc97147 100644 (file)
void initializeArgPromotionPass(PassRegistry&);
void initializeAtomicExpandPass(PassRegistry&);
void initializeSampleProfileLoaderPass(PassRegistry&);
+void initializeAlignmentFromAssumptionsPass(PassRegistry&);
void initializeBarrierNoopPass(PassRegistry&);
void initializeBasicAliasAnalysisPass(PassRegistry&);
void initializeCallGraphWrapperPassPass(PassRegistry &);
index 12ae11e4ee5c2681de48d606831061b51963a382..81e82638255f45061533d33e55f1fc10d75ab88c 100644 (file)
(void) llvm::createAliasAnalysisCounterPass();
(void) llvm::createAliasDebugger();
(void) llvm::createArgumentPromotionPass();
+ (void) llvm::createAlignmentFromAssumptionsPass();
(void) llvm::createBasicAliasAnalysisPass();
(void) llvm::createLibCallAliasAnalysisPass(nullptr);
(void) llvm::createScalarEvolutionAliasAnalysisPass();
index 413134e51c7ab043c8400f2c338eb4f6ec9a320c..7a561ee5b24afd31879208a8f4d693d318dcbee4 100644 (file)
//
FunctionPass *createConstantPropagationPass();
+//===----------------------------------------------------------------------===//
+//
+// AlignmentFromAssumptions - Use assume intrinsics to set load/store
+// alignments.
+//
+FunctionPass *createAlignmentFromAssumptionsPass();
+
//===----------------------------------------------------------------------===//
//
// SCCP - Sparse conditional constant propagation.
index 75714713172d4ce2f655a504f263ef331b72df3f..fb56088d3617ff2214b2e3459cf9d9ac1a21136b 100644 (file)
if (!DisableUnrollLoops)
MPM.add(createLoopUnrollPass()); // Unroll small loops
+ // After vectorization and unrolling, assume intrinsics may tell us more
+ // about pointer alignments.
+ MPM.add(createAlignmentFromAssumptionsPass());
+
if (!DisableUnitAtATime) {
// FIXME: We shouldn't bother with this anymore.
MPM.add(createStripDeadPrototypesPass()); // Get rid of dead prototypes
// More scalar chains could be vectorized due to more alias information
PM.add(createSLPVectorizerPass()); // Vectorize parallel scalar chains.
+ // After vectorization, assume intrinsics may tell us more about pointer
+ // alignments.
+ PM.add(createAlignmentFromAssumptionsPass());
+
if (LoadCombine)
PM.add(createLoadCombinePass());
diff --git a/lib/Transforms/Scalar/AlignmentFromAssumptions.cpp b/lib/Transforms/Scalar/AlignmentFromAssumptions.cpp
--- /dev/null
@@ -0,0 +1,420 @@
+//===----------------------- AlignmentFromAssumptions.cpp -----------------===//
+// Set Load/Store Alignments From Assumptions
+//
+// The LLVM Compiler Infrastructure
+//
+// This file is distributed under the University of Illinois Open Source
+// License. See LICENSE.TXT for details.
+//
+//===----------------------------------------------------------------------===//
+//
+// This file implements a ScalarEvolution-based transformation to set
+// the alignments of load, stores and memory intrinsics based on the truth
+// expressions of assume intrinsics. The primary motivation is to handle
+// complex alignment assumptions that apply to vector loads and stores that
+// appear after vectorization and unrolling.
+//
+//===----------------------------------------------------------------------===//
+
+#define AA_NAME "alignment-from-assumptions"
+#define DEBUG_TYPE AA_NAME
+#include "llvm/Transforms/Scalar.h"
+#include "llvm/ADT/SmallPtrSet.h"
+#include "llvm/ADT/Statistic.h"
+#include "llvm/Analysis/AssumptionTracker.h"
+#include "llvm/Analysis/LoopInfo.h"
+#include "llvm/Analysis/ValueTracking.h"
+#include "llvm/Analysis/ScalarEvolution.h"
+#include "llvm/Analysis/ScalarEvolutionExpressions.h"
+#include "llvm/IR/Constant.h"
+#include "llvm/IR/Dominators.h"
+#include "llvm/IR/Instruction.h"
+#include "llvm/IR/IntrinsicInst.h"
+#include "llvm/IR/Intrinsics.h"
+#include "llvm/IR/DataLayout.h"
+#include "llvm/Support/Debug.h"
+#include "llvm/Support/raw_ostream.h"
+using namespace llvm;
+
+STATISTIC(NumLoadAlignChanged,
+ "Number of loads changed by alignment assumptions");
+STATISTIC(NumStoreAlignChanged,
+ "Number of stores changed by alignment assumptions");
+STATISTIC(NumMemIntAlignChanged,
+ "Number of memory intrinsics changed by alignment assumptions");
+
+namespace {
+struct AlignmentFromAssumptions : public FunctionPass {
+ static char ID; // Pass identification, replacement for typeid
+ AlignmentFromAssumptions() : FunctionPass(ID) {
+ initializeAlignmentFromAssumptionsPass(*PassRegistry::getPassRegistry());
+ }
+
+ bool runOnFunction(Function &F);
+
+ virtual void getAnalysisUsage(AnalysisUsage &AU) const {
+ AU.addRequired<AssumptionTracker>();
+ AU.addRequired<ScalarEvolution>();
+ AU.addRequired<DominatorTreeWrapperPass>();
+
+ AU.setPreservesCFG();
+ AU.addPreserved<LoopInfo>();
+ AU.addPreserved<DominatorTreeWrapperPass>();
+ AU.addPreserved<ScalarEvolution>();
+ }
+
+ // For memory transfers, we need a common alignment for both the source and
+ // destination. If we have a new alignment for only one operand of a transfer
+ // instruction, save it in these maps. If we reach the other operand through
+ // another assumption later, then we may change the alignment at that point.
+ DenseMap<MemTransferInst *, unsigned> NewDestAlignments, NewSrcAlignments;
+
+ AssumptionTracker *AT;
+ ScalarEvolution *SE;
+ DominatorTree *DT;
+ const DataLayout *DL;
+
+ bool extractAlignmentInfo(CallInst *I, Value *&AAPtr, const SCEV *&AlignSCEV,
+ const SCEV *&OffSCEV);
+ bool processAssumption(CallInst *I);
+};
+}
+
+char AlignmentFromAssumptions::ID = 0;
+static const char aip_name[] = "Alignment from assumptions";
+INITIALIZE_PASS_BEGIN(AlignmentFromAssumptions, AA_NAME,
+ aip_name, false, false)
+INITIALIZE_PASS_DEPENDENCY(AssumptionTracker)
+INITIALIZE_PASS_DEPENDENCY(DominatorTreeWrapperPass)
+INITIALIZE_PASS_DEPENDENCY(ScalarEvolution)
+INITIALIZE_PASS_END(AlignmentFromAssumptions, AA_NAME,
+ aip_name, false, false)
+
+FunctionPass *llvm::createAlignmentFromAssumptionsPass() {
+ return new AlignmentFromAssumptions();
+}
+
+// Given an expression for the (constant) alignment, AlignSCEV, and an
+// expression for the displacement between a pointer and the aligned address,
+// DiffSCEV, compute the alignment of the displaced pointer if it can be
+// reduced to a constant.
+static unsigned getNewAlignmentDiff(const SCEV *DiffSCEV,
+ const SCEV *AlignSCEV,
+ ScalarEvolution *SE) {
+ // DiffUnits = Diff % int64_t(Alignment)
+ const SCEV *DiffAlignDiv = SE->getUDivExpr(DiffSCEV, AlignSCEV);
+ const SCEV *DiffAlign = SE->getMulExpr(DiffAlignDiv, AlignSCEV);
+ const SCEV *DiffUnitsSCEV = SE->getMinusSCEV(DiffAlign, DiffSCEV);
+
+ DEBUG(dbgs() << "\talignment relative to " << *AlignSCEV << " is " <<
+ *DiffUnitsSCEV << " (diff: " << *DiffSCEV << ")\n");
+
+ if (const SCEVConstant *ConstDUSCEV =
+ dyn_cast<SCEVConstant>(DiffUnitsSCEV)) {
+ int64_t DiffUnits = ConstDUSCEV->getValue()->getSExtValue();
+
+ // If the displacement is an exact multiple of the alignment, then the
+ // displaced pointer has the same alignment as the aligned pointer, so
+ // return the alignment value.
+ if (!DiffUnits)
+ return (unsigned)
+ cast<SCEVConstant>(AlignSCEV)->getValue()->getSExtValue();
+
+ // If the displacement is not an exact multiple, but the remainder is a
+ // constant, then return this remainder (but only if it is a power of 2).
+ uint64_t DiffUnitsAbs = abs64(DiffUnits);
+ if (isPowerOf2_64(DiffUnitsAbs))
+ return (unsigned) DiffUnitsAbs;
+ }
+
+ return 0;
+}
+
+// There is an address given by an offset OffSCEV from AASCEV which has an
+// alignment AlignSCEV. Use that information, if possible, to compute a new
+// alignment for Ptr.
+static unsigned getNewAlignment(const SCEV *AASCEV, const SCEV *AlignSCEV,
+ const SCEV *OffSCEV, Value *Ptr,
+ ScalarEvolution *SE) {
+ const SCEV *PtrSCEV = SE->getSCEV(Ptr);
+ const SCEV *DiffSCEV = SE->getMinusSCEV(PtrSCEV, AASCEV);
+
+ // What we really want to know is the overall offset to the aligned
+ // address. This address is displaced by the provided offset.
+ DiffSCEV = SE->getMinusSCEV(DiffSCEV, OffSCEV);
+
+ DEBUG(dbgs() << "AFI: alignment of " << *Ptr << " relative to " <<
+ *AlignSCEV << " and offset " << *OffSCEV <<
+ " using diff " << *DiffSCEV << "\n");
+
+ unsigned NewAlignment = getNewAlignmentDiff(DiffSCEV, AlignSCEV, SE);
+ DEBUG(dbgs() << "\tnew alignment: " << NewAlignment << "\n");
+
+ if (NewAlignment) {
+ return NewAlignment;
+ } else if (const SCEVAddRecExpr *DiffARSCEV =
+ dyn_cast<SCEVAddRecExpr>(DiffSCEV)) {
+ // The relative offset to the alignment assumption did not yield a constant,
+ // but we should try harder: if we assume that a is 32-byte aligned, then in
+ // for (i = 0; i < 1024; i += 4) r += a[i]; not all of the loads from a are
+ // 32-byte aligned, but instead alternate between 32 and 16-byte alignment.
+ // As a result, the new alignment will not be a constant, but can still
+ // be improved over the default (of 4) to 16.
+
+ const SCEV *DiffStartSCEV = DiffARSCEV->getStart();
+ const SCEV *DiffIncSCEV = DiffARSCEV->getStepRecurrence(*SE);
+
+ DEBUG(dbgs() << "\ttrying start/inc alignment using start " <<
+ *DiffStartSCEV << " and inc " << *DiffIncSCEV << "\n");
+
+ // Now compute the new alignment using the displacement to the value in the
+ // first iteration, and also the alignment using the per-iteration delta.
+ // If these are the same, then use that answer. Otherwise, use the smaller
+ // one, but only if it divides the larger one.
+ NewAlignment = getNewAlignmentDiff(DiffStartSCEV, AlignSCEV, SE);
+ unsigned NewIncAlignment = getNewAlignmentDiff(DiffIncSCEV, AlignSCEV, SE);
+
+ DEBUG(dbgs() << "\tnew start alignment: " << NewAlignment << "\n");
+ DEBUG(dbgs() << "\tnew inc alignment: " << NewIncAlignment << "\n");
+
+ if (NewAlignment > NewIncAlignment) {
+ if (NewAlignment % NewIncAlignment == 0) {
+ DEBUG(dbgs() << "\tnew start/inc alignment: " <<
+ NewIncAlignment << "\n");
+ return NewIncAlignment;
+ }
+ } else if (NewIncAlignment > NewAlignment) {
+ if (NewIncAlignment % NewAlignment == 0) {
+ DEBUG(dbgs() << "\tnew start/inc alignment: " <<
+ NewAlignment << "\n");
+ return NewAlignment;
+ }
+ } else if (NewIncAlignment == NewAlignment && NewIncAlignment) {
+ DEBUG(dbgs() << "\tnew start/inc alignment: " <<
+ NewAlignment << "\n");
+ return NewAlignment;
+ }
+ }
+
+ return 0;
+}
+
+bool AlignmentFromAssumptions::extractAlignmentInfo(CallInst *I,
+ Value *&AAPtr, const SCEV *&AlignSCEV,
+ const SCEV *&OffSCEV) {
+ // An alignment assume must be a statement about the least-significant
+ // bits of the pointer being zero, possibly with some offset.
+ ICmpInst *ICI = dyn_cast<ICmpInst>(I->getArgOperand(0));
+ if (!ICI)
+ return false;
+
+ // This must be an expression of the form: x & m == 0.
+ if (ICI->getPredicate() != ICmpInst::ICMP_EQ)
+ return false;
+
+ // Swap things around so that the RHS is 0.
+ Value *CmpLHS = ICI->getOperand(0);
+ Value *CmpRHS = ICI->getOperand(1);
+ const SCEV *CmpLHSSCEV = SE->getSCEV(CmpLHS);
+ const SCEV *CmpRHSSCEV = SE->getSCEV(CmpRHS);
+ if (CmpLHSSCEV->isZero())
+ std::swap(CmpLHS, CmpRHS);
+ else if (!CmpRHSSCEV->isZero())
+ return false;
+
+ BinaryOperator *CmpBO = dyn_cast<BinaryOperator>(CmpLHS);
+ if (!CmpBO || CmpBO->getOpcode() != Instruction::And)
+ return false;
+
+ // Swap things around so that the right operand of the and is a constant
+ // (the mask); we cannot deal with variable masks.
+ Value *AndLHS = CmpBO->getOperand(0);
+ Value *AndRHS = CmpBO->getOperand(1);
+ const SCEV *AndLHSSCEV = SE->getSCEV(AndLHS);
+ const SCEV *AndRHSSCEV = SE->getSCEV(AndRHS);
+ if (isa<SCEVConstant>(AndLHSSCEV)) {
+ std::swap(AndLHS, AndRHS);
+ std::swap(AndLHSSCEV, AndRHSSCEV);
+ }
+
+ const SCEVConstant *MaskSCEV = dyn_cast<SCEVConstant>(AndRHSSCEV);
+ if (!MaskSCEV)
+ return false;
+
+ // The mask must have some trailing ones (otherwise the condition is
+ // trivial and tells us nothing about the alignment of the left operand).
+ unsigned TrailingOnes =
+ MaskSCEV->getValue()->getValue().countTrailingOnes();
+ if (!TrailingOnes)
+ return false;
+
+ // Cap the alignment at the maximum with which LLVM can deal (and make sure
+ // we don't overflow the shift).
+ uint64_t Alignment;
+ TrailingOnes = std::min(TrailingOnes,
+ unsigned(sizeof(unsigned) * CHAR_BIT - 1));
+ Alignment = std::min(1u << TrailingOnes, +Value::MaximumAlignment);
+
+ Type *Int64Ty = Type::getInt64Ty(I->getParent()->getParent()->getContext());
+ AlignSCEV = SE->getConstant(Int64Ty, Alignment);
+
+ // The LHS might be a ptrtoint instruction, or it might be the pointer
+ // with an offset.
+ AAPtr = nullptr;
+ OffSCEV = nullptr;
+ if (PtrToIntInst *PToI = dyn_cast<PtrToIntInst>(AndLHS)) {
+ AAPtr = PToI->getPointerOperand();
+ OffSCEV = SE->getConstant(Int64Ty, 0);
+ } else if (const SCEVAddExpr* AndLHSAddSCEV =
+ dyn_cast<SCEVAddExpr>(AndLHSSCEV)) {
+ // Try to find the ptrtoint; subtract it and the rest is the offset.
+ for (SCEVAddExpr::op_iterator J = AndLHSAddSCEV->op_begin(),
+ JE = AndLHSAddSCEV->op_end(); J != JE; ++J)
+ if (const SCEVUnknown *OpUnk = dyn_cast<SCEVUnknown>(*J))
+ if (PtrToIntInst *PToI = dyn_cast<PtrToIntInst>(OpUnk->getValue())) {
+ AAPtr = PToI->getPointerOperand();
+ OffSCEV = SE->getMinusSCEV(AndLHSAddSCEV, *J);
+ break;
+ }
+ }
+
+ if (!AAPtr)
+ return false;
+
+ // Sign extend the offset to 64 bits (so that it is like all of the other
+ // expressions).
+ unsigned OffSCEVBits = OffSCEV->getType()->getPrimitiveSizeInBits();
+ if (OffSCEVBits < 64)
+ OffSCEV = SE->getSignExtendExpr(OffSCEV, Int64Ty);
+ else if (OffSCEVBits > 64)
+ return false;
+
+ AAPtr = AAPtr->stripPointerCasts();
+ return true;
+}
+
+bool AlignmentFromAssumptions::processAssumption(CallInst *ACall) {
+ Value *AAPtr;
+ const SCEV *AlignSCEV, *OffSCEV;
+ if (!extractAlignmentInfo(ACall, AAPtr, AlignSCEV, OffSCEV))
+ return false;
+
+ const SCEV *AASCEV = SE->getSCEV(AAPtr);
+
+ // Apply the assumption to all other users of the specified pointer.
+ SmallPtrSet<Instruction *, 32> Visited;
+ SmallVector<Instruction*, 16> WorkList;
+ for (User *J : AAPtr->users()) {
+ if (J == ACall)
+ continue;
+
+ if (Instruction *K = dyn_cast<Instruction>(J))
+ if (isValidAssumeForContext(ACall, K, DL, DT))
+ WorkList.push_back(K);
+ }
+
+ while (!WorkList.empty()) {
+ Instruction *J = WorkList.pop_back_val();
+
+ if (LoadInst *LI = dyn_cast<LoadInst>(J)) {
+ unsigned NewAlignment = getNewAlignment(AASCEV, AlignSCEV, OffSCEV,
+ LI->getPointerOperand(), SE);
+
+ if (NewAlignment > LI->getAlignment()) {
+ LI->setAlignment(NewAlignment);
+ ++NumLoadAlignChanged;
+ }
+ } else if (StoreInst *SI = dyn_cast<StoreInst>(J)) {
+ unsigned NewAlignment = getNewAlignment(AASCEV, AlignSCEV, OffSCEV,
+ SI->getPointerOperand(), SE);
+
+ if (NewAlignment > SI->getAlignment()) {
+ SI->setAlignment(NewAlignment);
+ ++NumStoreAlignChanged;
+ }
+ } else if (MemIntrinsic *MI = dyn_cast<MemIntrinsic>(J)) {
+ unsigned NewDestAlignment = getNewAlignment(AASCEV, AlignSCEV, OffSCEV,
+ MI->getDest(), SE);
+
+ // For memory transfers, we need a common alignment for both the
+ // source and destination. If we have a new alignment for this
+ // instruction, but only for one operand, save it. If we reach the
+ // other operand through another assumption later, then we may
+ // change the alignment at that point.
+ if (MemTransferInst *MTI = dyn_cast<MemTransferInst>(MI)) {
+ unsigned NewSrcAlignment = getNewAlignment(AASCEV, AlignSCEV, OffSCEV,
+ MTI->getSource(), SE);
+
+ DenseMap<MemTransferInst *, unsigned>::iterator DI =
+ NewDestAlignments.find(MTI);
+ unsigned AltDestAlignment = (DI == NewDestAlignments.end()) ?
+ 0 : DI->second;
+
+ DenseMap<MemTransferInst *, unsigned>::iterator SI =
+ NewSrcAlignments.find(MTI);
+ unsigned AltSrcAlignment = (SI == NewSrcAlignments.end()) ?
+ 0 : SI->second;
+
+ DEBUG(dbgs() << "\tmem trans: " << NewDestAlignment << " " <<
+ AltDestAlignment << " " << NewSrcAlignment <<
+ " " << AltSrcAlignment << "\n");
+
+ // Of these four alignments, pick the largest possible...
+ unsigned NewAlignment = 0;
+ if (NewDestAlignment <= std::max(NewSrcAlignment, AltSrcAlignment))
+ NewAlignment = std::max(NewAlignment, NewDestAlignment);
+ if (AltDestAlignment <= std::max(NewSrcAlignment, AltSrcAlignment))
+ NewAlignment = std::max(NewAlignment, AltDestAlignment);
+ if (NewSrcAlignment <= std::max(NewDestAlignment, AltDestAlignment))
+ NewAlignment = std::max(NewAlignment, NewSrcAlignment);
+ if (AltSrcAlignment <= std::max(NewDestAlignment, AltDestAlignment))
+ NewAlignment = std::max(NewAlignment, AltSrcAlignment);
+
+ if (NewAlignment > MI->getAlignment()) {
+ MI->setAlignment(ConstantInt::get(Type::getInt32Ty(
+ MI->getParent()->getContext()), NewAlignment));
+ ++NumMemIntAlignChanged;
+ }
+
+ NewDestAlignments.insert(std::make_pair(MTI, NewDestAlignment));
+ NewSrcAlignments.insert(std::make_pair(MTI, NewSrcAlignment));
+ } else if (NewDestAlignment > MI->getAlignment()) {
+ assert((!isa<MemIntrinsic>(MI) || isa<MemSetInst>(MI)) &&
+ "Unknown memory intrinsic");
+
+ MI->setAlignment(ConstantInt::get(Type::getInt32Ty(
+ MI->getParent()->getContext()), NewDestAlignment));
+ ++NumMemIntAlignChanged;
+ }
+ }
+
+ // Now that we've updated that use of the pointer, look for other uses of
+ // the pointer to update.
+ Visited.insert(J);
+ for (User *UJ : J->users()) {
+ Instruction *K = cast<Instruction>(UJ);
+ if (!Visited.count(K) && isValidAssumeForContext(ACall, K, DL, DT))
+ WorkList.push_back(K);
+ }
+ }
+
+ return true;
+}
+
+bool AlignmentFromAssumptions::runOnFunction(Function &F) {
+ bool Changed = false;
+ AT = &getAnalysis<AssumptionTracker>();
+ SE = &getAnalysis<ScalarEvolution>();
+ DT = &getAnalysis<DominatorTreeWrapperPass>().getDomTree();
+ DataLayoutPass *DLP = getAnalysisIfAvailable<DataLayoutPass>();
+ DL = DLP ? &DLP->getDataLayout() : nullptr;
+
+ NewDestAlignments.clear();
+ NewSrcAlignments.clear();
+
+ for (auto &I : AT->assumptions(&F))
+ Changed |= processAssumption(I);
+
+ return Changed;
+}
+
index 261ddda301505e6f93744ad55c70d6c199960f15..b3ee11ed67cd61b1911fa8638e9bb024eb568658 100644 (file)
add_llvm_library(LLVMScalarOpts
ADCE.cpp
+ AlignmentFromAssumptions.cpp
ConstantHoisting.cpp
ConstantProp.cpp
CorrelatedValuePropagation.cpp
index 4bebb426eec667fdcbc4cc86a66781e5acc0aca8..fbdc22771680d671f3f9570f7f8fb69f4b6608a9 100644 (file)
/// ScalarOpts library.
void llvm::initializeScalarOpts(PassRegistry &Registry) {
initializeADCEPass(Registry);
+ initializeAlignmentFromAssumptionsPass(Registry);
initializeSampleProfileLoaderPass(Registry);
initializeConstantHoistingPass(Registry);
initializeConstantPropagationPass(Registry);
unwrap(PM)->add(createAggressiveDCEPass());
}
+void LLVMAddAlignmentFromAssumptionsPass(LLVMPassManagerRef PM) {
+ unwrap(PM)->add(createAlignmentFromAssumptionsPass());
+}
+
void LLVMAddCFGSimplificationPass(LLVMPassManagerRef PM) {
unwrap(PM)->add(createCFGSimplificationPass());
}
diff --git a/test/Transforms/AlignmentFromAssumptions/simple.ll b/test/Transforms/AlignmentFromAssumptions/simple.ll
--- /dev/null
@@ -0,0 +1,215 @@
+target datalayout = "e-i64:64-f80:128-n8:16:32:64-S128"
+; RUN: opt < %s -alignment-from-assumptions -S | FileCheck %s
+
+define i32 @foo(i32* nocapture %a) nounwind uwtable readonly {
+entry:
+ %ptrint = ptrtoint i32* %a to i64
+ %maskedptr = and i64 %ptrint, 31
+ %maskcond = icmp eq i64 %maskedptr, 0
+ tail call void @llvm.assume(i1 %maskcond)
+ %0 = load i32* %a, align 4
+ ret i32 %0
+
+; CHECK-LABEL: @foo
+; CHECK: load i32* {{[^,]+}}, align 32
+; CHECK: ret i32
+}
+
+define i32 @foo2(i32* nocapture %a) nounwind uwtable readonly {
+entry:
+ %ptrint = ptrtoint i32* %a to i64
+ %offsetptr = add i64 %ptrint, 24
+ %maskedptr = and i64 %offsetptr, 31
+ %maskcond = icmp eq i64 %maskedptr, 0
+ tail call void @llvm.assume(i1 %maskcond)
+ %arrayidx = getelementptr inbounds i32* %a, i64 2
+ %0 = load i32* %arrayidx, align 4
+ ret i32 %0
+
+; CHECK-LABEL: @foo2
+; CHECK: load i32* {{[^,]+}}, align 16
+; CHECK: ret i32
+}
+
+define i32 @foo2a(i32* nocapture %a) nounwind uwtable readonly {
+entry:
+ %ptrint = ptrtoint i32* %a to i64
+ %offsetptr = add i64 %ptrint, 28
+ %maskedptr = and i64 %offsetptr, 31
+ %maskcond = icmp eq i64 %maskedptr, 0
+ tail call void @llvm.assume(i1 %maskcond)
+ %arrayidx = getelementptr inbounds i32* %a, i64 -1
+ %0 = load i32* %arrayidx, align 4
+ ret i32 %0
+
+; CHECK-LABEL: @foo2a
+; CHECK: load i32* {{[^,]+}}, align 32
+; CHECK: ret i32
+}
+
+define i32 @goo(i32* nocapture %a) nounwind uwtable readonly {
+entry:
+ %ptrint = ptrtoint i32* %a to i64
+ %maskedptr = and i64 %ptrint, 31
+ %maskcond = icmp eq i64 %maskedptr, 0
+ tail call void @llvm.assume(i1 %maskcond)
+ %0 = load i32* %a, align 4
+ ret i32 %0
+
+; CHECK-LABEL: @goo
+; CHECK: load i32* {{[^,]+}}, align 32
+; CHECK: ret i32
+}
+
+define i32 @hoo(i32* nocapture %a) nounwind uwtable readonly {
+entry:
+ %ptrint = ptrtoint i32* %a to i64
+ %maskedptr = and i64 %ptrint, 31
+ %maskcond = icmp eq i64 %maskedptr, 0
+ tail call void @llvm.assume(i1 %maskcond)
+ br label %for.body
+
+for.body: ; preds = %entry, %for.body
+ %indvars.iv = phi i64 [ 0, %entry ], [ %indvars.iv.next, %for.body ]
+ %r.06 = phi i32 [ 0, %entry ], [ %add, %for.body ]
+ %arrayidx = getelementptr inbounds i32* %a, i64 %indvars.iv
+ %0 = load i32* %arrayidx, align 4
+ %add = add nsw i32 %0, %r.06
+ %indvars.iv.next = add i64 %indvars.iv, 8
+ %1 = trunc i64 %indvars.iv.next to i32
+ %cmp = icmp slt i32 %1, 2048
+ br i1 %cmp, label %for.body, label %for.end
+
+for.end: ; preds = %for.body
+ %add.lcssa = phi i32 [ %add, %for.body ]
+ ret i32 %add.lcssa
+
+; CHECK-LABEL: @hoo
+; CHECK: load i32* %arrayidx, align 32
+; CHECK: ret i32 %add.lcssa
+}
+
+define i32 @joo(i32* nocapture %a) nounwind uwtable readonly {
+entry:
+ %ptrint = ptrtoint i32* %a to i64
+ %maskedptr = and i64 %ptrint, 31
+ %maskcond = icmp eq i64 %maskedptr, 0
+ tail call void @llvm.assume(i1 %maskcond)
+ br label %for.body
+
+for.body: ; preds = %entry, %for.body
+ %indvars.iv = phi i64 [ 4, %entry ], [ %indvars.iv.next, %for.body ]
+ %r.06 = phi i32 [ 0, %entry ], [ %add, %for.body ]
+ %arrayidx = getelementptr inbounds i32* %a, i64 %indvars.iv
+ %0 = load i32* %arrayidx, align 4
+ %add = add nsw i32 %0, %r.06
+ %indvars.iv.next = add i64 %indvars.iv, 8
+ %1 = trunc i64 %indvars.iv.next to i32
+ %cmp = icmp slt i32 %1, 2048
+ br i1 %cmp, label %for.body, label %for.end
+
+for.end: ; preds = %for.body
+ %add.lcssa = phi i32 [ %add, %for.body ]
+ ret i32 %add.lcssa
+
+; CHECK-LABEL: @joo
+; CHECK: load i32* %arrayidx, align 16
+; CHECK: ret i32 %add.lcssa
+}
+
+define i32 @koo(i32* nocapture %a) nounwind uwtable readonly {
+entry:
+ %ptrint = ptrtoint i32* %a to i64
+ %maskedptr = and i64 %ptrint, 31
+ %maskcond = icmp eq i64 %maskedptr, 0
+ tail call void @llvm.assume(i1 %maskcond)
+ br label %for.body
+
+for.body: ; preds = %entry, %for.body
+ %indvars.iv = phi i64 [ 0, %entry ], [ %indvars.iv.next, %for.body ]
+ %r.06 = phi i32 [ 0, %entry ], [ %add, %for.body ]
+ %arrayidx = getelementptr inbounds i32* %a, i64 %indvars.iv
+ %0 = load i32* %arrayidx, align 4
+ %add = add nsw i32 %0, %r.06
+ %indvars.iv.next = add i64 %indvars.iv, 4
+ %1 = trunc i64 %indvars.iv.next to i32
+ %cmp = icmp slt i32 %1, 2048
+ br i1 %cmp, label %for.body, label %for.end
+
+for.end: ; preds = %for.body
+ %add.lcssa = phi i32 [ %add, %for.body ]
+ ret i32 %add.lcssa
+
+; CHECK-LABEL: @koo
+; CHECK: load i32* %arrayidx, align 16
+; CHECK: ret i32 %add.lcssa
+}
+
+define i32 @koo2(i32* nocapture %a) nounwind uwtable readonly {
+entry:
+ %ptrint = ptrtoint i32* %a to i64
+ %maskedptr = and i64 %ptrint, 31
+ %maskcond = icmp eq i64 %maskedptr, 0
+ tail call void @llvm.assume(i1 %maskcond)
+ br label %for.body
+
+for.body: ; preds = %entry, %for.body
+ %indvars.iv = phi i64 [ -4, %entry ], [ %indvars.iv.next, %for.body ]
+ %r.06 = phi i32 [ 0, %entry ], [ %add, %for.body ]
+ %arrayidx = getelementptr inbounds i32* %a, i64 %indvars.iv
+ %0 = load i32* %arrayidx, align 4
+ %add = add nsw i32 %0, %r.06
+ %indvars.iv.next = add i64 %indvars.iv, 4
+ %1 = trunc i64 %indvars.iv.next to i32
+ %cmp = icmp slt i32 %1, 2048
+ br i1 %cmp, label %for.body, label %for.end
+
+for.end: ; preds = %for.body
+ %add.lcssa = phi i32 [ %add, %for.body ]
+ ret i32 %add.lcssa
+
+; CHECK-LABEL: @koo2
+; CHECK: load i32* %arrayidx, align 16
+; CHECK: ret i32 %add.lcssa
+}
+
+define i32 @moo(i32* nocapture %a) nounwind uwtable {
+entry:
+ %ptrint = ptrtoint i32* %a to i64
+ %maskedptr = and i64 %ptrint, 31
+ %maskcond = icmp eq i64 %maskedptr, 0
+ tail call void @llvm.assume(i1 %maskcond)
+ %0 = bitcast i32* %a to i8*
+ tail call void @llvm.memset.p0i8.i64(i8* %0, i8 0, i64 64, i32 4, i1 false)
+ ret i32 undef
+
+; CHECK-LABEL: @moo
+; CHECK: @llvm.memset.p0i8.i64(i8* %0, i8 0, i64 64, i32 32, i1 false)
+; CHECK: ret i32 undef
+}
+
+define i32 @moo2(i32* nocapture %a, i32* nocapture %b) nounwind uwtable {
+entry:
+ %ptrint = ptrtoint i32* %a to i64
+ %maskedptr = and i64 %ptrint, 31
+ %maskcond = icmp eq i64 %maskedptr, 0
+ tail call void @llvm.assume(i1 %maskcond)
+ %ptrint1 = ptrtoint i32* %b to i64
+ %maskedptr3 = and i64 %ptrint1, 127
+ %maskcond4 = icmp eq i64 %maskedptr3, 0
+ tail call void @llvm.assume(i1 %maskcond4)
+ %0 = bitcast i32* %a to i8*
+ %1 = bitcast i32* %b to i8*
+ tail call void @llvm.memcpy.p0i8.p0i8.i64(i8* %0, i8* %1, i64 64, i32 4, i1 false)
+ ret i32 undef
+
+; CHECK-LABEL: @moo2
+; CHECK: @llvm.memcpy.p0i8.p0i8.i64(i8* %0, i8* %1, i64 64, i32 32, i1 false)
+; CHECK: ret i32 undef
+}
+
+declare void @llvm.assume(i1) nounwind
+
+declare void @llvm.memset.p0i8.i64(i8* nocapture, i8, i64, i32, i1) nounwind
+declare void @llvm.memcpy.p0i8.p0i8.i64(i8* nocapture, i8* nocapture, i64, i32, i1) nounwind
+