summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: af4e764)
raw | patch | inline | side by side (parent: af4e764)
author | Duncan P. N. Exon Smith <dexonsmith@apple.com> | |
Wed, 6 Aug 2014 17:36:08 +0000 (17:36 +0000) | ||
committer | Duncan P. N. Exon Smith <dexonsmith@apple.com> | |
Wed, 6 Aug 2014 17:36:08 +0000 (17:36 +0000) |
I initially used a `SmallVector<>` for `UseListOrder::Shuffle`, which
was a silly choice. When I realized my error I quickly rolled a custom
data structure.
This commit simplifies it to a `std::vector<>`. Now that I've had a
chance to measure performance, this data structure isn't part of a
bottleneck, so the additional complexity is unnecessary.
This is part of PR5680.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214979 91177308-0d34-0410-b5e6-96231b3b80d8
was a silly choice. When I realized my error I quickly rolled a custom
data structure.
This commit simplifies it to a `std::vector<>`. Now that I've had a
chance to measure performance, this data structure isn't part of a
bottleneck, so the additional complexity is unnecessary.
This is part of PR5680.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214979 91177308-0d34-0410-b5e6-96231b3b80d8
include/llvm/IR/UseListOrder.h | patch | blob | history |
index 8a2a109578e0da0d1f30189902d2b7a26f9d6af5..c4e476160aa15362b08f9072c53671eafd65abe5 100644 (file)
class Function;
class Value;
-/// \brief Structure to hold a use-list shuffle vector.
-///
-/// Stores most use-lists locally, but large use-lists use an extra heap entry.
-/// Costs two fewer pointers than the equivalent \a SmallVector.
-class UseListShuffleVector {
- unsigned Size;
- union {
- unsigned *Ptr;
- unsigned Array[6];
- } Storage;
-
- bool isSmall() const { return Size <= 6; }
- unsigned *data() { return isSmall() ? Storage.Array : Storage.Ptr; }
- const unsigned *data() const {
- return isSmall() ? Storage.Array : Storage.Ptr;
- }
-
- void destroy() {
- if (!isSmall())
- delete[] Storage.Ptr;
- }
- void moveUnchecked(UseListShuffleVector &X) {
- std::memcpy(this, &X, sizeof(UseListShuffleVector));
- X.Size = 0;
- }
-
- UseListShuffleVector(const UseListShuffleVector &X) LLVM_DELETED_FUNCTION;
- UseListShuffleVector &
- operator=(const UseListShuffleVector &X) LLVM_DELETED_FUNCTION;
-
-public:
- UseListShuffleVector() : Size(0) {}
- UseListShuffleVector(UseListShuffleVector &&X) { moveUnchecked(X); }
- UseListShuffleVector &operator=(UseListShuffleVector &&X) {
- destroy();
- moveUnchecked(X);
- return *this;
- }
- explicit UseListShuffleVector(size_t Size) : Size(Size) {
- if (!isSmall())
- Storage.Ptr = new unsigned[Size];
- }
- ~UseListShuffleVector() { destroy(); }
-
- typedef unsigned *iterator;
- typedef const unsigned *const_iterator;
-
- size_t size() const { return Size; }
- iterator begin() { return data(); }
- iterator end() { return begin() + size(); }
- const_iterator begin() const { return data(); }
- const_iterator end() const { return begin() + size(); }
- unsigned &operator[](size_t I) { return data()[I]; }
- unsigned operator[](size_t I) const { return data()[I]; }
-};
-
/// \brief Structure to hold a use-list order.
struct UseListOrder {
const Value *V;
const Function *F;
- UseListShuffleVector Shuffle;
+ std::vector<unsigned> Shuffle;
UseListOrder(const Value *V, const Function *F, size_t ShuffleSize)
: V(V), F(F), Shuffle(ShuffleSize) {}