summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: c97db8d)
raw | patch | inline | side by side (parent: c97db8d)
author | Daniel Dunbar <daniel@zuster.org> | |
Wed, 14 Aug 2013 18:22:41 +0000 (18:22 +0000) | ||
committer | Daniel Dunbar <daniel@zuster.org> | |
Wed, 14 Aug 2013 18:22:41 +0000 (18:22 +0000) |
- For whatever reason, we have a lot of test files with bogus unicode
characters. This patch allows those scripts to still be parsed on Python3 by
changing the parsing logic to work on binary files, and only require the
actual script commands to be convertible to ascii.
- This patch has been tweaked to now ensure that the command strings are not of
unicode type on Python 2.6-7.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@188398 91177308-0d34-0410-b5e6-96231b3b80d8
characters. This patch allows those scripts to still be parsed on Python3 by
changing the parsing logic to work on binary files, and only require the
actual script commands to be convertible to ascii.
- This patch has been tweaked to now ensure that the command strings are not of
unicode type on Python 2.6-7.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@188398 91177308-0d34-0410-b5e6-96231b3b80d8
utils/lit/lit/TestRunner.py | patch | blob | history | |
utils/lit/tests/shtest-encoding.py | [new file with mode: 0644] | patch | blob |
index 068e4991b2110a67a5168021deed1c92688f726e..3c658eafcd9cb9e6d4d9813ba7d2a6b011e43e73 100644 (file)
return False
-def parseIntegratedTestScriptCommands(sourcepath):
+def parseIntegratedTestScriptCommands(source_path):
"""
parseIntegratedTestScriptCommands(source_path) -> commands
Parse the commands in an integrated test script file into a list of
(line_number, command_type, line).
"""
- line_number = 0
- for ln in open(sourcepath):
- line_number += 1
- if 'RUN:' in ln:
- yield (line_number, 'RUN', ln[ln.index('RUN:')+4:])
- elif 'XFAIL:' in ln:
- yield (line_number, 'XFAIL', ln[ln.index('XFAIL:') + 6:])
- elif 'REQUIRES:' in ln:
- yield (line_number, 'REQUIRES', ln[ln.index('REQUIRES:') + 9:])
- elif 'END.' in ln:
- yield (line_number, 'END', ln[ln.index('END.') + 4:])
+
+ # This code is carefully written to be dual compatible with Python 2.5+ and
+ # Python 3 without requiring input files to always have valid codings. The
+ # trick we use is to open the file in binary mode and use the regular
+ # expression library to find the commands, with it scanning strings in
+ # Python2 and bytes in Python3.
+ #
+ # Once we find a match, we do require each script line to be decodable to
+ # ascii, so we convert the outputs to ascii before returning. This way the
+ # remaining code can work with "strings" agnostic of the executing Python
+ # version.
+
+ def to_bytes(str):
+ # Encode to Latin1 to get binary data.
+ return str.encode('ISO-8859-1')
+ keywords = ('RUN:', 'XFAIL:', 'REQUIRES:', 'END.')
+ keywords_re = re.compile(
+ to_bytes("(%s)(.*)\n" % ("|".join(k for k in keywords),)))
+
+ f = open(source_path, 'rb')
+ try:
+ # Read the entire file contents.
+ data = f.read()
+
+ # Iterate over the matches.
+ line_number = 1
+ last_match_position = 0
+ for match in keywords_re.finditer(data):
+ # Compute the updated line number by counting the intervening
+ # newlines.
+ match_position = match.start()
+ line_number += data.count(to_bytes('\n'), last_match_position,
+ match_position)
+ last_match_position = match_position
+
+ # Convert the keyword and line to ascii strings and yield the
+ # command. Note that we take care to return regular strings in
+ # Python 2, to avoid other code having to differentiate between the
+ # str and unicode types.
+ keyword,ln = match.groups()
+ yield (line_number, str(keyword[:-1].decode('ascii')),
+ str(ln.decode('ascii')))
+ finally:
+ f.close()
def parseIntegratedTestScript(test, normalize_slashes=False,
extra_substitutions=[]):
diff --git a/utils/lit/tests/shtest-encoding.py b/utils/lit/tests/shtest-encoding.py
--- /dev/null
@@ -0,0 +1,3 @@
+# RUN: true
+
+# Here is a string that cannot be decoded in line mode: Â.