summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: dcc425c)
raw | patch | inline | side by side (parent: dcc425c)
author | Chandler Carruth <chandlerc@gmail.com> | |
Sat, 14 Sep 2013 09:28:14 +0000 (09:28 +0000) | ||
committer | Chandler Carruth <chandlerc@gmail.com> | |
Sat, 14 Sep 2013 09:28:14 +0000 (09:28 +0000) |
This pass was based on the previous (essentially unused) profiling
infrastructure and the assumption that by ordering the basic blocks at
the IR level in a particular way, the correct layout would happen in the
end. This sometimes worked, and mostly didn't. It also was a really
naive implementation of the classical paper that dates from when branch
predictors were primarily directional and when loop structure wasn't
commonly available. It also didn't factor into the equation
non-fallthrough branches and other machine level details.
Anyways, for all of these reasons and more, I wrote
MachineBlockPlacement, which completely supercedes this pass. It both
uses modern profile information infrastructure, and actually works. =]
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@190748 91177308-0d34-0410-b5e6-96231b3b80d8
infrastructure and the assumption that by ordering the basic blocks at
the IR level in a particular way, the correct layout would happen in the
end. This sometimes worked, and mostly didn't. It also was a really
naive implementation of the classical paper that dates from when branch
predictors were primarily directional and when loop structure wasn't
commonly available. It also didn't factor into the equation
non-fallthrough branches and other machine level details.
Anyways, for all of these reasons and more, I wrote
MachineBlockPlacement, which completely supercedes this pass. It both
uses modern profile information infrastructure, and actually works. =]
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@190748 91177308-0d34-0410-b5e6-96231b3b80d8
index aa06eca9b2916411f6a1a84473be0f547c110d95..1b50bb22654d732830ed194ba94a1ff939fa8239 100644 (file)
void initializeBasicTTIPass(PassRegistry&);
void initializeBlockExtractorPassPass(PassRegistry&);
void initializeBlockFrequencyInfoPass(PassRegistry&);
-void initializeBlockPlacementPass(PassRegistry&);
void initializeBoundsCheckingPass(PassRegistry&);
void initializeBranchFolderPassPass(PassRegistry&);
void initializeBranchProbabilityInfoPass(PassRegistry&);
index ec1ca49b4fa09b5b835b3bdbdc3daf73b6bd5356..0639ed1dad82531d9c7f5943f3bdffd4ff8dd1ba 100644 (file)
(void) llvm::createLibCallAliasAnalysisPass(0);
(void) llvm::createScalarEvolutionAliasAnalysisPass();
(void) llvm::createTypeBasedAliasAnalysisPass();
- (void) llvm::createBlockPlacementPass();
(void) llvm::createBoundsCheckingPass();
(void) llvm::createBreakCriticalEdgesPass();
(void) llvm::createCallGraphPrinterPass();
index eec9e591ee5208a84922543d9e328460e2d6f369..51aeba4a361743b334f7d0bbf92435fbb0553063 100644 (file)
bool useExpensiveEHSupport = false);
extern char &LowerInvokePassID;
-//===----------------------------------------------------------------------===//
-//
-// BlockPlacement - This pass reorders basic blocks in order to increase the
-// number of fall-through conditional branches.
-//
-FunctionPass *createBlockPlacementPass();
-
//===----------------------------------------------------------------------===//
//
// LCSSA - This pass inserts phi nodes at loop boundaries to simplify other loop
diff --git a/lib/Transforms/Scalar/BasicBlockPlacement.cpp b/lib/Transforms/Scalar/BasicBlockPlacement.cpp
+++ /dev/null
@@ -1,152 +0,0 @@
-//===-- BasicBlockPlacement.cpp - Basic Block Code Layout optimization ----===//
-//
-// The LLVM Compiler Infrastructure
-//
-// This file is distributed under the University of Illinois Open Source
-// License. See LICENSE.TXT for details.
-//
-//===----------------------------------------------------------------------===//
-//
-// This file implements a very simple profile guided basic block placement
-// algorithm. The idea is to put frequently executed blocks together at the
-// start of the function, and hopefully increase the number of fall-through
-// conditional branches. If there is no profile information for a particular
-// function, this pass basically orders blocks in depth-first order
-//
-// The algorithm implemented here is basically "Algo1" from "Profile Guided Code
-// Positioning" by Pettis and Hansen, except that it uses basic block counts
-// instead of edge counts. This should be improved in many ways, but is very
-// simple for now.
-//
-// Basically we "place" the entry block, then loop over all successors in a DFO,
-// placing the most frequently executed successor until we run out of blocks. I
-// told you this was _extremely_ simplistic. :) This is also much slower than it
-// could be. When it becomes important, this pass will be rewritten to use a
-// better algorithm, and then we can worry about efficiency.
-//
-//===----------------------------------------------------------------------===//
-
-#define DEBUG_TYPE "block-placement"
-#include "llvm/Transforms/Scalar.h"
-#include "llvm/ADT/Statistic.h"
-#include "llvm/Analysis/ProfileInfo.h"
-#include "llvm/IR/Function.h"
-#include "llvm/Pass.h"
-#include "llvm/Support/CFG.h"
-#include <set>
-using namespace llvm;
-
-STATISTIC(NumMoved, "Number of basic blocks moved");
-
-namespace {
- struct BlockPlacement : public FunctionPass {
- static char ID; // Pass identification, replacement for typeid
- BlockPlacement() : FunctionPass(ID) {
- initializeBlockPlacementPass(*PassRegistry::getPassRegistry());
- }
-
- virtual bool runOnFunction(Function &F);
-
- virtual void getAnalysisUsage(AnalysisUsage &AU) const {
- AU.setPreservesCFG();
- AU.addRequired<ProfileInfo>();
- //AU.addPreserved<ProfileInfo>(); // Does this work?
- }
- private:
- /// PI - The profile information that is guiding us.
- ///
- ProfileInfo *PI;
-
- /// NumMovedBlocks - Every time we move a block, increment this counter.
- ///
- unsigned NumMovedBlocks;
-
- /// PlacedBlocks - Every time we place a block, remember it so we don't get
- /// into infinite loops.
- std::set<BasicBlock*> PlacedBlocks;
-
- /// InsertPos - This an iterator to the next place we want to insert a
- /// block.
- Function::iterator InsertPos;
-
- /// PlaceBlocks - Recursively place the specified blocks and any unplaced
- /// successors.
- void PlaceBlocks(BasicBlock *BB);
- };
-}
-
-char BlockPlacement::ID = 0;
-INITIALIZE_PASS_BEGIN(BlockPlacement, "block-placement",
- "Profile Guided Basic Block Placement", false, false)
-INITIALIZE_AG_DEPENDENCY(ProfileInfo)
-INITIALIZE_PASS_END(BlockPlacement, "block-placement",
- "Profile Guided Basic Block Placement", false, false)
-
-FunctionPass *llvm::createBlockPlacementPass() { return new BlockPlacement(); }
-
-bool BlockPlacement::runOnFunction(Function &F) {
- PI = &getAnalysis<ProfileInfo>();
-
- NumMovedBlocks = 0;
- InsertPos = F.begin();
-
- // Recursively place all blocks.
- PlaceBlocks(F.begin());
-
- PlacedBlocks.clear();
- NumMoved += NumMovedBlocks;
- return NumMovedBlocks != 0;
-}
-
-
-/// PlaceBlocks - Recursively place the specified blocks and any unplaced
-/// successors.
-void BlockPlacement::PlaceBlocks(BasicBlock *BB) {
- assert(!PlacedBlocks.count(BB) && "Already placed this block!");
- PlacedBlocks.insert(BB);
-
- // Place the specified block.
- if (&*InsertPos != BB) {
- // Use splice to move the block into the right place. This avoids having to
- // remove the block from the function then readd it, which causes a bunch of
- // symbol table traffic that is entirely pointless.
- Function::BasicBlockListType &Blocks = BB->getParent()->getBasicBlockList();
- Blocks.splice(InsertPos, Blocks, BB);
-
- ++NumMovedBlocks;
- } else {
- // This block is already in the right place, we don't have to do anything.
- ++InsertPos;
- }
-
- // Keep placing successors until we run out of ones to place. Note that this
- // loop is very inefficient (N^2) for blocks with many successors, like switch
- // statements. FIXME!
- while (1) {
- // Okay, now place any unplaced successors.
- succ_iterator SI = succ_begin(BB), E = succ_end(BB);
-
- // Scan for the first unplaced successor.
- for (; SI != E && PlacedBlocks.count(*SI); ++SI)
- /*empty*/;
- if (SI == E) return; // No more successors to place.
-
- double MaxExecutionCount = PI->getExecutionCount(*SI);
- BasicBlock *MaxSuccessor = *SI;
-
- // Scan for more frequently executed successors
- for (; SI != E; ++SI)
- if (!PlacedBlocks.count(*SI)) {
- double Count = PI->getExecutionCount(*SI);
- if (Count > MaxExecutionCount ||
- // Prefer to not disturb the code.
- (Count == MaxExecutionCount && *SI == &*InsertPos)) {
- MaxExecutionCount = Count;
- MaxSuccessor = *SI;
- }
- }
-
- // Now that we picked the maximally executed successor, place it.
- PlaceBlocks(MaxSuccessor);
- }
-}
index 7fa7807990df9c9d99aba95b01ccbde8c3846737..3b89fd4cfd8990c8faf8485b48d8ed8ec3d82538 100644 (file)
add_llvm_library(LLVMScalarOpts
ADCE.cpp
- BasicBlockPlacement.cpp
CodeGenPrepare.cpp
ConstantProp.cpp
CorrelatedValuePropagation.cpp
index 952811b22b546db90cf3a5354cec6af28b353c81..0c3ffbc98310ccd69a0144dffeb2286406be5d04 100644 (file)
/// ScalarOpts library.
void llvm::initializeScalarOpts(PassRegistry &Registry) {
initializeADCEPass(Registry);
- initializeBlockPlacementPass(Registry);
initializeCodeGenPreparePass(Registry);
initializeConstantPropagationPass(Registry);
initializeCorrelatedValuePropagationPass(Registry);
diff --git a/test/Transforms/BlockPlacement/basictest.ll b/test/Transforms/BlockPlacement/basictest.ll
+++ /dev/null
@@ -1,15 +0,0 @@
-; RUN: opt < %s -block-placement -disable-output -print-function 2> /dev/null
-
-define i32 @test() {
- br i1 true, label %X, label %Y
-
-A: ; preds = %Y, %X
- ret i32 0
-
-X: ; preds = %0
- br label %A
-
-Y: ; preds = %0
- br label %A
-}
-