summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 61e341e)
raw | patch | inline | side by side (parent: 61e341e)
author | Bill Schmidt <wschmidt@linux.vnet.ibm.com> | |
Tue, 27 May 2014 15:57:51 +0000 (15:57 +0000) | ||
committer | Bill Schmidt <wschmidt@linux.vnet.ibm.com> | |
Tue, 27 May 2014 15:57:51 +0000 (15:57 +0000) |
In PPCISelLowering.cpp: PPCTargetLowering::LowerBUILD_VECTOR(), there
is an optimization for certain patterns to generate one or two vector
splats followed by a vector add or subtract. This operation is
represented by a VADD_SPLAT in the selection DAG. Prior to this
patch, it was possible for the VADD_SPLAT to be assigned the wrong
data type, causing incorrect code generation. This patch corrects the
problem.
Specifically, the code previously assigned the value type of the
BUILD_VECTOR node to the newly generated VADD_SPLAT node. This is
correct much of the time, but not always. The problem is that the
call to isConstantSplat() may return a SplatBitSize that is not the
same as the number of bits in the original element vector type. The
correct type to assign is a vector type with the same element bit size
as SplatBitSize.
The included test case shows an example of this, where the
BUILD_VECTOR node has a type of v16i8. The vector to be built is {0,
16, 0, 16, 0, 16, 0, 16, 0, 16, 0, 16, 0, 16, 0, 16}. isConstantSplat
detects that we can generate a splat of 16 for type v8i16, which is
the type we must assign to the VADD_SPLAT node. If we do not, we
generate a vspltisb of 8 and a vaddubm, which generates the incorrect
result {16, 16, 16, 16, 16, 16, 16, 16, 16, 16, 16, 16, 16, 16, 16,
16}. The correct code generation is a vspltish of 8 and a vadduhm.
This patch also corrected code generation for
CodeGen/PowerPC/2008-07-10-SplatMiscompile.ll, which had been marked
as an XFAIL, so we can remove the XFAIL from the test case.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209662 91177308-0d34-0410-b5e6-96231b3b80d8
is an optimization for certain patterns to generate one or two vector
splats followed by a vector add or subtract. This operation is
represented by a VADD_SPLAT in the selection DAG. Prior to this
patch, it was possible for the VADD_SPLAT to be assigned the wrong
data type, causing incorrect code generation. This patch corrects the
problem.
Specifically, the code previously assigned the value type of the
BUILD_VECTOR node to the newly generated VADD_SPLAT node. This is
correct much of the time, but not always. The problem is that the
call to isConstantSplat() may return a SplatBitSize that is not the
same as the number of bits in the original element vector type. The
correct type to assign is a vector type with the same element bit size
as SplatBitSize.
The included test case shows an example of this, where the
BUILD_VECTOR node has a type of v16i8. The vector to be built is {0,
16, 0, 16, 0, 16, 0, 16, 0, 16, 0, 16, 0, 16, 0, 16}. isConstantSplat
detects that we can generate a splat of 16 for type v8i16, which is
the type we must assign to the VADD_SPLAT node. If we do not, we
generate a vspltisb of 8 and a vaddubm, which generates the incorrect
result {16, 16, 16, 16, 16, 16, 16, 16, 16, 16, 16, 16, 16, 16, 16,
16}. The correct code generation is a vspltish of 8 and a vadduhm.
This patch also corrected code generation for
CodeGen/PowerPC/2008-07-10-SplatMiscompile.ll, which had been marked
as an XFAIL, so we can remove the XFAIL from the test case.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209662 91177308-0d34-0410-b5e6-96231b3b80d8
lib/Target/PowerPC/PPCISelLowering.cpp | patch | blob | history | |
test/CodeGen/PowerPC/2008-07-10-SplatMiscompile.ll | patch | blob | history | |
test/CodeGen/PowerPC/splat-bug.ll | [new file with mode: 0644] | patch | blob |
index 214c86920609eb25f50db74341b9a8a3ade7b054..cf4c9e61a58ddbace73266c57dbe5593463f0e51 100644 (file)
// we convert to a pseudo that will be expanded later into one of
// the above forms.
SDValue Elt = DAG.getConstant(SextVal, MVT::i32);
- EVT VT = Op.getValueType();
- int Size = VT == MVT::v16i8 ? 1 : (VT == MVT::v8i16 ? 2 : 4);
- SDValue EltSize = DAG.getConstant(Size, MVT::i32);
- return DAG.getNode(PPCISD::VADD_SPLAT, dl, VT, Elt, EltSize);
+ EVT VT = (SplatSize == 1 ? MVT::v16i8 :
+ (SplatSize == 2 ? MVT::v8i16 : MVT::v4i32));
+ SDValue EltSize = DAG.getConstant(SplatSize, MVT::i32);
+ SDValue RetVal = DAG.getNode(PPCISD::VADD_SPLAT, dl, VT, Elt, EltSize);
+ if (VT == Op.getValueType())
+ return RetVal;
+ else
+ return DAG.getNode(ISD::BITCAST, dl, Op.getValueType(), RetVal);
}
// If this is 0x8000_0000 x 4, turn into vspltisw + vslw. If it is
diff --git a/test/CodeGen/PowerPC/2008-07-10-SplatMiscompile.ll b/test/CodeGen/PowerPC/2008-07-10-SplatMiscompile.ll
index 00a402e0e4873a66ce24367566a31751294baf3a..8802b97d2a6a217b4953d9e14546c74a8aa4edc9 100644 (file)
; RUN: llc < %s -march=ppc32 -mcpu=g5 | grep vadduhm
; RUN: llc < %s -march=ppc32 -mcpu=g5 | grep vsubuhm
-; XFAIL: *
define <4 x i32> @test() nounwind {
ret <4 x i32> < i32 4293066722, i32 4293066722, i32 4293066722, i32 4293066722>
diff --git a/test/CodeGen/PowerPC/splat-bug.ll b/test/CodeGen/PowerPC/splat-bug.ll
--- /dev/null
@@ -0,0 +1,18 @@
+; RUN: llc -mcpu=ppc64 -O0 -fast-isel=false < %s | FileCheck %s
+
+; Checks for a previous bug where vspltisb/vaddubm were issued in place
+; of vsplitsh/vadduhm.
+
+target datalayout = "E-p:64:64:64-i1:8:8-i8:8:8-i16:16:16-i32:32:32-i64:64:64-f32:32:32-f64:64:64-v128:128:128-n32:64"
+target triple = "powerpc64-unknown-linux-gnu"
+
+@a = external global <16 x i8>
+
+define void @foo() nounwind ssp {
+; CHECK: foo:
+ store <16 x i8> <i8 0, i8 16, i8 0, i8 16, i8 0, i8 16, i8 0, i8 16, i8 0, i8 16, i8 0, i8 16, i8 0, i8 16, i8 0, i8 16>, <16 x i8>* @a
+; CHECK: vspltish [[REG:[0-9]+]], 8
+; CHECK: vadduhm {{[0-9]+}}, [[REG]], [[REG]]
+ ret void
+}
+