summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 6db0df8)
raw | patch | inline | side by side (parent: 6db0df8)
author | Chris Bieneman <beanz@apple.com> | |
Thu, 22 Jan 2015 21:01:12 +0000 (21:01 +0000) | ||
committer | Chris Bieneman <beanz@apple.com> | |
Thu, 22 Jan 2015 21:01:12 +0000 (21:01 +0000) |
Summary:
Some parsers need references back to the option they are members of. This is used for handling the argument string as well as by the various pass name parsers for making pass names into flags.
Making parsers that need to refer back to the option have a reference to the option eliminates some of the members of various parsers, and enables further code cleanup.
Reviewers: dexonsmith
Subscribers: llvm-commits
Differential Revision: http://reviews.llvm.org/D7131
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@226864 91177308-0d34-0410-b5e6-96231b3b80d8
Some parsers need references back to the option they are members of. This is used for handling the argument string as well as by the various pass name parsers for making pass names into flags.
Making parsers that need to refer back to the option have a reference to the option eliminates some of the members of various parsers, and enables further code cleanup.
Reviewers: dexonsmith
Subscribers: llvm-commits
Differential Revision: http://reviews.llvm.org/D7131
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@226864 91177308-0d34-0410-b5e6-96231b3b80d8
diff --git a/include/llvm/CodeGen/MachinePassRegistry.h b/include/llvm/CodeGen/MachinePassRegistry.h
index c962e687243e717ad64ecc6ea09b4dcf896c6cba..57d1a6d9b1927b883cf1bc0bb27fa1de72d18468 100644 (file)
class RegisterPassParser : public MachinePassRegistryListener,
public cl::parser<typename RegistryClass::FunctionPassCtor> {
public:
- RegisterPassParser() {}
+ RegisterPassParser(cl::Option &O)
+ : cl::parser<typename RegistryClass::FunctionPassCtor>(O) {}
~RegisterPassParser() { RegistryClass::setListener(nullptr); }
- void initialize(cl::Option &O) {
- cl::parser<typename RegistryClass::FunctionPassCtor>::initialize(O);
+ void initialize() {
+ cl::parser<typename RegistryClass::FunctionPassCtor>::initialize();
// Add existing passes to option.
for (RegistryClass *Node = RegistryClass::getList();
index e2e4912ef64e2eac70bbf16246abe4627d91b195..52db1c3bff55dada37b5d759682f35901c7f7ab3 100644 (file)
//
class PassNameParser : public PassRegistrationListener,
public cl::parser<const PassInfo*> {
- cl::Option *Opt;
public:
- PassNameParser();
+ PassNameParser(cl::Option &O);
virtual ~PassNameParser();
- void initialize(cl::Option &O) {
- Opt = &O;
- cl::parser<const PassInfo*>::initialize(O);
+ void initialize() {
+ cl::parser<const PassInfo*>::initialize();
// Add all of the passes to the map that got initialized before 'this' did.
enumeratePasses();
// Implement the PassRegistrationListener callbacks used to populate our map
//
void passRegistered(const PassInfo *P) override {
- if (ignorablePass(P) || !Opt) return;
+ if (ignorablePass(P)) return;
if (findOption(P->getPassArgument()) != getNumOptions()) {
errs() << "Two passes with the same argument (-"
<< P->getPassArgument() << ") attempted to be registered!\n";
index 778ddce390103deaf978492983b5488d3f5ed2e6..2d75c59cf207612fb487fb4f0b0a26f795894c79 100644 (file)
};
public:
+ generic_parser_base(Option &O) : Owner(O) {}
+
virtual ~generic_parser_base() {} // Base class should have virtual-dtor
// getNumOptions - Virtual function implemented by generic subclass to
printGenericOptionDiff(O, V, Default, GlobalWidth);
}
- void initialize(Option &O) {
- // All of the modifiers for the option have been processed by now, so the
- // argstr field should be stable, copy it down now.
- //
- hasArgStr = O.hasArgStr();
- }
+ void initialize() {}
void getExtraOptionNames(SmallVectorImpl<const char *> &OptionNames) {
// If there has been no argstr specified, that means that we need to add an
// argument for every possible option. This ensures that our options are
// vectored to us.
- if (!hasArgStr)
+ if (!Owner.hasArgStr())
for (unsigned i = 0, e = getNumOptions(); i != e; ++i)
OptionNames.push_back(getOption(i));
}
//
// If this is the case, we cannot allow a value.
//
- if (hasArgStr)
+ if (Owner.hasArgStr())
return ValueRequired;
else
return ValueDisallowed;
unsigned findOption(const char *Name);
protected:
- bool hasArgStr;
+ Option &Owner;
};
// Default parser implementation - This implementation depends on having a
SmallVector<OptionInfo, 8> Values;
public:
+ parser(Option &O) : generic_parser_base(O) {}
typedef DataType parser_data_type;
// Implement virtual functions needed by generic_parser_base
// parse - Return true on error.
bool parse(Option &O, StringRef ArgName, StringRef Arg, DataType &V) {
StringRef ArgVal;
- if (hasArgStr)
+ if (Owner.hasArgStr())
ArgVal = Arg;
else
ArgVal = ArgName;
//
class basic_parser_impl { // non-template implementation of basic_parser<t>
public:
+ basic_parser_impl(Option &O) {}
+
virtual ~basic_parser_impl() {}
enum ValueExpected getValueExpectedFlagDefault() const {
void getExtraOptionNames(SmallVectorImpl<const char *> &) {}
- void initialize(Option &) {}
+ void initialize() {}
// Return the width of the option tag for printing...
size_t getOptionWidth(const Option &O) const;
//
template <class DataType> class basic_parser : public basic_parser_impl {
public:
+ basic_parser(Option &O) : basic_parser_impl(O) {}
typedef DataType parser_data_type;
typedef OptionValue<DataType> OptVal;
};
// parser<bool>
//
template <> class parser<bool> : public basic_parser<bool> {
- const char *ArgStr;
-
public:
+ parser(Option &O) : basic_parser(O) {}
+
// parse - Return true on error.
bool parse(Option &O, StringRef ArgName, StringRef Arg, bool &Val);
- template <class Opt> void initialize(Opt &O) { ArgStr = O.ArgStr; }
+ void initialize() {}
enum ValueExpected getValueExpectedFlagDefault() const {
return ValueOptional;
// parser<boolOrDefault>
template <> class parser<boolOrDefault> : public basic_parser<boolOrDefault> {
public:
+ parser(Option &O) : basic_parser(O) {}
+
// parse - Return true on error.
bool parse(Option &O, StringRef ArgName, StringRef Arg, boolOrDefault &Val);
//
template <> class parser<int> : public basic_parser<int> {
public:
+ parser(Option &O) : basic_parser(O) {}
+
// parse - Return true on error.
bool parse(Option &O, StringRef ArgName, StringRef Arg, int &Val);
//
template <> class parser<unsigned> : public basic_parser<unsigned> {
public:
+ parser(Option &O) : basic_parser(O) {}
+
// parse - Return true on error.
bool parse(Option &O, StringRef ArgName, StringRef Arg, unsigned &Val);
template <>
class parser<unsigned long long> : public basic_parser<unsigned long long> {
public:
+ parser(Option &O) : basic_parser(O) {}
+
// parse - Return true on error.
bool parse(Option &O, StringRef ArgName, StringRef Arg,
unsigned long long &Val);
//
template <> class parser<double> : public basic_parser<double> {
public:
+ parser(Option &O) : basic_parser(O) {}
+
// parse - Return true on error.
bool parse(Option &O, StringRef ArgName, StringRef Arg, double &Val);
//
template <> class parser<float> : public basic_parser<float> {
public:
+ parser(Option &O) : basic_parser(O) {}
+
// parse - Return true on error.
bool parse(Option &O, StringRef ArgName, StringRef Arg, float &Val);
//
template <> class parser<std::string> : public basic_parser<std::string> {
public:
+ parser(Option &O) : basic_parser(O) {}
+
// parse - Return true on error.
bool parse(Option &, StringRef, StringRef Arg, std::string &Value) {
Value = Arg.str();
//
template <> class parser<char> : public basic_parser<char> {
public:
+ parser(Option &O) : basic_parser(O) {}
+
// parse - Return true on error.
bool parse(Option &, StringRef, StringRef Arg, char &Value) {
Value = Arg[0];
void done() {
addArgument();
- Parser.initialize(*this);
+ Parser.initialize();
}
// Command line options should not be copyable
// One option...
template <class M0t>
explicit opt(const M0t &M0)
- : Option(Optional, NotHidden) {
+ : Option(Optional, NotHidden), Parser(*this) {
apply(M0, this);
done();
}
// Two options...
template <class M0t, class M1t>
opt(const M0t &M0, const M1t &M1)
- : Option(Optional, NotHidden) {
+ : Option(Optional, NotHidden), Parser(*this) {
apply(M0, this);
apply(M1, this);
done();
// Three options...
template <class M0t, class M1t, class M2t>
opt(const M0t &M0, const M1t &M1, const M2t &M2)
- : Option(Optional, NotHidden) {
+ : Option(Optional, NotHidden), Parser(*this) {
apply(M0, this);
apply(M1, this);
apply(M2, this);
// Four options...
template <class M0t, class M1t, class M2t, class M3t>
opt(const M0t &M0, const M1t &M1, const M2t &M2, const M3t &M3)
- : Option(Optional, NotHidden) {
+ : Option(Optional, NotHidden), Parser(*this) {
apply(M0, this);
apply(M1, this);
apply(M2, this);
// Five options...
template <class M0t, class M1t, class M2t, class M3t, class M4t>
opt(const M0t &M0, const M1t &M1, const M2t &M2, const M3t &M3, const M4t &M4)
- : Option(Optional, NotHidden) {
+ : Option(Optional, NotHidden), Parser(*this) {
apply(M0, this);
apply(M1, this);
apply(M2, this);
template <class M0t, class M1t, class M2t, class M3t, class M4t, class M5t>
opt(const M0t &M0, const M1t &M1, const M2t &M2, const M3t &M3, const M4t &M4,
const M5t &M5)
- : Option(Optional, NotHidden) {
+ : Option(Optional, NotHidden), Parser(*this) {
apply(M0, this);
apply(M1, this);
apply(M2, this);
class M6t>
opt(const M0t &M0, const M1t &M1, const M2t &M2, const M3t &M3, const M4t &M4,
const M5t &M5, const M6t &M6)
- : Option(Optional, NotHidden) {
+ : Option(Optional, NotHidden), Parser(*this) {
apply(M0, this);
apply(M1, this);
apply(M2, this);
class M6t, class M7t>
opt(const M0t &M0, const M1t &M1, const M2t &M2, const M3t &M3, const M4t &M4,
const M5t &M5, const M6t &M6, const M7t &M7)
- : Option(Optional, NotHidden) {
+ : Option(Optional, NotHidden), Parser(*this) {
apply(M0, this);
apply(M1, this);
apply(M2, this);
void done() {
addArgument();
- Parser.initialize(*this);
+ Parser.initialize();
}
// Command line options should not be copyable
// One option...
template <class M0t>
explicit list(const M0t &M0)
- : Option(ZeroOrMore, NotHidden) {
+ : Option(ZeroOrMore, NotHidden), Parser(*this) {
apply(M0, this);
done();
}
// Two options...
template <class M0t, class M1t>
list(const M0t &M0, const M1t &M1)
- : Option(ZeroOrMore, NotHidden) {
+ : Option(ZeroOrMore, NotHidden), Parser(*this) {
apply(M0, this);
apply(M1, this);
done();
// Three options...
template <class M0t, class M1t, class M2t>
list(const M0t &M0, const M1t &M1, const M2t &M2)
- : Option(ZeroOrMore, NotHidden) {
+ : Option(ZeroOrMore, NotHidden), Parser(*this) {
apply(M0, this);
apply(M1, this);
apply(M2, this);
// Four options...
template <class M0t, class M1t, class M2t, class M3t>
list(const M0t &M0, const M1t &M1, const M2t &M2, const M3t &M3)
- : Option(ZeroOrMore, NotHidden) {
+ : Option(ZeroOrMore, NotHidden), Parser(*this) {
apply(M0, this);
apply(M1, this);
apply(M2, this);
template <class M0t, class M1t, class M2t, class M3t, class M4t>
list(const M0t &M0, const M1t &M1, const M2t &M2, const M3t &M3,
const M4t &M4)
- : Option(ZeroOrMore, NotHidden) {
+ : Option(ZeroOrMore, NotHidden), Parser(*this) {
apply(M0, this);
apply(M1, this);
apply(M2, this);
template <class M0t, class M1t, class M2t, class M3t, class M4t, class M5t>
list(const M0t &M0, const M1t &M1, const M2t &M2, const M3t &M3,
const M4t &M4, const M5t &M5)
- : Option(ZeroOrMore, NotHidden) {
+ : Option(ZeroOrMore, NotHidden), Parser(*this) {
apply(M0, this);
apply(M1, this);
apply(M2, this);
class M6t>
list(const M0t &M0, const M1t &M1, const M2t &M2, const M3t &M3,
const M4t &M4, const M5t &M5, const M6t &M6)
- : Option(ZeroOrMore, NotHidden) {
+ : Option(ZeroOrMore, NotHidden), Parser(*this) {
apply(M0, this);
apply(M1, this);
apply(M2, this);
class M6t, class M7t>
list(const M0t &M0, const M1t &M1, const M2t &M2, const M3t &M3,
const M4t &M4, const M5t &M5, const M6t &M6, const M7t &M7)
- : Option(ZeroOrMore, NotHidden) {
+ : Option(ZeroOrMore, NotHidden), Parser(*this) {
apply(M0, this);
apply(M1, this);
apply(M2, this);
void done() {
addArgument();
- Parser.initialize(*this);
+ Parser.initialize();
}
// Command line options should not be copyable
// One option...
template <class M0t>
explicit bits(const M0t &M0)
- : Option(ZeroOrMore, NotHidden) {
+ : Option(ZeroOrMore, NotHidden), Parser(*this) {
apply(M0, this);
done();
}
// Two options...
template <class M0t, class M1t>
bits(const M0t &M0, const M1t &M1)
- : Option(ZeroOrMore, NotHidden) {
+ : Option(ZeroOrMore, NotHidden), Parser(*this) {
apply(M0, this);
apply(M1, this);
done();
// Three options...
template <class M0t, class M1t, class M2t>
bits(const M0t &M0, const M1t &M1, const M2t &M2)
- : Option(ZeroOrMore, NotHidden) {
+ : Option(ZeroOrMore, NotHidden), Parser(*this) {
apply(M0, this);
apply(M1, this);
apply(M2, this);
// Four options...
template <class M0t, class M1t, class M2t, class M3t>
bits(const M0t &M0, const M1t &M1, const M2t &M2, const M3t &M3)
- : Option(ZeroOrMore, NotHidden) {
+ : Option(ZeroOrMore, NotHidden), Parser(*this) {
apply(M0, this);
apply(M1, this);
apply(M2, this);
template <class M0t, class M1t, class M2t, class M3t, class M4t>
bits(const M0t &M0, const M1t &M1, const M2t &M2, const M3t &M3,
const M4t &M4)
- : Option(ZeroOrMore, NotHidden) {
+ : Option(ZeroOrMore, NotHidden), Parser(*this) {
apply(M0, this);
apply(M1, this);
apply(M2, this);
template <class M0t, class M1t, class M2t, class M3t, class M4t, class M5t>
bits(const M0t &M0, const M1t &M1, const M2t &M2, const M3t &M3,
const M4t &M4, const M5t &M5)
- : Option(ZeroOrMore, NotHidden) {
+ : Option(ZeroOrMore, NotHidden), Parser(*this) {
apply(M0, this);
apply(M1, this);
apply(M2, this);
class M6t>
bits(const M0t &M0, const M1t &M1, const M2t &M2, const M3t &M3,
const M4t &M4, const M5t &M5, const M6t &M6)
- : Option(ZeroOrMore, NotHidden) {
+ : Option(ZeroOrMore, NotHidden), Parser(*this) {
apply(M0, this);
apply(M1, this);
apply(M2, this);
class M6t, class M7t>
bits(const M0t &M0, const M1t &M1, const M2t &M2, const M3t &M3,
const M4t &M4, const M5t &M5, const M6t &M6, const M7t &M7)
- : Option(ZeroOrMore, NotHidden) {
+ : Option(ZeroOrMore, NotHidden), Parser(*this) {
apply(M0, this);
apply(M1, this);
apply(M2, this);
diff --git a/lib/IR/Pass.cpp b/lib/IR/Pass.cpp
index 91d86ae40d1831418651c4a1d1c1eb11457fedb5..df45460a6ccaca930e41b2a7ca7f5e04b3cc1f35 100644 (file)
--- a/lib/IR/Pass.cpp
+++ b/lib/IR/Pass.cpp
PassRegistry::getPassRegistry()->enumerateWith(this);
}
-PassNameParser::PassNameParser()
- : Opt(nullptr) {
+PassNameParser::PassNameParser(cl::Option &O)
+ : cl::parser<const PassInfo *>(O) {
PassRegistry::getPassRegistry()->addRegistrationListener(this);
}