summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 18fdb39)
raw | patch | inline | side by side (parent: 18fdb39)
author | Rafael Espindola <rafael.espindola@gmail.com> | |
Sun, 7 Apr 2013 19:26:57 +0000 (19:26 +0000) | ||
committer | Rafael Espindola <rafael.espindola@gmail.com> | |
Sun, 7 Apr 2013 19:26:57 +0000 (19:26 +0000) |
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@178994 91177308-0d34-0410-b5e6-96231b3b80d8
include/llvm/Object/MachO.h | patch | blob | history | |
lib/Object/MachOObjectFile.cpp | patch | blob | history | |
tools/llvm-objdump/MachODump.cpp | patch | blob | history |
index 4cdf091fc166b66062c825ce1520a99e98baf99e..0d20146aae4c77cab91befade956c16679655cf2 100644 (file)
support::ulittle32_t DataOffset;
support::ulittle32_t DataSize;
};
+
+ struct Header {
+ support::ulittle32_t Magic;
+ support::ulittle32_t CPUType;
+ support::ulittle32_t CPUSubtype;
+ support::ulittle32_t FileType;
+ support::ulittle32_t NumLoadCommands;
+ support::ulittle32_t SizeOfLoadCommands;
+ support::ulittle32_t Flags;
+ };
}
class MachOObjectFile : public ObjectFile {
bool is64Bit() const;
const MachOFormat::LoadCommand *getLoadCommandInfo(unsigned Index) const;
void ReadULEB128s(uint64_t Index, SmallVectorImpl<uint64_t> &Out) const;
- const macho::Header &getHeader() const;
+ const MachOFormat::Header *getHeader() const;
unsigned getHeaderSize() const;
StringRef getData(size_t Offset, size_t Size) const;
index f011da1e3a04e25c0dbd68d9cfe77a19bb861c28..31e8be0f94b147f66cc88c9fd7a68bcd6889a02c 100644 (file)
DataRefImpl DRI;
moveToNextSection(DRI);
- uint32_t LoadCommandCount = getHeader().NumLoadCommands;
+ uint32_t LoadCommandCount = getHeader()->NumLoadCommands;
while (DRI.d.a < LoadCommandCount) {
Sections.push_back(DRI);
DRI.d.b++;
return MachOObj->ReadULEB128s(Index, Out);
}
-const macho::Header &MachOObjectFile::getHeader() const {
- return MachOObj->getHeader();
+const MachOFormat::Header *MachOObjectFile::getHeader() const {
+ StringRef Data = getData(0, sizeof(MachOFormat::Header));
+ return reinterpret_cast<const MachOFormat::Header*>(Data.data());
}
unsigned MachOObjectFile::getHeaderSize() const {
/*===-- Symbols -----------------------------------------------------------===*/
void MachOObjectFile::moveToNextSymbol(DataRefImpl &DRI) const {
- uint32_t LoadCommandCount = getHeader().NumLoadCommands;
+ uint32_t LoadCommandCount = getHeader()->NumLoadCommands;
while (DRI.d.a < LoadCommandCount) {
const MachOFormat::LoadCommand *Command = getLoadCommandInfo(DRI.d.a);
if (Command->Type == macho::LCT_Symtab) {
error_code MachOObjectFile::getSymbolSize(DataRefImpl DRI,
uint64_t &Result) const {
- uint32_t LoadCommandCount = getHeader().NumLoadCommands;
+ uint32_t LoadCommandCount = getHeader()->NumLoadCommands;
uint64_t BeginOffset;
uint64_t EndOffset = 0;
uint8_t SectionIndex;
symbol_iterator MachOObjectFile::end_symbols() const {
DataRefImpl DRI;
- DRI.d.a = getHeader().NumLoadCommands;
+ DRI.d.a = getHeader()->NumLoadCommands;
return symbol_iterator(SymbolRef(DRI, this));
}
/*===-- Sections ----------------------------------------------------------===*/
void MachOObjectFile::moveToNextSection(DataRefImpl &DRI) const {
- uint32_t LoadCommandCount = getHeader().NumLoadCommands;
+ uint32_t LoadCommandCount = getHeader()->NumLoadCommands;
while (DRI.d.a < LoadCommandCount) {
const MachOFormat::LoadCommand *Command = getLoadCommandInfo(DRI.d.a);
if (Command->Type == macho::LCT_Segment) {
section_iterator MachOObjectFile::end_sections() const {
DataRefImpl DRI;
- DRI.d.a = getHeader().NumLoadCommands;
+ DRI.d.a = getHeader()->NumLoadCommands;
return section_iterator(SectionRef(DRI, this));
}
for (unsigned i = 0; i < SymbolIdx; i++) {
Sym.d.b++;
moveToNextSymbol(Sym);
- assert(Sym.d.a < getHeader().NumLoadCommands &&
+ assert(Sym.d.a < getHeader()->NumLoadCommands &&
"Relocation symbol index out of range!");
}
}
StringRef MachOObjectFile::getFileFormatName() const {
if (!is64Bit()) {
- switch (getHeader().CPUType) {
+ switch (getHeader()->CPUType) {
case llvm::MachO::CPUTypeI386:
return "Mach-O 32-bit i386";
case llvm::MachO::CPUTypeARM:
case llvm::MachO::CPUTypePowerPC:
return "Mach-O 32-bit ppc";
default:
- assert((getHeader().CPUType & llvm::MachO::CPUArchABI64) == 0 &&
+ assert((getHeader()->CPUType & llvm::MachO::CPUArchABI64) == 0 &&
"64-bit object file when we're not 64-bit?");
return "Mach-O 32-bit unknown";
}
}
// Make sure the cpu type has the correct mask.
- assert((getHeader().CPUType & llvm::MachO::CPUArchABI64)
+ assert((getHeader()->CPUType & llvm::MachO::CPUArchABI64)
== llvm::MachO::CPUArchABI64 &&
"32-bit object file when we're 64-bit?");
- switch (getHeader().CPUType) {
+ switch (getHeader()->CPUType) {
case llvm::MachO::CPUTypeX86_64:
return "Mach-O 64-bit x86-64";
case llvm::MachO::CPUTypePowerPC64:
}
unsigned MachOObjectFile::getArch() const {
- switch (getHeader().CPUType) {
+ switch (getHeader()->CPUType) {
case llvm::MachO::CPUTypeI386:
return Triple::x86;
case llvm::MachO::CPUTypeX86_64:
index 9275fe147ab0a0a27b7234025f18d67f46aa9fbc..7c6565832eb6df0ec43b4d03ba3bd1658bc32ae6 100644 (file)
// Figure out the target triple.
if (TripleName.empty()) {
llvm::Triple TT("unknown-unknown-unknown");
- switch (MachOObj->getHeader().CPUType) {
+ switch (MachOObj->getHeader()->CPUType) {
case llvm::MachO::CPUTypeI386:
TT.setArch(Triple::ArchType(Triple::x86));
break;
Out << "}\n";
}
-static void getSectionsAndSymbols(const macho::Header &Header,
+static void getSectionsAndSymbols(const MachOFormat::Header *Header,
MachOObjectFile *MachOObj,
std::vector<SectionRef> &Sections,
std::vector<SymbolRef> &Symbols,
Sections.push_back(*SI);
}
- for (unsigned i = 0; i != Header.NumLoadCommands; ++i) {
+ for (unsigned i = 0; i != Header->NumLoadCommands; ++i) {
const MachOFormat::LoadCommand *Command = MachOObj->getLoadCommandInfo(i);
if (Command->Type == macho::LCT_FunctionStarts) {
// We found a function starts segment, parse the addresses for later
outs() << '\n' << Filename << ":\n\n";
- const macho::Header &Header = MachOOF->getHeader();
+ const MachOFormat::Header *Header = MachOOF->getHeader();
std::vector<SectionRef> Sections;
std::vector<SymbolRef> Symbols;