]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/commitdiff
Move REP out of the Prefix field of the X86 format. Give it its own bit. It had speci...
authorCraig Topper <craig.topper@gmail.com>
Fri, 31 Jan 2014 07:00:55 +0000 (07:00 +0000)
committerCraig Topper <craig.topper@gmail.com>
Fri, 31 Jan 2014 07:00:55 +0000 (07:00 +0000)
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@200520 91177308-0d34-0410-b5e6-96231b3b80d8

lib/Target/X86/MCTargetDesc/X86BaseInfo.h
lib/Target/X86/MCTargetDesc/X86MCCodeEmitter.cpp
lib/Target/X86/X86CodeEmitter.cpp
lib/Target/X86/X86InstrFormats.td
utils/TableGen/X86RecognizableInstr.cpp
utils/TableGen/X86RecognizableInstr.h

index c085f14781429e9565f8e0ef790655e302bb1218..b690de2d3fb2d482129253ca6aefc5dbfd93ad35 100644 (file)
@@ -324,9 +324,9 @@ namespace X86II {
 
     //===------------------------------------------------------------------===//
     // Op0Mask - There are several prefix bytes that are used to form two byte
-    // opcodes.  These are currently 0x0F, 0xF3, and 0xD8-0xDF.  This mask is
-    // used to obtain the setting of this field.  If no bits in this field is
-    // set, there is no prefix byte for obtaining a multibyte opcode.
+    // opcodes.  This mask is used to obtain the setting of this field.  If no
+    // bits in this field is set, there is no prefix byte for obtaining a
+    // multibyte opcode.
     //
     Op0Shift    = 9,
     Op0Mask     = 0x1F << Op0Shift,
@@ -335,10 +335,6 @@ namespace X86II {
     // starts with a 0x0F byte before the real opcode.
     TB          = 1 << Op0Shift,
 
-    // REP - The 0xF3 prefix byte indicating repetition of the following
-    // instruction.
-    REP         = 2 << Op0Shift,
-
     // D8-DF - These escape opcodes are used by the floating point unit.  These
     // values must remain sequential.
     D8 = 3 << Op0Shift,   D9 = 4 << Op0Shift,
@@ -445,9 +441,13 @@ namespace X86II {
     LOCKShift = FPTypeShift + 3,
     LOCK = 1 << LOCKShift,
 
-    // Execution domain for SSE instructions in bits 23, 24.
-    // 0 in bits 23-24 means normal, non-SSE instruction.
-    SSEDomainShift = LOCKShift + 1,
+    // REP prefix
+    REPShift = LOCKShift + 1,
+    REP = 1 << REPShift,
+
+    // Execution domain for SSE instructions.
+    // 0 means normal, non-SSE instruction.
+    SSEDomainShift = REPShift + 1,
 
     OpcodeShift   = SSEDomainShift + 2,
 
index 7d81bbe9857fd555bdc6ca2e42a677922634f507..986e257392a091df860d161f2039881b747d60b2 100644 (file)
@@ -1156,7 +1156,6 @@ void X86MCCodeEmitter::EmitOpcodePrefix(uint64_t TSFlags, unsigned &CurByte,
   switch (TSFlags & X86II::Op0Mask) {
   default: llvm_unreachable("Invalid prefix!");
   case 0: break;  // No prefix!
-  case X86II::REP: break; // already handled.
   case X86II::TB:  // Two-byte opcode prefix
   case X86II::T8:  // 0F 38
   case X86II::TA:  // 0F 3A
@@ -1273,7 +1272,7 @@ EncodeInstruction(const MCInst &MI, raw_ostream &OS,
                               MI, OS);
 
   // Emit the repeat opcode prefix as needed.
-  if ((TSFlags & X86II::Op0Mask) == X86II::REP)
+  if (TSFlags & X86II::REP)
     EmitByte(0xF3, CurByte, OS);
 
   // Emit the address size opcode prefix as needed.
index b377419c0d6cb233f1ae25984197d8d9c269f9dd..dc75e60345ebf7e3247910ae45df0c516a88ed2c 100644 (file)
@@ -667,7 +667,6 @@ void Emitter<CodeEmitter>::emitOpcodePrefix(uint64_t TSFlags,
     case X86II::A7:  // 0F A7
       Need0FPrefix = true;
       break;
-    case X86II::REP: break; // already handled.
     case X86II::PD:   // 66 0F
     case X86II::T8PD: // 66 0F 38
     case X86II::TAPD: // 66 0F 3A
@@ -1125,7 +1124,7 @@ void Emitter<CodeEmitter>::emitInstruction(MachineInstr &MI,
   emitSegmentOverridePrefix(TSFlags, MemoryOperand, MI);
 
   // Emit the repeat opcode prefix as needed.
-  if ((Desc->TSFlags & X86II::Op0Mask) == X86II::REP)
+  if (Desc->TSFlags & X86II::REP)
     MCE.emitByte(0xF3);
 
   // Emit the address size opcode prefix as needed.
index ded1d9033704131b5be03d22084fcc1b2f07e3a4..83cd7e1b9db303cabde6a7a1d24237f9490f20e0 100644 (file)
@@ -119,8 +119,8 @@ class OpSize16 { bit hasOpSize16Prefix = 1; }
 class AdSize { bit hasAdSizePrefix = 1; }
 class REX_W  { bit hasREX_WPrefix = 1; }
 class LOCK   { bit hasLockPrefix = 1; }
+class REP    { bit hasREPPrefix = 1; }
 class TB     { bits<5> Prefix = 1; }
-class REP    { bits<5> Prefix = 2; }
 class D8     { bits<5> Prefix = 3; }
 class D9     { bits<5> Prefix = 4; }
 class DA     { bits<5> Prefix = 5; }
@@ -205,6 +205,7 @@ class X86Inst<bits<8> opcod, Format f, ImmType i, dag outs, dag ins,
   FPFormat FPForm = NotFP;  // What flavor of FP instruction is this?
   bit hasLockPrefix = 0;    // Does this inst have a 0xF0 prefix?
   Domain ExeDomain = d;
+  bit hasREPPrefix = 0;     // Does this inst have a REP prefix?
   bit hasVEXPrefix = 0;     // Does this inst require a VEX prefix?
   bit hasVEX_WPrefix = 0;   // Does this inst set the VEX_W field?
   bit hasVEX_4VPrefix = 0;  // Does this inst require the VEX.VVVV field?
@@ -236,26 +237,27 @@ class X86Inst<bits<8> opcod, Format f, ImmType i, dag outs, dag ins,
   let TSFlags{18-15} = ImmT.Value;
   let TSFlags{21-19} = FPForm.Value;
   let TSFlags{22}    = hasLockPrefix;
-  let TSFlags{24-23} = ExeDomain.Value;
-  let TSFlags{32-25} = Opcode;
-  let TSFlags{33}    = hasVEXPrefix;
-  let TSFlags{34}    = hasVEX_WPrefix;
-  let TSFlags{35}    = hasVEX_4VPrefix;
-  let TSFlags{36}    = hasVEX_4VOp3Prefix;
-  let TSFlags{37}    = hasVEX_i8ImmReg;
-  let TSFlags{38}    = hasVEX_L;
-  let TSFlags{39}    = ignoresVEX_L;
-  let TSFlags{40}    = hasEVEXPrefix;
-  let TSFlags{41}    = hasEVEX_K;
-  let TSFlags{42}    = hasEVEX_Z;
-  let TSFlags{43}    = hasEVEX_L2;
-  let TSFlags{44}    = hasEVEX_B;
-  let TSFlags{46-45} = EVEX_CD8E;
-  let TSFlags{49-47} = EVEX_CD8V;
-  let TSFlags{50}    = has3DNow0F0FOpcode;
-  let TSFlags{51}    = hasMemOp4Prefix;
-  let TSFlags{52}    = hasXOP_Prefix;
-  let TSFlags{53}    = hasEVEX_RC;
+  let TSFlags{23}    = hasREPPrefix;
+  let TSFlags{25-24} = ExeDomain.Value;
+  let TSFlags{33-26} = Opcode;
+  let TSFlags{34}    = hasVEXPrefix;
+  let TSFlags{35}    = hasVEX_WPrefix;
+  let TSFlags{36}    = hasVEX_4VPrefix;
+  let TSFlags{37}    = hasVEX_4VOp3Prefix;
+  let TSFlags{38}    = hasVEX_i8ImmReg;
+  let TSFlags{39}    = hasVEX_L;
+  let TSFlags{40}    = ignoresVEX_L;
+  let TSFlags{41}    = hasEVEXPrefix;
+  let TSFlags{42}    = hasEVEX_K;
+  let TSFlags{43}    = hasEVEX_Z;
+  let TSFlags{44}    = hasEVEX_L2;
+  let TSFlags{45}    = hasEVEX_B;
+  let TSFlags{47-46} = EVEX_CD8E;
+  let TSFlags{50-48} = EVEX_CD8V;
+  let TSFlags{51}    = has3DNow0F0FOpcode;
+  let TSFlags{52}    = hasMemOp4Prefix;
+  let TSFlags{53}    = hasXOP_Prefix;
+  let TSFlags{54}    = hasEVEX_RC;
 }
 
 class PseudoI<dag oops, dag iops, list<dag> pattern>
index e0b4be2eb39e05df0f9c19566ca9e543400653c7..f84fafdde10a7269f26a93d4fbeb5274b6dd0cc8 100644 (file)
@@ -77,7 +77,6 @@ namespace X86Local {
 
   enum {
     TB  = 1,
-    REP = 2,
     D8 = 3, D9 = 4, DA = 5, DB = 6,
     DC = 7, DD = 8, DE = 9, DF = 10,
     XD = 11,  XS = 12,
@@ -250,6 +249,7 @@ RecognizableInstr::RecognizableInstr(DisassemblerTables &tables,
   HasEVEX_KZ       = Rec->getValueAsBit("hasEVEX_Z");
   HasEVEX_B        = Rec->getValueAsBit("hasEVEX_B");
   HasLockPrefix    = Rec->getValueAsBit("hasLockPrefix");
+  HasREPPrefix     = Rec->getValueAsBit("hasREPPrefix");
   IsCodeGenOnly    = Rec->getValueAsBit("isCodeGenOnly");
   ForceDisassemble = Rec->getValueAsBit("ForceDisassemble");
 
@@ -480,7 +480,7 @@ InstructionContext RecognizableInstr::insnContext() const {
              Prefix == X86Local::TAXD)
       insnContext = IC_XD;
     else if (Prefix == X86Local::XS || Prefix == X86Local::T8XS ||
-             Prefix == X86Local::REP)
+             HasREPPrefix)
       insnContext = IC_XS;
     else
       insnContext = IC;
@@ -1090,7 +1090,6 @@ void RecognizableInstr::emitDecodePath(DisassemblerTables &tables) const {
     filter = new ExactFilter(Opcode);
     opcodeToSet = 0xd8 + (Prefix - X86Local::D8);
     break;
-  case X86Local::REP:
   case 0:
     opcodeType = ONEBYTE;
     switch (Opcode) {
index 08e984e9509cccccf2a213c0c3c7eec040adbd7e..bf758ed2bbd41350ecbe43e49e05a1b8fac78aef 100644 (file)
@@ -78,6 +78,8 @@ private:
   bool HasEVEX_B;
   /// The hasLockPrefix field from the record
   bool HasLockPrefix;
+  /// The hasREPPrefix field from the record
+  bool HasREPPrefix;
   /// The isCodeGenOnly field from the record
   bool IsCodeGenOnly;
   /// The ForceDisassemble field from the record