summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: b82f8a2)
raw | patch | inline | side by side (parent: b82f8a2)
author | Jim Grosbach <grosbach@apple.com> | |
Wed, 26 Mar 2014 17:27:01 +0000 (17:27 +0000) | ||
committer | Jim Grosbach <grosbach@apple.com> | |
Wed, 26 Mar 2014 17:27:01 +0000 (17:27 +0000) |
In some cases it is possible for CGP to attempt to reuse a base address from
another basic block. In those cases we have to be sure that all the address
math was either done at the same bit width, or that none of it overflowed
before it was extended.
Patch by Louis Gerbarg <lgg@apple.com>
rdar://16307442
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@204833 91177308-0d34-0410-b5e6-96231b3b80d8
another basic block. In those cases we have to be sure that all the address
math was either done at the same bit width, or that none of it overflowed
before it was extended.
Patch by Louis Gerbarg <lgg@apple.com>
rdar://16307442
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@204833 91177308-0d34-0410-b5e6-96231b3b80d8
lib/CodeGen/CodeGenPrepare.cpp | patch | blob | history | |
test/CodeGen/X86/sunkaddr-ext.ll | [new file with mode: 0644] | patch | blob |
index 428d8af359ef001814e4a04b3f6fae1046b3289a..a3961e80031c472f9b8558612b04c8189bfc106f 100644 (file)
@@ -2438,7 +2438,14 @@ bool CodeGenPrepare::OptimizeMemoryInst(Instruction *MemoryInst, Value *Addr,
cast<IntegerType>(V->getType())->getBitWidth()) {
V = Builder.CreateTrunc(V, IntPtrTy, "sunkaddr");
} else {
- V = Builder.CreateSExt(V, IntPtrTy, "sunkaddr");
+ // It is only safe to sign extend the BaseReg if we know that the math
+ // required to create it did not overflow before we extend it. Since
+ // the original IR value was tossed in favor of a constant back when
+ // the AddrMode was created we need to bail out gracefully if widths
+ // do not match instead of extending it.
+ if (Result != AddrMode.BaseReg)
+ cast<Instruction>(Result)->eraseFromParent();
+ return false;
}
if (AddrMode.Scale != 1)
V = Builder.CreateMul(V, ConstantInt::get(IntPtrTy, AddrMode.Scale),
diff --git a/test/CodeGen/X86/sunkaddr-ext.ll b/test/CodeGen/X86/sunkaddr-ext.ll
--- /dev/null
@@ -0,0 +1,26 @@
+; RUN: llc < %s | FileCheck %s
+
+; Test to make sure that if math that can roll over has been used we don't
+; use the potential overflow as the basis for an address calculation later by
+; sinking it into a different basic block.
+
+target datalayout = "e-m:o-i64:64-f80:128-n8:16:32:64-S128"
+target triple = "x86_64-apple-macosx10.9.0"
+
+; Function Attrs: nounwind ssp uwtable
+define void @test_sink(i8* %arg1, i32 %arg2, i8 %arg3) #0 {
+ %tmp1 = add i32 -2147483648, %arg2
+ %tmp2 = add i32 -2147483648, %tmp1
+ %tmp3 = getelementptr i8* %arg1, i32 %arg2
+ br label %bb1
+
+bb1:
+ %tmp4 = getelementptr i8* %arg1, i32 %tmp2
+ store i8 %arg3, i8* %tmp4
+ ret void;
+}
+
+; CHECK-LABEL: test_sink:
+; CHECK: movslq %esi, [[TEMP:%[a-z0-9]+]]
+; CHECK: movb %dl, (%rdi,[[TEMP]])
+; CHECK: retq