summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: ecd37bc)
raw | patch | inline | side by side (parent: ecd37bc)
author | Duncan Sands <baldrick@free.fr> | |
Tue, 6 Sep 2011 13:37:06 +0000 (13:37 +0000) | ||
committer | Duncan Sands <baldrick@free.fr> | |
Tue, 6 Sep 2011 13:37:06 +0000 (13:37 +0000) |
init.trampoline and adjust.trampoline intrinsics, into two intrinsics
like in GCC. While having one combined intrinsic is tempting, it is
not natural because typically the trampoline initialization needs to
be done in one function, and the result of adjust trampoline is needed
in a different (nested) function. To get around this llvm-gcc hacks the
nested function lowering code to insert an additional parent variable
holding the adjust.trampoline result that can be accessed from the child
function. Dragonegg doesn't have the luxury of tweaking GCC code, so it
stored the result of adjust.trampoline in the memory GCC set aside for
the trampoline itself (this is always available in the child function),
and set up some new memory (using an alloca) to hold the trampoline.
Unfortunately this breaks Go which allocates trampoline memory on the
heap and wants to use it even after the parent has exited (!). Rather
than doing even more hacks to get Go working, it seemed best to just use
two intrinsics like in GCC. Patch mostly by Sanjoy Das.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@139140 91177308-0d34-0410-b5e6-96231b3b80d8
like in GCC. While having one combined intrinsic is tempting, it is
not natural because typically the trampoline initialization needs to
be done in one function, and the result of adjust trampoline is needed
in a different (nested) function. To get around this llvm-gcc hacks the
nested function lowering code to insert an additional parent variable
holding the adjust.trampoline result that can be accessed from the child
function. Dragonegg doesn't have the luxury of tweaking GCC code, so it
stored the result of adjust.trampoline in the memory GCC set aside for
the trampoline itself (this is always available in the child function),
and set up some new memory (using an alloca) to hold the trampoline.
Unfortunately this breaks Go which allocates trampoline memory on the
heap and wants to use it even after the parent has exited (!). Rather
than doing even more hacks to get Go working, it seemed best to just use
two intrinsics like in GCC. Patch mostly by Sanjoy Das.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@139140 91177308-0d34-0410-b5e6-96231b3b80d8
19 files changed:
diff --git a/docs/LangRef.html b/docs/LangRef.html
index 2b9ee24bf41a66f85632eea4636191e132942bba..0ec08eb0a0589c22edc1a9b4e4eb46924a252a7e 100644 (file)
--- a/docs/LangRef.html
+++ b/docs/LangRef.html
</li>
<li><a href="#int_debugger">Debugger intrinsics</a></li>
<li><a href="#int_eh">Exception Handling intrinsics</a></li>
- <li><a href="#int_trampoline">Trampoline Intrinsic</a>
+ <li><a href="#int_trampoline">Trampoline Intrinsics</a>
<ol>
<li><a href="#int_it">'<tt>llvm.init.trampoline</tt>' Intrinsic</a></li>
+ <li><a href="#int_at">'<tt>llvm.adjust.trampoline</tt>' Intrinsic</a></li>
</ol>
</li>
<li><a href="#int_atomics">Atomic intrinsics</a>
<!-- ======================================================================= -->
<h3>
- <a name="int_trampoline">Trampoline Intrinsic</a>
+ <a name="int_trampoline">Trampoline Intrinsics</a>
</h3>
<div>
-<p>This intrinsic makes it possible to excise one parameter, marked with
+<p>These intrinsics make it possible to excise one parameter, marked with
the <a href="#nest"><tt>nest</tt></a> attribute, from a function.
The result is a callable
function pointer lacking the nest parameter - the caller does not need to
<pre class="doc_code">
%tramp = alloca [10 x i8], align 4 ; size and alignment only correct for X86
%tramp1 = getelementptr [10 x i8]* %tramp, i32 0, i32 0
- %p = call i8* @llvm.init.trampoline(i8* %tramp1, i8* bitcast (i32 (i8*, i32, i32)* @f to i8*), i8* %nval)
+ call i8* @llvm.init.trampoline(i8* %tramp1, i8* bitcast (i32 (i8*, i32, i32)* @f to i8*), i8* %nval)
+ %p = call i8* @llvm.adjust.trampoline(i8* %tramp1)
%fp = bitcast i8* %p to i32 (i32, i32)*
</pre>
<h5>Syntax:</h5>
<pre>
- declare i8* @llvm.init.trampoline(i8* <tramp>, i8* <func>, i8* <nval>)
+ declare void @llvm.init.trampoline(i8* <tramp>, i8* <func>, i8* <nval>)
</pre>
<h5>Overview:</h5>
-<p>This fills the memory pointed to by <tt>tramp</tt> with code and returns a
- function pointer suitable for executing it.</p>
+<p>This fills the memory pointed to by <tt>tramp</tt> with executable code,
+ turning it into a trampoline.</p>
<h5>Arguments:</h5>
<p>The <tt>llvm.init.trampoline</tt> intrinsic takes three arguments, all
<h5>Semantics:</h5>
<p>The block of memory pointed to by <tt>tramp</tt> is filled with target
- dependent code, turning it into a function. A pointer to this function is
- returned, but needs to be bitcast to an <a href="#int_trampoline">appropriate
- function pointer type</a> before being called. The new function's signature
- is the same as that of <tt>func</tt> with any arguments marked with
- the <tt>nest</tt> attribute removed. At most one such <tt>nest</tt> argument
- is allowed, and it must be of pointer type. Calling the new function is
- equivalent to calling <tt>func</tt> with the same argument list, but
- with <tt>nval</tt> used for the missing <tt>nest</tt> argument. If, after
- calling <tt>llvm.init.trampoline</tt>, the memory pointed to
- by <tt>tramp</tt> is modified, then the effect of any later call to the
- returned function pointer is undefined.</p>
+ dependent code, turning it into a function. Then <tt>tramp</tt> needs to be
+ passed to <a href="#int_at">llvm.adjust.trampoline</a> to get a pointer
+ which can be <a href="#int_trampoline">bitcast (to a new function) and
+ called</a>. The new function's signature is the same as that of
+ <tt>func</tt> with any arguments marked with the <tt>nest</tt> attribute
+ removed. At most one such <tt>nest</tt> argument is allowed, and it must be of
+ pointer type. Calling the new function is equivalent to calling <tt>func</tt>
+ with the same argument list, but with <tt>nval</tt> used for the missing
+ <tt>nest</tt> argument. If, after calling <tt>llvm.init.trampoline</tt>, the
+ memory pointed to by <tt>tramp</tt> is modified, then the effect of any later call
+ to the returned function pointer is undefined.</p>
+</div>
+
+<!-- _______________________________________________________________________ -->
+<h4>
+ <a name="int_at">
+ '<tt>llvm.adjust.trampoline</tt>' Intrinsic
+ </a>
+</h4>
+
+<div>
+
+<h5>Syntax:</h5>
+<pre>
+ declare i8* @llvm.adjust.trampoline(i8* <tramp>)
+</pre>
+
+<h5>Overview:</h5>
+<p>This performs any required machine-specific adjustment to the address of a
+ trampoline (passed as <tt>tramp</tt>).</p>
+
+<h5>Arguments:</h5>
+<p><tt>tramp</tt> must point to a block of memory which already has trampoline code
+ filled in by a previous call to <a href="#int_it"><tt>llvm.init.trampoline</tt>
+ </a>.</p>
+
+<h5>Semantics:</h5>
+<p>On some architectures the address of the code to be executed needs to be
+ different to the address where the trampoline is actually stored. This
+ intrinsic returns the executable address corresponding to <tt>tramp</tt>
+ after performing the required machine specific adjustments.
+ The pointer returned can then be <a href="#int_trampoline"> bitcast and
+ executed</a>.
+</p>
</div>
index 7f5625cd5e8e62dcfef2a864c7d8dec5399f3702..14b1378e7260a92e70f848688fd8cedfa3a99dc2 100644 (file)
// HANDLENODE node - Used as a handle for various purposes.
HANDLENODE,
- // TRAMPOLINE - This corresponds to the init_trampoline intrinsic.
- // It takes as input a token chain, the pointer to the trampoline,
- // the pointer to the nested function, the pointer to pass for the
- // 'nest' parameter, a SRCVALUE for the trampoline and another for
- // the nested function (allowing targets to access the original
- // Function*). It produces the result of the intrinsic and a token
- // chain as output.
- TRAMPOLINE,
+ // INIT_TRAMPOLINE - This corresponds to the init_trampoline intrinsic. It
+ // takes as input a token chain, the pointer to the trampoline, the pointer
+ // to the nested function, the pointer to pass for the 'nest' parameter, a
+ // SRCVALUE for the trampoline and another for the nested function (allowing
+ // targets to access the original Function*). It produces a token chain as
+ // output.
+ INIT_TRAMPOLINE,
+
+ // ADJUST_TRAMPOLINE - This corresponds to the adjust_trampoline intrinsic.
+ // It takes a pointer to the trampoline and produces a (possibly) new
+ // pointer to the same trampoline with platform-specific adjustments
+ // applied. The pointer it returns points to an executable block of code.
+ ADJUST_TRAMPOLINE,
// TRAP - Trapping instruction
TRAP,
index 947cf1be7d40850c88dded9f768dc2991ea493d3..7646eaaf67fa80dd7e8b0fbeab48f74ef5bfef91 100644 (file)
//===------------------------ Trampoline Intrinsics -----------------------===//
//
-def int_init_trampoline : Intrinsic<[llvm_ptr_ty],
+def int_init_trampoline : Intrinsic<[],
[llvm_ptr_ty, llvm_ptr_ty, llvm_ptr_ty],
- [IntrReadWriteArgMem]>,
- GCCBuiltin<"__builtin_init_trampoline">;
+ [IntrReadWriteArgMem, NoCapture<0>]>,
+ GCCBuiltin<"__builtin_init_trampoline">;
+
+def int_adjust_trampoline : Intrinsic<[llvm_ptr_ty], [llvm_ptr_ty],
+ [IntrReadArgMem]>,
+ GCCBuiltin<"__builtin_adjust_trampoline">;
//===------------------------ Overflow Intrinsics -------------------------===//
//
index b9d841e9d8dc5c728f9c1a8533fd01b4b0945c7d..e672512256f51e78568e6f3b143eaf64171be9a5 100644 (file)
if (Action == TargetLowering::Legal)
Action = TargetLowering::Expand;
break;
- case ISD::TRAMPOLINE:
+ case ISD::INIT_TRAMPOLINE:
+ case ISD::ADJUST_TRAMPOLINE:
case ISD::FRAMEADDR:
case ISD::RETURNADDR:
// These operations lie about being legal: when they claim to be legal,
index 1c7b93af3b1463be58ffd3ae2f0305ed51521741..ec7bfbe495ca36fbbebc5c8cb8ab902f07b4aeba 100644 (file)
case ISD::CTLZ: return "ctlz";
// Trampolines
- case ISD::TRAMPOLINE: return "trampoline";
+ case ISD::INIT_TRAMPOLINE: return "init_trampoline";
+ case ISD::ADJUST_TRAMPOLINE: return "adjust_trampoline";
case ISD::CONDCODE:
switch (cast<CondCodeSDNode>(this)->get()) {
diff --git a/lib/CodeGen/SelectionDAG/SelectionDAGBuilder.cpp b/lib/CodeGen/SelectionDAG/SelectionDAGBuilder.cpp
index 0b0b98d834ece8cc1d251409ad09b411d89ddb76..d8fa0c93dbdda3806a7758fd498ea6cfc26aeb82 100644 (file)
@@ -5016,12 +5016,15 @@ SelectionDAGBuilder::visitIntrinsicCall(const CallInst &I, unsigned Intrinsic) {
Ops[4] = DAG.getSrcValue(I.getArgOperand(0));
Ops[5] = DAG.getSrcValue(F);
- Res = DAG.getNode(ISD::TRAMPOLINE, dl,
- DAG.getVTList(TLI.getPointerTy(), MVT::Other),
- Ops, 6);
+ Res = DAG.getNode(ISD::INIT_TRAMPOLINE, dl, MVT::Other, Ops, 6);
- setValue(&I, Res);
- DAG.setRoot(Res.getValue(1));
+ DAG.setRoot(Res);
+ return 0;
+ }
+ case Intrinsic::adjust_trampoline: {
+ setValue(&I, DAG.getNode(ISD::ADJUST_TRAMPOLINE, dl,
+ TLI.getPointerTy(),
+ getValue(I.getArgOperand(0))));
return 0;
}
case Intrinsic::gcroot:
index be94b08e75a52e919e9c1078b6a7e8b8e24376ad..39e6c2412f64055bdb4c5d8da168a27f333021c4 100644 (file)
setOperationAction(ISD::TRAP, MVT::Other, Legal);
// TRAMPOLINE is custom lowered.
- setOperationAction(ISD::TRAMPOLINE, MVT::Other, Custom);
+ setOperationAction(ISD::INIT_TRAMPOLINE, MVT::Other, Custom);
+ setOperationAction(ISD::ADJUST_TRAMPOLINE, MVT::Other, Custom);
// VASTART needs to be custom lowered to use the VarArgsFrameIndex
setOperationAction(ISD::VASTART , MVT::Other, Custom);
return DAG.getLoad(VT, dl, InChain, Result, MachinePointerInfo(), false, false, 0);
}
-SDValue PPCTargetLowering::LowerTRAMPOLINE(SDValue Op,
- SelectionDAG &DAG) const {
+SDValue PPCTargetLowering::LowerADJUST_TRAMPOLINE(SDValue Op,
+ SelectionDAG &DAG) const {
+ return Op.getOperand(0);
+}
+
+SDValue PPCTargetLowering::LowerINIT_TRAMPOLINE(SDValue Op,
+ SelectionDAG &DAG) const {
SDValue Chain = Op.getOperand(0);
SDValue Trmp = Op.getOperand(1); // trampoline
SDValue FPtr = Op.getOperand(2); // nested function
// Lower to a call to __trampoline_setup(Trmp, TrampSize, FPtr, ctx_reg)
std::pair<SDValue, SDValue> CallResult =
- LowerCallTo(Chain, Op.getValueType().getTypeForEVT(*DAG.getContext()),
+ LowerCallTo(Chain, Type::getVoidTy(*DAG.getContext()),
false, false, false, false, 0, CallingConv::C, false,
/*isReturnValueUsed=*/true,
DAG.getExternalSymbol("__trampoline_setup", PtrVT),
Args, DAG, dl);
- SDValue Ops[] =
- { CallResult.first, CallResult.second };
-
- return DAG.getMergeValues(Ops, 2, dl);
+ return CallResult.second;
}
SDValue PPCTargetLowering::LowerVASTART(SDValue Op, SelectionDAG &DAG,
@@ -4499,7 +4502,8 @@ SDValue PPCTargetLowering::LowerOperation(SDValue Op, SelectionDAG &DAG) const {
case ISD::GlobalTLSAddress: llvm_unreachable("TLS not implemented for PPC");
case ISD::JumpTable: return LowerJumpTable(Op, DAG);
case ISD::SETCC: return LowerSETCC(Op, DAG);
- case ISD::TRAMPOLINE: return LowerTRAMPOLINE(Op, DAG);
+ case ISD::INIT_TRAMPOLINE: return LowerINIT_TRAMPOLINE(Op, DAG);
+ case ISD::ADJUST_TRAMPOLINE: return LowerADJUST_TRAMPOLINE(Op, DAG);
case ISD::VASTART:
return LowerVASTART(Op, DAG, PPCSubTarget);
index a4f8e2a839e0bd6e134ab92a41c2d72dafc7532f..602f70abfc4a28c288e5659dc48018fbe73b76d2 100644 (file)
SDValue LowerGlobalAddress(SDValue Op, SelectionDAG &DAG) const;
SDValue LowerJumpTable(SDValue Op, SelectionDAG &DAG) const;
SDValue LowerSETCC(SDValue Op, SelectionDAG &DAG) const;
- SDValue LowerTRAMPOLINE(SDValue Op, SelectionDAG &DAG) const;
+ SDValue LowerINIT_TRAMPOLINE(SDValue Op, SelectionDAG &DAG) const;
+ SDValue LowerADJUST_TRAMPOLINE(SDValue Op, SelectionDAG &DAG) const;
SDValue LowerVASTART(SDValue Op, SelectionDAG &DAG,
const PPCSubtarget &Subtarget) const;
SDValue LowerVAARG(SDValue Op, SelectionDAG &DAG,
index 8005408412b33e0ac0be87a3799727edb81e5eb3..fa5f720ef0ebef6762f6c85fd4e88bfb88934fd2 100644 (file)
setOperationAction(ISD::FRAME_TO_ARGS_OFFSET, MVT::i32, Custom);
setOperationAction(ISD::FRAME_TO_ARGS_OFFSET, MVT::i64, Custom);
- setOperationAction(ISD::TRAMPOLINE, MVT::Other, Custom);
+ setOperationAction(ISD::INIT_TRAMPOLINE, MVT::Other, Custom);
+ setOperationAction(ISD::ADJUST_TRAMPOLINE, MVT::Other, Custom);
setOperationAction(ISD::TRAP, MVT::Other, Legal);
@@ -9406,8 +9407,13 @@ SDValue X86TargetLowering::LowerEH_RETURN(SDValue Op, SelectionDAG &DAG) const {
Chain, DAG.getRegister(StoreAddrReg, getPointerTy()));
}
-SDValue X86TargetLowering::LowerTRAMPOLINE(SDValue Op,
- SelectionDAG &DAG) const {
+SDValue X86TargetLowering::LowerADJUST_TRAMPOLINE(SDValue Op,
+ SelectionDAG &DAG) const {
+ return Op.getOperand(0);
+}
+
+SDValue X86TargetLowering::LowerINIT_TRAMPOLINE(SDValue Op,
+ SelectionDAG &DAG) const {
SDValue Root = Op.getOperand(0);
SDValue Trmp = Op.getOperand(1); // trampoline
SDValue FPtr = Op.getOperand(2); // nested function
MachinePointerInfo(TrmpAddr, 22),
false, false, 0);
- SDValue Ops[] =
- { Trmp, DAG.getNode(ISD::TokenFactor, dl, MVT::Other, OutChains, 6) };
- return DAG.getMergeValues(Ops, 2, dl);
+ return DAG.getNode(ISD::TokenFactor, dl, MVT::Other, OutChains, 6);
} else {
const Function *Func =
cast<Function>(cast<SrcValueSDNode>(Op.getOperand(5))->getValue());
MachinePointerInfo(TrmpAddr, 6),
false, false, 1);
- SDValue Ops[] =
- { Trmp, DAG.getNode(ISD::TokenFactor, dl, MVT::Other, OutChains, 4) };
- return DAG.getMergeValues(Ops, 2, dl);
+ return DAG.getNode(ISD::TokenFactor, dl, MVT::Other, OutChains, 4);
}
}
@@ -10356,7 +10358,8 @@ SDValue X86TargetLowering::LowerOperation(SDValue Op, SelectionDAG &DAG) const {
return LowerFRAME_TO_ARGS_OFFSET(Op, DAG);
case ISD::DYNAMIC_STACKALLOC: return LowerDYNAMIC_STACKALLOC(Op, DAG);
case ISD::EH_RETURN: return LowerEH_RETURN(Op, DAG);
- case ISD::TRAMPOLINE: return LowerTRAMPOLINE(Op, DAG);
+ case ISD::INIT_TRAMPOLINE: return LowerINIT_TRAMPOLINE(Op, DAG);
+ case ISD::ADJUST_TRAMPOLINE: return LowerADJUST_TRAMPOLINE(Op, DAG);
case ISD::FLT_ROUNDS_: return LowerFLT_ROUNDS_(Op, DAG);
case ISD::CTLZ: return LowerCTLZ(Op, DAG);
case ISD::CTTZ: return LowerCTTZ(Op, DAG);
index db5909757764c1873fb39d41d3fd1b89d64a7076..e83fea95cbac4c1bcf679afb2942d495326edbe3 100644 (file)
SDValue LowerFRAMEADDR(SDValue Op, SelectionDAG &DAG) const;
SDValue LowerFRAME_TO_ARGS_OFFSET(SDValue Op, SelectionDAG &DAG) const;
SDValue LowerEH_RETURN(SDValue Op, SelectionDAG &DAG) const;
- SDValue LowerTRAMPOLINE(SDValue Op, SelectionDAG &DAG) const;
+ SDValue LowerINIT_TRAMPOLINE(SDValue Op, SelectionDAG &DAG) const;
+ SDValue LowerADJUST_TRAMPOLINE(SDValue Op, SelectionDAG &DAG) const;
SDValue LowerFLT_ROUNDS_(SDValue Op, SelectionDAG &DAG) const;
SDValue LowerCTLZ(SDValue Op, SelectionDAG &DAG) const;
SDValue LowerCTTZ(SDValue Op, SelectionDAG &DAG) const;
index d23cfe0b92dcb5d3ed968b1e41e18696b791ed22..3926a7f87f460a3ab06d6182bf37255ff2d1c49b 100644 (file)
setOperationAction(ISD::DYNAMIC_STACKALLOC, MVT::i32, Expand);
// TRAMPOLINE is custom lowered.
- setOperationAction(ISD::TRAMPOLINE, MVT::Other, Custom);
+ setOperationAction(ISD::INIT_TRAMPOLINE, MVT::Other, Custom);
+ setOperationAction(ISD::ADJUST_TRAMPOLINE, MVT::Other, Custom);
maxStoresPerMemset = maxStoresPerMemsetOptSize = 4;
maxStoresPerMemmove = maxStoresPerMemmoveOptSize
case ISD::ADD:
case ISD::SUB: return ExpandADDSUB(Op.getNode(), DAG);
case ISD::FRAMEADDR: return LowerFRAMEADDR(Op, DAG);
- case ISD::TRAMPOLINE: return LowerTRAMPOLINE(Op, DAG);
+ case ISD::INIT_TRAMPOLINE: return LowerINIT_TRAMPOLINE(Op, DAG);
+ case ISD::ADJUST_TRAMPOLINE: return LowerADJUST_TRAMPOLINE(Op, DAG);
default:
llvm_unreachable("unimplemented operand");
return SDValue();
}
SDValue XCoreTargetLowering::
-LowerTRAMPOLINE(SDValue Op, SelectionDAG &DAG) const {
+LowerADJUST_TRAMPOLINE(SDValue Op, SelectionDAG &DAG) const {
+ return Op.getOperand(0);
+}
+
+SDValue XCoreTargetLowering::
+LowerINIT_TRAMPOLINE(SDValue Op, SelectionDAG &DAG) const {
SDValue Chain = Op.getOperand(0);
SDValue Trmp = Op.getOperand(1); // trampoline
SDValue FPtr = Op.getOperand(2); // nested function
MachinePointerInfo(TrmpAddr, 16), false, false,
0);
- SDValue Ops[] =
- { Trmp, DAG.getNode(ISD::TokenFactor, dl, MVT::Other, OutChains, 5) };
- return DAG.getMergeValues(Ops, 2, dl);
+ return DAG.getNode(ISD::TokenFactor, dl, MVT::Other, OutChains, 5);
}
//===----------------------------------------------------------------------===//
index 246da9eee5504ae2f14b142da409f1e47f83ebe5..d6c5b329a0a07c94840047438bd2447d1a86ae5c 100644 (file)
SDValue LowerUMUL_LOHI(SDValue Op, SelectionDAG &DAG) const;
SDValue LowerSMUL_LOHI(SDValue Op, SelectionDAG &DAG) const;
SDValue LowerFRAMEADDR(SDValue Op, SelectionDAG &DAG) const;
- SDValue LowerTRAMPOLINE(SDValue Op, SelectionDAG &DAG) const;
+ SDValue LowerINIT_TRAMPOLINE(SDValue Op, SelectionDAG &DAG) const;
+ SDValue LowerADJUST_TRAMPOLINE(SDValue Op, SelectionDAG &DAG) const;
// Inline asm support
std::pair<unsigned, const TargetRegisterClass*>
index c6bdb089982a4183cc904561c7de614fcf249be2..be4454b878991c50c647532fbb9e733246fb0ed0 100644 (file)
#define INSTCOMBINE_INSTCOMBINE_H
#include "InstCombineWorklist.h"
+#include "llvm/IntrinsicInst.h"
#include "llvm/Operator.h"
#include "llvm/Pass.h"
#include "llvm/Analysis/ValueTracking.h"
Instruction *visitCallSite(CallSite CS);
Instruction *tryOptimizeCall(CallInst *CI, const TargetData *TD);
bool transformConstExprCastCall(CallSite CS);
- Instruction *transformCallThroughTrampoline(CallSite CS);
+ Instruction *transformCallThroughTrampoline(CallSite CS,
+ IntrinsicInst *Tramp);
Instruction *transformZExtICmp(ICmpInst *ICI, Instruction &CI,
bool DoXform = true);
Instruction *transformSExtICmp(ICmpInst *ICI, Instruction &CI);
diff --git a/lib/Transforms/InstCombine/InstCombineCalls.cpp b/lib/Transforms/InstCombine/InstCombineCalls.cpp
index 4c9cbdb4e63f5034798d196f8c2086499d1deb37..7da3343fb4ed7ad06b623d5e76890501ba9bd1a6 100644 (file)
//===----------------------------------------------------------------------===//
#include "InstCombine.h"
-#include "llvm/IntrinsicInst.h"
#include "llvm/Support/CallSite.h"
#include "llvm/Target/TargetData.h"
#include "llvm/Analysis/MemoryBuiltins.h"
@@ -821,6 +820,83 @@ Instruction *InstCombiner::tryOptimizeCall(CallInst *CI, const TargetData *TD) {
return Simplifier.NewInstruction;
}
+static IntrinsicInst *FindInitTrampolineFromAlloca(Value *TrampMem) {
+ // Strip off at most one level of pointer casts, looking for an alloca. This
+ // is good enough in practice and simpler than handling any number of casts.
+ Value *Underlying = TrampMem->stripPointerCasts();
+ if (Underlying != TrampMem &&
+ (!Underlying->hasOneUse() || *Underlying->use_begin() != TrampMem))
+ return 0;
+ if (!isa<AllocaInst>(Underlying))
+ return 0;
+
+ IntrinsicInst *InitTrampoline = 0;
+ for (Value::use_iterator I = TrampMem->use_begin(), E = TrampMem->use_end();
+ I != E; I++) {
+ IntrinsicInst *II = dyn_cast<IntrinsicInst>(*I);
+ if (!II)
+ return 0;
+ if (II->getIntrinsicID() == Intrinsic::init_trampoline) {
+ if (InitTrampoline)
+ // More than one init_trampoline writes to this value. Give up.
+ return 0;
+ InitTrampoline = II;
+ continue;
+ }
+ if (II->getIntrinsicID() == Intrinsic::adjust_trampoline)
+ // Allow any number of calls to adjust.trampoline.
+ continue;
+ return 0;
+ }
+
+ // No call to init.trampoline found.
+ if (!InitTrampoline)
+ return 0;
+
+ // Check that the alloca is being used in the expected way.
+ if (InitTrampoline->getOperand(0) != TrampMem)
+ return 0;
+
+ return InitTrampoline;
+}
+
+static IntrinsicInst *FindInitTrampolineFromBB(IntrinsicInst *AdjustTramp,
+ Value *TrampMem) {
+ // Visit all the previous instructions in the basic block, and try to find a
+ // init.trampoline which has a direct path to the adjust.trampoline.
+ for (BasicBlock::iterator I = AdjustTramp,
+ E = AdjustTramp->getParent()->begin(); I != E; ) {
+ Instruction *Inst = --I;
+ if (IntrinsicInst *II = dyn_cast<IntrinsicInst>(I))
+ if (II->getIntrinsicID() == Intrinsic::init_trampoline &&
+ II->getOperand(0) == TrampMem)
+ return II;
+ if (Inst->mayWriteToMemory())
+ return 0;
+ }
+ return 0;
+}
+
+// Given a call to llvm.adjust.trampoline, find and return the corresponding
+// call to llvm.init.trampoline if the call to the trampoline can be optimized
+// to a direct call to a function. Otherwise return NULL.
+//
+static IntrinsicInst *FindInitTrampoline(Value *Callee) {
+ Callee = Callee->stripPointerCasts();
+ IntrinsicInst *AdjustTramp = dyn_cast<IntrinsicInst>(Callee);
+ if (!AdjustTramp ||
+ AdjustTramp->getIntrinsicID() != Intrinsic::adjust_trampoline)
+ return 0;
+
+ Value *TrampMem = AdjustTramp->getOperand(0);
+
+ if (IntrinsicInst *IT = FindInitTrampolineFromAlloca(TrampMem))
+ return IT;
+ if (IntrinsicInst *IT = FindInitTrampolineFromBB(AdjustTramp, TrampMem))
+ return IT;
+ return 0;
+}
+
// visitCallSite - Improvements for call and invoke instructions.
//
Instruction *InstCombiner::visitCallSite(CallSite CS) {
return EraseInstFromFunction(*CS.getInstruction());
}
- if (BitCastInst *BC = dyn_cast<BitCastInst>(Callee))
- if (IntrinsicInst *In = dyn_cast<IntrinsicInst>(BC->getOperand(0)))
- if (In->getIntrinsicID() == Intrinsic::init_trampoline)
- return transformCallThroughTrampoline(CS);
+ if (IntrinsicInst *II = FindInitTrampoline(Callee))
+ return transformCallThroughTrampoline(CS, II);
PointerType *PTy = cast<PointerType>(Callee->getType());
FunctionType *FTy = cast<FunctionType>(PTy->getElementType());
return true;
}
-// transformCallThroughTrampoline - Turn a call to a function created by the
-// init_trampoline intrinsic into a direct call to the underlying function.
+// transformCallThroughTrampoline - Turn a call to a function created by
+// init_trampoline / adjust_trampoline intrinsic pair into a direct call to the
+// underlying function.
//
-Instruction *InstCombiner::transformCallThroughTrampoline(CallSite CS) {
+Instruction *
+InstCombiner::transformCallThroughTrampoline(CallSite CS,
+ IntrinsicInst *Tramp) {
Value *Callee = CS.getCalledValue();
PointerType *PTy = cast<PointerType>(Callee->getType());
FunctionType *FTy = cast<FunctionType>(PTy->getElementType());
if (Attrs.hasAttrSomewhere(Attribute::Nest))
return 0;
- IntrinsicInst *Tramp =
- cast<IntrinsicInst>(cast<BitCastInst>(Callee)->getOperand(0));
+ assert(Tramp &&
+ "transformCallThroughTrampoline called with incorrect CallSite.");
Function *NestF =cast<Function>(Tramp->getArgOperand(1)->stripPointerCasts());
PointerType *NestFPTy = cast<PointerType>(NestF->getType());
index 572018105aa09c402f6137c7313423af3af381a8..04221d461d7e9d22aee6eefb045f0d351758cf21 100644 (file)
switch (Name[0]) {
default: break;
+ case 'i':
+ // This upgrades the old llvm.init.trampoline to the new
+ // llvm.init.trampoline and llvm.adjust.trampoline pair.
+ if (Name == "init.trampoline") {
+ // The new llvm.init.trampoline returns nothing.
+ if (FTy->getReturnType()->isVoidTy())
+ break;
+
+ assert(FTy->getNumParams() == 3 && "old init.trampoline takes 3 args!");
+
+ // Change the name of the old intrinsic so that we can play with its type.
+ std::string NameTmp = F->getName();
+ F->setName("");
+ NewFn = cast<Function>(M->getOrInsertFunction(
+ NameTmp,
+ Type::getVoidTy(M->getContext()),
+ FTy->getParamType(0), FTy->getParamType(1),
+ FTy->getParamType(2), (Type *)0));
+ return true;
+ }
case 'p':
// This upgrades the llvm.prefetch intrinsic to accept one more parameter,
// which is a instruction / data cache identifier. The old version only
CI->eraseFromParent();
break;
}
+ case Intrinsic::init_trampoline: {
+
+ // Transform
+ // %tramp = call i8* llvm.init.trampoline (i8* x, i8* y, i8* z)
+ // to
+ // call void llvm.init.trampoline (i8* %x, i8* %y, i8* %z)
+ // %tramp = call i8* llvm.adjust.trampoline (i8* %x)
+
+ Function *AdjustTrampolineFn =
+ cast<Function>(Intrinsic::getDeclaration(F->getParent(),
+ Intrinsic::adjust_trampoline));
+
+ IRBuilder<> Builder(C);
+ Builder.SetInsertPoint(CI);
+
+ Builder.CreateCall3(NewFn, CI->getArgOperand(0), CI->getArgOperand(1),
+ CI->getArgOperand(2));
+
+ CallInst *AdjustCall = Builder.CreateCall(AdjustTrampolineFn,
+ CI->getArgOperand(0),
+ CI->getName());
+ if (!CI->use_empty())
+ CI->replaceAllUsesWith(AdjustCall);
+ CI->eraseFromParent();
+ break;
+ }
}
}
index eb4ac769be01b43a38bb5ac5721f38d76893781e..daffa3d3af958ac3d86b4e0c4738e7313e33fbdd 100644 (file)
tail call void @llvm.prefetch(i8* %ptr, i32 0, i32 1)
ret void
}
+
+declare i32 @nest_f(i8* nest, i32)
+declare i8* @llvm.init.trampoline(i8*, i8*, i8*)
+
+define void @test_trampolines() {
+; CHECK: call void @llvm.init.trampoline(i8* null, i8* bitcast (i32 (i8*, i32)* @nest_f to i8*), i8* null)
+; CHECK: call i8* @llvm.adjust.trampoline(i8* null)
+
+ call i8* @llvm.init.trampoline(i8* null,
+ i8* bitcast (i32 (i8*, i32)* @nest_f to i8*),
+ i8* null)
+ ret void
+}
index bc05bb176352fa31d1be525943e8a4a78c8b03ec..91b201146b6d89fdef10ab99d5b9f9d777994375 100644 (file)
store %struct.NSBitmapImageRep* %4, %struct.NSBitmapImageRep** %3, align 4
%TRAMP.91 = bitcast %struct.__builtin_trampoline* %TRAMP.9 to i8* ; <i8*> [#uses=1]
%FRAME.72 = bitcast %"struct.FRAME.-[NSBitmapImageRep copyWithZone:]"* %FRAME.7 to i8* ; <i8*> [#uses=1]
- %tramp = call i8* @llvm.init.trampoline(i8* %TRAMP.91, i8* bitcast (void (%"struct.FRAME.-[NSBitmapImageRep copyWithZone:]"*, %struct.__block_1*, %struct.CGImage*)* @__helper_1.1632 to i8*), i8* %FRAME.72) ; <i8*> [#uses=1]
+ call void @llvm.init.trampoline(i8* %TRAMP.91, i8* bitcast (void (%"struct.FRAME.-[NSBitmapImageRep copyWithZone:]"*, %struct.__block_1*, %struct.CGImage*)* @__helper_1.1632 to i8*), i8* %FRAME.72) ; <i8*> [#uses=1]
+ %tramp = call i8* @llvm.adjust.trampoline(i8* %TRAMP.91)
store i8* %tramp, i8** %0, align 4
%5 = getelementptr %"struct.FRAME.-[NSBitmapImageRep copyWithZone:]"* %FRAME.7, i32 0, i32 1 ; <void (%struct.__block_1*, %struct.CGImage*)**> [#uses=1]
%6 = load i8** %0, align 4 ; <i8*> [#uses=1]
ret %struct.objc_object* %retval5
}
-declare i8* @llvm.init.trampoline(i8*, i8*, i8*) nounwind
+declare void @llvm.init.trampoline(i8*, i8*, i8*) nounwind
+declare i8* @llvm.adjust.trampoline(i8*) nounwind
define internal void @__helper_1.1632(%"struct.FRAME.-[NSBitmapImageRep copyWithZone:]"* nest %CHAIN.8, %struct.__block_1* %_self, %struct.CGImage* %cgImage) nounwind {
entry:
index 4e1aba025b2fbd24837d69c468a14a83283c87d4..6b42134997bf3fd82ce7332e7f0f76f8cbedfcb6 100644 (file)
%FRAME.0 = alloca %struct.FRAME.f, align 4
%TRAMP.23.sub = getelementptr inbounds [20 x i8]* %TRAMP.23, i32 0, i32 0
%FRAME.02 = bitcast %struct.FRAME.f* %FRAME.0 to i8*
- %tramp = call i8* @llvm.init.trampoline(i8* %TRAMP.23.sub, i8* bitcast (i32 (%struct.FRAME.f*)* @g.1101 to i8*), i8* %FRAME.02)
+ call void @llvm.init.trampoline(i8* %TRAMP.23.sub, i8* bitcast (i32 (%struct.FRAME.f*)* @g.1101 to i8*), i8* %FRAME.02)
+ %tramp = call i8* @llvm.adjust.trampoline(i8* %TRAMP.23.sub)
%0 = getelementptr inbounds %struct.FRAME.f* %FRAME.0, i32 0, i32 1
%1 = bitcast i8* %tramp to i32 ()*
store i32 ()* %1, i32 ()** %0, align 4
ret i32 %1
}
-declare i8* @llvm.init.trampoline(i8*, i8*, i8*) nounwind
+declare void @llvm.init.trampoline(i8*, i8*, i8*) nounwind
+declare i8* @llvm.adjust.trampoline(i8*) nounwind
declare void @h(i32 ()*)
diff --git a/test/Transforms/InstCombine/2008-01-14-VarArgTrampoline.ll b/test/Transforms/InstCombine/2008-01-14-VarArgTrampoline.ll
index 9bb940893935f6ed54c1deeaeb4719963201e1cc..aacea9df5b31e5192d06f6dd56713c0ae27db4b7 100644 (file)
%struct.FRAME.nest = type { i32, i32 (...)* }
%struct.__builtin_trampoline = type { [10 x i8] }
-declare i8* @llvm.init.trampoline(i8*, i8*, i8*) nounwind
+declare void @llvm.init.trampoline(i8*, i8*, i8*) nounwind
+declare i8* @llvm.adjust.trampoline(i8*) nounwind
declare i32 @f(%struct.FRAME.nest* nest , ...)
%tmp3 = getelementptr %struct.FRAME.nest* %FRAME.0, i32 0, i32 0 ; <i32*> [#uses=1]
store i32 %n, i32* %tmp3, align 8
%FRAME.06 = bitcast %struct.FRAME.nest* %FRAME.0 to i8* ; <i8*> [#uses=1]
- %tramp = call i8* @llvm.init.trampoline( i8* %TRAMP.216.sub, i8* bitcast (i32 (%struct.FRAME.nest*, ...)* @f to i8*), i8* %FRAME.06 ) ; <i8*> [#uses=1]
+ call void @llvm.init.trampoline( i8* %TRAMP.216.sub, i8* bitcast (i32 (%struct.FRAME.nest*, ...)* @f to i8*), i8* %FRAME.06 ) ; <i8*> [#uses=1]
+ %tramp = call i8* @llvm.adjust.trampoline( i8* %TRAMP.216.sub)
%tmp7 = getelementptr %struct.FRAME.nest* %FRAME.0, i32 0, i32 1 ; <i32 (...)**> [#uses=1]
%tmp89 = bitcast i8* %tramp to i32 (...)* ; <i32 (...)*> [#uses=2]
store i32 (...)* %tmp89, i32 (...)** %tmp7, align 8