summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: ec2e968)
raw | patch | inline | side by side (parent: ec2e968)
author | Eli Bendersky <eliben@google.com> | |
Tue, 19 Mar 2013 15:26:24 +0000 (15:26 +0000) | ||
committer | Eli Bendersky <eliben@google.com> | |
Tue, 19 Mar 2013 15:26:24 +0000 (15:26 +0000) |
(and possibly others). The attached patch removes it, and tries to
update comments accordingly.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@177406 91177308-0d34-0410-b5e6-96231b3b80d8
update comments accordingly.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@177406 91177308-0d34-0410-b5e6-96231b3b80d8
include/llvm/Linker.h | patch | blob | history | |
lib/Linker/LinkModules.cpp | patch | blob | history | |
lib/Linker/Linker.cpp | patch | blob | history |
diff --git a/include/llvm/Linker.h b/include/llvm/Linker.h
index 8bf9efa8e2c7d4f264c016717c819f7a108a1e01..679638427d67ef7cb549545d4906ec19eec41eb9 100644 (file)
--- a/include/llvm/Linker.h
+++ b/include/llvm/Linker.h
// License. See LICENSE.TXT for details.
//
//===----------------------------------------------------------------------===//
-//
-// This file defines the interface to the module/file/archive linker.
-//
-//===----------------------------------------------------------------------===//
#ifndef LLVM_LINKER_H
#define LLVM_LINKER_H
#include <vector>
namespace llvm {
- namespace sys { class Path; }
class Module;
class LLVMContext;
/// In this case the Linker still retains ownership of the Module. If the
/// releaseModule() method is used, the ownership of the Module is transferred
/// to the caller and the Linker object is only suitable for destruction.
-/// The Linker can link Modules from memory. It retains a set of search paths
-/// in which to find any libraries presented to it. By default, the linker
+/// The Linker can link Modules from memory. By default, the linker
/// will generate error and warning messages to stderr but this capability can
/// be turned off with the QuietWarnings and QuietErrors flags. It can also be
/// instructed to verbosely print out the linking actions it is taking with
/// must arrange for its destruct. After this method is called, the Linker
/// terminates the linking session for the returned Module. It will no
/// longer utilize the returned Module but instead resets itself for
- /// subsequent linking as if the constructor had been called. The Linker's
- /// LibPaths and flags to be reset, and memory will be released.
+ /// subsequent linking as if the constructor had been called.
/// @brief Release the linked/composite module.
Module* releaseModule();
- /// This method gets the list of libraries that form the path that the
- /// Linker will search when it is presented with a library name.
- /// @brief Get the Linkers library path
- const std::vector<sys::Path>& getLibPaths() const { return LibPaths; }
-
/// This method returns an error string suitable for printing to the user.
/// The return value will be empty unless an error occurred in one of the
/// LinkIn* methods. In those cases, the LinkIn* methods will have returned
/// @name Mutators
/// @{
public:
- /// Add a path to the list of paths that the Linker will search. The Linker
- /// accumulates the set of libraries added
- /// library paths for the target platform. The standard libraries will
- /// always be searched last. The added libraries will be searched in the
- /// order added.
- /// @brief Add a path.
- void addPath(const sys::Path& path);
-
- /// Add a set of paths to the list of paths that the linker will search. The
- /// Linker accumulates the set of libraries added. The \p paths will be
- /// added to the end of the Linker's list. Order will be retained.
- /// @brief Add a set of paths.
- void addPaths(const std::vector<std::string>& paths);
-
- /// This method augments the Linker's list of library paths with the system
- /// paths of the host operating system, include LLVM_LIB_SEARCH_PATH.
- /// @brief Add the system paths.
- void addSystemPaths();
-
- /// Control optional linker behavior by setting a group of flags. The flags
- /// are defined in the ControlFlags enumeration.
- /// @see ControlFlags
- /// @brief Set control flags.
- void setFlags(unsigned flags) { Flags = flags; }
-
/// This method links the \p Src module into the Linker's Composite module
/// by calling LinkModules.
/// @see LinkModules
private:
LLVMContext& Context; ///< The context for global information
Module* Composite; ///< The composite module linked together
- std::vector<sys::Path> LibPaths; ///< The library search paths
unsigned Flags; ///< Flags to control optional behavior.
std::string Error; ///< Text of error that occurred.
std::string ProgramName; ///< Name of the program being linked
index 0acbcfadafb258043265ce4fbd028891f8daba8a..74cbdadd61eba980e69aa22c382beb5b8e9d5e94 100644 (file)
#include "llvm/ADT/Optional.h"
#include "llvm/ADT/SetVector.h"
#include "llvm/ADT/SmallPtrSet.h"
+#include "llvm/ADT/SmallString.h"
#include "llvm/IR/Constants.h"
#include "llvm/IR/DerivedTypes.h"
#include "llvm/IR/Instructions.h"
#include "llvm/IR/Module.h"
#include "llvm/IR/TypeFinder.h"
#include "llvm/Support/Debug.h"
-#include "llvm/Support/Path.h"
#include "llvm/Support/raw_ostream.h"
#include "llvm/Transforms/Utils/Cloning.h"
#include "llvm/Transforms/Utils/ValueMapper.h"
diff --git a/lib/Linker/Linker.cpp b/lib/Linker/Linker.cpp
index c8ea8ff0a9e33ffcc36480e88fe57165459034dd..74d24f278b7778223762f75b44627a3bed8e13b4 100644 (file)
--- a/lib/Linker/Linker.cpp
+++ b/lib/Linker/Linker.cpp
#include "llvm/Bitcode/ReaderWriter.h"
#include "llvm/IR/Module.h"
#include "llvm/Support/MemoryBuffer.h"
-#include "llvm/Support/Path.h"
#include "llvm/Support/raw_ostream.h"
#include "llvm/Support/system_error.h"
using namespace llvm;
LLVMContext& C, unsigned flags):
Context(C),
Composite(new Module(modname, C)),
- LibPaths(),
Flags(flags),
Error(),
ProgramName(progname) { }
Linker::Linker(StringRef progname, Module* aModule, unsigned flags) :
Context(aModule->getContext()),
Composite(aModule),
- LibPaths(),
Flags(flags),
Error(),
ProgramName(progname) { }
errs() << " " << message << "\n";
}
-void
-Linker::addPath(const sys::Path& path) {
- LibPaths.push_back(path);
-}
-
-void
-Linker::addPaths(const std::vector<std::string>& paths) {
- for (unsigned i = 0, e = paths.size(); i != e; ++i)
- LibPaths.push_back(sys::Path(paths[i]));
-}
-
-void
-Linker::addSystemPaths() {
- sys::Path::GetBitcodeLibraryPaths(LibPaths);
- LibPaths.insert(LibPaths.begin(),sys::Path("./"));
-}
-
Module*
Linker::releaseModule() {
Module* result = Composite;
- LibPaths.clear();
Error.clear();
Composite = 0;
Flags = 0;