summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 0f2f62d)
raw | patch | inline | side by side (parent: 0f2f62d)
author | Paul Robinson <paul_robinson@playstation.sony.com> | |
Thu, 14 Nov 2013 18:47:23 +0000 (18:47 +0000) | ||
committer | Paul Robinson <paul_robinson@playstation.sony.com> | |
Thu, 14 Nov 2013 18:47:23 +0000 (18:47 +0000) |
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@194720 91177308-0d34-0410-b5e6-96231b3b80d8
docs/Passes.rst | patch | blob | history | |
docs/ProgrammersManual.rst | patch | blob | history |
diff --git a/docs/Passes.rst b/docs/Passes.rst
index d30c3ca4a00ffe8745ea897730f2eb7a75169d6a..029e472bcd37d00f83178706f80ce8b27929f6c7 100644 (file)
--- a/docs/Passes.rst
+++ b/docs/Passes.rst
-------------------------------------------------
This pass munges the code in the input function to better prepare it for
-SelectionDAG-based code generation. This works around limitations in it's
+SelectionDAG-based code generation. This works around limitations in its
basic-block-at-a-time approach. It should eventually be removed.
``-constmerge``: Merge Duplicate Global Constants
index 2910a2aa1c1990fa05c42992008554d142a327ed..99aa5c7877b4e2230e68629fb3156560c48907cb 100644 (file)
set and has the sum of constant factors from the set-like container and the
sequential container that it uses. Use it **only** if you need to iterate over
the elements in a deterministic order. SetVector is also expensive to delete
-elements out of (linear time), unless you use it's "pop_back" method, which is
+elements out of (linear time), unless you use its "pop_back" method, which is
faster.
``SetVector`` is an adapter class that defaults to using ``std::vector`` and a
Note that both of these calls must be made *in isolation*. That is to say that
no other LLVM API calls may be executing at any time during the execution of
-``llvm_start_multithreaded()`` or ``llvm_stop_multithreaded``. It's is the
+``llvm_start_multithreaded()`` or ``llvm_stop_multithreaded``. It is the
client's responsibility to enforce this isolation.
The return value of ``llvm_start_multithreaded()`` indicates the success or