summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: dc8a318)
raw | patch | inline | side by side (parent: dc8a318)
author | Chandler Carruth <chandlerc@gmail.com> | |
Sun, 28 Jul 2013 09:05:49 +0000 (09:05 +0000) | ||
committer | Chandler Carruth <chandlerc@gmail.com> | |
Sun, 28 Jul 2013 09:05:49 +0000 (09:05 +0000) |
I forgot that we had two totally independent things here. :: sigh ::
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@187327 91177308-0d34-0410-b5e6-96231b3b80d8
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@187327 91177308-0d34-0410-b5e6-96231b3b80d8
lib/Transforms/Scalar/SROA.cpp | patch | blob | history |
index ef4558878ac574557931cd6ce3c2e0102276218e..1525caa868b801bc2ccf95814fa4aadca475e014 100644 (file)
/// \brief Construct the slices of a particular alloca.
AllocaSlices(const DataLayout &DL, AllocaInst &AI);
- /// \brief Whether we determined during the trivial analysis of the alloca
- /// that it was immediately promotable with mem2reg.
- bool isAllocaPromotable() const { return IsAllocaPromotable; }
-
- /// \brief A list of directly stored values when \c isAllocaPromotable is
- /// true.
- ///
- /// The contents are undefined if the alloca is not trivially promotable.
- /// This is used to detect other allocas which should be iterated on when
- /// doing direct promotion.
- ArrayRef<Value *> getStoredValues() const { return StoredValues; }
-
/// \brief Test whether a pointer to the allocation escapes our analysis.
///
/// If this is true, the slices are never fully built and should be
class SliceBuilder;
friend class AllocaSlices::SliceBuilder;
+#if !defined(NDEBUG) || defined(LLVM_ENABLE_DUMP)
/// \brief Handle to alloca instruction to simplify method interfaces.
AllocaInst &AI;
-
- /// \brief A flag indicating if the alloca is trivially promotable.
- ///
- /// While walking the alloca's uses we track when the uses exceed what
- /// mem2reg can trivially handle. This essentially should match the logic in
- /// \c isAllocaPromotable but re-using the existing walk of the pointer uses.
- bool IsAllocaPromotable;
-
- /// \brief Storage for stored values.
- ///
- /// Only used while the alloca is trivially promotable.
- SmallVector<Value *, 8> StoredValues;
+#endif
/// \brief The instruction responsible for this alloca not having a known set
/// of slices.
SmallPtrSet<Instruction *, 4> VisitedDeadInsts;
public:
- SliceBuilder(const DataLayout &DL, AllocaSlices &S)
+ SliceBuilder(const DataLayout &DL, AllocaInst &AI, AllocaSlices &S)
: PtrUseVisitor<SliceBuilder>(DL),
- AllocSize(DL.getTypeAllocSize(S.AI.getAllocatedType())), S(S) {}
+ AllocSize(DL.getTypeAllocSize(AI.getAllocatedType())), S(S) {}
private:
void markAsDead(Instruction &I) {
if (GEPI.use_empty())
return markAsDead(GEPI);
- // FIXME: mem2reg shouldn't care about the nature of the GEP, but instead
- // the offsets of the loads. Until then, we short-circuit here for the
- // promotable case.
- if (GEPI.hasAllZeroIndices())
- return Base::enqueueUsers(GEPI);
-
- // Otherwise, there is something in the GEP, so we disable mem2reg and
- // accumulate it.
- S.IsAllocaPromotable = false;
return Base::visitGetElementPtrInst(GEPI);
}
bool IsSplittable =
Ty->isIntegerTy() && !IsVolatile && Offset == 0 && Size >= AllocSize;
- // mem2reg can only promote non-volatile loads and stores which exactly
- // load the alloca (no offset and the right type).
- if (IsVolatile || Offset != 0 || Ty != S.AI.getAllocatedType())
- S.IsAllocaPromotable = false;
- if (S.IsAllocaPromotable)
- assert(Offset == 0);
-
insertUse(I, Offset, Size, IsSplittable);
}
return markAsDead(SI);
}
- if (S.IsAllocaPromotable)
- S.StoredValues.push_back(ValOp);
-
assert((!SI.isSimple() || ValOp->getType()->isSingleValueType()) &&
"All simple FCA stores should have been pre-split");
handleLoadOrStore(ValOp->getType(), SI, Offset, Size, SI.isVolatile());
if (!IsOffsetKnown)
return PI.setAborted(&II);
- S.IsAllocaPromotable = false;
-
insertUse(II, Offset,
Length ? Length->getLimitedValue()
: AllocSize - Offset.getLimitedValue(),
if (!IsOffsetKnown)
return PI.setAborted(&II);
- S.IsAllocaPromotable = false;
-
uint64_t RawOffset = Offset.getLimitedValue();
uint64_t Size = Length ? Length->getLimitedValue()
: AllocSize - RawOffset;
return;
}
- S.IsAllocaPromotable = false;
-
Base::visitIntrinsicInst(II);
}
return;
}
- S.IsAllocaPromotable = false;
-
insertUse(PN, Offset, PHISize);
}
if (SI.use_empty())
return markAsDead(SI);
if (Value *Result = foldSelectInst(SI)) {
- if (Result == *U) {
+ if (Result == *U)
// If the result of the constant fold will be the pointer, recurse
// through the select as if we had RAUW'ed it.
enqueueUsers(SI);
-
- // FIXME: mem2reg should support this pattern, but it doesn't.
- S.IsAllocaPromotable = false;
- } else {
+ else
// Otherwise the operand to the select is dead, and we can replace it
// with undef.
S.DeadOperands.push_back(U);
- }
return;
}
return;
}
- S.IsAllocaPromotable = false;
-
insertUse(SI, Offset, SelectSize);
}
};
AllocaSlices::AllocaSlices(const DataLayout &DL, AllocaInst &AI)
- : AI(AI), IsAllocaPromotable(true), PointerEscapingInstr(0) {
- SliceBuilder PB(DL, *this);
+ :
+#if !defined(NDEBUG) || defined(LLVM_ENABLE_DUMP)
+ AI(AI),
+#endif
+ PointerEscapingInstr(0) {
+ SliceBuilder PB(DL, AI, *this);
SliceBuilder::PtrInfo PtrI = PB.visitPtr(AI);
if (PtrI.isEscaped() || PtrI.isAborted()) {
// FIXME: We should sink the escape vs. abort info into the caller nicely,
if (S.begin() == S.end())
return Changed;
- // Trivially promotable, don't go through the splitting and rewriting.
- if (S.isAllocaPromotable()) {
- DEBUG(dbgs() << " Directly promoting alloca: " << AI << "\n");
- PromotableAllocas.push_back(&AI);
-
- // Walk through the stored values quickly here to handle directly
- // promotable allocas that require iterating on other allocas.
- ArrayRef<Value *> StoredValues = S.getStoredValues();
- for (ArrayRef<Value *>::iterator SVI = StoredValues.begin(),
- SVE = StoredValues.end();
- SVI != SVE; ++SVI)
- if ((*SVI)->getType()->isPointerTy())
- if (AllocaInst *SAI =
- dyn_cast<AllocaInst>((*SVI)->stripInBoundsOffsets()))
- PostPromotionWorklist.insert(SAI);
- return true;
- }
-
Changed |= splitAlloca(AI, S);
DEBUG(dbgs() << " Speculating PHIs\n");