summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 30cbccb)
raw | patch | inline | side by side (parent: 30cbccb)
author | Hal Finkel <hfinkel@anl.gov> | |
Mon, 19 Aug 2013 23:35:46 +0000 (23:35 +0000) | ||
committer | Hal Finkel <hfinkel@anl.gov> | |
Mon, 19 Aug 2013 23:35:46 +0000 (23:35 +0000) |
This adds a llvm.copysign intrinsic; We already have Libfunc recognition for
copysign (which is turned into the FCOPYSIGN SDAG node). In order to
autovectorize calls to copysign in the loop vectorizer, we need a corresponding
intrinsic as well.
In addition to the expected changes to the language reference, the loop
vectorizer, BasicTTI, and the SDAG builder (the intrinsic is transformed into
an FCOPYSIGN node, just like the function call), this also adds FCOPYSIGN to a
few lists in LegalizeVector{Ops,Types} so that vector copysigns can be
expanded.
In TargetLoweringBase::initActions, I've made the default action for FCOPYSIGN
be Expand for vector types. This seems correct for all in-tree targets, and I
think is the right thing to do because, previously, there was no way to generate
vector-values FCOPYSIGN nodes (and most targets don't specify an action for
vector-typed FCOPYSIGN).
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@188728 91177308-0d34-0410-b5e6-96231b3b80d8
copysign (which is turned into the FCOPYSIGN SDAG node). In order to
autovectorize calls to copysign in the loop vectorizer, we need a corresponding
intrinsic as well.
In addition to the expected changes to the language reference, the loop
vectorizer, BasicTTI, and the SDAG builder (the intrinsic is transformed into
an FCOPYSIGN node, just like the function call), this also adds FCOPYSIGN to a
few lists in LegalizeVector{Ops,Types} so that vector copysigns can be
expanded.
In TargetLoweringBase::initActions, I've made the default action for FCOPYSIGN
be Expand for vector types. This seems correct for all in-tree targets, and I
think is the right thing to do because, previously, there was no way to generate
vector-values FCOPYSIGN nodes (and most targets don't specify an action for
vector-typed FCOPYSIGN).
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@188728 91177308-0d34-0410-b5e6-96231b3b80d8
diff --git a/docs/LangRef.rst b/docs/LangRef.rst
index 47c89e8d24ad00fb5acc2584da2a7a99b4ee7597..68ac96f9b5a8579c47885ff9a7ffa2e6abdbd5ac 100644 (file)
--- a/docs/LangRef.rst
+++ b/docs/LangRef.rst
This function returns the same values as the libm ``fabs`` functions
would, and handles error conditions in the same way.
+'``llvm.copysign.*``' Intrinsic
+^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^
+
+Syntax:
+"""""""
+
+This is an overloaded intrinsic. You can use ``llvm.copysign`` on any
+floating point or vector of floating point type. Not all targets support
+all types however.
+
+::
+
+ declare float @llvm.copysign.f32(float %Mag, float %Sgn)
+ declare double @llvm.copysign.f64(double %Mag, double %Sgn)
+ declare x86_fp80 @llvm.copysign.f80(x86_fp80 %Mag, x86_fp80 %Sgn)
+ declare fp128 @llvm.copysign.f128(fp128 %Mag, fp128 %Sgn)
+ declare ppc_fp128 @llvm.copysign.ppcf128(ppc_fp128 %Mag, ppc_fp128 %Sgn)
+
+Overview:
+"""""""""
+
+The '``llvm.copysign.*``' intrinsics return a value with the magnitude of the
+first operand and the sign of the second operand.
+
+Arguments:
+""""""""""
+
+The arguments and return value are floating point numbers of the same
+type.
+
+Semantics:
+""""""""""
+
+This function returns the same values as the libm ``copysign``
+functions would, and handles error conditions in the same way.
+
'``llvm.floor.*``' Intrinsic
^^^^^^^^^^^^^^^^^^^^^^^^^^^^
index 856e0a5824dbf78c07575aa73abb148e2bf00784..c7414e063fef4fd1bb2a7f9bbfa936366575976a 100644 (file)
def int_exp : Intrinsic<[llvm_anyfloat_ty], [LLVMMatchType<0>]>;
def int_exp2 : Intrinsic<[llvm_anyfloat_ty], [LLVMMatchType<0>]>;
def int_fabs : Intrinsic<[llvm_anyfloat_ty], [LLVMMatchType<0>]>;
+ def int_copysign : Intrinsic<[llvm_anyfloat_ty],
+ [LLVMMatchType<0>, LLVMMatchType<0>]>;
def int_floor : Intrinsic<[llvm_anyfloat_ty], [LLVMMatchType<0>]>;
def int_ceil : Intrinsic<[llvm_anyfloat_ty], [LLVMMatchType<0>]>;
def int_trunc : Intrinsic<[llvm_anyfloat_ty], [LLVMMatchType<0>]>;
index ef532357c5c6500e702f5b6053a80043d78b2201..0883ab0ce7f1e54179cd1a5f9f250ade891d50f1 100644 (file)
case Intrinsic::log10: ISD = ISD::FLOG10; break;
case Intrinsic::log2: ISD = ISD::FLOG2; break;
case Intrinsic::fabs: ISD = ISD::FABS; break;
+ case Intrinsic::copysign: ISD = ISD::FCOPYSIGN; break;
case Intrinsic::floor: ISD = ISD::FFLOOR; break;
case Intrinsic::ceil: ISD = ISD::FCEIL; break;
case Intrinsic::trunc: ISD = ISD::FTRUNC; break;
diff --git a/lib/CodeGen/SelectionDAG/LegalizeVectorOps.cpp b/lib/CodeGen/SelectionDAG/LegalizeVectorOps.cpp
index 237a33a0cfff155a3cc740fcc52d0b85b995de63..b768f39e570debc5622547cf103adf1d0c8e7ddc 100644 (file)
case ISD::FP_TO_UINT:
case ISD::FNEG:
case ISD::FABS:
+ case ISD::FCOPYSIGN:
case ISD::FSQRT:
case ISD::FSIN:
case ISD::FCOS:
diff --git a/lib/CodeGen/SelectionDAG/LegalizeVectorTypes.cpp b/lib/CodeGen/SelectionDAG/LegalizeVectorTypes.cpp
index bf65319295b1a4d8fee9459e27644f1e47e5804b..fd5f97718f55a6278b6104ea92fe3dff4cfddfdd 100644 (file)
case ISD::ADD:
case ISD::AND:
case ISD::FADD:
+ case ISD::FCOPYSIGN:
case ISD::FDIV:
case ISD::FMUL:
case ISD::FPOW:
case ISD::SUB:
case ISD::MUL:
case ISD::FADD:
+ case ISD::FCOPYSIGN:
case ISD::FSUB:
case ISD::FMUL:
case ISD::SDIV:
diff --git a/lib/CodeGen/SelectionDAG/SelectionDAGBuilder.cpp b/lib/CodeGen/SelectionDAG/SelectionDAGBuilder.cpp
index 3b9f3581a4cdaf6cc8e22b95c14c8e615021ba88..df9293da261e74559b93606198ffcdc8d3fba382 100644 (file)
@@ -4925,6 +4925,12 @@ SelectionDAGBuilder::visitIntrinsicCall(const CallInst &I, unsigned Intrinsic) {
getValue(I.getArgOperand(0))));
return 0;
}
+ case Intrinsic::copysign:
+ setValue(&I, DAG.getNode(ISD::FCOPYSIGN, sdl,
+ getValue(I.getArgOperand(0)).getValueType(),
+ getValue(I.getArgOperand(0)),
+ getValue(I.getArgOperand(1))));
+ return 0;
case Intrinsic::fma:
setValue(&I, DAG.getNode(ISD::FMA, sdl,
getValue(I.getArgOperand(0)).getValueType(),
index 55125bd23f9fd60cc6189517233353cf88d16d56..a2ea35e64a193b958eaff7341ec30ecc21abfac6 100644 (file)
// These library functions default to expand.
setOperationAction(ISD::FROUND, (MVT::SimpleValueType)VT, Expand);
+
+ // These operations default to expand for vector types.
+ if (VT >= MVT::FIRST_VECTOR_VALUETYPE &&
+ VT <= MVT::LAST_VECTOR_VALUETYPE)
+ setOperationAction(ISD::FCOPYSIGN, (MVT::SimpleValueType)VT, Expand);
}
// Most targets ignore the @llvm.prefetch intrinsic.
index d9f132363b15e359ac76419bcbf7b0096de0d51e..4224ae2d273c991a775f7d574fec16b49c0bf77e 100644 (file)
case Intrinsic::sin:
case Intrinsic::cos:
return true;
+ case Intrinsic::copysign:
+ if (CI->getArgOperand(0)->getType()->getScalarType()->
+ isPPC_FP128Ty())
+ return true;
+ else
+ continue; // ISD::FCOPYSIGN is never a library call.
case Intrinsic::sqrt: Opcode = ISD::FSQRT; break;
case Intrinsic::floor: Opcode = ISD::FFLOOR; break;
case Intrinsic::ceil: Opcode = ISD::FCEIL; break;
diff --git a/lib/Transforms/Vectorize/LoopVectorize.cpp b/lib/Transforms/Vectorize/LoopVectorize.cpp
index e452acdafac2dab36dc62c51bb0ca62bcf89413f..a7026f68a2c259e750869705156a59b74186f019 100644 (file)
case Intrinsic::log10:
case Intrinsic::log2:
case Intrinsic::fabs:
+ case Intrinsic::copysign:
case Intrinsic::floor:
case Intrinsic::ceil:
case Intrinsic::trunc:
case LibFunc::fabsf:
case LibFunc::fabsl:
return Intrinsic::fabs;
+ case LibFunc::copysign:
+ case LibFunc::copysignf:
+ case LibFunc::copysignl:
+ return Intrinsic::copysign;
case LibFunc::floor:
case LibFunc::floorf:
case LibFunc::floorl:
diff --git a/test/Transforms/LoopVectorize/intrinsic.ll b/test/Transforms/LoopVectorize/intrinsic.ll
index 566dcc75cd8175e156b08cab9dcc72b28fbb9e73..216b937ad6d0b2045ac688634d85f1ad114e2c1e 100644 (file)
declare double @llvm.fabs(double) nounwind readnone
+;CHECK-LABEL: @copysign_f32(
+;CHECK: llvm.copysign.v4f32
+;CHECK: ret void
+define void @copysign_f32(i32 %n, float* noalias %y, float* noalias %x, float* noalias %z) nounwind uwtable {
+entry:
+ %cmp6 = icmp sgt i32 %n, 0
+ br i1 %cmp6, label %for.body, label %for.end
+
+for.body: ; preds = %entry, %for.body
+ %indvars.iv = phi i64 [ %indvars.iv.next, %for.body ], [ 0, %entry ]
+ %arrayidx = getelementptr inbounds float* %y, i64 %indvars.iv
+ %0 = load float* %arrayidx, align 4
+ %arrayidx1 = getelementptr inbounds float* %z, i64 %indvars.iv
+ %1 = load float* %arrayidx1, align 4
+ %call = tail call float @llvm.copysign.f32(float %0, float %1) nounwind readnone
+ %arrayidx2 = getelementptr inbounds float* %x, i64 %indvars.iv
+ store float %call, float* %arrayidx2, align 4
+ %indvars.iv.next = add i64 %indvars.iv, 1
+ %lftr.wideiv = trunc i64 %indvars.iv.next to i32
+ %exitcond = icmp eq i32 %lftr.wideiv, %n
+ br i1 %exitcond, label %for.end, label %for.body
+
+for.end: ; preds = %for.body, %entry
+ ret void
+}
+
+declare float @llvm.copysign.f32(float, float) nounwind readnone
+
+define void @copysign_f64(i32 %n, double* noalias %y, double* noalias %x, double* noalias %z) nounwind uwtable {
+entry:
+ %cmp6 = icmp sgt i32 %n, 0
+ br i1 %cmp6, label %for.body, label %for.end
+
+for.body: ; preds = %entry, %for.body
+ %indvars.iv = phi i64 [ %indvars.iv.next, %for.body ], [ 0, %entry ]
+ %arrayidx = getelementptr inbounds double* %y, i64 %indvars.iv
+ %0 = load double* %arrayidx, align 8
+ %arrayidx1 = getelementptr inbounds double* %z, i64 %indvars.iv
+ %1 = load double* %arrayidx, align 8
+ %call = tail call double @llvm.copysign(double %0, double %1) nounwind readnone
+ %arrayidx2 = getelementptr inbounds double* %x, i64 %indvars.iv
+ store double %call, double* %arrayidx2, align 8
+ %indvars.iv.next = add i64 %indvars.iv, 1
+ %lftr.wideiv = trunc i64 %indvars.iv.next to i32
+ %exitcond = icmp eq i32 %lftr.wideiv, %n
+ br i1 %exitcond, label %for.end, label %for.body
+
+for.end: ; preds = %for.body, %entry
+ ret void
+}
+
+declare double @llvm.copysign(double, double) nounwind readnone
+
;CHECK-LABEL: @floor_f32(
;CHECK: llvm.floor.v4f32
;CHECK: ret void