summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 14b5bac)
raw | patch | inline | side by side (parent: 14b5bac)
author | Jakob Stoklund Olesen <stoklund@2pi.dk> | |
Wed, 29 Aug 2012 00:37:58 +0000 (00:37 +0000) | ||
committer | Jakob Stoklund Olesen <stoklund@2pi.dk> | |
Wed, 29 Aug 2012 00:37:58 +0000 (00:37 +0000) |
The isTied bit is set automatically when a tied use is added and
MCInstrDesc indicates a tied operand. The tie is broken when one of the
tied operands is removed.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@162814 91177308-0d34-0410-b5e6-96231b3b80d8
MCInstrDesc indicates a tied operand. The tie is broken when one of the
tied operands is removed.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@162814 91177308-0d34-0410-b5e6-96231b3b80d8
include/llvm/CodeGen/MachineInstr.h | patch | blob | history | |
lib/CodeGen/MachineInstr.cpp | patch | blob | history |
index 27756abf3f544c8ba84363117504c9765b7d5c57..e88351cb989ec372ce0a3f2f2345c87dc67de8c2 100644 (file)
const TargetInstrInfo *TII,
const TargetRegisterInfo *TRI) const;
+ /// findTiedOperandIdx - Given the index of a tied register operand, find the
+ /// operand it is tied to. Defs are tied to uses and vice versa. Returns the
+ /// index of the tied operand which must exist.
+ unsigned findTiedOperandIdx(unsigned OpIdx) const;
+
/// isRegTiedToUseOperand - Given the index of a register def operand,
/// check if the register def is tied to a source operand, due to either
/// two-address elimination or inline assembly constraints. Returns the
/// return null.
MachineRegisterInfo *getRegInfo();
+ /// untieRegOperand - Break any tie involving OpIdx.
+ void untieRegOperand(unsigned OpIdx) {
+ const MachineOperand &MO = getOperand(OpIdx);
+ if (MO.isReg() && MO.isTied())
+ getOperand(findTiedOperandIdx(OpIdx)).setIsTied(false);
+ }
+
/// addImplicitDefUseOperands - Add all implicit def and use operands to
/// this instruction.
void addImplicitDefUseOperands();
index 24078f8943f4a6ad9d9ff72a987cc9196309b3c6..bfb722bf3bb86ec63ea6c40297893b7f3dd90f34 100644 (file)
/// the specified value. If an operand is known to be an immediate already,
/// the setImm method should be used.
void MachineOperand::ChangeToImmediate(int64_t ImmVal) {
+ assert((!isReg() || !isTied()) && "Cannot change a tied operand into an imm");
// If this operand is currently a register operand, and if this is in a
// function, deregister the operand from the register's use/def list.
if (isReg() && isOnRegUseList())
RegInfo = &MF->getRegInfo();
// If this operand is already a register operand, remove it from the
// register's use/def lists.
- if (RegInfo && isReg())
+ bool WasReg = isReg();
+ if (RegInfo && WasReg)
RegInfo->removeRegOperandFromUseList(this);
// Change this to a register and set the reg#.
IsDebug = isDebug;
// Ensure isOnRegUseList() returns false.
Contents.Reg.Prev = 0;
+ // Preserve the tie bit when the operand was already a register.
+ if (!WasReg)
+ IsTied = false;
// If this operand is embedded in a function, add the operand to the
// register's use/def list.
if (Operands[OpNo].isReg()) {
// Ensure isOnRegUseList() returns false, regardless of Op's status.
Operands[OpNo].Contents.Reg.Prev = 0;
+ // Ignore existing IsTied bit. This is not a property that can be copied.
+ Operands[OpNo].IsTied = false;
// Add the new operand to RegInfo.
if (RegInfo)
RegInfo->addRegOperandToUseList(&Operands[OpNo]);
///
void MachineInstr::RemoveOperand(unsigned OpNo) {
assert(OpNo < Operands.size() && "Invalid operand number");
+ untieRegOperand(OpNo);
MachineRegisterInfo *RegInfo = getRegInfo();
// Special case removing the last one.
return -1;
}
+/// Given the index of a tied register operand, find the operand it is tied to.
+/// Defs are tied to uses and vice versa. Returns the index of the tied operand
+/// which must exist.
+unsigned MachineInstr::findTiedOperandIdx(unsigned OpIdx) const {
+ // It doesn't usually happen, but an instruction can have multiple pairs of
+ // tied operands.
+ SmallVector<unsigned, 4> Uses, Defs;
+ unsigned PairNo = ~0u;
+ for (unsigned i = 0, e = getNumOperands(); i != e; ++i) {
+ const MachineOperand &MO = getOperand(i);
+ if (!MO.isReg() || !MO.isTied())
+ continue;
+ if (MO.isUse()) {
+ if (i == OpIdx)
+ PairNo = Uses.size();
+ Uses.push_back(i);
+ } else {
+ if (i == OpIdx)
+ PairNo = Defs.size();
+ Defs.push_back(i);
+ }
+ }
+ // For each tied use there must be a tied def and vice versa.
+ assert(Uses.size() == Defs.size() && "Tied uses and defs don't match");
+ assert(PairNo < Uses.size() && "OpIdx must be a tied register operand");
+
+ // Find the matching operand.
+ return (getOperand(OpIdx).isDef() ? Uses : Defs)[PairNo];
+}
+
/// isRegTiedToUseOperand - Given the index of a register def operand,
/// check if the register def is tied to a source operand, due to either
/// two-address elimination or inline assembly constraints. Returns the